fs23 fail to enter LPOFF I'm using the S32K312 to communicate with the FS23 via SPI in order to control the FS23 to enter LPOFF mode. I sent the LPOFF command through SPI as follows: First, I read the value of the SBC_FS23_M_SYS_CFG_ADDR register: Sbc_fs23_ReadRegister(1, SBC_FS23_M_SYS_CFG_ADDR, &M_Sys_Cfg_RxData); Second, I wrote the read value of the SBC_FS23_M_SYS_CFG_ADDR register, with the SBC_FS23_M_GO2LPOFF_MASK set to 0x0040 (1<<6) for the LPOFF sleep mode: Sbc_fs23_WriteRegister(1, SBC_FS23_M_SYS_CFG_ADDR, M_Sys_Cfg_RxData | SBC_FS23_M_GO2LPOFF_MASK, &pu16RxData_LDT); However, the FS23 did not enter LPOFF mode, and when I read the register value again, it hadn't changed. I can confirm that the SPI communication is working properly.There are no external wakeup sources connected Can you guide me on whether there might be an issue with my configuration or if there are other registers that need to be configured? Re: fs23 fail to enter LPOFF I found that it should be because the SPI failed to write to the register, which led to this situation. However, fs23 is indeed in normal mode, and the watchdog timer is also disabled.But I have no problem reading data through SPI, and writing data also returns successfully. Re: fs23 fail to enter LPOFF I think it might be that writing to any register is not working. Can you tell me what else I need to pay attention to? //step1 Sbc_fs23_ReadRegister(1,SBC_FS23_M_IOWU_EN_ADDR,&M_IOWU_EN_RxData); Sbc_fs23_WriteRegister(1,SBC_FS23_M_IOWU_EN_ADDR,(M_IOWU_EN_RxData)|((SBC_FS23_M_WK1_WUEN_MASK)|(SBC_FS23_M_WK2_WUEN_MASK)),&M_IOWU_EN_RxData); //step2 Sbc_fs23_ReadRegister(1,SBC_FS23_M_IOWU_FLG_ADDR,&M_IOWU_FLG_RxData); Sbc_fs23_WriteRegister(1,SBC_FS23_M_IOWU_FLG_ADDR,0xFFFF,&M_IOWU_FLG_RxData1); step3 Sbc_fs23_ReadRegister(1,SBC_FS23_M_WU1_FLG_ADDR,&M_WU1_FLG); Sbc_fs23_WriteRegister(1,SBC_FS23_M_WU1_FLG_ADDR,M_WU1_FLG|0x03F7,&M_WU1_FLG); step4 Sbc_fs23_ReadRegister(1,SBC_FS23_M_SYS_CFG_ADDR,&M_Sys_Cfg_RxData); Sbc_fs23_WriteRegister(1,SBC_FS23_M_SYS_CFG_ADDR,M_Sys_Cfg_RxData|SBC_FS23_M_GO2LPOFF_LPOFF,&M_Sys_Cfg_RxData); Re: fs23 fail to enter LPOFF I have already cleared M_IOWU_FLG and M_WU1_FLG, but it still doesn't work. Here's the code: //IOWUE Sbc_fs23_ReadRegister(1,SBC_FS23_M_IOWU_EN_ADDR,&M_IOWU_EN_RxData); Sbc_fs23_WriteRegister(1,SBC_FS23_M_IOWU_EN_ADDR,(M_IOWU_EN_RxData)|((SBC_FS23_M_WK1_WUEN_MASK)|(SBC_FS23_M_WK2_WUEN_MASK)),&M_IOWU_EN_RxData); //clear IO wakeup flag Sbc_fs23_ReadRegister(1,SBC_FS23_M_IOWU_FLG_ADDR,&M_IOWU_FLG_RxData); Sbc_fs23_WriteRegister(1,SBC_FS23_M_IOWU_FLG_ADDR,0xFFFF,&M_IOWU_FLG_RxData1); //clear M_WU1_FLG Sbc_fs23_ReadRegister(1,SBC_FS23_M_WU1_FLG_ADDR,&M_WU1_FLG); Sbc_fs23_WriteRegister(1,SBC_FS23_M_WU1_FLG_ADDR,M_WU1_FLG|0x03F7,&M_WU1_FLG); //entry lpoff mode Sbc_fs23_ReadRegister(1,SBC_FS23_M_SYS_CFG_ADDR,&M_Sys_Cfg_RxData); Sbc_fs23_WriteRegister(1,SBC_FS23_M_SYS_CFG_ADDR,M_Sys_Cfg_RxData|SBC_FS23_M_GO2LPOFF_LPOFF,&M_Sys_Cfg_RxData); I think it might be that writing to any register is not working. Can you tell me what else I need to pay attention to? Re: fs23 fail to enter LPOFF I have already cleared M_IOWU_FLG and M_WU1_FLG, but it still doesn't work. Here's the code: //IOWUEN Sbc_fs23_ReadRegister(1,SBC_FS23_M_IOWU_EN_ADDR,&M_IOWU_EN_RxData); Sbc_fs23_WriteRegister(1,SBC_FS23_M_IOWU_EN_ADDR,(M_IOWU_EN_RxData)|((SBC_FS23_M_WK1_WUEN_MASK)|(SBC_FS23_M_WK2_WUEN_MASK)),&M_IOWU_EN_RxData); //clear flag Sbc_fs23_ReadRegister(1,SBC_FS23_M_IOWU_FLG_ADDR,&M_IOWU_FLG_RxData); Sbc_fs23_WriteRegister(1,SBC_FS23_M_IOWU_FLG_ADDR,0xFFFF,&M_IOWU_FLG_RxData); //clear M_WU1_FLG Sbc_fs23_ReadRegister(1,SBC_FS23_M_WU1_FLG_ADDR,&M_WU1_FLG); Sbc_fs23_WriteRegister(1,SBC_FS23_M_WU1_FLG_ADDR,M_WU1_FLG|0x03F7,&M_WU1_FLG); //entry lpoff Sbc_fs23_ReadRegister(1,SBC_FS23_M_SYS_CFG_ADDR,&M_Sys_Cfg_RxData); Sbc_fs23_WriteRegister(1,SBC_FS23_M_SYS_CFG_ADDR,M_Sys_Cfg_RxData|SBC_FS23_M_GO2LPOFF_LPOFF,&M_Sys_Cfg_RxData); Re: fs23 fail to enter LPOFF M_IOWU_FLG register Re: fs23 fail to enter LPOFF Can you tell me which register it is in? Re: fs23 fail to enter LPOFF Following your method, I tried writing arbitrary values, but it still didn't succeed. The read value remains the default, as shown in the screenshot. This problem has been bothering me for a long time. Could you please help guide me again? Re: fs23 fail to enter LPOFF 1.The value of the M_SYS_CFG register is 21507 (0101010000000011). 2.The written value is 21571 (0101010001000011). 3.To verify if the write was successful, the value I re-read is also 21507 (0101010000000011). This problem has been bugging me for days. Can you please give me some guidance? Re: fs23 fail to enter LPOFF Step 1: Read the value of the register SBC_FS23_M_SYS_CFG_ADDR (0x05) via SPI.
[gw]读出来的值是多少这个寄存器?
Step 2: Perform a bitwise OR operation between this value and SBC_FS23_M_GO2LPOFF_LPOFF (0x0001U << SBC_FS23_M_GO2LPOFF_SHIFT), and then write the result back to SBC_FS23_M_SYS_CFG_ADDR (0x05) to put fs23 into sleep mode.
[gw]写进去 M_SYS_CFG register 的值是多少?写过以后有没有再读一下验证写成功有否? Re: fs23 fail to enter LPOFF I am sure it's in normal mode, and I want to enter LPOFF mode by writing to the register SBC_FS23_M_SYS_CFG_ADDR (0x05). My steps are as follows: Step 1: Read the value of the register SBC_FS23_M_SYS_CFG_ADDR (0x05) via SPI. Step 2: Perform a bitwise OR operation between this value and SBC_FS23_M_GO2LPOFF_LPOFF (0x0001U << SBC_FS23_M_GO2LPOFF_SHIFT), and then write the result back to SBC_FS23_M_SYS_CFG_ADDR (0x05) to put fs23 into sleep mode. Re: fs23 fail to enter LPOFF Regarding the M_STATES register value of 12295 (binary representation: 0011000000000111), with bit13 being 1 indicating normal mode。 The value of the M_SYS_CFG register is 21507 (0101010000000011), but it has not been successfully modified. Re: fs23 fail to enter LPOFF Are you sure it is normal mode? What command did you send to enter LPOFF mode? Re: fs23 fail to enter LPOFF You write M_SYS_CFG register as 'xxxx x000 0100 0011' Try it, 'x' represents any value
查看全文