1917267_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1917267_en-US

1917267_en-US

The compilation of the "Etpu_Pwm_Ip_Example_S32K396" example program reports an error

When I used the ETPU example program of S32K396, there were compilation problems. It indicated that the files "Clock_Ip_Types.h", "Clock_Ip_Cfg.h", "Clock_Ip.h", "Etpu_Ip_Cfg.h", "Etpu_Ip_Types.h", and "Etpu_Ipw_Cfg.h" were missing.

qingwang_a_0-1721918235404.png

The integrated environment I use is S32DS version 3.5. I have installed the SDK, RTD, and ETPU SW.

qingwang_a_1-1721918392446.png

The software configuration is shown as follows in the figure.

qingwang_a_2-1721918512578.png


Re: The compilation of the "Etpu_Pwm_Ip_Example_S32K396" example program reports an error

Hi .@VaneB,

     Is there a manual for programming the eTPU of the S32K396 using C language, or what tools are used for eTPU development? I have noticed that eTPU has some function sets, including the implementation of a resolver, but this part is already compiled into binary code. If eTPU can only use these function sets, are there corresponding examples or documentation available?

Re: The compilation of the "Etpu_Pwm_Ip_Example_S32K396" example program reports an error

Hi @qingwang_a 

Since the S32K396 devices have only recently been released to the mass market, the example codes available are those provided in the S32K3 Standard Software and the S32K3 Reference Software.

Re: The compilation of the "Etpu_Pwm_Ip_Example_S32K396" example program reports an error

Thank you for your reply. I would like to use the S32K396 for resolver decoding. Do you have any examples from DS or EB?

Re: The compilation of the "Etpu_Pwm_Ip_Example_S32K396" example program reports an error

Hi @qingwang_a 

Sorry for the inconvenience. This issue has already been reported to the relevant team and is expected to be resolved in future software releases.

Also, there is a note in the software release notes mentioning that PWM ETPU supports only EB driver example.

VaneB_0-1722275199710.png


BR, VaneB


Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 12:54 PM
Updated by: