RTD file Package issue using S32K324 MC Hi Team, I am using S32K324 MC using S32DS.3.6.12 IDE, i have installed all packeges, even i installed RTD( SW32K3_S32M27x_RTD_R23-11_7.0.1_D2603_DesignStudio_updatesite i have installed this one from NXP website and inserted in IDE then installed). Problem: while creating time the project for S32K324, SDK file is not showing i have check the all possiblities but still not getting please check the bellow image you can get easily. Please help me to fix this issue. Looking Forward for you response. #S32K3 AUTOMOTIVE-RTD Re: RTD file Package issue using S32K324 MC hi @danielmartynek okay, @danielmartynek thank you for the support. thank you and regards, sunil ladwa Re: RTD file Package issue using S32K324 MC Because the RTD (SDK) 7.0.1 supports GCC 10.2 only, not GCC 11.4.
So yes, GCC 10.2 is the only GCC that can be used with RTD 7.0.1.
BR, Daniel Re: RTD file Package issue using S32K324 MC Hi @danielmartynek , thank you for you guide, just i have one more question for GCC 11.4 it is not showing i want to know why? and if i select GCC 10.2 is it okay or is it suitable for latest tool and MC? thank you and regard, sunil ladwa. Re: RTD file Package issue using S32K324 MC Hello Sunil Ladwa,
Yes, that is correct, select 10.2.
Regards,
Daniel Re: RTD file Package issue using S32K324 MC hi @danielmartynek , while creating time i got this option like GCC 11.4, GCC 10.2, GCC9.2. is this correct right? if i select the GCC 10.2 i am getting in the SDK package this is correct right? i need your conformation. thank you and regards, sunil ladwa Re: RTD file Package issue using S32K324 MC Hi @sunil0509,
Please create a new thread if your follow-up questions are unrelated to the original topic.
Regards,
Daniel Re: RTD file Package issue using S32K324 MC Hi @sunil0509,
Refer to the release notes of the RTD, it supports GCC 10.2:
Regards,
Daniel Re: RTD file Package issue using S32K324 MC Hi @danielmartynek , i have selected this one GCC 11.4. it this correct? I also have a small doubt regarding AUTOSAR and RTOS. Is the SW32K3_S32M27x_RTD_R23-11_7.0.1_D2603_DesignStudio_updatesite package applicable to both AUTOSAR and RTOS, or are separate packages required? If separate packages are required, could you please share the download links for both? thank you and regards sunil ladwa Re: RTD file Package issue using S32K324 MC Hi @sunil0509,
Which compiler have you selected?
The RTD supports GCC 10.2 in S32DS.
Regards,
Daniel
View full article