Renaming the project caused the entire project to be lost. Starving and looking up S32DS 3.5 Facing a similar new project Rename an old project The new project hasn't even been created yet, so be it. They also deleted my old project!! Explorer can no longer find the original Project Folder. chkdsk indicates no error! How can I salvage an existing old project? NXPrename.png Also, why is the [Project Name starting with a number] invalid? Spoiler (Highlight to read) S32DS-ARM S32DS-S32PLATFORM #rename #rename Re: Project [Rename] , 造成 整個 Project 丟失 I manually added many subfolders to this project folder for writing some small tools in Python for other users of the same project. You know, there exist LOTs of garbagessss for python's `venv` function and PyInstall . Is it possible that there are too many subfolders/files for `Project Rename` function !? Re: Project [Rename] , 造成 整個 Project 丟失 > 1. Recycling bin. Order by datetime UndeleteRecycleBin.png > 2. Workspace path and look for the new renamed project (under C:\Users\'xxx'\workspaceS32DS.3.5), or whichever custom path you've used to create the project. No "Wxxx" folder under C:\Users\user\ UndeleteUserFolder.png No free Space on C: UndeleteSpace.png FreeSpace on 😧 was under 100GB ... BEFORE `RENAME` Project Custom path on D:\Project\NXP\xxx\ disappear now. > 3. Windows File History, if enabled. None 😞 .metadata folder only have log files , and .plugins\ folder If you are referring to this issue : Eclipse: All my projects disappeared from Project Explorer - Stack Overflow , Their folders are still exist! So, they can `5. Do File->Import` In my case, all the folders from the previous project were DELETED ! Re: Project [Rename] , 造成 整個 Project 丟失 Hello @CY9,
Eclipse's "Rename" feature creates a new project, copies the whole old project, and deletes the old one to keep the new one. It seems Eclipse only renames the project folder if it is under the default workspace, if you create the project in a custom location, the project's folder will not be renamed, only internal references and the .project file are renamed.
Unless you've deleted the previous project, it is most likely still in your hard drive, have you tried checking:
1. Recycling bin.
2. Workspace path and look for the new renamed project (under C:\Users\'xxx'\workspaceS32DS.3.5), or whichever custom path you've used to create the project.
3. Windows File History, if enabled.
Lastly, you can also try checking the .metadata folder, and look for the project reference old or new name.
Sources: m2eclipse - Should renaming a project in Eclipse also rename project folder on file system? - Stack Overflow, Eclipse: All my projects disappeared from Project Explorer - Stack Overflow, java - Renamed a project in my Eclipse workspace via the filesystem and now cannot open it. - Stack Overflow, Renaming a project Eclipse Help
Hope this helps.
Best regards, Julián Re: Project [Rename] , 造成 整個 Project 丟失 Hello @CY9,
I do not think this is because of the subfolder count. From the log in metadata, I can see that a rename operation failed on '2026-08-10':
!ENTRY com.nxp.s32ds.ext.ide.core 4 0 2026-08-10 08:50:24.109
!MESSAGE Unexpected error during rename
!STACK 1
I infer that the project you were renaming was "202503021_App_118", and you tried to rename to "ADB22pxAPP_VR", correct? I can see the following error:
org.eclipse.core.internal.resources.ResourceException(/ADB22pxAPP_VR)[374]: java.lang.Exception: Resource '/ADB22pxAPP_VR' already exists.
However, I am not sure if this the root cause, as I've tried to rename a project to an already existing one, and I am not able to:
Julin_AragnM_1-1786480276599.png
Julin_AragnM_0-1786480052303.png
So, I really cannot come to a conclusion from this information alone. The only actions I can recommend is to look for both 202503021_App_118 & ADB22pxAPP_VR with Recuva scan through the whole disk. If project recovery is not possible, I am not sure there are any other solutions available.
Best regards, Julián Re: Project [Rename] , 造成 整個 Project 丟失 Yeap, I am sure `ADB22pxAPP_VR\` is *NOT* exist . Even it really exist, and your program found it. Should it STOP the rename function !? Actually, it deleted whole directory. I have no idea what's happened. Recuva can NOT find any folder out. I am trying to rescue some files ASAP. Thanks for your concern.
View full article