2425192_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2425192_en-US

2425192_en-US

P3B1602 I2C/I3C PCIe CEM Spec Compliant

Dear Forum,

PCIe CEM Spec Revision 6.0.1 defines SMBus (I2C) with 3.3V and I3C with 1.8V

Does the P3B1602 support 3.3V in I2C mode (internal resistors to 3.3V) and 1.8V in I3C Mode?  

I suppose to comply to both modes the supply voltage of P3B1602 needs to be changed, right? 


Thank you. 

Kind regards

Moritz

Re: P3B1602 I2C/I3C PCIe CEM Spec Compliant

Hi Guo, 

thank you for the clarification.
Can I use 2 P3B1602 in parallel on the same SCL and SDA nets but with 1.8V and 3.3V VCCB Supply. 

Just pulling only the one I need active with the OE pin?


Kind regards
Moritz

Re: P3B1602 I2C/I3C PCIe CEM Spec Compliant

HI Moritz

P3B1602 supports both voltage levels, but if the same B-side bus needs to switch between 3.3 V SMBus/I²C and 1.8 V I3C, the corresponding VCCB must be switched, and all external pull-up resistors and connected devices' level requirements must be verified.

Thanks!

BR

Re: P3B1602 I2C/I3C PCIe CEM Spec Compliant

Hi Guo, 

my plan looks like this. 

Moritz_1-1794210244705.png
Kind regards

Moritz



Re: P3B1602 I2C/I3C PCIe CEM Spec CompliantHi Moritz Could you please give your connection diagram for better understand! BRRe: P3B1602 I2C/I3C PCIe CEM Spec CompliantHi Guo,
I think this can be handled in the FPGA.
In summay, if the mutual exclusivity is ensured and a delay between enables is implemented, you see no issue correct?
I've omitted the pull down resistors for clarity.

Kind regards
Moritz
Re: P3B1602 I2C/I3C PCIe CEM Spec Compliant

HI Moritz

The 1.8 V or 3.3 V channels can be selected through OE. However, OE is not just a simple software signal selection; it must ensure mutual exclusivity, default off state, and switching dead zone.

Re: P3B1602 I2C/I3C PCIe CEM Spec CompliantHi Moritz Could you please give your connection diagram for better understand! BRRe: P3B1602 I2C/I3C PCIe CEM Spec Compliant

Hi Moritz

If there is no external pull up for these B side pins, it should be no problem.

guoweisun_0-1794271862940.png


Tags (1)
No ratings
Version history
Last update:
a week ago
Updated by: