Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
DDR Configuration on LX2160ARDB - HX430C16FB3_32   We are working with an LX2160ARDB reference board and attempting to use a 32GB DDR4 RAM module on the DDR1 controller. However, in CodeWarrior's DDR Memory Controller Configuration, we couldn't find an option for a 32GB device under DRAM Configuration per Device. Could you please provide guidance on: How to configure the DDR Memory Controller for 32GB RAM on the LX2160ARDB? Steps to validate the 32GB DDR RAM on this platform. Instructions for updating the firmware (if necessary) to support 32GB DDR RAM. Re: DDR Configuration on LX2160ARDB - HX430C16FB3_32 Hi Yiping, We have loaded the RCW file(rcw_2000_700_2900_19_5_2_sd.bin) into SD card and in DDR configuration panel, when Read SPD is done we are getting as "Unsupported raw card revision. Set the CLK to DQS skew values manually."  Re: DDR Configuration on LX2160ARDB - HX430C16FB3_32 To configure 32GB DDR4 RAM on your LX2160ARDB, as CodeWarrior lacks a direct option, you'll need to use the **NXP QorIQ Configuration and Validation Suite (QCVS)**. Obtain your 32GB DIMM's detailed specifications (density, ranks, device width) and input them into QCVS to generate custom DDR controller configuration code. This code must then be **integrated into the U-Boot bootloader** source from the latest Layerscape Software Development Kit (LSDK). After building U-Boot, **flash the updated firmware** to your board. Validate the 32GB RAM by checking U-Boot boot messages and using Linux commands like `free -h` once the system boots. Re: DDR Configuration on LX2160ARDB - HX430C16FB3_32 In DDR configuration panel, please select "Read SPD" and "DIMM" as Configuration mode, then click "Read SPD" to read parameters from SPD and finish the DDR project creating. After creating QCVS DDR project, please check all "Validation stage" and "Operational DDR tests" to to connect to the target board to finish all the validation. Please refer to QCVS DDR Tool user manual  https://www.nxp.com.cn/docs/en/user-guide/QCVS_DDR_User_Guide.pdf No need specific firmware when doing validation with QCVS DDRv tool.
View full article
KE18F512VLH16 ECC RAM 单比特纠错 我有一个与@sean_dvorscak前几天的帖子( KE1 ECC RAM 单比特纠错)相关的后续问题。 @Celeste_Liu回复道: 如果要实现可选的清理功能,请根据实际访问大小或清理粒度来对齐访问,而不是盲目地依赖原始的 MCM_LMFAR 值。此外,除非您已正确对齐地址并确认访问大小有效,否则请勿使用固定的 4 字节访问。 MCM_LMFATR[PEFSIZE] 能否用于确定访问大小?如果可以,能否将其与 MCM_LMFAR 结合使用,以实现读取-正确-写回操作?例如,如果 MCM_LMFATR[PEFSIZE] 为 3'b000,表示 8 位访问,我能否从 MCM_LMFAR 指示的地址执行 8 位读取,然后对同一地址执行 8 位写入以纠正错误?同样地,如果 MCM_LMFATR[PEFSIZE] 为 3'b010,表示 32 位访问,我是否可以对 MCM_LMFAR 指示的地址执行 32 位写入,而无需担心对齐问题? Re: KE18F512VLH16 ECC RAM Single Bit Correction 你好@rseigle77 , 我已看过你的帖子。我需要一些时间来调查这个问题,一旦有更多信息,我会尽快回复您。 BR 塞莱斯特 Re: KE18F512VLH16 ECC RAM Single Bit Correction 嗨@Celeste_Liu - P7 是最终应用程序的名称。 Re: KE18F512VLH16 ECC RAM Single Bit Correction 你好@rseigle77 , 关于您的问题,我需要将其上报给内部团队进行进一步调查。根据我们的流程,请提供最终应用程序名称。 谢谢您的合作。 BR 塞莱斯特 Re: KE18F512VLH16 ECC RAM Single Bit Correction @Celeste_Liu你好,请问这件事有任何进展吗? Re: KE18F512VLH16 ECC RAM Single Bit Correction 你好@rseigle77 , 抱歉,我还没有收到内部回复。 我会再次跟进此事,并将其作为我的首要任务。一旦收到回复,我会立即通知你。 BR 塞莱斯特 Re: KE18F512VLH16 ECC RAM Single Bit Correction 感谢@Celeste_Liu的回复,但这并没有回答我关于MCM_LMFATR[PEFSIZE] 的问题: “ MCM_LMFATR[PEFSIZE] 能否用于确定访问大小?如果可以,能否将其与 MCM_LMFAR 结合使用,实现读取-纠错-写回操作?例如,如果 MCM_LMFATR[PEFSIZE] 为 3'b000,表示 8 位访问,我能否先从 MCM_LMFAR 指示的地址读取 8 位数据,然后再向同一地址写入 8 位数据以纠正错误?类似地,如果 MCM_LMFATR[PEFSIZE] 为 3'b010,表示 32 位访问,我能否直接向 MCM_LMFAR 指示的地址写入 32 位数据而无需考虑对齐问题?” Re: KE18F512VLH16 ECC RAM Single Bit Correction 你好@rseigle77 , 感谢您的耐心等待。我收到了内部回复。 ECC“纠错”是指将纠正后的数据返回给CPU,而不是修复存储在SRAM中的底层位。自动修复需要单独的擦除/回写机制。 使用软件清理的推荐流程: ECC在读取时纠正数据。 引发单比特错误中断/状态。请参阅 RM 6.3.1.1确定中断源。MCM_LMPECR [ER1BR] =1 软件读取故障地址。MCM_LMPEIR [PEELOC] = 5'h08 - 来自 SRAM_L 的 1 位可纠正 ECC 事件,MCM_LMFAR 指示故障地址。 软件会将更正后的值写回原地址。 生成并存储新的 ECC 综合征。 BR 塞莱斯特
View full article
KE18F512VLH16 ECC RAM Single Bit Correction I have a follow up question related to @sean_dvorscak's post the other day (KE1 ECC RAM Single Bit Corrrection). @Celeste_Liu replied, ->> If implementing an optional scrub, please align the access according to the actual access size or scrub granularity, not blindly to the raw MCM_LMFAR value. Also don't use a fixed 4-byte access unless you first align the address appropriately and confirm the access size is valid. Can MCM_LMFATR[PEFSIZE] be used to determine the access size? If so, can this be used in tandem with MCM_LMFAR to implement a read-correct-writeback operation? For example, if MCM_LMFATR[PEFSIZE] is 3'b000 indicating an 8-bit access, can I perform an 8-bit read from the address indicated by MCM_LMFAR then perform an 8-bit write to the same address to correct the error. Similarly, if MCM_LMFATR[PEFSIZE] is 3'b010 indicating a 32-bit access, can I perform a 32-bit write to the address indicated by MCM_LMFAR without worrying about alignment? Re: KE18F512VLH16 ECC RAM Single Bit Correction Hello @rseigle77 , I have seen your post. Let me spend some time investigating this issue, and I will get back to you once I have more information. BR Celeste Re: KE18F512VLH16 ECC RAM Single Bit Correction Hello @rseigle77 , Regarding your question, I need to escalate it to our internal team for further investigation. According to our process, please provide the end application name. Thanks for your cooperation. BR Celeste Re: KE18F512VLH16 ECC RAM Single Bit Correction Hi @Celeste_Liu  - P7 is the name of the end application. Re: KE18F512VLH16 ECC RAM Single Bit Correction Hi @Celeste_Liu, is there any update on this? Re: KE18F512VLH16 ECC RAM Single Bit Correction Hello @rseigle77 , Sorry, I still haven't received a response from the internal yet. I'll follow up with them again and make this my top priority. As soon as I hear anything back, I'll let you know right away. BR Celeste Re: KE18F512VLH16 ECC RAM Single Bit Correction Thanks for the response @Celeste_Liu, but that does not answer my question regarding MCM_LMFATR[PEFSIZE]: "Can MCM_LMFATR[PEFSIZE] be used to determine the access size? If so, can this be used in tandem with MCM_LMFAR to implement a read-correct-writeback operation? For example, if MCM_LMFATR[PEFSIZE] is 3'b000 indicating an 8-bit access, can I perform an 8-bit read from the address indicated by MCM_LMFAR then perform an 8-bit write to the same address to correct the error. Similarly, if MCM_LMFATR[PEFSIZE] is 3'b010 indicating a 32-bit access, can I perform a 32-bit write to the address indicated by MCM_LMFAR without worrying about alignment?" Re: KE18F512VLH16 ECC RAM Single Bit Correction Hello @rseigle77 , Thanks for your patience. I got the reply from the internal. ECC "correction" means returning corrected data to the CPU, not fixing the underlying bit stored in SRAM. Automatic repair requires a separate scrub/write-back mechanism. The recommended flow to use software scrub: ECC corrects data on read. Single-bit error interrupt/status is raised. Refer to RM 6.3.1.1 Determining source of the interrupt. MCM_LMPECR[ER1BR]=1 Software reads the fault address. MCM_LMPEIR[PEELOC] = 5'h08 - a 1-bit correctable ECC event from SRAM_L, MCM_LMFAR indicates fault address. Software rewrites the corrected value back to the same address. New ECC syndrome is generated and stored. BR Celeste
View full article
Regression/bug in U-Boot USB ID vs mainline Hello, `commit a5c91319731f ("MLK-25803-2: Update VID/PID")`, in U-Boot lf-6.18.20-2.0.0 branch,  introduces a regression in any user of USB. It forces a hard-coded USB product ID, instead of taking the value from the configuration. This is breaking any board that is using a different value from 0x0151. The issue is happening when using this U-Boot branch with non-NXP boards (using NXP SoC). This value needs to come from the configuration, and not be hard-coded. The following patch fixes the problem, can you apply it to your branch? ``` diff --git a/arch/arm/mach-imx/spl.c b/arch/arm/mach-imx/spl.c index 165cc82d9c72..46e26d138cf9 100644 --- a/arch/arm/mach-imx/spl.c +++ b/arch/arm/mach-imx/spl.c @@ -199,7 +199,7 @@ int g_dnl_bind_fixup(struct usb_device_descriptor *dev, const char *name) snprintf(serial_string, sizeof(serial_string), "%08x%08x", serialnr.high, serialnr.low); g_dnl_set_serialnumber(serial_string); #endif - put_unaligned(0x0151, &dev->idProduct); + put_unaligned(CONFIG_USB_GADGET_PRODUCT_NUM + 0xfff, &dev->idProduct); return 0; } ``` Re: Regression/bug in U-Boot USB ID vs mainline The issue is not your specific NXP needs that you just described. The issue is that hard coding the number in the code is preventing any user to configure it from the kconfig, as it is designed to be and effectively creating a regression. That change is disregarding any existing user that has a different need, actively breaking working use cases. Just grep for CONFIG_USB_GADGET_PRODUCT_NUM in the code and you'll see the multiple use cases this is breaking. You need to have a different solution that is not introducing a regression. Re: Regression/bug in U-Boot USB ID vs mainline Hello,  The change was intentional,  VID 0x525 and PID 0xa4a5 already registered as PLX Technology, Inc. Linux-USB File-backed Storage Gadget But fastboot device is not mass storage devices windowns 10 latest update already cached above vid/pid Change to use Freescale VID 0x1fc9 PID 0x151, for SPL SDP HID download PID 0x152, for Fastboot PID 0x153, for Kernel fastboot Need update uuu above 1.4.182  Re: Regression/bug in U-Boot USB ID vs mainline Hello,  I will inform the internal team of this so they will check if the patch is needed for the next release, at this moment you can implement your workaround.  Regards. Re: Regression/bug in U-Boot USB ID vs mainline > I will inform the internal team of this so they will check if the patch is needed for the next release, at this moment you can implement your workaround.  This is not working for us. We are implementing multiple fixes on your branch, and this one is just an example. We need a feedback from the developer if they are going to accept this patch or solve the issue in a different way. Sending patches and fixes and getting no feedback and having to wait to some future release, in which we will not even be notified on the decision, is not an effective way to collaborate. Can you please advise on a different way to move this forward? Thanks, Francesco Re: Regression/bug in U-Boot USB ID vs mainline Hello, A fix was pushed, so the issue should be resolved starting with our Q3 RC2 2026 release. Simona
View full article
无法在 MCIMX8Q!XP-CPU (Si B0) 上获取串口控制台或启动 Linux 系统 - UART 接口仅输出乱码。 你好, 我在启动MCIMX8QXP-CPU(硅版本 B0)板时遇到问题。 硬件: MCIMX8QXP-CPU(Si B0) MCIMX8-8X-BB 踢脚板 IMX-LVDS-HDMI 适配器连接到 J1 套装内附带的原装 16GB SD 卡 我还尝试了一张新刷入官方 Linux BSP(L6.18.20 / MX8QXPC0 镜像)的 32 GB SD 卡。 问题: 串行控制台(J11)始终只显示乱码字符(□□□□),地址为 115200 8N1。 尝试了多个 COM 端口 尝试过不同的终端软件(PuTTY、Docklight) 在两台不同的Windows笔记本电脑上都试过了。 已安装最新的 FTDI VCP 驱动程序 使用原装套件SD卡和新刷机的SD卡,结果相同。 UUU始终无法在串行下载模式下检测到电路板(SW2 = 1000)。uuu -lsusb显示没有设备。下载模式下,主板未出现在设备管理器中。 HDMI – 目前没有显示输出(在 J1 上使用 IMX-LVDS-HDMI)。 尝试的启动开关: SD卡启动:SW2 = 开 开 关 关 串口下载:SW2 = 开 关 关 关 eMMC:SW2 = 关闭 开启 关闭 关闭 我已经完成了以下工作: 使用 Balena Etcher 和 Rufus 刷入了官方的.SD 卡镜像。 已确认SD卡已正确插入J12插槽 二手原装电源 检查了多根用于调试端口的 USB 线缆 请问有人能提供一些建议吗? Si B0 开发板在调试 UART 方面是否存在已知问题? 还有其他步骤可以获得清晰的控制台输出吗? 恢复/验证主板是否健康的推荐方法是什么?    HW-开源 i.MX 8 系列 | i.MX 8QuadMax (8QM) | 8QuadPlus Re: Unable to get serial console or boot linux on MCIMX8Q!XP-CPU (Si B0) - only garbage on UART 你好@drupadh , 感谢您联系恩智浦技术支持! 您遇到的错误是由于该镜像为 C0 硅版本构建的。 遗憾的是,我们没有为 B0 硅片版本提供预编译的 6.18.20 内核映像。不过,您可以使用 Yocto 自行构建。 版本时,请使用以下机器配置“ imx8qxpmek ” 如果您在搭建过程中需要任何帮助,请告诉我。 此致, 亚历杭德罗·加西亚 Re: Unable to get serial console or boot linux on MCIMX8Q!XP-CPU (Si B0) - only garbage on UART 有没有一步一步的指导指南可以参考?那将非常有帮助。 Re: Unable to get serial console or boot linux on MCIMX8Q!XP-CPU (Si B0) - only garbage on UART 另外,我想运行Windows系统,你能帮我选择一下适用于这个主板的文件吗?
View full article
虚拟机 vm mc9s08qg8 NXP支持Windows 11上的虚拟机吗?我想建一个 vm 然后下载 cw(经典 IDE)v5.2 这样我就可以使用我的 wiztronics 烧录板了!这能用NXP软件实现吗?你支持这一行动吗!!!!!!! Re: virtual machine vm mc9s08qg8 Hello 不建议使用虚拟机,我们无法保证在虚拟机内运行 IDE 中的工具时能够正常运行; 推荐的做法是在受支持的操作系统上以原生方式安装该工具,并使用相应的版本。在本例中,Windows 11 的 CodeWarrior 版本为 11.1。 顺祝商祺!
View full article
家をリノベーションしましょう 皆さん、こんにちは。 100平方メートルの家をどうやってリノベーションし、必要なだけスマートにするか考え始めたところです。家はかなり大規模なリノベーション(床暖房、エアコン、電動シャッターなど)を行う予定なので、ついでに何かをセットアップできます。私はエンジニアなので、システムをいじって動かすことに全く問題はありません。見てみると、最も経済的で汎用性の高い解決策は、すでに持っているRaspberry PiでHome Assistantをローカルに動かし、必要なすべてのデバイスを揃え、5〜7インチのディスプレイですべてを見たり操作したりすることです。プロトコルについて迷っています。Wi-Fiベースのプロトコルを使うべきか、それとも有線接続(KNXと聞いたのですが?)を使うべきか…。有線接続の方が効率的だとは思うのですが、その分コストも高くなります。それだけの価値はあるのか?リノベーション中だけどスマートホームの仕組みにあまり詳しくない人への追加のアドバイスはありますか? Re: Renovate your home こんにちは、 @ozipin さん。 すべてのデバイスを連携させる通信方法は、あなたのニーズや要件によって大きく異なりますが、一般的にZigbeeのような特定のプロトコルはスマートホームのニーズをカバーするために作られているので、Zigbee対応のデバイスを調べることをおすすめします。これにより、有線通信と同等の信頼性を確保しつつ、はるかに高い柔軟性を実現し、コストを削減できるはずです。 ビルディング&ホームオートメーション |NXPセミコンダクターズのウェブページで、スマートホームを実現する方法について詳しく知ることができます。 BR、 エドウィン。
View full article
CodeWarrior Build error Every so-often I get a build error:- mingw32-make: *** No rule to make target Dropbox//Projects/\Project_x/\Project_Headers/\../\Sources/\Events.c',                     needed by `Sources/Events_c.obj'.  Stop. The file Events_c.obj does, of course, exist, but the usual remedies do not work. I tried a Clean build, I deleted Events_c.obj', I deleted the whole Flash folder, I tried shutting down and re-starting but nothing worked. I ended up creating a new project and cut and pasted the source file content. This problem occurs once every few weeks and on a couple of occasions, after the computer was "sleeping", the problem cleared itself. Re: CodeWarrior Build error This sounds less like an issue with the .obj file itself and more like a stale or malformed dependency path in the generated Makefile. The Dropbox//Projects/\Project_x... path with the odd slashes is a big clue. I’d check whether the project is being built directly from a Dropbox-synced folder and try moving it to a local, non-synced directory. Also, compare the generated dependency/Makefile entries when the problem occurs with a working build. If the error disappears after the Dropbox folder syncs or the PC wakes, that would further point toward Dropbox/file-system timing rather than the source file.      Re: CodeWarrior Build error Thanks, the sync issue makes sense, but it will be a few days before I can try it. Re: CodeWarrior Build error Hello, Which version of CodeWarrior are you using? Does the Clean build that you tried is by using the commander>Clean (All)? When you move to a new project it works and after a few weeks happens again? Probably your make files doesn’t match according to your directory. Please try this to clean and make a re-creation of the make files On the Project view>Clean>Select your project to build   luis_maravilla_1-1787091476012.png Also, as a recommendation do not use the Dropbox folder, kindly change to a local path and add it or change it in the build directory. Please refer to this post for more information No rule to make target | MCU on Eclipse Best Regards, Luis
View full article
FlexIO0 SPIコントローラーのTXシフター(SHIFTCTL, PINCFG=11b)は、SHIFTSにもかかわらず出力ピンを駆動しません 取締役会: FRDM-MCXN236(MCX N236、デュアルCortex-M33) ツールチェーン: MCUXpresso IDE 25.6.136,ベアメタルレジスタレベルC(SDK周辺機器ドライバーなし) RMの参考文献: MCX N23x リファレンスマニュアル Rev. 4、2025-03-05、第53章(FlexIO)、表453(SPIコントローラ、CPHA=0構成) 私が作っているもの: FlexIO0はRM表453に従いSPIコントローラとして構成:シフター2台(shifter0 = TX、shifter1 = RX)+タイマー1台(timer0 = SCK、デュアル8ビットカウンタボーモード)、SPI経由でBME280センサーを読み込みます。ピン: P1_0/P1_1/P1_2 は ALT6 (FLEXIO0_D8/D9/D10) に多重化され、PORT1->PCR の読み取りによって正しいことが確認されています。 観察: RXシフターとSCKタイマー出力はどちらも完全に動作します。SCKは正常にスケジュール通りに切り替わり(2つの独立したレジスタで確認済み、下記参照)、SHIFTSTAT/TIMSTATはすべての転送が正常に、時間通りに、エラーなく完了したことを報告します。しかし、 TXシフターの出力ピン(SDO、D8)は、私が思いつく限りのあらゆるバリエーションで、そこに何が書き込まれていても、電気的な動きを全く示しません。センサーからのチップIDレジスタの読み込みは常に 0x00 であり、期待される 0x60 ではありません(同じボード、同じセンサー、同じブート上の動作する FlexComm/LPSPI3 ドライバーが正しく読み取れます)。 レジスタ構成(RMテーブル453と完全に一致、PINSELは実際のピンに置き換えられています) SHIFTCFG0 = 0x0000_0000 (RM: 0000_0000h -- スタート/ストップビット無効) SHIFTCTL0 = 0x0083_0002 (RM: 0083_0002h、PINSEL=8 (実際のD8/SDOの場合)) デコード結果: TIMSEL=0、TIMPOL=1(負エッジ)、PINCFG=3(11b、駆動出力) PINSEL=8、PINPOL=0、SMOD=2(送信) -- すべてのフィールドがRMのものと照合されます 文字通りの例では、PINSELのみが置換されています。 SHIFTCFG1 = 0x0000_0000 SHIFTCTL1 = 0x0000_0101 (RM: 0000_0101h、PINSEL=10 (実際のD10/SDIの場合)) TIMCMP0 = RM独自の式に基づいて算出(8ビットフレーム、1MHz SCK用のボー分周器) TIMCFG0 = 0x0100_2222 (RMリテラル値、ピン置換不要) TIMCTL0 = 0x01C3_0201 (RM: 01C3_0201h、PINSEL=9 (実際のD9/SCKの場合)) 私が除外した可能性は、それぞれハードウェアの直接的な証拠(デバッガによるレジスタ/メモリの検査、オシロスコープは使用不可)に基づいている。 ピンマルチプレクサがALT6に到達していません -- PCRの読み取り結果から、使用されている4つのピンすべてでALT6の設定が正しいことが確認されました。 センサ/配線の故障――別の動作するFlexComm/LPSPI3 SPIドライバが同じ物理センサ、同じ起動時にチップID(0x60)を正しく読み取ります。 SCKは物理ピンで一度もトグルしなかった――同時にサンプリングされた2つの独立したレジスタ、FLEXIO0->PIN(ビット9)とGPIO1->PDIR(ビット1、完全に別の周辺ブロックで、FlexIO内部ロジックを経由しない)によってトグルが確認された。両者はリアルタイムで、サンプルごとに一致する。 SHIFTBUFBIS (ビットスワップされたエイリアスレジスタ) 内の TX バイトレーンの配置 -- 下位バイト、上位バイト (RM 53.3.1 から再導出) を試しました。シフトレジスタのマイクロアーキテクチャ記述(サマリーテーブルだけでなく)、バイトレーンに依存しない完全な32ビット交互書き込み(0xAAAAAAAA)など、すべて同一の永続的にフラットなSDOを生成します。 TXバッファアンダーラン(SHIFTERR)-- RX準備完了待機が成功した直後にキャプチャされ、毎回0x0(クリーン)を読み取ります。 ピン/パッド固有の障害 -- shifter0 の PINSEL をまったく異なる物理ピン (D8 ではなく D9) に再ターゲットしましたが、依然として平坦です。タイマーは、同一のPINCFG=11b「駆動出力」機構を使用して、どちらのピンも正しく駆動します。 「有効化時の暗黙的なロード」(RM 53.3.1:シフターの状態フラグは、「データがSHIFTBUFからシフターにロードされたとき、またはシフターが送信モード用に最初に構成されたとき」に設定されます。つまり、最初のサイクルでロードされた古いデータが存在する可能性があります)は、最初の転送を破棄し、続いてトレースされた明確な2番目の転送を行うことで除外されました。結果は同一で、フラットな状態でした。 SHIFTBUFBIS エイリアス書き込みパスの非対称性 -- SHIFTBUFBIS[0] の代わりに、エイリアスされていないプレーンな SHIFTBUF[0] レジスタを介して同じバイトレーン非依存パターンを書き込みました: 同じフラットな結果。 FLEXIO0->PINOUTD/PINOUTE/PINOUTDIS(グローバルなピンごとのソフトウェア出力オーバーライドレジスタ、RM 53.3.3)-- ライブ読み取りでは、動作中のSCKピンと動作していないSDOピンの両方で、すべてゼロが表示されます。これは、「タイマー/シフター構成によって制御されている」(通常の状態)ことを意味します。原因ではない。 FLEXIO0->PINの読み取り自体が信頼できない - 上記の#3を参照。GPIO1->PDIRを介して独立して確認済み。 Shifter0インスタンス固有の不具合 -- 代わりに、ビット単位で同一のSHIFTCTL値で構成されたshifter2を使用して、全く同じフラットな結果を再現しました。同じ失敗。特定のインスタンスに限った話ではありません。 RM 53.7.1.27の文書化された 2 段階の PINCFG 書き込みシーケンス (最初に 10b を書き込み、次に 11b に別途書き込み、最初の構成時の短い低グリッチを回避する) -- 直接適用: 同じフラットな結果。 また、この部分に関する唯一の公開されたマスクセットエラッタ文書(MCXN23x_0P21K Rev. 2.0)も確認しましたが、FlexIO関連の項目は一切ありません。また、NXP自身のFlexIO-SPIアプリケーションノート(AN12780)も確認しました。後者はRM表453がすでに記載しているもの以上の指針を加えていません。 質問: シフターの内部帳簿(SHIFTSTAT、SHIFTERR、TIMSTAT)は、すべてのテストで完全に正常で、スケジュールどおりで、エラーのない送信モード動作を報告しており、同じCSブラケットトランザクション内の複数の転送にわたってTX準備完了フラグが正しくクリアおよび再設定されています。これはRM 53.3.1によれば、真のタイマートリガーによるリロードでのみ発生するはずです。また、シフトクロック自体(同じPINCFG=11b「駆動出力」メカニズムですが、SHIFTCTLではなくTIMCTL経由)が物理ピンに正しく到達することが独立して証明されています。 レジスタレベルの設定がすべてRMテーブル453の具体的な例と完全に一致するにもかかわらず、シフタのSHIFTCTL.PINCFG=11b送信モード出力(タイマーの同じPINCFG=11b出力とは対照的に)がMCXN23xマスクセット上の割り当てられたピンに到達できないような、既知のシリコン動作、文書化されていない前提条件、またはRMのギャップは存在するのでしょうか? 必要であれば、レジスタレベルのプロジェクトソースコード全体と、完全な追記専用の調査ログ(試行したすべての仮説、すべての撤回、およびそれぞれの正確なハードウェア証拠)を喜んで共有します。     MCX N Re: FlexIO0 SPI-controller TX shifter (SHIFTCTL, PINCFG=11b) never drives its output pin, despite SH こんにちは、 @hafeezmhdさん 提供された情報に基づくと、 SHIFTCTL.PINCFG = 11b で送信モードに構成されたシフターが割り当てられたピンを駆動している間、同じFlexIOインスタンス上のタイマー出力が正常に動作することを妨げるような、既知のMCXN23xシリコンの制限、エラー、または文書化されたFlexIO要件は見当たりません。 タイマー出力が物理ピンに正しく到達していることが確認されており、FlexIOステータスフラグもシフターの正常な動作を示しているため、お客様が観察されている動作は、FlexIO SPI構成に関するドキュメントに記載されている通常の動作とは異なります。 この時点で、完全なソースコードと初期化シーケンス、および初期化後と転送直前に取得した完全なレジスタダンプを確認することが役立つでしょう。これは、レジスタ抜粋だけでは明らかにならない、微妙な構成上の依存関係を特定するのに役立つ可能性があります。 可能であればプロジェクトの情報源を教えていただければ、詳しくご覧いただけます。 BR ハリー
View full article
S32K311NHT0MPAST During MCU sleep mode, should the GPIO output state be retained (latched) or reset to its default state?Please confirm Re: S32K311NHT0MPAST Hi During S32K3 standby mode the GPIO output state is retained (latched).  For more detail please read the discussion in Where does the program start running after S32K344 wakes up from standby? Best Regards, Robin
View full article
virtual machine vm mc9s08qg8 does nxp support vm on windows 11 ? i want to build a vm and download cw(classic IDE) v5.2 so i can use my wiztronics burner board! Is this possible with NXP software. Do u support this action!!!!!!!! Re: virtual machine vm mc9s08qg8 Hello The usage of Virtual machines is not recommended, we cannot guarantee proper functionality when running tools in the IDE inside a virtual machine; The recommended path is to install the tool natively on a supported OS and using the corresponding version, In this case for windows 11 the CodeWarrior version is 11.1 Best Regards
View full article
CodeWarriorのビルドエラー 時々ビルドエラーが出ます: mingw32-make: *** ターゲットにするルールはありません Dropbox//Projects/\Project_x/\Project_Headers/\../\Sources/\イベント情報.c',`Sources/Events_c.obj` で必要です。  停止。 ファイル Events_c.obj は確かに存在しますが、通常の対処法では解決しません。クリーンビルドを試しました。Events_c.obj を削除しました。Flashフォルダ全体を削除し、シャットダウンと再起動も試しましたが、何も効果がありませんでした。結局、新しいプロジェクトを作成し、ソースファイルの内容をコピー&ペーストしました。この問題は数週間に一度発生し、数回はコンピューターが「スリープ状態」になった後に自然に解消されました。 Re: CodeWarrior Build error ありがとうございます。同期の問題は納得できますが、試せるまで数日かかりそうです。 Re: CodeWarrior Build error これは.objファイルの問題というよりは、ファイル自体、あるいは生成された Makefile 内の古いまたは不正な依存関係パスのようなものです。Dropbox//Projects/\Project_x... というパスに奇妙なスラッシュが含まれていることが大きな手がかりです。プロジェクトがDropboxと同期されたフォルダから直接ビルドされているかどうかを確認し、ローカルの同期されていないディレクトリに移動してみてください。また、問題が発生した際に生成された依存関係/Makefileのエントリを、正常にビルドできた場合と比較してください。Dropboxフォルダの同期後、またはPCのスリープ解除後にエラーが解消される場合は、ソースファイルではなく、Dropbox/ファイルシステムのタイミングに問題がある可能性が高いでしょう。 Re: CodeWarrior Build error こんにちは、 CodeWarriorのどのバージョンを使用していますか? あなたが試したクリーンビルドは、コマンド>クリーン(すべて)を使用したものですか? 新しいプロジェクトに移るとうまくいくのに、数週間後にまた同じことが起こる? おそらく、あなたのMakefileがディレクトリに合わせていないのでしょう。 メイクファイルをクリーンアップして再作成するには、以下の手順をお試しください。 プロジェクトビューで > クリーン > ビルドするプロジェクトを選択   luis_maravilla_1-1787091476012.png また、推奨事項として、Dropboxフォルダは使用せず、ローカルパスに変更してビルドディレクトリに追加または変更してください。 詳細はこの投稿をご覧ください。 ターゲットにするルールはありません |MCUのエクリプス 敬具、ルイス
View full article
Renovate your home Hi everyone, I'm just starting to think about how to renovate a 100-square-meter house and make it as smart as I need. The house will be undergoing a fairly extensive renovation (underfloor heating, air conditioning, electric shutters, etc.), so I can set something up while I'm at it. I'm an engineer, so I have no problem messing around with some system to get it working. Looking around, I think the most economical and versatile solution is to have Home Assistant running locally on a Raspberry Pi (which I already have) and then all the devices I need, with a 5-7 inch display from which I can view and control everything. I'm unsure about the protocol: should I rely on Wi-Fi-based protocols or something wired (I read KNX?)? Obviously, I think wired is more efficient, but also more expensive. Is it worth it? Do you have any additional advice for someone who's renovating but isn't very familiar with the ins and outs of the smart home world? Re: Renovate your home Hi @ozipin, The communication method to coordinate all devices really depends on your needs and requirements, but generally specific protocols like Zigbee were created precisely to cover the needs of smart homes, so I would suggest looking into Zigbee capable devices. This should provide similar reliability to wired communication, while allowing for much more flexibility and reducing the costs. I highly recommend taking a look at the Building and Home Automation | NXP Semiconductors webpage to get more insight on how our can enable your smart home. BR, Edwin.
View full article
LX2160A JTAG (CCS) connection fails I'm trying to use DDR Tool with my LX2160A, but I can't connect. I think the cause is that the CCS cannot confirm the JTAG connection. Attach the result of the IDcode verification. KAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.png When I tried connecting a while ago, I was able to confirm a connection from JTAG, but the files were corrupted, and since revisions were not carefully managed, recovery was not possible. We are unaware that downloading from the internet via "check for update" can sometimes result in file corruption, and therefore we are currently unable to match the software's status. Since I was able to connect once, I suspect it might be a software issue. If you know a solution, please let me know. Thank you very much for your understanding. Re: LX2160AのJTAG(CCS)接続が失敗する Thank you for your reply. I performed the installation using "CodeWarrior for ARMv8 v11.5.0 b200629 Windows Offline Installer". After that, I tried updating using CodeWarrior IDE by selecting Help → Install New Software → Add → Archive and specifying com.freescale.armv8.11.5.12.GA.Win.updatesite.221209.zip, but an error occurred during installation. The error message is as follows: KAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.png An error occurred while installing the items session context was:(profile=epp.package.cpp, phase=org.eclipse.equinox.internal.p2.engine.phases.Install, operand=[R]com.freescale.core.debugger.fsl_gdb13.0.0.202003111126 --> [R]com.freescale.core.debugger.fsl_gdb14.0.0.202204131357, action=com.freescale.updater.customactions.actions.FreescaleProcessCheck). NLS missing message: param_not_set in: com.freescale.updater.customactions.Messages Could you please advise me on how to deal with this? Thank you very much for your understanding. Re: LX2160AのJTAG(CCS)接続が失敗する Please check whether you have installed the latest CodeWarrior for ARMv8 11.5.12. Please open CodeWarrior IDE and check the version from Help->About CodeWarrior Development Studio for QorIQ LS series - ARM V8 ISA. If you have already installed this version CodeWarrior, please plug off USB cable from CodeWarrior TAP and plug in again. Re: LX2160AのJTAG(CCS)接続が失敗する Thank you for your reply. The version information for CodeWarrior currently in use is as follows: CodeWarrior Development Studio for QorIQ LS series - ARM V8 ISA Version: 11.5.0 Build ID: 200629GA Compared to the latest version you provided, my environment appears to be running an older version. By the way, if I select "com.freescale.armv8.11.5.12.GA.Win.updatesite.221209.zip" via "Install New Software" → "Add" → "Archive", which items should I install? Selecting "Select All" results in an error and the installation fails. Re: LX2160AのJTAG(CCS)接続が失敗する Please install CW_ARMv8_v2020.06_b200629GA_Win_Offline.exe first, then open CodeWarrior IDE and install service pack com.freescale.armv8.11.5.12.GA.Win.updatesite.221209.zip from Help->Install New Software->Add->Archive. If your problem persists, please provide screenshot to show your error. Re: LX2160AのJTAG(CCS)接続が失敗する Please download my installation file from the following link, and reinstall CodeWarrior for ARMv8 11.5.12. https://support.nxp.com/s/case/500Te00000eeSJXIA2/community-lx2160a%E3%81%AEjtagccs%E6%8E%A5%E7%B6%9A%E3%81%8C%E5%A4%B1%E6%95%97%E3%81%99%E3%82%8B?language=en_US Re: LX2160AのJTAG(CCS)接続が失敗する Are you installing CodeWarrior for ARMv8 in Windows 10? Please remove all your CodeWarrior installation file first. Please install CW_ARMv8_v2020.06_b200629GA_Win_Offline.exe from my tar ball. Then open CodeWarrior IDE in a new workspace, and install service pack com.freescale.armv8.11.5.12.GA.Win.updatesite.221209.zip from Help->Install New Software->Add->Archive. Re: LX2160AのJTAG(CCS)接続が失敗する Thank you for your support. As requested, I attempted to reinstall CodeWarrior for ARMv8 11.5.12 using the download link you provided. However, an error occurred while installing the update package. I have already replied within the download link page with the details of the error, so could you please check it? Do you have any idea what might be causing this issue? I would appreciate your continued support in resolving this matter. This message was translated using machine translation. Re: LX2160AのJTAG(CCS)接続が失敗する 1. Please remove your CodeWarrior installation folder. 2. Please don't use your original installation file. Please use both .exe and zip files from my download link. 3. After installation the exe file, please open CodeWarrior IDE in a new workspace to install the zip service package. Re: LX2160AのJTAG(CCS)接続が失敗する At "Work with" you selected "Only local sites", this is also incorrect, please don't select anything, just keep it empty. Then click "Add" -> "Archive", and specify the location of the service Package. Please refer to my following screenshot. yipingwang_0-1787913595385.pngyipingwang_0-1787913595385.pngyipingwang_0-1787913595385.pngyipingwang_0-1787913595385.pngyipingwang_0-1787913595385.pngyipingwang_0-1787913595385.pngyipingwang_0-1787913595385.pngyipingwang_0-1787913595385.pngyipingwang_0-1787913595385.pngyipingwang_0-1787913595385.pngyipingwang_0-1787913595385.pngyipingwang_0-1787913595385.pngyipingwang_0-1787913595385.pngyipingwang_0-1787913595385.png Re: LX2160AのJTAG(CCS)接続が失敗する Please install service pack com.freescale.armv8.11.5.12.GA.Win.updatesite.221209.zip from Help->Install New Software->Add->Archive. Not from "Available Software Sites" Please also delete Cache folder. C:\Users\ \.p2 or C:\Users\ \.p2\org.eclipse.equinox.p2.* Re: LX2160AのJTAG(CCS)接続が失敗する Thank you for your reply. Suspecting that the downloaded files might have been corrupted, I downloaded them again and attempted the updates as follows. In Available Software Sites, I selected: Add → Archive → com.freescale.armv8.11.5.12.GA.Win.updatesite.221209.zip from the extracted download package. After doing so, "CodeWarrior Updates" was added to the list, and I enabled only this update site. To simplify the investigation, I then used Available Updates and installed the updates one by one, starting from the top of the list. The following updates failed with errors. The error messages are listed below. • CodeWarrior Debugger GTA 14.0.0.202212090959 An error occurred while installing the items. session context was: (profile=epp.package.cpp, phase=org.eclipse.equinox.internal.p2.engine.phases.Install, operand=[R]com.freescale.core.debugger.gta 14.0.0.202006241928 --> [R]com.freescale.core.debugger.gta 14.0.0.202212090959, action=com.freescale.updater.customactions.actions.FreescaleProcessCheck). NLS missing message: param_not_set in: com.freescale.updater.customactions.Messages • NXP GDB 14.0.0.202204131357 An error occurred while installing the items. session context was: (profile=epp.package.cpp, phase=org.eclipse.equinox.internal.p2.engine.phases.Install, operand=[R]com.freescale.core.debugger.fsl_gdb 13.0.0.202003111126 --> [R]com.freescale.core.debugger.fsl_gdb 14.0.0.202204131357, action=com.freescale.updater.customactions.actions.FreescaleProcessCheck). NLS missing message: param_not_set in: com.freescale.updater.customactions.Messages • QorIQ Configuration and Validation Suite - Common Layout 4.24.0.FSL20221019_2247 An error occurred while installing the items. session context was: (profile=epp.package.cpp, phase=org.eclipse.equinox.internal.p2.engine.phases.Install, operand=null --> [R]com.freescale.cw.qcvs.feature_root 4.24.0.FSL20221019_2247, action=com.freescale.updater.customactions.actions.FreescaleProcessCheck). NLS missing message: param_not_set in: com.freescale.updater.customactions.Messages I did not test CodeWarrior Core IDE 14.0.0.202212091004 and CodeWarrior Debugger 14.0.0.202212091004, since these packages appear to include the software listed above. All other updates were installed successfully without any issues. As an additional verification step, I will try installing the software packages available through "Install New Software." The results of testing the individual update packages have already been provided above. If you have any information regarding the cause of these errors or any known issues related to them, I would greatly appreciate your advice. Thank you for your assistance. This message was translated using machine translation. Re: LX2160AのJTAG(CCS)接続が失敗する Thank you for your support. I followed the procedure you suggested and performed the following steps: Completely uninstalled the entire CodeWarrior installation (not only the service pack). Deleted the following cache folders: C:\Users\ \.p2 C:\Users\ \.p2\org.eclipse.equinox.p2 Reinstalled CodeWarrior. Opened Help → Install New Software → Add → Archive and specified the file com.freescale.armv8.11.5.12.GA.Win.updatesite.221209.zip. After adding the archive, I attempted both Install and Update operations for the plugins provided by the service pack through Install New Software. As a result, most of the plugins from the service pack were downloaded and installed successfully. However, the plugins shown in the attached screenshot failed during the installation/update process and could not be updated. KAZU_ISHI_0-1787912782459.pngKAZU_ISHI_0-1787912782459.pngKAZU_ISHI_0-1787912782459.pngKAZU_ISHI_0-1787912782459.pngKAZU_ISHI_0-1787912782459.pngKAZU_ISHI_0-1787912782459.pngKAZU_ISHI_0-1787912782459.pngKAZU_ISHI_0-1787912782459.pngKAZU_ISHI_0-1787912782459.pngKAZU_ISHI_0-1787912782459.pngKAZU_ISHI_0-1787912782459.png Best regards, Re: LX2160AのJTAG(CCS)接続が失敗する Thank you for your guidance. I reviewed the update configuration as you suggested. Starting from a clean installation, I configured the settings to match those shown in the attached screenshot and then attempted the installation. KAZU_ISHI_0-1787974046471.pngKAZU_ISHI_0-1787974046471.pngKAZU_ISHI_0-1787974046471.pngKAZU_ISHI_0-1787974046471.pngKAZU_ISHI_0-1787974046471.pngKAZU_ISHI_0-1787974046471.pngKAZU_ISHI_0-1787974046471.pngKAZU_ISHI_0-1787974046471.pngKAZU_ISHI_0-1787974046471.pngKAZU_ISHI_0-1787974046471.png However, as shown in the attached video file, the installation still fails with an error even when the settings are configured exactly the same way. I also noticed that the number of items displayed differs from the screenshot you provided. Could this difference be related to the issue, or do you have any idea what might be causing it? I would appreciate any advice you may have. Thank you for your assistance. I look forward to hearing from you. This message was translated using machine translation. Re: LX2160AのJTAG(CCS)接続が失敗する Thank you for your clarification. Today, I repeated the installation process and confirmed the following. First, I uninstalled the following applications from Windows Settings > Installed Apps: - CodeWarrior Development Studio for QorIQ LS series - ARM V8 ISA v11.5.0 - CodeWarrior for ARMv8 v2020.06 Next, I deleted the following folders under my Windows user directory: - .codewarrior - .eclipse - .p2 I then downloaded the package again, extracted it, and performed a fresh installation. At that point, the Available Software Sites configuration matched the screenshot you provided, as shown in the attached screenshot. KAZU_ISHI_1-1788156348600.pngKAZU_ISHI_1-1788156348600.pngKAZU_ISHI_1-1788156348600.pngKAZU_ISHI_1-1788156348600.pngKAZU_ISHI_1-1788156348600.pngKAZU_ISHI_1-1788156348600.pngKAZU_ISHI_1-1788156348600.pngKAZU_ISHI_1-1788156348600.pngKAZU_ISHI_1-1788156348600.png However, when I attempted to install the update package, an error occurred. I would also like to correct the information I provided previously. The screenshot I sent before was captured after the update error had occurred and after the IDE had been restarted. As a result, the screenshot did not represent the state immediately after the fresh installation. I apologize for sending the wrong screenshot and for any confusion this may have caused. Thank you for your assistance. I look forward to hearing from you. This message was translated using machine translation. Re: LX2160AのJTAG(CCS)接続が失敗する Hello, Attached are the configuration text files for the following scenarios: 1.Fresh installation 2.After applying the update package (the update failed before completion) 3.After performing the update again using the update icon shown in the bottom-right corner of the CodeWarrior IDE window after the failure in scenario 2 Best regards, Re: LX2160AのJTAG(CCS)接続が失敗する Please refer to my following screenshot, the first item is different from yours. yipingwang_0-1788146095643.pngyipingwang_0-1788146095643.pngyipingwang_0-1788146095643.pngyipingwang_0-1788146095643.pngyipingwang_0-1788146095643.pngyipingwang_0-1788146095643.pngyipingwang_0-1788146095643.png Did you reinstall file CW_ARMv8_v2020.06_b200629GA_Win_Offline.exe provided by me? Re: LX2160AのJTAG(CCS)接続が失敗する Probably this issue is related with your Windows 11 OS. Please open CodeWarrior IDE, and click Help->Install New Software->Already installed->Configuration, this copy the configuration to a txt file and send it to me. Re: LX2160AのJTAG(CCS)接続が失敗する In addition please check the property of the service Pack, whether the size the same. yipingwang_0-1788251622006.pngyipingwang_0-1788251622006.pngyipingwang_0-1788251622006.pngyipingwang_0-1788251622006.pngyipingwang_0-1788251622006.png Re: LX2160AのJTAG(CCS)接続が失敗する I didn't find obvious difference except the language setting. Please edit C:\Freescale\CW4NET_v2020.06\CW_ARMv8\eclipse\eclipse.ini to add the following lines. -Dfile.encoding=Cp1252 -Dsun.jnu.encoding=Cp1252 -Dorg.osgi.framework.language=en Open CodeWarrior IDE with  C:\Freescale\CW4NET_v2020.06\CW_ARMv8\eclipse\eclipse.exe -nl en Then try whether it is possible to do upgrade. Re: LX2160AのJTAG(CCS)接続が失敗する Please run CodeWarrior as Administrator. Do you have a PC with Windows 10 22H2? If yes, please try whether you can install CodeWarrior for ARMv8 11.5.12 on Windows 10 22H2. Re: LX2160AのJTAG(CCS)接続が失敗する Hello, I followed the requested procedure, modified eclipse.ini as instructed, launched CodeWarrior with the following command: C:\Freescale\CW4NET_v2020.06\CW_ARMv8\eclipse\eclipse.exe -nl en and then attempted the update using Help -> Install New Software. However, the update still failed. I have attached the error log file for your review. I also noticed that some errors are already present in the log immediately after a fresh installation, before any update attempt. Could these errors be related to the update failure? The attached log includes both: - the initial startup after installation, and - the subsequent update attempt performed via Help -> Install New Software. Best regards, Re: LX2160AのJTAG(CCS)接続が失敗する Please refer to the supported OS in "3. System Requirements" in https://www.nxp.com/docs/en/release-note/CW-ARMV8-RN.pdf
View full article
S32K311NHT0MPAST MCUスリープモード中、GPIOの出力状態は保持(ラッチ)されるべきか、それともデフォルト状態にリセットすべきか?必ず確認してください Re: S32K311NHT0MPAST ハイ S32K3のスタンバイモード中は、GPIO出力状態が保持(ラッチ)されます。 詳細については、 「S32K344がスタンバイ状態から復帰した後、プログラムはどこで実行を開始しますか?」の議論を参照してください。 よろしくお願いいたします ロビン
View full article
如何初始化J3H081智能卡 您好,我购买了一张J3H081 JCOP卡。 我还收到了 、 、 、 、 、 以及一条 APDU 线“ 00F0 0000 10 ” 我使用 GlobalPlatformPro 尝试了 APDU 线路,它返回 6A82。 我完全不知道如何初始化这张卡。 我没有说明书,我想学习如何编写Java卡的程序。 Re: How to initialize J3H081 SmartCard JCOP 是一款高度安全的元件产品,因此,所有技术支持、文档访问和软件/工具请求都必须通过您授权的 NXP 代理商处理。 请联系您向其购买 JCOP 卡的代理商。   此致敬礼, 阿隆德拉 Re: How to initialize J3H081 SmartCard 所以,我不明白为什么 neven.cz 只卖给我一张卡。 他们告诉我“买家必须知道如何使用它,我们不知道怎么用”。 所以 neven.cz 与 NXP 没有合作关系,他们只是从其他地方购买显卡然后转售。灰色市场。 由于多次操作错误,我最终把卡弄坏了。 所以我给neven.cz发了邮件,他们说会给我退款。 我后来买了一张 ACOSJ,那张卡是 OP_READY 的,带有默认密钥,而且非常好用。 很抱歉占用NXP社区的时间。
View full article
仮想マシン vm mc908qg8 NXPはWindows 11でVMをサポートしていますか?VMを構築して、CW(クラシックIDE)v5.2をダウンロードして、Wiztronicsのバーナーボードを使いたいと思っています!これはNXPのソフトウェアで可能でしょうか?この行動を支持しますか!!!!!!! Re: virtual machine vm mc9s08qg8 Hello 仮想マシンの使用は推奨されません。仮想マシン内でIDE内でツールを動かす際に適切な機能を保証することはできません。 推奨される方法は、サポートされているOSにネイティブインストールし、対応するバージョンを使うことです。この場合、Windows 11のCodeWarriorバージョンは11.1です よろしくお願いいたします。
View full article
LX2160AのJTAG(CCS)接続が失敗する LX2160Aに対し、DDR toolの使用を考えていますが、Connectができません。 原因はCCSより、JTAGの接続が確認できないことだと思います。 IDcodeの確認結果を添付します。 KAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.pngKAZU_ISHI_0-1786615924736.png 少し前に接続を試した際はJTAGからの接続が確認できましたが、ファイルが破損してしまったことと、細かくリビジョンを管理しておらず復元できておりません。 check for Updateより、インターネットからダウンロードを実施するとファイルが破損するケースが存在することを把握しておらず、現在ソフトウェアの状態を一致させることができないでいます。 一度接続できたため、ソフトウェアの問題かと思いますが、解決方法をご存じでしたらご教授願います。 以上よろしくお願いいたします。 Re: LX2160AのJTAG(CCS)接続が失敗する まずCW_ARMv8_v2020.06_b200629GA_Win_Offline.exeをインストールし、その後CodeWarrior IDEを開き、Help->Install New Software->Add->Archiveからサービスパックcom.freescale.armv8.11.5.12.GA.Win.updatesite.221209.zipをインストールしてください。 問題が解決しない場合は、エラー画面のスクリーンショットをご提供ください。 Re: LX2160AのJTAG(CCS)接続が失敗する 最新版のCodeWarrior for ARMv8 11.5.12がインストールされているかどうか確認してください。 CodeWarrior IDEを開き、QorIQ LSシリーズ(ARM V8 ISA)のHelp->About CodeWarrior Development Studioのバージョンを確認してください。 既にこのバージョンのCodeWarriorをインストールしている場合は、CodeWarrior TAPからUSBケーブルを抜き、再度差し込んでください。 Re: LX2160AのJTAG(CCS)接続が失敗する ご返信ありがとうございます。 現在使用しているCodeWarriorのバージョン情報は以下の通りです。 CodeWarrior Development Studio for QorIQ LS series - ARM V8 ISA Version: 11.5.0 Build Id: 200629GA ご連絡いただいた最新バージョンと比較すると、私の環境は古いバージョンのようです。 ちなみに、「Install New Software」→「Add」→「Archive」から 「com.freescale.armv8.11.5.12.GA.Win.updatesite.221209.zip」を選択した場合、どの項目をインストールすればよいでしょうか。 「Select All」を選択すると、エラーが発生し、インストールが成功しません。 Re: LX2160AのJTAG(CCS)接続が失敗する ご返信ありがとうございます。 「CodeWarrior for ARMv8 v11.5.0 b200629 Windows Offline Installer」からインストールを実行しました。 その後、CodeWarrior IDEで、Help → Install New Software → Add → Archive から com.freescale.armv8.11.5.12.GA.Win.updatesite.221209.zip を指定して更新を試みましたが、インストール中にエラーが発生します。 エラーメッセージは以下の通りです KAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.pngKAZU_ISHI_0-1786959225115.png An error occurred while installing the items session context was:(profile=epp.package.cpp, phase=org.eclipse.equinox.internal.p2.engine.phases.Install, operand=[R]com.freescale.core.debugger.fsl_gdb 13.0.0.202003111126 --> [R]com.freescale.core.debugger.fsl_gdb 14.0.0.202204131357, action=com.freescale.updater.customactions.actions.FreescaleProcessCheck). NLS missing message: param_not_set in: com.freescale.updater.customactions.Messages 対処方法についてご教示いただけますでしょうか? 以上よろしくお願いいたします。 Re: LX2160AのJTAG(CCS)接続が失敗する 以下のリンクからインストールファイルをダウンロードし、CodeWarrior for ARMv8 11.5.12を再インストールしてください。 https://support.nxp.com/s/case/500Te00000eeSJXIA2/community-lx2160a%E3%81%AEjtagccs%E6%8E%A5%E7%B6%9A%E3%81%8C%E5%A4%B1%E6%95%97%E3%81%99%E3%82%8B?language=en_US Re: LX2160AのJTAG(CCS)接続が失敗する Windows 10にCodeWarrior for ARMv8をインストールしようとしていますか? まず、CodeWarriorのインストールファイルをすべて削除してください。 私のtarボールからCW_ARMv8_v2020.06_b200629GA_Win_Offline.exeをインストールしてください。 その後、 新しいワークスペースでCodeWarrior IDEを開き、Help->Install New Software->Add->Archiveからサービスパックcom.freescale.armv8.11.5.12.GA.Win.updatesite.221209.zipをインストールします。 Re: LX2160AのJTAG(CCS)接続が失敗する 1. CodeWarriorのインストールフォルダを削除してください。 2. 元のインストールファイルは使用しないでください。.exe を両方とも使用してください。私のダウンロードリンクからzipファイルをダウンロードしてください。 3. exeファイルのインストール後、新しいワークスペースでCodeWarrior IDEを開き、zipサービスパッケージをインストールしてください。 Re: LX2160AのJTAG(CCS)接続が失敗する 再開まで今しばらくお待ちください。 ご依頼どおり、ご提供いただいたダウンロードリンクを使用して、CodeWarrior for ARMv8 11.5.12の再インストールを試みました。しかし、アップデートパッケージのインストール中にエラーが発生しました。 ダウンロードリンクのページにエラーの詳細をすでに返信していますので、ぜひ確認していただけますか? この問題の原因が何か心当たりはありますか? このマターの解決に向けて引き続きご支援いただけるとありがたいです。 このメッセージは機械翻訳によって翻訳されました。 Re: LX2160AのJTAG(CCS)接続が失敗する 「作業対象」で「ローカルサイトのみ」を選択されていますが、これも誤りです。何も選択せず、空欄のままにしてください。次に「追加」→「アーカイブ」>、サービスパッケージの場所を指定します。 以下のスクリーンショットをご参照ください。 yipingwang_0-1787913595385.pngyipingwang_0-1787913595385.pngyipingwang_0-1787913595385.pngyipingwang_0-1787913595385.pngyipingwang_0-1787913595385.pngyipingwang_0-1787913595385.pngyipingwang_0-1787913595385.pngyipingwang_0-1787913595385.pngyipingwang_0-1787913595385.pngyipingwang_0-1787913595385.pngyipingwang_0-1787913595385.pngyipingwang_0-1787913595385.pngyipingwang_0-1787913595385.pngyipingwang_0-1787913595385.png Re: LX2160AのJTAG(CCS)接続が失敗する 再開まで今しばらくお待ちください。 ご提示いただいた手順に従って、以下の手順を実行しました。 CodeWarriorのインストール全体(サービスパックだけでなく)を完全にアンインストールしました。 以下のキャッシュフォルダを削除しました: C:\Users\ \.p2 C:\Users\ \.p2\org.eclipse.equinox.p2 CodeWarriorを再インストールしました。 ヘルプ→新しいソフトウェアをインストールする→アーカイブを追加→ファイルcom.freescale.armv8.11.5.12.GA.Win.updatesite.221209.zip指定しました。 アーカイブを追加した後、サービスパックが提供するプラグインのインストールと更新操作の両方を「新しいソフトウェアのインストール」を試みました。 その結果、サービスパックに含まれるプラグインのほとんどが正常にダウンロードされ、インストールされました。しかし、添付のスクリーンショットに示されたプラグインはインストールや更新の過程で失敗し、更新できませんでした。 KAZU_ISHI_0-1787912782459.pngKAZU_ISHI_0-1787912782459.pngKAZU_ISHI_0-1787912782459.pngKAZU_ISHI_0-1787912782459.pngKAZU_ISHI_0-1787912782459.pngKAZU_ISHI_0-1787912782459.pngKAZU_ISHI_0-1787912782459.pngKAZU_ISHI_0-1787912782459.pngKAZU_ISHI_0-1787912782459.pngKAZU_ISHI_0-1787912782459.pngKAZU_ISHI_0-1787912782459.pngKAZU_ISHI_0-1787912782459.pngKAZU_ISHI_0-1787912782459.png よろしくお願いいたします。 Re: LX2160AのJTAG(CCS)接続が失敗する ヘルプ ->インストール新ソフトウェア->Add->アーカイブ)からサービスパックcom.freescale.armv8.11.5.12.GA.Win.updatesite.221209.zipをインストールしてください。 「利用可能なソフトウェアサイト」からではない キャッシュフォルダも削除してください。 C:\Users\ \.p2 または C:\Users\ \.p2\org.eclipse.equinox.p2.* Re: LX2160AのJTAG(CCS)接続が失敗する ご返信よろしくお願いします。 ダウンロードしたファイルが破損している可能性があると考え、再度ダウンロードして、以下のようにアップデートを試みました。 利用可能なソフトウェアサイトでは、以下を選びました: アーカイブ→追加→ com.freescale.armv8.11.5.12.GA.Win.updatesite.221209.zip 解凍されたダウンロードパッケージから。 その後、「CodeWarrior Updates」がリストに追加され、このアップデートサイトだけを有効にしました。 調査を簡略化するため、次に「利用可能な更新プログラム」を使用し、リストの上から順に更新プログラムを一つずつインストールしました。以下のアップデートはエラーにより失敗しました。 エラーメッセージは以下のとおりです。 • CodeWarrior Debugger GTA 14.0.0.202212090959 アイテムのインストール中にエラーが発生しました。 セッションの文脈は以下の通りです: (profile=epp.package.cpp、 phase=org.eclipse.equinox.internal.p2.engine.phases.Install、 operand=[R]com.freescale.core.debugger.gta 14.0.0.202006241928 --> [R]com.freescale.core.debugger.gta 14.0.0.202212090959, action=com.freescale.updater.customactions.actions.FreescaleProcessCheck) NLS 欠落メッセージ: param_not_set in: com.freescale.updater.customactions.Messages •NXP GDB 14.0.0.202204131357 アイテムのインストール中にエラーが発生しました。 セッションの文脈は以下の通りです: (profile=epp.package.cpp、 phase=org.eclipse.equinox.internal.p2.engine.phases.Install、 operand=[R]com.freescale.core.debugger.fsl_gdb13.0.0.202003111126 --> [R]com.freescale.core.debugger.fsl_gdb14.0.0.202204131357、 action=com.freescale.updater.customactions.actions.FreescaleProcessCheck) NLS 欠落メッセージ: param_not_set in: com.freescale.updater.customactions.Messages • QorIQ構成および検証スイート - 共通レイアウト 4.24.0.FSL20221019_2247 アイテムのインストール中にエラーが発生しました。 セッションの文脈は以下の通りです: (profile=epp.package.cpp、 phase=org.eclipse.equinox.internal.p2.engine.phases.Install、 operand=null --> [R]com.freescale.cw.qcvs.feature_root4.24.0.FSL20221019_2247、 action=com.freescale.updater.customactions.actions.FreescaleProcessCheck) NLS 欠落メッセージ: param_not_set in: com.freescale.updater.customactions.Messages CodeWarrior Core IDE 14.0.0.202212091004およびCodeWarrior Debugger 14.0.0.202212091004はテストしていません。これらのパッケージには上記のソフトウェアが含まれているようです。 その他のアップデートはすべて問題なく正常にインストールされました。 追加の検証ステップとして、「新しいソフトウェアをインストールする」で利用可能なソフトウェアパッケージをインストールしてみます。個別のアップデートパッケージのテスト結果はすでに上記で示されています。 これらのエラーの原因や、それに関連する既知の問題について何か情報をお持ちでしたら、ぜひご教示いただければ幸いです。 ご協力ありがとうございました。 このメッセージは機械翻訳によって翻訳されました。 Re: LX2160AのJTAG(CCS)接続が失敗する ご指導ありがとうございました。 ご指摘いただいたとおり、アップデート設定を確認しました。 クリーンインストールから始め、添付のスクリーンショットに示されている設定に合わせて構成し、インストールを試みました。 KAZU_ISHI_0-1787974046471.pngKAZU_ISHI_0-1787974046471.pngKAZU_ISHI_0-1787974046471.pngKAZU_ISHI_0-1787974046471.pngKAZU_ISHI_0-1787974046471.pngKAZU_ISHI_0-1787974046471.pngKAZU_ISHI_0-1787974046471.pngKAZU_ISHI_0-1787974046471.pngKAZU_ISHI_0-1787974046471.pngKAZU_ISHI_0-1787974046471.png しかし、添付の動画ファイルに示されているように、設定を全く同じように構成しても、インストールはエラーで失敗します。 また、表示されているアイテム数が、あなたが提供してくれたスクリーンショットと異なっていることにも気づきました。この違いは問題に関連しているのでしょうか?それとも何が原因か分かりますか? 何かアドバイスがあれば、ぜひお聞かせください。 ご協力ありがとうございました。ご連絡をお待ちしております。 このメッセージは機械翻訳によって翻訳されました。 Re: LX2160AのJTAG(CCS)接続が失敗する ご説明いただきありがとうございます。 本日、インストール手順を再度実行し、以下のことを確認しました。 まず、Windows設定>インストールアプリから以下のアプリケーションをアンインストールしました。 - CodeWarrior Development Studio for QorIQ LS シリーズ - ARM V8 ISA v11.5.0 - CodeWarrior for ARMv8 v2020.06 次に、Windowsユーザーディレクトリ内の以下のフォルダを削除しました: - .codewarrior - .eclipse - .p2 その後、再度パッケージをダウンロードし、解凍してクリーンインストールを行いました。 その時点で、利用可能なソフトウェアサイトの設定は、添付のスクリーンショットに示されている通り、あなたが提供したスクリーンショットと一致していました。 KAZU_ISHI_1-1788156348600.pngKAZU_ISHI_1-1788156348600.pngKAZU_ISHI_1-1788156348600.pngKAZU_ISHI_1-1788156348600.pngKAZU_ISHI_1-1788156348600.pngKAZU_ISHI_1-1788156348600.pngKAZU_ISHI_1-1788156348600.pngKAZU_ISHI_1-1788156348600.pngKAZU_ISHI_1-1788156348600.png しかし、アップデートパッケージをインストールしようとしたところ、エラーが発生しました。 また、以前提供した情報について訂正させていただきたいと思います。先ほど送ったスクリーンショットは、アップデートエラーが発生してIDEが再起動された後に撮影したものです。 そのため、スクリーンショットは新規インストール直後の状態を正確に反映していませんでした。誤ったスクリーンショットをお送りしてしまい、ご迷惑をおかけしたことをお詫び申し上げます。 ご協力ありがとうございました。ご連絡をお待ちしております。 このメッセージは機械翻訳によって翻訳されました。 Re: LX2160AのJTAG(CCS)接続が失敗する こんにちは、 以下のシナリオに対応する設定テキストファイルを添付します。 1. 新たに設置された 2. アップデートパッケージを適用した後(更新が完了する前に失敗) 3. シナリオ2の失敗後にCodeWarrior IDEウィンドウ右下に表示される更新アイコンを使って再度アップデートを実行しました よろしくお願いいたします。 Re: LX2160AのJTAG(CCS)接続が失敗する おそらくこの問題は、お使いのWindows 11 OSに関連していると思われます。 CodeWarrior IDEを開き、「ヘルプ→>新しいソフトウェアのインストール→>すでにインストール済み→>設定」をクリックしてください。これにより設定をtxtファイルにコピーして私に送信してください。 Re: LX2160AのJTAG(CCS)接続が失敗する 以下のスクリーンショットを参照してください。最初の項目があなたのものとは異なります。 yipingwang_0-1788146095643.pngyipingwang_0-1788146095643.pngyipingwang_0-1788146095643.pngyipingwang_0-1788146095643.pngyipingwang_0-1788146095643.pngyipingwang_0-1788146095643.png 私が提供したファイル「CW_ARMv8_v2020.06_b200629GA_Win_Offline.exe」を再インストールしましたか? Re: LX2160AのJTAG(CCS)接続が失敗する さらに、サービスパックの仕様、特にサイズが同じかどうかをご確認ください。 yipingwang_0-1788251622006.pngyipingwang_0-1788251622006.pngyipingwang_0-1788251622006.pngyipingwang_0-1788251622006.pngyipingwang_0-1788251622006.png Re: LX2160AのJTAG(CCS)接続が失敗する 言語設定以外に明確な違いは感じませんでした。 C:\Freescale\CW4NET_v2020.06\CW_ARMv8\eclipse\eclipse.ini ファイルを編集して、以下の行を追加してください。 -Dfile.encoding=Cp1252 -Dsun.jnu.encoding=Cp1252 -Dorg.osgi.framework.language=en Open CodeWarrior IDE を C:\Freescale\CW4NET_v2020.06\CW_ARMv8\eclipse\eclipse.exe -nl en 次に、アップグレードが可能かどうか試してみてください。 Re: LX2160AのJTAG(CCS)接続が失敗する CodeWarriorを管理者として実行してください。 Windows 10 22H2を搭載したPCをお持ちですか? もし可能なら、Windows 10 22H2にCodeWarrior for ARMv8 11.5.12をインストールできるか試してみてください。 Re: LX2160AのJTAG(CCS)接続が失敗する こんにちは、 指示された手順に従い、指示通りにeclipse.iniを修正し、以下のコマンドでCodeWarriorを起動しました。 C:\Freescale\CW4NET_v2020.06\CW_ARMv8\eclipse\eclipse.exe -nl en その後、「Help -> 新規ソフトウェアをインストールする」を使ってアップデートを試みました。 しかし、アップデートはやはり失敗した。 エラーログファイルを添付しましたので、ご確認ください。 また、新規インストール直後、アップデートを試みる前に、ログに既にいくつかのエラーが記録されていることに気づきました。これらのエラーはアップデート失敗と関係があるのでしょうか? 添付のログには以下の両方が含まれています: - インストール後の初期起動、 - その後の更新はHelp -> Install New ソフトウェアを通じて実施されます。 よろしくお願いいたします。 Re: LX2160AのJTAG(CCS)接続が失敗する サポートされているOSについては「3」を参照してください。システム要件については、 https://www.nxp.com/docs/en/release-note/CW-ARMV8-RN.pdfを参照してください。
View full article
J3H081スマートカードの初期化方法 こんにちは。J3H081 JCOPカードを購入しました。 私はまた、 、 、 、 、 、 を受け取りました。 そして1つのAPDUライン「 00F0 0000 10 」 GlobalPlatformProを使用してAPDUラインを試したところ、6A82が返されました。 そして、カードの初期化方法が全く分かりません。 説明書が何もないので、Javaカードのプログラミング方法を学びたいと思いました。 Re: How to initialize J3H081 SmartCard JCOPは非常に安全な要素製品であり、すべての技術サポート、ドキュメントアクセス、ソフトウェアやツールのリクエストは 、認可されたNXP代理店を通じて処理しなければなりません。 JCOPカードを購入した代理店にお問い合わせください。   よろしくお願いします、 アロンドラ Re: How to initialize J3H081 SmartCard ええ、だからこそ、neven.czが私にカードを1枚だけ売った理由が私には理解できません。 彼らは「買い手は使い方を知っていなければならない、私たちは知らない」と言いました。 つまり neven.cz NXPと提携しておらず、どこかでカードを購入して販売しているのです。グレーマーケット。 度重なる操作ミスで、カードを壊してしまいました。 そこで neven.cz にメールを送ったところ、返金すると言われました。 その後ACOSJを購入しましたが、そのカードはデフォルトのキーでOP_READY状態になっており、問題なく動作します。 NXPコミュニティから時間を取ってしまい申し訳ありません。
View full article
CodeWarrior 版本错误 我偶尔会遇到版本错误: mingw32-make:*** 没有规则可以创建目标 Dropbox//Projects/\Project_x/\Project_Headers/\../\Sources/\Events.c'`Sources/Events_c.obj` 需要此文件。  停止。 文件 Events_c.obj 当然存在,但通常的解决方法却不起作用。我尝试了全新版本,删除了 Events_c.obj 文件。我删除了整个 Flash 文件夹,也尝试过关机重启,但都没用。最后我新建了一个项目,然后剪切粘贴了源文件的内容。这个问题每隔几周就会发生一次,而且有几次,在电脑“休眠”后,问题就自行消失了。 Re: CodeWarrior Build error 谢谢,同步问题确实有道理,但我需要几天时间才能尝试。 Re: CodeWarrior Build error 这听起来不太像是 .obj 文件的问题。文件本身有问题,更像是生成的 Makefile 中存在过时或格式错误的依赖路径。Dropbox//Projects/\Project_x... 路径中奇怪的斜杠是一个重要的线索。我会检查项目是否直接从 Dropbox 同步的文件夹构建,并尝试将其移动到本地的非同步目录。此外,请将出现问题时生成的依赖项/Makefile 条目与正常版本时生成的条目进行比较。如果Dropbox文件夹同步或电脑唤醒后错误消失,则进一步表明问题出在Dropbox/文件系统的时序问题上,而不是源文件本身。 Re: CodeWarrior Build error 你好, 你使用的是哪个版本的CodeWarrior? 您尝试的清理版本是否是通过命令>清理(全部)实现的? 当你转到新项目时,一切正常,但几周后问题又出现了? 可能是你的 make 文件与你的目录不匹配。 请尝试此方法清理并重新生成 make 文件。 在“项目”视图中 > “清理” > 选择要版本项目   luis_maravilla_1-1787091476012.png 另外,建议不要使用 Dropbox 文件夹,请更改为本地路径,并将其添加到版本目录中或进行更改。 请参阅此帖子了解更多信息:没有规则可以创建目标 | Eclipse 上的 MCU 此致敬礼,路易斯
View full article