Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
LS1028A Felix (swp0): Hardware TX Timestamp Not Produced for Custom-EtherType Frames on the CPU-Inje 1. Environment Platform: NXP LS1028ARDB (VSC9959 / Felix switch) Kernel: Linux 6.18.2-rt3 (NXP Yocto real-time-edge, PREEMPT_RT) Topology (DSA): eno2 (ENETC) = DSA conduit / NPI port swp0 = Felix user port (CPU-injection path: CPU → eno2 → NPI → egress swp0 physical port) eno0 (ENETC) = separate test port (now directly cabled to swp0, used to verify the actual egress frame content) Application: AF_PACKET SOCK_RAW socket bound to swp0, SO_TIMESTAMPING(TX_HARDWARE|RAW_HARDWARE), transmitting frames with custom EtherType 0x88B5, expecting the hardware TX timestamp from the socket error queue (SCM_TIMESTAMPING). ptp4l is running on swp0 (HWTSTAMP_TX_ON, syncing normally, unaffected). 2. Goal Obtain a hardware TX timestamp for custom 0x88B5 (non-PTP) frames transmitted on swp0, without breaking PTP synchronization on swp0. 3. Confirmed working PTP frames DO get timestamps: using the same AF_PACKET raw socket on swp0, transmitting 0x88F7 + a valid PTP header, 30/30 frames returned a hardware TX timestamp via the error queue (ocelot_get_txtstamp matched, timestamp delivered to the socket error queue). The driver timestamp-request path works for the custom frames: 0x88B5 frames reach ocelot_port_txtstamp_request (dmesg shows felix-tx-ts: port 0 non-PTP=1 ts_id=0..3), i.e. ocelot_port->ptp_cmd is non-zero (set by ptp4l) and a timestamp ID is allocated. 4. Problem For 0x88B5 frames, a timestamp ID is allocated, but the hardware produces no timestamp: SYS_PTP_STATUS PTP_MESS_VLD = 0 immediately after sending a burst of 0x88B5 frames (no FIFO entries, no overflow). The socket error queue stays empty. 5. What we checked and ruled out (evidence) Check Result ocelot_port->ptp_cmd (two-step enable) ✅ non-zero (set by ptp4l) IFH BYPASS (bit 127) ✅ =1 (driver ocelot_ifh_set_bypass) IFH REW_OP1 (bits 125–117) ✅ confirmed by code: two-step(3) + ts_id written for 0x88B5 frames REW_PTP_CFG.PTP_2STEP_DIS ✅ =0 (two-step not disabled) PTP_CFG_MISC.PTP_ENA ✅ =1 SYS_PORT_MODE.DATA_WO_TS (ports 0/4/6) ✅ =0 (inline timestamp write not disabled) REW_PORT_CFG.FCS_UPDATE_CPU_ENA ✅ =1 (CPU frames always get FCS recomputed, no bad-CRC drops) IS2 rules adding two-step authorization for 0x88B5 (ingress swp0, then swp0|NPI) ❌ no effect (CPU-injected frames have BYPASS=1, analyzer/IS2 is skipped) Inline timestamp insertion SYS_TIMESTAMP_OFFSET (ETH_TYPE_CFG=0x88B5, TIMESTAMP_OFFSET=14; register write/readback verified) ❌ no effect (with swp0↔eno0 direct cable, no timestamp at absolute byte 28 of the egress frame) 6. Questions for Official Confirmation Does the VSC9959/Felix two-step TX timestamping (IFH REW_OP1, REW_OP[2:0]=3) actually work for CPU-injected frames with a non-PTP EtherType? The reference manual (16.4.13.12.3.1) states "can be applied to any frame, also non-PTP frames", but we measure SYS_PTP_STATUS VLD=0 (zero FIFO entries). Is the actual silicon behavior that, even with BYPASS=1 and REW_OP1 in the IFH, the rewriter still requires the frame to be classified as PTP (by EtherType / PTP header) before it produces a timestamp FIFO entry? Does SYS_TIMESTAMP_OFFSET (inline timestamp insertion) have any hidden enable/trigger condition beyond the ETH_TYPE_CFG match? We verified: the register is written correctly (ETH_TYPE_CFG=0x88B5, offset=14), FCS update is enabled, DATA_WO_TS=0, and with a direct swp0↔eno0 cable we confirmed the egress frame content — but no timestamp was written into the frame. Is this feature also restricted on the CPU-injection (BYPASS) path? On the CPU-injection (BYPASS=1) path, is there an officially supported way to get a hardware TX timestamp for arbitrary-EtherType custom frames transmitted on swp0? (e.g., some enable bit, a PTP classification table configuration, or a required frame format.) If neither of the two manual-documented mechanisms supports non-PTP frames on this silicon, is there a known erratum or a recommended alternative? Re: LS1028A Felix (swp0): Hardware TX Timestamp Not Produced for Custom-EtherType Frames on the CPU- Two-step TX timestamping for non-PTP CPU-injected frames The RM documents REW_OP[2:0] = 3 in the CPU Injection Header as “Two-step PTP,” with REW_OP[8:3] carrying the timestamp identifier; IDs 0–3 are explicitly pre-allocated for CPU-injected frames. It also states that two-step timestamping can be applied to “any frame, also non-PTP frames,” because the frame itself is not modified, and the TX timestamp is stored in SYS::PTP_STATUS / SYS::PTP_TXSTAMP .  So, from the RM, BYPASS=1 + IFH REW_OP[2:0]=3 should be a valid mechanism for CPU-injected two-step timestamping, including non-PTP frames . I did not find RM evidence that the rewriter must first classify the frame as PTP by EtherType/header when the IFH supplies the two-step command. The contradictory part is your measurement: SYS_PTP_STATUS.PTP_MESS_VLD=0 after confirmed IFH REW_OP1 , which is not explained by the RM text I retrieved. SYS_TIMESTAMP_OFFSET / inline timestamp insertion ES_SYS_SYSTEM_TIMESTAMP_OFFSET is documented as matching ETH_TYPE_CFG and placing a 64-bit nanosecond TX timestamp at TIMESTAMP_OFFSET ; the manual even gives a “generic timestamp insert (Chronos)” example where offset 14 places the timestamp at absolute byte 28 in the Ethernet frame.  I did not retrieve documentation that states an additional hidden enable bit beyond the general PTP enable / timestamp-offset configuration, nor documentation that explicitly says this feature is supported or blocked on CPU-injected BYPASS=1 frames. The RM wording supports the generic mechanism, but your direct-cable observation that no bytes are written at the expected offset indicates that, in this CPU-injection path, ETH_TYPE_CFG match alone is not sufficient in your setup. Officially supported way under Linux DSA to timestamp arbitrary EtherType frames on swp0 The strongest software-side evidence says: generic packet timestamping is not supported by the DSA framework used by the LS1028A switch driver, even though the switch hardware is capable of it .  Therefore, under the stock/standard DSA Felix driver model, I would treat PTP/IEEE-1588 event message timestamping as the supported path , and arbitrary EtherType 0x88B5 TX timestamping via SO_TIMESTAMPING on swp0 as not officially supported by that software stack . That aligns with your observation that valid 0x88F7 PTP frames timestamp reliably while 0x88B5 does not. Erratum / recommended alternative I did not retrieve a timestamp-specific LS1028A/Felix erratum for this behavior. The evidence I found says the published Felix erratum mentioned in the retrieved ticket material is ERR A-050484 , related to NPI flow control / frame-loss management rather than timestamp FIFO generation. 
View full article
RT1180 EVKのETH1/ETH2/ETH3をlwIP用に1Gbpsで初期化する方法は? 私はMIMXRT1180-EVKを使用しています。利用可能なSDKの例、例えばlwIP pingやiPerfでは、イーサネット初期化は ETH4のみで示されています。 私たちの製品は、RT1180と外部デバイス間のデータ交換のために ETH1/ETH2/ETH3 を1Gbpsで使用する必要があります。 ETH1/ETH2/ETH3のイーサネット初期化と設定は自分たちで開発することが期待されているのか、それとも既存のリファレンス実装があるのか? よろしくお願いします! Re: How to Initialize RT1180 EVK ETH1/ETH2/ETH3 at 1 Gbps for lwIP? @JuiHung様、 現時点では、この特定の要件をカバーした参考例やユーザーガイドは存在しません。 もう少しお待ちいただけますか?社内の専門家が現在、関連するサンプルプロジェクトを準備中ですが、公開できるまでにはもう少し時間がかかります。 ご理解とご辛抱に感謝いたします。進捗状況については随時ご報告いたします。 よろしくお願いいたします。 シェリー
View full article
添加 HSE 元器件失败 我使用的是S32 Design Studio IDE 3.6.8版本,RTD 版本 7.0.1,采用 S32K314 项目。我无法在外围配置视图中添加 HSE IP 核,这导致配置工具无法在生成的文件中自动生成 hse_mu 驱动程序。我该如何解决这个问题? 1131_0-1788401575417.png 我还需要添加哪些元器件? 1131_1-1788401624401.png Re: Failed to add the HSE component HI 您还需要安装一个单独的补丁包,其描述包含“加密驱动程序”,例如S32K3 实时驱动程序 ASR R23-11 版本 7.0.1 P02 。 SW32K3_RTD_R23-11_7.0.1_P02_D2603_ReleaseNotes.pdf ,特别是第2.5 节“支持和提供的驱动程序插件” ,提到了Hse_IP 。 此致敬礼, Robin
View full article
LS1028A Felix (swp0):CPU-Inje 上的 Custom-EtherType 帧未生成硬件发送时间戳 1. 环境 平台:NXP LS1028ARDB(VSC9959 / Felix 交换机) 内核:Linux 6.18.2-rt3 (NXP Yocto real-time-edge, PREEMPT_RT) 拓扑结构(DSA): eno2 (ENETC) = DSA 导管 / NPI 端口 swp0 = Felix 用户端口(CPU 注入路径:CPU → eno2 → NPI → 出口 swp0 物理端口) eno0 (ENETC) = 单独的测试端口(现在直接连接到 swp0,用于验证实际的出口帧内容) 应用程序:AF_PACKET SOCK_RAW套接字绑定到swp0 , SO_TIMESTAMPING(TX_HARDWARE|RAW_HARDWARE) ,使用自定义 EtherType 0x88B5发送帧,期望从套接字错误队列 (SCM_TIMESTAMPING) 获取硬件 TX 时间戳。 ptp4l 在 swp0 上运行( HWTSTAMP_TX_ON ,同步正常,不受影响)。 2. 目标 获取在 swp0 上传输的自定义 0x88B5(非 PTP) 帧 的硬件 TX 时间戳 ,而不破坏 swp0 上的 PTP 同步。 3. 已确认正常工作 PTP 帧确实会获取时间戳:在 swp0 上使用相同的 AF_PACKET 原始套接字,发送 0x88F7 + 有效的 PTP 标头,30/30 个帧通过错误队列返回硬件 TX 时间戳( ocelot_get_txtstamp匹配,时间戳已传递到套接字错误队列)。 驱动程序时间戳请求路径适用于自定义帧:0x88B5 帧到达ocelot_port_txtstamp_request (dmesg 显示felix-tx-ts:端口 0 非 PTP=1 ts_id=0..3 ),即ocelot_port->ptp_cmd非零(由 ptp4l 设置),并且分配了时间戳 ID。 4. 问题 对于 0x88B5 帧,会分配一个时间戳 ID,但硬件不会生成时间戳: 发送 0x88B5 帧突发后, SYS_PTP_STATUS PTP_MESS_VLD = 0 (无 FIFO 条目,无溢出)。 套接字错误队列保持为空。 5. 我们检查并排除的内容(证据) 检查结果 ocelot_port->ptp_cmd (两步启用) ✅ 非零值(由 ptp4l 设置) IFH旁路(位127) ✅ =1(驱动程序 ocelot_ifh_set_bypass ) IFH REW_OP1 (位 125–117) ✅ 代码已确认:two-step(3) + ts_id 已写入 0x88B5 帧 REW_PTP_CFG.PTP_2STEP_DIS ✅ =0(两步走未禁用) PTP_CFG_MISC.PTP_ENA ✅ =1 SYS_PORT_MODE.DATA_WO_TS (端口 0/4/6) ✅ =0(未禁用内联时间戳写入) REW_PORT_CFG.FCS_UPDATE_CPU_ENA ✅ =1(CPU帧总是重新计算FCS,不会出现CRC校验错误丢帧) IS2 规则为 0x88B5 添加两步授权(入口 swp0,然后 swp0|NPI) ❌ 无影响(CPU注入的帧具有BYPASS=1,分析器/IS2被跳过) 内联时间戳插入SYS_TIMESTAMP_OFFSET (ETH_TYPE_CFG=0x88B5, TIMESTAMP_OFFSET=14; 寄存器写入/读取已验证) ❌ 无影响(使用 swp0↔eno0 直连电缆,出口帧第 28 个字节无时间戳) 6. 需要官方确认的问题 VSC9959/Felix 的两步发送时间戳(IFH REW_OP1,REW_OP[2:0]=3)是否真的适用于 CPU 注入的非 PTP 以太网类型帧?参考手册 (16.4.13.12.3.1) 指出“可应用于任何帧,包括非 PTP 帧”,但我们测量到SYS_PTP_STATUS VLD=0(FIFO 条目为零)。实际的芯片行为是否是,即使 BYPASS=1 且 IFH 中设置了 REW_OP1,重写器仍然需要先将帧分类为 PTP(通过以太网类型/PTP 头部),然后才会生成时间戳 FIFO 条目? SYS_TIMESTAMP_OFFSET (内联时间戳插入)除了 ETH_TYPE_CFG 匹配之外,是否还有其他隐藏的启用/触发条件?我们已验证:寄存器写入正确(ETH_TYPE_CFG=0x88B5,偏移量=14),FCS 更新已启用,DATA_WO_TS=0,并且使用直接连接 swp0↔eno0 的线缆确认了输出帧的内容——但帧中并未写入时间戳。此功能是否也仅限于 CPU 注入(旁路)路径? 在 CPU 注入(BYPASS=1)路径下,是否存在官方支持的方法,可以为通过 swp0 发送的任意以太网类型自定义帧获取硬件发送时间戳? (例如,通过启用位、PTP 分类表配置或所需的帧格式。) 如果这两种手册中记录的机制都不支持此硅芯片上的非 PTP 帧,是否有已知的勘误或推荐的替代方案? Re: LS1028A Felix (swp0): Hardware TX Timestamp Not Produced for Custom-EtherType Frames on the CPU- 对非PTP CPU注入帧采用两步发送时间戳 RM 文档在 CPU 注入头中将 REW_OP[2:0] = 3 表示为“两步 PTP”,其中 REW_OP[8:3] 携带时间戳标识符;ID 0-3 已明确预先分配给 CPU 注入的帧。它还指出,两步时间戳可以应用于“任何帧,包括非PTP帧”,因为帧本身不会被修改,发送时间戳存储在SYS::PTP_STATUS/SYS::PTP_TXSTAMP中。 因此,从 RM 来看,BYPASS=1 + IFH REW_OP[2:0]=3 应该是 CPU 注入的两步时间戳的有效机制,包括非 PTP 帧。我没有找到 RM 证据表明,当 IFH 提供两步命令时,重写器必须首先根据 EtherType/报头将帧分类为 PTP。矛盾之处在于您的测量结果:在确认 IFH REW_OP1 之后,SYS_PTP_STATUS.PTP_MESS_VLD=0,而我检索到的 RM 文本并未对此进行解释。 SYS_TIMESTAMP_OFFSET / 内联时间戳插入 ES_SYS_SYSTEM_TIMESTAMP_OFFSET 的文档说明是与 ETH_TYPE_CFG 匹配,并在 TIMESTAMP_OFFSET 处放置一个 64 位纳秒级的发送时间戳;手册甚至给出了一个“通用时间戳插入(Chronos)”示例,其中偏移量 14 将时间戳放置在以太网帧的绝对第 28 个字节处。 我没有找到任何文档说明除了通用的 PTP 启用/时间戳偏移配置之外,还有额外的隐藏启用位,也没有找到任何文档明确说明 CPU 注入的 BYPASS=1 帧是否支持或阻止此功能。RM 的措辞支持通用机制,但您通过直接电缆观察到,在预期的偏移量处没有写入任何字节,这表明,在此 CPU 注入路径中,仅 ETH_TYPE_CFG 匹配在您的设置中是不够的。 Linux DSA 官方支持的方法,用于在 swp0 上为任意 EtherType 帧添加时间戳 最有力的软件方面证据表明:尽管LS1028A交换机硬件具备通用数据包时间戳功能,但LS1028A交换机驱动程序使用的DSA框架并不支持该功能。 因此,在标准的 DSA Felix 驱动程序模型下,我会将 PTP/IEEE-1588 事件消息时间戳视为支持的路径,而通过 swp0 上的 SO_TIMESTAMPING 进行任意 EtherType 0x88B5 TX 时间戳则不被该软件栈正式支持。这与您的观察结果一致,即有效的 0x88F7 PTP 帧的时间戳可靠,而 0x88B5 帧的时间戳则不可靠。 勘误/推荐替代方案 我没有找到针对此行为的特定时间戳的 LS1028A/Felix 勘误表。我找到的证据表明,已发布的Felix勘误表(在检索到的工单材料中提到)是ERR A-050484,它与NPI流程控制/丢帧管理有关,而不是与时间戳FIFO生成有关。
View full article
关于支持 WoA 的 Cortex-A53 SoC 的咨询 尊敬的恩智浦技术支持人员: 我想请教您关于 NXP S32G2/S32G3 平台上的 Cortex-A53 内核的问题。 据我了解,NXP 官方为 Cortex-A53 内核提供了 Linux BSP。但是,我们想研究一下是否有可能在 Arm 上运行 Linux 以外的操作系统,特别是 Windows。 根据我的初步研究,Windows on Arm 支持 AArch64 (ARM64) 架构,而 Cortex-A53 基于 ARMv8-A 64 位架构。因此,从 CPU 架构的角度来看,它们似乎是兼容的。但是,我明白仅凭 CPU 架构兼容性可能不足以在特定硬件平台上运行 Windows。 请您就以下几点提供建议? 除了 Linux BSP 之外,是否有可能在 S32G2/S32G3 的 Cortex-A53 内核上运行 Windows on Arm? 如果可行,有哪些方法可以实现? 例如,是否有现成的 电路板支持包。 或移植解决方案可用,或者是否需要移植和开发诸如引导加载程序/UEFI、ACPI 配置和 设备驱动程序等 元器件? 如果 Windows on Arm 可以在 S32G2/S32G3 平台上运行,那么硬件和驱动程序的兼容性可以达到什么水平? 我们尤其想了解现有的外围设备和驱动程序在 Windows 下是否受支持。 如果 Windows on Arm 运行在 Cortex-A53 内核上,是否仍然可以使用 Cortex-A53 的锁定步进功能? 如果是这样,锁步是如何配置的?与 Linux 电路板支持包。环境相比,有哪些不同或限制? 我们项目的目标不仅是在 S32G 平台上运行 Arm 架构的 Windows,还要验证 Cortex-A53 的锁步功能是否可以在 Windows 环境下使用。 我们非常希望您能就此主题提出建议和意见。 Re: Inquiry about Cortex-A53 SoC supporting WoA 你好, @Toan 感谢你的帖子。 1.除了 Linux 电路板支持包。 之外,一些客户可能在 S32G 上使用其他操作系统,例如 QNX、Vxworks、各种 RTOS 等。 2. 没有任何关于将 Windows(ARM 版本)移植到 S32G 平台的参考资料/示例/文档。 3. 据我了解,理论上,由于与 Arm64 兼容,ARM 版 Windows 可以在 S32G 的 A53 内核上使用。然而,ACPI、GPU、UEFI 等可能是 Windows(ARM 版本)所必需的,它们与 S32G 的现有软件实现完全不同,要实现运行 Windows for ARM 所需的所有项目并不容易。 BR 陈银 
View full article
MCUXpresso Secure Provisioning Tool无法通过USB连接目标板 Hi NXP, 请教一下问题: 开发板:MIMXRT1170-EVKB,使用MCUXpresso Secure Provisioning Tool无法连接,如图显示: hayden178_0-1788428456159.pnghayden178_0-1788428456159.pnghayden178_0-1788428456159.pnghayden178_0-1788428456159.png 电脑设备管理器显示如下: hayden178_1-1788428566738.pnghayden178_1-1788428566738.pnghayden178_1-1788428566738.pnghayden178_1-1788428566738.png 开发板拨码开关如图: hayden178_2-1788428637373.pnghayden178_2-1788428637373.pnghayden178_2-1788428637373.pnghayden178_2-1788428637373.png 另外使用IDE下载程序,debug都没问题。请问如何排查?谢谢 Re: MCUXpresso Secure Provisioning Tool无法通过USB连接目标板 Hi @hayden178 , 感谢提问! 我检查了您提供的拨码开关配置和供电选项,都没有问题。选择的也是USB OTG1没有问题。 因此怀疑可能是有什么异常导致flashloader没有及时通过usb端口加载到SRAM。建议您先换用UART接口试一下。如果UART接口没问题,再换到USB接口,此时flashloader已经在运行了,usb端口应当也没有问题了。 如果UART端口也有问题,那就需要检查具体的输出,在工作目录下的,gen_scripts/init_flashloader_win.bat 中详细列举了具体的命令。重新执行test之前先删除之前的log,在新的log中核对具体是哪一步失败。 Best regards, Gavin Re: MCUXpresso Secure Provisioning Tool无法通过USB连接目标板 Hi @Gavin_Jia , 感谢您的支持! 我换成UART连接MIMXRT1170-EVKB,已经解决问题。 我遇到一个新的问题,请帮忙看看问题出在哪里: 使用MCUXpresso Secure Provisioning Tool上的自带的示例,跑不通mcuboot_opensource&ota_mcuboot,现象为一致复位,如图: hayden178_0-1789004746339.pnghayden178_0-1789004746339.png 工程配置如下: hayden178_1-1789004822575.pnghayden178_1-1789004822575.png hayden178_2-1789004848902.pnghayden178_2-1789004848902.png hayden178_4-1789005368832.pnghayden178_4-1789005368832.png hayden178_3-1789005332451.pnghayden178_3-1789005332451.png 另外我用IDE已经跑通这两个工程,但是把生成的bin文件使用SPSP下载到板子上同样一致复位 hayden178_5-1789005846515.pnghayden178_5-1789005846515.png Re: MCUXpresso Secure Provisioning Tool无法通过USB连接目标板 Hi @hayden178 , 感谢分享你那边的好消息,很高兴第一个SPT连接的问题已经解决了。 关于mcuboot这个操作流程,你参考的guide是哪个能同步下吗?之前一直是通过python脚本和imgtool来做签名的,没尝试过这个SPT的方案。 关于这个新的问题,欢迎重新创建一个ticket以保持每个thread下的主题一致。 感谢您的理解和协作! Best regards, Gavin
View full article
The MCUXpresso Secure Provisioning Tool cannot connect to the target board via USB. Hi NXP, I have a question: Development board: MIMXRT1170-EVKB, unable to connect using MCUXpresso Secure Provisioning Tool, as shown in the image: hayden178_0-1788428456159.pnghayden178_0-1788428456159.pnghayden178_0-1788428456159.pnghayden178_0-1788428456159.png The computer's Device Manager displays the following: hayden178_1-1788428566738.pnghayden178_1-1788428566738.pnghayden178_1-1788428566738.pnghayden178_1-1788428566738.png The development board's DIP switches are shown in the figure: hayden178_2-1788428637373.pnghayden178_2-1788428637373.pnghayden178_2-1788428637373.pnghayden178_2-1788428637373.png I've downloaded and debugged the program using an IDE without any issues. How can I troubleshoot this? Thank you. Re: MCUXpresso Secure Provisioning Tool无法通过USB连接目标板 Hi @hayden178 , Thank you for your question! I checked the DIP switch configuration and power options you provided, and there are no issues. USB OTG1 was also selected without any problems. Therefore, it's suspected that some anomaly might be preventing the flashloader from loading data into SRAM promptly via the USB port. We suggest you try using a UART interface first. If the UART interface works fine, then switch to the USB interface. At this point, the flashloader should be running, and the USB port should also be working correctly. If the UART port also has a problem, you need to check the specific output. The detailed commands are listed in gen_scripts/init_flashloader_win.bat in the working directory. Before re-running the test, delete the previous log and check the new log to see which step failed. Best regards, Gavin Re: MCUXpresso Secure Provisioning Tool无法通过USB连接目标板 Hi @Gavin_Jia , Thank you for your support! I switched to UART to connect the MIMXRT1170-EVKB, and the problem was solved. I've encountered a new problem; could you please help me figure out where the problem lies? The built-in example in the MCUXpresso Secure Provisioning Tool fails to run mcuboot_opensource&ota_mcuboot, resulting in a consistent reset, as shown in the image. hayden178_0-1789004746339.pnghayden178_0-1789004746339.png The project configuration is as follows: hayden178_1-1789004822575.pnghayden178_1-1789004822575.png hayden178_2-1789004848902.pnghayden178_2-1789004848902.png hayden178_4-1789005368832.pnghayden178_4-1789005368832.png hayden178_3-1789005332451.pnghayden178_3-1789005332451.png I've successfully run both projects using the IDE, but downloading the generated bin files to the board using SPSP results in the same reset issue. hayden178_5-1789005846515.pnghayden178_5-1789005846515.png Re: MCUXpresso Secure Provisioning Tool无法通过USB连接目标板 Hi @hayden178 , Thanks for sharing the good news. I'm glad the first SPT connection issue has been resolved. Regarding the mcuboot operation process, which guide did you refer to? Could you please share it? I've always used Python scripts and imgtool for signing before, and I haven't tried this SPT solution. Regarding this new question, you are welcome to create a new ticket to keep the topic consistent across all threads. Thank you for your understanding and cooperation! Best regards, Gavin
View full article
S32K312ファームウェアの互換性 こんにちは、NXPサポートの皆さん、 私たちはS32K312HVS MCUを使ったTPMSコントローラーを開発しています。 現在は中国から調達しています(改良版:0P09C)、マレーシアでの生産(同じMCUモデル)に移行中です。 フェーズ1の検証については、以下の点をご確認ください。 1. シリコンおよびファームウェアの互換性 - (当社が独自に開発した)同一のファームウェアバイナリは、再コンパイルせずにマレーシア製のS32K312HVS上で完全に動作しますか? 中国製とマレーシア製のMCU(同じ部品番号)の間には、シリコンレベルで何らかの差異はありますか? 2. 仕様の一貫性 マレーシア製MCUと完全に一致するか? - モジュールのリセット (RGM: FREC/FRET/DREC/DRET カウンター) – 同じ動作ですか? - FlexCANペリフェラル(500 kbps、ISO-TP)– バリエーションはない? クロック精度とPLLロック時間 – 同じ仕様ですか? 3. 訂正と回避策 - 現在のファームウェアには回避策(RGMエスカレーション、CANタイムアウト処理)が含まれています。 これらの回避策はマレーシア製MCUでもまだ有効ですか?それとも調整が必要ですか? マレーシア生産に関する新たな訂正事項はありますか? 4. 工程変動 電気的パラメータ(タイミング、電力、温度係数など)に変化はありますか? マレーシア製のフラッシュメモリ/不揮発性メモリにおけるECCの信頼性の違い? 確認してください:同じファームウェアバイナリを使って同じ製品を期待できますか? マレーシアのMCUでの挙動はどうでしょうか、それとも調整が必要ですか? スケジュール:フェーズ1の検証は9月末に開始されます。迅速なご回答をいただければ幸いです。 Re: S32K312 Firmware-Compatibility こんにちは、 S32K3xx発注部品番号システムは、「N」接頭辞を「非中国製造の適格注文品番号」を示します。これはあくまで調達・ご注文指定です。重要な点として、これは新しいマスクセットやシリコンの改訂を示すものではなく、同じダイ/マスク(0P09C)が使用されていることを示しています。マレーシアの組み立て・試験拠点はATKL(ペタリンジャヤ、マレーシア)で、NXPがS32Kファミリーの認定組立・試験施設としています。 注意すべき点はマスクの改訂です petervlna_0-1788419667576.png petervlna_1-1788419699369.png 「N」という接頭辞は、基本的にサプライチェーンの回復力と地政学的リスクを軽減するためのツールです。お客様には以下のようなものがあります: 中国以外での組み立てとテストを保証します。このデバイスは、中国以外の場所(例:マレーシアのATKLペタリンジャヤ)でのみ組み立てとテストが行われます。中国産製造を避けるための契約、規制、または政策上の要件があるお客様は、それらの要件を満たすために「N」バリアントを調達することができます。 輸出管理・貿易コンプライアンス — 特に防衛関連の政府や規制対象の自動車サプライチェーンの一部の顧客は、部品の原産国を文書化し管理することが求められています。「N」バリアントは、明確な監査証跡を提供します。 供給の多様化 — 「S」と「N」両方の認定バリアントを持つことで、両バリアントは同じシリコンダイ、マスクセット、電気仕様を共有するため、再認定なしで供給交換の柔軟性が確保されます。 よろしくお願いいたします。 ピーター
View full article
SR040およびSR150にはアクセスNDAが必要です 上記のICについて話し合うミーティングを開きたいと思っていますが、簡単に行う方法やNDAにSR040やSR150に関する知識を得られるよう求める方法が見つからず、正しい方向へのアドバイスをいただけるとありがたいです。ありがとう! Re: Access NDA required for SR040 and SR150 こんにちは、 あなたの調子が良いといいのですが。ご不便をおかけして申し訳ありませんが、この製品の情報はNDA(秘密保持契約)に基づいており、公開されていません。 チップについての詳細は、代理店ネットワークで利用可能な当社の代理店のいずれかにお問い合わせください。NXPですか?または、このデバイスを手に入れるのを手伝った直接の連絡先がいれば、ぜひ連絡してください。 もし当社のUWB製品に関する情報をお探しの方やこのテクノロジに興味がある方は、パートナー(Trimension UWB Partners)のこれらの開発キットとモジュールをご確認いただくことをお勧めします。 これらのキットやモジュールに興味がある場合は、直接彼らに相談してプロセスやサポートを受けられるかを知る必要があります。なぜなら、このテクノロジのサポートは彼らを通じて行われるからです。 ドキュメントとソフトウェアは対応するUWBモジュールパートナーによって配布されます。モジュールを選択すると、パートナーのページに案内され、データシート、アプリケーションノート、必要なイネーブルメントにアクセスできます よろしくお願いいたします。 リカルド
View full article
Inquiry about Cortex-A53 SoC supporting WoA Dear NXP technical supporter, I would like to ask for your advice regarding the Cortex-A53 cores on the NXP S32G2/S32G3 platform. I understand that NXP officially provides a Linux BSP for the Cortex-A53 cores. However, we would like to investigate whether it is possible to run an operating system other than Linux, particularly Windows on Arm. Based on my initial research, Windows on Arm supports the AArch64 (ARM64) architecture, while the Cortex-A53 is based on the ARMv8-A 64-bit architecture. Therefore, from the CPU architecture perspective, they appear to be compatible. However, I understand that CPU architecture compatibility alone may not be sufficient to run Windows on a specific hardware platform. Could you please advise us on the following points? Apart from the Linux BSP, is it possible to run Windows on Arm on the Cortex-A53 cores of the S32G2/S32G3? If it is possible, what approaches are available? For example, is there an existing BSP or porting solution available, or would it be necessary to port and develop components such as the bootloader/UEFI, ACPI configuration, and device drivers? If Windows on Arm can run on the S32G2/S32G3 platform, what level of hardware and driver compatibility can be expected? In particular, we would like to understand whether the existing peripherals and drivers can be supported under Windows. If Windows on Arm is running on the Cortex-A53 cores, is it still possible to use the Cortex-A53 lockstep functionality? If so, how is lockstep configured, and are there any differences or limitations compared with the Linux BSP environment? The goal of our project is not only to run Windows on Arm on the S32G platform, but also to verify whether the Cortex-A53 lockstep functionality can be used in the Windows environment. We would greatly appreciate your advice and recommendations on this topic. Re: Inquiry about Cortex-A53 SoC supporting WoA Hello, @Toan  Thanks for your post. 1. Besides Linux BSP, some customer may use other OS on S32G, like QNX, Vxworks, various RTOS, etc. 2. There are no any reference/samples/documents related to porting Windows(ARM version) to S32G platform. 3. From my understanding, theoretically, windows for ARM may be used on A53 cores of S32G since compatible with Arm64. However, ACPI, GPU, UEFI, etc., they may be required for Windows(ARM version), they are totally different from the existing software implementation of S32G, it is not easy to implement all items that are required for running Windows for ARM. BR Chenyin 
View full article
LS1021AXE7KQBのピンディレイを教えていただけますか? こんにちは、 現在、私は自分の基板用のプリント基板を設計しています。DDR4インターフェースの重要なタイミング要件のために、PCB上のLS1021AXE7KQBパッケージのピン遅延差を補正する必要があります。ですので、LS1021AXE7KQBのピンディレイ情報を教えていただけますか? よろしくお願いいたします! よろしくお願いいたします! ジェイソン QorIQ LS1デバイス Re: Could you please provide me the pin delay of LS1021AXE7KQB? DDR4インターフェースの内部ダイからパッドへの配線はすべてパッケージ内で長さがマッチングされているため、レイアウトトレース長のタスクはプロセッサとSDRAMのピン間で行われます。設計アプローチには必要ないため、具体的なパッケージ遅延値は提供されませんでした。 Re: Could you please provide me the pin delay of LS1021AXE7KQB? こんにちは、イーピン LS1021AのDDR4インターフェースの場合、PCBのパッケージ内のピン遅延差を補正する必要がありますか? よろしくお願いいたします! よろしくお願いいたします! ジェイソン Re: Could you please provide me the pin delay of LS1021AXE7KQB? 要求された文書はNXP機密所有のものであり、秘密保持契約(NDA)の下でのみ提供可能です。   NXPと秘密保持契約(NDA)を締結しましたか?はいの場合、NDAのコピーまたはNDA番号をご提供いただけますでしょうか?   新しいNDAを歌うこともできます https://www.nxp.com/webapp-signup/ndaReqForm Re: Could you please provide me the pin delay of LS1021AXE7KQB? AEチームに必要な情報を依頼しました。 Re: Could you please provide me the pin delay of LS1021AXE7KQB? こんにちは、 どんなご意見でも歓迎いたします! よろしくお願いいたします! よろしくお願いいたします! ジェイソン Re: Could you please provide me the pin delay of LS1021AXE7KQB? こんにちは、イーピン: 入手できました、本当にありがとうございます! ところで、もう一つ質問があります。LS1021AのeTSEC1およびeTSEC3は、ドライバーPHYに対してRGMIIモードとして設定されます。しかし、私の基板のサイズが非常に大きいため、PCBのトレースが長すぎるとRGMIIインターフェース(1回あたり250Mbps)のドライブ能力が不足するのではと心配しています。RGMIIインターフェースのルート制約、特に一般的なFR-4 PCB(Dk 4.2~4.4)に基づくPCB上のトレース長について教えていただけますか。Df 0.022)?なぜなら、NXPのウェブサイトでPCB設計に関する考慮事項が見つからないからです。また、チェックリストAN4878_Design回路図の設計要件のみを表示します。 よろしくお願いいたします! よろしくお願いいたします! ジェイソン Re: Could you please provide me the pin delay of LS1021AXE7KQB? 新しい質問のために新しいスレッドを作ってもらえますか? ありがとうございます。 Re: Could you please provide me the pin delay of LS1021AXE7KQB? 了解! ご返信よろしくお願いします。 よろしくお願いいたします! ジェイソン
View full article
如何将 RT1180 EVK ETH1/ETH2/ETH3 初始化为 1 Gbps 以用于 lwIP? 我使用的是 MIMXRT1180-EVK。在可用的 SDK 示例中,如 lwIP ping 和 iPerf,以太网初始化仅针对ETH4进行了演示。 我们的产品需要使用ETH1/ETH2/ETH3以 1 Gbps 的速度在 RT1180 和外部设备之间进行数据交换。 我们需要自己开发 ETH1/ETH2/ETH3 的以太网初始化和配置,还是有现成的参考实现可用? 谢谢您! Re: How to Initialize RT1180 EVK ETH1/ETH2/ETH3 at 1 Gbps for lwIP? 亲爱的@JuiHung , 目前,我们没有涵盖此特定要求的参考示例或用户指南。 您介意再等一会儿吗?我们的内部专家目前正在准备一个相关的示例项目,但还需要一些时间才能准备好分享。 感谢您的耐心和理解。我们会及时向您汇报进展情况。 顺祝商祺! 雪莉
View full article
How to Initialize RT1180 EVK ETH1/ETH2/ETH3 at 1 Gbps for lwIP? I am using the MIMXRT1180-EVK. In the available SDK examples, such as lwIP ping and iPerf, Ethernet initialization is only demonstrated for ETH4. Our product needs to use ETH1/ETH2/ETH3 at 1 Gbps for data exchange between the RT1180 and an external device. Are we expected to develop the Ethernet initialization and configuration for ETH1/ETH2/ETH3 ourselves, or is there an existing reference implementation available? Thanks! Re: How to Initialize RT1180 EVK ETH1/ETH2/ETH3 at 1 Gbps for lwIP? Dear @JuiHung , At present, we do not have a reference example or user guide that covers this specific requirement. Would you mind waiting a little longer? Our internal experts are currently preparing a related example project, but it will take some additional time before it is ready to be shared. Thank you for your patience and understanding. We will keep you updated on the progress. Best Regards, Shelly
View full article
S32K312 固件兼容性 您好,NXP技术支持, 我们正在使用 S32K312HVS MCU 开发胎压监测系统控制器。 目前我们从中国采购(版本:0P09C),我们正在过渡到马来西亚生产(相同的MCU型号)。 第一阶段验证阶段,请确认以下内容: 1. 芯片和固件兼容性 - 我们自己开发的相同固件二进制文件,无需重新编译,能否在马来西亚产的 S32K312HVS 上完全运行? - 中国和马来西亚的MCU(相同型号)在芯片层面上是否存在任何差异? 2. 规范一致性 – 与马来西亚MCU完全匹配? - RESET 模块(RGM:FREC/FRET/DREC/DRET 计数器)——行为是否相同? - FlexCAN 外设(500 kbps,ISO-TP)——没有其他变体吗? 时钟精度和锁相环锁定时间——规格相同吗? 3. 勘误表及解决方法 - 当前固件包含变通方法(RGM 升级、CAN 超时处理)。 - 这些变通方法在马来西亚的MCU上仍然有效吗?还是需要进行调整? - 是否有针对马来西亚生产的新勘误? 4. 过程变异 - 是否有任何电气参数变化(正时、功率、温度系数)? - 马来西亚产闪存/NVM的ECC可靠性是否存在差异? 请确认:我们能否使用相同的固件二进制文件并期望获得完全相同的产品? 马来西亚MCU的行为是否正常,还是需要进行调整? 时间表:第一阶段验证将于九月底开始。非常感谢您的快速回复。 Re: S32K312 Firmware-Compatibility 你好, S32K3xx订购零件编号系统使用“N”前缀来表示“非中国制造的合格订购零件编号”。这纯粹是一个采购/订购标识。关键是,它并不表示新的掩模组或硅片修订版——使用的是相同的芯片/掩模(0P09C)。马来西亚的组装/测试基地是 ATKL(马来西亚八打灵再也),它是 NXP 为 S32K 系列产品提供的合格组装和测试设施。 你需要注意的是口罩的修改。 petervlna_0-1788419667576.png petervlna_1-1788419699369.png “N”前缀本质上是一种供应链韧性和地缘政治风险缓解工具。它为顾客提供: 保证非中国组装和测试——该设备完全在中国以外的地点(例如,马来西亚八打灵再也的 ATKL)进行组装和测试。如果客户因合同、监管或政策要求而必须避免使用中国制造的产品,则可以采购“N”型产品来满足这些要求。 出口管制/贸易合规——一些客户(尤其是在国防相关、政府或受监管的汽车供应链中)需要记录和控制元器件的原产国。“N”变体提供了清晰的审计跟踪。 供应多样化——同时拥有“S”和“N”合格变体,使客户能够灵活地切换采购来源而无需重新认证,因为这两个变体共享相同的硅芯片、掩模组和电气规格。 顺祝商祺! Peter
View full article
查阅 SR040 和 SR150 需要签署保密协议 我对召开一次会议讨论上述集成电路很感兴趣——但我似乎找不到简单的方法来做到这一点,或者申请保密协议以获取更多关于 SR040 和 SR150 的信息,希望有人能指点一下正确的方向。谢谢你! Re: Access NDA required for SR040 and SR150 你好, 希望你一切都好。很抱歉给您带来不便,但由于该产品的信息受保密协议(NDA)约束,因此不对外公开。 如需了解有关该芯片的更多信息,请联系我们代理商网络|NXP中的一位代理商。或者,如果您有任何直接联系人曾帮助您获得此设备,请与他们联系。 如果您正在寻找有关我们 UWB 产品的信息,或者您对这项技术感兴趣,我建议您查看我们合作伙伴( Trimension UWB 合作伙伴)提供的这些开发套件和模块。 如果您对这些套件/模块感兴趣,您需要直接与他们联系,了解流程以及他们能够提供的支持,因为这项技术的支持途径是通过他们。 文档和软件由相应的UWB模块合作伙伴分发。选择模块后,您将被引导至我们合作伙伴的页面,您可以在该页面访问数据表、应用笔记和所需的启用信息。 此致, 里卡多
View full article
i.MX95 Neutron:同じINT4 LLMで4問中1回答でNPU/CPUの不一致が発生します 概要 i.MX95 上で量子化された ONNX を 1 つ実行します。1 つは CPUExecutionProvider の下、もう 1 つは ニュートロン実行プロバイダー。2つの腕は同じ答えを出しません:2,466対 選択式問題では25.7%が異なる答えを返します(MMLUでは43.6%)。無料で 世代ごとに同じことが起こります - MMLU プロンプトでは、19 世代のうち 13 世代で 異なる回答の手紙。 これは言葉遣いの違いではありません。それはモデルが答える内容の違いです。一方、総合的なベンチマーク精度はわずか-1.8ポイントの変動にとどまった。 私たちは、Neutronランタイムが数値的に何をして生成するかを理解したいのです この大きさが予想されるかどうかも重要です。 設定 あなたの側で再現可能:モデルは表2からUG10166、量子化は 自分だけのレシピ、修正なし。 - ボード:i.MX95 19x19 EVK(IMX95LPD5EVK-19)、LPDDR5 - BSP: LF6.18.2_1.0.0、デバイスツリー imx95-19x19-evk-neutron.dtb - ランタイム:BSP + NeutronExecutionProviderからのONNX Runtime 1.22.0 - Neutron コンバータ:3.1.3 - モデル:meta-llama/Llama-3.2-1B-Instruct - 量子化:NXP/eiq-olive rev aae820e、 例/Llama3/llama3_2-1B_Spinquant_RTN_ONNX_4bits.json - 変換:convert_ort_models_to_neutron.py、CPU Armのモデルに適用されます。onnx - 環境: NEUTRON_CMA_512SLOTS=6 両方のArmは1つの量子化されたモデルから来ています。NPUアームはそのモデルを通過させるものです convert_ort_models_to_neutron.py。ソースのSHA-256を記録します - グラフ と 外部重み - 換算時に測定し、測定のたびに再確認します。 2回目の量子化実行や2回目のエクスポートはありません。 私たちが観察すること 1.4つの項目のうち1つは異なる回答が得られる。 MMLU、ARC-Challenge、PIQAからの2,466組のペアアイテム、0ショット、対数尤度でスコアリング 候補者の継続については、候補者ごとに1つのフォワード、生成なし、サンプリングなし。 各ベンチマークについて、ANSWER が変化した項目の割合、次に、 正確性が変更されました: - MMLU(4つの選択肢):回答変更率43.6%、正誤変更率27.1% - ARCチャレンジ(4つの選択肢):回答変更率21.3%、正誤変更率13.3% - PIQA(2つの選択肢):回答変更率9.4%、正誤変更率9.4% - 合計:回答変更率25.7%、正誤変更率17.3% 2つの数字が異なるのは、変更の3分の1(634件中208件)が1つの間違いから移動しているためです。 別の間違った答えへの答え - 正確さを失わせる真の行動の変化 手つかず。PIQAはバイナリであるため、そのような盲点はなく、2つの数値は一致する。 その通り。 2. 自由生成の場合も同様で、答え自体が変わります。 プロンプト数50、貪欲解読、トークン数64。MMLUプロンプトでは期待される出力が始まります 回答文字を含んで、その答えは世代から直接読み取ることができます (n = 19): - 両Arm間で異なる回答文字:19件中13件 - CPUで正解:19中7 - Neutronで正解:19題中6題 - 両Armが間違っていて、異なる誤答が出る意見の相違:13回中6回 回答の3分の2が変わったが、点数はほぼ同じだった(7対6)。 サンプル数は少ないので、ここでは例として報告します。上記の2,466項目の測定結果 これは定量的なものです。 以下に、一字一句そのままの例を示します。プロンプトには 4 つの選択肢がリストされており、文字を求められ、 期待される答えは 😧 CPU: " A\n説明: 式 9(9m + 3t) は 81m + 27t と同等です。 正解はAです。 NPU:「C\n正解はCです。」 どちらも間違っているが、その間違い方は異なり、それを記録できるベンチマークスコアは存在しない。 3. 乖離は累積ではなく、最初のフォワードで発生します。 このレター形式では、最初に生成されたトークンが答えであり、生成の 60% が 既に違いが生じているのは、デコードを行う前の、プリフィルパスのみで生成されたトークンである。 ステップ。50のプロンプトすべてにおいて、乖離曲線は急激に上昇した後、平坦化する。84%は トークン4、トークン64による98%。これが初期差分の伝播の様子です 貪欲なデコードの場合、KVキャッシュを通じてエラーが蓄積されることはありません。 4. 集計精度はそれらすべてを隠してしまう。 CPUは50.28%、Neutronは48.50%、-1.78ポイント差、そして 3つのベンチマークは個別に重要です。634項目に限定して 意見は異なっています。CPUは37.1%の確率で正しかったのに対し、Neutronは30.1%、235%の確率で正解です。 決定された項目のうち191、すなわち対称ノイズが50/50となる場合、55/45です。 除外したもの - サイレントCPUフォールバック: ORTプロファイリングレポートでは、80/80 MatMulNBitsが NeutronExecutionProvider、CPU使用率0。部分的な配置はできません。 - 2つの異なるモデル:同じソースファイル、グラフのSHA-256および外部重み コンバージョン時に記録され、得点前に再確認されました。 - サンプリング: 全体を通して貪欲なデコード。温度、トップk、トップpは使用しません。 - 異なる入力:両方のアームが同じアイテムファイルを同じ順序で消費します。 同じ固定シードです。 - 成果物のスコアリング:ボードはトークンごとの対数確率のみを捉えます;すべての決定 ロジックはホスト側でオフラインで動作し、両アームで同じように動作します。 - NPUのラン・トゥ・ランノイズ:同じNeutronセッション内で同じ項目を再生すること ビット同一の対数確率が得られます。NPUアームは再現可能であり、その不一致 それはCPUに対してであり、自分自身に対してではありません。 私たちの質問 これはニュートロンSのINT4経路に期待される挙動でしょうか?もしそうなら、どのようにすべきでしょうか NPU上でのLLM展開を検証し、集計ベンチマーク精度を明確に示します 表面に浮かび上がらない? 私たちは欠陥を想定しているわけではありません。浮動小数点CPUカーネルと 整数のNPU経路は通常であり、どのくらいの大きさを考えているのか知りたいです 通常、そしてどの基準でNEUTRONへのLLMポートを受け入れますか?もし 回答の4分の1が変わるのは期待内であり、それは私たちにとって有益なことです 知っていて、それを中心に設計する。 Re: i.MX95 Neutron: NPU/CPU discrepancy on one answer in four with the same INT4 LLM 迅速なご回答ありがとうございます! DS Re: i.MX95 Neutron: NPU/CPU discrepancy on one answer in four with the same INT4 LLM こんにちは、 @DamienSCHNEBELEN さん。 IMX95 NPUはmatmulしか動作できず、NPUでのLLMのパフォーマンスは実際には平均的なレベルです。したがって、あなたが観察した現象は予測可能な範囲内であり、NPU上でLLMモデルを動かすことは推奨しません。 B.R
View full article
CASPERによるECDA署名検証 ネタバレ (ハイライトして読む)     こんにちは、 ECDSA(MBEDTLS_ECP_DP_SECP256R1)で署名を検証するために、mbedTLSを独自に構築することに成功しました。 代替実装がない場合(すべての計算がCPUによって行われる場合)、LPC55S06では署名検証の計算に最大4秒かかります。 今、mbedTLS ecdsa_verify()関数をCASPER FSLドライバーにリンクしようとしています。しかし、ECDSA検証は単一の操作ではないように思われるため、私にはよく分かりません。 CAPSERの基本プリミティブ(SECP256R1_MulとSECP256R1_MulAdd)をmbedTLS関数ECDSA_verify()にリンクするにはどうすればよいですか? ご回答をよろしくお願いいたします。 LPC55xx Re: ECDA signature verification with CASPER こんにちは、peter89jeanさん。 お返事ありがとうございます。あなたが言及した方法は私が考えていたものですが、mbedTLS 設定ファイルには、シンプルで分かりやすい SECP256R1_MULADD _ALTまたは SECP256R1_MUL _ALTの定義が見当たらないようです。mbdedTLSに特化したフォーラムでこの質問をした方が良いかもしれない。 再度、感謝します。 よろしくお願いいたします。 Re: ECDA signature verification with CASPER 通常、mbedtls_ecdsa_verify() 自体を置き換える必要はありません。CASPER アクセラレーションは、mbedTLS が内部的に使用する楕円曲線/乗算レイヤーに統合されているはずです。ECDSA検証ではスカラー乗算とその和を計算する必要があるため、SECP256R1_Mul()は個々のスカラー点の乗算を処理し、SECP256R1_MulAdd()は結合操作を加速できます。正確な統合はmbedTLSのバージョンとNXP CASPARドライバーAPIによって異なりますが、一般的なアプローチは、ecdsa_verify()から直接CASPERを呼ぶのではなく、P-256のスカラー乗算プリミティブに対してmbedTLSの代替/最適化された実装を提供することです。 回复: ECDA signature verification with CASPER こんにちは、 @s_hdl ECDSA検証は複数の算術および楕円曲線演算で構成されているため、単一のCASPARプリミティブにマッピングされません。 MCUXpresso SDKでは、この統合はすでにCASPER PSA Cryptoポートで実装されています。casper_mbedtls_ecdsa_verify() 関数は、u1 と u2 の計算を含む、標準的な ECDSA 検証フローを実行します。そして、次のように呼び出します。 casper_mbedtls_ecp_muladd(grp, &R, u1, &grp->G, u2, Q); 計算する: R = u1 × G + u2 × Q ECP適応レイヤーは、mbedTLS MPI値と楕円曲線点を CASPER が 必要とする 形式 に変換し 、 この 操作を CASPER_ECC_SECP256R1_MulAdd() に マッピングします 。 同様に、 単一 の スカラー 乗算を に casper_mbedtls_ecp_mul() マッピングします CASPER_ECC_SECP256R1_Mul() 。 したがって、 直接 を変更する mbedtls_ecdsa_verify() のではなく 、 SDK が提供する CASPER 統合 の 完全な 再 利用 を推奨 します 。 component/psa_crypto_driver/casper_driver 特に、以下をご参照ください。 mcux_psa_casper_ecdsa_port.c mcux_psa_casper_ecp_port.c mbedTLSを別途構築したので、mbedTLSのバージョンがMCUXpresso SDK CASPARポートに対応しているかも確認してください。 lpcxpresso55s06_psa_crypto_examplesを参照してください。 Harry_Zhang_0-1788493275769.pngHarry_Zhang_0-1788493275769.png BR ハリー 回复: ECDA signature verification with CASPER こんにちは、ハリーさん。 あなたの回答は大変参考になりました。ありがとうございました。CASPERの実装を使うようになってからはすべて正常に動作するようになりました。 よろしくお願いします。
View full article
FXLS8964AFR3のマーキング FXLS8964AFR3のためにボディマーキングを手伝ってもらえます か?ありがとうございます。 Re: Marking for FXLS8964AFR3 こんにちは、エルフィンさん、 なお、2026年2月2日現在、NXPのMEMSセンサ製品ラインナップ(FXLS8964AFR3を含む)はSTMicroelectronicsに移行されました。NXPはもはやこの製品を所有またはサポートしていません。FXLS8964AFR3に関するお問い合わせやボディマーク情報については、STMicroelectronicsのサポートチャネル( st.com)から直接お問い合わせください。 参考までに、半導体製品のボディマーク情報は一般的に製造者によって偽造防止のため機密扱いされており、このような要求は通常、正規の流通や製造者の商業チームを通じて処理されます。これは現在STマイクロエレクトロニクスの管轄に入ります。 BRs、トーマス
View full article
Could you please provide me the pin delay of LS1021AXE7KQB? Hi, Currently, I'm designing PCB for my board. For critical timing requirement of DDR4 interface, I need to compensate the pin delay difference in the  LS1021AXE7KQB package on the PCB. So, could you please provide me the pin delay information of LS1021AXE7KQB? Thanks in advance! Best regards! Jason QorIQ LS1 Devices Re: Could you please provide me the pin delay of LS1021AXE7KQB? All internal die to pad wires of the DDR4 interface are length matched within the package, so the layout trace length task is to be done between processor's and SDRAM's pins. No specific package delay values were provided as they are not needed for the design approach. Re: Could you please provide me the pin delay of LS1021AXE7KQB? Hi,yiping For DDR4 interface of LS1021A, is it necessary to compensate pin delay difference in the package on the PCB?  Thanks in advance! Best regards! Jason Re: Could you please provide me the pin delay of LS1021AXE7KQB? The requested documents are NXP Confidential Proprietary and can only be provided under non-disclosure agreement (NDA).   Did you sign NDA with NXP? If yes, would you please provide your NDA copy or your NDA number?   You could sing a new NDA from https://www.nxp.com/webapp-signup/ndaReqForm Re: Could you please provide me the pin delay of LS1021AXE7KQB? Asked for the required information from the AE team. Re: Could you please provide me the pin delay of LS1021AXE7KQB? Hi, Any response is welcome! Thanks in advance! Best regards! Jason Re: Could you please provide me the pin delay of LS1021AXE7KQB? Hi, yiping: Get it, many thanks to you!!! BTW, I have another question.  eTSEC1 and eTSEC3 of LS1021A will be configured as RGMII mode to driver PHY. But the size of my board is very big,  I'm afraid that the too long trace on PCB will cause insufficient drive capability for RGMII interface(250Mbps per data signal) . Could you please provide the route constraint for RGMII interface, especially trace length on PCB based on common FR-4 PCB(Dk 4.2~4.4, Df 0.022)? Cause, I can't find any PCB design consideration on NXP website.  Also AN4878_Design Checklist only show the design requirement of schematic. Thanks in advance! Best regards! Jason Re: Could you please provide me the pin delay of LS1021AXE7KQB? Would you please create a new thread for your new question? Thanks. Re: Could you please provide me the pin delay of LS1021AXE7KQB? copy that! Thank you very much! Best regards! Jason
View full article
my JLINK can't connect to the S32K118 Hi Team, My current situation is that I read the STATUS  in MDM-AP through SWD and it returns 0x0001003A.Protection bit from 0x400 ~ 0x40f is 0xFFFFFFFFFFFFFFFFFFFFFFFFFE7FFFFF.But my JLINK can not connect to the S32K118.How should I go about troubleshooting the problem? Thanks & regards, Lika. Re: my JLINK can't connect to the S32K118 And I have connected RESET_b. Re: my JLINK can't connect to the S32K118 Hi Robin_Shen, The value of the MDM-AP control registers is 0x00000000.I have completed SWD host debugging for the S32K14x. For the S32K11x chip, my code follows the same debugging process as for the S32K14x, but the situation I described occurred.I would like to ask if there are any differences in the SWD debugging process between the S32K11x and S32K14x. Currently, my personal programmer can access the SWD debug port of the S32K118, but after I use MASS ERASE, the algorithm executed via RAM returns an ack fault, which did not occur before MASS ERASE. Thanks & regards, Lika. Re: my JLINK can't connect to the S32K118 Hi The values ​​of MDM-AP STATUS and FSEC appear to be correct. By the way, what are the values ​​of the MDM-AP control registers? Please check if the debug interface conforms to Table 8. S32K1xx - JTAG and SWD interface of AN5426 Hardware Design Guidelines for S32K1xx Microcontrollers. It is strongly recommended to connect RESET_b. Also, make sure you don't get the pull-up/pull-down resistors on the debugging interface wrong. Table 8. S32K1xx - JTAG and SWD interface AN5426.png Alternatively, try the method mentioned in Unbricking S32K146. Best Regards, Robin 回复: my JLINK can't connect to the S32K118 Is there any  detail  need me to add? 回复: my JLINK can't connect to the S32K118 Before the JLINK connection failed, my own programmer device couldn't read the data at 0x40c~0x40f, and I can confirm that the chip wasn't in a secure state or had any protection set. After I tried  MASS ERASE, none of the devices I had could fully operate the S32K118. After that, it went exactly like I described when I asked for help.
View full article