Platform: NXP LS1028ARDB (VSC9959 / Felix switch)
Kernel: Linux 6.18.2-rt3 (NXP Yocto real-time-edge, PREEMPT_RT)
Topology (DSA):
eno2 (ENETC) = DSA conduit / NPI port
swp0 = Felix user port (CPU-injection path: CPU → eno2 → NPI → egress swp0 physical port)
eno0 (ENETC) = separate test port (now directly cabled to swp0, used to verify the actual egress frame content)
Application: AF_PACKET SOCK_RAW socket bound to swp0, SO_TIMESTAMPING(TX_HARDWARE|RAW_HARDWARE), transmitting frames with custom EtherType 0x88B5, expecting the hardware TX timestamp from the socket error queue (SCM_TIMESTAMPING).
ptp4l is running on swp0 (HWTSTAMP_TX_ON, syncing normally, unaffected).
Obtain a hardware TX timestamp for custom 0x88B5 (non-PTP) frames transmitted on swp0, without breaking PTP synchronization on swp0.
PTP frames DO get timestamps: using the same AF_PACKET raw socket on swp0, transmitting 0x88F7 + a valid PTP header, 30/30 frames returned a hardware TX timestamp via the error queue (ocelot_get_txtstamp matched, timestamp delivered to the socket error queue).
The driver timestamp-request path works for the custom frames: 0x88B5 frames reach ocelot_port_txtstamp_request (dmesg shows felix-tx-ts: port 0 non-PTP=1 ts_id=0..3), i.e. ocelot_port->ptp_cmd is non-zero (set by ptp4l) and a timestamp ID is allocated.
For 0x88B5 frames, a timestamp ID is allocated, but the hardware produces no timestamp:
SYS_PTP_STATUS PTP_MESS_VLD = 0 immediately after sending a burst of 0x88B5 frames (no FIFO entries, no overflow).
The socket error queue stays empty.
Check Result
| ocelot_port->ptp_cmd (two-step enable) | |
| IFH BYPASS (bit 127) | |
| IFH REW_OP1 (bits 125–117) | |
| REW_PTP_CFG.PTP_2STEP_DIS | |
| PTP_CFG_MISC.PTP_ENA | |
| SYS_PORT_MODE.DATA_WO_TS (ports 0/4/6) | |
| REW_PORT_CFG.FCS_UPDATE_CPU_ENA | |
| IS2 rules adding two-step authorization for 0x88B5 (ingress swp0, then swp0|NPI) | |
| Inline timestamp insertion SYS_TIMESTAMP_OFFSET (ETH_TYPE_CFG=0x88B5, TIMESTAMP_OFFSET=14; register write/readback verified) |
Does the VSC9959/Felix two-step TX timestamping (IFH REW_OP1, REW_OP[2:0]=3) actually work for CPU-injected frames with a non-PTP EtherType? The reference manual (16.4.13.12.3.1) states "can be applied to any frame, also non-PTP frames", but we measure SYS_PTP_STATUS VLD=0 (zero FIFO entries). Is the actual silicon behavior that, even with BYPASS=1 and REW_OP1 in the IFH, the rewriter still requires the frame to be classified as PTP (by EtherType / PTP header) before it produces a timestamp FIFO entry?
Does SYS_TIMESTAMP_OFFSET (inline timestamp insertion) have any hidden enable/trigger condition beyond the ETH_TYPE_CFG match? We verified: the register is written correctly (ETH_TYPE_CFG=0x88B5, offset=14), FCS update is enabled, DATA_WO_TS=0, and with a direct swp0↔eno0 cable we confirmed the egress frame content — but no timestamp was written into the frame. Is this feature also restricted on the CPU-injection (BYPASS) path?
On the CPU-injection (BYPASS=1) path, is there an officially supported way to get a hardware TX timestamp for arbitrary-EtherType custom frames transmitted on swp0? (e.g., some enable bit, a PTP classification table configuration, or a required frame format.)
If neither of the two manual-documented mechanisms supports non-PTP frames on this silicon, is there a known erratum or a recommended alternative?
Two-step TX timestamping for non-PTP CPU-injected frames
The RM documents REW_OP[2:0] = 3 in the CPU Injection Header as “Two-step PTP,” with REW_OP[8:3] carrying the timestamp identifier; IDs 0–3 are explicitly pre-allocated for CPU-injected frames. It also states that two-step timestamping can be applied to “any frame, also non-PTP frames,” because the frame itself is not modified, and the TX timestamp is stored in SYS::PTP_STATUS / SYS::PTP_TXSTAMP .
So, from the RM, BYPASS=1 + IFH REW_OP[2:0]=3 should be a valid mechanism for CPU-injected two-step timestamping, including non-PTP frames . I did not find RM evidence that the rewriter must first classify the frame as PTP by EtherType/header when the IFH supplies the two-step command. The contradictory part is your measurement: SYS_PTP_STATUS.PTP_MESS_VLD=0 after confirmed IFH REW_OP1 , which is not explained by the RM text I retrieved.
SYS_TIMESTAMP_OFFSET / inline timestamp insertion
ES_SYS_SYSTEM_TIMESTAMP_OFFSET is documented as matching ETH_TYPE_CFG and placing a 64-bit nanosecond TX timestamp at TIMESTAMP_OFFSET ; the manual even gives a “generic timestamp insert (Chronos)” example where offset 14 places the timestamp at absolute byte 28 in the Ethernet frame.
I did not retrieve documentation that states an additional hidden enable bit beyond the general PTP enable / timestamp-offset configuration, nor documentation that explicitly says this feature is supported or blocked on CPU-injected BYPASS=1 frames. The RM wording supports the generic mechanism, but your direct-cable observation that no bytes are written at the expected offset indicates that, in this CPU-injection path, ETH_TYPE_CFG match alone is not sufficient in your setup.
Officially supported way under Linux DSA to timestamp arbitrary EtherType frames on swp0
The strongest software-side evidence says: generic packet timestamping is not supported by the DSA framework used by the LS1028A switch driver, even though the switch hardware is capable of it .
Therefore, under the stock/standard DSA Felix driver model, I would treat PTP/IEEE-1588 event message timestamping as the supported path , and arbitrary EtherType 0x88B5 TX timestamping via SO_TIMESTAMPING on swp0 as not officially supported by that software stack . That aligns with your observation that valid 0x88F7 PTP frames timestamp reliably while 0x88B5 does not.
Erratum / recommended alternative
I did not retrieve a timestamp-specific LS1028A/Felix erratum for this behavior. The evidence I found says the published Felix erratum mentioned in the retrieved ticket material is ERR A-050484 , related to NPI flow control / frame-loss management rather than timestamp FIFO generation.