Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
IPCF setup between R52_0_0 and R52_0_1 Trying to set up IPCF project between 2 R52 RTU0 cores. Facing issues with core sync and MRU IRQ not being hit. I am attaching my .mex file for reference. Can you please help me resolving the issues. currently I have 2 issues: 1. Core 0 and Core 1 sync issues , race issues. 2. IRQ firing is not proper, unsure if I have used the right MRU channels.  Re: IPCF setup between R52_0_0 and R52_0_1 Hi,PrabhanjanKopp Thank you for contacting us. 1.Before sending, the function ipc_shm_is_remote_ready() should be called to confirm that the remote end is ready. 2.It is necessary to refer to the S32Z2 manual to confirm the respective MRU instance and channel for core 0 and core 1 of the RTU0. Could you tell me the version of S32DS/RTD/IPCF you are using? If possible, could you send your IPCF project to me? It is better help to check it and handle this issue. BR Joey Re: IPCF setup between R52_0_0 and R52_0_1 PrabhanjanKopp_0-1789991578266.pngPrabhanjanKopp_0-1789991578266.pngPrabhanjanKopp_0-1789991578266.pngPrabhanjanKopp_0-1789991578266.png I use the S32E2 controller eval board. I suspect I am missing some configuration. It seemed to work on SMU-R52 but not here, Please have a look and get back if you see something wrong. Some transport code has been added on top of IPCF framework. Re: IPCF setup between R52_0_0 and R52_0_1 Any update on this? @Joey_z  Re: IPCF setup between R52_0_0 and R52_0_1 Hi,PrabhanjanKopp I have preliminarily inspected your project and noticed that there is a conflict in the address allocation of your two projects. The .intc_vector is at the same address, and running two cores simultaneously would cause a conflict. BR Joey Re: IPCF setup between R52_0_0 and R52_0_1 Hi,PrabhanjanKopp I'm currently assisting you in checking the issues. This will raise the priority of this case. I'll get back to you once there's any progress! BR Joey Re: IPCF setup between R52_0_0 and R52_0_1 Hi,PrabhanjanKopp I am helping you to check and reproduce the problem, and I can reply to you when there is progress! BR Joey Re: IPCF setup between R52_0_0 and R52_0_1 Hi Joey, can you point me to the code where this repeated initialization of interrupt resource? Can you also verify if the MRU channels I have used for the communication are actually correct? If you can give me a pseudocode to do a proper initialization of interrupt resource, it would be most helpful.  Thanks, Prabhanjan Re: IPCF setup between R52_0_0 and R52_0_1 Hi,PrabhanjanKopp I'm very sorry for the late reply. After checking your project, both projects have undergone resource initialization, which can easily lead to resource conflicts, including the repeated initialization of interrupted resources. Please check the relevant resource settings. Another way to test the IPCF project is to use the clipped GreenVIP program to avoid the synchronization of resource initialization. Hope this information can help you. BR Joey Re: IPCF setup between R52_0_0 and R52_0_1 Hi,PrabhanjanKopp Thank you for your reply. Sorry, we did not provide the pseudo code you mentioned. And not was an existing demo for IPCF setup between R52_0_0 and R52_0_1 provided. Please try to set the required interrupts in the Platform interrupt configuration for the two projects. The MRU channels settings did not reveal obvious issues; However, further testing is also necessary.  Recently, I will be on vacation. If you need my continued support, I will be back on October 8th. If you are in a hurry, you can create a new ticket.  My colleagues who are currently working normally will assist you with your new ticket. I apologize for the inconvenience caused. BR Joey
View full article
アプリケーションコマンド 皆さん freeMASTERアプリケーションコマンドはNODE REDノードでは利用できないようです。何らかの方法でそれらを呼び出すことは可能でしょうか? よろしくお願いいたします パオロ Re: Application commands こんにちは、@pberna67 さん。 残念ながら、アプリケーションコマンドはFreeMASTERに追加されませんでした。Node-REDノードです。 現時点で追加できる唯一の方法は、『FreeMASTER Node.js Modules』で利用可能な「node-red-contrib-freemaster」Node.jsモジュールを拡張し、手動でインストールすることで以下の動作を実行することです: npm i path_to_the_updated_node-red-contrib-freemaster Node-REDのホームフォルダ($HOME/.node-red)から。 敬具、 イウリアン Re: Application commands 親愛なるイウリアン それは残念だ 😞 ! コマンドが必要です 1) freeMASTER / FreeMaster lite はまだ開発中ですか? 2) 次のリリースでアプリケーションコマンドを統合する計画はありますか?   FreeMaster(ライト版ではなく)でアプリケーションコマンドがあるバージョンにアプローチしようとしていますが、ここではNode Redはサポートされていません 😞 ! パオロ Re: Application commands こんにちは、パオロさん。 FreeMASTERは積極的に開発・改良されている一方、 FreeMASTER Liteは主にバグ修正と重要なアップデートによって維持されている。 アプリケーションコマンド機能は長年利用可能です。FreeMASTERでは現在もメンテナンスとテストが行われていますが、現時点ではさらなる機能強化の予定はありません。可能な限り、アプリケーションを制御するための代替的な仕組み(例:フラグ変数の使用)を推奨します。   Iulian  
View full article
U4GM NBA 2K27: Turn Challenges Into Better MyTEAM Depth The most interesting part of NBA 2K27 Season 1 is not always the headline reward. Often, it is the way a small challenge changes how a player approaches the next few games. A three-point objective can turn a normal matchup into a shooting laboratory, while a dunk requirement can suddenly make a forgotten athletic wing worth testing. With 2K27 MT available as part of the wider team-building economy, the trick is not simply adding expensive names to a lineup but making sure new resources actually improve how the team plays. Recent Play Now Challenges have leaned into this idea by rotating objectives instead of leaving players with one static checklist. Current Season 1 activities have included winning games, using Holo Parallel cards, completing dunk objectives, adding new player cards, and playing through Triple Threat-related challenges. The rotation gives MyTEAM a more active daily rhythm and makes collection depth more valuable. A useful way to approach these challenges is to build a temporary lineup around the objective rather than forcing the objective into the strongest possible lineup. Suppose the task involves three-pointers. Instead of taking the usual lineup and repeatedly forcing difficult shots with one player, use two players who can create space and one reliable shooter who can punish defensive help. The challenge then becomes part of the game rather than an annoying side task. Dunk-focused objectives work in the opposite direction. Spacing becomes extremely important because an athletic finisher needs a clear lane. If the paint is constantly occupied by another interior scorer, the lineup may technically contain a powerful dunker while making it difficult for that player to do what the challenge requires. A better setup can involve one creator on the perimeter, one player who can stretch the defense, and a finisher who attacks after the defense has been pulled away. Triple Threat makes these experiments even more noticeable. With only three players on the floor, there is nowhere to hide a weakness. If two players cannot shoot, the defense can shrink the court. If nobody can defend on the perimeter, one opposing creator can control the game. That is why complementary skill sets often matter more than simply selecting the three highest-rated cards available. Player XP adds another layer to this process. In NBA 2K27, cards can earn XP through gameplay, giving players another reason to put different cards into real matches. A card being tested for a challenge can therefore provide progression at the same time. This creates a nice feedback loop: the challenge encourages the player to use the card, gameplay develops the card, and the improved card may eventually become useful outside the original challenge. The revamped Exchange makes collection management more flexible as well. Instead of viewing every lower-tier or duplicate card as something that simply occupies space, players can evaluate whether it has future lineup value, challenge value, or Exchange value. That does not mean every card should immediately be exchanged. Keeping a small reserve of useful players is sensible because challenge requirements can change quickly, and a card that looks ordinary today may suddenly become convenient tomorrow. Season 1's shared progression also encourages players to alternate between modes. MyTEAM and The City contribute to the same Season XP progression, so a player who gets tired of one mode can switch activities without completely abandoning seasonal progress. The City includes events such as Midway and Blackout, while MyTEAM has its own challenges and competitive activities. That variety can make a long season feel less repetitive because progress does not depend on playing exactly the same type of game every session. There is also a practical lesson here for roster construction: do not build only for one game mode. A card with excellent half-court defense may be valuable in a slower matchup but less comfortable in a fast Triple Threat environment. A high-level scorer may dominate when given space but become less effective when an opponent constantly switches and pressures the ball. Having several styles available gives a collection more flexibility and reduces the need to rebuild everything whenever the objective changes. This is where resource planning becomes more important than simply chasing the newest card. Before spending, look at the positions that are actually limiting the lineup. A missing ball handler, weak perimeter defense, unreliable shooting, or poor rebounding can each change the team's performance more than a small overall-rating increase. U4GM can provide a convenient option for players who want to add NBA 2K27 resources while keeping an eye on affordability, delivery speed, and account safety, but the purchase makes more sense when it is tied to a specific roster goal. A good Season 1 session can therefore accomplish several things at once. You might enter a challenge with a card that needs Player XP, complete an objective that earns another reward, improve the card through gameplay, and finish the session closer to a seasonal milestone. That is much more satisfying than grinding a checklist without understanding why the pieces matter. As Season 1 continues, the value of a flexible collection should become clearer. New challenges can shift attention toward different player types, while Exchange rewards and Player XP give older cards additional uses. Rather than building one rigid lineup and refusing to change it, players can treat MyTEAM like an evolving roster, keeping a core group while maintaining enough depth to respond to whatever the next objective demands. When extra resources are needed to make those adjustments, buy NBA 2K MT through U4GM can be part of that preparation, giving players a convenient and relatively budget-friendly way to support their next roster experiment. FRDM-Training
View full article
UTEST書き込みデータ処理 こんにちは Utestにデータを書き込むには、データの消去が必要ですか? UTEST_program.jpegUTEST_program.jpeg AN13388では、UTESTセクターにデータを書き込むプロセスは、他のブロックにプログラムを書き込むプロセスと同じであると述べられている。 しかし、UTESTは一度しか実行されないプログラムなので、書き込み前に消去する必要があるのでしょうか? リカ 回复: UTEST写数据流程 また、UTESTのどの部分をDEBUGデバッグを使って変更できるのかも知りたいです。 Re: UTEST写数据流程 最初に消去しないでください。UTESTセクターはOTP(ワンタイムプログラマブル)です。 Example_S32K344_decouple_RTD400_Ip_C40_DS35には、参考としてUTESTのサンプルが含まれています。 申し訳ありませんが、「UTEST中にDEBUGで変更できる領域」の意味が分かりませんでした。デバッグ中にレジスタを操作して、標準のフラッシュプログラムシーケンス(AN13388で説明されているのと同じプロセス)を実行するという意味でしょうか?S32K3XXRM.pdf Rev12の「表837」を参照してください。「ライフサイクルとビット構成に基づくデバッグアクセス」という表現は、ライフサイクルのさまざまな段階におけるデバッグ権限について言及しています。これは、あなたが言及している内容でしょうか? 添付ファイルS32K3xx_DCF_clients.xlsxからS32K3XXRM.pdfにあるUTESTメモリマップテーブルの「アクセス権限」列と「プログラム作成者」列は、アクセス権限を示しています。また、異なるライフサイクルごとに異なる色で読み取り/書き込み権限が示されています。 Re: UTEST写数据流程 はい、デバッグ中に、レジスタ操作による標準フラッシュプログラムシーケンスを実行することで、CUST_DEL LCステージのUTESTの内容を変更することは可能ですか?1から0へのいくつかの位置をクリアしたいのです。 Re: UTEST写数据流程 utest nvm ユーザー空間プログラミングの回答を参照してください。 Re: UTEST写数据流程 はい、どうもありがとうございました。
View full article
CBTL04083ABS こんにちは、みんな、 現在、 CBTL04083ABS (4チャンネル、2:1 PCIe Gen3マルチプレクサ/デマルチプレクサ)を含むレイアウトおよび信号整合性シミュレーションプロジェクトに取り組んでいます。 残念ながら、公開製品ページやデザインリソースの中から直接IBISモデルを見つけることはできませんでした。私は個人開発者で企業向けの企業アカウントを持っていないので、このデバイスのIBISモデル(または利用可能ならタッチストーン/Sパラメータファイル)をどなたか教えていただけませんか? よろしくお願いいたします。 よろしくお願いします、 ヴォルフガング Re: CBTL04083ABS こんにちは、ヴォルフガングさん。 添付の報復IBISモデルをご覧ください。 BRs、トーマス
View full article
UTEST write data process Hello Does writing data to Utest require erasing? UTEST_program.jpegUTEST_program.jpeg The AN13388 said the process to write a data in the UTEST Sector is the same process used to program in other blocks. However, UTEST is a one-time program, so does it need to be erased before writing? Lika 回复: UTEST写数据流程 I'd also like to know which areas of UTEST can be modified using DEBUG debugging. Re: UTEST写数据流程 Do not erase first; UTEST Sector is an OTP (One Time Programmable). Example_S32K344_decouple_RTD400_Ip_C40_DS35 contains a UTEST example for your reference. I apologize, I didn't understand "Which areas can be modified via DEBUG during UTEST". Do you mean executing a standard Flash Program sequence (the same process described in AN13388) by manipulating registers during debugging? See "Table 837" in S32K3XXRM.pdf Rev12.The phrase "Debug access based on LifeCycle and bit configurations" mentions debug permissions at different LifeCycle stages. Are you referring to this? The Accessibility and Programmed by columns of the UTEST Memory Map table in the attachment S32K3xx_DCF_clients.xlsx to S32K3XXRM.pdf specify the permissions. Additionally, different colors indicate read/write permissions for different Lifecycles. Re: UTEST写数据流程 Yes, during debugging, can the UTEST content be modified in the CUST_DEL LC stage by executing a standard Flash Program sequence through register manipulation? I want to clear some positions of 1 to 0. Re: UTEST写数据流程 Please refer to the answer in utest nvm user space programming . Re: UTEST写数据流程 Okay, thank you very much.
View full article
CBTL04083ABS Hello everyone, I am currently working on a layout and signal integrity simulation project that includes the CBTL04083ABS (4-channel, 2:1 PCIe Gen3 multiplexer/demultiplexer). Unfortunately, I couldn't find an IBIS model directly on the public product page or under the design resources. Since I am an individual developer and do not have an enterprise corporate account, could anyone please provide me with the IBIS model (or touchstone/S-parameter files if available) for this device? Thank you very much for your help! Best regards, Wolfgang Re: CBTL04083ABS Hello Wolfgang, Please find attached the requited IBIS model. BRs, Tomas
View full article
S32DS S32K358 项目咨询 wj_kwak_0-1789777426372.pngwj_kwak_0-1789777426372.png 我有一个关于创建 S32K358 项目的问题。 我很好奇为什么会创建两个项目,M7_0 和 M7_2。 我想知道“继承启动核心工具链”按钮的功能。 我的队友说参考文档中指出 M7_0 是引导加载程序区域,M7_2 是应用程序区域,但我还没有在文档中找到证据来验证这一点。我想确认一下。 Re: S32DS S32K358 Project Inquiry 嗨@wj_kwak 对于 S32K358,S32DS 默认创建两个独立的项目,一个用于 M7_0,一个用于 M7_2。这些项目对应于两个处理核心。它们并不代表引导加载程序区域和应用程序区域。 S32DS 项目创建向导通常不会创建一个包含两个内核应用程序的单个项目。如果需要这样的项目结构,则必须手动创建/配置。然而,在大多数情况下,没有必要这样做,通常的做法是使用两个独立的项目,每个核心一个项目。 在为其他核心创建项目时,可以使用“继承启动核心工具链”选项从启动核心项目继承工具链配置。如果启用此功能,您可以仅为 Cortex-M7_0_0 选择工具链。Cortex-M7_0_2 的工具链选择将显示为灰色,因为将应用 Cortex-M7_0_0 的配置。 您还可以参考这里提供的多核示例和文档: community.nxp.com/t5/S32K/S32K324-Multi-Core-Example-Project-based-on-Whiteboard/m-p/1547771 该软件包演示了两种方法:每个核心的独立项目和两个核心的单个项目编译成单个 ELF 文件。 因此,M7_0 和 M7_2 不应被理解为引导加载程序和应用程序项目。它们只是与各个核心相关的项目。 顺祝商祺! Lukas
View full article
U4GM NBA 2K27:将挑战转化为更强的MyTEAM阵容深度 NBA 2K27 第一赛季最有趣的部分并不总是最引人注目的奖励。通常情况下,一次小小的挑战就能改变一名球员对待接下来几场比赛的态度。三分球目标可以将一场普通的比赛变成投篮实验室,而扣篮要求则可以突然让一位被遗忘的运动型侧翼球员值得一试。由于 2K27 MT 是更广泛的球队建设经济体系的一部分,所以诀窍不仅仅是给阵容添加昂贵的球员,而是要确保新的资源能够真正改善球队的比赛方式。 最近的“立即畅玩挑战”活动也采用了这种理念,通过轮换目标来代替给玩家留下一个静态的清单。目前第 1 赛季的活动包括赢得比赛、使用全息平行卡、完成扣篮目标、添加新球员卡以及进行与三威胁相关的挑战。轮换机制让MyTEAM拥有更活跃的日常节奏,也让收藏深度更有价值。 应对这些挑战的一个有效方法是围绕目标构建一个临时阵容,而不是强行将目标融入最强阵容。假设这项任务涉及投三分球。不要采用常规阵容,反复让一名球员强行出手高难度投篮,而是使用两名能够创造空间的球员和一名能够惩罚防守协防的可靠射手。这样一来,挑战就变成了游戏的一部分,而不是令人讨厌的附加任务。 以扣篮为目标的策略则适得其反。保持间距至关重要,因为优秀的冲刺选手需要畅通无阻的冲刺路线。如果禁区内始终有另一名内线得分手占据,那么阵容理论上可能包含一名强力扣篮手,但这会使该球员难以完成比赛所需的挑战。更好的阵容可以包括一名外线组织者、一名能够拉开防守的球员,以及一名在防守被吸引后发起进攻的终结者。 三重威胁让这些实验更加引人注目。场上只有三名球员,任何弱点都无处遁形。如果两名球员都无法投篮,防守方可以缩小场地范围。如果外线无人防守,对方一名进攻球员就能掌控比赛。因此,互补的技能组合往往比简单地选择三张评分最高的卡牌更重要。 玩家经验值给这个过程增添了另一层意义。在 NBA 2K27 中,卡片可以通过游戏获得经验值,这给了玩家另一个理由在真实比赛中使用不同的卡片。因此,一张用于挑战的卡牌也可以同时提供进度推进。这形成了一个良好的反馈循环:挑战鼓励玩家使用卡牌,游戏玩法促进卡牌发展,而改进后的卡牌最终可能会在最初的挑战之外发挥作用。 改版后的交易所也使收款管理更加灵活。玩家不再将每张低级或重复的卡牌视为仅仅占据空间的东西,而是可以评估它是否具有未来的阵容价值、挑战价值或交换价值。但这并不意味着每张卡都应该立即更换。保留少量有用的球员储备是明智的,因为挑战要求可能会快速变化,今天看起来很普通的卡牌明天可能突然变得有用。 第一赛季的共享进度也鼓励玩家在不同模式之间交替进行。MyTEAM 和 The City 模式都计入赛季经验值进度,因此玩家如果对某种模式感到厌倦,可以切换活动而不会完全放弃赛季进度。城市活动包括 Midway 和 Blackout 等,而 MyTEAM 则有自己的挑战和竞技活动。这种多样性可以让漫长的赛季感觉不那么重复,因为进步并不取决于每次都玩完全相同类型的游戏。 这里还有一个关于阵容构建的实用经验:不要只针对一种游戏模式进行构建。一张拥有出色半场防守能力的卡牌在节奏较慢的比赛中可能很有价值,但在快节奏的三威胁比赛中则不太适应。高水平得分手在获得空间时可能占据主导地位,但当对手不断转移球并施压时,其效率就会降低。提供多种风格可以使作品集更具灵活性,并减少在目标改变时重新构建所有内容的需要。 这时,资源规划就比单纯追求最新卡片更重要了。在投入资金之前,先看看哪些位置实际上限制了阵容。缺少一名控球后卫、外线防守薄弱、投篮不准或篮板能力差,这些因素对球队表现的影响,都可能比球队整体评分的小幅提升更大。U4GM 可以为想要添加 NBA 2K27 资源的玩家提供一个方便的选择,同时兼顾价格、交付速度和账户安全,但当购买与特定的阵容目标联系起来时,这种购买方式就更有意义了。 因此,一季精彩的剧集可以同时实现几个目标。你可能会带着一张需要玩家经验值的卡牌参加挑战,完成一个目标以获得另一个奖励,通过游戏提升卡牌,并在游戏结束时更接近赛季里程碑。这比漫无目的地完成清单上的任务,却不明白每个步骤的重要性要有意义得多。 随着第一季的进行,灵活系列产品的价值应该会更加明显。新的挑战可能会将注意力转移到不同类型的玩家身上,而兑换奖励和玩家经验值则为旧卡牌提供了额外的用途。玩家与其构建一个固定的阵容并拒绝改变,不如将 MyTEAM 视为一个不断发展的阵容,保留核心阵容的同时保持足够的深度,以应对下一个目标所需的任何情况。当需要额外资源来进行这些调整时,通过 U4GM 购买 NBA 2K MT 可以成为准备工作的一部分,为玩家提供一种方便且相对经济实惠的方式来支持他们的下一个阵容实验。 FRDM 培训
View full article
UTEST写数据流程 您好 请问往Utest中写入数据需要擦除吗 UTEST_program.jpegUTEST_program.jpeg The AN13388 said the process to write a data in the UTEST Sectorr is the same process used to program in other blocks. 但是UTEST属于一次性编程,写入前需要擦除吗? Lika 回复: UTEST写数据流程 同时我想知道UTEST哪些区域可以通过DEBUG调试修改 Re: UTEST写数据流程 不要先擦除,UTEST Sector 属于OTP (One Time Programmable)。 Example_S32K344_decouple_RTD400_Ip_C40_DS35 这里有写UTEST的例程可供你参考。 抱歉我没明白“UTEST哪些区域可以通过DEBUG调试修改”。请问你是指调试的时候通过操作寄存器执行标准的 Flash Program 序列(与 AN13388 中描述的流程相同)?S32K3XXRM.pdf Rev12 的"Table 837. Debug access based on LifeCycle and bit configurations" 有提到不同LifeCycle阶段的调试权限,请问你是指这个? S32K3XXRM.pdf的附件S32K3xx_DCF_clients.xlsx 的 UTEST Memory Map 表格Accessibility、Programmed by列有写明权限。另外不同的颜色表示不同LifeCycle时候的读写权限。 Re: UTEST写数据流程 对的,调试的时候通过操作寄存器执行标准的Flash Program序列可以在CUST_DEL LC阶段修改UTEST内容吗,我想将一些位置的1清0 Re: UTEST写数据流程 请参考 utest nvm user space programming 里的答复。 Re: UTEST写数据流程 好的,非常感谢
View full article
R52_0_0とR52_0_1間のIPCF設定 2つのR52 RTU0コア間でIPCFプロジェクトをセットアップしようとしています。コア同期とMRU IRQがヒットしないという問題が発生しています。.mexファイルを添付します参考資料として保管してください。問題解決を手伝ってもらえますか?現在、私には2つの問題があります。 1. Core 0とCore 1の同期問題、レースの問題。 2. IRQの発射が正しくなく、正しいMRUチャネルを使っているか不明です。 Re: IPCF setup between R52_0_0 and R52_0_1 PrabhanjanKopp_0-1789991578266.pngPrabhanjanKopp_0-1789991578266.pngPrabhanjanKopp_0-1789991578266.pngPrabhanjanKopp_0-1789991578266.pngプラバンジャンコップ_0-1789991578266.png 私はS32E2コントローラー評価ボードを使っています。何らかの設定が不足しているのではないかと思います。SMU-R52では動作したようですが、こちらでは動作しません。ご確認いただき、何か問題がございましたらご連絡ください。IPCFフレームワークの上に、いくつかのトランスポートコードが追加されました。 Re: IPCF setup between R52_0_0 and R52_0_1 こんにちは、 PrabhanjanKopp お問い合わせいただきありがとうございます。 1.送信前に、ipc_shm_is_remote_ready()関数を呼び出して、リモート側が準備完了であることを確認する必要があります。 2.It、RTU0のコア0およびコア1のそれぞれのMRUインスタンスとチャネルを確認するために、S32Z2マニュアルを参照する必要があります。 S32DS/RTD/IPCF のどのバージョンを使っているか教えてもらえますか?可能であれば、IPCFのプロジェクトを私に送ってもらえますか?確認してこの問題に対処する方が良いでしょう。 BR ジョーイ Re: IPCF setup between R52_0_0 and R52_0_1 この件について何か進展はありますか? @Joey_z Re: IPCF setup between R52_0_0 and R52_0_1 こんにちは、 PrabhanjanKopp あなたのプロジェクトを予備的に調査したところ、2つのプロジェクトのアドレス割り当てに競合があることがわかりました。.intc_vectorは同じアドレスにあり、2つのコアを同時に実行すると競合が発生します。 BR ジョーイ Re: IPCF setup between R52_0_0 and R52_0_1 こんにちは、 PrabhanjanKopp 現在、問題の確認をお手伝いしております。これにより、このCASEの優先度が上がります。 進展があればまたご連絡します! BR ジョーイ Re: IPCF setup between R52_0_0 and R52_0_1 こんにちは、 PrabhanjanKopp 問題の確認と再現を手伝っており、進展があればご返信します! BR ジョーイ Re: IPCF setup between R52_0_0 and R52_0_1 こんにちは、ジョーイ。 この割り込みリソースの繰り返し初期化が起こるコードを教えてもらえますか?私が通信に使ったMRUチャネルが本当に正しいかどうかも確認できますか?もし割り込みリソースの初期化を適切に行うための擬似コードを教えていただければ、とても助かります。 ありがとうございます プラバンジャン Re: IPCF setup between R52_0_0 and R52_0_1 こんにちは、 PrabhanjanKopp ご返信よろしくお願いします。 申し訳ありませんが、ご指摘いただいた擬似コードは提供しておりません。また、R52_0_0とR52_0_1間のIPCF設定に関する既存のデモも提供されませんでした。2つのプロジェクトでプラットフォーム割り込み設定で必要な割り込みを設定してみてください。MRUのチャネル設定では明らかな問題は見られませんでした。しかし、さらなるテストも必要です。 最近、私は休暇を取ります。もし私の継続的なサポートが必要なら、10月8日に戻ってきます。急いでいる場合は、新しいチケットを作成できます。現在通常勤務中の同僚が新しいチケットの作成をサポートします。 ご迷惑をおかけして申し訳ございません。 BR ジョーイ Re: IPCF setup between R52_0_0 and R52_0_1 こんにちは、 PrabhanjanKopp 返信が遅くなり大変申し訳ありません。 プロジェクトを確認すると、両方のプロジェクトがリソース初期化を経ており、これによりリソースの競合や中断されたリソースの繰り返し初期化が起こりやすいです。関連するリソース設定を確認してください。 IPCFプロジェクトをテストするもう1つの方法は、リソース初期化の同期を回避するために、GreenVIPプログラムの一部を切り取って使用することです。 この情報があなたの助けになれば幸いです。 BR ジョーイ
View full article
Application commands Dear All I see that freeMASTER Application Commands are not available in NODE RED nodes. Is it possibile to invoke them in some way ? Regards Paolo Re: Application commands Hi @pberna67, Unfortunately, application commands were not added to FreeMASTER;s Node-RED nodes. Currently, the only way you could add them is by extending `node-red-contrib-freemaster` Node.js module available in `FreeMASTER Node.js Modules` and then install them manually by running: npm i path_to_the_updated_node-red-contrib-freemaster from Node-RED's home folder ($HOME/.node-red). Kind regards, Iulian Re: Application commands Dear Iulian It is a pity 😞 ! need command  1) Are freeMASTER / FreeMaster lite still under development ? 2) Any plan to integrate Application commands in  the next release ?   I'm try approaching  FreeMaster (not lite) version which has the Application command, however here Node Red is not supported 😞 ! Paolo Re: Application commands Hi Paolo, FreeMASTER is actively developed and enhanced, whereas FreeMASTER Lite is primarily maintained through bug fixes and critical updates. The Application Commands feature has been available for many years. While it is still maintained and tested in FreeMASTER, there are currently no plans for further enhancements. Where possible, we recommend using alternative mechanisms to control the application (ex: using flag variables).   Iulian  
View full article
U4GM NBA 2K27:チャレンジをMyTEAMの深みを増す NBA 2K27シーズン1で最も興味深い部分は、必ずしも目玉となる報酬ではない。多くの場合、それは小さな困難が選手のその後の数試合への取り組み方を変えるという点にある。3ポイントの目標は普通の対戦をシュート実験室に変え、ダンクの要件が忘れ去られていたアスレチックなウイングを試す価値を突然変えてしまう。2K27 MTがチームビルディング経済の一部として利用可能であることから、単に高額な名前をラインナップに加えるだけでなく、新しいリソースがチームのプレースタイルを実際に向上させることがポイントです。 最近のPlay Now Challengeでは、プレイヤーに一つの固定的なチェックリストを置くのではなく、目標をローテーションで行うというこの考え方が取り入れられています。シーズン1の現在のアクティビティには、ゲームに勝利すること、ホロパラレルカードを使用すること、ダンクの目標を達成すること、新しいプレイヤーカードを追加すること、トリプルスレット関連のチャレンジをプレイすることなどが含まれています。このローテーションにより、MyTEAMはよりアクティブな日々のリズムを手に入れ、コレクションの充実度をより価値あるものにする。 こうした課題に取り組む上で有効な方法は、目標を最強のラインナップに無理やり押し込むのではなく、目標を中心に一時的なラインナップを構築することである。仮に、その課題がスリーポイントシュートに関するものだとしましょう。通常のラインナップで1人で難しいシュートを繰り返すのではなく、スペースを作る2人の選手と、守備の助けを罰せる信頼できるシューター1人を使うのが良いでしょう。そうすれば、その課題は煩わしい付随的な作業ではなく、ゲームの一部となる。 ダンクシュートに特化した目標は、逆の方向で機能します。アスリートがフィニッシュするには明確なレーンが必要なので、間隔が非常に重要になる。ペイントエリアが常に他のインサイドスコアラーによって占められている場合、ラインナップには強力なダンカーが含まれているように見えるかもしれないが、その選手がチャレンジに必要なことを実行するのは困難になるだろう。より良い構成は、外周にクリエイター1人、守備を広げる選手1人、そして守備が崩れた後に攻撃するフィニッシャーがいる形です。 『トリプル・スレット』は、こうした実験をさらに際立たせる作品となっている。コート上に選手が3人しかいない状況では、弱点を隠す場所はない。2人の選手がシュートできない場合、ディフェンス側はコートを縮小させることができます。誰も外周で守れなければ、一方の相手クリエイターが試合を支配できます。だからこそ、補完的なスキルセットの方が、単に3枚の最高評価カードを選ぶよりも重要になることが多いのです。 プレイヤー経験値は、このプロセスにさらに別の要素を加える。NBA 2K27では、カードはゲームプレイを通じてXPを獲得できるため、プレイヤーが実際の試合に異なるカードを配置するもう一つの理由を与えています。チャレンジでテストされるカードは、同時に進行を促すことができます。これは良いフィードバックループを生み出します。チャレンジによってプレイヤーはカードを使うようになり、ゲームプレイによってカードが進化し、改良されたカードは最終的に元のチャレンジ以外でも役立つようになるでしょう。 刷新されたエクスチェンジは、債権回収マネジメントもより柔軟にしています。すべての下位カードや重複カードを単にスペースを占有するものと見るのではなく、プレイヤーはそのカードが将来のラインナップ価値、チャレンジ価値、交換価値があるかどうかを評価できます。それは、すべてのカードをすぐに交換すべきだという意味ではない。チャレンジの条件が急速に変わる可能性があるため、少数の有用なプレイヤーを残しておくのは賢明です。今日は普通に見えるカードが明日には突然便利になるかもしれません。 シーズン1の共有進行システムは、プレイヤーがモードを交互にプレイすることを促します。MyTEAMとThe Cityは同じシーズンXP進行に寄与しているため、あるモードに飽きたプレイヤーはシーズン進行を完全に放棄せずにアクティビティを切り替えることができます。シティにはミッドウェイやブラックアウトなどのイベントがあり、MyTEAMも独自のチャレンジや競技活動を行っています。この多様性のおかげで、毎回同じタイプのゲームをプレイすることが進捗に依存しないため、長いシーズンの単調さが和らぎます。 選手編成に関する実践的な教訓もここにはある。それは、一つのゲームモードだけを基準に選手を編成してはいけないということだ。ハーフコートディフェンスに優れたカードは、スローペースな対戦では有効かもしれないが、スピード重視のトリプルスレット環境ではあまり適していないかもしれない。高レベルのスコアラーはスペースがあれば支配力を発揮しますが、相手が絶えずスイッチしてプレッシャーをかけると効果が低下します。複数のスタイルを用意しておくことで、コレクションの柔軟性が高まり、目的が変わるたびにすべてを再構築する必要性が軽減されます。 こうした状況では、単に最新のカードを追い求めるよりも、リソース計画がより重要になる。支出する前に、実際にラインナップを制限しているポジションを見てください。ボールハンドリングの欠如、外周防御の弱さ、信頼性の低いシュート、リバウンドの不振は、わずかな総合評価の向上以上にチームのパフォーマンスに影響を与えることがあります。U4GMは、手頃な価格、配送速度、アカウントのセーフティに注意を払いながらNBA 2K27のリソースを追加したいプレイヤーにとって便利な選択肢を提供しますが、特定のロースター目標に結びついた方が購入の方が理にかなっています。 したがって、良いシーズン1のセッションは複数のことを同時に達成できます。プレイヤーXPが必要なカードを使ってチャレンジに挑戦したり、別の報酬を獲得できる目標を達成したり、ゲームプレイを通してカードを強化したり、セッションを終える頃にはシーズンのマイルストーンに近づいているかもしれません。なぜピースが重要なのか理解せずにチェックリストを繰り返し練習するよりも、はるかに満足感があります。 シーズン1が進むにつれて、柔軟なコレクションの価値がより明確になるはずだ。新しいチャレンジは異なるプレイヤータイプに注目を向けることができ、交換報酬やプレイヤー経験値は古いカードに追加の使い方を与えます。一つの厳格なラインナップを作り変えないのではなく、プレイヤーはMyTEAMを進化し続けるロースターとして扱い、コアメンバーを維持しつつ次の目標に対応できる層の厚さを保つことができます。調整に必要な追加のリソースが必要な場合は、U4GMを通じてNBA 2K MTを購入することも準備の一部となり、プレイヤーに次のロースター実験を便利かつ比較的予算的にサポートできる方法を提供します。 FRDMトレーニング
View full article
应用程序命令 各位 我发现 node red 节点中没有 freeMASTER 应用程序命令。是否有可能以某种方式调用它们? 问候 Paolo Re: Application commands 嗨@pberna67 , 遗憾的是,FreeMASTER 的 Node-RED 节点中没有添加应用程序命令。 目前,添加这些模块的唯一方法是扩展 `FreeMASTER Node.js Modules` 中提供的 `node-red-contrib-freemaster` Node.js 模块,然后手动运行以下命令进行安装: npm i path_to_the_updated_node-red-contrib-freemaster 从 Node-RED 的主文件夹( $HOME/.node-red)。 亲切的问候, 尤利安 Re: Application commands 亲爱的尤利安 很可惜 😞 需要命令 1)freeMASTER/FreeMaster lite还在开发中吗? 2)是否有计划在下一个版本中集成应用程序命令? 我尝试使用带有应用程序命令的 FreeMaster(非精简版),但是它不支持 Node-RED。 😞 ! Paolo Re: Application commands 嗨,保罗, FreeMASTER正在积极开发和改进,而FreeMASTER Lite主要通过修复错误和进行关键更新来维护。 应用程序命令功能已经推出多年。虽然FreeMASTER仍在维护和测试该功能,但目前没有进一步增强的计划。如果可能,我们建议使用替代机制来控制应用程序(例如:使用标志变量)。   Iulian  
View full article
R52_0_0 和 R52_0_1 之间建立 IPCF 连接 尝试在 2 个 R52 RTU0 内核之间建立 IPCF 项目。遇到核心同步问题,且最近使用的中断请求 (MRU IRQ) 未被触发。我附上了我的.mex文件。文件供参考。请您帮我解决这些问题。目前我遇到两个问题: 1. 核心 0 和核心 1 同步问题、竞争问题。 2. IRQ触发不正确,我不确定是否使用了正确的MRU通道。 Re: IPCF setup between R52_0_0 and R52_0_1 你好, PrabhanjanKopp 感谢您与我们联系。 1.发送之前,应调用函数ipc_shm_is_remote_ready()确认远程端已准备就绪。 2.需要参考 S32Z2 手册,以确认 RTU0 的内核 0 和内核 1 的相应 MRU 实例和通道。 请问您使用的是哪个版本的S32DS/RTD/IPCF?如果可以的话,能否将您的 IPCF 项目发送给我?最好检查并处理这个问题。 BR 乔伊 Re: IPCF setup between R52_0_0 and R52_0_1 PrabhanjanKopp_0-1789991578266.pngPrabhanjanKopp_0-1789991578266.pngPrabhanjanKopp_0-1789991578266.pngPrabhanjanKopp_0-1789991578266.png 我使用的是S32E2控制器评估板。我怀疑我漏掉了一些配置。它在 SMU-R52 上似乎可以运行,但在这里却不行。请检查一下,如果发现问题请告知。在 IPCF 框架之上添加了一些传输代码。 Re: IPCF setup between R52_0_0 and R52_0_1 这件事有进展吗? @Joey_z Re: IPCF setup between R52_0_0 and R52_0_1 你好, PrabhanjanKopp 我已初步检查了您的项目,并注意到您的两个项目在地址分配方面存在冲突。.intc_vector 位于同一地址,同时运行两个核心会导致冲突。 BR 乔伊 Re: IPCF setup between R52_0_0 and R52_0_1 你好, PrabhanjanKopp 我正在协助您检查这些问题。这将提高此案的优先级别。 一旦有任何进展,我会立即回复你! BR 乔伊 Re: IPCF setup between R52_0_0 and R52_0_1 你好, PrabhanjanKopp 我正在协助您检查和重现问题,如有进展我会及时回复您! BR 乔伊 Re: IPCF setup between R52_0_0 and R52_0_1 嗨,乔伊, 能否指出重复初始化中断资源的代码位置?您能否也确认一下我用于通信的MRU通道是否正确?如果您能提供一份用于正确初始化中断资源的伪代码,那将对我非常有帮助。 谢谢! 普拉班詹 Re: IPCF setup between R52_0_0 and R52_0_1 你好, PrabhanjanKopp 感谢您的回复。 抱歉,我们没有提供您提到的伪代码。而且没有提供 R52_0_0 和 R52_0_1 之间 IPCF 设置的现有演示。请尝试在平台中断配置中为这两个项目设置所需的中断。MRU通道设置未发现明显问题;但是,仍需进行进一步测试。 最近我将休假。如果您需要我继续提供支持,我将于10月8日回归。如果您时间紧迫,可以创建一个新的工单。目前正在正常工作的同事会协助您处理新工单。 给您带来的不便,我深表歉意。 BR 乔伊 Re: IPCF setup between R52_0_0 and R52_0_1 你好, PrabhanjanKopp 非常抱歉回复晚了。 经检查,您的项目已进行资源初始化,这很容易导致资源冲突,包括对已中断资源的重复初始化。请检查相关资源设置。 测试 IPCF 项目的另一种方法是使用裁剪后的 GreenVIP 程序,以避免资源初始化的同步。 希望这些信息对您有所帮助。 BR 乔伊
View full article
S32DS S32K358 プロジェクトに関するお問い合わせ wj_kwak_0-1789777426372.pngwj_kwak_0-1789777426372.png S32K358プロジェクトの作成について質問があります。 M7_0とM7_2という2つのプロジェクトが作成されている理由が気になります。 「ブートコアツールチェーンを継承する」ボタンの機能を知りたいです。 チームメイトによると、参考ドキュメントではM7_0がブートローダー領域、M7_2がアプリケーションエリアと書かれていますが、ドキュメントで確認できていません。この点について確認させてください。 Re: S32DS S32K358 Project Inquiry こんにちは、 @wj_kwak S32K358の場合、S32DSはデフォルトで2つの独立したプロジェクトを作成します。1つはM7_0用、もう1つはM7_2用です。これらのプロジェクトは2つのプロセッシングコアに対応しています。これらはブートローダー領域やアプリケーション領域を表していません。 S32DSのプロジェクト作成ウィザードは通常、両方のコアのアプリケーションを含む単一のプロジェクトを作成することはありません。そのようなプロジェクト構造が必要な場合は、手動で作成/設定する必要があります。しかし、ほとんどの場合、これは必要なく、一般的なアプローチは各コアごとに独立したプロジェクトを2つずつ使うことです。 「ブートコアツールチェーンを継承する」オプションは、ブートコアプロジェクトからツールチェーン構成を継承するために使えます。有効にすれば、ツールチェーンはCortex-M7_0_0専用に選択できます。Cortex-M7_0_2のツールチェーン選択は、Cortex-M7_0_0の設定が適用されるためグレーアウトになります。 また、ここに提供されているマルチコアの例やドキュメントも参照できます: community.nxp.com/t5/S32K/S32K324-Multi-Core-Example-Project-based-on-Whiteboard/m-p/1547771 このパッケージは両方のアプローチを示しています:各コアごとに独立したプロジェクト、そして両方のコアに対して単一のプロジェクトを単一のELFファイルにコンパイルします。 SO、M7_0とM7_2はブートローダーやアプリケーションプロジェクトとして理解すべきではありません。これらは、それぞれのコアに関連付けられたプロジェクトにすぎません。 よろしくお願いいたします。 ルーカス
View full article
IMX8ulpにおけるファルコンモード起動の問題 チームの皆さん、こんにちは。 Falconモード でボードを起動する際に問題が発生しています 。 meta-imx-fastboot レイヤーをYoctoのソースディレクトリに クローンしました 。 構築中に imx-boot やデバイスツリー に関する問題に直面しました 。カスタムDTSを使っていて、それをボードに読み込む必要があるからです。これに対処するために、machine.confのFalcon Mode引数を 次のように 設定しました: FALCON_KERNEL_DEVICETREE = "imx8ulp-custom" この設定後、 Falcon Modeの手順で説明されているとおり、 imx8ulp_no_ubootローダーを生成することができました。 fitImageを使用しています KERNEL_IMAGETYPE = "fitImage" KERNEL_CLASSES:append = " kernel-fitimage" IMAGE_BOOT_FILES = "fitImage" 次に、以下のコマンドを使用してボードにファームウェアを書き込みました。 sudo uuu -b emmc_all *.wic sudo uuu -b emmc ファームウェアの書き込み後、ボードを起動すると、起動に失敗し、以下のエラーが発生します。 U-Boot SPL 2025.04-gb9f705c183f0(2025年6月4日 09:48:20 +0000) 通常起動 ELEファームウェアバージョン2.0.2-85b63cb9 upower_apd_inst_isr: エントリ upower_init: soc_id=48 upower_init: バージョン:11.11.13 upower_init: uPower RAMサービスを開始します user_upwr_rdy_callb: soc=b user_upwr_rdy_callb: RAMバージョン:12.18 スイッチを入れる... スイッチを入れてみて、OK 記憶を起動する... メモリーをオンにして DDRの保持をクリアします... DDRの保持はクリアです 第0節:RNGのインスタンス化 MMC1からの起動を試みています パーティション1がデバイス0で無効 spl_register_fat_device:ファットレジスター err - -1 パーティション1がデバイス0で無効 spl_register_fat_device:ファットレジスター err - -1 spl_load_image_fat: error reading image u-boot-atf-container.img, err - -1 誤差:-2 SPL:すべての起動デバイスから起動に失敗 ### ERROR ### ボードをリセットしてください### このエラーの原因を理解し、Falcon Modeの起動問題を解決する方法を教えていただけませんか? Re: Falcon Mode Boot Issue in IMX8ulp こんにちは@elgin_1950  もしDTSコンテンツとdefconfigをFalconがデフォルトでサポートしているEVKコードに同期した場合、問題は起きるのでしょうか? よろしくお願いします、 志明 Re: Falcon Mode Boot Issue in IMX8ulp @Zhiming_Liuさん、返信が遅れて申し訳ありません。 FalconモードでfitImageではなく通常のカーネルイメージが使用されていたため、問題を修正しました。 しかし、 Falconモードを通してfitImageを読み込む方法はありますか?
View full article
IMX8ulp 中的猎鹰模式启动问题 大家好, 我在以 Falcon 模式 启动主板时遇到问题 。 我将meta-imx-fastboot层克隆到我的 Yocto 源代码目录中。 在构建过程中,我遇到了一些与 imx-boot 和设备树 相关的问题 ,因为我使用的是需要加载到我们开发板上的自定义 DTS。为了解决这个问题,我在 machine.conf 文件中配置了 Falcon 模式参数, 如下所示: FALCON_KERNEL_DEVICETREE = "imx8ulp-custom" 完成此配置后,我能够按照 Falcon 模式步骤中所述生成imx8ulp_no_uboot加载器。 我正在使用 fitImage KERNEL_IMAGETYPE = "fitImage" KERNEL_CLASSES:append = " kernel-fitimage" IMAGE_BOOT_FILES = "fitImage" 然后我使用以下命令对开发板进行了烧录: sudo uuu -b emmc_all *.wic sudo uuu -b emmc 刷写固件后,启动开发板时,启动失败并出现以下错误: U-Boot SPL 2025.04-gb9f705c183f0(2025年6月4日 - 09:48:20 +0000) 正常启动 ELE固件版本2.0.2-85b63cb9 upower_apd_inst_isr:入口 upower_init: soc_id=48 upower_init:版本:11.11.13 upower_init:启动 uPower RAM 服务 user_upwr_rdy_callb: soc=b user_upwr_rdy_callb:内存版本:12.18 打开开关…… 打开开关,没问题 唤醒记忆…… 打开记忆功能 清除DDR数据保留... 清除DDR数据保留正常 SEC0:RNG 实例化 尝试从 MMC1 启动 设备 0 上的分区 1 无效 spl_register_fat_device:fat 设备寄存器错误 -1 设备 0 上的分区 1 无效 spl_register_fat_device:fat 设备寄存器错误 -1 spl_load_image_fat:读取镜像 u-boot-atf-container.img 时出错,错误代码 -1 错误:-2 SPL:无法从所有引导设备启动 # ## ERROR ## # 请 RESET 该板 ### 请问您能否帮我了解一下这个错误的原因,并建议一下如何解决 Falcon 模式启动问题? Re: Falcon Mode Boot Issue in IMX8ulp 你好@elgin_1950 如果将 DTS 内容和 defconfig 同步到 Falcon 默认支持的 EVK 代码,是否还会出现任何问题? 此致, 志明 Re: Falcon Mode Boot Issue in IMX8ulp 您好@Zhiming_Liu,抱歉回复晚了。 我已经解决了这个问题,因为 Falcon 模式使用的是普通内核图像而不是fitImage 。 但是,有没有办法通过 Falcon 模式加载fitImage ?
View full article
S32DS S32K358 Project Inquiry wj_kwak_0-1789777426372.pngwj_kwak_0-1789777426372.png I have a question about creating the S32K358 project. I am curious why two projects, M7_0 and M7_2, are being created. I want to know the function of the Inherit boot core toolchain button.. My teammate says that the reference documentation states M7_0 is the bootloader area and M7_2 is the application area, but I haven't been able to verify this in the documentation. I would like to confirm this. Re: S32DS S32K358 Project Inquiry Hi @wj_kwak  For S32K358, S32DS creates two independent projects by default, one for M7_0 and one for M7_2. These projects correspond to the two processing cores. They do not represent a bootloader area and an application area. The S32DS project creation wizard does not normally create a single project containing the application for both cores. If such a project structure is required, it has to be created/configured manually. However, in most cases there is no need to do this and the typical approach is to use two independent projects, one for each core. The "Inherit boot core toolchain" option can be used to inherit the toolchain configuration from the boot-core project when creating the project for the other core. If it is enabled, you can select the toolchain only for Cortex-M7_0_0. The toolchain selection for Cortex-M7_0_2 will be greyed-out because the configuration from the Cortex-M7_0_0 will apply. You can also refer to the multicore examples and documentation provided here: community.nxp.com/t5/S32K/S32K324-Multi-Core-Example-Project-based-on-Whiteboard/m-p/1547771 The package demonstrates both approaches: independent projects for each core and a single project for both cores compiled into a single ELF file. So, M7_0 and M7_2 should not be understood as bootloader and application projects. They are simply the projects associated with the respective cores. Best regards, Lukas
View full article
S32K311引导加载程序移植 我目前正在将一个可运行的 Bootloader 项目从 S32K312 移植到 S32K311。我正在使用 S32 Design Studio、NXP RTD 4.9.0 和 GCC 编译器。我遇到了两个与矢量表和复位处理程序相关的严重问题,这些问题似乎是 S32K311 / RTD 4.9 环境特有的。 问题 1:立即使用调试器 RESET 故障 启动 PEMicro 调试器时,内核在 RESET 脚本执行期间立即崩溃,甚至在到达 main() 之前就崩溃了。 重置脚本(……)已完成。 UsageFault:执行指令时使用了无效的 EPSR.T 或 EPSR.IT 字段。 硬故障:故障已升级为硬故障。 我们检查了 startup_cm7.s和 Vector_Table.s。我们注意到 Reset_Handler 缺少 .type。Reset_Handler 的 %function 指令导致 ELF 入口点为偶数地址(例如,0x00402420 而不是 0x00402421),这自然会导致 Cortex-M7 上出现 ARM 模式 UsageFault。 即使在修复了 .type 指令并确保向量表已为 Thumb 模式设置了 LSB 之后,PEMicro 调试器仍然偶尔会在复位后立即抛出此 UsageFault。 问题 2:中断跳转到 0x0(未初始化的 RAM 向量表)当我们成功绕过复位问题并到达 main() 时,一旦硬件中断(如 FlexCAN 或 SWT)触发,系统就会崩溃。PC跳转到0x00000000。 在检查内存时,我们发现 __interrupts_ram_start (0x20000000) 处的 RAM 向量表完全未初始化(填充为零)。我们发现: startup_cm7.s在初始化结束时将 VTOR 设置为 __RAM_INTERRUPT_START,但从未从 ROM 复制该表。 IntCtrl_Ip_Init(&IntCtrlConfig_0)(由平台元器件生成)在启用 INT_CTRL_IP_ENABLE_VTOR_CONFIG 时设置 VTOR,但它也不会将默认向量表从闪存复制到 RAM。 为了解决这个问题,我们不得不在 main.c 中编写一个手动 for 循环,将向量表从 __interrupts_init_start 物理复制到 __interrupts_ram_start,并在调用 IntCtrl_Ip_InstallHandler() 之前更新 S32_SCB->VTOR。 基础代码来自统一引导加载程序演示 有人知道哪里有移植并发布了适用于带 CAN 总线的 S32K311 的引导加载程序吗? Re: S32K311 bootloader porting 你好@ujwal12 对于 Cortex-M7,向量表中的复位处理程序条目必须通过使用 LSB 已设置的地址来指示 Thumb 模式。如果 Reset_Handler 符号没有正确生成为函数符号,链接器可能会在向量表中放置偶数地址,这可能会导致启动期间出现 UsageFault。因此,我们通常不建议修改 startup_cm7.s 文件。或 Vector_Table.s。 S32K3 RTD 采用基于 RAM 的可重定位中断向量表设计。启动时,向量表从闪存复制到 RAM,并且 VTOR 更新为指向基于 RAM 的表。 关于 S32K311 引导加载程序示例的可用性,目前还没有专门针对 S32K311 的官方引导加载程序示例。最接近的参考资料是Example S32K312 Bootloader to Application Jump DS3.5 RTD300和您已经在使用的 Unified Bootloader Demo。 另外请注意,统一引导加载程序是 NXP 的非官方演示程序,仅发布在社区论坛上,因此 NXP 技术支持不提供任何支持。 BR,VaneB
View full article