Multi Source Translation Content

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multi Source Translation Content

讨论

排序依据:
S32G274 baremetal code I want to use a bare-metal program on the S32G274 development board, including bare-metal drivers for modules such as powering up the A53 processor, LINFlexD serial port, and Ethernet. I would like it to run successfully right out of the box. The drivers generated by S32DS only include processor power-up functionality. I have attempted to implement the LINFlexD serial port myself (enabling pins, enabling clocks, initializing the serial interface), but I'm unclear about how to properly handle clock enablement. I hope you can provide me with a ready-to-use bare-metal program that can be directly compiled in S32DS. Re: S32G274 baremetal code Hello, @Tatu_dd  Thanks for your post. 1. NXP's software enablement strategy for S32G274A positions the A53 cores primarily for Linux BSP operation rather than bare-metal development. The S32 Design Studio 3.6.8 examples for A53 cores are intentionally limited to boot/startup code, as the intended use case involves running a full Linux distribution on these cores. chenyin_h_0-1783303897346.png 2. For bare-metal A53 development, there are not much reference code released, there is only a demo existed, but it is not pure bare metal code on A53, but a heterogenous implementation instead chenyin_h_1-1783304026380.png As a result, you may have to implement or port the existing Linux driver or RTD driver according to your requirement, sorry that there is no directly formal examples/software releases provisioned by NXP.   BR Chenyin
查看全文
MBDT FOR S32K1XX MEIDEI_0-1783149479446.png 请问为什么这种配置会导致消息无法成功发送?是否需要其他模块? Re: MBDT FOR S32K1XX 你好, 你用的是什么主板?如果您使用的是 S32K146 评估板,请注意连接到 microUSB 的 UART 实例实际上是 LPUART1。如果您使用的是外部串行变流器,请检查电路板的原理图,确认它是否实际连接到 LPUART0(您在模型中配置的实例)。 您可以查看工具箱中包含的示例,了解如何配置和使用不同的外围设备。 您可以查看 S32K146 的快速入门指南,了解其上最重要的连接器概览: S32K146 通用评估板入门指南 此致, 索林·班西拉。
查看全文
激活码过渡 项目描述S32 Design Studio for ARM v2018 订单号S32-DS-ARM_v2018_169264627 您能帮我延长许可证的有效吗?激活码EBF4-DE52-80C0-FD65非常感谢。 Re: 激活码过期 你好, 您的S32DS许可证已延期。
查看全文
激活码过期 tem DescriptionS32 Design Studio for ARM v2018 Order NumberS32-DS-ARM_v2018_169264627 您能帮我延长许可证的有效期吗? 激活码EBF4-DE52-80C0-FD65 非常感谢。 Re: 激活码过期 Hi,  your S32DS license has been extended. 
查看全文
MBDT FOR S32K1XX MEIDEI_0-1783149479446.png Could you please explain why this configuration prevents the message from being sent successfully? Is there a need for additional modules? Re: MBDT FOR S32K1XX Hello, What board are you using? If you are using the S32K146 evaluation board, please note that the UART instance connected to the microUSB is actually LPUART1. If you are using an external serial converter, please check the schematic for the board to see that it is actually connected to LPUART0 (the instance you configured in the model). You might want to check included examples in the toolbox to see how to configure and use different peripherals. You can check the Quick Start Guide for S32K146 to have an overview of the most important connectors found on it: Getting Started with the S32K146 Evaluation Board for General Purpose  Best regards, Sorin Bancila.
查看全文
S32G274 ベアメタルコード S32G274の開発ボード上でベアメタルプログラムを使いたいと思っています。A53プロセッサの電源供給、LINFlexDシリアルポート、イーサネットなどのモジュール用のベアメタルドライバも含めて。箱から出してすぐに正常に動作させたいです。S32DSで生成されるドライバには、プロセッサの電源アップ機能のみが含まれています。 自分でLINFlexDシリアルポートの実装(ピンの有効化、クロックの有効化、シリアルインターフェースの初期化)を試みましたが、クロックの有効化の適切な扱い方がよくわかりません。 S32DSで直接コンパイルできる、すぐに使えるベアメタルプログラムを提供していただければ幸いです。 Re: S32G274 baremetal code こんにちは、 @Tatu_dd 投稿ありがとうございます。 1. NXPのソフトウェア支援S32G274A戦略では、A53コアは主にベアメタル開発ではなくLinux BSP運用に割り当てられています。A53コア向けのS32 Design Studio 3.6.8の例は、意図的に起動/起動コードに限定されており、意図された使用ケースはこれらのコア上で完全なLinuxディストリビューションを実行することが目的です。 chenyin_h_0-1783303897346.png 2. ベアメタルA53開発に関しては、公開されているリファレンスコードはほとんどなく、デモは存在するものの、それはA53上の純粋なベアメタルコードではなく、異種実装である。 chenyin_h_1-1783304026380.png そのため、既存のLinuxドライバやRTDドライバを必要に応じて実装または移植する必要があるかもしれません。申し訳ありませんが、NXPによる直接的な例やソフトウェアリリースは提供されていません。 BR チェイン
查看全文
S32K344芯片,在SPD中添加eMCEM_1模块后,使用引导加载程序下载失败。 理清逻辑并重写:正如标题所示,当我在应用程序代码中启用 eMCEM_1 时,使用官方引导加载程序下载应用程序失败。如果我不擦除芯片,我就无法再次进入启动状态,即使重新启动也无法解决问题。我怀疑重新启动后,启动程序跳转到了应用程序,但应用程序没有运行。禁用 eMCEM_1 后,此问题不会出现。启用 eMCEM_1 后,如何使用启动 来刷写应用程序? Re: S32K344 chip, failed to download using bootloader after adding eMCEM_1 module in spd 嗨@XPW , 问题描述不够清晰。 如果应用程序是通过引导加载程序进行编程的,则应用程序中包含的 eMCEM_1 配置不应影响编程过程本身,因为应用程序在下载期间不会执行,它只是一个二进制文件。 只有在引导加载程序将执行权移交给应用程序之后,与 eMCEM/FCCU 相关的配置才会变得重要,此时检查以下内容会很有帮助: FCCU状态登记册 DCM 标志,MC_RGM 标志。 或者应用程序是否真的执行到了 main() 函数。 根据目前的描述,尚不清楚是编程操作失败,还是编程成功但问题在应用程序开始执行后才出现。 您能详细说明一下事件的具体顺序吗? 此致, 丹尼尔 Re: S32K344 chip, failed to download using bootloader after adding eMCEM_1 module in spd 经过调查,我发现启用 时,一些全局变量没有按定义进行初始化 。 请选择部分进行解释: 首先,当我没有启用目标时 XPW_0-1783494597992.png RTD 文件中的 Clock_ip.c 文件 XPW_1-1783494731850.png XPW_2-1783494792174.png 电源IP。c 在 RTD 文件下 XPW_3-1783494883662.png XPW_4-1783494909192.png 可以正确初始化。 但是,当我激活它时: XPW_5-1783495188492.png XPW_6-1783495223242.png RTD 文件中的 Clock_ip.c 文件 XPW_7-1783495794585.png XPW_8-1783495823066.png RTD 文件中的 Power_ip.c XPW_9-1783495866324.png XPW_10-1783495886502.png 全局变量初始化失败。 请问是否有更好的解决方案? Re: S32K344 chip, failed to download using bootloader after adding eMCEM_1 module in spd 嗨@XPW , 根据截图来看,变量最初初始化是正确的。但是,在 eMCEM 初始化之后,Clock_Ip_pfkNotificationsCallback 包含一个无效指针。 eMCEM 并不会神奇地改变指针值。这看起来更像是以下几种问题之一: 启动初始化(.data 副本 / .bss)初始化)未正确完成。 在 main() 函数之前发生 RAM 损坏。 连接段重叠。 堆栈损坏。 您能否使用 SPD 演示项目中的链接器文件进行测试? BR,丹尼尔 Re: S32K344 chip, failed to download using bootloader after adding eMCEM_1 module in spd 链接文件已修改如下。 XPW_0-1783992772039.png XPW_1-1783993101988.png 我定义了三个全局变量: XPW_2-1783993317537.png 我发现当未启用 时,执行init_data-bss后, XPW_3-1783993342206.png XPW_4-1783993406406.png 它似乎已按 4 字节对齐并正确赋值。 但是当我启用 后,执行init_data-bss后 XPW_5-1783994068084.png XPW_6-1783994226472.png 它似乎没有对齐。 Re: S32K344 chip, failed to download using bootloader after adding eMCEM_1 module in spd 这种现象的原因是什么?我应该如何调查和解决它? Re: S32K344 chip, failed to download using bootloader after adding eMCEM_1 module in spd 嗨@XPW , 根据截图来看,我并不认为变量初始化本身存在问题。variable_a 是一个 8 位变量,启用 eMCEM 会引入其他变量,这可能会改变 .data 的布局。部分。因此,看到变量处于不同的偏移量是正常的,这本身并不表示存在数据损坏。 我认为关键问题是,当应用程序独立组网 \\(SA\\)时会出现此问题,还是只有在通过引导加载程序编程和启动时才会出现此问题。 能否在不使用引导加载程序的情况下,直接使用调试器对应用程序进行编程并运行该程序,从而重现该问题?如果问题仅在通过引导加载程序加载应用程序后出现,则调查应集中在引导加载程序编程过程、映像布局或引导加载程序交接上,而不是应用程序本身。 BR,丹尼尔
查看全文
TEF82xx Low Level Drivers build issue Hi,  I'm trying to build the TEF82xx API Low Level Drivers RFP9.3.0 20240920_PROD to run the included examples and have an issue: Cannot find source file: src/plf_sys.c And this file is really missing. Like some others (plf_cap.c, plf_crc.c, plf_hio.c, etc) required by the bc_api\bc_api_src\plf\CMakeLists.txt. Where can I find these files? Re: TEF82xx Low Level Drivers build issue Hello, Yes, you are right. I do not see that file in the TEF82xx API Low Level Drivers RFP9.3.0 20240920_PROD.zip package. It must be from other packages. Name plf_sys.c points to the platform - most probably driver expects it is coming from OS. From TEF82xx API Low Level Drivers RFP9.3.0 20240920_PROD\TEF82xx_API_RN_V9.3.0.pdf petervlna_0-1783494576622.png I have found no further information in the documentation. Best regards, Peter Re: TEF82xx Low Level Drivers build issue Hello, Yes, you are right. I do not see that file in the TEF82xx API Low Level Drivers RFP9.3.0 20240920_PROD.zip package. It must be from other packages. Name plf_sys.c points to the platform - most probably driver expects it is coming from OS. From TEF82xx API Low Level Drivers RFP9.3.0 20240920_PROD\TEF82xx_API_RN_V9.3.0.pdf petervlna_0-1783494576622.png I have found no further information in the documentation. Best regards, Peter
查看全文
Is there a simple 8 bit microcontroller/assembly language that is nice to work with? I'm searching for an 8 bit microcontroller where I can look at the actual hex/binary code. I've been learning 8051 assembly in university and I absolutely love seeing and understand every single instruction and value in the memory. But those microcontrollers are antiquated and need a bunch of "hacks" for compatibility. At least that's what it feels like everytime I put my code onto real hardware. So is there a simple 8 bit assembly language with actual chips I can program simple electronics projects with ? Re: Is there a simple 8 bit microcontroller/assembly language that is nice to work with? Hello, NXP has  catalog for 8 Bit devices, you could use S08SG|8-bit Small Package SG MCUs | NXP Semiconductors devices, S08SG family is an entry-level to mid-range device with general features. S08SG devices are included in the CodeWarrior Tool. The CodeWarrior tool version 11.1, is supported in windows 11, this tool supports different connections [P&E USB Multilink Universal / USB Multilink, P&E Cyclone, Open Source BDM, P&E Full chip simulation] You can download the tool from this link: CodeWarrior® for MCUs (Eclipse IDE) v11.1 In the CW tool when enter debug, there is a section for  Disassembly view that shows the loaded program as assembly language instructions mixed with source code for comparison. Best Regards, Luis Re: Is there a simple 8 bit microcontroller/assembly language that is nice to work with? Here are some of the 8-bit controllers you can also explore pic16lf18326-i-sl/2263047  PIC16LF18326-I/SL BY MICROCHIP IS A 14-PIN 8-BIT MICROCONTROLLER WITH 16KB FLASH 1KB RAM 12-BIT ADC 10 PWM CHANNELS I2C SPI UART INTERFACES LOW POWER CONSUMPTION AND OPERATING VOLTAGE OF 2.3V TO 5.5V. atmega8l-8mu/258363  ATMEGA8L-8MU by MICROCHIP is an 8-bit AVR microcontroller with 8MHz frequency, 8KB Flash, 32-pin VQFN, I2C, SPI, UART interfaces, operating at 2.7V-5.5V, and -40°C to 85°C temperature range.
查看全文
The S32K344 development board cannot be flashed using OpenSDA. The S32K344 development board cannot be flashed using OpenSDA. djaylou_3-1783083734014.png djaylou_2-1783083701367.png Re: The S32K344 development board cannot be flashed using OpenSDA. Hi @djaylou  Which board are you currently using: FRDM-A-S32K344, S32K3X4EVB-T172, or S32K344-WB? Also, can you confirm that the device is being powered correctly? BR, VaneB
查看全文
RD33772C14VEVMボード上のCAN通信の確認に助けが必要です こんにちは、 私の名前はチャン・ヘウンです。 現在、RD33772C14VEVMボードのテストを行っており、以下のように環境をセットアップしました。 ソフトウェア: BMS 1.2.0用MBDT + S32K3xx 1.4.3用MBDT (最初にバージョン1.4.0をインストールし、その後1.4.3のパッチを適用しました。) モデル: BMSのMBDT→ BMS_Examples →rd33772c14vevm → rd33772c14vevm_s32ct → rd33772c14vevm_s32ct.mdl ハードウェア: ハードウェアは添付写真のように接続されています。 今のところ、まずモデルの基本的な動作を確認したいので、バッテリーは接続していません。基板には12Vの電源のみを供給しています。 上記の環境を設定した後、モデルをボードにダウンロードしようとしましたが、ダウンロード過程で「ターゲットに接続できません」と表示されます。 そこで生成されたコードをS32 Design Studio 3.5にインポートし、そこからダウンロードしようとしました。S32DSでは、ビルドプロセスが正常に完了します。 そこで、ボードをVector CANalyzerに接続し、CANメッセージが基板から送信されていないか確認しました。しかし、CANalyzerにはCANメッセージが表示されません。 問題の原因がJ-Linkデバッガにある可能性を疑ったため、TRACE32を使用してボードを接続することも試してみました。しかし、リセットインジケーターが繰り返し赤色に点灯し、TRACE32には「ターゲット電源障害」というエラーメッセージが表示されます。 現時点では、CANメッセージが送信されていないか確認してボードが正常に動作しているか確認したいだけです。 この問題をぜひ解決したいと思っています。 もし確認すべき項目があれば、ぜひ教えていただけるとありがたいです。あなたの指示に従い、各ステップを試してみます。 この問題を解決するために何をすべきかアドバイスをいただけますか? #rd33772c14vevm、#CAN、#s32k344、#JTAG、#MBDT Re: Need help verifying CAN communication on the RD33772C14VEVM board こんにちは、 まず、返信が遅くなり申し訳ありません。 お送りいただいたメッセージから判断すると、基板に正しく電源が供給されていないのではないかと推測されます。S32DSでアプリケーションを構築したようですが、ビルドプロセスではアプリケーションをボードにデプロイする必要がありません。S32K344に対応したデバッグ構成を作成し、.elfファイルをデプロイする必要があります。そこから。 まだバッテリーを接続していないので、EVBにある頑丈なネジではなく、セルエミュレーターからボードに電源を供給することをお勧めします。シャント抵抗(R62)で基板に電力を供給できるかはわかりませんので、回路図をしっかり確認してください。 モデルのREADMEには、エミュレーターボードから電源を入れられると書かれています: エミュレータボードに電源を接続します:12V → BH1(K30_12V_L)、GND → BH2(GND_KL31_DOWN) これで問題が解決するかどうか教えてください。 よろしくお願いします、 ソリン・バンシラ
查看全文
S32K358 MBDT参照モデルビルド失敗 こんにちは、 私はMATLAB R2024bとNXP MBDT for S32K358を使用しています。 私はハードウェア(10Hz CAN Tx/Rx)上で正しくビルド、フラッシュ、動作するスタンドアロンのNXP CAN通信モデルを持っています。 また、参照モデル、ステートマシン、推定器、故障マネジメントロジックを含む別のBMSアルゴリズムモデル(Offline_Test)も持っています。 BMSアルゴリズムを動作中のNXPモデルに統合してビルドすると、MBDTは参照モデル(BMS_Out_Config)用の別の設定フォルダを生成し、以下で失敗します: 致命的なエラー: Mcl.h:そのようなファイル、又はディレクトリはありません #include エラーの原因は次のとおりです。 コントローラー/BMS_Out_Config/src/mbdt_board_init.c Mcl.h は、以下の環境では生成されません。 コントローラ/BMS_Out_Config/RTD/インクルーブ 私の質問は次のとおりです。 アルゴリズムのみ参照されたモデルには、独自のハードウェア構成やRTD生成が必要でしょうか? それとも最上位のハードウェアモデル構成を引き継ぐべきでしょうか? 既存のS32K3ハードウェアプロジェクトに大規模なアルゴリズム参照モデルを統合するための推奨ワークフローはありますか? 動作中のNXPモデル、BMSアルゴリズムモデル、ビルドエラーのスクリーンショットを添付します。 ありがとうございます。
查看全文
S32K344 开发板无法使用 OpenSDA 进行固件烧录。 S32K344 开发板无法使用 OpenSDA 进行固件烧录。 djaylou_3-1783083734014.png djaylou_2-1783083701367.png Re: The S32K344 development board cannot be flashed using OpenSDA. 嗨@djaylou 您目前使用的是哪款主板:FRDM-A-S32K344、S32K3X4EVB-T172 还是 S32K344-WB?另外,您能否确认设备已正常通电? BR,VaneB
查看全文
S32K358 MBDT 参考模型构建失败 您好, 我正在使用 MATLAB R2024b 和 NXP MBDT 开发 S32K358 模块。 我有一个独立的 NXP CAN 通信模型,它可以在硬件上正确构建、烧录和运行(10 Hz CAN Tx/Rx)。 我还有一个单独的电池管理系统算法模型(离线测试),其中包含参考模型、状态机、估计器和故障管理逻辑。 当我将 BMS 算法集成到 NXP 工作模型中并构建时,MBDT 会为引用的模型生成一个单独的配置文件夹 (BMS_Out_Config),并出现以下错误: 致命错误:Mcl.h:没有这样的文件或目录 #include 错误源自: Controller/BMS_Out_Config/src/mbdt_board_init.c Mcl.h 文件未在以下情况下生成: Controller/BMS_Out_Config/RTD/include 我的问题是: 仅算法参考模型是否应该有自己的硬件配置/RTD生成机制? 或者它们应该继承顶层硬件型号配置? 对于将大型算法参考模型集成到现有的 S32K3 硬件项目中,是否有推荐的工作流程? 附件中包含 NXP 工作模型、电池管理系统算法模型和版本错误的屏幕截图。 谢谢。
查看全文
TEF82xx 底层驱动程序构建问题 你好, 我正在尝试版本 TEF82xx API 底层驱动程序 RFP9.3.0 20240920_PROD 以运行其中包含的示例,但遇到了问题: 找不到源文件:src/plf_sys.c 这个文件确实丢失了。与其他一些文件(plf_cap.c,plf_crc.c,plf_hio.c,等等)bc_api\bc_api_src\plf\CMakeLists.txt 所要求的。我可以在哪里找到这些文件? Re: TEF82xx Low Level Drivers build issue 你好, 是的你是对的。我在 TEF82xx API 底层驱动程序 RFP9.3.0 20240920_PROD.zip 软件包中没有看到该文件。 肯定是从其他代码包,软件包里拿出来的。名称plf_sys.c指向平台——驱动程序很可能期望它来自操作系统。 摘自 TEF82xx API 底层驱动程序 RFP9.3.0 20240920_PROD\TEF82xx_API_RN_V9.3.0.pdf petervlna_0-1783494576622.png 我在文档中没有找到更多信息。 顺祝商祺! Peter Re: TEF82xx Low Level Drivers build issue 你好, 是的你是对的。我在 TEF82xx API 底层驱动程序 RFP9.3.0 20240920_PROD.zip 软件包中没有看到该文件。 肯定是从其他代码包,软件包里拿出来的。名称plf_sys.c指向平台——驱动程序很可能期望它来自操作系统。 摘自 TEF82xx API 底层驱动程序 RFP9.3.0 20240920_PROD\TEF82xx_API_RN_V9.3.0.pdf petervlna_0-1783494576622.png 我在文档中没有找到更多信息。 顺祝商祺! Peter
查看全文
IMX95LPD5EVK-19CM: UUU eMMC flash of L6.18.2 fails (LIBUSB errors on Linux and Windows) Hello NXP team, I need help upgrading IMX95LPD5EVK-19CM from the factory BSP to LF_v6.18.2-1.0.0 for eIQ Neutron NPU YOLO inference. UUU eMMC flashing fails on both Linux and Windows with different libusb errors at SDPS:boot. Details below. --- ## 1. Hardware | Item | Detail | |------|--------| | Board | IMX95LPD5EVK-19CM (i.MX 95 19×19 EVK, SOM + baseboard) | | Yocto machine / hostname | imx95-a1-19x19-lpddr5-evk | | Silicon | i.MX 95 A1 | | Storage | 64 GB eMMC (factory pre-flashed Linux) | | Power | 12 V on J5, SW4 ON | | Debug | J31 USB-C → host (serial, 115200) | | Flash port | J8 USB1 OTG USB-C → host | | Camera | Logitech C920 on J7 (/dev/video13) | --- ## 2. Software versions ### Current (factory eMMC — Linux boots normally) | Component | Version | |-----------|---------| | BSP | LF6.12.34_2.1.0 | | Kernel | 6.12.34-lts-next-gbe78e49cb433 | | Boot cmdline | root=/dev/mmcblk0p2 | | Neutron delegate | v1.0.0-be8bf399 | | libneutron_delegate.so | /usr/lib/libneutron_delegate.so | | Host converter (old) | eIQ Toolkit 1.17 / neutron-converter 2.1.3 | ### Target (downloaded, not yet flashed to eMMC) | Component | Version / file | |-----------|----------------| | BSP release | LF_v6.18.2-1.0.0 (SCR-6.18.2-1.0.0) | | Kernel (expected) | 6.18.2-1.0.0 | | Image package | LF_v6.18.2-1.0.0_images_IMX95 | | Boot image | imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all | | Rootfs | imx-image-full-imx95evk.wic (~11 GB) | | Neutron delegate (expected) | v1.0.0-7399a58e | | Host converter (ready on host) | eIQ Neutron SDK 3.0.1 (converter 3.0.1+0Xd5d7918e) | Reference: NXP forum engineer (Zhiming_Liu) validated YOLOv8m on i.MX95 with L6.18.2 + eIQ Neutron SDK 3.0.1 + delegate 7399a58e. --- ## 3. Application goal USB webcam person detection with YOLO (v8n / v11n) using: - INT8 TFLite export (Ultralytics) - neutron-converter --target imx95 - tflite_runtime + libneutron_delegate.so on board On current BSP (6.12.34): - NXP forum yolov8m_full_integer_quant_converted.tflite → SEGFAULT on NPU invoke (exit 139) - Custom yolov8n_neutron.tflite → invoke OK but 0 person detections - Headless backbone on NPU → constant garbage output (~1.13); CPU split pipeline works (56–90% detections) Conclusion: need L6.18.2 BSP on eMMC before NPU models converted with SDK 3.0.1 can be validated. --- ## 4. Host setup | Host | UUU version | Path | |------|-------------|------| | Ubuntu 24.04 (x86_64) | libuuu_1.5.243-0-g230f1b1 | /usr/local/bin/uuu | | Windows 10/11 | libuuu_1.5.243-0-g230f1b1 | uuu.exe (from mfgtools uuu_1.5.243 release) | Image directory on both hosts: LF_v6.18.2-1.0.0_images_IMX95 --- ## 5. Boot switch SW7 (per IMX95LPD5EVK-19CM QSG, 1=ON 0=OFF) | Mode | SW7-1 | SW7-2 | SW7-3 | SW7-4 | |------|-------|-------|-------|-------| | Serial Download (UUU) | 1 | 0 | 0 | 1 | | eMMC boot (normal) | 1 | 0 | 1 | 0 | eMMC boot (SW7=1010) works normally. Full power cycle performed before each SW7 change. --- ## 6. Flash procedure (eMMC via UUU) Board preparation (same for Linux and Windows): - SW7 = 1001 (Serial Download) - J8 (USB1 OTG) connected to host PC (not J31) - J31 connected for optional serial console - J5 12 V power connected - Board powered ON when uuu displays "Wait for Known USB Device" Command: uuu -b emmc_all imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all imx-image-full-imx95evk.wic (Linux: sudo uuu ... | Windows: uuu.exe ... from image directory) --- ## 7. UUU errors — Linux (Ubuntu 24.04) sudo /usr/local/bin/uuu -b emmc_all \ imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all \ imx-image-full-imx95evk.wic Output: uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.243-0-g230f1b1 Success 0 Failure 1 1:6-E3C50910 1/1 [HID(W): LIBUSB_ERROR_NO_DEVICE (-4)] SDPS: boot -scanterm -f imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all ... Notes: - lsusb briefly shows NXP USB device (1fc9:015d) in SDP mode - uuu sometimes prints "New USB Device Attached" then fails at SDPS: boot - Without sudo: permission denied (errno=13) - eMMC was not modified (flash did not complete) --- ## 8. UUU errors — Windows Host: Windows 10/11, PowerShell, uuu.exe 1.5.243 Working directory: C:\Users\Hardware.Team\Downloads\LF_v6.18.2-1.0.0_images_IMX95 ### Attempt — flash_all (expected correct boot image) PS C:\Users\Hardware.Team\Downloads\LF_v6.18.2-1.0.0_images_IMX95> & '..\uuu (2).exe' -b emmc_all imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all imx-image-full-imx95evk.wic uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.243-0-g230f1b1 Success 0 Failure 1 1:3-E3C50910 1/1 [HID(W): LIBUSB_ERROR_PIPE (-9)] SDPS: boot -scanterm -f imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all ... Summary of USB errors across hosts: | Host | Boot image | libusb error | |------|------------|--------------| | Ubuntu 24.04 | flash_all | LIBUSB_ERROR_NO_DEVICE (-4) | | Windows | flash_all | LIBUSB_ERROR_PIPE (-9) | All failures occur at the same step: SDPS: boot (before eMMC write progress). --- ## 9. What works today - SW7=1010 → boots factory eMMC Linux (6.12.34) normally - SSH over eth0 works - USB webcam (/dev/video13) detected - libneutron_delegate.so present (be8bf399) - CPU-side inference validated; NPU output incorrect on current BSP --- ## 10. Questions for NXP 1. For SDPS:boot failures with uuu 1.5.243 on IMX95LPD5EVK-19CM (A1), device 1fc9:015d, SW7=1001, J8 — what causes LIBUSB_ERROR_NO_DEVICE (-4) on Linux vs LIBUSB_ERROR_PIPE (-9) / LIBUSB_ERROR_IO (-1) on Windows? 2. Are there known uuu 1.5.243 + IMX95 A1 compatibility requirements (driver, WinUSB/Zadig on Windows, udev rules on Linux)? 3. Confirm imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all + imx-image-full-imx95evk.wic is the correct pair for IMX95LPD5EVK-19CM eMMC flash (not sd-ecc unless ECC RAM). 4. Any known Neutron delegate differences between be8bf399 (6.12.34) and 7399a58e (6.18.2) affecting YOLOv8 INT8 models? 5. Is there an alternative supported method to flash L6.18.2 to eMMC if UUU USB path fails on both Linux and Windows? --- ## 11. Logs available on request - Full uuu verbose log: uuu -v -b emmc_all ... (Linux and Windows) - Host lsusb / Device Manager / dmesg when board enters SDP mode - Serial console log (factory eMMC boot — working) - Board: uname -r, strings libneutron_delegate.so, NPU test results on 6.12.34 Thank you for guidance on completing the eMMC upgrade to L6.18.2-1.0.0 for Neutron NPU development. Best regards Re: IMX95LPD5EVK-19CM: UUU eMMC flash of L6.18.2 fails (LIBUSB errors on Linux and Windows) The A1 silicon of the i.MX 95 is no longer supported from our latest BSPs, 6.12.34 seems to be last one supporting A1. There is no workaround, you can't make the latest BSP work on A1 silicon, you need to upgrade your EVK with a new daughter card. The A1 silicon card is blue, the B0 silicon card is green. I didn't test a UUU download onto an old EVK using the 6.18.2 .wic image, but I expect that it fails the same way as it fails on your side. I'll do this in the next days. You could do a test with an SD-Card, program the .wic image on your PC to an SD-Card and try to run it on your EVK with boot mode set to SD-Card. Regards, Bernhard. Re: IMX95LPD5EVK-19CM: UUU eMMC flash of L6.18.2 fails (LIBUSB errors on Linux and Windows) Hello, Thanks for response. i have another query regrading same board. I am trying to run an M7 application on IMX95LPD5EVK-19 following AN14748, but I cannot flash flash.bin with UUU. The board is detected briefly, then SDPS boot fails immediately. Hardware: IMX95LPD5BB-19 REV A1 (2024 NXP B.V.) Boot switch (SW7[1:4]): 1001 (Serial Download) Target: eMMC Host: Ubuntu Linux UUU: libuuu_1.5.243-0-g230f1b1 SDKs tried (MCUXpresso SDK Builder): SDK_26.06.00_IMX95LPD5EVK-19 SDK_2.15.000_IMX95LPD5EVK-19 Both produce the same result. Command: cd IMX95LPD5EVK/build_/tmp/deploy/images/imx95-a1-19x19-lpddr5-evk sudo uuu -b emmc flash.bin   Error: Success 0 Failure 1 1:2-E3C50910 1/ 1 [HID(W): LIBUSB_ERROR_NO_DEVICE (-4)] SDPS: boot -f flash.bin   Steps followed (per AN14748): Set SW7 = 1001 with board powered off Connect USB to host Run sudo uuu -b emmc flash.bin Power-cycle board Fails at SDPS boot every time Questions: Which MCUXpresso SDK version is validated for IMX95LPD5BB-19 REV A1 M7 flashing? Is build target imx95-a1-19x19-lpddr5-evk correct for this hardware? Any known UUU issues or extra steps beyond AN14748 for this board revision? Should I use -b emmc or -b sd first, and which USB port should be used?
查看全文
S32K344 chip, failed to download using bootloader after adding eMCEM_1 module in spd Sort out the logic and rewrite: As the title suggests, when I enabled eMCEM_1 in the app code, downloading the app using the official bootloader failed. If I didn't erase the chip, I couldn't enter the boot again, and even after powering it back on, it wouldn't solve the problem. I suspect that after powering it back on, the boot jumped to the app, but the app didn't run. When I disable eMCEM_1, this issue does not occur. How can I use boot to flash the app when eMCEM_1 is enabled Re: S32K344 chip, failed to download using bootloader after adding eMCEM_1 module in spd Hi @XPW, The problem description is not entirely clear. If the application is being programmed through the bootloader, the eMCEM_1 configuration contained in the application should not affect the programming process itself, since the application is not executed during download, it is just a binary. Only after the bootloader transfers execution to the application would eMCEM/FCCU-related configuration become relevant, and at that point, it would be useful to check: FCCU status registers DCM flags, MC_RGM flags. Or whether the application actually reaches main() Based on the current description, it is unclear whether the programming operation fails, or whether programming succeeds and the issue occurs later when the application starts executing. Could you clarify the exact sequence of events? Regards, Daniel Re: S32K344 chip, failed to download using bootloader after adding eMCEM_1 module in spd After my investigation, I found that some global variables were not initialized as defined when was enabled 。 Select a portion for explanation: Firstly, when I haven't enabled the target XPW_0-1783494597992.png Clock_ip. c under RTD file XPW_1-1783494731850.png XPW_2-1783494792174.png Power_ip. c under RTD file XPW_3-1783494883662.png XPW_4-1783494909192.png Can initialize correctly。 However, when I activated it: XPW_5-1783495188492.png XPW_6-1783495223242.png Clock_ip. c under RTD file XPW_7-1783495794585.png XPW_8-1783495823066.png Power_ip. c under RTD file XPW_9-1783495866324.png XPW_10-1783495886502.png Global variable initialization failed。 May I ask if there is a better solution? Re: S32K344 chip, failed to download using bootloader after adding eMCEM_1 module in spd Hi @XPW, Based on what I see in the screenshots, the variables are initialized correctly at first. However, after the eMCEM initialization, Clock_Ip_pfkNotificationsCallback contains an invalid pointer. eMCEM does not magically change the pointer value. This looks much more like one of the following issues: Startup initialization (.data copy / .bss initialization) is not completed correctly. RAM corruption occurs before main(). Linker sections overlap. Stack corruption. Can you test it with the linker file from the SPD demo project? BR, Daniel Re: S32K344 chip, failed to download using bootloader after adding eMCEM_1 module in spd The link file has been modified for the following. XPW_0-1783992772039.png XPW_1-1783993101988.png I have defined three global variables: XPW_2-1783993317537.png I found that when is not enabled, after executing init_data-bss, XPW_3-1783993342206.png XPW_4-1783993406406.png It seems to be aligned with 4 bytes and assigned correctly. But when I enable , after executing init_data-bss XPW_5-1783994068084.png XPW_6-1783994226472.png It doesn't seem to be aligned. Re: S32K344 chip, failed to download using bootloader after adding eMCEM_1 module in spd What is the cause of this phenomenon and how should I investigate and solve it. Re: S32K344 chip, failed to download using bootloader after adding eMCEM_1 module in spd HI @XPW, Based on the screenshots, I am not convinced there is actually a problem with the variable initialization itself. variable_a is an 8-bit variable, and enabling eMCEM will introduce additional variables, which can change the layout of the .data section. Therefore, seeing the variables at different offsets is expected and does not by itself indicate corruption. I think the key question is whether the issue occurs when the application is run standalone, or only when it is programmed and started through the bootloader. Can you reproduce the issue when programming the application directly with the debugger and running it without the bootloader? If the problem only occurs after loading the application through the bootloader, then the investigation should focus on the bootloader programming process, image layout, or bootloader handover rather than the application itself. BR, Daniel
查看全文
Need help verifying CAN communication on the RD33772C14VEVM board Hello, My name is Hyewoon Jang. I am currently trying to test the RD33772C14VEVM board, and I have set up my environment as follows: Software: MBDT for BMS 1.2.0 + MBDT for S32K3xx 1.4.3 (I installed version 1.4.0 first and then applied the 1.4.3 patch.) Model: MBDT for BMS → BMS_Examples → rd33772c14vevm → rd33772c14vevm_s32ct → rd33772c14vevm_s32ct.mdl Hardware: The hardware is connected as shown in the attached photo. For now, I have not connected a battery, since I would like to check the basic operation of the model first. I am only supplying 12 V power to the board. After setting up the environment as described above, I tried to download the model to the board, but the download process shows “Could not connect to target.” Therefore, I imported the generated code into S32 Design Studio 3.5 and tried to download it from there. In S32DS, the build process completes successfully. Therefore, I connected the board to Vector CANalyzer in order to check whether any CAN messages are being transmitted from the board. However, no CAN messages are displayed in CANalyzer. Since I suspected that the issue might be related to the J-Link debugger, I also tried connecting the board using TRACE32. However, the reset indicator repeatedly turns red, and TRACE32 shows the error message “target power fail.” At this point, I simply want to verify whether the board is operating properly by checking if any CAN messages are transmitted. I really would like to resolve this issue. If there are any items that I should check, I would greatly appreciate it if you could let me know. I will follow your guidance and try each step. Could you please advise me on what I should do to solve this problem? #rd33772c14vevm, #CAN, #s32k344, #JTAG, #MBDT Re: Need help verifying CAN communication on the RD33772C14VEVM board Hello, First of all, I am sorry for the late reply. From the message you sent, I suspect that the board is not properly powered. I see that you built the application in S32DS too, but the build process to do not involve to deploy the application to the board. You have to create a Debug Configuration compatible for S32K344 and deploy the .elf from there. Since you didn't connect a battery yet, I recommend you to power the board from cell emulator instead of the beefy screws found on the EVB. I am not sure that you can power up the board using the Shunt resistor (R62), please thoroughly check the schematic. In the readme for the model, it states that you can power up the board from the emulator board: Connect the power supply to the emulator board: 12V -> BH1(K30_12V_L) and GND -> BH2(GND_KL31_DOWN) Let me know if this solves your problem. Best regards, Sorin Bancila
查看全文
IMX95LPD5EVK-19CM:L6.18.2のUUU eMMCフラッシュが失敗(LinuxおよびWindowsでのLIBUSBエラー) NXPチームの皆様、こんにちは。 純正BSPからIMX95LPD5EVK-19CMをeIQ Neutron NPU YOLO推論のためにLF_v6.18.2-1.0.0にアップグレードするのに助けが必要です。UUU eMMCのフラッシュは、LinuxとWindowsの両方でSDPS:bootで異なるlibusbエラーで失敗します。詳細は下記をご覧ください。 --- ## 1. ハードウェア |アイテム|詳細 | |------|--------| |ボード|IMX95LPD5EVK-19CM(i.MX 95 19×19 EVK、SOM + ベースボード) | |Yocto マシン / ホスト名 |IMX95-a1-19x19-LPDDR5-EVK | |シリコン |i.MX 95 A1 | |ストレージ |64GB eMMC(工場出荷時の事前フラッシュ済みLinux) | |パワー|J5に12V、SW4オン | |デバッグ |J31 USB-C →ホスト(シリアル番号115200) | |フラッシュポート |J8 USB1 OTG USB-C →ホスト | |カメラ |J7上のLogitech C920(/dev/video13) | --- ## 2.ソフトウェアのバージョン ### 現在(純正eMMC — Linuxは通常起動) | コンポーネント | バージョン | |-----------|---------| | BSP | LF6.12.34_2.1.0| |カーネル |6.12.34-lts-next-gbe78e49cb433 | |Boot cmdline |root=/dev/mmcblk0p2 | |Neutron delegate |v1.0.0-be8bf399 | |libneutron_delegate.so |/usr/lib/libneutron_delegate.so | |ホストコンバータ(旧) |eIQツールキット1.17 / Neutronコンバーター2.1.3| ### ターゲット(ダウンロード済み、eMMCへの書き込みはまだ完了していません) |コンポーネント |バージョン / ファイル | |-----------|----------------| |BSPリリース |LF_v6.18.2-1.0.0 (SCR-6.18.2-1.0.0) | |カーネル(期待値) |6.18.2-1.0.0 | |画像パッケージ |LF_v6.18.2-1.0.0_images_IMX95 | |ブートイメージ |imx-boot-imx95-19x19-lpddr5-evk-sd.bin flash_all| |根源 |imx-image-full-imx95evk.wic(~11 GB) | |Neutron代理(期待) |v1.0.0-7399A58E | |ホストコンバータ(ホストで準備完了) |eIQ Neutron SDK 3.0.1 (converter 3.0.1+0Xd5d7918e)| 参考:NXPフォーラムエンジニア(Zhiming_Liu)がi.MX95上でYoloV8mをL6.18.2+eIQ Neutron SDK 3.0.1+delegate 7399a58eで検証しました。 --- ## 3.アプリケーション目的 YOLO(v8n / v11n)でのUSBウェブカメラの人物検出方法: - INT8 TFLite エクスポート(Ultralytics) - Neutron コンバータ --ターゲットIMX95 - tflite_runtime + libneutron_delegate.SO 搭載 現在のBSP(6.12.34)では: - NXPフォーラム yolov8m_full_integer_quant_converted.tflite → NPU呼び出しでセグメンテーション違反 (終了コード139) - カスタム yolov8n_neutron.tflite → 呼び出しは成功しましたが、人物検出数は0です - NPU上のヘッドレスバックボーン → 常にガベージ出力(約1.13)CPU分割パイプラインは正常に動作する(検出率56~90%) 結論:SDK 3.0.1で変換されたNPUモデルを検証するには、eMMC上でL6.18.2 BSPが必要です。 --- ## 4. ホスト設定 | ホスト | UUU バージョン | パス | |------|-------------|------| | Ubuntu 24.04 (x86_64) | libuuu_1.5.243-0-g230f1b1 | /usr/local/bin/uuu | | Windows 10/11 | libuuu_1.5.243-0-g230f1b1 | uuu.exe (mfgtools uuu_1.5.243 リリースより) | 両ホスト上のイメージディレクトリ: LF_v6.18.2-1.0.0_images_IMX95 --- ## 5.ブートスイッチSW7(IMX95LPD5EVK-19CM QSGごと、1=ON 0=OFF) | モード | SW7-1 | SW7-2 | SW7-3 | SW7-4 | |------|-------|-------|-------|-------| |シリアルダウンロード (UUU) | 1 | 0 | 0 | 1 | | eMMC ブート (通常) | 1 | 0 | 1 | 0 | eMMCブート(SW7=1010)は正常に動作します。SW7の交換前には必ず、電源の完全な投入サイクルを実施してください。 --- ## 6. フラッシュ手順 (UUU 経由の eMMC) 基板準備(LinuxとWindowsでも同様): - SW7 = 1001(シリアルダウンロード) - J8(USB1 OTG)はホストPCにコネクテッド(J31ではありません) - オプションのシリアルコンソール用にJ31コネクテッド - J5 12 V電源コネクテッド - 「既知のUSBデバイスを待機中」と表示されたときにボードが電源オン コマンド: uuu -b emmc_all imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_allimx-image-full-imx95evk.wic (Linux: sudo uuu ... |ウィンドウズ:uuu.exe...画像ディレクトリより) --- ## 7.UUU errors — Linux (Ubuntu 24.04) sudo /usr/local/bin/uuu -b emmc_all \ imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all\ imx-image-full-imx95evk.wic 出力: NXP IMXチップ用uuu(Universal Update Utility)-- libuuu_1.5.243-0-g230f1b1 成功 0 失敗 1 1:6-E3C50910 1/1 [HID(W): LIBUSB_ERROR_NO_DEVICE (-4)] SDPS: boot -scanterm -f imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all... 注: - lsusb は、NXP USB デバイス (1fc9:015d) が SDP モードであることを短時間表示します。 - uuu は時々「新しい USB デバイスが接続されました」と表示した後、SDPS: ブートで失敗します - sudoなしの場合:権限が拒否されました(errno=13) - eMMCは変更されませんでした(フラッシュ書き込みが完了しませんでした) --- ## 8. UUUエラー — Windows ホスト: Windows 10/11、PowerShell、uuu.exe 1.5.243 作業ディレクトリ:C:\Users\Hardware.Team\Downloads\LF_v6.18.2-1.0.0_images_IMX95 ### 試行 — flash_all (正しいブートイメージが期待される) PS C:\Users\Hardware.Team\Downloads\LF_v6.18.2-1.0.0_images_IMX95> & '..\uuu (2).exe' -b emmc_all imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_allimx-image-full-imx95evk.wic NXP IMXチップ用uuu(Universal Update Utility)-- libuuu_1.5.243-0-g230f1b1 成功 0 失敗 1 1:3-E3C50910 1/1 [HID(W): LIBUSB_ERROR_PIPE (-9)] SDPS: boot -scanterm -f imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all... 各ホストにおけるUSBエラーの概要: | ホスト | ブートイメージ | libusb エラー | |------|------------|--------------| | Ubuntu 24.04 | flash_all | LIBUSB_ERROR_NO_DEVICE (-4) | | Windows | flash_all | LIBUSB_ERROR_PIPE (-9) | すべての障害は同じステップで発生します:SDPS:ブート(eMMC書き込み処理前)。 --- ## 9. 今日通用するもの - SW7=1010 →通常、工場出荷時のeMMC Linux(6.12.34)を起動します - eth0上のSSH作業 - USBウェブカメラ(/dev/video13)を検出 - libneutron_delegate.so present(be8bf399) - CPU側の推論検証;現在のBSPでのNPU出力が不正確です --- ## 10.NXPへの質問 1.IMX95LPD5EVK-19CM(A1)、デバイス1fc9:015d、SW7=1001、J8でuuu 1.5.243を搭載したSDPS:ブート失敗の場合、LinuxでLIBUSB_ERROR_NO_DEVICE(-4)がLIBUSB_ERROR_PIPE(-9)/LIBUSB_ERROR_IO(-1)になる原因は何ですか? 2. 既知のuuu 1.5.243はありますか?+ IMX95 A1の互換性要件(ドライバ、WindowsのWinUSB/Zadig、Linuxのudevルール)について? 3. imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all + imx-image-full-imx95evk.wic が IMX95LPD5EVK-19CM eMMC フラッシュ (ECC RAM でない限り sd-ecc ではない) の正しい組み合わせであることを確認します。 4. be8bf399(6.12.34)と7399a58e(6.18.2)の間に、YOLOv8 INT8モデルに影響を与える既知のNeutronデリゲートの違いはありますか? 5. LinuxとWindowsの両方でUUUのUSBパスが失敗した場合に、L6.18.2をeMMCにフラッシュする代替の方法はありますか? --- ## 11.ログはご要望に応じて提供いたします。 - 完全なuuuu詳細ログ:uuu -v -b emmc_all...(LinuxおよびWindows) - ボードがSDPモードに入った際のホストLSUSB / デバイスマネージャー / dmesg - シリアルコンソールログ(工場出荷時のeMMC起動 — 動作中) - ボード:uname -r、文字列libneutron_delegate.so、NPUテスト結果は1934年12月6日 Neutron NPU開発のためのeMMCアップグレードをL6.18.2-1.0.0に完成させるためのご指導ありがとうございます。 よろしくお願いいたします。 Re: IMX95LPD5EVK-19CM: UUU eMMC flash of L6.18.2 fails (LIBUSB errors on Linux and Windows) i.MX 95のA1シリコンは、最新のBSPではサポートされなくなりました。6.12.34がA1をサポートする最後のバージョンと思われます。 回避策はありません。最新のBSPをA1シリコンで動かすことはできません。EVKを新しいドーターカードでアップグレードする必要があります。A1シリコンカードは青色、B0シリコンカードは緑色です。 6.18.2の.wicファイルを使用して古いEVKにUUUダウンロードをテストしていません。画像ですが、おそらくそちら側と同じように失敗すると思います。数日中にやります。SDカードでテストして、.wicをプログラムすることもできますPC上のイメージをSDカードにコピーし、ブートモードをSDカードに設定してEVKで実行してみてください。 よろしくお願いいたします。 ベルンハルト。 Re: IMX95LPD5EVK-19CM: UUU eMMC flash of L6.18.2 fails (LIBUSB errors on Linux and Windows) こんにちは、 ご回答ありがとうございます。同じ掲示板に関して、もう一つ質問があります。 IMX95LPD5EVK-19 follow AN14748 でM7アプリケーションを実行しようとしていますが、フラッシュできません flash.binUUUと共に。ボードは短時間検出されるが、その後すぐにSDPSの起動に失敗する。 ハードウェア: IMX95LPD5BB-19 REV A1 (2024 NXP B.V.) ブートスイッチ(SW7[1:4]): 1001(シリアルダウンロード) ターゲット: eMMC ホスト: Ubuntu Linux うーん: libuuu_1.5.243-0-g230f1b1 試したSDKs(MCUXpresso SDK Builder): SDK_26.06.00_IMX95LPD5EVK-19 SDK_2.15.000_IMX95LPD5EVK-19 どちらも同じ結果を生み出す。 コマンド: cd IMX95LPD5EVK/build_/tmp/deploy/images/imx95-a1-19x19-lpddr5-evk sudo uuu -b emmc flash.bin   エラー: 成功 0 失敗 1 1:2-E3C50910 1/1 [HID(W): LIBUSB_ERROR_NO_DEVICE (-4)] SDPS: boot -f flash.bin   実施された手順(AN14748に基づく): ボードの電源をオフにした状態で、SW7を1001に設定します。 USBをホストに接続します 走る sudo uuu -b emmc flash.bin 電源サイクルボード SDPSの起動に毎回失敗する 質問: どのMCUXpresso SDKバージョンが IMX95LPD5BB-19 REV A1 M7のフラッシュに有効ですか? ビルドターゲット imx95-a1-19x19-lpddr5-evk このハードウェアには正しいですか? この基板改訂版に関して、既知のUUUに関する問題や、AN14748以外に追加の手順はありますか? 使うべきでしょうか -b emmc または -b sd まず、どのUSBポートを使用すればよいでしょうか?
查看全文
TEF82xx 低レベルドライバーのビルド問題 こんにちは、 TEF82xx API Low Level ドライバ RFP9.3.0 20240920_PRODをビルドして、含まれている例を実行しようとしているのですが、問題が発生しています: ソースファイルが見つからない:src/plf_sys.c そして、このファイルは本当に見つからないのです。他のいくつかの例と同様に (plf_cap.c、plf_crc.c、plf_hio.c、bc_api\bc_api_src\plf\CMakeLists.txt で必要とされるものなど。これらのファイルはどこで見つけられますか? Re: TEF82xx Low Level Drivers build issue こんにちは、 はい、おっしゃる通りです。TEF82xx API Low Level ドライバ RFP9.3.0 20240920_PROD.zipパッケージにはそのファイルが見当たりません。 他のパッケージからのものに違いない。名前plf_sys.cプラットフォームを指している可能性が高いです。おそらくドライバはOSからのものだと想定しているのでしょう。 TEF82xx API 低レベルドライバ RFP9.3.0 20240920_PROD\TEF82xx_API_RN_V9.3.0.pdf petervlna_0-1783494576622.png ドキュメントにはそれ以上の情報は見つかっていません。 よろしくお願いいたします。 ピーター Re: TEF82xx Low Level Drivers build issue こんにちは、 はい、おっしゃる通りです。TEF82xx API Low Level ドライバ RFP9.3.0 20240920_PROD.zipパッケージにはそのファイルが見当たりません。 他のパッケージからのものに違いない。名前plf_sys.cプラットフォームを指している可能性が高いです。おそらくドライバはOSからのものだと想定しているのでしょう。 TEF82xx API 低レベルドライバ RFP9.3.0 20240920_PROD\TEF82xx_API_RN_V9.3.0.pdf petervlna_0-1783494576622.png ドキュメントにはそれ以上の情報は見つかっていません。 よろしくお願いいたします。 ピーター
查看全文