2390306_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2390306_en-US

2390306_en-US

IMX95LPD5EVK-19CM: UUU eMMC flash of L6.18.2 fails (LIBUSB errors on Linux and Windows)

Hello NXP team,

I need help upgrading IMX95LPD5EVK-19CM from the factory BSP to LF_v6.18.2-1.0.0 for eIQ Neutron NPU YOLO inference. UUU eMMC flashing fails on both Linux and Windows with different libusb errors at SDPS:boot. Details below.

---

## 1. Hardware

| Item | Detail |
|------|--------|
| Board | IMX95LPD5EVK-19CM (i.MX 95 19×19 EVK, SOM + baseboard) |
| Yocto machine / hostname | imx95-a1-19x19-lpddr5-evk |
| Silicon | i.MX 95 A1 |
| Storage | 64 GB eMMC (factory pre-flashed Linux) |
| Power | 12 V on J5, SW4 ON |
| Debug | J31 USB-C → host (serial, 115200) |
| Flash port | J8 USB1 OTG USB-C → host |
| Camera | Logitech C920 on J7 (/dev/video13) |

---

## 2. Software versions

### Current (factory eMMC — Linux boots normally)

| Component | Version |
|-----------|---------|
| BSP | LF6.12.34_2.1.0 |
| Kernel | 6.12.34-lts-next-gbe78e49cb433 |
| Boot cmdline | root=/dev/mmcblk0p2 |
| Neutron delegate | v1.0.0-be8bf399 |
| libneutron_delegate.so | /usr/lib/libneutron_delegate.so |
| Host converter (old) | eIQ Toolkit 1.17 / neutron-converter 2.1.3 |

### Target (downloaded, not yet flashed to eMMC)

| Component | Version / file |
|-----------|----------------|
| BSP release | LF_v6.18.2-1.0.0 (SCR-6.18.2-1.0.0) |
| Kernel (expected) | 6.18.2-1.0.0 |
| Image package | LF_v6.18.2-1.0.0_images_IMX95 |
| Boot image | imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all |
| Rootfs | imx-image-full-imx95evk.wic (~11 GB) |
| Neutron delegate (expected) | v1.0.0-7399a58e |
| Host converter (ready on host) | eIQ Neutron SDK 3.0.1 (converter 3.0.1+0Xd5d7918e) |

Reference: NXP forum engineer (Zhiming_Liu) validated YOLOv8m on i.MX95 with L6.18.2 + eIQ Neutron SDK 3.0.1 + delegate 7399a58e.

---

## 3. Application goal

USB webcam person detection with YOLO (v8n / v11n) using:
- INT8 TFLite export (Ultralytics)
- neutron-converter --target imx95
- tflite_runtime + libneutron_delegate.so on board

On current BSP (6.12.34):
- NXP forum yolov8m_full_integer_quant_converted.tflite → SEGFAULT on NPU invoke (exit 139)
- Custom yolov8n_neutron.tflite → invoke OK but 0 person detections
- Headless backbone on NPU → constant garbage output (~1.13); CPU split pipeline works (56–90% detections)

Conclusion: need L6.18.2 BSP on eMMC before NPU models converted with SDK 3.0.1 can be validated.

---

## 4. Host setup

| Host | UUU version | Path |
|------|-------------|------|
| Ubuntu 24.04 (x86_64) | libuuu_1.5.243-0-g230f1b1 | /usr/local/bin/uuu |
| Windows 10/11 | libuuu_1.5.243-0-g230f1b1 | uuu.exe (from mfgtools uuu_1.5.243 release) |

Image directory on both hosts:
LF_v6.18.2-1.0.0_images_IMX95

---

## 5. Boot switch SW7 (per IMX95LPD5EVK-19CM QSG, 1=ON 0=OFF)

| Mode | SW7-1 | SW7-2 | SW7-3 | SW7-4 |
|------|-------|-------|-------|-------|
| Serial Download (UUU) | 1 | 0 | 0 | 1 |
| eMMC boot (normal) | 1 | 0 | 1 | 0 |

eMMC boot (SW7=1010) works normally. Full power cycle performed before each SW7 change.

---

## 6. Flash procedure (eMMC via UUU)

Board preparation (same for Linux and Windows):
- SW7 = 1001 (Serial Download)
- J8 (USB1 OTG) connected to host PC (not J31)
- J31 connected for optional serial console
- J5 12 V power connected
- Board powered ON when uuu displays "Wait for Known USB Device"

Command:

uuu -b emmc_all imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all imx-image-full-imx95evk.wic

(Linux: sudo uuu ... | Windows: uuu.exe ... from image directory)

---

## 7. UUU errors — Linux (Ubuntu 24.04)

sudo /usr/local/bin/uuu -b emmc_all \
imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all \
imx-image-full-imx95evk.wic

Output:

uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.243-0-g230f1b1

Success 0 Failure 1

1:6-E3C50910 1/1 [HID(W): LIBUSB_ERROR_NO_DEVICE (-4)] SDPS: boot -scanterm -f imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all ...

Notes:
- lsusb briefly shows NXP USB device (1fc9:015d) in SDP mode
- uuu sometimes prints "New USB Device Attached" then fails at SDPS: boot
- Without sudo: permission denied (errno=13)
- eMMC was not modified (flash did not complete)

---

## 8. UUU errors — Windows

Host: Windows 10/11, PowerShell, uuu.exe 1.5.243
Working directory: C:\Users\Hardware.Team\Downloads\LF_v6.18.2-1.0.0_images_IMX95

### Attempt — flash_all (expected correct boot image)

PS C:\Users\Hardware.Team\Downloads\LF_v6.18.2-1.0.0_images_IMX95> & '..\uuu (2).exe' -b emmc_all imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all imx-image-full-imx95evk.wic

uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.243-0-g230f1b1

Success 0 Failure 1

1:3-E3C50910 1/1 [HID(W): LIBUSB_ERROR_PIPE (-9)] SDPS: boot -scanterm -f imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all ...

Summary of USB errors across hosts:

| Host | Boot image | libusb error |
|------|------------|--------------|
| Ubuntu 24.04 | flash_all | LIBUSB_ERROR_NO_DEVICE (-4) |
| Windows | flash_all | LIBUSB_ERROR_PIPE (-9) |

All failures occur at the same step: SDPS: boot (before eMMC write progress).

---

## 9. What works today

- SW7=1010 → boots factory eMMC Linux (6.12.34) normally
- SSH over eth0 works
- USB webcam (/dev/video13) detected
- libneutron_delegate.so present (be8bf399)
- CPU-side inference validated; NPU output incorrect on current BSP

---

## 10. Questions for NXP

1. For SDPS:boot failures with uuu 1.5.243 on IMX95LPD5EVK-19CM (A1), device 1fc9:015d, SW7=1001, J8 — what causes LIBUSB_ERROR_NO_DEVICE (-4) on Linux vs LIBUSB_ERROR_PIPE (-9) / LIBUSB_ERROR_IO (-1) on Windows?

2. Are there known uuu 1.5.243 + IMX95 A1 compatibility requirements (driver, WinUSB/Zadig on Windows, udev rules on Linux)?

3. Confirm imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all + imx-image-full-imx95evk.wic is the correct pair for IMX95LPD5EVK-19CM eMMC flash (not sd-ecc unless ECC RAM).

4. Any known Neutron delegate differences between be8bf399 (6.12.34) and 7399a58e (6.18.2) affecting YOLOv8 INT8 models?

5. Is there an alternative supported method to flash L6.18.2 to eMMC if UUU USB path fails on both Linux and Windows?

---

## 11. Logs available on request

- Full uuu verbose log: uuu -v -b emmc_all ... (Linux and Windows)
- Host lsusb / Device Manager / dmesg when board enters SDP mode
- Serial console log (factory eMMC boot — working)
- Board: uname -r, strings libneutron_delegate.so, NPU test results on 6.12.34

Thank you for guidance on completing the eMMC upgrade to L6.18.2-1.0.0 for Neutron NPU development.

Best regards

Re: IMX95LPD5EVK-19CM: UUU eMMC flash of L6.18.2 fails (LIBUSB errors on Linux and Windows)

The A1 silicon of the i.MX 95 is no longer supported from our latest BSPs, 6.12.34 seems to be last one supporting A1.

There is no workaround, you can't make the latest BSP work on A1 silicon, you need to upgrade your EVK with a new daughter card. The A1 silicon card is blue, the B0 silicon card is green.

I didn't test a UUU download onto an old EVK using the 6.18.2 .wic image, but I expect that it fails the same way as it fails on your side. I'll do this in the next days. You could do a test with an SD-Card, program the .wic image on your PC to an SD-Card and try to run it on your EVK with boot mode set to SD-Card.

Regards,
Bernhard.

Re: IMX95LPD5EVK-19CM: UUU eMMC flash of L6.18.2 fails (LIBUSB errors on Linux and Windows)

Hello,

Thanks for response. i have another query regrading same board.

I am trying to run an M7 application on IMX95LPD5EVK-19 following AN14748, but I cannot flash flash.bin with UUU. The board is detected briefly, then SDPS boot fails immediately.

Hardware: IMX95LPD5BB-19 REV A1 (2024 NXP B.V.)
Boot switch (SW7[1:4]): 1001 (Serial Download)
Target: eMMC
Host: Ubuntu Linux
UUU: libuuu_1.5.243-0-g230f1b1

SDKs tried (MCUXpresso SDK Builder):

  • SDK_26.06.00_IMX95LPD5EVK-19
  • SDK_2.15.000_IMX95LPD5EVK-19

Both produce the same result.

Command:

cd IMX95LPD5EVK/build_/tmp/deploy/images/imx95-a1-19x19-lpddr5-evk
sudo uuu -b emmc flash.bin
 

Error:

Success 0 Failure 1
1:2-E3C50910 1/ 1 [HID(W): LIBUSB_ERROR_NO_DEVICE (-4)] SDPS: boot -f flash.bin
 

Steps followed (per AN14748):

  1. Set SW7 = 1001 with board powered off
  2. Connect USB to host
  3. Run sudo uuu -b emmc flash.bin
  4. Power-cycle board
  5. Fails at SDPS boot every time

Questions:

  1. Which MCUXpresso SDK version is validated for IMX95LPD5BB-19 REV A1 M7 flashing?
  2. Is build target imx95-a1-19x19-lpddr5-evk correct for this hardware?
  3. Any known UUU issues or extra steps beyond AN14748 for this board revision?
  4. Should I use -b emmc or -b sd first, and which USB port should be used?
标记 (1)
无评分
版本历史
最后更新:
‎07-21-2026 02:31 AM
更新人: