Multi Source Translation Content

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multi Source Translation Content

讨论

排序依据:
MFS2323BMBA5EP OTP 配置冲突:SPI 与 I2C 模式识别 尊敬的恩智浦工程师和社区专家们: 我目前正在使用以下技术进行开发 MFS2323BMBA5EP 功能安全单板计算机 (SBC) 的配置文件与数据手册中关于一次性密码 (OTP) 出厂配置的报告存在重大冲突。非常感谢您能凭借专业知识对此进行澄清。 配置冲突: 1. 来自以下方面的证据 .cfg 文件: 在我的 FS2320_BA5_CONFIG_Rev_A.cfg 文件中,有一个直接的寄存器值: 0x30 : 0x00 根据 FS23 数据表(表 229), OTP_MAIN_SYS_I2C_CFG😞 位 4 ( SPI_EN_OTP ) : 0 方法 I2C 已启用,SPI 已禁用; 1 表示SPI已启用。 位 3~0 ( I2CDEVADDR_OTP ) : 0000 意思是 I2C 从机地址是 0x20 。 这清楚地表明该芯片是出厂时就已配置好的。 I2C模式。 2. 来自配置报告 PDF 的证据: 然而,在我的 R_MFS2323BMBA5_Rev_A_test.pdf 文件,在 表 2. 设备 OTP 配置,报告中明确指出: SPI 使能:SPI 引脚已启用。 这表明硬件引脚被锁定。 SPI模式。 我的实际硬件测试结果: 当我将我的MCU(S32K344)配置为SPI主设备以与该PMIC通信时: MISO引脚保持恒定 0.3伏 (表示高阻抗,内部下拉电阻较弱,意味着从设备无法驱动线路)。 PMIC 侧的 SCK 引脚实际上会自行输出时钟信号。 我怀疑该芯片可能被锁定在 OTP 仿真模式或配置为 I2C 从设备,这导致 SPI 通信完全失败。 我的具体问题: 请您确认一下。 MFS2323BMBA5EP的实际出厂OTP配置是什么?是SPI还是I2C? 当两者之间发生冲突时 .cfg 寄存器文件( 0x30:0x00 )和PDF配置报告,哪个才是硬件配置的绝对权威?PDF报告是否存在文档错误的可能性? (我已附上) FS2320_BA5_CONFIG_Rev_A.cfg 以及 R_MFS2323BMBA5_Rev_A_test.pdf (参见此帖)。 提前感谢您的帮助! Re: MFS2323BMBA5EP OTP Configuration Conflict: SPI vs I2C Mode Identification 好的谢谢您 Re: MFS2323BMBA5EP OTP Configuration Conflict: SPI vs I2C Mode Identification 请问你们是哪个公司?目前您是用的自己的邮箱属于C客户优先级很低的 这个是需要检查您的原理图,驱动CRC一系列的东西。 我建议您用公司的邮箱提交一个ticket Home  Re: MFS2323BMBA5EP OTP Configuration Conflict: SPI vs I2C Mode Identification 目前不能,我现在是在DEBUG模式下去通讯,我单独测试344端的SCK和MOSI的波形是能发出我写的数据的,但是由于,FS23的SCK引脚也在发信号,这两个接在一块后,MCU发出来的SCK信号被FS23对顶后拉低了,我发送给FS23回复的都是0,我也配置了CRC了 紫色的线是对顶后的SCK信号 黄色是数据信号 刻度都是5V 发送的数据是 {0x02, 0x00, 0x00,CRC} 如果强行把SCK看成正常波形是能看出来数据是对的,第一位是2然后00和CRC Re: MFS2323BMBA5EP OTP Configuration Conflict: SPI vs I2C Mode Identification 你配置成SPI 能通信成功吗? Re: MFS2323BMBA5EP OTP Configuration Conflict: SPI vs I2C Mode Identification 会出现与S32K344SPI通讯时FS23的SCK信号也在发送吗,因为如果我不配置SPI与FS23通讯,我去抓FS23的SCK脚是没有波形的,只有344和他通讯的时候这两个的SCK引脚都在发信号,而且SCK和CS引脚的波形是一模一样的 Re: MFS2323BMBA5EP OTP Configuration Conflict: SPI vs I2C Mode Identification 我在GUI upload .cfg文件到mirror register显示就是SPI 模式
查看全文
From Simulation to Vehicle Control: Real-Time Decision Making on the S32N55 1 Table of Contents • Introduction • Overview • Context • References • Conclusion 2 Introduction Modern vehicle development increasingly relies on digital validation before physical prototypes are available. Simulation enables rapid testing and iteration, but engineering teams also need to demonstrate how virtual behavior maps to real hardware. In the Hello World demonstrator, this connection is handled by the Main Node application running on the NXP S32N55. The Main Node acts as the central execution point of the demonstrator, transforming vehicle information generated inside MATLAB ® and Simulink ® into decisions and actions that can be observed on physical hardware. By combining Model-Based Design, CAN communication, and centralized decision making, the system creates a bidirectional link between the virtual vehicle and the physical demonstrator. This article explains how the Main Node converts simulation inputs into coordinated vehicle behavior while maintaining synchronization between the digital and physical domains. 3 Overview As introduced in the previous article, the S32N55 functions as the communication hub of the demonstrator, aggregating information from distributed modules and distributing commands throughout the system. Beyond communication, however, the Main Node also serves as the decision-making layer responsible for interpreting vehicle state and translating it into actionable control signals. Developed using the NXP Model-Based Design Toolbox (MBDT), the application is entirely modeled in Simulink and deployed directly onto the target hardware. This workflow enables engineers to focus on vehicle functionality and system behavior while leveraging automated code generation and integrated CAN communication support. The Main Node receives data from simulated and physical sources, maintains a coherent vehicle-state view, runs vehicle-level control logic, and sends commands to the actuator nodes that make up the demonstrator. This centralized architecture reflects the direction of modern software-defined vehicle platforms, where coordination moves from isolated ECUs toward higher-level compute nodes. Figure 1. Main Node overview showing how the S32N55 coordinates simulation inputs, vehicle-state processing, and commands to distributed hardware modules. 4 Context The Main Node is positioned between the virtual vehicle environment and the physical hardware modules that form the demonstrator. Driver inputs generated through the Driver-in-the-Loop simulation environment are transmitted over CAN and received by the S32N55, where they are processed alongside feedback arriving from multiple distributed nodes. Commands such as vehicle speed, steering angle, gear selection, braking requests, and lighting controls enter the Main Node from the simulation environment. These inputs are then evaluated by the application and translated into CAN messages that drive the corresponding hardware modules. This architecture enables the physical demonstrator to mirror the behavior of the virtual vehicle. When the simulated vehicle accelerates, the speed command is interpreted by the Main Node and forwarded to the motor control subsystem. Steering-wheel movements are translated into steering-angle commands for the steering module, while lighting commands activate headlights, fog lights, hazard lights, and turn indicators on the physical hardware. Figure 2. System context illustrating the Main Node as the bridge between the virtual vehicle environment and the physical demonstrator hardware. The Main Node can be driven either by the Driver-in-the-Loop simulation or by the External Control model. In both cases, the command source publishes the same DBC-defined CAN frames, so the S32N55 receives speed, steering, brake, gear, and lighting commands through the same interface. This allows the same deployed application to be exercised from two sources without changing the Main Node software. This approach is especially useful during integration, demonstrations, and incremental validation. Engineers can exercise the Main Node and the downstream actuator modules even when the complete virtual environment is not active, while still preserving the exact communication contract used by the full system. As a result, the application can be validated against two different input sources without changing the deployed software on the board. Rather than acting as a simple gateway, the Main Node continuously evaluates received information and executes vehicle-level decisions. One example is the processing of motor feedback data, where information from multiple motors is combined to derive a representative vehicle speed used throughout the system. Centralizing this functionality simplifies system coordination while ensuring consistency across all connected modules. Gear selection is handled as part of this centralized decision layer. The incoming gear command is interpreted as a driving mode that affects how the requested speed is applied: Park and Neutral block motion commands, Reverse changes the sign of the velocity reference, and Drive or Sport propagate the requested speed as a forward-driving command. This keeps speed-control behavior aligned with the selected driving mode while preserving the same driver-input signal set. The target-speed command is computed from the requested speed reference, the selected gear mode, the reported vehicle speed, and the effective brake command. Motor feedback is fused into a representative reported speed, which provides the actual-speed reference used during braking decisions. Under normal driving conditions, the requested target speed passes through the gearbox-aware logic and is converted into the motor-speed command sent over CAN. When braking is active, the Main Node bases the outgoing command on the detected speed and brake value, reducing the command until the vehicle is considered stopped. The Main Node also hosts the demonstrator's automated emergency braking functionality. Parking sensor nodes continuously report obstacle distances over CAN. The application evaluates these measurements and determines whether an object has entered a predefined safety zone. When this condition is met, the braking command issued by the driver can be overridden and replaced with an emergency braking request generated by the system. Figure 3. Parking sensors in action detecting nearby obstacles and providing distance feedback used by the Main Node to support emergency braking decisions. An important aspect of this implementation is that the braking behavior is reflected across both domains. The physical hardware responds to the braking request, while the simulation environment can receive corresponding vehicle-state updates through the same CAN-based loop. This closed-loop behavior demonstrates bidirectional interaction between simulation and embedded execution, allowing safety-related functionality to be validated in a realistic environment before a full vehicle prototype is available. Figure 4. Closed-loop emergency braking flow showing how parking sensor feedback can trigger an automated braking request across both the physical and simulated domains. CAN communication is the key enabler of this architecture. Every subsystem communicates through DBC-defined interfaces, allowing functionality to be distributed across multiple independent nodes while preserving a consistent and scalable communication framework. The shared DBC approach ensures that signal definitions remain synchronized across all parts of the demonstrator. To support this workflow, MathWorks Vehicle Network Toolbox ™ provides direct integration between MATLAB ® , Simulink ® , and CAN communication interfaces. DBC files can be used directly throughout the development process, simplifying signal management and ensuring consistency across the virtual vehicle, the Main Node, and all peripheral modules. As the demonstrator grows to include additional functionality, the same network definition can be reused across all participating systems, reducing integration effort and helping accelerate development. Note: The combination of NXP Model-Based Design Toolbox and MathWorks Vehicle Network Toolbox creates a workflow in which vehicle behavior, communication interfaces, and deployed software remain aligned from modeling through system integration. Figure 5. CAN and DBC workflow showing how shared signal definitions keep the virtual vehicle, Main Node, and distributed hardware modules synchronized. 5 References NXP Model-Based Design Toolbox (MBDT) NXP S32N Vehicle Super-Integration Processors Vehicle Network Toolbox ™ NXP Model-Based Design Toolbox Community 6 Conclusion The Main Node demonstrates how a centralized compute platform can act as more than a communication gateway. Running on the NXP S32N55, it combines signal aggregation, decision making, and command distribution into a single application that coordinates the entire demonstrator. By transforming simulation-generated inputs into physical vehicle behavior and feeding real-world information back into the virtual environment, the Main Node creates a practical closed-loop development platform. Together, NXP Model-Based Design Toolbox, MathWorks Vehicle Network Toolbox, and CAN-based communication enable rapid iteration, simplified integration, and efficient validation of vehicle functionality across simulated and physical domains.
查看全文
i.MX8M Plus — Secondary image boot (IMG_CNTN_SET1_OFFSET) on ECSPI/SPI NOR: does ROM fall back in OP i.MX8M Plus -- Secondary image boot (IMG_CNTN_SET1_OFFSET) on ECSPI/SPI NOR: does ROM fall back in OPEN config? ==== Setup ==== - SoC: i.MX8M Plus (custom SMARC module) - Boot device: serial NOR on ECSPI2 / CS1 (Winbond W25Q128, 16 MiB). This is the legacy eCSPI controller, NOT FlexSPI. - Security: OPEN configuration (device is not HAB-closed). - Fuse IMG_CNTN_SET1_OFFSET (fuse read 2 1) = 0x00000000. - Flash map: primary bootloader at 0x000000, secondary copy at 0x400000 (4 MiB). Per the documented SPI mapping: "For SPI: secondary boot disabled if fuse > 10; n == 0 -> Offset = 4 MB; n == 2 -> 1 MB; others & n <= 10 -> 1 MB * 2^n." With fuse n = 0 (factory default, no burn needed) the secondary offset should be exactly 0x400000. ==== The problem ==== We placed a byte-identical, cmp.b-verified copy of the primary image at 0x400000, then invalidated the primary boot header (sf erase 0 0x1000) and reset. The ROM does NOT fall back to the secondary image -- the board is bricked (recoverable only via USB SDP). We also tried erasing a hole inside the primary body (sf erase 0x100000 0x40000) with the same result. ==== Questions ==== 1. On SPI/ECSPI NOR, what exactly triggers the ROM to switch to the secondary image at the IMG_CNTN_SET1_OFFSET? Is it any invalid primary boot header / failed image parse, or specifically a HAB authentication failure? 2. Does secondary-image boot work in OPEN (non-secured) configuration, or only when the device is HAB-closed? 3. Does it fall back on the same reset, or does it require a power cycle / second reset (persistent-boot style)? 4. Must the secondary image at 0x400000 be a separately-built bootable image (its own IVT/boot data for that offset), or is a byte-identical copy of the primary sufficient? ==== Logic-analyzer evidence (SPI bus captured during reset) ==== We probed the ECSPI2 bus (CLK, MOSI, MISO, CS) with a Saleae Logic Pro 16 at 500 MS/s and decoded every SPI transaction during reset. For comparison we did the same on an i.MX8QM module which boots from FlexSPI NOR and does fall back to secondary successfully. ---- i.MX8M Plus (ECSPI NOR), primary corrupted ---- The ROM issues only 0x03 READ commands, reading strictly sequentially from offset 0: 0x03 00 00 FC -> READ 0x0000FC 0x03 00 04 EC -> READ 0x0004EC 0x03 00 08 DC -> READ 0x0008DC ... (~50 reads per 64 KiB block, strictly increasing) ... 0x03 00 13 xx -> read count drops here (erased hole 0x100000-0x140000, MISO=0xFF) 0x03 00 18 xx -> continues LINEARLY past the hole ... up to ~0x1A69E8 ... The ROM reads linearly through the entire primary region, straight through the erased/invalid area (getting 0xFF back), and NEVER issues a read to 0x400000 or 0x800000 (the secondary region). There is no "0x03 40 xx xx" anywhere in the full capture (25 million samples, 654 decoded transactions). On a fully-erased-header case the ROM loads 0xFF, executes it, and crashes with a Synchronous Abort -- no fallback of any kind. ---- i.MX8QM (FlexSPI NOR), for contrast -- secondary fallback DOES work ---- When only the primary container header is invalidated (FCB left intact at 0x000400), the QM ROM does: 0x0B 00 04 00 -> Fast-Read FCB @0x000400, MISO: 46 43 46 42 ("FCFB" magic, FlexSPI config valid) ... reads FCB configuration data ... 0x0B 00 10 00 -> Fast-Read primary container @0x001000, MISO: FF FF FF FF (invalid!) 0x0B 40 10 00 -> Fast-Read SECONDARY container @0x401000, MISO: valid <-- ROM switched, SAME reset 0x0B 40 30 00, 0x0B 40 40 00, ... -> loads whole secondary image (~90 reads at 0x40xxxx) The QM ROM reads FCB, configures FlexSPI, checks the primary container at 0x001000, sees 0xFF, and immediately (same reset) switches to the secondary container at 0x401000. This works. If we instead erase the whole first 4 MB (including the FCB), the QM ROM makes only 2 reads at 0x000400, gets 0xFF, and does NOT fall back -- so a valid FCB is required for the fallback to engage. ---- Comparison ---- i.MX8M Plus (this board): Controller : eCSPI (legacy SPI) Read opcode: 0x03 READ FCB present: No (eCSPI has no FCB concept) Reads secondary on corrupt primary: NO -- bus never shows "0x03 40 xx xx" Result: bricks (loads 0xFF -> crash) i.MX8QM (reference): Controller : FlexSPI Read opcode: 0x0B Fast Read FCB present: Yes (0x400, magic "FCFB") Reads secondary on corrupt primary: YES -- "0x0B 40 10 00", same reset Result: boots secondary successfully ==== Summary ==== From the bus captures, the IMG_CNTN_SET1_OFFSET secondary-image boot on i.MX8M Plus appears to be either FlexSPI-only, or gated by HAB-closed config, and does not engage for eCSPI NOR in OPEN config. Could NXP please confirm: - Whether eCSPI (as opposed to FlexSPI) NOR is supported for secondary-image boot at all on i.MX8M Plus; - Whether the trigger is HAB-auth-failure (closed config only) vs. any invalid header (open config too); - Whether fallback is same-reset or requires a power cycle; - Whether the secondary must be separately built for that offset, or a byte-identical copy is OK. Thank you. Re: i.MX8M Plus — Secondary image boot (IMG_CNTN_SET1_OFFSET) on ECSPI/SPI NOR: does ROM fall back i Hello @djordje_nod  Hope you are doing very well. Q1. What triggers the ROM to fall back to secondary on ECSPI NOR? In OPEN mode, the ROM/HAB performs image authentication but all authentication errors are ignored and the image is still allowed to execute. In CLOSED mode (SEC_CONFIG fused), when HAB authentication of the primary image fails, the ROM sets PERSIST_SECONDARY_BOOT (SRC_GPR10[30]) to 1 and performs a software reset. Q2. Does secondary image boot work in OPEN configuration? In OPEN mode, The ROM will never autonomously set PERSIST_SECONDARY_BOOT because it ignores HAB errors. Q3. Same reset or second reset? Primary boot fails HAB auth (closed mode) ----> ROM sets SRC_GPR10[30] = 1 ----> triggers software reset. On the next reset cycle, ROM reads the persistent bit, sees it is 1, and loads from the secondary offset instead of the primary. Q4. Byte-identical copy or separately-built image at 0x400000? A byte-identical copy is sufficient as the IVT/boot-data fields contain RAM addresses, not flash addresses. Best regards, Salas.
查看全文
IMX95EVK-19-REV-A1 flash problem Dear NXP, I'm trying to flash a linux image(6.18.20_2.0.0/ 6.18.2_1.0.0/6.12.49_2.2.0) to eMMC/SD Card on IMX95LP5-19 EVK REV A1 and none of them is successful. The command prompt shows [HID(W): LIBUSB_ERROR_PIPE (-9) ] SDPS: boot -f imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all. IMX95LPD5EVK-19CM: UUU eMMC flash of L6.18.2 fails (LIBUSB errors on Linux and Windows) The reference above mentioned that A1 silicon does not support current images on official site(6.12.34 does not have IMX95EVK patch). so I wonder if there is an unpublished official link that includes suitable images?  Looking forward to your reply, Thanks. BR/david Here is a reference IMX95LPD5EVK-19CM: UUU eMMC flash of L6.18.2 fails (LIBUSB errors on Linux and Windows) Re: IMX95EVK-19-REV-A1 flash problem A1 silicon: The recommended BSP is LF 6.6.52_2.2.x Please download demo image L6.6.52_2.2.2_MX95 And use image imx-boot-imx95-a1-19x19-lpddr5-evk-sd.bin-flash_all I just verified the following command, it worked. uuu.exe -b emmc imx-boot-imx95-a1-19x19-lpddr5-evk-sd.bin-flash_all
查看全文
ls1021a eTSEC tx timeout I have a LS1021A IOT and a prototype board based on this cpu. On both we use our boot loader. It works perfectly in the IOT board but on my board I get TX timeout on the Ethernet port. I get a few pings going and then tx timeout and more pings.  This makes tftp rarely possible. There are hardware difference of course. Our MAC is connected to a BCM54616S then to a LAN9514. The autonegotiation is limited to 100FD. TX timeout also happens in loopback mode. In order to transmit data, I had to set bit SGMII_AN bit in the TBI PHY on my boards while I did not have to on the IOT (IOT can negotiate at 1000FD). Not sure why the TX is so intermittent. Could it be related to this speed limitation? Re: ls1021a eTSEC tx timeout Hello, For 100FD SGMII , verify these items in your boot loader on the prototype board: Set LS1021A eTSEC for SGMII 100 Mbps ECNTRL[TBIM] = 1 ECNTRL[SGMIIM] = 1 ECNTRL[R100M] = 1 MACCFG2[I/F Mode] = 01 for 10/100 mode The LS1021A RM specifically notes setting R100M = 1 for SGMII 100 Mbps. Reset and program the internal TBI PHY The RM states that SGMII uses the TBI register set and that it is important to reset the TBI for all interface modes, including SGMII. Keep SGMII_AN set The TBI SGMII_AN bit is documented as “must be set to 1.” So the fact that your board only transmits after setting this bit is not surprising; it suggests your boot-loader initialization was incomplete for this PHY/MAC mode. Do not rely on 1G-style SGMII AN behavior at 100 Mbps There are known LS1021A reports where 100 Mbps SGMII operation shows “SGMII link is not ok” or intermittent no-packet behavior after link cycling, while 1G operation is clean. That does not prove your exact TX timeout root cause, but it makes 100FD SGMII configuration a strong suspect. The loopback result matters. If your “loopback mode” is external PHY loopback or SGMII-side loopback, the 100FD SGMII/TBI setup can still be involved. If it is internal MAC/eTSEC loopback , then the external BCM54616S/LAN9514 path is mostly out of the picture, and I would focus on eTSEC initialization, descriptor-ring handling, cache coherency, and TX halt/error status. For debugging, check the eTSEC TX halt status when the timeout occurs. The RM says the transmit halt bits are set when eTSEC is no longer processing transmit frames from a TxBD ring; repeatable causes include bus errors, invalid BD/data addresses, uncorrectable BD/data read errors, and TxBD programming errors such as Ready = 1 with length 0 . Also check whether you are seeing IEVENT_BSY ; NXP material describes BSY as dropped RX frames due to lack of buffers/software not servicing the BD ring fast enough, which is a software/BD-ring symptom rather than a pure SGMII electrical symptom. Recommended isolation sequence: 1. Force external PHY to 100FD, no autoneg toward copper if needed. 2. Force LS1021A MAC/eTSEC to SGMII 100 Mbps: TBIM=1, SGMIIM=1, R100M=1, MACCFG2 I/F mode=10/100. 3. Reset/reinitialize TBI after setting SGMII mode. 4. Set TBI SGMII_AN=1. 5. Confirm TBI link/AN status, eTSEC ECNTRL/MACCFG2, and PHY SGMII-side status. 6. On timeout, dump IEVENT, TX halt registers, DMA status, and TXBD ring contents. regards  Re: ls1021a eTSEC tx timeout Forgot to say my port is set for SGMII mode. Re: ls1021a eTSEC tx timeout Adding messages or 1ms delay in the send functions allows the correct transfer of data without loss. I added a DMA flush to the TX descriptors in the send function and this helps. Though, this should not be necessary considering the descriptors are allocated in uncached memory. It could be a defect in the MMU library to which I added LPAE support. Now I remember that a long time ago I removed the dma-coherent property in the enet device node and this was enough for the LS1021A-IOT to work. This is forcing a DMA flush while allocating uncached memory for the descriptors. But there was no cache flush in the send functions which updates the TX descriptors on each packet. Not sure why it does not work on my prototype (difference in frequency, DDR3L vs DDR4,...) Re: ls1021a eTSEC tx timeout Hi, Thank you for the detailed findings — the combination of workarounds you identified (1 ms delay, manual DMA flush, and removing dma-coherent ) is a textbook fingerprint of a cache alias problem. Here is the root cause explanation and the recommended fix path. Root cause: cached virtual alias over the TX descriptor region The LS1021A ENET DMA is a non-cache-coherent bus master — it reads DDR directly, with no visibility into the CPU cache. The correct operating model for gianfar on LS1021A is the non-coherent software-managed model: descriptors allocated in uncached memory, with explicit dma_sync_* calls whenever the CPU updates a descriptor field. What your LPAE changes most likely introduced is a page table entry for the descriptor physical address range that carries the wrong cache attribute — Normal Writeback instead of Device or Normal Non-cacheable. This creates two virtual aliases to the same physical memory with different cacheability: the allocation path (via dma_alloc_noncoherent ) maps it uncached, but the per-packet TX descriptor update path in the send function accesses it through a cached alias. The CPU writes the updated descriptor fields into the cache line, they never reach DDR, and the ENET DMA reads stale data and underruns. Why your three workarounds all mask the same defect 1 ms delay / message insertion: adds enough latency for the CPU writeback buffer to drain naturally under low load — timing-dependent, will fail under traffic or frequency change. Manual dma_flush in the send function: forces a cache clean-to-PoC before the DMA reads the descriptor — correct behaviour, but should not be necessary if the region is genuinely uncached. Removing dma-coherent from the enet device node: causes the kernel to call dma_map_single() / dma_sync_single_for_device() on each TX descriptor before submission, which explicitly cleans the cache — also correct, and explains why the LS1021A-IOT worked reliably without a send-path flush. The absence of the send-path flush is the missing piece. The LS1021A-IOT worked with dma-coherent removed because the kernel's DMA mapping layer inserted the sync automatically; your prototype does not have that path because the LPAE changes altered the descriptor region's cache attributes without re-introducing the sync. DDR3L vs DDR4 / frequency difference This is not the root cause. Different DRAM type and frequency change write latency and buffer drain timing, which is why the failure is more visible on your prototype — but the underlying defect is architectural and will be present on both boards under sufficient load. Recommended fix The correct and self-consistent fix is to combine both of the following: Keep dma-coherent removed from the enet device node (non-coherent model). This causes the kernel DMA layer to issue dma_sync_single_for_device() automatically before DMA ownership is transferred for descriptors allocated via dma_alloc_noncoherent . Add explicit dma_sync_single_for_device() calls in the TX send path at the point where TX descriptor fields ( status , data_length , data_pointer ) are written on each packet. This is the flush you added manually — but it should be formally placed as a dma_sync_single_for_device(dev, desc_dma_addr, sizeof(txbd), DMA_TO_DEVICE) before writing TDAR . This makes the model explicit and correct regardless of how the MMU attributes the descriptor region. Separately, audit the LPAE MMU library change for the AttrIndx / TEX+C+B fields assigned to the physical address range used for ENET descriptors. The descriptor pool should be mapped as Device-nGnRnE (strongly ordered) or Normal Non-cacheable — not Normal Writeback. You can verify the actual attributes in use with the kernel's ptdump debug interface by checking the virtual address of the descriptor pool after allocation. The DMA flush you added is not a workaround — it is the correct mechanism. The real defect is that it was absent from the send path in the first place, and the LPAE changes exposed this because they altered the effective cacheability of the region.   Regards
查看全文
MTC40F2046S1RC64BD2 Are you able to confirm if this mpn: MTC40F2046S1RC64BD2 is X-ray sensitive?  Re: MTC40F2046S1RC64BD2 That's not true. X-ray exposure is a common testing procedure and will not cause damage. We suggest you find a seller with a Certificate of Conformity (COC) for safety assurance.
查看全文
Support Request: HD-SDI Interface Using i.MX8M Plus LVDS Output Dear Sir, We are designing a system based on the NXP i.MX8M Plus processor and would like your guidance regarding the implementation of an HD-SDI interface. Our requirement is to support three HD-SDI outputs. We are planning to use the LVDS interface of the i.MX8M Plus and convert it to HD-SDI using the following devices: LMH0340SQE/NOPB – LVDS to HD-SDI Serializer 2 × LMH0324RTWT – 1-to-3 HD-SDI Distribution Amplifiers Could you please confirm whether the LVDS interface of the i.MX8M Plus is compatible with this architecture for generating three HD-SDI outputs? If this approach is not recommended or supported, could you please suggest an alternative solution for implementing three HD-SDI interfaces while continuing to use the i.MX8M Plus processor? We would prefer to retain the i.MX8M Plus in our design, as it satisfies all of our other system requirements. We would appreciate your recommendations and any reference designs or application notes that may help us implement this interface successfully. Thank you for your support. We look forward to your guidance. Best regards, Samudralankaiah Jampani Analog(ADC|CMP|DAC|OpAmps) Board Design MCXA MCXC Re: Support Request: HD-SDI Interface Using i.MX8M Plus LVDS Output Hello, Unfortunately I'm not really used to this kind of use case, as I was investigating the part you have shared it seem that it is expected to use with an FPGA not an LVDS channel, so I'm not sure that you may use this interface for that. Maybe using a different bridge or other of the interfaces in the i.MX8MP or even another layer (FPGA) in between could be a solution. Best regards/Saludos, Aldo.
查看全文
ICODE SLI 无法切换到 ICODE SLIX 我的客户一直在使用我提供的 ICODE SLI 芯片,但该芯片已经停产了。我们正在尝试切换到 ICODE SLIX,但客户的 RFID 阅读器无法识别它。 Re: ICODE SLI can't be switch to ICODE SLIX 你好, ICODE SLIX 旨在向后兼容 ISO15693 级别的 ICODE SLI,因此读卡器至少应该在盘点期间检测到 SLIX UID。如果读卡器无法识别,请先检查故障是出在射频存货层面还是出在应用程序的标签识别逻辑层面。常见原因包括 AFI/UID 过滤、硬编码的 SLI 产品识别、旧的读卡器固件,或者在迁移过程中使用 SLIX 特有的网络安全/功能。对于第一个测试,禁用 AFI 过滤和标签白名单,执行标准的 ISO15693 清单,读取 UID/DSFID/AFI,然后将应用程序的接受逻辑与旧的 SLI 标签进行比较。 此致 Re: ICODE SLI can't be switch to ICODE SLIX 请将此帖移至合适的社区。这不是Coldfire或68k零件。
查看全文
i.MX8M Plus - SPDIFプロトコル実装例 こんにちは、チームのみなさん。 どなたか、i.MX8M plusでSPDIFプロトコルを実装し検証する方法を教えていただけませんか? Re: i.MX8M Plus - SPDIF Protocol Implementation Example 最もシンプルな i.MX 8M Plus S/PDIF実装については、i.MX Audio Board / MCIMX8M-AUDを最も近いNXPの参照ハードウェアとして使用し、ベース i.MX 8M Plus EVK単独ではありません。オーディオボードは8M Plus i.MX をサポートし、RCAおよびTOSLINKコネクタを備えたS/PDIF I/Oを提供し、最大192 kHzまでのTOSLINK対応であることが文書化されています。 推奨されるシンプルなアプローチ: 可能であれば、まず光S/PDIFを使用してください。 最も簡単なハードウェアパス:i.MX8MP SPDIF_OUT →光式TOSLINKトランスミッタ。 受信用:光TOSLINK受信モジュール→ i.MX8MP SPDIF_IN。 これにより、同軸75Ωライン駆動、トランス/カップリング、および接地に関する問題を回避できます。 i.MX 8M PlusのS/PDIFピンをIOMUX経由で使用する i.MX 8M PlusオーディオサブシステムはSPDIFの入出力を備えています。 リファレンスマニュアルには、選択可能なパッドのAUDIOMIX_SPDIF1_OUTとAUDIOMIX_SPDIF1_INのIOMUXオプションが示されています。 Linuxでは対応するIOMUX定義にはMX8MP_IOMUXC_SPDIF_TX__AUDIOMIX_SPDIF_OUTとMX8MP_IOMUXC_SPDIF_RX__AUDIOMIX_SPDIF_INが含まれます。 同軸RCAが必要な場合は SoCピンを直接RCAのラインドライバーのように扱わないでください。 選択したトランスミッタ/インターフェース回路ごとに適切な75 Ω S/PDIF同軸ケーブル出力ネットワーク/結合を追加してください。 光ファイバー方式は、通常、よりシンプルで安全な最初の実装方法です。 参考資料 MCIMX8M-AUD / i.MX オーディオボード:i.MX 8MファミリのS/PDIF I/OおよびRCAおよびTOSLINKに最適なNXPリファレンス。 i.MX 8M Plusリファレンスマニュアル:AUDIOMIX_SPDIF1_INおよびAUDIOMIX_SPDIF1_OUT用のpinmux / IOMUXセットアップ。 i.MX 8M Plusのデータシート:クロックのハイ/ロータイミングを含む、S/PDIFのタイミングパラメータが記載されています。 最も単純な設計では、AUDIOMIX_SPDIF1_OUT/INを光TOSLINKモジュールにルーティングし、MCIMX8M-AUDをNXPのS/PDIF I/O挙動の基準点として使用します。 Re: i.MX8M Plus - SPDIF Protocol Implementation Example こんにちは、Yipingwangさん、 SPDIFを最もシンプルに実装するための参考回路図を教えていただけませんか? Re: i.MX8M Plus - SPDIF Protocol Implementation Example i.MX8M Plusで既存のLinux ALSA Audio XCVR / S/PDIFドライバーを使用;通常、S/PDIFプロトコルを最初から実装することはありません。i.MX8M Plus Audio XCVRはeARC、ARC、S/PDIFモードをサポートし、LinuxのS/PDIF対応では、ALSAを通じてTx用の再生デバイスとRx用のキャプチャデバイスを1台公開します。 推奨される実装方法: カーネルドライバーを有効にしてください有効化: CONFIG_SND_IMX_SPDIF メニューパス: コピー デバイスドライバー -> サウンドカードサポート -> 高度なLinuxサウンドアーキテクチャ -SoCオーディオサポート> ALSA - フリースケール i.MX CPU向けの> SoC オーディオ - > S/PDIF対応 i.MX ボード向けのSoCオーディオサポート ドキュメント化されたDTバインディングは、ドキュメント/devicetree/bindings/sound/fsl spdif.txtおよびドキュメント/devicetree/bindings/sound/imx-audio-spdfif.txtにあります。 デバイスツリーの設定i.MX8M Plusでは、xcvrオーディオブロックを使い、サウンドカード/DAIリンクを有効にしてください。代表的な構成例は以下のとおりです。 サウンドトランスフォーマー { 互換 = 「FSL,IMX-オーディオカード」; model = "imx-audio-xcvr"; pri-dai-link { リンク名 = "XCVR PCM"; CPU { sound-dai = <&xcvr>;         }; }; }; &xcvr { #sound-dai-cells = <0>; pinctrl-names = "default"; pinctrl-0 = <&pinctrl_xcvr>; ステータス = "正常"; }; Tx ピンの多重化については、文書化された例の 1 つで MX8MP_IOMUXC_SPDIF_TX__AUDIOMIX_SPDIF1_OUT が使用されています。 ボードのルーティングやジャンパーを確認してくださいNXPオーディオボードを使用する場合、意図するS/PDIFパスの物理ルーティングを設定します。i.MX8M Plusの場合、J1500=1-2は同軸コネクタをi.MX8M Plusにルーティングし、J1500=4-5は光コネクタをi.MX8M Plusにルーティングします。CPLD/HDMIカードを経由してルーティングする場合、J2511=1-3は「i.MX 8M PlusからCPLD、そしてHDMIカードへ」として文書化されています。 ALSA / IEC958を正しく使いましょうS/PDIF Txドライバーは32、44.1、48 kHzのサンプリングレートをサポートし、S16_LEおよびS24_LEフォーマットに対応しています。24ビット出力の場合、ファイルは1チャネルフレームあたり32ビットを使用し、有効な24個のLSBのみを使用します。パスが生のPCMではなくIEC958サブフレームを想定する場合は、ユーザー空間でPCMからIEC958への変換を行い、例えばALSA PCMプラグインを使って行います。 検証手順: aplay -l arecord -l これらを使用して、S/PDIF再生/キャプチャカードおよびデバイスIDを特定します。ドキュメントには、S/PDIFデバイスがIMXSPDIF[imx-spdif]のようなALSAカードとして表示され、デバイス0: S/PDIF PCMとして表示されています。 トランザクション検証: aplay -D hw: , audio48k24S.wav リファレンス検証方法 は、M-Audio Transit USBサウンドカードとWaveLabを組み合わせた外部の光S/PDIF レシーバ を使用し、ストリームを外部に録音して再生して正確性を確認します。 処方箋の検証: arecord -D hw: , -c 2 -d 20 -r 48000 -f S24_LE record.wav レコードに渡されるサンプルレートは、入力されるS/PDIFストリームのサンプルレートと一致している必要があります。Rxの場合、アプリケーションフローはS/PDIF Rx PCMデバイスを開き、内部DPLLが入力ビットストリームにロックされるのを待ち、入力サンプリングレートを取得し、チャネル/フォーマット/レートパラメータを設定し、準備してキャプチャをトリガーすることです。 プロトコルレベルのチェックには、以下を使用してください。 iecset -c iecsetはIEC958ステータスビットの設定またはダンプに記載された標準ユーティリティであり、ドライバはALSA制御インターフェースを通じてチャネル状態処理も公開します。 i.MX8M Plus EVKスタイルの検証については、NXPはimxaudioxcvrカードを用いたループバックスタイルのLinuxテストも記録しており、例えばimxaudioxcvrからの録音とwm8960audioへの再生などがあります。 arecord -Dsysdefault:CARD=imxaudioxcvr -c2 -r48000 -fS32_LE -twav | \ aplay -Dsysdefault:CARD=wm8960audio 簡単に言うと、i.MX S/PDIF / XCVR ALSAドライバーを有効にし、xcvrデバイスツリーとボードルーティングを設定し、aplay 、arecord、iecset 、および外部の光/同軸S/PDIFソースまたはシンクでTx/Rxを検証します。
查看全文
Facemesh Landmark 模型 ptq 转换中的性能下降 本仓库中使用的是 NXP 在 ptq 之后发布的 Google FaceMesh 模型: nxp-demo-experience-demos-list/downloads.json 位于 lf-6.12.3_1.0.0 · nxp-imx-support/nxp-demo-experience-demos-list 但该模型基于谷歌旧的 FaceMesh 模型,该模型有 468 个地标点。 现在我们想升级到谷歌新的 FaceMesh 模型,它有 478 个地标点。我们希望在 iMX 95 FRDM 板 NPU 上运行此程序。所以,我们想把它量化。我们使用的是NXP的eIQ-neutron-sdk-linux-3.1.3量化该模型。 经过量化之后,我们发现模型性能显著下降,几乎无法实际使用。 最初我们使用 MIN-MAX 选项对其进行量化。那个模型根本没法用。然后我们尝试使用百分位数选项,发现将百分位数设置为 95 时性能更好(即使这是回归器的输出)。 但这仍然无法带来理想的性能。 1)NXP为旧版FaceMesh(468)模型创建ptq文件时,使用了MIN-MAX选项吗?或者百分位数? 2)量化后性能急剧下降时,我们还需要检查其他方面吗? 3) 我们使用 CelebA 数据集进行性能分析,在 scripts 目录中使用 serialize_image.py 脚本并设置了模型特定选项。我们应该运行完整的媒体管道并创建校准数据集,还是应该修改 serialize 脚本? 提供的选项 serialize_image.py : -i //218 x 178 正面 RGB 图像 -o -f bin -t float32 -m 0到1 -s 256,256 -布局 NHWC -co RGB tflite-profiler: --input --dataset --输出 tflite-quantizer: --input --profile --quantize-inputs=false --quantize-outputs=false --quantization-calibration-method= //最小值、最大值或百分位数 Re: Performance degradation in Facemesh Landmark model ptq conversion 嗨@dhilshad , 感谢您联系恩智浦技术支持! 1)很遗憾,我们目前没有相关信息。 2)这种行为是预期的。量化只是部署过程的一部分;将模型转换为嵌入式硬件上执行并进行优化还涉及几个额外的步骤,例如图优化、运算符映射、硬件特定的转换和运行时验证。因此,即使模型已经量化,模型的行为和性能也可能发生变化。 对于新的设计和评估,我建议使用 eIQ Olive,因为它为 NXP i.MX 平台上的模型优化和部署提供了一个更现代化的框架。它包括更新的工作流程和对当前机器学习部署场景的改进支持。 更多信息请参考以下教程和文档: https://eiq.nxp.com/learning-hub/tools/olive/index.html 这些资源涵盖了在 i.MX 设备上部署机器学习模型的推荐工作流程和最佳实践。 此致, 查维拉 Re: Performance degradation in Facemesh Landmark model ptq conversion @Chavira你好,谢谢你的回复。并指出相关文档 在这里需要澄清的是,我们主要关注的是模型的准确性。对于 FaceMesh 模型,我们发现输出的特征点精度不足以满足我们的应用需求。正如我之前所说,我们发现保持 95 百分位截断值比 MIN MAX 截断值略好一些。但仍然无法与 NXP 的 ptq 模型(FaceMesh 468)的精度相提并论。 我们还有一点需要说明: 1)我们尝试只提供生产环境中的 8 个样本作为代表性数据集。这样略微改善了结果。然后我们添加了来自同一环境的 250 张图像,并进行了分析和量化。但这导致准确率下降。 你知道这种行为可能是什么原因造成的吗? 2)另外,NXP 是否已经将 Google 的新 FaceMesh 模型(具有 478 个地标)转换为 ptq 模型?
查看全文
S32K148 FlexCAN 仅输出 SOF 脉冲,然后进入总线关闭状态 我用S32DS开发了这个程序。当尝试发送 CAN 帧时,TX 引脚上只会输出一个短的低电平脉冲,后续的 ID 和数据位会被截断,因此无法发送完整的帧。USB-CAN 分析仪未收到任何数据,FlexCAN 控制器直接进入总线关闭状态。 我已经检查了时钟配置和寄存器值,并测试了不同的 CAN 通道,但问题仍然没有解决。我想找出哪个配置参数设置错误。感谢您的帮助。 Re: S32K148 FlexCAN Only Output SOF Pulse then Enter BusOff 嗨,朱利安, 感谢你的回复。我想更正并补充我之前匆忙写成的消息中的一些重要细节。 主板:这是第三方主板(不是 NXP EVB),型号为 S32K148_REV2_Q144。值得注意的是:我发现卖家提供的原理图存在错误(标注的收发器位置与实际 PCB 丝印不符),因此该电路板的参考设计文档可能并不完全可靠。 官方 CAN 示例:我尝试构建 Can_example_S32K148,但遇到了与 CAN 本身无关的环境问题(缺少工具链/包含路径,最终 Port_Ci_Port_Ip.h 和 Port_Ci_Port_Ip_Cfg.h 之间出现版本不匹配错误——“不同的供应商 ID”/“AutoSar 版本号不同”)。这看起来像是 RTD 包版本与我的项目不匹配,而不是 IDE 版本问题。我会尝试解决这个问题,但我认为这与硬件问题的核心无关。 新证据(来自您已审阅过的我自己的项目):自从我上次留言以来,我使用逻辑分析仪进行了更深入的验证: MB8 内容 100% 正确— 直接从 CDD_CanTransmit() 之后的寄存器读取:CS=0x0C080000 (CODE=0xC 待定,DLC=8),ID=0x00400304 (>>18 = 0x10,与配置匹配),DATA=0x01020304/0x05060708 (与我的 8 字节有效载荷完全匹配)。 引脚上的 TX 信号也正确——同时探测 PTE5 和收发器的 TXD 输入(200MHz 逻辑分析仪),两个波形相同,证实 PCB 走线良好。 但传输在大约 8-9 位转换后中止(大致为 SOF + 几个仲裁位),控制器随后进入总线关闭状态(ESR1 确认 FLTCONF=11,TXERRCNT 每次尝试递增)。 即使正确连接了 USB-CAN 分析仪并启用了 120Ω 终端(总线未浮空), CANH/CANL 也显示为零活动。作为对照测试,我在另一块已知可正常工作的 STM32 板上运行了相同的设置(浮空与终端),终端后 CANH 显示出了正确的转换。在我的 S32K148 板上,在相同的端接条件下,CANH/CANL 保持完全平坦。 在 CAN1 上也出现了同样的结果(不同的引脚/收发器)。 由于 MCU 端的 TXD 信号在收发器输入端之前均已确认正常,但即使正确端接,CANH/CANL 信号也始终没有响应,因此我怀疑是收发器输出级(或两个通道共用的某个部分,例如……)出现了问题。电源瞬态行为——我只能用逻辑分析仪检查,无法用示波器检查。 问题: “TXD 在收发器输入端正确,但 CANH/CANL 在正确端接下完全平坦”是否更强烈地表明收发器硬件故障,还是存在其他常见的板级问题(使能/待机电路、电源去耦)也可能导致这种症状? 当总线上没有实际活动时,FlexCAN 是否应该在发送完前几个仲裁位后中止(而不是完成整个帧并在 ACK 时失败)?我想确认一下我对位监控机制的理解是否正确。 对于示例项目中的 RTD 版本不匹配问题——是否有办法检查哪个 RTD 版本与给定的 S32 配置工具版本匹配,以便我可以获取匹配的示例包? 再次感谢您的帮助。 此致敬礼,艾普丽尔 Re: S32K148 FlexCAN Only Output SOF Pulse then Enter BusOff 嗨,朱利安, 我非常惊讶,也很感谢您回复我的问题。   我使用的是自己设计的硬件板;只有电源电路与官方 EVB 原理图不同,而其余电路与参考设计一致。 我测试了官方的 CAN 示例项目。我只配置了 CAN0 引脚,而没有启用和配置 MCAL 层中的 PORT 模块,但项目一直编译失败。   具体的编译错误是: “f ../board/Port_Ci_Port_Ip_Cfg.h:47:10: 致命错误: Port_Ci_Port_Ip_Types.h: 没有该文件或目录”。   我的自定义项目文件中已有此头文件,但是导入此官方示例项目后,代码生成过程中并未自动生成此头文件。 缺少头文件错误是否可能是由于 IDE 软件版本不匹配造成的?目前我正在使用S32DS 为 S32 平台进行开发,现在我正在下载S32DS for ARM 2.2.2来切换开发环境。 期待您的指导。   顺祝商祺!   四月 Re: S32K148 FlexCAN Only Output SOF Pulse then Enter BusOff 你好@April , 从你的项目来看,配置和流程似乎都是正确的。请问您使用的是恩智浦半导体的S32K148EVB芯片,还是您自己设计的芯片? 您是否尝试过测试 RTD 中包含的 Can_example_S32K148 项目?您可以简单地添加 CAN0 引脚并禁用环回模式以启用 Tx/Rx 并测试该程序。 最后,您是否确认两个节点(S32K148 和 CAN 分析仪)都设置为相同的位时序和协议配置(CAN 与 CAN FD)?您可以使用以下工具来计算值: MPC5xxx/S32Kxx/LPCxxxx:CAN / CAN FD 位定时计算。 如果您使用的是自定义设计,您可以参考S32K148 EVB 的原理图和S32K1xx 硬件设计指南,了解 CAN 接口设计和建议。 此致, 朱利安 Re: S32K148 FlexCAN Only Output SOF Pulse then Enter BusOff 你好@April , 1. 是的,这表明是收发器故障,而不是模块配置问题。能否确认一下您的定制设计中使用的是哪种收发器? 我建议检查 STB、EN、S、RS、WAKE、INH 或类似引脚与实际安装的收发器是否匹配。 S32K148 EVB 使用UJA1132HW ,但是,如果您使用的是TJA1043之类的芯片,则必须将其配置为正常模式( STB_N = 高EN = 高)。 2. 是的,如果收发器实际上没有驱动总线,那么在几个仲裁位之后提前中止是合理的。 3. 通常情况下,“不同的供应商 ID”/“AutoSAR 版本号不同”错误会在导入项目并尝试使用不同的 RTD / S32 配置工具版本更新配置时出现;但是,如果您只是从“文件 -> 新建 -> 从示例创建 S32DS 项目”导入示例,则应该不会有任何兼容性问题: 从您分享的项目来看,您使用的是 S32K1 RTD 3.0.0。然而,当我导入 QLP04 项目时,从属性中可以看到配置的是 GCC 11.4: 根据 RTD 版本说明,3.0.0QLP04 仅支持 NXP GCC 10.2: 我不确定你是如何导入和编译这个项目的,但请确保你至少安装了 S32DS 3.6.4 版本。仅安装了一个RTD软件包。S32DS不支持同时安装多个RTD版本。 此致, 朱利安 Re: S32K148 FlexCAN Only Output SOF Pulse then Enter BusOff 你好@April , 感谢您提供的补充信息。 1. 关于 TJA1051,确实该收发器只有 S 引脚用于配置正常模式,但是,请检查您是否使用的是TJA1051T/E衍生型号,因为该型号有一个额外的 EN 引脚,您必须将其拉高: 2. “找不到文件”错误很可能是由于端口配置错误,从而导致工具生成了错误的代码。您在端口容器中遇到的错误是由于“引脚”功能组名称应该以“端口容器名称”+“外围设备功能组名称”的形式命名造成的,在您的情况下应该是“ PortContainer_0_VS_0 ”。 在申请RMA之前,能否请您测试一下我附上的项目?这是 MCAL 中的一个简单的测试代码,它使 Rx 以中断模式运行,Tx 以轮询模式运行。成功回波 10 帧后,绿色 LED 指示灯会切换状态。 我使用 PCAN-USB 分析仪,通过 J11 CAN 接头对该程序进行了测试,设置如下: 我可以看到帧已成功回放,并且绿色 LED 指示灯每 10 帧切换一次: 由于我使用的是 S32K148-EVB,因此不需要启用收发器,但是,在您的设置中,请检查TJA1051 是否已正确启用(以及是否还需要启用 EN 引脚)。 此致, 朱利安 Re: S32K148 FlexCAN Only Output SOF Pulse then Enter BusOff 嗨,朱利安, 再次感谢您的耐心等待——自从我上次发消息以来,又有一些更新。 收发器检查:我仔细查看后确认它是TJA1051 ,而不是 UJA1132 系列 SBC。这个只有一个使能引脚(S 引脚),在我的板上硬连接到地(= 正常模式),所以你提到的多引脚 STB_N/EN 逻辑在这里并不适用——控制电路的这一部分看起来已经是正确的了。 与第二个独立项目进行交叉验证:我为该板(从经销商处购买)构建并运行了一个完全不同的 CAN 演示,使用了较旧的 Processor Expert/S32 SDK 堆栈 — can_pal — 而不是 RTD/AUTOSAR。按下按钮后,CAN_Send() 函数被正确调用,但我注意到返回值始终为 STATUS_BUSY (0x002),这意味着之前的传输实际上从未完成。就像我的 RTD 项目一样,USB-CAN 分析仪在所有三个通道上都没有接收到任何信号。现在我有两个完全独立的驱动程序堆栈,它们都给出了相同的结果,这让我相当确信这不是我这边的软件/配置问题。 关于官方示例项目:我按照您的建议将 GCC 版本切换回 10.2,但在构建过程中仍然遇到同样的“文件未找到”错误。我进一步研究了一下,现在怀疑这可能与端口模块(MCAL 层)未完全配置有关——似乎存在一个与端口模块和引脚工具的功能组链接方式相关的验证错误,但我无论尝试什么都无法正确配置它。 它们就是一个例子: 这是我之前自己搭建的项目的一部分: 鉴于目前的情况——控制引脚接线看起来正确,引脚上的 TXD 也已确认正确,并且两个独立的软件堆栈在所有三个通道上都显示出一致的“无总线活动”/传输卡顿行为——您认为这是否足以将其视为硬件故障并进行 RMA,或者还有其他值得先检查的地方吗? 再次感谢你在这件事上提供的帮助。 此致敬礼,艾普丽尔 Re: S32K148 FlexCAN Only Output SOF Pulse then Enter BusOff 你好@April , 我很高兴现在一切都按预期运行了! 请问之前的错误原因是什么?是简单的硬件连接问题吗? 祝你今天也过得愉快! 此致, 朱利安 Re: S32K148 FlexCAN Only Output SOF Pulse then Enter BusOff 你好,朱利安, 我迫不及待地想告诉你,现在一切都完美运行了!我非常激动地与大家分享这个好消息。我已经订购了全新的MCU板和CAN收发器进行重新测试,这次通信运行完美无瑕。原来我之前遇到的持续 BusOff 错误完全是硬件故障。 我还加载了您附加的测试项目,它也运行良好。你的示例代码可以像你描述的那样流畅地发送和接收 CAN 帧。 我非常感谢您这些天来给予我的所有耐心指导。我完全被这个问题难住了,独自一人根本无法解决这个问题,是你的详细回复帮我摆脱了困境。 祝您身体健康,工作顺利,天天幸福! 此致, 四月 Re: S32K148 FlexCAN Only Output SOF Pulse then Enter BusOff 你好@Julián_AragónM , 哈哈,不是线路问题。原有的 TJA1051 收发器模块存在缺陷,导致了 BusOff 问题。 再次非常感谢您的帮助!^_^ 此致, 四月
查看全文
IPCFのバージョンに関する問題 私は以下のRTDバージョンを使用しています:SW32K3_S32M27x_RTD_R21-11_6.0.0_QLP01&04、IPCFバージョン:SW32K3_IPCF_4.2.1_D2504、EBバージョン:29.0。Excampleにインポートする際...プロジェクト「IPCF_AutosarOS_S32K358_M7_0」でエラーが発生しました。内容は以下のとおりです。 エラー (11061) モジュール OS TS T40D34M413R184 をインストールしていません - プロジェクト IPCF AutosarOS S32K358 M7 0 のモジュール構成を作成できません 0 (11061) モジュール「pc TS T40D34M4210R0」がインストールされていないため、プロジェクト「IPCF AutosarOS $32K358 M7 0」のモジュール構成を作成できません。 0 (11061) モジュールリソースTS T40D34M5010Roをインストールせずにプラグインします - プロジェクトIPCF AutosarOS $32K358 M7 0°のモジュール構成を作成できません @ (11061) モジュール「BaseNXP TS T40D34M50I0RO」がインストールされていません - プロジェクト IPCF AutosarOS $32K358 M7 0 のモジュール構成を作成できません @ (11061) モジュール「Mcu TS T40D34M5010R0」を含むプラグインがインストールされていません - プロジェクト「IPCF AutosarOS $32K358 M7 0」のモジュール構成を作成できません 適切なIPCFまたはEBバージョンを使用して、この問題を解決するにはどうすればよいでしょうか? Re: IPCF版本问题 こんにちは@liyongfeng 現在EB Tresos環境にインストールされているプラグインのバージョンを教えていただけますか? また、RTDパッケージを再インストールして、その後も問題が続くか確認してみてはどうでしょうか? BR、VaneB
查看全文
マーキングの詳細 マーキングの意味を教えてください。 MPN: PCA9553DP/01,118 用 04 01 616
查看全文
NFCカードについて助けが必要です 最近、AmazonでMIFARE Classic 1Kに対応しているACR122U-A9と13.56MHzのRFID近接IDカードキータグを買いました。書き込み可能な再書き込み可能なCUIDフォブタグです。MWT V.1.6.8424.424.63をインストールして、4tagくらいは動作しましたが、今はカードを読み取れないか、64で63くらいで止まってしまいます。どなたか助けていただけますか?私は本当にテクノロジーにはあまり詳しくありません NFCリーダー・ライブラリ Re: I need help with my NFC card お世話になります。 弊社製品をご利用いただきありがとうございます。 ACR122U-A9の使用についてですが、公式ページでは新しいデザインにはこのリーダーは推奨されていないと記載されているのに気づきました。私の推奨は、推奨されサポートされているものに移行することです。 インストールされたミドルウェアについてですが、公式ページで見つけることができなかったので、どこで入手されたのか教えていただけますか? MIFARE Classicに対応しているタグが4タグのように動作するというのはどういう意味か理解したいです。MIFARE ClassicカードはISO14443〜3コマンドしかサポートできません。正確なコマンドの説明については データシート をご覧ください。 もしプロジェクトについてもっと詳しく教えていただければ、 MIFARE Classic カードもセキュリティ上の理由で推奨されていないので、より良いおすすめができるかもしれません。
查看全文
MTC40F2046S1RC64BD2 请问您能否确认一下这个产品型号: MTC40F2046S1RC64BD2是否对X射线敏感? Re: MTC40F2046S1RC64BD2 那不是真的。X射线照射是一种常见的检测程序,不会造成损害。为了功能安全起见,我们建议您寻找拥有合格证书(COC)的卖家。
查看全文
ICODE SLI can't be switch to ICODE SLIX My client has been using the ICODE SLI chip I provided, but this chip has been EOL. We are trying to switch to the ICODE SLIX, but the client's RFID reader cannot recognize it. Re: ICODE SLI can't be switch to ICODE SLIX Hello, ICODE SLIX is intended to be backward compatible with ICODE SLI at the ISO15693 level, so the reader should at least detect the SLIX UID during inventory. If the reader cannot recognize it, please first check whether the failure is at RF inventory level or in the application’s tag-identification logic. Common causes are AFI/UID filtering, hardcoded SLI product recognition, old reader firmware, or use of SLIX-specific security/features during migration. For the first test, disable AFI filtering and tag whitelisting, perform a standard ISO15693 inventory, read UID/DSFID/AFI, then compare the application’s acceptance logic against the old SLI tag. Regards Re: ICODE SLI can't be switch to ICODE SLIX Please move this thread to the appropriate community. This isn't a Coldfire or 68k part.
查看全文
LX2160A: Pull down value on receiver for SerDes lanes not used Hello, Chip: LX2160A The application note AN5407 specifies pull down on SerDes lanes if not used:  If some SerDes lanes are a no-connect, pull down their receiver pins to GND. Could you tell me the pull down value please? Or should I connect the receiver pins directly to GND? Thanks. Re: LX2160A: Pull down value on receiver for SerDes lanes not used Hello, The AN5407 language "pull down their receiver pins to GND" is intentionally ambiguous about method — NXP's clarification is that a direct 0 Ω connection to GND is the correct and preferred approach. SerDes power-down Even with the RX pins tied to GND, if the SerDes block remains powered, AN5407 also recommends powering down unused lanes via firmware: configure the General Control 0 register during the PBI phase to power down unused SerDes lanes. If the entire SerDes block is already powered down, individual lane power-down is not needed Regards
查看全文
ls1021a eTSEC 发送超时 我有一个 LS1021A 物联网芯片和一个基于该芯片的原型板。两者都使用引导加载程序。 它在物联网板上运行完美,但在我的板上,以太网端口出现TX超时错误。我发出几个 ping 请求后,发送超时,然后又发出更多 ping 请求。这使得TFTP几乎无法使用。 当然,硬件方面也存在差异。我们的 MAC 连接到 BCM54616S,然后连接到 LAN9514。自动协商的上限为 100FD。TX超时在环回模式下也会发生。 为了传输数据,我必须在我的板子上的 TBI PHY 中设置 SGMII_AN 位,而 IOT 则不需要这样做(IOT 可以协商 1000FD)。 不确定为什么TX信号如此不稳定。这是否与速度限制有关? Re: ls1021a eTSEC tx timeout 你好, 对于 100FD SGMII,请在原型板的引导加载程序中验证以下项目: 设置 LS1021A eTSEC 用于 SGMII 100 Mbps ECNTRL[TBIM] = 1 ECNTRL[SGMIIM] = 1 ECNTRL[R100M] = 1 MACCFG2[I/F Mode] = 01 表示 10/100 模式 LS1021A RM 特别指出,对于 SGMII 100 Mbps,应将 R100M = 1 。 重置和编程内部 TBI PHY。RM 指出 SGMII 使用 TBI 寄存器集,并且对于所有接口模式(包括 SGMII)重置 TBI 非常重要。 保持 SGMII_AN 设置为 TBI SGMII_AN 位“必须设置为 1”。因此,您的电路板只有在设置此位后才会发送数据,这并不奇怪;这表明您的引导加载程序初始化对于此 PHY/MAC 模式不完整。 不要依赖 100 Mbps 下的 1G 式 SGMII AN 行为。已知 LS1021A 报告显示,100 Mbps SGMII 操作在链路循环后会出现“SGMII 链路不正常”或间歇性无数据包行为,而 1G 操作则正常。这并不能证明您的 TX 超时的确切根本原因,但这足以证明 100FD SGMII 配置是一个强烈的怀疑对象。 回环结果很重要。如果您的“环回模式”是外部 PHY 环回或 SGMII 侧环回,则 100FD SGMII/TBI 设置仍然可能参与其中。如果是内部 MAC/eTSEC 环回,那么外部 BCM54616S/LAN9514 路径基本无关紧要,我会重点关注 eTSEC 初始化、描述符环处理、缓存一致性和 TX 停止/错误状态。 为了进行调试,请检查超时发生时 eTSEC TX 停止状态。RM 表示,当 eTSEC 不再处理来自 TxBD 环的发送帧时,会设置发送停止位;可重复出现的原因包括总线错误、无效的 BD/数据地址、无法纠正的 BD/数据读取错误以及 TxBD 编程错误,例如 Ready = 1 长度为 0 。还要检查是否看到 IEVENT_BSY ;NXP 的资料将 BSY 描述为由于缓冲区不足/软件无法足够快地服务于 BD 环而导致的 RX 帧丢失,这是一种软件/BD 环的症状,而不是纯粹的 SGMII 电气症状。 推荐的分离步骤: 1.强制外部PHY为 100FD ,如果需要,不进行铜缆自动协商。2.强制LS1021A MAC / eTSEC 为SGMII 100 Mbps : TBIM = 1 , SGMIIM = 1 , R100M = 1 , MACCFG2 I / F模式= 10 / 100。3. 设置 SGMII 模式后 RESET / 重新初始化 TBI 。4.设置TBI SGMII_AN = 1。 5.确认TBI链路/ AN状态、 eTSEC ECNTRL / MACCFG2和PHY SGMII侧状态。6.超时时,转储IEVENT 、 TX停止寄存器、 DMA状态和TXBD环内容。 此致敬礼 Re: ls1021a eTSEC tx timeout 忘了说了,我的端口设置为SGMII模式。 Re: ls1021a eTSEC tx timeout 在发送函数中添加消息或 1 毫秒延迟,可以确保数据正确传输而不丢失。 我在发送函数中为 TX 描述符添加了 DMA 刷新,这很有帮助。不过,考虑到描述符是在非缓存内存中分配的,这应该不是必要的。这可能是我添加了 LPAE 支持的 MMU 库的缺陷。 现在我想起来了,很久以前我删除了 enet 设备节点中的 dma-coherent 属性,这足以让 LS1021A-IOT 工作。这样会在为描述符分配未缓存内存时强制执行 DMA 刷新。但是发送函数中没有缓存刷新,无法更新每个数据包的 TX 描述符。不确定为什么在我的原型机上不起作用(频率不同,DDR3L 与 DDR4 的区别……) Re: ls1021a eTSEC tx timeout 您好, 感谢您提供的详细调查结果——您发现的解决方法组合(1 毫秒延迟、手动 DMA 刷新和删除 dma-coherent )是缓存别名问题的典型特征。以下是根本原因分析和推荐的修复方案。 根本原因:TX描述符区域中缓存的虚拟别名 LS1021A ENET DMA 是一个非缓存一致性总线主控器——它直接读取 DDR,无法访问 CPU 缓存。LS1021A 上 gianfar 的正确操作模型是非一致性软件管理模型:描述符分配在非缓存内存中,每当 CPU 更新描述符字段时,都会显式调用 dma_sync_* 。 您的 LPAE 更改最有可能引入的是描述符物理地址范围的页表项,该条目携带错误的缓存属性——普通写回而不是设备或普通不可缓存。这为同一物理内存创建了两个具有不同缓存性的虚拟别名:分配路径(通过 dma_alloc_noncoherent )将其映射为未缓存,但发送函数中每个数据包的 TX 描述符更新路径通过缓存别名访问它。CPU 将更新后的描述符字段写入缓存行,这些字段永远不会到达 DDR,导致 ENET DMA 读取到过时的数据并出现欠载。 为什么你的三种变通方案都掩盖了同一个缺陷 1 毫秒延迟/消息插入:在低负载下,增加足够的延迟,使 CPU 回写缓冲区自然耗尽——与时间相关,在流量或频率变化时会失效。 发送函数中的手动 dma_flush :强制在 DMA 读取描述符之前执行缓存清理到 PoC 的操作——这是正确的行为,但如果该区域确实没有缓存,则无需执行此操作。 从 enet 设备节点中移除 dma-coherent :导致内核在提交之前对每个 TX 描述符调用 dma_map_single() / dma_sync_single_for_device() ,从而显式地清除缓存——这也是正确的,并解释了为什么 LS1021A-IOT 无需发送路径刷新即可可靠地工作。 缺少发送路径刷新是关键所在。LS1021A-IOT 在移除 dma-coherent 后可以正常工作,因为内核的 DMA 映射层会自动插入同步信号;你的原型没有这条路径,因为 LPAE 的更改改变了描述符区域的缓存属性,而没有重新引入同步信号。 DDR3L 与 DDR4 的频率差异 这不是根本原因。不同的动态随机存取存储器(DRAM)类型和频率会改变写入延迟和缓冲区漏电时间,这就是为什么故障在您的原型上更明显的原因——但根本缺陷是架构上的,在足够的负载下,两个板上都会出现这种缺陷。 推荐修复方案 正确且自洽的解决方案是将以下两种方法结合起来: 将 dma-coherent 从 enet 设备节点中移除(非相干模型)。这导致内核 DMA 层在通过 dma_alloc_noncoherent 分配的描述符的 DMA 所有权转移之前自动发出 dma_sync_single_for_device() 。 在 TX 发送路径中,于每个数据包上写入 TX 描述符字段( status 、 data_length 、 data_pointer )的位置,添加显式的 dma_sync_single_for_device() 调用。这是你手动添加的冲洗——但在编写 TDAR 之前,应该正式地将其放置为 dma_sync_single_for_device(dev, desc_dma_addr, sizeof(txbd), DMA_TO_DEVICE) 。无论 MMU 如何对描述符区域进行归属,该模型都明确且正确。 另外,审核分配给 ENET 描述符使用的物理地址范围的 AttrIndx / TEX+C+B 字段的 LPAE MMU 库更改。描述符池应映射为 Device-nGnRnE(强有序)或 Normal Non-cacheable — 而不是 Normal Writeback。您可以通过在分配后检查描述符池的虚拟地址,使用内核的 ptdump 调试接口来验证实际使用的属性。 你添加的 DMA 刷新不是一种权宜之计,而是正确的机制。真正的缺陷在于它一开始就不在发送路径中,而 LPAE 的更改暴露了这一点,因为它们改变了该区域的有效缓存性。   此致
查看全文
Facemesh Landmarkモデルptq変換におけるパフォーマンス低下 このリポジトリでは、ptq後にNXPがリリースしたGoogleのFaceMeshモデルを使っていました: nxp-demo-experience-demos-list/downloads.json at lf-6.12.3_1.0.0 ·NXP-IMX-support/NXP-demo-experience-demos-list しかしこのモデルは、468のランドマークポイントを持つGoogleの旧FaceMeshモデルに基づいています。 次に、Googleの新しいFaceMeshモデルに移行したいと考えています。これには478のランドマークポイントがあります。これをiMX 95 FRDMボードのNPU上で実行したいと考えています。そこで、これを量子化したかったのです。NXPのeIQ-neutron-sdk-linux-3.1.3を使っていますこのモデルを量子化するために。 この量子化の後、モデルのパフォーマンスは著しく劣化し、実際に使うにはほとんど使えない状態です。 当初はMIN-MAXオプションを使用して量子化していました。そのモデルは使い物にならなかった。次に、パーセンタイルオプションを使用してみたところ、パーセンタイルを95に設定した方がパフォーマンスが向上することがわかりました(これは回帰モデルの出力でしたが)。 しかし、それでも十分な性能は得られていません 1) NXPが古いFaceMesh(468)モデルのptqファイルを作成した際、どのオプションを使っていましたか?MIN-MAX?それともパーセンタイル? 2) 量子化後にパフォーマンスが著しく低下した場合、他に確認すべき事項はありますか? 3) CelebAデータセットでプロファイリングを行い、スクリプトのserialize_image.pyをモデルオプションで使いました。メディアパイプ全体を実行してキャリブレーションデータセットを作成するか、シリアル化スクリプトで変更すべきか オプション提供 serialize_image.py: -i //218 x 178 前面向けRGB画像 -<パス/トゥ/calib_bins> -Fビン -T float32 -0to1 -256、256 -NHWCレイアウト -コRGB TFLITE-Profiler: --input --データセット --出力 TFLITE-クオンタイザ: --input --プロファイル --quantize-inputs=false --quantize-outputs=false --量子化-キャリブレーション-方法= //最小最大値またはパーセンタイル Re: Performance degradation in Facemesh Landmark model ptq conversion こんにちは@dhilshad。 NXPサポートにご連絡いただきありがとうございます! 1) 残念ながら、現時点ではその情報は入手できません。 2) この挙動は想定内です。クオンタイズは展開プロセスの一部に過ぎません。組み込みハードウェア上でモデルを変換・最適化するには、グラフ最適化、演算子マッピング、ハードウェア固有の変換、ランタイム検証など、いくつかの追加ステップが必要です。その結果、モデルがすでに量子化されていても、モデルの挙動や性能は異なることがあります。 新しいデザインや評価には、eIQ Oliveの使用をおすすめします。NXP i.MX プラットフォームでのモデル最適化と展開のためのよりモダンなフレームワークを提供するからです。ワークフローの更新と、現在の機械学習展開シナリオへのサポート強化が含まれています。 詳細については、以下のチュートリアルおよびドキュメントをご参照ください。 https://eiq.nxp.com/learning-hub/tools/olive/index.html これらのリソースは、i.MX デバイスに機械学習モデルを導入するための推奨ワークフローやベストプラクティスをカバーしています。 よろしくお願いします、 チャビラ Re: Performance degradation in Facemesh Landmark model ptq conversion こんにちは、 @Chavira さん。返信ありがとうございます。そして、ドキュメントを指摘しています ここで念のために言うと、主な関心はモデルの正確さです。FaceMeshモデルの場合、出力するランドマークポイントはアプリケーションに対して十分に正確でないことがわかります。先ほど申し上げたように、95パーセンタイルをカットオフ値として設定する方が、MIN MAXよりもわずかに良い結果が得られることが分かりました。しかし、それでもNXPのptqモデル(FaceMesh 468)で見られる精度には及びません。 もう一つ気づいた点があります。 1) 代表的なデータセットとして、本番環境から8つのサンプルだけを用意して試してみました。これは結果をわずかに改善させた。次に、同じ環境から250枚の画像を追加し、プロファイリングと量子化を行った。しかし、これによって精度が低下した。 なぜこのような行動が起こるのか、何か心当たりはありますか? 2) また、NXPはすでにGoogleの新しいFaceMeshモデル(478ランドマーク搭載)をPTQに変換していますか?
查看全文
IPCF版本问题 我使用的RTD版本:SW32K3_S32M27x_RTD_R21-11_6.0.0_QLP01&04;IPCF版本:SW32K3_IPCF_4.2.1_D2504;EB版本:29.0,在导入excample project:IPCF_AutosarOS_S32K358_M7_0时报错,内容如下: Errors (11061) Plug in with a module Os TS T40D34M413R184" is not instald - cannot create module configurations for project IPCF AutosarOS S32K358 M7 0" 0 (11061) Plug in with a module "pc TS T40D34M4210R0 is not installed cannot create module configurations for project "IPCF AutosarOS $32K358 M7 0" 0 (11061) Plug in with a module Resource TS T40D34M5010Ro is notinstaled -cannet create module configurations for prcject IPCF AutosarOS $32K358 M7 0° @ (11061) Plug in with a module 'BaseNXP TS T40D34M50I0RO is notinstalled - cannot create module configurations for prgject IPCF AutosarOS $32K358 M7 0 @ (11061) Plug-in with a module "Mcu TS T40D34M5010R0 "is not instaled - cannot create module configurations for project 'IPCF AutosarOS $32K358 M7 0" 请问我该如何使用合适的IPCF或者EB版本解决这个问题? Re: IPCF版本问题 嗨@liyongfeng 请问您能否告知我您的 EB tresos 环境中当前安装了哪些插件版本? 另外,您能否尝试重新安装 RTD 软件包,并验证问题是否仍然存在? BR,VaneB
查看全文