2397106_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2397106_en-US

2397106_en-US

IMX95EVK-19-REV-A1 flash problem

Dear NXP,


I'm trying to flash a linux image(6.18.20_2.0.0/ 6.18.2_1.0.0/6.12.49_2.2.0) to eMMC/SD Card on IMX95LP5-19 EVK REV A1 and none of them is successful.

The command prompt shows [HID(W): LIBUSB_ERROR_PIPE (-9) ] SDPS: boot -f imx-boot-imx95-19x19-lpddr5-evk-sd.bin-flash_all.

IMX95LPD5EVK-19CM: UUU eMMC flash of L6.18.2 fails (LIBUSB errors on Linux and Windows)

The reference above mentioned that A1 silicon does not support current images on official site(6.12.34 does not have IMX95EVK patch). so I wonder if there is an unpublished official link that includes suitable images? 


Looking forward to your reply, Thanks.


BR/david


Here is a reference IMX95LPD5EVK-19CM: UUU eMMC flash of L6.18.2 fails (LIBUSB errors on Linux and Windows)

Re: IMX95EVK-19-REV-A1 flash problem

A1 silicon: The recommended BSP is LF 6.6.52_2.2.x

Please download demo image L6.6.52_2.2.2_MX95

And use image imx-boot-imx95-a1-19x19-lpddr5-evk-sd.bin-flash_all

I just verified the following command, it worked.

uuu.exe -b emmc imx-boot-imx95-a1-19x19-lpddr5-evk-sd.bin-flash_all

Tags (1)
No ratings
Version history
Last update:
‎07-22-2026 02:39 AM
Updated by: