MIMXRT1176 ADP – SEGGER J-Link debugging issue Hi everyone, I am currently working with the MIMXRT1176 / i.MX RT1170 platform. I initially used the MIMXRT1170-EVKB for development, but have now shifted to the MIMXRT1176-ADP for interfacing a parallel RGB panel. I am facing an issue with SEGGER J-Link debugging on the ADP board. Environment: Board: MIMXRT1176-ADP Board revision: 700-51950 REV A1 Schematic revision: SCH-51950 REV B1 MCUXpresso IDE: v25.6.136 MCUXpresso SDK: v25.09.00 SEGGER J-Link: latest version On the EVKB, both J-Link and LinkServer worked without any issues. However, on the ADP: Firmware flashes successfully. Debugger reaches the first line of main(). If I Step Over once, it stops at: Break at address "0xdeadbeee" with no debug information available, or outside of program code. Breakpoints at other locations work and are hit correctly. However, Resume/Continue from a breakpoint again results in 0xDEADBEEE. Could someone please confirm whether J-Link is fully supported with MCUXpresso IDE on the MIMXRT1176-ADP, and whether there is any specific J-Link script, reset/debug configuration, or ADP-specific initialization required? Could this be related to the memory configuration, external flash/SDRAM, or startup code on the ADP? Any guidance or working J-Link configuration for the ADP would be greatly appreciated. Thanks! Re: MIMXRT1176 ADP – SEGGER J-Link debugging issue Hi @HasanIqbalKhan ,
Thanks for your questions!
As far as I know, when using JLink with the RT1170-ADP in MCUXpresso IDE, only "attach" is supported while direct debugging is not supported. This is likely a support issue with the JLink flashloader. In IAR, this issue has been resolved. We apologize for any inconvenience this may cause.
Best regards, Gavin Re: MIMXRT1176 ADP – SEGGER J-Link debugging issue One more thing I tried, I connected an external MCU-Link and then tried debugging via the LinkServer in MCUXpresso IDE. The Execution reached main, I am able to step through from there, but when I try to resume execution it gives "Break at address "0x0" with no debug information available, or outside of program code.", and sometimes when I try to restart execution, it gives "Break at address "0x2230c8" with no debug information available, or outside of program code." For reference I am trying to run the "MIMXRT1176_dashboard_bt_ble_multiprofile" project, SW1 on the board is set to 01 and SW5 on the board is set to 000000000000. I tried to test with MCU-Link because the EVKB board uses the same and works fine. Also I do not think we can use Jlink, as it is clearly mentioned on their website that there is no support for octal flash, which the ADP board uses. Thanks. Re: MIMXRT1176 ADP – SEGGER J-Link debugging issue Is it possible to use debug via USB (J33) ? Re: MIMXRT1176 ADP – SEGGER J-Link debugging issue Hi @HasanIqbalKhan ,
1. J33 is USB-OTG1 and cannot be used for debugging.
2. It’s not that JLink doesn’t support Octal Flash; it’s just that by default, it only recognizes the flash found on the EVK/EVKB. As for IAR, this is because a corresponding download algorithm is provided. If you’re interested in this topic, you can refer to the RT-UFL project.
3. For information on current debugger/IDE support, please refer to: AN14387: https://docs.nxp.com/bundle/AN14378/page/topics/download_images_to_ADP_board.html
Best regards, Gavin
查看全文