Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
Using iMX8MP GPU on a process that call mlockall(MCL_FUTURE) causes kernel BUG() A customer reported an issue related to the use of the iMX8MP GPU (drawing using EGL). When the process that initializes the GPU previously called mlockall(MCL_FUTURE), as soon as the CMA area is mapped into userspace, the kernel reports the following BUG(): Kernel BUG at remap_pfn_range_internal+0x23c/0x2c8 Internal error: Oops - BUG: 00000000f2000800 [#1] PREEMPT SMP CPU: 0 PID: 3197 Comm: galcore_window_ Tainted: G O 6.6.142-7.7.0-devel #1-Torizon Hardware name: Toradex Verdin iMX8M Plus WB on Verdin Development Board (DT) pc : remap_pfn_range_internal+0x23c/0x2c8 x27: 00000000a2100000 x20: 0068000000000fcb x19: 0000007f90000000 ^^^^^^^^^^^^^^^^^^^^^^ the PTE already present Call trace: remap_pfn_range_internal+0x23c/0x2c8 remap_pfn_range+0x24/0x58 dma_direct_mmap+0xf4/0x150 dma_mmap_attrs+0x18/0x3c _CMAFSLMapUser+0x9c/0x150 [galcore] gckOS_LockPages+0xe4/0x148 [galcore] gckKERNEL_MapVideoMemory+0x90/0x1dc [galcore] gckVIDMEM_NODE_LockCPU+0x1b4/0x250 [galcore] _LockVideoMemory.isra.0+0x1f4/0x28c [galcore] gckKERNEL_Dispatch+0x210/0x1730 [galcore] gckDEVICE_Dispatch+0xcc/0x220 [galcore] drv_ioctl+0x340/0x444 [galcore] __arm64_sys_ioctl+0xac/0xf0 Kernel panic - not syncing: Oops - BUG: Fatal exception mlockall(MCL_FUTURE) is commonly used by real time applications, and the customer who reported the issue is using CODESYS to drive their HMI. We executed an AI-assisted analysis of the issue, and uncovered a plausible explanation for the reason the issue is being triggered: The CMA allocator in the galcore driver doesn't include an .mmap() hook. During the _CMAFSLMapUser() execution, it calls mmap() to get a vma, which is then used to locate the CMA area using find_vma(). The way mmap() is called causes the kernel to lazilly allocate a SHM area to fullfil the request. In normal cases, this allocation gets discarded moments later when the CMA are is found and remapped. However, when MCL_FUTURE is active the kernel cannot lazilly allocate the SHM area anymore, so it goes and populates the entire area before mmap() returns. In this case we have valid pages on this address, and the later call to remap_pfn_range() would end up silently discarding the memory management housekeeping information, which is exactly what the BUG() prevents. I'll attach a zip file which contains the source code of a program that reproduces the issue consistently without the need to run CODESYS. The AI agent suggested the following patch to fix it: diff -uNr a/hal/kernel/inc/gc_hal_options.h b/hal/kernel/inc/gc_hal_options.h --- a/hal/kernel/inc/gc_hal_options.h 2026-09-04 13:00:44.596621860 +0000 +++ b/hal/kernel/inc/gc_hal_options.h 2026-09-04 13:01:15.643862002 +0000 @@ -1471,9 +1471,17 @@ * Enable this macro can replace the /dev/zero by anon_inode: * [galcore] in /proc/ /maps. * Without the macro, run 'cat /proc/ /maps' will print "/dev/zero". + * + * It is also what gives the allocators an ->mmap handler, which is + * required so that the reservation made by vm_mmap() is created as a + * device mapping (VM_IO | VM_PFNMAP) rather than as ordinary anonymous + * memory. Without it, a process that has called mlockall(MCL_FUTURE) + * gets the range pre-faulted inside vm_mmap(), and the subsequent + * remap_pfn_range() then hits BUG_ON(!pte_none()) in remap_pte_range(). + * See tmp_mmap() in gc_hal_kernel_allocator.c. */ #ifndef gcdANON_FILE_FOR_ALLOCATOR -# define gcdANON_FILE_FOR_ALLOCATOR 0 +# define gcdANON_FILE_FOR_ALLOCATOR 1 #endif /* diff -uNr a/hal/os/linux/kernel/allocator/freescale/gc_hal_kernel_allocator_cma.c b/hal/os/linux/kernel/allocator/freescale/gc_hal_kernel_allocator_cma.c --- a/hal/os/linux/kernel/allocator/freescale/gc_hal_kernel_allocator_cma.c 2026-09-04 13:00:44.605314869 +0000 +++ b/hal/os/linux/kernel/allocator/freescale/gc_hal_kernel_allocator_cma.c 2026-09-04 13:01:15.644216883 +0000 @@ -400,7 +400,13 @@ gcmkHEADER_ARG("Allocator=%p Mdl=%p Cacheable=%d", Allocator, Mdl, Cacheable); #if LINUX_VERSION_CODE >= KERNEL_VERSION(3, 4, 0) +#if gcdANON_FILE_FOR_ALLOCATOR + /* Same as the gfp, dma and reserved_mem allocators: go through the + * allocator's anon file so that its ->mmap handler runs. */ + userLogical = (gctPOINTER)vm_mmap(Allocator->anon_file, +# else userLogical = (gctPOINTER)vm_mmap(gcvNULL, +# endif 0L, Mdl->numPages * PAGE_SIZE, PROT_READ | PROT_WRITE, diff -uNr a/hal/os/linux/kernel/gc_hal_kernel_allocator.c b/hal/os/linux/kernel/gc_hal_kernel_allocator.c --- a/hal/os/linux/kernel/gc_hal_kernel_allocator.c 2026-09-04 13:00:44.603242857 +0000 +++ b/hal/os/linux/kernel/gc_hal_kernel_allocator.c 2026-09-04 13:01:15.644041018 +0000 @@ -104,6 +104,36 @@ static int tmp_mmap(struct file *fp, struct vm_area_struct *vma) { + /* + * Declare the reservation as a device mapping with raw PFNs, before + * mmap() returns it to the caller. remap_pfn_range() sets both flags + * anyway; setting them here only makes them effective from the moment + * the VMA is created, and that is what matters: + * + * - the kernel treats VM_IO | VM_PFNMAP as VM_SPECIAL, documented in + * include/linux/mm.h as "Special vmas that are non-mergable, + * non-mlock()able". mmap_region() therefore clears VM_LOCKED from + * this VMA and leaves mm->locked_vm alone, and __mm_populate() + * skips it outright ("if (vma->vm_flags & (VM_IO | VM_PFNMAP)) + * continue;" in mm/gup.c). + * + * - so a process that has called mlockall(MCL_FUTURE) no longer has + * this range pre-faulted inside vm_mmap(). Every other mapping in + * that process keeps being locked and pre-faulted as before; only + * device memory, which is neither pageable nor swappable and gains + * nothing from being pre-faulted, is left out. + * + * - and the allocator's own remap_pfn_range(), a few microseconds + * later, therefore finds an empty range instead of one the kernel + * has just populated, so it no longer trips + * BUG_ON(!pte_none(ptep_get(pte))) in remap_pte_range(). + */ +#if LINUX_VERSION_CODE >= KERNEL_VERSION(6, 3, 0) + vm_flags_set(vma, VM_IO | VM_PFNMAP); +#else + vma->vm_flags |= VM_IO | VM_PFNMAP; +#endif + return 0; } The upstream driver uses a different mechanism which bypasses this issue. Other galcore allocators use the same pattern (calling vm_mmap to get a vma) and thus are likely succeptible to the same BUG(). Could you please look into this and fix the galcore driver? This issue prevents a real use case from working properly, and is affecting our customer directly. Thank you, Rafael Re: Using iMX8MP GPU on a process that call mlockall(MCL_FUTURE) causes kernel BUG() Hi @rbeims  Let me run the test and then check with the GPU team. Best Regards, Zhiming
View full article
S32K3X8EVB-Q289HWUMのオープンボードデバッガを用いた外部MCU(S32K358)のプログラミング こんにちは、 外部MCU S32K358を、S32K3X8EVB-Q289HWUMボードのオンボードデバッガと20ピンのCortex Debug D ETMコネクタに接続し、J55ケーブルケーブルを使ってプログラムしようとしています。しかし、エラーが発生します。コントローラーをうまくプログラムするために実際に何をすればいいのか教えてください。 Yash2530_0-1789183591258.jpegYash2530_0-1789183591258.jpegYash2530_0-1789183591258.jpeg CMD>VC オブジェクトファイルのCRC-16をデバイス範囲と照合しています... ブロック 00400000-0042F4B7 ... 計算されたCRC-16がブロックと一致しません。(ファイル = $A9EE、デバイス = $EDEF) デバイスのフラッシュメモリの検証エラー Flashプログラミング中にエラーが発生しました。 情報: DAP IDCODE = 0x6BA02477 情報:DAPの電源投入に成功しました。DP CTRL/STAT = 0xF0000000 リセットスクリプトを開始します (C:\NXP\S32DS.3.6.7\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_6.1.8.202603121731\supportFiles_ARM\NXP\S32K3xx\S32K358.mac)... REM MC_MEモジュールで選択したコアのクロックを有効にする 200ミリ秒遅延します... 終わり。 REM RAMとDMAを初期化します。 REM DMA TCD の初期化: REM 使用する各コアに対して、有効な実行可能コードをRAMにコピーします。 REM MC_ME で必要なコアを有効にする: 20ミリ秒遅延します... 終わり。 20ミリ秒遅延します... 終わり。 リセットスクリプト (C:\NXP\S32DS.3.6.7\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_6.1.8.202603121731\supportFiles_ARM\NXP\S32K3xx\S32K358.mac)完了しました。 PEmicro GDB 起動失敗: フラッシュプログラミング中にエラーが発生しました。デバッグセッションを終了します。 PEエラー:デバイスへのダウンロード中にエラーが発生しました。デバッグセッションを終了します。 127.0.0.1 経由で「127.0.0.1」から切断されました。ポート「53100」による6224からの切断 PEエラー: エラー: 応答を送信しようとしましたが、接続が既に閉じられています。 127.0.0.1 経由で「127.0.0.1」から切断されました。ポート「53104」による7224からの切断 情報: DAP IDCODE = 0x6BA02477 ターゲットとの接続が切断されました。 よろしくお願いいたします。 ヤシュ・グプタ Re: Programming External MCU (S32K358) using open board debugger of S32K3X8EVB-Q289HWUM ハイ まず第一に、オンボードデバッガーの使用はお勧めしません。S32K3X8EVBのオンボードデバッガは、評価ボード上でMCUのプログラミングとデバッグを行うために設計されています。このデバッガを使って外部カスタムS32K358ボードをプログラムまたはデバッグすることは、PEmicroによる公式推奨のユースケースではありません。したがって、NXPはこの構成での適切な動作を保証することはできません。 オンボードデバッガに関する制限事項については、以前に「 S32K142-Q48のプログラム/デバッグに関する問題」という議論の中で言及しました。PEmicroがS32K3オンボードデバッガの制限を変更したかどうかは把握していません。 たとえPEmicroにそのような制限がなくても、オンボードS32K358がデバッグャインターフェース回路を通じて電源供給されていないか(オンボードVDD_HV_A、VDD_HV_B、V11などを測定して確認)、またはJTAG_TCLK/SWD_CLKラインがオンボードS32K358から切り離されているかを必ず確認してください。 さらに、オンボードのデバッガインターフェースの信号電圧がカスタムボードの電圧と一致しているかも確認する必要があります。 よろしくお願いいたします ロビン
View full article
使用 S32K3X8EVB-Q289HWUM 的开放式板调试器对外部 MCU (S32K358) 进行编程 你好, 我正在尝试使用连接到 20 针 Cortex Debug D ETM 连接器的 S32K3X8EVB-Q289HWUM 板的板载调试器,以及 J55 电缆,对我的外部 MCU S32K358 进行编程。但我遇到了错误。请告诉我我究竟需要做些什么才能成功对我的控制器进行编程。 Yash2530_0-1789183591258.jpegYash2530_0-1789183591258.jpegYash2530_0-1789183591258.jpeg CMD>VC 正在验证目标文件 CRC-16 校验值是否与设备范围匹配…… 区块 00400000-0042F4B7 ... 计算出的 CRC-16 值与数据块不匹配。(文件 = $A9EE,设备 = $EDEF) 验证设备闪存时出错 Flash编程过程中发生错误。 信息:DAP IDCODE = 0x6BA02477 信息:DAP 已成功启动。DP CTRL/STAT = 0xF0000000 启动 RESET 脚本 (C:\NXP\S32DS.3.6.7\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_6.1.8.202603121731\supportFiles_ARM\NXP\S32K3xx\S32K358.mac)... REM 启用 MC_ME 模块中选定内核的时钟 延迟200毫秒…… 完毕。 REM 初始化 RAM 和 DMA: REM 初始化 DMA TCD: REM 将有效的可执行代码复制到每个要使用的核心的 RAM 中。 REM 启用 MC_ME 中所需的内核: 延迟20毫秒…… 完毕。 延迟20毫秒…… 完毕。 重置脚本 (C:\NXP\S32DS.3.6.7\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_6.1.8.202603121731\supportFiles_ARM\NXP\S32K3xx\S32K358.mac)完全的。 PEmicro GDB 启动失败:闪存编程期间出错。调试会话结束。 PE错误:下载到设备时出错。调试会话结束。 通过 127.0.0.1 与“127.0.0.1”断开连接。通过端口“53100”与6224断开连接 PE-ERROR:错误:尝试发送响应,但连接已关闭。 通过 127.0.0.1 与“127.0.0.1”断开连接。通过端口“53104”与7224断开连接 信息:DAP IDCODE = 0x6BA02477 目标设备已断开连接。 问候, 亚什·古普塔 Re: Programming External MCU (S32K358) using open board debugger of S32K3X8EVB-Q289HWUM HI 首先,我不建议使用板载调试器。S32K3X8EVB 板载调试器设计用于在评估板上对 MCU 进行编程和调试。使用此调试器对外部定制的 S32K358 板进行编程或调试并非 PEmicro 官方推荐的使用场景;因此,NXP 无法保证在此配置下正常运行。 关于板载调试器的局限性,之前在“ S32K142-Q48 的程序/调试问题”讨论中已经提到过。我不知道 PEmicro 是否更改了 S32K3 板载调试器的限制。 即使 PEmicro 没有此类限制,您仍然必须确保板载 S32K358 没有通过调试器接口电路供电(通过测量板载 VDD_HV_A、VDD_HV_B、V11 等进行验证),或者 JTAG_TCLK/SWD_CLK 线已与板载 S32K358 断开。 此外,您还需要验证板载调试器接口的信号电压是否与您的定制板上的电压相匹配。 此致敬礼, Robin
View full article
在调用 mlockall(MCL_FUTURE) 的进程中使用 iMX8MP GPU 会导致内核 BUG() 一位客户报告了一个与使用 iMX8MP GPU(使用 EGL 绘图)相关的问题。当初始化 GPU 的进程先前调用 mlockall(MCL_FUTURE) 时,一旦 CMA 区域被映射到用户空间,内核就会报告以下 BUG(): Kernel BUG at remap_pfn_range_internal+0x23c/0x2c8 Internal error: Oops - BUG: 00000000f2000800 [#1] PREEMPT SMP CPU: 0 PID: 3197 Comm: galcore_window_ Tainted: G O 6.6.142-7.7.0-devel #1-Torizon Hardware name: Toradex Verdin iMX8M Plus WB on Verdin Development Board (DT) pc : remap_pfn_range_internal+0x23c/0x2c8 x27: 00000000a2100000 x20: 0068000000000fcb x19: 0000007f90000000 ^^^^^^^^^^^^^^^^^^^^^^ the PTE already present Call trace: remap_pfn_range_internal+0x23c/0x2c8 remap_pfn_range+0x24/0x58 dma_direct_mmap+0xf4/0x150 dma_mmap_attrs+0x18/0x3c _CMAFSLMapUser+0x9c/0x150 [galcore] gckOS_LockPages+0xe4/0x148 [galcore] gckKERNEL_MapVideoMemory+0x90/0x1dc [galcore] gckVIDMEM_NODE_LockCPU+0x1b4/0x250 [galcore] _LockVideoMemory.isra.0+0x1f4/0x28c [galcore] gckKERNEL_Dispatch+0x210/0x1730 [galcore] gckDEVICE_Dispatch+0xcc/0x220 [galcore] drv_ioctl+0x340/0x444 [galcore] __arm64_sys_ioctl+0xac/0xf0 Kernel panic - not syncing: Oops - BUG: Fatal exception mlockall(MCL_FUTURE) 通常用于实时应用程序,而报告此问题的客户正在使用 CODESYS 来驱动其 HMI。 我们利用人工智能辅助分析了该问题,并找到了该问题触发原因的合理解释: galcore 驱动程序中的 CMA 分配器不包含 .mmap() 方法。钩。在 _CMAFSLMapUser() 执行期间,它调用 mmap() 获取 vma,然后使用该 vma 通过 find_vma() 定位 CMA 区域。mmap() 的调用方式导致内核延迟分配 SHM 区域以满足请求。正常情况下,当找到 CMA 区域并重新映射时,此分配会在片刻后被丢弃。 但是,当 MCL_FUTURE 处于活动状态时,内核不能再延迟分配 SHM 区域,因此它会在 mmap() 返回之前填充整个区域。在这种情况下,该地址上有有效的页面,而稍后对 remap_pfn_range() 的调用最终会默默地丢弃内存管理维护信息,这正是 BUG() 所阻止的。 我将附上一个 zip 文件,其中包含一个程序的源代码,该程序可以稳定地重现该问题,而无需运行 CODESYS。AI代理建议使用以下补丁来修复此问题: diff -uNr a/hal/kernel/inc/gc_hal_options.h b/hal/kernel/inc/gc_hal_options.h --- a/hal/kernel/inc/gc_hal_options.h 2026-09-04 13:00:44.596621860 +0000 +++ b/hal/kernel/inc/gc_hal_options.h 2026-09-04 13:01:15.643862002 +0000 @@ -1471,9 +1471,17 @@ * Enable this macro can replace the /dev/zero by anon_inode: * [galcore] in /proc/ /maps. * Without the macro, run 'cat /proc/ /maps' will print "/dev/zero". + * + * It is also what gives the allocators an ->mmap handler, which is + * required so that the reservation made by vm_mmap() is created as a + * device mapping (VM_IO | VM_PFNMAP) rather than as ordinary anonymous + * memory. Without it, a process that has called mlockall(MCL_FUTURE) + * gets the range pre-faulted inside vm_mmap(), and the subsequent + * remap_pfn_range() then hits BUG_ON(!pte_none()) in remap_pte_range(). + * See tmp_mmap() in gc_hal_kernel_allocator.c. */ #ifndef gcdANON_FILE_FOR_ALLOCATOR -# define gcdANON_FILE_FOR_ALLOCATOR 0 +# define gcdANON_FILE_FOR_ALLOCATOR 1 #endif /* diff -uNr a/hal/os/linux/kernel/allocator/freescale/gc_hal_kernel_allocator_cma.c b/hal/os/linux/kernel/allocator/freescale/gc_hal_kernel_allocator_cma.c --- a/hal/os/linux/kernel/allocator/freescale/gc_hal_kernel_allocator_cma.c 2026-09-04 13:00:44.605314869 +0000 +++ b/hal/os/linux/kernel/allocator/freescale/gc_hal_kernel_allocator_cma.c 2026-09-04 13:01:15.644216883 +0000 @@ -400,7 +400,13 @@ gcmkHEADER_ARG("Allocator=%p Mdl=%p Cacheable=%d", Allocator, Mdl, Cacheable); #if LINUX_VERSION_CODE >= KERNEL_VERSION(3, 4, 0) +#if gcdANON_FILE_FOR_ALLOCATOR + /* Same as the gfp, dma and reserved_mem allocators: go through the + * allocator's anon file so that its ->mmap handler runs. */ + userLogical = (gctPOINTER)vm_mmap(Allocator->anon_file, +# else userLogical = (gctPOINTER)vm_mmap(gcvNULL, +# endif 0L, Mdl->numPages * PAGE_SIZE, PROT_READ | PROT_WRITE, diff -uNr a/hal/os/linux/kernel/gc_hal_kernel_allocator.c b/hal/os/linux/kernel/gc_hal_kernel_allocator.c --- a/hal/os/linux/kernel/gc_hal_kernel_allocator.c 2026-09-04 13:00:44.603242857 +0000 +++ b/hal/os/linux/kernel/gc_hal_kernel_allocator.c 2026-09-04 13:01:15.644041018 +0000 @@ -104,6 +104,36 @@ static int tmp_mmap(struct file *fp, struct vm_area_struct *vma) { + /* + * Declare the reservation as a device mapping with raw PFNs, before + * mmap() returns it to the caller. remap_pfn_range() sets both flags + * anyway; setting them here only makes them effective from the moment + * the VMA is created, and that is what matters: + * + * - the kernel treats VM_IO | VM_PFNMAP as VM_SPECIAL, documented in + * include/linux/mm.h as "Special vmas that are non-mergable, + * non-mlock()able". mmap_region() therefore clears VM_LOCKED from + * this VMA and leaves mm->locked_vm alone, and __mm_populate() + * skips it outright ("if (vma->vm_flags & (VM_IO | VM_PFNMAP)) + * continue;" in mm/gup.c). + * + * - so a process that has called mlockall(MCL_FUTURE) no longer has + * this range pre-faulted inside vm_mmap(). Every other mapping in + * that process keeps being locked and pre-faulted as before; only + * device memory, which is neither pageable nor swappable and gains + * nothing from being pre-faulted, is left out. + * + * - and the allocator's own remap_pfn_range(), a few microseconds + * later, therefore finds an empty range instead of one the kernel + * has just populated, so it no longer trips + * BUG_ON(!pte_none(ptep_get(pte))) in remap_pte_range(). + */ +#if LINUX_VERSION_CODE >= KERNEL_VERSION(6, 3, 0) + vm_flags_set(vma, VM_IO | VM_PFNMAP); +#else + vma->vm_flags |= VM_IO | VM_PFNMAP; +#endif + return 0; } 上游驱动程序使用了一种不同的机制来绕过这个问题。其他 galcore 分配器使用相同的模式(调用 vm_mmap 获取 vma),因此很可能容易受到相同的 BUG() 的影响。 请您调查并修复 galcore 驱动程序?这个问题导致实际应用场景无法正常运行,直接影响到我们的客户。 谢谢! 拉斐尔 Re: Using iMX8MP GPU on a process that call mlockall(MCL_FUTURE) causes kernel BUG() 嗨@rbeims 让我先运行一下测试,然后再和GPU团队确认。 此致, 志明
View full article
S32 Design Studio for Power Architecture 版本 2.1激活码即将开始 您好,我的产品为S32 Design Studio for Power Architecture Version 2.1,激活码B9B6-A787-E3B4-585C即将于9.28日继续,请帮我续期或允许重新申请 Re: S32 Design Studio for Power Architecture Version 2.1激活码即将到期 你好, 您的S32DS许可证已延期。请将现有许可证存入S32DS系统,并使用您之前的激活码重新激活。
View full article
S32 Design Studio for Power Architecture Version 2.1激活码即将到期 您好,我的产品为S32 Design Studio for Power Architecture Version 2.1,激活码 B9B6-A787-E3B4-585C 即将于9.28日到期,请帮我续期或允许重新申请 Re: S32 Design Studio for Power Architecture Version 2.1激活码即将到期 Hi,  your S32DS license has been extended. Please return existing license in S32DS and activate it again with your old code. 
View full article
Programming External MCU (S32K358) using open board debugger of S32K3X8EVB-Q289HWUM Hello,  I am trying to program my external MCU S32K358 using an onboard debugger of S32K3X8EVB-Q289HWUM board connected at 20-pin Cortex Debug D ETM connector, along with cable J55 cable. But I get errors. Please let me know what I actually need to do to successfully program my controller. Yash2530_0-1789183591258.jpegYash2530_0-1789183591258.jpegYash2530_0-1789183591258.jpeg CMD>VC Verifying object file CRC-16 to device ranges ... block 00400000-0042F4B7 ... Calculated CRC-16 does not match block. (File = $A9EE, Device = $EDEF) Error verifying flash of device Error occured during Flash programming. INFO: DAP IDCODE = 0x6BA02477 INFO: DAP successfully powered up. DP CTRL/STAT = 0xF0000000 Starting reset script (C:\NXP\S32DS.3.6.7\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_6.1.8.202603121731\supportFiles_ARM\NXP\S32K3xx\S32K358.mac) ... REM Enable clocks for selected cores in MC_ME module Delaying for 200mS ... Done. REM Initialize RAM and DMA: REM Initialize DMA TCD: REM Copy valid executable code to RAM for each core to be used. REM Enable required cores in MC_ME: Delaying for 20mS ... Done. Delaying for 20mS ... Done. Reset script (C:\NXP\S32DS.3.6.7\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_6.1.8.202603121731\supportFiles_ARM\NXP\S32K3xx\S32K358.mac) completed. PEmicro GDB Launch Failure : Error during flash programming. Terminating debug session. PE-ERROR: Error downloading to the device. Terminating debug session. Disconnected from "127.0.0.1" via 127.0.0.1. Disconnection by port "53100" from 6224 PE-ERROR: Error : Attempted to send response but connection already closed. Disconnected from "127.0.0.1" via 127.0.0.1. Disconnection by port "53104" from 7224 INFO: DAP IDCODE = 0x6BA02477 Target Disconnected. Regards, Yash Gupta Re: Programming External MCU (S32K358) using open board debugger of S32K3X8EVB-Q289HWUM Hi First of all, I do not recommend using the onboard debugger. The onboard debugger on the S32K3X8EVB is designed for programming and debugging the MCU on the evaluation board itself. Using this debugger to program or debug an external custom S32K358 board is not an officially recommended use case by PEmicro; therefore, NXP cannot guarantee proper operation in this configuration. Limitations regarding the onboard debugger were previously mentioned in the "Program/Debug issue with S32K142-Q48" discussion. I am not aware if PEmicro has changed the limitations for the S32K3 onboard debugger. Even if there are no such limitations from PEmicro, you must still ensure that the onboard S32K358 is not being powered through the debugger interface circuitry (verify by measuring onboard VDD_HV_A, VDD_HV_B, V11, etc.) or that the JTAG_TCLK/SWD_CLK lines are disconnected from the onboard S32K358. Additionally, you need to verify that the signal voltage of the onboard debugger interface matches the voltage on your custom board. Best Regards, Robin
View full article
S32 Design Studio for Power Architecture バージョン 2.1激活码即将到期 您好,我的产品为S32 Design Studio for Power Architecture Version 2.1,激活码 B9B6-A787-E3B4-585C 即将于9.28日到期,请帮我续期或允许重新申请 Re: S32 Design Studio for Power Architecture Version 2.1激活码即将到期 こんにちは、 お客様のS32DSライセンスが延長されました。S32DSに既存のライセンスを返却し、以前のコードで再度アクティベートしてください。
View full article
Flash Drives # which is best flash drive avialble now in the market ## Please tell me Re: Flash Drives Hi@reedjhn9 I didn't quite understand your question. Could you describe it in more detail—specifically, the product you are using and the exact issue you want to know about?
View full article
U盘 目前市面上最好的U盘是哪一款? ## 请告诉我 Re: Flash Drives 你好@ reedjhn9 我不太明白你的问题。您能否更详细地描述一下——具体来说,您正在使用的产品以及您想了解的具体问题?
View full article
mlockall(MCL_FUTURE)を呼び出すプロセスでiMX8MP GPUを使用すると、カーネルBUG() あるお客様がiMX8MPのGPU使用(EGLによる描画)に関する問題を報告しました。以前mlockall(MCL_FUTURE)と呼ばれていたGPU初期化プロセスが、CMA領域がユーザースペースにマッピングされると、カーネルは以下のBUG()を報告します: Kernel BUG at remap_pfn_range_internal+0x23c/0x2c8 Internal error: Oops - BUG: 00000000f2000800 [#1] PREEMPT SMP CPU: 0 PID: 3197 Comm: galcore_window_ Tainted: G O 6.6.142-7.7.0-devel #1-Torizon Hardware name: Toradex Verdin iMX8M Plus WB on Verdin Development Board (DT) pc : remap_pfn_range_internal+0x23c/0x2c8 x27: 00000000a2100000 x20: 0068000000000fcb x19: 0000007f90000000 ^^^^^^^^^^^^^^^^^^^^^^ the PTE already present Call trace: remap_pfn_range_internal+0x23c/0x2c8 remap_pfn_range+0x24/0x58 dma_direct_mmap+0xf4/0x150 dma_mmap_attrs+0x18/0x3c _CMAFSLMapUser+0x9c/0x150 [galcore] gckOS_LockPages+0xe4/0x148 [galcore] gckKERNEL_MapVideoMemory+0x90/0x1dc [galcore] gckVIDMEM_NODE_LockCPU+0x1b4/0x250 [galcore] _LockVideoMemory.isra.0+0x1f4/0x28c [galcore] gckKERNEL_Dispatch+0x210/0x1730 [galcore] gckDEVICE_Dispatch+0xcc/0x220 [galcore] drv_ioctl+0x340/0x444 [galcore] __arm64_sys_ioctl+0xac/0xf0 Kernel panic - not syncing: Oops - BUG: Fatal exception mlockall(MCL_FUTURE)はリアルタイムアプリケーションで一般的に使われており、問題を報告した顧客はCODESYSを使ってHMIを駆動しています。 AIを活用した分析を実施した結果、問題が発生する理由として考えられる説明が明らかになりました。 galcoreドライバーのCMAアロケーターには.mmap()が含まれていません。フック。_CMAFSLMapUser() の実行中に、mmap() を呼び出して vma を取得し、それを使用して find_vma() を使用して CMA 領域を特定します。mmap() の呼び出し方法により、カーネルは要求を満たすために SHM 領域を遅延的に割り当てることになります。通常の場合、CMAが見つかって再マッピングされると、この割り当てはすぐに破棄されます。 しかし、MCL_FUTUREがアクティブなとカーネルはもはやSHM領域を怠惰に割り当てることができなくなり、mmap()が戻る前にエリア全体を埋め尽くします。この場合、このアドレスには有効なページがあり、後のremap_pfn_range()への呼び出しはメモリ管理のハウスキーピング情報を静かに破棄することになり、これはまさにBUG()が防いでいることです。 CODESYSを実行せずに問題を再現できるプログラムのソースコードを含むzipファイルを添付します。AIエージェントは、この問題を修正するために以下のパッチを提案しました。 diff -uNr a/hal/kernel/inc/gc_hal_options.h b/hal/kernel/inc/gc_hal_options.h --- a/hal/kernel/inc/gc_hal_options.h 2026-09-04 13:00:44.596621860 +0000 +++ b/hal/kernel/inc/gc_hal_options.h 2026-09-04 13:01:15.643862002 +0000 @@ -1471,9 +1471,17 @@ * Enable this macro can replace the /dev/zero by anon_inode: * [galcore] in /proc/ /maps. * Without the macro, run 'cat /proc/ /maps' will print "/dev/zero". + * + * It is also what gives the allocators an ->mmap handler, which is + * required so that the reservation made by vm_mmap() is created as a + * device mapping (VM_IO | VM_PFNMAP) rather than as ordinary anonymous + * memory. Without it, a process that has called mlockall(MCL_FUTURE) + * gets the range pre-faulted inside vm_mmap(), and the subsequent + * remap_pfn_range() then hits BUG_ON(!pte_none()) in remap_pte_range(). + * See tmp_mmap() in gc_hal_kernel_allocator.c. */ #ifndef gcdANON_FILE_FOR_ALLOCATOR -# define gcdANON_FILE_FOR_ALLOCATOR 0 +# define gcdANON_FILE_FOR_ALLOCATOR 1 #endif /* diff -uNr a/hal/os/linux/kernel/allocator/freescale/gc_hal_kernel_allocator_cma.c b/hal/os/linux/kernel/allocator/freescale/gc_hal_kernel_allocator_cma.c --- a/hal/os/linux/kernel/allocator/freescale/gc_hal_kernel_allocator_cma.c 2026-09-04 13:00:44.605314869 +0000 +++ b/hal/os/linux/kernel/allocator/freescale/gc_hal_kernel_allocator_cma.c 2026-09-04 13:01:15.644216883 +0000 @@ -400,7 +400,13 @@ gcmkHEADER_ARG("Allocator=%p Mdl=%p Cacheable=%d", Allocator, Mdl, Cacheable); #if LINUX_VERSION_CODE >= KERNEL_VERSION(3, 4, 0) +#if gcdANON_FILE_FOR_ALLOCATOR + /* Same as the gfp, dma and reserved_mem allocators: go through the + * allocator's anon file so that its ->mmap handler runs. */ + userLogical = (gctPOINTER)vm_mmap(Allocator->anon_file, +# else userLogical = (gctPOINTER)vm_mmap(gcvNULL, +# endif 0L, Mdl->numPages * PAGE_SIZE, PROT_READ | PROT_WRITE, diff -uNr a/hal/os/linux/kernel/gc_hal_kernel_allocator.c b/hal/os/linux/kernel/gc_hal_kernel_allocator.c --- a/hal/os/linux/kernel/gc_hal_kernel_allocator.c 2026-09-04 13:00:44.603242857 +0000 +++ b/hal/os/linux/kernel/gc_hal_kernel_allocator.c 2026-09-04 13:01:15.644041018 +0000 @@ -104,6 +104,36 @@ static int tmp_mmap(struct file *fp, struct vm_area_struct *vma) { + /* + * Declare the reservation as a device mapping with raw PFNs, before + * mmap() returns it to the caller. remap_pfn_range() sets both flags + * anyway; setting them here only makes them effective from the moment + * the VMA is created, and that is what matters: + * + * - the kernel treats VM_IO | VM_PFNMAP as VM_SPECIAL, documented in + * include/linux/mm.h as "Special vmas that are non-mergable, + * non-mlock()able". mmap_region() therefore clears VM_LOCKED from + * this VMA and leaves mm->locked_vm alone, and __mm_populate() + * skips it outright ("if (vma->vm_flags & (VM_IO | VM_PFNMAP)) + * continue;" in mm/gup.c). + * + * - so a process that has called mlockall(MCL_FUTURE) no longer has + * this range pre-faulted inside vm_mmap(). Every other mapping in + * that process keeps being locked and pre-faulted as before; only + * device memory, which is neither pageable nor swappable and gains + * nothing from being pre-faulted, is left out. + * + * - and the allocator's own remap_pfn_range(), a few microseconds + * later, therefore finds an empty range instead of one the kernel + * has just populated, so it no longer trips + * BUG_ON(!pte_none(ptep_get(pte))) in remap_pte_range(). + */ +#if LINUX_VERSION_CODE >= KERNEL_VERSION(6, 3, 0) + vm_flags_set(vma, VM_IO | VM_PFNMAP); +#else + vma->vm_flags |= VM_IO | VM_PFNMAP; +#endif + return 0; } 上流ドライバーはこの問題を回避する別のメカニズムを使用しています。他の galcore アロケータも同じパターン (vm_mmap を呼び出して vma を取得する) を使用しているため、同じ BUG() の影響を受ける可能性があります。 この件について調べて、galcoreドライバーを直してもらえますか?この問題は実際のユースケースが正常に動作することを妨げており、直接的にお客様に影響を及ぼしています。 ありがとうございました。 ラファエル Re: Using iMX8MP GPU on a process that call mlockall(MCL_FUTURE) causes kernel BUG() こんにちは@rbeims  テストを実行してからGPUチームに確認させてください。 よろしくお願いします、 志明
View full article
S32K344 – HSE_BファームウェアをインストールしたアプリケーションでPFLASH Block 2が利用可能ですか? こんにちは、 S32K344 (HSE_FW_S32K344_0_2_55_0、0.2.55.0 ビルド pb150130 (2025 年 1 月 30 日)) を中心とした配電ユニットを開発中です。タイプ:標準FW構成)デュアルバンクブートローダーとセキュアファームウェアアップデート付き。Flashレイアウトのある一点で行き詰まっており、明確な回答をいただけると幸いです。 問題点 NVMの設定領域(アプリケーションが書き込むランタイムパラメータ)は現在、実行中のコードと同じブロック内のPFLASHブロック0に存在しています。実行時にそれらに書き込むと、コア上で書き込み中の読み取り停止が発生し、プログラム/消去操作の間、ユニットがフリーズします。これは私たちのアプリケーションには受け入れられません(PDUはセーフティに関わる負荷を駆動します)。 最も簡単な解決策は、これらの領域を実行コードを含まないブロックに移動することです。ブロック2(0x600000–0x6FFFFF、セクター368–381)が自然な候補です。アプリケーションバンクでは使用されておらず、HSEがデータを保存するブロックでもありません。 これまでに確認したこと – S32K3xxリファレンスマニュアルにはPFLASHブロック構造が説明されていますが、HSE予約については何も触れていません。 – 公開されているHSE Basic FW FAQによると、ブロック0と1はアプリケーションに対して保証されており、HSEファームウェアはブロック3の一部(FULL_MEM構成で176KB)を予約しています。ブロック2については全く言及されていません。 – 私たちが検討したHSEデモアプリケーションやRTDの例もBlock 2を使用していないため、そこから何も推測できません。 – HSEファームウェアリファレンスマニュアルv2.4のNDA/DocStoreアクセス申請を提出しましたが、この内容はこの内容をカバーしていると理解しています。リクエストは保留中です。 質問 HSE_Bファームウェアをインストールした場合、Block 2はFULL_MEM設定のアプリケーション(コードとデータ)に完全に利用可能でしょうか?AB_SWAPについてはどうでしょうか? アプリケーションコアから実行時にブロック2を消去・プログラミングすることに関して、HSE関連の制限はありますか?HSE、SBAF、またはセキュアブートによってロックまたは監視されているセクター)? HSEファームウェア、SBAF、アプリケーション間のPFLASHブロックの完全な割り当てを説明した公開文書はありますか?もしなければ、NDA申請が処理される間にHSEファームウェア リファレンス・マニュアルへのアクセスを手伝ってもらえませんか? 確定的な答えが出るまでは、設計は意図的にブロック0と1に限定されており、そのため読み書きの問題が残ります。 ご協力ありがとうございます。 Re: S32K344 – Is PFLASH Block 2 available to the application with HSE_B firmware installed? 共有していただきありがとうございます 😉 Re: S32K344 – Is PFLASH Block 2 available to the application with HSE_B firmware installed? こんにちは、 @manu_fenixecu さん、 A1。はい、ブロック2は完全にユーザーフラッシュです。 S32K344、S32K314、およびS32K324のフラッシュメモリのレイアウトについては、HSE-B FW RM v2.7の図33(FULL_MEM)および図34(AB_SWAP)を参照してください。 A2.HSE-B FW RM v2.7、セクション14.6.4.2(HSE_CONFIG_GPR3)— アプリケーションはビット27を読み取るべきです。 A3。公開されている唯一の参考資料は、S32K3xx RM rev12、表198(「HSE_Bファームウェア使用機能フラグが有効になっている場合の構成の詳細」)です。HSE-B FW RMはNDAなしに共有できません。HSE関連のサポートについては、この公開コミュニティではなくサポートチケットを使用してください。 よろしくお願いいたします。 ダニエル
View full article
i.MX RT1170 は、スペクトラム拡散クロックを有効にした後、起動に失敗しました。 MCUXpressoを使用してRT1170 EVKでSSCを有効にしようとしています。 参照番号:AN12879 手順: 1. ベースプロジェクト:SDKの例evkmimxrt1170_semc_cm7 2. IDEを使ってSSCを設定する IDE_Clocking.pngIDE_Clocking.png source_diff.pngsource_diff.png 3. 起動に失敗しました Boot_Failed.pngBoot_Failed.png 4. 時々正常に起動できる(~ 1/50) 何か手順を飛ばしてしまったでしょうか? よろしくお願いします。 見た Re: i.MX RT1170 Failed to boot after Spread Spectrum Clocking is enabled ここで行われた変更点を、単にデモコードを投稿するだけでなく詳しく教えてもらえますか?この投稿から3年経った今、私がこの元の投稿で詳述したのと同じ問題を抱えている状況では、何が必要なのかを判断するのは難しい。 よろしくお願いします。 Re: i.MX RT1170 Failed to boot after Spread Spectrum Clocking is enabled こんにちは、 @SeenFan さん。 SDRAMはDCDと起動ROMで初期化できます。その後、起動ROMがアプリケーションコードをSDRAMにコピーします。一番重要なのはキャッシュの問題だと思います。こちらのリンクを参照してください。 https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/How-to-move-CM4-core-project-to-SDRAM-in-RT1176/ta-p/1363185 2. SDRAMでのデバッグ https://community.nxp.com/t5/MCUXpresso-IDE/Running-and-debugging-program-in-SDRAM/mp/1405167 3. i.MXRTでキャッシュされていないメモリを使用する https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/Using-NonCached-Memory-on-i-MXRT/ta-p/1183369 よろしくお願いいたします。 ジン Re: i.MX RT1170 Failed to boot after Spread Spectrum Clocking is enabled こんにちは、ジンさん SDRAM上のプログラムを検索して実行したい場合。 注意すべき点は何ですか? よろしくお願いします。 見た Re: i.MX RT1170 Failed to boot after Spread Spectrum Clocking is enabled こんにちは、ジンさん それは動作します。どうもありがとう。 よろしくお願いします。 見た Re: i.MX RT1170 Failed to boot after Spread Spectrum Clocking is enabled こんにちは、 @SeenFan さん。 これは、RT1170 FlexSPIがデフォルト設定時にクロックソースとしてPLL2を使用するためです。PLL2の周波数を変更すると、FlexSPIが次の命令を取得できなくなる場合があります。これを解決するには、fsl_clock.cをSRAMに変換できます。私のデモコードを参照してください。 よろしくお願いいたします。 ジン
View full article
Eureka on PIC CLB Certain PIC MCUs (e.g., pic16f13145 family) have FPGA-like programmable logic called Configurable Logic Block. The pic16f13115 I'm using has 32 cells each with a 4-input lookup table and a D flip-flop. To learn to use the tools, today I implemented and simulated support for Charlieplexing of 6 LEDs with PWM brightness control. I used Verilog to define the circuit instead of using the logic CAD canvas. I was pounding my head on the wall for about half my time. Slowly, I got the Verilog right, got it to synthesize (build), then got it simulating. It is cool that the CLB programmed logic works even when the CPU is sleeping. It's perfect for safety-critical applications. Can be used, for example, to implement complex interrupt trigger logic. There is great flexibility in hooking up CLB logic to peripheral inputs and outputs. It's much more flexible than the clunkier CLC programmable logic that's been a fixture of PICs. Just thought I'd share my Eureka experience. Power
View full article
PIC CLB 上的 Eureka 某些 PIC MCU(例如 pic16f13145 系列)具有类似 FPGA 的可编程逻辑,称为可配置逻辑块。 我使用的 pic16f13115 有 32 个单元,每个单元都有一个 4 输入查找表和一个 D 触发器。 为了学习如何使用这些工具,今天我实现了对 6 个 LED 的 Charlieplexing 的 PWM 亮度控制支持,并进行了模拟。我使用 Verilog 来定义电路,而不是使用逻辑 CAD 画布。 我差不多有一半的时间都在用头撞墙。我慢慢地把 Verilog 代码写对了,让它能够综合(构建),然后让它能够仿真。 CLB 编程逻辑即使在 CPU 休眠状态下也能正常工作,这很棒。它非常适合功能安全至关重要的应用。例如,可用于实现复杂的触发信号逻辑。CLB 逻辑与外围输入输出的连接方式非常灵活。它比PIC单片机中一直使用的笨重的CLC可编程逻辑电路灵活得多。 只是想和大家分享一下我的 Eureka 经历。 电源
View full article
学ぶ 私はNXP S32K144を使い始めたばかりです。初心者におすすめの開発環境は何ですか?また、最初に何を学ぶべきでしょうか? Re: LEARNING こんにちは、 @JASAMANG さん、 初心者には、 S32 Design Studio for S32 Platform とS32K144評価ボードを組み合わせて使うことをおすすめします。 IDEに加えて、 S32K1リアルタイム・ドライバ (RTD) パッケージをインストールしてください。現在の開発フローでは、推奨される組み合わせは S32 Design Studio v3.6.0とS32K1 RTD 3.0.0です。RTDパッケージはHelp > S32DS拡張機能とアップデートを通じてインストール可能です。 以下の学習経路をたどることをお勧めします。 既存のS32K144 RTDサンプル(LED点滅サンプルやGPIOサンプルなど)をインポートして実行します。 基本的なプロジェクト構造、ビルドプロセス、フラッシュ書き込み、デバッグについて学びます。 S32の設定ツール、特にピン、クロック、ペリフェラルの設定に慣れておく。 GPIO、割り込み、タイマー、PWM、ADCについて引き続き説明します。 これらの基礎が明らかになったら、FreeMASTERやMCATなどのモータ制御の例やツールに進みましょう。 既存の例から始める方が、最初からアプリケーション全体を作るよりも一般的に簡単です。 RTDの設置手順については、 S32K1 RTDオフライン設置ガイドを参照してください。この記事は古いS32DS/RTDの組み合わせを示しつつ、パッケージ依存関係や一般的なオフラインインストールフローについて説明しています。ダウンロードするRTDバージョンのリリースノートで、必要なS32DSバージョンおよび依存パッケージを必ず確認してください。 この議論も役立つかもしれません: S32 Design StudioにSDK/RTDをインストールする。レガシーSDKとRTDの違いを説明し、AUTOSARおよび非AUTOSARの点滅LED例へのリンクを提供しています S32Kナレッジベースには、役立つ事例や技術記事も掲載されています。 問題が発生した場合は、まずS32Kコミュニティフォーラムを検索することをお勧めします。多くのよくある質問や問題点は、すでにそこで議論され、回答されています。 また、特定の問題に直面した場合は 専用Thread を作成してください。これにより議論が明確になり、他のユーザーが関連情報を見つけやすくなります。   最後の返信から7日間Threadを積極的に監視しています。その後は、更新のための購読メールのみを受け取り、それらは時折見逃されることもあります。この期間以降に関連する質問があれば、新しいThreadを作成し、元のThreadを参照してください。   回答がご質問への回答となっている場合は、 「解決策として承認」をクリックしてください。関連する質問がある場合は、新しいThreadを作成し、元のThreadを参照してください。   よろしくお願いいたします。 パベル Re: LEARNING 情報提供ありがとうございます。 🙏  Re: LEARNING 情報提供ありがとうございます 🙏
View full article
S32K344 – 安装 HSE_B 固件的应用程序是否可以使用 PFLASH Block 2? 你好, 我们正在围绕 S32K344 (HSE_FW_S32K344_0_2_55_0, 0.2.55.0 版本 pb150130 (2025 年 1 月 30 日)) 开发配电单元。类型:标准固件配置)具有双库引导加载程序和安全固件更新。我们在 Flash 布局的某一点上遇到了困难,希望能得到一个明确的答案。 问题 我们的 NVM 配置区域(应用程序写入的运行时参数)目前位于 PFLASH 块 0 中,与正在执行的代码位于同一块中。在运行时向它们写入数据会触发内核的读写停顿,从而在编程/擦除操作期间冻结单元。对于我们的应用来说,这是不可接受的(PDU 驱动与功能安全相关的负载)。 显而易见的解决方法是将这些区域移动到不包含已执行代码的块中。块 2(0x600000–0x6FFFFF,扇区 368–381)是自然的候选者:它没有被我们的应用程序银行使用,而且它也不是 HSE 存储其数据的块。 我们目前已核查的内容 – S32K3xx 参考手册描述了 PFLASH 块结构,但没有提及 HSE 预留。 – 公开的 HSE 基本固件常见问题解答指出,第 0 和 1 块保证供应用程序使用,并且 HSE 固件保留了第 3 块的一部分(在 FULL_MEM 配置中为 176 KB)。它完全没有提到第二区。 – 我们看到的 HSE 演示应用程序和 RTD 示例也没有使用 Block 2,因此我们无法从中推断出任何信息。 – 我们已提交 HSE 固件参考手册 v2.4 的 NDA / DocStore 访问请求,据我们了解,该手册涵盖了此内容。请求正在处理中。 问题 安装 HSE_B 固件后,在 FULL_MEM 配置下,Block 2 是否完全可供应用程序(代码和数据)使用?AB_SWAP 呢? 在运行时从应用程序核心擦除/编程 Block 2 是否存在任何与 HSE 相关的限制(例如,(由 HSE、SBAF 或安全启动锁定或监测的扇区)? 是否有公开文档描述了 HSE 固件、SBAF 和应用程序之间完整的 PFLASH 块分配情况?如果不行,能否请哪位好心人帮我们在保密协议申请处理期间获取 HSE 固件参考手册? 在得到确切答案之前,我们的设计特意限制在模块 0 和 1 内,这就给我们留下了边读边写的问题。 提前感谢您的帮助。 Re: S32K344 – Is PFLASH Block 2 available to the application with HSE_B firmware installed? 谢谢分享 😉 Re: S32K344 – Is PFLASH Block 2 available to the application with HSE_B firmware installed? 你好@manu_fenixecu , A1. 是的,Block 2 完全是用户闪存。 有关 S32K344、S32K314 和 S32K324 的闪存布局,请参阅 HSE-B FW RM v2.7 中的图 33(FULL_MEM)和图 34(AB_SWAP)。 A2. HSE-B FW RM v2.7,第 14.6.4.2 节 (HSE_CONFIG_GPR3) — 应用程序应读取第 27 位。 A3.唯一公开的参考资料是 S32K3xx RM rev12,表 198(“启用 HSE_B 固件使用功能标志时的配置详细信息”)。没有签署保密协议,HSE-B FW RM 不能共享。如需 HSE 相关支持,请使用支持工单,而不是在此公共社区中提问。 此致, 丹尼尔
View full article
i.MX RT1170 Failed to boot after Spread Spectrum Clocking is enabled Trying to enable SSC on RT1170 EVK with MCUXpresso. Ref: AN12879 Steps: 1. Base project: SDK Example evkmimxrt1170_semc_cm7 2. Using IDE to config SSC  IDE_Clocking.pngIDE_Clocking.png source_diff.pngsource_diff.png 3. Boot failed Boot_Failed.pngBoot_Failed.png 4. Sometimes can boot normally (~ 1/50) Any step I missed? Regards Seen Re: i.MX RT1170 Failed to boot after Spread Spectrum Clocking is enabled Can you detail the changes that were made here, rather than just post demo code? It's difficult to determine what is needed 3 years after this post, when I am having the same problem detailed in this original post. Thank you. Re: i.MX RT1170 Failed to boot after Spread Spectrum Clocking is enabled Hi @SeenFan , SDRAM can be initialized by DCD and boot ROM.  Then boot ROM will copy your application code to SDRAM. I think the most important thing is the cache problem. You can refer to these link. https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/How-to-move-CM4-core-project-to-SDRAM-in-RT1176/ta-p/1363185 2.debug in sdram https://community.nxp.com/t5/MCUXpresso-IDE/Running-and-debugging-program-in-SDRAM/m-p/1405167 3.Using NonCached Memory on i.MXRT https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/Using-NonCached-Memory-on-i-MXRT/ta-p/1183369 Regards, Jing Re: i.MX RT1170 Failed to boot after Spread Spectrum Clocking is enabled Hi Jin, If I want to locate and run program on SDRAM.  What I need to pay attention to? Regards Seen Re: i.MX RT1170 Failed to boot after Spread Spectrum Clocking is enabled Hi Jing, It works. Thanks a lot. Regards Seen Re: i.MX RT1170 Failed to boot after Spread Spectrum Clocking is enabled Hi @SeenFan , This is because RT1170 FlexSPI use PLL2 as clock source when use default configure. When you change PLL2 frequency, FlexSPI may fail to get next instruction. To resolve this, you can put fsl_clock.c to SRAM. Please refer to my demo code. Regards, Jing
View full article
学习 我是NXP S32K144的新手。对于初学者来说,推荐的开发环境是什么?我应该首先学习什么? Re: LEARNING 你好@JASAMANG , 对于初学者,我建议使用S32 Design Studio for S32 Platform以及 S32K144 评估板。 除了 IDE 之外,请安装S32K1 实时驱动程序 (RTD)软件包。对于当前的开发流程,推荐的组合是S32 Design Studio v3.6.0 与 S32K1 RTD 3.0.0 。可以通过“帮助”>“S32DS 扩展和更新”安装 RTD 软件包。 我建议按照以下学习路径进行学习: 导入并运行现有的 S32K144 RTD 示例,例如闪烁 LED 或 GPIO 示例。 学习项目的基本结构、构建过程、烧录和调试。 熟悉 S32 配置工具,特别是引脚、时钟和外设配置。 继续讲解 GPIO、中断、定时器、PWM 和 ADC。 一旦这些基本概念清晰明了,就可以开始学习电机控制示例和工具,例如 FreeMASTER 和 MCAT。 通常来说,从现有示例入手比从头开始创建完整的应用程序要容易得多。 有关 RTD 安装指导,请参阅S32K1 RTD 离线安装指南。虽然这篇文章演示的是较旧的 S32DS/RTD 组合,但它解释了软件包依赖关系和一般的离线安装流程。务必在下载的 RTD 版本的发行说明中核实所需的 S32DS 版本和依赖软件包。 您可能也会发现以下讨论很有用:将 SDK/RTD 安装到 S32 Design Studio 中。它解释了传统 SDK 和 RTD 之间的区别,并提供了 AUTOSAR 和非 AUTOSAR LED 闪烁示例的链接。 您还可以在S32K 知识库中找到有用的示例和技术文章。 如果遇到问题,我建议先在S32K 社区论坛上搜索一下。许多常见问题和疑虑已经在那里讨论并得到了解答。 另外,如果您遇到具体问题,请另开新帖。这有助于保持讨论的清晰性,也使其他用户更容易找到相关信息。   我们会在最后一条回复发出后的七天内持续监测帖子。此后,我们只会收到更新订阅邮件,偶尔可能会错过这些邮件。此后如有任何相关问题,请另开新帖并引用原帖。   如果某个回复解答了您的问题,请点击“接受为解决方案”。如有任何相关问题,请另开新帖并引用原帖。   顺祝商祺! 帕维尔 Re: LEARNING 感谢您提供信息 🙏 Re: LEARNING 我非常感谢您提供的信息。 🙏 
View full article
启用扩频时钟后,i.MX RT1170 无法启动。 尝试使用 MCUXpresso 在 RT1170 EVK 上启用 SSC。 参考编号:AN12879 步骤: 1. 基础项目:SDK 示例 evkmimxrt1170_semc_cm7 2. 使用IDE配置SSC IDE_Clocking.pngIDE_Clocking.png source_diff.pngsource_diff.png 3. 启动失败 Boot_Failed.png启动失败.png 4. 有时可以正常启动(约 1/50) 我漏掉了什么步骤吗? 此致 已见 Re: i.MX RT1170 Failed to boot after Spread Spectrum Clocking is enabled 能否详细说明一下这里做了哪些更改,而不仅仅是贴出示例代码?时隔三年,我仍然遇到与原帖中详细描述的相同问题,因此很难确定需要什么。 谢谢! Re: i.MX RT1170 Failed to boot after Spread Spectrum Clocking is enabled 嗨@SeenFan , 同步动态随机存取存储器(SDRAM) 可由 DCD 和启动 ROM 初始化。然后启动 ROM 会将您的应用程序代码复制到同步动态随机存取存储器(SDRAM)。我认为最重要的是缓存问题。您可以参考这些链接。 https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/How-to-move-CM4-core-project-to-SDRAM-in-RT1176/ta-p/1363185 2.在 同步动态随机存取存储器(SDRAM) 中调试 https://community.nxp.com/t5/MCUXpresso-IDE/Running-and-debugging-program-in-SDRAM/mp/1405167 3.在 i.MXRT 上使用非缓存内存 https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/Using-NonCached-Memory-on-i-MXRT/ta-p/1183369 此致, 景 Re: i.MX RT1170 Failed to boot after Spread Spectrum Clocking is enabled 嗨,金, 如果我想在同步动态随机存取存储器(SDRAM)上定位并运行程序。 我需要注意什么? 此致 已见 Re: i.MX RT1170 Failed to boot after Spread Spectrum Clocking is enabled 嗨,静, 有用。多谢。 此致 已见 Re: i.MX RT1170 Failed to boot after Spread Spectrum Clocking is enabled 嗨@SeenFan , 这是因为 RT1170 FlexSPI 在使用默认配置时使用 PLL2 作为时钟源。当您更改 PLL2 频率时,FlexSPI 可能无法获取下一条指令。要解决这个问题,你可以把 fsl_clock.c 放到 SRAM 里。请参考我的示例代码。 此致, 景
View full article