Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
启用扩频时钟后,i.MX RT1170 无法启动。 尝试使用 MCUXpresso 在 RT1170 EVK 上启用 SSC。 参考编号:AN12879 步骤: 1. 基础项目:SDK 示例 evkmimxrt1170_semc_cm7 2. 使用IDE配置SSC IDE_Clocking.pngIDE_Clocking.png source_diff.pngsource_diff.png 3. 启动失败 Boot_Failed.png启动失败.png 4. 有时可以正常启动(约 1/50) 我漏掉了什么步骤吗? 此致 已见 Re: i.MX RT1170 Failed to boot after Spread Spectrum Clocking is enabled 能否详细说明一下这里做了哪些更改,而不仅仅是贴出示例代码?时隔三年,我仍然遇到与原帖中详细描述的相同问题,因此很难确定需要什么。 谢谢! Re: i.MX RT1170 Failed to boot after Spread Spectrum Clocking is enabled 嗨@SeenFan , 同步动态随机存取存储器(SDRAM) 可由 DCD 和启动 ROM 初始化。然后启动 ROM 会将您的应用程序代码复制到同步动态随机存取存储器(SDRAM)。我认为最重要的是缓存问题。您可以参考这些链接。 https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/How-to-move-CM4-core-project-to-SDRAM-in-RT1176/ta-p/1363185 2.在 同步动态随机存取存储器(SDRAM) 中调试 https://community.nxp.com/t5/MCUXpresso-IDE/Running-and-debugging-program-in-SDRAM/mp/1405167 3.在 i.MXRT 上使用非缓存内存 https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/Using-NonCached-Memory-on-i-MXRT/ta-p/1183369 此致, 景 Re: i.MX RT1170 Failed to boot after Spread Spectrum Clocking is enabled 嗨,金, 如果我想在同步动态随机存取存储器(SDRAM)上定位并运行程序。 我需要注意什么? 此致 已见 Re: i.MX RT1170 Failed to boot after Spread Spectrum Clocking is enabled 嗨,静, 有用。多谢。 此致 已见 Re: i.MX RT1170 Failed to boot after Spread Spectrum Clocking is enabled 嗨@SeenFan , 这是因为 RT1170 FlexSPI 在使用默认配置时使用 PLL2 作为时钟源。当您更改 PLL2 频率时,FlexSPI 可能无法获取下一条指令。要解决这个问题,你可以把 fsl_clock.c 放到 SRAM 里。请参考我的示例代码。 此致, 景
記事全体を表示
S32K344 – Is PFLASH Block 2 available to the application with HSE_B firmware installed? Hello, We are developing a Power Distribution Unit around the S32K344 (HSE_FW_S32K344_0_2_55_0, 0.2.55.0 build pb150130 (30 janvier 2025). Type : Standard FW configuration) with a dual-bank bootloader and secure firmware update. We are stuck on one point of the flash layout and would appreciate a definitive answer. The problem Our NVM configuration regions (runtime parameters written by the application) currently live in PFLASH Block 0, in the same block as the executing code. Writing to them at runtime triggers read-while-write stalls on the core, which freezes the unit for the duration of the program/erase operation. This is not acceptable for our application (the PDU drives safety-relevant loads). The obvious fix is to move these regions to a block that does not contain executed code. Block 2 (0x600000–0x6FFFFF, sectors 368–381) is the natural candidate: it is not used by our application banks, and it is not the block where HSE stores its data. What we have checked so far – The S32K3xx Reference Manual describes the PFLASH block structure but does not say anything about HSE reservations. – The public HSE Basic FW FAQ states that Blocks 0 and 1 are guaranteed for the application, and that the HSE firmware reserves part of Block 3 (176 KB in FULL_MEM configuration). It does not mention Block 2 at all. – The HSE demo application and RTD examples we looked at do not use Block 2 either, so we cannot infer anything from them. – We have submitted an NDA / DocStore access request for the HSE Firmware Reference Manual v2.4, which we understand covers this. The request is pending. Questions With HSE_B firmware installed, is Block 2 entirely available to the application (code and data) in FULL_MEM configuration? What about AB_SWAP? Is there any HSE-related restriction on erasing/programming Block 2 at runtime from the application core (e.g. sectors locked or monitored by HSE, SBAF or secure boot)? Is there a public document that describes the full PFLASH block allocation between HSE firmware, SBAF and the application? If not, could someone help us get access to the HSE Firmware Reference Manual while our NDA request is processed? Until we have a confirmed answer, our design is deliberately confined to Blocks 0 and 1, which leaves us with the read-while-write issue. Thank you in advance for your help. Re: S32K344 – Is PFLASH Block 2 available to the application with HSE_B firmware installed? Hello @manu_fenixecu, A1. Yes, Block 2 is entirely user flash. Refer to HSE-B FW RM v2.7, Figure 33 (FULL_MEM) and Figure 34 (AB_SWAP) for the flash memory layout of S32K344, S32K314, and S32K324. A2. HSE-B FW RM v2.7, Section 14.6.4.2 (HSE_CONFIG_GPR3) — the application should read bit 27. A3. The only publicly available reference is the S32K3xx RM rev12, Table 198 ("Configuration details when the HSE_B firmware usage feature flag is enabled"). The HSE-B FW RM cannot be shared without an NDA in place. For HSE-related support, please use support tickets rather than this public community. Regards, Daniel Re: S32K344 – Is PFLASH Block 2 available to the application with HSE_B firmware installed? Thank you for sharing 😉
記事全体を表示
SC16IS740 最大水晶周波数 NXP技術サポートチームへ、 弊社では、3.3V電源でSC16IS740を使用しています。 XTAL1とXTAL2間で直接接続可能な最大外部結晶発振器の周波数を確認していただけますか? データシートには以下のように記載されています。 外部クロック、水晶発振器(最大24MHz)に適用されます。 再開まで今しばらくお待ちください。 よろしくお願いいたします。 アビシェク Re: SC16IS740 Maximum Crystal Frequency こんにちは、AbishekDevanさん 良い一日! はい、おっしゃる通りです。外部水晶発振器を使用した場合の限界周波数は24MHzです。 良い一日をお過ごしください。幸運を祈ります。
記事全体を表示
主题:MPC5605 内存读取问题,地址为 0x00100010 你好, 我们遇到一个使用 MPC5605 的 ECU 问题。 在执行 EOL 内存转储操作期间,我们的工具箱使用直接 CPU 字节访问来读取内存: *((uint8_t *)地址) 从 CAN 日志中可以看到: ```文本 从 0x00100008 读取 8 个字节 -> 成功 从 0x00100010 读取 8 个字节 -> ECU 停止响应并重置 ``` 我们查阅了 MPC5606BK 参考手册,`16234_MPC5606BRM`,修订版 2: - 表 3-1,第 49 页显示“0x00100000 - 0x001FFFFF”为**保留**。 - 第 871-872 页描述了闪存映射和闪存仿真映射。 请问您能否澄清一下: 1. `0x00100010` 是 MPC5605 的有效/可读地址吗? 2. 如果这是一个保留地址,当软件直接读取它时会发生什么?它会导致异常或 RESET 吗? 3. 我们应该使用哪一参考手册章节来获取准确的 MPC5605 内存映射? 我们还会从 ECU 硬件中收集完整的 MPC5605 零件编号和芯片版本。 此致, 卡西拉詹 C 开发板 Re: Subject: MPC5605 memory-read issue at 0x00100010 你好, 地址 0x00100010 属于 0x00100000-0x001FFFFF 范围,该范围在 MPC560xB 内存映射中标记为保留。应用程序不得访问保留区域。访问此类位置可能会产生与总线相关的异常或其他设备特定的故障响应,如果不处理该异常,可能会导致通信丢失或RESET。 第三章 记忆映射 petervlna_0-1789455244473.pngpetervlna_0-1789455244473.png 顺祝商祺! Peter
記事全体を表示
i.MX95 - UUUツールのフラッシュが時々失敗する 専門家の皆様へ 私はi.MX95 EVKを使用しており、imx-bootと(カーネル+ルートファイルシステム)をemmcにフラッシュしています。フラッシュ書き込みには、UUUスクリプトのemmc_allオプションを使用しました。 時々、そのオプションを使ったフラッシュ書き込みで失敗する現象が見られました。以下に、エラー発生時のコードスニペットを示します。 0x200000002:13-294A7876CE324A4D>Okay (0.403s) 2:13-294A7876CE324A4D>Start Cmd:FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi; 2:13-294A7876CE324A4D>Okay (0.008s) 2:13-294A7876CE324A4D>Start Cmd:FB: ucmd sleep 1 2:13-294A7876CE324A4D>Okay (1.007s) 2:13-294A7876CE324A4D>Start Cmd:FB: ucmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0 2:13-294A7876CE324A4D>Fail (0.187s) 同様の不具合を経験された方がいらっしゃいましたら、また、この問題を軽減するための解決策をご存知でしたら、ぜひお知らせください。 よろしくお願いいたします! BR、 アルン・クマール Re: i.MX95 - UUU tool flashing fails occasionally こんにちは、 使っているコマンドの全文を共有してもらえますか?また、FRDMボードのEVKやBSP版、UUU版でテストしている場合も教えてください。 よろしくお願いいたします。
記事全体を表示
件名:MPC5605のメモリ読み取りに関する問題(アドレス:0x00100010) こんにちは、 MPC5605を使用しているECUに問題が発生しています。 EOLメモリダンプ操作中、ツールボックスはCPUの直接バイトアクセスを使ってメモリを読み込みます。 *((uint8_t *)address) CANのログより: 「`テキスト」 0x00100008から8バイトを読み込みました -> 成功 0x00100010から8バイトを読み取ると、ECUが応答しなくなりリセットされる。 「`」 MPC5606BKリファレンスマニュアル『16234_MPC5606BRM』、リバノリファレンス2を確認しました: - 表3-1、49ページでは、`0x00100000 - 0x001FFFFF`が**予約済み**と表示されています。 - 871~872ページでは、フラッシュメモリマップとフラッシュエミュレーションマッピングについて説明しています。 もう少し詳しく教えていただけますか: 1. 「0x00100010」はMPC5605にとって有効で読みやすいアドレスか? 2. 予約済みアドレスの場合、ソフトウェアが直接読み取った場合どうなりますか?CANは例外やリセットを引き起こすことはできますか? 3. 正確なMPC5605メモリマップにはどのリファレンス・マニュアルセクションを使うべきか? また、ECUハードウェアからMPC5605の完全な部品番号とシリコンリビジョンも収集しています。 よろしくお願いします、 カシラジャン C 開発ボード Re: Subject: MPC5605 memory-read issue at 0x00100010 こんにちは、 アドレス0x00100010は、MPC560xBメモリマップで予約済みとしてマークされている0x00100000-0x001FFFFFの範囲に属します。予約済み地域はアプリケーションソフトウェアでアクセスしてはなりません。そのような場所へのアクセスはバス関連の例外やデバイス固有の故障応答を引き起こす可能性があり、例外が処理されない場合、通信の喪失やリセットにつながることがあります。 第3章 メモリーマップ petervlna_0-1789455244473.pngpetervlna_0-1789455244473.png よろしくお願いいたします。 ピーター
記事全体を表示
ユーザーガイドで言及されているPIDパラメータの重要性と、それらの計算方法について教えてください。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 私はBLDC制御用にMagniV開発ボードを使っています......。速度と電流ループ制御とPI制御についてはNXPのコードも参考にしました。PI制御ループのパラメータ計算はfreemasterツールを使用して行います。PIDループのパラメータ計算にも同様のツールはありますか?また、コードに付属していたユーザーガイドに記載されているNXP PID機能で使用されるPIDパラメータの重要性を定義してください。 Re: PID parameters significance mentioned in User guide and how to calculate them ? 別のプロセスの場合: 1. モーター95W、12V、抵抗Rは約1.2Ω、インダクタンスLは約2.5mH 2. スイッチの周波数は160Hz、つまり1000 rad/s(1000/3.1416/2=160Hz)であることを示唆しています。 3. そしてZ_finalは1である。 SO: S = 1/(R+2*pi*L*freq) = 1/(1.2+2*3.14156*2.5e-3*160)= 1/(1.2+2.5) ジャンプはこちらです: 1.Kp = 2*3.1416*2.5e-3*160-R= 5-1.2= 3.8 2.Ki = w^2*L = 2500 3. Vol curr はスタンドリズであるため、 :Kp = 3.8 * 8/12 = 3.8 * 0.667=2.5 この段階で、AIはLが間違っている可能性があると述べた。 ---------------- 適切なモーターパラメータを計算してみましょう。 エンジンがcos(theta)=0.85の場合 >>> import numpy as np >>> np.acos(0.85) np.float64(0.5548110329800715) >>> np.sin(0.555) np.float64(0.5269433002033014) するとsin(θ)=0.5。 つまり、エンジンがSTDで停止したとき、Curr_RとCurr_Lは等しいです。 so:R = 12*0.707/(8*0.707)= 1.5オーム、これは正しいです。 L:9000rpmは150Hzなので、誤差は帯域幅の問題だと思います。1500Hz、あるいは3000Hzより高くあるべきです もし freq_std=1500なら、Lは12*0.85/(2*π*1.5e3)であるはずです。= 10mH ~ 5mH つまり、Ki = 14e3*10e-3 = 140 または 70。 Kp = 2*pi*1.5e3*L-R = 94-1.5= ... それでも間違っている…。 Re: PID parameters significance mentioned in User guide and how to calculate them ? やあ。 私はPID制御に関しては初心者です。 これが私が見つけた最初の投稿です。 以下は、このフォーラムにおける私の発見と知識の一部です。 S32K344 - FreeRTOSと統合されたFOC これが最初の行です。 EVボードをインストールした後、PMSM_appconfig.hを取得しました。PIDパララム、initパララムは: #define CLOOP_D_KP(0.368399F) #define CLOOP_D_KI(0.0298853F) #define CLOOP_Q_KP(0.371817F) #define CLOOP_Q_KI(0.0298853F) これはFOCコントロールなので、ここには2つのPIパラメータがあります。 したがって、Kpが最も重要なものです。 では、私の計算は以下の通りです: PID(err_of_vol) = カール。 電圧範囲は12Vです モーターの出力は95Wで、出力カールは :95/12=8A です。 SO: Kp = 8/12 = 0.67...しかしモーターは前述と後ろのロールをサポートCANできるため、Volは2つの部分に分割しなければなりません。 SO :   if you using +12V to サポート all roll on roll back, kp should be 8*2/12=1.33 DC+とDC-を反転させるようなものを使用する場合は、0.67になるはずです。 調整する場合、常に小さい値から始まります。例えば、その20%。つまり、最終的に0.37は20%×1.33=より大きいです。0.27 KiはKpの約10%であり、Ki = 1/12*Kpとなる。 しかし、それは全くの間違いのようだ。 Qianwen(AIチャット)について何か聞いたんだけど 1. NXPは、最初の段階では、現在の株価と株価を据え置くべきである。 2. 計算の基準となるのは、制御空間のゼロ点と極点です。 後で調べてみます。 それによると、モーターの PID パラメータは、まずモーターの L、R を測定し、次に計算します。 Re: PID parameters significance mentioned in User guide and how to calculate them ? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、 私たちはウェブ上のモータ制御の例の構造にPIコントローラを使用しています。ご指摘の通り、McatはPIコントローラのパラメータ計算に役立ちます(カスケード制御構造におけるPMSMや、6ステップ構造におけるBLDCの制御)。現時点では、PIDコントローラー付きの構造や設定支援ツールを使った例はウェブ上にありませんが、もちろんAMCLIBライブラリも顧客制御構造の構成要素としてこの機能を提供しています。 お役に立てれば幸いです。 よろしくお願いいたします。 ダイアナ
記事全体を表示
NXP Matlab Simulink Interaction I am Trying to flash Simulink model into S32K312 MINI-EVB. It is using CAN interface for input and output of the model. Need to understand why my traces are not matching with what i am getting in Simulink Simulation model. There are differences in the model run in Simulink and that on NXP hardware, maybe because of timestep and other factors, just need support to check what i might be doing wrong.
記事全体を表示
NXP Matlab Simulink 交互 我正在尝试将 Simulink 模型刷写到 S32K312 MINI-EVB 中。该模型采用CAN接口进行输入输出。我需要了解为什么我的轨迹与我在 Simulink 仿真模型中得到的结果不符。Simulink 中的模型运行结果与 NXP 硬件上的模型运行结果存在差异,可能是由于时间步长和其他因素造成的,我需要帮助来检查我可能做错了什么。
記事全体を表示
FRDM-IMX93 ASCII ボードファイル こんにちは、 このリンクからFRDM-IMX93デザインファイルを取得しました: https://www.nxp.com/design/design-center/development-boards-and-designs/frdm-i-mx-93-development-board:FRDM-IMX93 しかし、それらをAltiumにインポートするためのAllegroやExtracta.exeを持っていません。LAY-94611_B.brdをACII形式で提供してもらえますか?それならAltiumにインポートできます。 ありがとうございます Re: FRDM-IMX93 ASCII Board File こんにちは、 私もこのファイルが必要です。ボードをよりよく理解し、開発に役立てたいからです。送ってくれる? Re: FRDM-IMX93 ASCII Board File こんにちは、 @Cwootton さん! NXPサポートにご連絡いただきありがとうございます! 必要なファイルは近日中にメールでお送りします。 よろしくお願いします、 チャビラ
記事全体を表示
PID parameters significance mentioned in User guide and how to calculate them ? I am using MagniV development board for for BLDC control .... I have also took reference from NXP code for speed and current loop control with PI control ..... for PI control loop parameters calculations are done using freemaster tool....Is there any such tool for PID loop parameter calculation ? Also please define significance of PID parameters used in NXP PID function mentioned in user guide that came with code . Re: PID parameters significance mentioned in User guide and how to calculate them ? for another process: 1. motor 95W, 12V, the R is about: 1.2ohm, and L is about:2.5mH 2. it suggest the switch freq is 160Hz, which is 1000 rad/s( 1000/3.1416/2=160Hz) 3. and it suggest the Z_final is 1. so: s = 1/(R+2*pi*L*freq) = 1/(1.2+2*3.14156*2.5e-3*160) = 1/(1.2+2.5)  here is a jump: 1.Kp = 2*3.1416*2.5e-3*160-R = 5-1.2 = 3.8 2.Ki = w^2*L = 2500 3.because the Vol, curr is standlize, so :Kp = 3.8 * 8/12 = 3.8*0.667=2.5 at this stage, AI said the L maybe wrong. ---------------- let me try to calc the right motor params. if engine is cos(theta)=0.85 >>> import numpy as np >>> np.acos(0.85) np.float64(0.5548110329800715) >>> np.sin(0.555) np.float64(0.5269433002033014) then sin(theta)=0.5. so: when engine at std power out. the Curr_R and Curr_L is equal. so:R = 12*0.707/(8*0.707) = 1.5ohm, this is right. L:9000rpm is 150Hz,so, I think the error is bandwith, it should be higher than 1500Hz, and maybe 3000Hz if freq_std=1500, which means the L should be 12*0.85/(2*pi*1.5e3) = 10mH ~5mH so:Ki = 14e3*10e-3 = 140 or 70. Kp = 2*pi*1.5e3*L -R = 94-1.5 = ... still wrong.... Re: PID parameters significance mentioned in User guide and how to calculate them ? hi,there. I am a naive to pid ctrl. this is the first post I found. here are some my foundings in this forum and knowledge. S32K344 - FOC integrated with FreeRTOS this is the beginning line. After I install the EV boards, I got the PMSM_appconfig.h,  the pid params, init params is : #define CLOOP_D_KP (0.368399F) #define CLOOP_D_KI (0.0298853F) #define CLOOP_Q_KP (0.371817F) #define CLOOP_Q_KI (0.0298853F) this is FOC controler, so there are two PI params here. so the Kp is the most important one. so,here is my calc: the PID(err_of_vol) = Curr. Vol range is 12V the motor power is 95W, so the output Curr is :95/12=8A. so: Kp = 8/12 = 0.67... but  the motor can support forword and backword rolling, so the  Vol must split into 2Parts. so :   if you using +12V to support all roll on roll back, kp should be 8*2/12=1.33 if you using something like revert the DC+ DC-, it should be just 0.67. if you tune it, it always start an a more small value. for example 20% of it.  so at last, the 0.37 is more larger than 20%*1.33= 0.27 Ki is about 10percent of Kp, here is Ki = 1/12*Kp but it seems it is totally wrong. I heard sth about Qianwen(An AI-Chat) 1. NXP should Standlize the Curr & Vol, for the very first stage. 2.what the calc is based Zero,and Polor Point of Control Space.  I will try to figure it out later,  it said, the motor's PID params will first try to measure motors' L,R then calc. Re: PID parameters significance mentioned in User guide and how to calculate them ? Hello, We use PI controllers in the structures of our motor control examples on the web. As you write, Mcat helps with the calculation of parameters for the PI controllers used (for PMSM in the cascade control structure for BLDC in the structure for sixstep). At the moment we do not have an example on the web that would use a structure with a PID controller or a tool that would help to set it, but of course, our AMCLIB library also offers this function as a building block for customer control structures. I hope it helps. Best regards, Diana
記事全体を表示
FRDM-IMX93 ASCII 板文件 你好, 我从这个链接下载了FRDM-IMX93设计文件: https://www.nxp.com/design/design-center/development-boards-and-designs/frdm-i-mx-93-development-board:FRDM-IMX93 但是我没有 Allegro 或 Extracta.exe 来将它们导入 Altium。请提供 ACII 格式的 LAY-94611_B.brd 文件,以便我将其导入 Altium 系统。 谢谢! Re: FRDM-IMX93 ASCII Board File 你好, 我也需要这份文件来更好地了解电路板并帮助进行开发。你能发给我吗? Re: FRDM-IMX93 ASCII Board File 嗨@Cwootton ! 感谢您联系恩智浦技术支持! 我稍后会通过电子邮件将所需文件发送给您。 此致, 查维拉
記事全体を表示
NXP Matlab Simulinkとの連携 SimulinkモデルをMINI-EVBにフラッシュしようS32K312。モデルの入出力にCANインターフェースを使用しています。なぜ自分のトレースがSimulinkシミュレーションモデルで得られているものと一致しないのか理解したいです。SimulinkでのモデルとNXPハードウェアでのモデルには違いがあります。おそらくタイムステップやその他の要因が原因かもしれませんが、何が間違っているのか確認するためにサポートが必要です。
記事全体を表示
用户指南中提到的PID参数的含义以及如何计算它们? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 我正在使用MagniV开发板进行BLDC控制……我还参考了NXP关于速度和电流回路的PI控制代码……PI控制回路参数的计算是用Freemaster工具完成的……请问有没有类似的工具可以用于PID回路参数的计算?另外,请解释一下代码附带的用户指南中提到的NXP PID函数中使用的PID参数的含义。 Re: PID parameters significance mentioned in User guide and how to calculate them ? 用于另一个流程: 1. 电机功率95W,电压12V,电阻R约为1.2Ω,电感L约为2.5mH 2. 这表明开关频率为 160Hz,即 1000 rad/s(1000/3.1416/2=160Hz)。 3. 这表明 Z_final 为 1。 所以:s = 1/(R+2*pi*L*freq) = 1/(1.2+2*3.14156*2.5e-3*160)= 1/(1.2+2.5) 这里有一个跳跃: 1.Kp = 2*3.1416*2.5e-3*160-R= 5-1.2= 3.8 2. Ki = w^2*L = 2500 3. 因为 Vol,curr 是标准化的,所以:Kp = 3.8 * 8/12 = 3.8 * 0.667 = 2.5 现阶段,人工智能表示 L 可能错了。 ---------------- 让我尝试计算一下正确的电机参数。 如果引擎的 cos(theta)=0.85 >>> import numpy as np >>> np.acos(0.85) np.float64(0.5548110329800715) >>> np.sin(0.555) np.float64(0.5269433002033014) 那么 sin(θ)=0.5。 所以:当发动机处于 STD 功率输出时,Curr_R 和 Curr_L 相等。 所以:R = 12*0.707/(8*0.707)= 1.5欧姆,没错。 L:9000rpm 对应的频率是 150Hz,所以我认为误差出在带宽上,带宽应该高于 1500Hz,可能是 3000Hz。 如果 freq_std=1500,则 L 应为 12*0.85/(2*pi*1.5e3)= 10mH ~5mH 所以:Ki = 14e3*10e-3 = 140 或 70。 Kp = 2*pi*1.5e3*L-R = 94-1.5= ... 还是错了…… Re: PID parameters significance mentioned in User guide and how to calculate them ? 你好呀。 我对 pid ctrl 完全不了解。 这是我找到的第一篇帖子。 以下是我在这个论坛上的一些心得和知识。 S32K344 - FOC 与 FreeRTOS 集成 这是起始行。 安装完电动汽车电路板后,我得到了 PMSM_appconfig.h 文件。进程 ID 参数、初始化参数为: #define CLOOP_D_KP (0.368399F) #define CLOOP_D_KI (0.0298853F) #define CLOOP_Q_KP (0.371817F) #define CLOOP_Q_KI (0.0298853F) 这是 FOC 控制器,所以这里有两个 PI 参数。 所以Kp是最重要的。 这是我的计算结果: PID(err_of_vol) = Curr。 电压范围为12V 电机功率为 95W,因此输出电流为:95/12=8A。 所以:Kp = 8/12 = 0.67...但是电机可以支持向前和向后滚动,所以 Vol 必须分成 2 部分。 所以:如果您使用 +12V 来支持所有回滚操作,则 kp 值应为 8*2/12=1.33 如果你使用类似反转 DC+ DC- 的方法,它应该只是 0.67。 如果你调整它,它总是从一个较小的值开始。例如,其中20%。所以最终,0.37 比 20%*1.33 更大。0.27 Ki 大约是 Kp 的 10%,所以 Ki = 1/12 * Kp 但这似乎完全错误。 我听说过千文(一款人工智能聊天应用)的事。 1. NXP 应该在第一阶段就实现 Curr & Vol 的标准化。 2. 计算基于零点和控制空间的极点。 我稍后会想办法弄明白。 它说,电机的 PID 参数将首先尝试测量电机的 L、R,然后进行计算。 Re: PID parameters significance mentioned in User guide and how to calculate them ? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好, 我们在网络上的电机控制示例中使用了 PI 控制器。在您编写代码时,Mcat 会帮助计算所用 PI 控制器的参数(对于级联控制结构中的 PMSM,对于六步结构中的 BLDC)。目前,网上还没有使用 PID 控制器结构的示例,也没有可以帮助设置它的工具,但当然,我们的 AMCLIB 库也提供了此功能,作为客户控制结构的构建模块。 希望对您有所帮助。 顺祝商祺! 戴安娜
記事全体を表示
FRDM-IMX93 ASCII Board File Hello, I have pulled the FRDM-IMX93 Design Files from this link: https://www.nxp.com/design/design-center/development-boards-and-designs/frdm-i-mx-93-development-board:FRDM-IMX93 However I do not have Allegro or Extracta.exe to import them to Altium. Can you please supply the LAY-94611_B.brd in ACII format so I can import that into Altium? Thanks, Re: FRDM-IMX93 ASCII Board File Hello, I´m also in need for this file to understand the board better and help development. can you send it to me? Re: FRDM-IMX93 ASCII Board File HI @Cwootton! Thank you for reaching out to NXP Support! I will be sending the required files to you via email shortly. Best regards, Chavira
記事全体を表示
Subject: MPC5605 memory-read issue at 0x00100010 Hello, We have an issue with an ECU using MPC5605. During an EOL memory-dump operation, our toolbox reads memory using a direct CPU byte access: *((uint8_t *)address) From the CAN log: ```text Read 8 bytes from 0x00100008 -> successful Read 8 bytes from 0x00100010 -> ECU stops responding and resets ``` We checked the MPC5606BK Reference Manual, `16234_MPC5606BRM`, Rev. 2: - Table 3-1, page 49, shows `0x00100000 - 0x001FFFFF` as **Reserved**. - Pages 871-872 describe the flash-memory map and flash-emulation mapping. Could you please clarify: 1. Is `0x00100010` a valid/readable address for MPC5605? 2. If it is a reserved address, what happens when software reads it directly? Can it cause an exception or reset? 3. Which reference manual section should we use for the exact MPC5605 memory map? We are also collecting the full MPC5605 part number and silicon revision from the ECU hardware. Best regards, kasirajan C Development Board Re: Subject: MPC5605 memory-read issue at 0x00100010 Hello, Address 0x00100010 belongs to the range 0x00100000-0x001FFFFF, which is marked as Reserved in the MPC560xB memory map. Reserved regions must not be accessed by application software. Accessing such locations may generate a bus-related exception or other device-specific fault response, which can result in loss of communication or a reset if the exception is not handled. Chapter 3 Memory Map petervlna_0-1789455244473.pngpetervlna_0-1789455244473.png Best regards, Peter
記事全体を表示
SC16IS740 最大晶体频率 尊敬的恩智浦技术支持团队: 我们使用 SC16IS740,电源电压为 3.3V。 请问能否确认可以直接连接在 XTAL1 和 XTAL2 之间的外部晶振(晶体振荡器)的最大频率是多少? 数据手册中提到: 适用于外部时钟,晶振(晶体振荡器)最大频率为 24 MHz。 感谢您的支持。 此致, 阿比舍克 Re: SC16IS740 Maximum Crystal Frequency 你好 AbishekDevan 再会! 是的,你说得对;使用外部晶体的极限是 24 MHz。 祝你今天过得愉快,一切顺利。
記事全体を表示
BAM ROMダンプリクエスト - MPC5604B(またはMPC560xBファミリ) 検閲されていないMPC5604B(またはMPC560xB/C評価ボード)をお持ちで、BAMマスクROM(16KB、0xFFFFC000-0xFFFFFFFF)をダンプして共有してくれる方はいらっしゃいますか?自分のチップでMCUの個人的な研究プロジェクトの参考資料として必要です。 よろしくお願いします! Re: BAM ROM dump request - MPC5604B (or MPC560xB family) こんにちは、 こちらにはそのようなEVBはありませんが、チップをサンプリングして自分でダンプを行うことができます。 工場出荷時のサンプルはすべて検閲を受けていません。 https://www.nxp.com/support/sample-and-buy/order-samples:ORDER_SAMPLES?partnum=SPC5604BAVLQ6 こうすることで複数の無料のチップを試すことができます。 よろしくお願いいたします。 ピーター
記事全体を表示
i.MX95 - UUU 工具刷写偶尔会失败 各位专家: 我正在使用 i.MX95 EVK,并将 imx-启动 和(内核 + 根文件系统)刷入 emmc。我在UUU脚本中使用了emmc_all选项进行刷写。 有时,我发现使用此选项进行刷机时会出现失败。以下是失败代码片段。 0x200000002:13-294A7876CE324A4D>Okay (0.403s) 2:13-294A7876CE324A4D>Start Cmd:FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi; 2:13-294A7876CE324A4D>Okay (0.008s) 2:13-294A7876CE324A4D>Start Cmd:FB: ucmd sleep 1 2:13-294A7876CE324A4D>Okay (1.007s) 2:13-294A7876CE324A4D>Start Cmd:FB: ucmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0 2:13-294A7876CE324A4D>Fail (0.187s) 请问是否有人遇到过类似的故障,以及是否有解决办法可以缓解这个问题? 提前感谢! BR, 阿伦·库马尔 Re: i.MX95 - UUU tool flashing fails occasionally 你好, 请问您能否分享一下您使用的完整命令?另外,请告知您测试时使用的是 EVK 还是 FRDM 开发板,以及 BSP 版本和 UUU 版本。 问候。
記事全体を表示
i.MX95 - UUU tool flashing fails occasionally Dear Experts, I am using i.MX95 EVK and flashing the imx-boot and the (kernel + rootfs) in emmc. I used emmc_all option in UUU script for flashing. Sometimes, I observed failures in flashing with that option. Please find below the failure snippets 0x200000002:13-294A7876CE324A4D>Okay (0.403s) 2:13-294A7876CE324A4D>Start Cmd:FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi; 2:13-294A7876CE324A4D>Okay (0.008s) 2:13-294A7876CE324A4D>Start Cmd:FB: ucmd sleep 1 2:13-294A7876CE324A4D>Okay (1.007s) 2:13-294A7876CE324A4D>Start Cmd:FB: ucmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0 2:13-294A7876CE324A4D>Fail (0.187s) Please let me know if anyone has faced similar failures and if there are solutions available to mitigate this problem Thanks in Advance ! BR, Arun Kumar Re: i.MX95 - UUU tool flashing fails occasionally Hello,  Can you please share the complete command you are using?, also let me know if you are testing with an EVK of FRDM board and the BSP version and UUU version. Regards.  
記事全体を表示