Multi Source Translation Content

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multi Source Translation Content

讨论

排序依据:
rw612 sdk 26.06 Hi, I downloaded SDK 26.06 for rw612, but it is not available in vs code, i imported the sdk, but i cannot generate project, it is not in the list also cannot open existing project which i created by 26.03 gtecaskari_0-1782801151226.png gtecaskari_1-1782801204966.png it is not in the dropdown list  Re: rw612 sdk 26.06 Hi. I did, but did not work. When I want to import the project, it says board not supported ( or something like this). but i generated SDK from https://mcuxpresso.nxp.com/ for my board. Re: rw612 sdk 26.06 Hello, Hope you are doing well. I am not able to reproduce this behavior. Ricardo_Zamora_1-1782845633134.png I would recommend updating the MCUXpresso Installer, and checking that all Software Kits are updated. Best Regards, Ricardo Re: rw612 sdk 26.06 Hello, Could you please try importing repository? Regards, Ricardo Re: rw612 sdk 26.06 hi, it worked, but I should delete other sdks and then add
查看全文
RW612 SDK 26.06 您好,我下载了适用于 RW612 的 SDK 26.06,但它在 VS Code 中不可用。我已经导入了 SDK,但无法生成项目,它不在列表中,也无法打开我使用 26.03 版本创建的现有项目。 gtecaskari_0-1782801151226.png gtecaskari_1-1782801204966.png 它不在下拉列表中 Re: rw612 sdk 26.06 你好。我试过了,但是没成功。当我尝试导入项目时,它显示“不支持的板”(或类似信息)。但我已从https://mcuxpresso.nxp.com/为我的开发板生成了 SDK。 Re: rw612 sdk 26.06 你好, 希望你一切都好。我无法重现此现象。 Ricardo_Zamora_1-1782845633134.png 我建议更新 MCUXpresso 安装程序,并检查所有软件包是否已更新。 顺祝商祺! 里卡多 Re: rw612 sdk 26.06 你好, 请问您能否尝试导入仓库? 此致, 里卡多 Re: rw612 sdk 26.06 嗨,它奏效了,但我应该先删除其他 SDK,然后再添加。
查看全文
Can I use memory config from tflm_label_image_ext_mem for the example tflm_cifar10_cm33_core0? Have a nice day. Currently I am using eiq example tflm_cifar10_cm33_core0 to model on NPU mode. Modeldata is saved in SRAM. Inference time is good. And here is memory configuration. I modified this eiq example for my models with 5 classes nnxxpp_0-1782788058723.png https://docs.nxp.com/bundle/AN14700/page/topics/eiq_enablement.html But now my model is larger and I want to locate NPU tflite model on external memory. Modeldata is located in Flash. And here is configuration from eiq example tflm_label_image_ext_mem nnxxpp_2-1782788224534.png nnxxpp_1-1782788176608.png https://docs.nxp.com/bundle/AN14700/page/topics/imx_rt700_system_details.html My target is that, I want to keep source code from tflm_cifar10_cm33_core0 (I dont want to create new source code with tflm_label_image_ext_mem), but I want to locate my NPU tflite model on external memory.  My solution that I will change only memory configuration from SRAM to external memory as above images. Is that right? Or I need to change more other configurations. Re: Can I use memory config from tflm_label_image_ext_mem for the example tflm_cifar10_cm33_core0? Hi @nnxxpp , Thanks for your clarification. Please do not use `--use-sequencer` together with external-memory model execution. For the `tflm_label_image_ext_mem` example, please keep `--fetch-constants-to-sram` and remove `--use-sequencer`, since the model is executed from external memory. Please try converting the model as below: ./neutron-converter \ --input QAT.tflite \ --output QAT_NPU.tflite \ --target imxrt700 \ --dump-header-file-output \ --dump-header-file-input \ --fetch-constants-to-sram   mayliu1_0-1782872651573.png mayliu1_1-1782872691770.png Wish it helps you Best Regards May Re: Can I use memory config from tflm_label_image_ext_mem for the example tflm_cifar10_cm33_core0? @mayliu1  Hi. This is new issue (not resolved yet). This issue is related to deploy NPU tflite model on external memory (not on SRAM). Currently, I am using eiq sample tflm_label_image_ext_mem from SDK of MIMRT700. I could successfully run this example. This example is for model mobilenetv1, size=224 and number of classes=1000. I tried to replace the sample's model by my model (same classification model) but with different number of classes. I have changed labels.h (for label names),  I replaced the sample's model by my model and I keep the same name I also change model_data_len in the file model_data.h I could build, but when running debug, the program is stopping at "Static processing" and did not give result. nnxxpp_0-1782812429613.png There is an message in the above image Unable to save model handle, call neutronModelUnprepare() when done but one NXP's employee said that it is not error. https://community.nxp.com/t5/eIQ-Machine-Learning-Software/eIQ-FAQ/ta-p/1099741 I see that in the case NPU model is located on external memory, we use model with extension .tflite (not header file .h in the case we locate model on SRAM). I convert model with flag --fetch-constants-to-sram to locate NPU model on external memory like this ./neutron-converter \ --input QAT.tflite \ --output QAT_NPU.tflite \ --target imxrt700 \ --dump-header-file-output \ --dump-header-file-input \ --use-sequencer \ --fetch-constants-to-sram   Because I did not see any tutorial from NXP to set up and configs (where and how to change source code), so I tried with the above steps, but it did not work. Could you help me? Thank you. Re: Can I use memory config from tflm_label_image_ext_mem for the example tflm_cifar10_cm33_core0? Hi @nnxxpp , Thank you so much for your interest in our products and for using our community. I apologize for the delayed response. I noticed that in your previous post, you mentioned that the issue has already been resolved. I’m glad to hear that everything is working now. Thank you again for your understanding. Best regards, May Re: Can I use memory config from tflm_label_image_ext_mem for the example tflm_cifar10_cm33_core0? Thank you so much for supporting me. It worked correctly
查看全文
Accessing my kernel rpmsg buffer from user space Hi, I have been able to communicate between my imx8mp MPU and the MCU.  However, I want to access the data in the shared memory from the user space.  Is there an example for this? I would also like to ask if the imx_rpmsg_pinpong.c device driver can be extended to handle linux Userspace I/O for the communication between the kernel space and the user space. Thanks i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Re: Accessing my kernel rpmsg buffer from user space Hi, I am also looking at the same issue. The example you provided works with the kernel module. However, I am actually looking for a example userspace application. Could you provide a sample C program i can run on the linux side within userspace. Thanks! Re: Accessing my kernel rpmsg buffer from user space Hi @ababatola , I hope you're doing well! Sorry for the late reply. I'd recommend taking a look at the rpmsg_lite_str_echo_rtos multicore example found in the i.MX 8M Plus SDK. It's a simple application which allows you to send a message from the Cortex A to the Cortex M and then M4 displays what is received, and echoes back the same message as an acknowledgement.  You can build and download the SDK from https://mcuxpresso.nxp.com/ Let me know if this works for you. Best regards, Hector.
查看全文
RW612 SDK 26.06 こんにちは、rw612用のSDK 26.06をダウンロードしましたが、VS Codeでは利用できません。SDKをインポートしましたが、プロジェクトを生成できず、リストにも表示されません。また、26.03で作成した既存プロジェクトを開けられません gtecaskari_0-1782801151226.png gtecaskari_1-1782801204966.png ドロップダウンリストにありません Re: rw612 sdk 26.06 こんにちは。やってみたが、うまくいかなかった。プロジェクトをインポートしようとすると、「ボードがサポートされていません」(またはこれに類するメッセージ)と表示されます。でも、ボード用のSDKsは https://mcuxpresso.nxp.com/ から生成しました。 Re: rw612 sdk 26.06 こんにちは、 あなたの調子が良いといいのですが。この現象を再現することができません。 Ricardo_Zamora_1-1782845633134.png MCUXpressoインストーラーを更新し、すべてのソフトウェアキットが更新されているか確認することをお勧めします。 よろしくお願いいたします。 リカルド Re: rw612 sdk 26.06 こんにちは、 リポジトリのインポートを試していただけますか? よろしくお願いいたします。 リカルド Re: rw612 sdk 26.06 こんにちは、うまくいきましたが、他のSDKを削除してから追加しなければなりません
查看全文
我能否将 tflm_label_image_ext_mem 中的内存配置用于示例 tflm_cifar10_cm33_core0? 祝你今天过得愉快。 目前我正在使用 eIQ 示例tflm_cifar10_cm33_core0在 NPU 模式下进行建模。模型数据保存在SRAM中。推理时间不错。以下是内存配置。我修改了这个 eIQ 示例,使其适用于我的 5 类模型。 nnxxpp_0-1782788058723.png https://docs.nxp.com/bundle/AN14700/page/topics/eiq_enablement.html 但现在我的模型更大了,我想把 NPU tflite 模型放在外部存储器上。模型数据位于闪存中。以下是来自 eiq 示例tflm_label_image_ext_mem的配置 nnxxpp_2-1782788224534.png nnxxpp_1-1782788176608.png https://docs.nxp.com/bundle/AN14700/page/topics/imx_rt700_system_details.html 我的目标是,我想保留tflm_cifar10_cm33_core0的源代码(我不想使用tflm_label_image_ext_mem 创建新的源代码),但我想将我的 NPU tflite 模型放在外部存储器上。 我的解决方法是,仅将内存配置从 SRAM 更改为外部存储器,如上图所示。是这样吗?或者我还需要更改其他配置。 Re: Can I use memory config from tflm_label_image_ext_mem for the example tflm_cifar10_cm33_core0? 嗨@nnxxpp , 谢谢你的解释。 请勿将 `--use-sequencer` 与外部存储器模型执行一起使用。 对于 `tflm_label_image_ext_mem` 示例,请保留 `--fetch-constants-to-sram` 并删除 `--use-sequencer`,因为该模型是从外部存储器执行的。 请尝试按如下方式转换模型: ./neutron-变流器 \ --输入 QAT.tflite\ --输出 QAT_NPU.tflite\ --target imxrt700 \ --dump-header-file-output \ --dump-header-file-input \ --fetch-constants-to-sram   mayliu1_0-1782872651573.png mayliu1_1-1782872691770.png 希望对你有帮助 顺祝商祺! 5月 Re: Can I use memory config from tflm_label_image_ext_mem for the example tflm_cifar10_cm33_core0? @mayliu1 你好。这是一个新问题(尚未解决)。这个问题与将 NPU tflite 模型部署到外部存储器(而不是 SRAM)有关。 目前,我正在使用 MIMRT700 SDK 中的 eiq 示例tflm_label_image_ext_mem 。我成功运行了这个示例。此示例适用于模型 mobilenetv1,大小=224,类别数=1000。 我尝试用我的模型(相同的分类模型)替换样本的模型,但类别数量不同。 我修改了 labels.h 文件。(用于标签名称) 我用自己的模型替换了示例中的模型,并保留了相同的名称。 我还修改了 model_data.h 文件中的model_data_len 参数。 我可以版本成功,但是运行调试程序时,程序在“静态处理”阶段停止,没有给出结果。 nnxxpp_0-1782812429613.png 上图中显示一条消息“无法保存模型句柄,完成后请调用 neutronModelUnprepare()”,但一位恩智浦员工表示这不是错误。https ://community.nxp.com/t5/eIQ-Machine-Learning-Software/eIQ-FAQ/ta-p/1099741 我看到,如果 NPU 模型位于外部存储器上,我们使用扩展名为 .tflite 的模型。(如果模型位于 SRAM 上,则不是头文件 .h)。 我使用 ` --fetch-constants-to-sram`标志转换模型,以便将 NPU 模型定位到外部存储器上,如下所示。 ./neutron-变流器 \ --输入QAT.tflite \ --输出QAT_NPU.tflite \ --target imxrt700 \ --dump-header-file-output \ --dump-header-file-input \ --use-sequencer \ --fetch-constants-to-sram   由于我没有看到 NXP 提供的任何设置和配置教程(在哪里以及如何更改源代码),所以我尝试了上述步骤,但没有成功。 你能帮帮我吗?谢谢。 Re: Can I use memory config from tflm_label_image_ext_mem for the example tflm_cifar10_cm33_core0? 嗨@nnxxpp , 非常感谢您对我们产品的关注以及对我们社区的使用。 很抱歉回复晚了。 我注意到您在之前的帖子中提到这个问题已经解决了。很高兴听到一切都恢复正常了。 再次感谢您的理解。 顺祝商祺! 5月 Re: Can I use memory config from tflm_label_image_ext_mem for the example tflm_cifar10_cm33_core0? 非常感谢你的支持。它运行正常。
查看全文
S32K3MCU 发送慢通道 无法接收数据。 大家好 我正在使用 S32K311 的 SENT 接口接收数据,我遇到了这样一种情况:快通道正常接收数据,但慢通道无法接收任何数据。 我监测了 SENT 错误通知功能,没有发现任何异常。 MCU 型号为 S32K311 RTD 版本:S32DS 3.6.2RTD6.0.0 发送传感器:Sensata 压力传感器增强型慢速消息 首先,我知道 SENT 逻辑是在“Flexio_Sent_Ip_ProcessSerialMsg”函数中处理的,随后,在外层函数中,它会监测“Data->SerialState”和“FastMsgCount”变量,以确定慢通道是否已完成接收数据。 khty_0-1782783940723.png 于是,我捕获了相关的比特信息。 bit(x):已发送快速通道状态半字节位 S: " STATUS_SENT_SERIAL_SHORT" 。 E:" STATUS_SENT_SERIAL_ENHANCED" khty_3-1782786765437.png 我发现慢速通道的解析逻辑反复跳转,无法正常解析。 在特定情况下,SENT 的处理逻辑是否存在错误? 谢谢! Re: S32K3MCU SENT slow channel Cannot receive data. SOC端有任何错误日志吗? Re: S32K3MCU SENT slow channel Cannot receive data. 你好@khty , 能否分享一下Sensata传感器的发送配置信息?从你的图片中,我可以看到第 8 位 C 位被设置为 0;我假设使用的是 8 位消息 ID,12 位数据格式。 由于您的快速通道已正确接收,并且没有报告 SENT 错误通知,因此我了解到问题与处理功能有关。 我尚未发现任何关于频道接收速度慢的已知问题;但是,我已经与内部团队展开了讨论,让我尝试获取有关此问题的更多信息。 最后,您能否提供至少 18 个连续的 SENT 帧的完整捕获文件?这样我们就可以进一步检查RTD状态机的行为是否与预期的增强型串行解码序列相匹配。 此致, 朱利安 Re: S32K3MCU SENT slow channel Cannot receive data. 您好,感谢您快速回复我的问题。 Sensata提供的传感器配置信息如下图所示: khty_0-1783154149669.png 关于您最后一个要求,我需要至少连续 18 个 SENT 帧的完整捕获数据。我已经将其放在“bitChange.xlsx”文件中。文件在附录中。 我在表格中显示了每个捕获的状态半字的第二位和第三位。 表格中,每一列代表一条已发送的消息。每个大的黑色方框内包含一条 slowChannel 消息。蓝色区域为ID区域,绿色区域为CRC校验区域,黄色区域为数据区域。底部的信息为人工分析结果。 khty_1-1783154875344.png 如果您需要任何其他信息,请告诉我,我会尽快回复。 Re: S32K3MCU SENT slow channel Cannot receive data. 发送的快速错误通知和慢速错误通知均未报告任何故障。 您可以读取记录在“bitchange.xlsx”中的数据。用于分析,因为它包含我记录的快速通道的每个状态半字的第 2 位和第 3 位的信息。Bit1 和 Bit0 信息被丢弃,因为它们在慢速信道中没有意义。 同时,我手动解析了慢速频道信息,并用黑色方块进行了标识。 在“bitchange.xlsx”中,“State”行中的数据对应于代码中的“ Flexio_Sent_Ip_axFastData[Instance][ChannelId].SerialState ”。它负责检测和识别慢通道是“短”还是“增强”。“计数”代表“ Flexio_Sent_Ip_axFastData[Instance][ChannelId].FastMsgCount ”,它负责计算慢速通道的接收长度。 我认为我们没有收到任何慢通道数据的原因是代码无法正确识别慢通道是“短”通道还是“增强”通道。您可以阅读“bitchange.xlsx”来发现识别状态在“ STATUS_SENT_SERIAL_IDLE ”、“ STATUS_SENT_SERIAL_SHORT ”和“ STATUS_SENT_SERIAL_ENHANCED ”之间不断跳转。 khty_0-1783299454656.png 当识别状态发生转换时,“ Flexio_Sent_Ip_ProcessSerialMsg ()”函数返回“ STATUS_FLEXIO_SENT_IP_ERROR ”,但该返回值仅重置了上层函数“ Flexio_Sent_Ip_DmaDataProcessing ()”中的SerialState和FastMsgCount ,并未调用SentFastErrorNotif ()。因此,我无法通过快速错误通知获取任何错误信息。 在“bitChange.xlsx”中 khty_1-1783300326735.png 我们可以从 T 列开始,此时SerialState = STATUS_SENT_SERIAL_IDLE , FastMsgCount = 0。 当我们收到 U 列时, Flexio_Sent_Ip_ProcessSerialMsg()认为 bit3 == 1,因此它将其视为慢通道的开始信号,并将SerialState设置为STATUS_SENT_SERIAL_SHORT , FastMsgCount设置为 1。 当我们收到 V 列时, Flexio_Sent_Ip_ProcessSerialMsg () 认为 bit3 == 0,因此它保持SerialState = STATUS_SENT_SERIAL_SHORT并将FastMsgCount加 2。 当我们收到 W 列时, Flexio_Sent_Ip_ProcessSerialMsg () 认为 bit3 == 1。此时,由于FastMsgCount == 2,不满足跳转到STATUS_SENT_SERIAL_ENHANCED 的条件,只能返回STATUS_FLEXIO_SENT_IP_ERROR 。在Flexio_Sent_Ip_DmaDataProcessing () 中,它会重置SerialState和FastMsgCount 。 顺便说一下,我使用 DMA 接收 SENT 数据,目前只确认了 DMA 接收方式存在问题。目前,我无法确认中断和轮询方法是否也存在同样的问题。 Re: S32K3MCU SENT slow channel Cannot receive data. 嗨@khty , 感谢您提供的补充信息。这样就更清楚了。 这似乎表明解析增强型慢消息时可能存在 RTD 问题,但是,由于我没有特定的硬件配置,因此我无法重现该问题。 我已经将此信息转发给内部团队,如有任何新消息,我会及时通知您。 此致, 朱利安
查看全文
ADC配置问题 嗨@Senlent , 我也有和你上面提到的同样的问题。 我们的外部振荡器时钟频率为 25 MHz。根据 S32K322 数据手册,ADC 支持最高 80 MHz 的频率,所以我将预分频器设置为 2。我还将采样时间设置为 1.2 微秒,并将 BCTU 模式设置为触发模式。但是,当在同一个 ADC0 外设上同时执行 BCTU 方法和常规链式方法时,仍然会得到噪声数据。是否有解决方法或替代方法可以安全地在同一个 ADC0 外设上运行这两种方法? praveen_ext_0-1782473167287.png praveen_ext_1-1782473350906.png praveen_ext_2-1782473423830.png S32K1系列的S32SDK Re: ADC Configuration Issue 你好@praveen_ext , 考虑到之前的社区讨论,BCTU 控制模式下的行为是预期的:当 ADC 由 BCTU 在控制模式下控制时,无法在同一个 ADC 实例上独立启动正常的转换。这就解释了为什么在控制模式下电流检测变得更加稳定,但正常链中配置的电压和温度通道停止工作。 在触发信号模式下,情况就不同了。此模式允许 BCTU 触发信号的转换以及正常/注入的转换,但所有这些转换仍然共享同一个 ADC 实例,因此共享相同的 ADC 转换资源。对于时间要求严格的电流检测应用场景,特别是与 PWM 同步时,重要的不仅是转换是否可行,而且采样时刻是否保持确定性。 从共享数据来看,电流感知信号似乎基本稳定,但偶尔会出现较大的尖峰/下降。这些看起来不像普通的随机模拟噪声。它们看起来更像是与事件相关的异常值,可能是由转换调度、结果处理或 BCTU 触发信号的转换与同一 ADC 外设上的正常链转换之间的交互引起的。 因此,我建议首先确定问题是否是由 ADC 实例的混合使用引起的: 1. 请仅在触发模式下运行 BCTU 触发信号电流检测,并完全禁用正常链执行。 - 电流感知尖峰现象是否仍然存在? 2. 请仅运行正常的链式转换,并禁用 BCTU 触发信号的电流检测。 电压和温度通道是否仍然稳定? 3. 请检查电流感知尖峰是否与应用程序开始正常链转换的时刻相关。  您能否也说明一下,在 BCTU 触发信号电流检测运行时,正常的链式转换是如何启动的?例如,正常链是否由软件、中断或另一个调度程序任务定期启动? 还有一点需要确认:从您的通道列表中,ADC1-P2 和 ADC1-P3 似乎既被提及为 BCTU 电流检测通道,也被提及为正常链通道。请问这些通道是否是两种采集方式有意使用的,还是仅仅是描述/配置不符?  如果禁用正常采集链后尖峰消失,则问题可能不在于ADC的电气配置本身,而在于同一ADC实例上两个采集流程的时序/调度。在这种情况下,可能的解决方法包括: - 确保电流检测通道完全由BCTU控制, - 如果可用,将速度较慢的电压/温度测量移至另一个ADC实例进行测量。 - 或者仅在不会干扰 BCTU/PWM 同步电流测量的时间窗口内安排正常的链式转换。   完成隔离测试后,仍建议检查模拟前端,特别是对于持续存在噪声的信号: - 被测信号的源阻抗, - 外部RC滤波器值, - ADC输入电容值, - 将电容放置在靠近MCU ADC输入引脚的位置, - 配置的采样时间是否足以满足给定的源阻抗和外部元器件的要求。   关于ADC精度/噪声的类似讨论,请参见此处: - S32K3 ADC 值不准确的问题: https://community.nxp.com/t5/S32K/Issue-with-Inaccurate-ADC-Values-on-S32K3/mp/2033042   - 与 FS32K146HAT0MLLT 接口的烟雾探测器: https://community.nxp.com/t5/S32K/Smoke-detector-interfacing-with-FS32K146HAT0MLLT/mp/1773787   - S32K3 关于 ADC 精度和结果的困惑: https://community.nxp.com/t5/S32K/S32K3-Confusion-about-ADC-accuracy-and-results/mp/2006783   顺祝商祺! 帕维尔
查看全文
CAN+DMAルーチンの助けを求めています 現在、s32ds3.4のコンパイラバージョンを搭載したcan+dmaプロジェクトが必要です。RTDバージョン2.0.0、チップはS32K344。どこでそれを見つけるCANですか? Re: Seeking help with a CAN+DMA routine 実は、このグラフィカルインターフェースの設定を見たいんです。バージョン番号が間違っていると、グラフィカルインターフェースを開けません。だから私は前述のバージョンでプロジェクトを依頼したのです。 ssslz_0-1782868321796.png よろしくお願いいたします。 ssslz Re: Seeking help with a CAN+DMA routine こんにちは、 @ssslz さん、 既存の例を参照できます: TX/RX/EnhanceRXFIFO DMAテストS32K344 FlexCAN_Ip S32DS3.5 RTD400の例。 DMAは拡張RXFIFOの読み取りに使用され、ウォーターマークは5に設定されています。S32DS 3.5およびRTD 4.0.0に基づいています。しかし、設定をコピーするだけでも大丈夫です。 よろしくお願いします、 ジュリアン Re: Seeking help with a CAN+DMA routine こんにちは、 @ssslz さん。 はい、残念ながらこれはS32DSと他のRTDバージョンの制限で、同時にインストールすることはできません。 新しいS32DSインスタンスをダウンロードしてRTD 4.0.0をインストールしてインポートし、プロジェクトの設定を確認することもできますし、 「インポート > S32 設定ツール > 設定のインポート (*mex)」を使用して、サンプルの設定を新しい 2.0.0 プロジェクトにインポートし、バージョン不一致によって発生したエラーを修正します。 ともかく、RTD 4.0.0の設定も共有できます参考までにFlexCAN DMAの例を示します。 Julin_AragnM_2-1782938742350.png Julin_AragnM_3-1782938747483.png Julin_AragnM_4-1782938751216.png よろしくお願いします、 ジュリアン
查看全文
2026年最佳IPTV服务——我今年测试过的最可靠的IPTV提供商 过去几年,电视流媒体发生了显著变化。随着有线电视价格持续上涨,越来越多的人开始寻找价格实惠的替代方案,以便无需签订长期合同或支付高昂的月费,即可观看直播电视、体育赛事、电影和国际娱乐节目。 官方网站: 4Kiptvusa 最大的挑战在于找到一家能够提供稳定流畅服务的IPTV供应商。许多服务商宣称拥有数千个频道和各种高级功能,但用户订阅后却经常遇到缓冲、频道离线、画质差以及服务器不稳定等问题。 在对 Firestick、Android TV、智能电视和移动设备上的多种 IPTV 服务进行评估后, 4Kiptvusa.online 平台始终提供流畅的使用体验。 4Kiptvusa.online 似乎更注重流媒体的质量和稳定性 ,而非仅仅追求频道数量 。对大多数观众而言,稳定的流媒体播放和快速的频道加载速度远比拥有成千上万个经常无法正常播放的频道重要得多。 视频质量是该服务表现良好的领域之一。高清频道画面清晰细腻,而支持的 4K 内容可在大屏幕上提供清晰的观看体验。在体育赛事直播、动作电影和付费娱乐节目播出期间,这种差异会变得尤为明显。 IPTV 服务通常在观看高峰时段面临挑战。大型足球比赛、篮球比赛、格斗赛事和其他高需求直播节目都可能使性能较弱的系统不堪重负。在测试过程中, 4Kiptvusa.online在繁忙时段仍能保持稳定的播放和可靠的性能,帮助用户避免了低质量 IPTV 服务商常见的卡顿问题。 该平台提供广泛的内容,包括体育直播频道、娱乐频道、电影、电视剧、新闻频道、纪录片、儿童节目以及来自各个地区的国际内容。在线点播库会定期更新,让订阅用户能够观看热门版本和流行内容。 Re: Best IPTV Service 2026 – The Most Reliable IPTV Provider I Tested This Year 嗨nigmatv 感谢您联系恩智浦半导体并对我们的产品感兴趣。 请您与我们联系并告知您的咨询是否与任何特定的恩智浦产品或设备有关?如果您需要进一步的帮助,我们很乐意效劳。 请访问我们的恩智浦网站,查找您需要的零件: https://www.nxp.com/ 如果您的问题与恩智浦产品无关,恐怕我们在这方面提供详细支持的能力有限。非常感谢您的理解。 如有需要,请随时分享更多详情——我们非常乐意尽力提供帮助。 祝你今天过得愉快。
查看全文
LPC1518JBD64 VScode におけるMCUXpressoのSDK 私のターゲットMCUはLPC1518JBD64です。このMCUをVScodeで扱いたいです。VScodeでMCUXpresso ideをダウンロードしました。 MCUXpressoでコーディングを始めるためのLPC1518JBD64 SDKを見つけるのに苦労しています。必要なSDKのガイドや役立つダウンロードリンクが必要です。そうすれば、MCUのコードを書くためにVScode LPC1518JBD64作業を始められます。 Re: LPC1518JBD64 SDK for MCUXpresso in VScode こんにちは、 LPC1518JBD64、MCUXpresso SDK Builderに直接デバイス固有のMCUXpresso SDKsパッケージが見つからない場合もあります。このMCUはLPC15xxファミリに属し、NXPのこのファミリのサポートは主にLPCOpenの例やライブラリを通じて提供されています。 以下のオプションをご確認ください。 NXPのLPCOpenソフトウェア開発プラットフォームページからLPC15xx用のLPCOpenパッケージをダウンロードしてください。 すでにMCUXpresso IDEをインストールしているなら、このフォルダもチェックしてください: \ide\Examples MCUXpresso IDEは通常、LPCOpenのサンプルパッケージを含んでいます。 LPC15xx/LPC1549のサンプルプロジェクトから始めて、LPC1518JBD64用にプロジェクト設定を調整してください。 起動ファイル、リンカースクリプト、フラッシュ/RAMサイズ、クロック設定、およびピン構成がLPC1518JBD64と一致していることを確認してください。 VS Codeについては、MCUXpresso for VS Code拡張機能を使い、既存のプロジェクトやリポジトリをインポートしてください。その後、LinkServer、J-Link、または他の対応SWDプローブを使ってビルドやデバッグが可能です。 また、LPC1518JBD64は64KBのフラッシュと12KBのSRAMを持っているため、別のLPC15xx例からポートする際はリンカーファイルを慎重に確認する必要があります。 NXPの役立つページはこちら: MCUXpresso SDK Builder LPCOpenライブラリとサンプル LPC15xx用LPCOpenソフトウェア MCUXpresso for Visual Studio Code LPC1518JBD64製品ページ 要するに、LPC15xx用のLPCOpenを出発点として使い、最新のMCUXpresso SDKs Builderパッケージだけを探すのではなく、 Re: LPC1518JBD64 SDK for MCUXpresso in VScode 解決策が見つかりました。 LPCXpresso IDEをダウンロードしました。 無料版を使用するには、ライセンスを追加してください。公式ウェブサイトからライセンスを取得し、それを使ってLPCXpresso IDEを起動しています。 次に、LPC15xxライブラリとサンプルコードをダウンロードします。例コードをIDEで開いてコンパイルできます。 ターゲットMCUとして、Project >オプション(プロジェクトを右クリック)でC/C++built >MCU設定>LPC1518を選択していました。
查看全文
Using the uart port for high baud rate on NXP i.MX6 We plan to use UART communication on the NXP i.MX6 (Cortex-A9) at baud rates of 230.4 kbps or 460.8 kbps. According to the following resolved thread, Solved: Re: how to enhance uart baud rate for imx6 - NXP Community it is stated that at baud rates higher than 115.2 kbps, the processor seemed can't receive all bytes timely and the kernel returns "Rx FIFO overrun" random. To solve this matter, two ways are suggested: Modify the driver code to enable DMA transfer Increase the buffer of DMA receive which above of bytes per frame I have two questions. (The second one is optional.) ① Could you tell me the specific procedure to modify the driver code to enable DMA transfer? ② If there is any information regarding the error rate when operating under the above conditions, we would appreciate it if you could share that as well. Re: Using the uart port for high baud rate on NXP i.MX6 HI @INOUE, Thank you for contacting NXP Support! Unfortunately, we do not have any documentation or application note that describes this procedure. You will need to implement and validate it on your own based on the information provided in the Reference Manual. Please refer to the RM for the hardware details, register descriptions, and recommended programming sequence. Best regards, Chavira Re: Using the uart port for high baud rate on NXP i.MX6 Sorry for the delayed response. First, I understand. We will implement based on the Reference Manual.
查看全文
NXPには外部メモリでtflite NPUモデルを動かすチュートリアルはありますか? NXPが外部にNPUモデルをeiqで動かす記事tflm_label_image_ext_mem例メモリ https://docs.nxp.com/bundle/AN14700/page/topics/external_memory.html を見ました EIQ例については言及だけで、外部メモリの新しいNPUモデルに適用する例をどのように修正するかの詳細は触れられていませんでした。一方、NXPはSRAM上で新しいNPUモデルを動かすためのソースコード変更の詳細なガイドラインを https://docs.nxp.com/bundle/AN14700/page/topics/Note_about_the_source_code_in_the_document.html 現在、外部メモリ上でNPUモデルを展開したいと考えています。 詳細なガイドラインをお持ちでしたら、ぜひ共有してください。 よろしくお願いします。 Re: Does NXP have any tutorial to run tflite NPU model on external memory? こんにちは、 @nnxxpp さん。 私たちの製品にご関心を寄せ、コミュニティをご利用いただき、本当にありがとうございます。 外部メモリからNPUモデルを実行したい場合は、通常のSRAMベースのtflm_label_image例ではなく、tflm_label_image_ext_mem例から始めることをお勧めします。 詳細については、tflm_label_image_ext_mem MCUXpresso SDKのドキュメントをご参照ください。 tflm_label_image_ext_mem — MCUXpresso SDK ドキュメント mayliu1_0-1782871879601.png お役に立てれば幸いです。 よろしくお願いいたします。 5月 Re: Does NXP have any tutorial to run tflite NPU model on external memory? @mayliu1 ありがとう。いくつかの試行を試しましたが、あなたが言及したように、モデルを外部メモリで見つける際に シーケンサー は使わないべきだと分かりました。 あなたが添付したNXPのドキュメントを初めて見ました。役立つドキュメントをありがとうございます。 Re: Does NXP have any tutorial to run tflite NPU model on external memory? こんにちは、 @nnxxpp さん。 ご意見ありがとうございます。ドキュメントが役に立ってよかったです。 今後新しい質問があれば、どうぞNXPコミュニティに投稿してください。 喜んでお手伝いいたします。 よろしくお願いいたします。 5月
查看全文
Does NXP have any tutorial to run tflite NPU model on external memory? I see that NXP has this article about running NPU model on external with eiq tflm_label_image_ext_mem example memory https://docs.nxp.com/bundle/AN14700/page/topics/external_memory.html It only mentioned about eiq example, but did not mention details how to modify this example for new NPU models on external memory. In opposite, NXP have very detailed guideline how to modify source code to run new NPU models on SRAM https://docs.nxp.com/bundle/AN14700/page/topics/Note_about_the_source_code_in_the_document.html Currently, I want to deploy NPU model on external memory. If you have detailed guideline, please share with us. Thank you. Re: Does NXP have any tutorial to run tflite NPU model on external memory? Hi @nnxxpp , Thank you so much for your interest in our products and for using our community. If you want to run the NPU model from external memory, I suggest starting from the tflm_label_image_ext_mem example instead of the normal SRAM-based tflm_label_image example. Please refer to the tflm_label_image_ext_mem MCUXpresso SDK documentation for more details. tflm_label_image_ext_mem — MCUXpresso SDK Documentation mayliu1_0-1782871879601.png Wish it helps you Best Regards May Re: Does NXP have any tutorial to run tflite NPU model on external memory? Hi @nnxxpp , Thank you for your feedback. I'm glad the documentation was helpful. If you have any new questions in the future, please feel free to post them in the NXP Community. We'll be happy to help. Best Regards May Re: Does NXP have any tutorial to run tflite NPU model on external memory? @mayliu1  Thank you. I have tried several trials and found that we must to not use sequencer when locate model on external memory same as you mentioned. This is the first time I see NXP's documentation that you attached. Thank you so much for helpful documentation.
查看全文
Best IPTV Service 2026 – The Most Reliable IPTV Provider I Tested This Year Television streaming has changed significantly over the last few years. As cable prices continue to rise, more people are looking for affordable alternatives that provide access to live TV, sports, movies, and international entertainment without long-term contracts or expensive monthly bills. web site official  : 4Kiptvusa The biggest challenge is finding an IPTV provider that delivers consistent performance. Many services advertise thousands of channels and premium features, but users often encounter buffering, offline channels, poor picture quality, and unreliable servers after subscribing. After evaluating multiple IPTV services across Firestick, Android TV, Smart TVs, and mobile devices, one platform that consistently delivered a smooth experience was 4Kiptvusa.online Rather than focusing only on channel numbers, 4Kiptvusa.online appears to prioritize streaming quality and reliability. For most viewers, stable streams and quick channel loading times are far more important than having access to thousands of channels that rarely function properly. Video quality is one of the areas where the service performs well. HD channels appear clear and detailed, while supported 4K content provides a sharp viewing experience on larger screens. This difference becomes especially noticeable during live sports, action movies, and premium entertainment broadcasts. Peak viewing hours are often where IPTV services struggle. Major football matches, basketball games, combat sports events, and other high-demand broadcasts can overload weaker systems. During testing, 4Kiptvusa.online maintained stable playback and reliable performance during busy periods, helping viewers avoid the interruptions commonly experienced with lower-quality IPTV providers. The platform offers a broad range of content, including live sports channels, entertainment networks, movies, TV series, news channels, documentaries, kids programming, and international content from various regions. The video-on-demand library is updated frequently, giving subscribers access to popular releases and trending content. Re: Best IPTV Service 2026 – The Most Reliable IPTV Provider I Tested This Year Hi nigmatv Thank you for reaching out to NXP and for your interest in our products. Could you please let us know if your inquiry is related to any specific NXP product or device? We would be happy to assist you further if so. Pls review our NXP website to find which part do you need:  https://www.nxp.com/ If your question is not related to NXP products, we’re afraid we may have limited ability to provide detailed support in this case. We truly appreciate your understanding. Please feel free to share more details if applicable — we’re always glad to help where we can. Have a nice day.
查看全文
MLB The Show 26: Ultimate Guide to Unlocking 96 OVR Ronald Acuña Jr. If you are looking to inject some serious power and speed into your Diamond Dynasty squad without spending a single Stub, you need to fire up your console right now. The limited-time June Countdown Program is officially in its final hours, expiring tonight, June 30, 2026, at 11:59 PM PT. Sitting right at the 100-point checkpoint of this program is the highly coveted 96 OVR Awards Series Ronald Acuña Jr. This Red Diamond center fielder is an absolute game-changer for budget squads and god-squads alike. If you miss tonight's deadline, your only option will be pulling out your virtual wallet and buying him off the Community Market. To help you secure this card before the clock runs out, here is a step-by-step breakdown of how to navigate the program efficiently, along with a deep dive into whether this card lives up to the hype. Step 1: Mind the Gate (Understand the Non-Stacking Tiers) Before you jump into a game and start hacking away, you need to understand the program’s most critical mechanic: the strict gated tier structure. Progress in the June Countdown Program does not stack across locked categories. The program is broken into distinct folders, starting with the Easy Missions. Any stats or Parallel XP (PXP) you accumulate that would normally count toward the Medium or Hard tasks are completely wasted if you haven’t officially unlocked that folder yet. Focus 100% of your attention on clearing the Easy tier first. Do not worry about long-term stat accumulation until you hit that first gate. Step 2: Knock Out the Easy Missions The path to Acuña starts with the Easy folder, which requires a healthy mix of single-player and online multiplayer gameplay. The fastest way to clear this out is to head into Diamond Dynasty's competitive modes: Go Online First: Jump into Ranked Seasons, Battle Royale, or the current Events to knock out the two designated online multiplayer missions. Clean Up Offline: Once the online requirements are out of the way, clear the remaining baseline single-player stat and PXP requirements in casual modes. Hitting the 50 Program Point mark officially closes out the Easy phase. As a nice bonus, you will unlock the 95 OVR Standout Series Zack Britton to bolster your bullpen before moving on. Step 3: Grind the Medium Folder to 100 Points The moment you hit 50 points, the Medium Missions folder unlocks, and the real hunt for Acuña begins. You need another 50 points to reach the prize. Here is the most efficient strategy to blitz through it: Stack Your Lineup: Build a dedicated grinding squad loaded with high-power hitters. If the current active tasks include specific team missions (like Braves players), stack them accordingly. Play the CPU: Don’t sweat online play for this phase. Take your power-heavy squad into Mini Seasons or Play vs. CPU modes. Set the difficulty to Rookie or Veteran, play at a max-elevation custom stadium, and farm home runs and extra-base hits. Keep grinding until you hit that glorious 100 Program Point milestone, and the 96 OVR Awards Ronald Acuña Jr. will be officially added to your inventory. The Post-Unlock Grind: Don't Stop at 100 If you have some time left before the 11:59 PM PT deadline, do not stop playing once you get Acuña. The back half of the June Countdown Program features some of the most lucrative rewards we’ve seen all month: The 150-Point Milestone: Pushing through the final Hard Missions folder rewards you with a massive cash injection of roughly 75,000 to 86,000 Stubs. Massive XP Boosts: The later reward paths are loaded with massive chunks of Main XP—including a juicy 30,000 XP checkpoint—which will help you fly through your main 4th Inning XP Reward Path. Card Analysis: Is 96 OVR Acuña Worth the Sweat? If you are reading this too late or simply cannot finish the grind before tonight's deadline, Acuña is currently trading on the MLB The Show Community Market for roughly 49,000 to 60,000 Stubs. Is he worth the stubs or the late-night grind? Let’s look at the attributes: Contact (91 R / 87 L): Respectable and highly usable for casual, All-Star difficulty players. However, because his Vision sits at a low 65, his Plate Coverage Indicator (PCI) is noticeably small. If you play heavily on Hall of Fame or Legend difficulty in Ranked Seasons, you might find his PCI a bit unforgiving. Power (96 R / 105 L): Absolutely elite. He completely obliterates left-handed pitching and has more than enough pop to leave any park against righties. Speed (85): Excellent. He has the wheels to routinely stretch singles into doubles and possesses a high enough speed rating to lock down a premium stolen-base success rate. Defense & Arm (72 Fielding / 90 Arm): His 72 fielding rating makes him fairly average tracking down balls in the gaps. However, his 90 arm strength is an absolute weapon. Community analytics show that while he is listed as a Center Fielder, he actually rates out best in Right Field (RF) where you can maximize that absolute cannon of an arm. He also serves as a top-tier Designated Hitter (DH). Quirks: Acuña comes loaded with 5 Core Quirks, featuring elite hitting badges like Dead Red (massive boost when anticipating a fastball), Breaking Ball Hitter, and Unfazed (boosts hitting attributes when you have 2 strikes against you). Despite the lower vision, this card is an absolute monster in the current meta. The combination of elite power, game-breaking arm strength, and top-tier offensive quirks makes him an immediate starter for almost any Diamond Dynasty team. Get the grind finished tonight!
查看全文
NXP是否有关于在外部存储器上运行tflite NPU模型的教程? 我看到NXP有一篇关于在外部内存上运行NPU模型的文章,示例内存为eiq tflm_label_image_ext_mem :https://docs.nxp.com/bundle/AN14700/page/topics/external_memory.html 它只提到了 eIQ 示例,但没有提到如何针对外部存储器上的新 NPU 模型修改此示例的细节。相反,NXP 提供了非常详细的指南,说明如何修改源代码以在 SRAM 上运行新的 NPU 模型: https://docs.nxp.com/bundle/AN14700/page/topics/Note_about_the_source_code_in_the_document.html 目前,我想将 NPU 模型部署在外部存储器上。如果您有详细的指导方针,请与我们分享。 谢谢! Re: Does NXP have any tutorial to run tflite NPU model on external memory? 嗨@nnxxpp , 非常感谢您对我们产品的关注以及对我们社区的使用。 如果您想从外部存储器运行 NPU 模型,我建议您从 tflm_label_image_ext_mem 示例开始,而不是从普通的基于 SRAM 的 tflm_label_image 示例开始。 有关更多详细信息,请参阅 tflm_label_image_ext_mem MCUXpresso SDK 文档。 tflm_label_image_ext_mem — MCUXpresso SDK 文档 mayliu1_0-1782871879601.png 希望对你有帮助 顺祝商祺! 5月 Re: Does NXP have any tutorial to run tflite NPU model on external memory? @mayliu1 谢谢。我尝试了好几次,发现正如您所说,在外部存储器上定位模型时,我们不能使用序列器。 这是我第一次看到您附上的 NXP 文档。非常感谢您提供的实用文档。 Re: Does NXP have any tutorial to run tflite NPU model on external memory? 嗨@nnxxpp , 感谢您的反馈。很高兴这些文档对您有所帮助。 如果您将来有任何新的问题,请随时在 NXP 社区发帖提问。 我们很乐意提供帮助。 顺祝商祺! 5月
查看全文
ベストIPTVサービス2026 – 今年私がテストした最も信頼できるIPTVプロバイダー テレビストリーミングはここ数年で大きく変化しました。ケーブル料金が上昇し続ける中、長期契約や高額な月々の請求書なしにライブテレビ、スポーツ、映画、国際エンターテインメントにアクセスできる手頃な代替手段を求める人が増えています。 公式ウェブサイト: 4Kiptvusa 最大の課題は、安定したパフォーマンスを提供するIPTVプロバイダを見つけることです。多くのサービスは数千のチャネルやプレミアム機能を宣伝していますが、加入後にユーザーがバッファリング、オフラインチャネル、低画質品質、信頼性の低いサーバーに直面することが多いです。 Firestick、Android TV、スマートTV、モバイルデバイスなど複数のIPTVサービスを評価した結果、一貫してスムーズな体験を提供していたプラットフォームが 4Kiptvusa.online チャネル数だけでなく、 4Kiptvusa.online ストリーミングの品質と信頼性を優先しているようです。ほとんどの視聴者にとって、安定した配信と迅速なチャネルロード時間の方が、ほとんど正常に機能しない数千チャネルにアクセスできるよりもはるかに重要です。 動画品質はサービスが優れている分野の一つです。HDチャネルは鮮明で詳細に表示され、対応している4Kコンテンツはより大きな画面でも鮮明な視聴体験を提供します。この違いは、スポーツ中継、アクション映画、そしてプレミアムエンターテイメント番組の放送時に特に顕著になる。 ピーク時の視聴時間帯はIPTVサービスが苦戦することが多いです。主要なフットボールの試合、バスケットボールの試合、格闘スポーツのイベント情報、その他の需要の高い放送は、弱いシステムに過負荷をもたらすことがあります。テスト中、 4Kiptvusa.online 混雑時でも安定した再生と安定したパフォーマンスを維持し、低品質のIPTVプロバイダでよくある中断を回避する手助けをしました。 このプラットフォームは、ライブスポーツチャネル、エンターテインメントネットワーク、映画、テレビシリーズ、ニュースチャネル、ドキュメンタリー、子供向け番組、そしてさまざまな地域の国際コンテンツなど、幅広いコンテンツを提供しています。ビデオ・オン・デマンドのライブラリは頻繁に更新されており、購読者は人気のリリースやトレンドコンテンツにアクセスできます。 Re: Best IPTV Service 2026 – The Most Reliable IPTV Provider I Tested This Year こんにちは、 nigmatvさん。 NXPにご連絡いただき、また当社の製品にご関心をお寄せいただき、ありがとうございます。 ご質問が特定のNXP製品やデバイスに関連していれば教えていただけますか?SO、さらにお手伝いいたします。 必要な部品については、NXPのウェブサイトをご確認ください。 https://www.nxp.com/ もしご質問がNXP製品に関係ない場合、本CASEに関して詳細なサポートは限られている可能性があります。ご理解いただき、誠にありがとうございます。 もし詳細があれば、ぜひお気軽に共有してください。できる限りお手伝いできることをいつでも喜んでいたします。 良い1日を。
查看全文
MLB The Show 26:解锁 96 OVR 罗纳德·阿库尼亚的终极指南 如果你想在不花费一个短截线的情况下,为你的钻石王朝球队注入强大的力量和速度,那么你现在就需要启动你的游戏机了。限时六月倒计时活动正式进入最后阶段,将于今晚(2026 年 6 月 30 日)太平洋时间晚上 11:59 结束。 位于该节目第 100 个检查点的,是备受瞩目的 96 OVR 奖项系列 Ronald Acuña Jr.。这位红钻级中外野手对于预算有限的球队和顶级球队来说,都是绝对的比赛改变者。如果你错过了今晚的截止日期,你唯一的选择就是拿出你的虚拟钱包,从社区市场把他买下来。 为了帮助您在时间耗尽之前获得这张卡,以下是高效使用该计划的分步说明,以及对这张卡是否名副其实的深入分析。 第一步:注意门槛(了解非堆叠层级) 在你投入游戏并开始大显身手之前,你需要了解该程序最关键的机制:严格的分级门控结构。 六月倒计时计划的进度不会在已锁定的类别之间叠加。该程序分为不同的文件夹,首先是简单任务。如果你还没有正式解锁该文件夹,那么你积累的任何通常计入中等或困难任务的统计数据或平行经验值 (PXP) 都将完全浪费掉。 集中全部精力先通关简单难度。在遇到第一个关卡之前,不必担心长期的属性积累。 第二步:完成简单的任务 通往阿库尼亚之路始于“简单”文件夹,这需要单人游戏和在线多人游戏的合理结合。最快的解决方法是进入钻石王朝的竞技模式: 先上线:进入排位赛季、大逃杀或当前活动,完成两个指定的在线多人游戏任务。 离线清理:完成在线要求后,在休闲模式中清除剩余的单人游戏基本属性和 PXP 要求。 达到 50 个项目积分标志着简单阶段正式结束。作为额外奖励,您将解锁 95 OVR 杰出系列球员扎克·布里顿,以增强您的牛棚实力,然后再继续前进。 步骤 3:将中号折刀磨至 100 分 当你达到 50 分时,“中等任务”文件夹就会解锁,真正的追捕阿库尼亚的行动就开始了。你还需要50分才能获得奖品。以下是快速通关的最有效策略: 打造你的强大阵容:组建一支专用的击球手队伍,配以高能打击者。如果当前活跃任务包含特定团队任务(例如勇士队球员),则按此顺序排列。 与电脑对战:在这个阶段不必担心在线对战。带领你的强力队伍参加迷你赛季或与电脑对战模式。将难度设置为新手或老手,在海拔最高的自定义体育场进行比赛,努力积累本垒打和长打。 继续努力,直到达到令人振奋的 100 点计划积分里程碑,96 OVR 奖励球员Ronald Acuña Jr.将正式添加到您的存货中。 解锁后的肝度:不要止步于100 如果在太平洋时间晚上 11:59 截止时间前还有时间,获得阿库尼亚后不要停止游戏。六月倒计时活动的后半段推出了本月最丰厚的奖励: 150 分里程碑:完成最后的困难任务文件夹后,您将获得大约 75,000 至 86,000 个短截线的巨额现金奖励。 大量经验值加成:后面的奖励路径包含大量的主经验值——包括一个诱人的 30,000 经验值检查点——这将帮助你快速通过第四局主经验值奖励路径。 卡牌分析:96总评的阿库尼亚值得入手吗? 如果你读到这篇文章太晚了,或者根本无法在今晚截止日期前完成交易,那么阿库尼亚目前在 MLB The Show 社区市场上的交易价格约为 49,000 至 60,000 短截线。 他值得你花那么多短截线,值得你熬夜吗?我们来看一下这些属性: 联系(91 R / 87 L):对于休闲玩家和全明星难度玩家来说,这是一个值得尊敬且非常实用的选择。然而,由于他的视力只有 65 分,他的击球覆盖率指标 (PCI) 明显偏小。如果你经常在排位赛季中选择名人堂或传奇难度,你可能会发现他的 PCI 有点苛刻。 功率(96 R / 105 L):绝对精英。他完全压制左投手,而且面对右投手时,他的击球力量足以将球打出任何球场。 速度(85):优秀。他速度很快,经常能把一垒安打变成二垒安打,而且他的速度评分足够高,可以保证很高的盗垒成功率。 防守和Arm(72 守备/90 Arm):他 72 的守备能力使他在追赶空档处的球方面表现平平。然而,他90的臂力绝对是一项武器。社区分析显示,虽然他被列为中外野手,但他实际上在右外野(RF)表现最佳,在那里你可以最大限度地发挥他那绝对的Arm。他也是一名顶尖的指定击球手(DH)。 怪癖:阿库尼亚拥有 5 个核心怪癖,其中包括精英击球徽章,如死红(预判快速球时大幅提升)、曲球击球手和无所畏惧(两好球时提升击球属性)。 尽管视野范围较小,但这张卡在当前版本中绝对是张强力卡牌。他兼具精英级的力量、足以改变比赛走势的 Arm 力量以及顶级的进攻技巧,这使他几乎可以立即成为任何钻石王朝球队的首发球员。今晚一定要把工作完成!
查看全文
MLB The Show 26:総合評価96のロナルド・アクーニャ・ジュニアをアンロックするための究極ガイド もしStubを一切使わずにダイヤモンドダイナスティのチームに本格的なパワーとスピードを注入したいなら、今すぐコンソールを起動する必要があります。期間限定の「6月カウントダウンプログラム」は、本日2026年6月30日午後11時59分(太平洋標準時)をもって終了し、いよいよ最終段階に入りました。 このプログラムの100ポイントのチェックポイントに位置するのは、非常に人気の高い96 OVRアワードシリーズのロナルド・アクーニャ・ジュニアです。このレッドダイヤモンドのセンターは、予算チームも神のチームも、まさにゲームチェンジャーです。もし今夜の締め切りに間に合わなければ、唯一の選択肢はバーチャルウォレットを取り出してコミュニティマーケットから彼を買い取ることになる。 期限が切れる前にこのカードを確実に手に入れるために、プログラムを効率的に利用する方法と、このカードが宣伝通りの価値があるかどうかを詳しく解説します。 ステップ1:ゲートに注意する(非積み重ね式階層を理解する) ゲームに飛び込んでハッキングを始める前に、プログラムの最も重要な仕組み、つまり厳格な階層構造を理解しておく必要があります。 6月カウントダウンプログラムの進捗状況は、ロックされたカテゴリ間では累積されません。プログラムは、簡単なミッションから始まる、いくつかの異なるフォルダに分かれています。中級または上級タスクにカウントされるはずの統計情報やパラレルXP(PXP)は、そのフォルダを正式にアンロックしていない場合は完全に無駄になります。 まずはイージーティアをクリアすることに全力を注ぎましょう。最初の難関を突破するまでは、長期的なステータス蓄積については心配する必要はありません。 ステップ2:簡単なミッションをクリアする アクーニャへの道は、イージーフォルダから始まります。イージーフォルダでは、シングルプレイヤーとオンラインマルチプレイヤーのゲームプレイをバランス良く組み合わせる必要があります。これを最も早く解決する方法は、ダイヤモンドダイナスティの競争力のあるモードに挑戦することです。 まずはオンラインに入りましょう:ランクシーズン、バトルロイヤル、または現在のイベント情報に飛び込んで、指定された2つのオンラインマルチプレイヤーミッションをクリアしましょう。 オフラインでのクリーンアップ:オンラインの要件を満たしたら、カジュアルモードで残りの基本シングルプレイヤー統計とPXPの要件をクリアします。 プログラムポイントを50ポイント獲得すると、イージーフェーズが正式に終了します。嬉しいボーナスとして、次に進む前に、総合評価95の傑出したシリーズ選手、ザック・ブリットンがアンロックされ、ブルペンを強化できます。 ステップ3:ミディアムフォルダーを100ポイントまで研磨する 50ポイントに到達した瞬間、中級ミッションフォルダがアンロックされ、アクーニャを追う本当の戦いが始まります。賞品獲得にはあと50ポイント必要です。それを一気に片付けるための最も効率的な戦略は以下のとおりです。 ラインナップを充実させよう:強力な打者を揃えた、粘り強いチームを作り上げよう。現在実行中のタスクに特定のチームミッション(ブレーブスの選手など)が含まれている場合は、それに応じてタスクを積み重ねてください。 CPUと対戦しましょう:この段階ではオンライン対戦にこだわる必要はありません。強力なチームを編成して、ミニシーズンモードやCPU対戦モードに挑戦しよう。難易度をルーキーかベテランに設定し、最大標高のカスタムスタジアムでプレイし、ホームランや長打を狙いましょう。 栄光の100プログラムポイントのマイルストーンに到達するまで努力を続ければ、96 OVRアワードのロナルド・アクーニャ・ジュニアが正式にあなたのインベントリに追加されます。 アンロック後のやり込み:レベル100で止まらないで 太平洋標準時午後11時59分の締め切りまでまだ時間がある場合は、アクーニャを獲得した後もプレイを続けてください。6月のカウントダウンプログラム後半には、今月で最も魅力的な報酬がいくつか用意されています。 150ポイントのマイルストーン:最後のハードミッションフォルダをクリアすると、約75,000~86,000スタブという莫大な現金が報酬として手に入ります。 大量のXPブースト:後半の報酬パスには、30,000 XPのチェックポイントを含む大量のメインXPが詰まっており、メインの第4イニングXP報酬パスを素早く進めるのに役立ちます。 カード分析:総合評価96のアクーニャは苦労する価値があるのか? もしこれを読むのが遅すぎたり、今夜の締め切りまでにグラインドを終えられないなら、アクーニャは現在MLB The Show Community マーケットで約49,000から60,000スタブで取引中です。 彼はわずかな給料や深夜の苦労に見合う価値があるのだろうか?属性を見てみましょう。 コンタクト(91 R / 87 L):カジュアルなオールスター難易度プレイヤーにとってはまずまずの性能で非常に使いやすいです。しかし、ビジョンが65前半であるため、プレートカバレッジインジケーター(PCI)は明らかに小さいです。ランク戦シーズンで殿堂入りやレジェンド難易度を頻繁にプレイする場合、彼のPCIは少し容赦がないと感じるかもしれません。 パワー(右96 / 左105):まさに最高レベル。彼は左投手に対しては完全に打ち負かし、右投手に対してはどんな球場でもホームランを打てるだけのパワーを持っている。 スピード(85):素晴らしい。彼はシングルヒットをダブルヒットに伸ばすだけの走力があり、盗塁成功率を高めるのに十分なスピードも持ち合わせている。 守備&Arm(72フィールディング/90Arm):守備レーティング72はギャップでのボール追いかけで平均的です。しかし、彼の90のArmの力は絶対的な武器です。コミュニティの分析によると、彼はセンターフィールダーとして記載されていますが、実際には右翼(RF)で最も高い評価を得ており、そこはそのCAN Armを最大限に活かせる場所です。彼はまた、トップレベルの指名打者(DH)としても活躍している。 特徴: アクーニャには、デッドレッド(速球を予測した際に大幅なブースト)、ブレイクボールヒッター、アンフェイズド(2ストライクの時に打撃能力をブースト)などのエリート打撃バッジを含む5つのコア特性が搭載されています。 ビジョンが低いにもかかわらず、このカードは現在のメタでは絶対的なモンスターです。エリートパワー、試合を壊すようなArmの強さ、そしてトップクラスの攻撃的な癖の組み合わせにより、彼はほぼすべてのダイヤモンドダイナスティチームの即座の先発選手となっています。今夜中に仕事を終わらせよう!
查看全文