2388001_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2388001_en-US

2388001_en-US

MLB The Show 26: Ultimate Guide to Unlocking 96 OVR Ronald Acuña Jr.

If you are looking to inject some serious power and speed into your Diamond Dynasty squad without spending a single Stub, you need to fire up your console right now. The limited-time June Countdown Program is officially in its final hours, expiring tonight, June 30, 2026, at 11:59 PM PT.

Sitting right at the 100-point checkpoint of this program is the highly coveted 96 OVR Awards Series Ronald Acuña Jr. This Red Diamond center fielder is an absolute game-changer for budget squads and god-squads alike. If you miss tonight's deadline, your only option will be pulling out your virtual wallet and buying him off the Community Market.

To help you secure this card before the clock runs out, here is a step-by-step breakdown of how to navigate the program efficiently, along with a deep dive into whether this card lives up to the hype.

Step 1: Mind the Gate (Understand the Non-Stacking Tiers)

Before you jump into a game and start hacking away, you need to understand the program’s most critical mechanic: the strict gated tier structure.

Progress in the June Countdown Program does not stack across locked categories. The program is broken into distinct folders, starting with the Easy Missions. Any stats or Parallel XP (PXP) you accumulate that would normally count toward the Medium or Hard tasks are completely wasted if you haven’t officially unlocked that folder yet.

Focus 100% of your attention on clearing the Easy tier first. Do not worry about long-term stat accumulation until you hit that first gate.

Step 2: Knock Out the Easy Missions

The path to Acuña starts with the Easy folder, which requires a healthy mix of single-player and online multiplayer gameplay. The fastest way to clear this out is to head into Diamond Dynasty's competitive modes:

  1. Go Online First: Jump into Ranked Seasons, Battle Royale, or the current Events to knock out the two designated online multiplayer missions.

  2. Clean Up Offline: Once the online requirements are out of the way, clear the remaining baseline single-player stat and PXP requirements in casual modes.

Hitting the 50 Program Point mark officially closes out the Easy phase. As a nice bonus, you will unlock the 95 OVR Standout Series Zack Britton to bolster your bullpen before moving on.

Step 3: Grind the Medium Folder to 100 Points

The moment you hit 50 points, the Medium Missions folder unlocks, and the real hunt for Acuña begins. You need another 50 points to reach the prize. Here is the most efficient strategy to blitz through it:

  • Stack Your Lineup: Build a dedicated grinding squad loaded with high-power hitters. If the current active tasks include specific team missions (like Braves players), stack them accordingly.

  • Play the CPU: Don’t sweat online play for this phase. Take your power-heavy squad into Mini Seasons or Play vs. CPU modes. Set the difficulty to Rookie or Veteran, play at a max-elevation custom stadium, and farm home runs and extra-base hits.

Keep grinding until you hit that glorious 100 Program Point milestone, and the 96 OVR Awards Ronald Acuña Jr. will be officially added to your inventory.

The Post-Unlock Grind: Don't Stop at 100

If you have some time left before the 11:59 PM PT deadline, do not stop playing once you get Acuña. The back half of the June Countdown Program features some of the most lucrative rewards we’ve seen all month:

  • The 150-Point Milestone: Pushing through the final Hard Missions folder rewards you with a massive cash injection of roughly 75,000 to 86,000 Stubs.

  • Massive XP Boosts: The later reward paths are loaded with massive chunks of Main XP—including a juicy 30,000 XP checkpoint—which will help you fly through your main 4th Inning XP Reward Path.

Card Analysis: Is 96 OVR Acuña Worth the Sweat?

If you are reading this too late or simply cannot finish the grind before tonight's deadline, Acuña is currently trading on the MLB The Show Community Market for roughly 49,000 to 60,000 Stubs.

Is he worth the stubs or the late-night grind? Let’s look at the attributes:

  • Contact (91 R / 87 L): Respectable and highly usable for casual, All-Star difficulty players. However, because his Vision sits at a low 65, his Plate Coverage Indicator (PCI) is noticeably small. If you play heavily on Hall of Fame or Legend difficulty in Ranked Seasons, you might find his PCI a bit unforgiving.

  • Power (96 R / 105 L): Absolutely elite. He completely obliterates left-handed pitching and has more than enough pop to leave any park against righties.

  • Speed (85): Excellent. He has the wheels to routinely stretch singles into doubles and possesses a high enough speed rating to lock down a premium stolen-base success rate.

  • Defense & Arm (72 Fielding / 90 Arm): His 72 fielding rating makes him fairly average tracking down balls in the gaps. However, his 90 arm strength is an absolute weapon. Community analytics show that while he is listed as a Center Fielder, he actually rates out best in Right Field (RF) where you can maximize that absolute cannon of an arm. He also serves as a top-tier Designated Hitter (DH).

  • Quirks: Acuña comes loaded with 5 Core Quirks, featuring elite hitting badges like Dead Red (massive boost when anticipating a fastball), Breaking Ball Hitter, and Unfazed (boosts hitting attributes when you have 2 strikes against you).

Despite the lower vision, this card is an absolute monster in the current meta. The combination of elite power, game-breaking arm strength, and top-tier offensive quirks makes him an immediate starter for almost any Diamond Dynasty team. Get the grind finished tonight!

标记 (1)
无评分
版本历史
最后更新:
‎07-01-2026 02:38 AM
更新人: