Multi Source Translation Content

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multi Source Translation Content

讨论

排序依据:
LX2160A 上的 VSC8254 PHY 在 1G SGMII 模式下启动需要协助 大家好, 我们正在开发一款基于 LX2160A Rev2 SoC 的定制电路板,其中 VSC8254 PHY 通过 eMDIO1 连接到 SoC。目前我们在 1G SGMII 模式下启动 PHY 时遇到问题。 到目前为止,我们已经通过在 DPC 文件和 Linux 内核设备树中配置固定链路,成功地在 10G XFI 模式下启动了 PHY。启动后,我们执行 NXP 提供的 mdio_cl45_write 脚本来对所需的 Clause 45 寄存器进行编程,之后链接建立并正常运行。 但是,当我们将配置切换到 1G SGMII 模式时,我们会进行以下更改: 更新 DPC 和 Linux 设备树,使其使用 SGMII 而不是 XFI。 执行 1G 对应的 Clause 45 寄存器初始化序列。 根据新配置的要求,将 SERDES 参考时钟从 125 MHz 更新为 100 MHz。 尽管做了这些更改,PHY 链路仍然无法建立。 供参考: VSC8254 PHY 连接到 SERDES1 MAC3 和 MAC4。 我们使用 RCW 6 进行 10G XFI 配置。 我们对 1G SGMII 配置采用 RCW 4。 关于在 1G SGMII 模式下启动 PHY 是否需要任何额外的配置更改或初始化步骤,请与我们联系。 感谢您的时间和支持。 @yipingwang @chenyin_h Re: Assistance Required for VSC8254 PHY Bring-up in 1G SGMII Mode on LX2160A 1. 请将 RCW[SRDS_PLL_REF_CLK_SEL_S1] 配置为“00”。 2. 请在 Linux 内核中配置“CONFIG_VITESSE_PHY”。 3. 在 Linux 启动 dts 文件 arch/arm64/boot/dts/freescale/fsl-lx2160a-rdb.dts 中,请修改 dpmac3 和 dpmac4 的配置,使其与下面的配置类似。 &dpmac3 { phy-handle = <&aquantia_phy1>; phy-connection-type = "usxgmii"; managed = "带内状态"; }; aquantia_phy1:以太网物理层@4 { /* AQR107 PHY */ 兼容 = "ethernet-phy-ieee802.3-c45"; interrupts-extended = <&extirq 2 IRQ_TYPE_LEVEL_LOW>; reg = <0x4>; }; 修改为: &dpmac3 { phy-handle = <&sgmii_phy1>; phy-connection-type = "sgmii"; managed = "带内状态"; }; sgmii_phy1:以太网物理层@xx{ reg = <0xxx>;//指定与dpmac3相关的MDIO PHY地址         }; 4. 请按如下方式修改 dtc 文件 dpc-usxgmii.dts。 板信息 { 港口 { mac@3 { link_type = "MAC_LINK_TYPE_PHY"; enet_if = "USXGMII";                         }; mac@4 { link_type = "MAC_LINK_TYPE_PHY"; enet_if = "USXGMII";                         }; 修改为: 板信息 { 港口 { mac@3 { link_type = "MAC_LINK_TYPE_PHY";                         }; mac@4 { link_type = "MAC_LINK_TYPE_PHY";                         }; Re: Assistance Required for VSC8254 PHY Bring-up in 1G SGMII Mode on LX2160A [ 8.088037] fsl_dpaa2_eth dpni.12(未命名网络设备)(未初始化):phylink_fwnode_phy_connect() = -19 [ 8.097693] fsl_dpaa2_eth dpni.12 (未命名网络设备) (未初始化): 连接到 MAC 端点时出错:-ENODEV [ 8.149621] fsl_dpaa2_eth dpni.12:fsl_mc_driver_probe 失败:-19 [ 8.268214] fsl_dpaa2_eth dpni.11(未命名网络设备)(未初始化):phylink_fwnode_phy_connect() = -19 [ 8.277867] fsl_dpaa2_eth dpni.11 (未命名网络设备) (未初始化): 连接到 MAC 端点时出错:-ENODEV [ 8.329780] fsl_dpaa2_eth dpni.11:fsl_mc_driver_probe 失败:-19 进行上述更改后,我们在内核中得到上述错误打印结果,并且 ls-listni 显示两个 mac 都没有任何端点。 ls-listni dprc.1/dpni.12(端点:dpmac.3) dprc.1/dpni.11(端点:dpmac.4) 还有什么我们遗漏的吗?
查看全文
S32E2 IPCF latency timings between M33 and R52 I am working with S32E2 and configuring the IPCF framework and here is my setup Device: S32E288 IPCF transport: Shared Memory + MRU notification Communication: M33 ↔ R52 IPCF channel type: Managed channel 1 IPCF channel configured Interrupt mode (not polling) Ping/Pong RTT test implemented Communication is functioning correctly in both directions. I use STM to measure the timing ticks between the 2 cores. Measurement flow: R52: timestamp send PING   M33: receive PING immediately send PONG from RX callback   R52: receive PONG compute RTT The values computed for a STM running on 24Mhz are close to 200us RTT(Round trip time). My transport overhead is about 30us but the transfer itself takes up bulk of the time. I have tried various things like increasing MRU IRQ notification but has not improved the timings. Having optimisation in code from -o0 to -o1 helped but -o2 didnt make any difference. The payload itself is 16 bytes. Questions: 1. what is expected IPCF latency for managed /unmanaged channels. 2. can we acheive a low double digit latency? If you need any more details, please reply back. Re: S32E2 IPCF latency timings between M33 and R52 Hi,PrabhanjanKopp Thank you for contacting us. For your testing scenario, you can try to refer to GreenVIP. The Loop Time is about 20-30us.(S32ZE_GreenVIP_1.x.1/doc/UG_S32ZE_GreenVIP.pdf) Joey_z_0-1789354232929.pngJoey_z_0-1789354232929.pngJoey_z_0-1789354232929.pngJoey_z_0-1789354232929.pngJoey_z_0-1789354232929.png Joey_z_1-1789354243644.pngJoey_z_1-1789354243644.pngJoey_z_1-1789354243644.pngJoey_z_1-1789354243644.pngJoey_z_1-1789354243644.png If you have other issue, you can contact us at any time. BR Joey Re: S32E2 IPCF latency timings between M33 and R52 Hi Joey, Thank you for your reply. I am using S32 DS for setting up my cores and was wondering is GreenVIP is any different? Also , it will be most helpful to get the document link(or the doc itself)  that you referring in your message. Is there a reference project that I can compare my settings against? I suspect there might be some configuration mismatch. Thanks, Prabhanjan Re: S32E2 IPCF latency timings between M33 and R52 Hi,Prabhanjan Thank you for your reply. The link of GreenVIP download as the following: S32E2 Safe and Secure High-Performance Real-Time Processors with Actuation Support | NXP Semiconductors Automotive Software Package Manager | NXP Semiconductors Joey_z_0-1789452520972.pngJoey_z_0-1789452520972.pngJoey_z_0-1789452520972.png Joey_z_1-1789452649226.pngJoey_z_1-1789452649226.pngJoey_z_1-1789452649226.png The EB tresos IDE is used for the GreenVIP, both S32DS and EB tresos can be used to develop applications for S32E. Hope this information can help you; you can contact us at any time if you still have question about this. BR Joey Re: S32E2 IPCF latency timings between M33 and R52 Thank you for that. I found that I can get the timings down when I switch to unmanaged channel. It is close to 60us . Will see if I can get it further down.  Re: S32E2 IPCF latency timings between M33 and R52 Hi,PrabhanjanKopp Thank you for your reply and information. For the 60us result, was it tested by your customer program or by our Greenvip? BR Joey
查看全文
S32E2 IPCF 延迟时间介于 M33 和 R52 之间 我正在使用 S32E2 并配置 IPCF 框架,以下是我的设置。 设备:S32E288 IPCF 传输:共享内存 + MRU 通知 通信:M33 ↔ R52 IPCF通道类型:管理通道 配置了 1 个 IPCF 通道 中断模式(非轮询) 已实施 Ping/Pong RTT 测试 双向沟通正常。 我使用STM来测量两个核心之间的时序滴答数。 测量流程: R52: 时间戳 发送 PING   M33: 收到 PING 立即从 RX 回调发送 PONG 请求   R52: 收到 PONG 计算 RTT 计算得出,运行在 24Mhz 的 STM 的 RTT(往返时间)接近 200us。我的传输开销大约是 30 微秒,但传输本身占用了大部分时间。我尝试过各种方法,例如增加 MRU IRQ 通知,但并没有改善时序问题。代码优化级别从 -o0 到 -o1 有所提升,但 -o2 没有任何效果。有效载荷本身为 16 字节。 问题: 1. 托管/非托管通道的预期 IPCF 延迟是多少? 2. 我们能否实现两位数的低延迟? 如果您需要更多详细信息,请回复。 Re: S32E2 IPCF latency timings between M33 and R52 你好,PrabhanjanKopp 感谢您与我们联系。 对于您的测试场景,您可以参考 GreenVIP。循环时间约为 20-30 微秒。(S32ZE_GreenVIP_1.x.1/doc/UG_S32ZE_GreenVIP.pdf) Joey_z_0-1789354232929.pngJoey_z_0-1789354232929.pngJoey_z_0-1789354232929.pngJoey_z_0-1789354232929.pngJoey_z_0-1789354232929.png Joey_z_1-1789354243644.pngJoey_z_1-1789354243644.pngJoey_z_1-1789354243644.pngJoey_z_1-1789354243644.pngJoey_z_1-1789354243644.png 如果您还有其他问题,可以随时联系我们。 BR 乔伊 Re: S32E2 IPCF latency timings between M33 and R52 嗨,乔伊, 感谢你的回复。我目前使用 S32 DS 来设置我的核心,想知道 GreenVIP 是否有任何不同之处?另外,如果您能提供您在消息中提到的文档链接(或文档本身),将非常有帮助。是否有可供参考的项目,我可以将我的设置与之进行比较?我怀疑可能是配置不匹配的问题。 谢谢! 普拉班詹 Re: S32E2 IPCF latency timings between M33 and R52 你好,普拉班詹 感谢您的回复。 GreenVIP下载链接如下: S32E2 安全可靠、高性能的实时处理器,支持执行器功能 | 恩智浦半导体 汽车软件代码包,软件包管理器 | 恩智浦半导体 Joey_z_0-1789452520972.pngJoey_z_0-1789452520972.pngJoey_z_0-1789452520972.png Joey_z_1-1789452649226.pngJoey_z_1-1789452649226.pngJoey_z_1-1789452649226.png EB tresos IDE 用于 GreenVIP,S32DS 和 EB tresos 都可用于开发 S32E 应用程序。希望这些信息对您有所帮助;如果您还有任何疑问,可以随时联系我们。 BR 乔伊 Re: S32E2 IPCF latency timings between M33 and R52 谢谢。我发现切换到非托管通道后,可以缩短传输时间。接近 60 微秒。我看看能不能再往下挪挪。 Re: S32E2 IPCF latency timings between M33 and R52 你好, PrabhanjanKopp 感谢您的回复和提供的信息。 对于 60us 的结果,是由你们的客户程序测试的,还是由我们的 Greenvip 测试的? BR 乔伊
查看全文
Regarding the establishment of the tick clock and the selection of the base clock Hello: I want to configure a bare-metal tick clock (S32K358 device). My BaseNXP settings are shown in Figure 1. Is this configuration sufficient to connect to the tick clock?2. Which clock in the device tree does the set 48MHz correspond to? sunshine88_0-1789971547489.png sunshine88_1-1789971658567.png After setting it up, can it be called using OsIf_Init(NULL_PTR); OsIfDelay(x);? Thank you so much! Re: 关于滴答时钟建立及基时钟的选择 Hello @sunshine88 , OsIfSystemTimerClockFreq corresponds to CORE_CLK, which is 160MHz in my case: PavelL_0-1789999751219.png PavelL_1-1789999832315.png Best regards, Pavel
查看全文
S32E2のM33とR52間のIPCFレイテンシタイミング 私はS32E2を使用してIPCFフレームワークを構成しており、これが私の設定です。 デバイス: S32E288 IPCFトランスポート:共有メモリ+MRU通知 通信:M33 ↔ R52 IPCFチャネルタイプ:マネージドチャネル 1つのIPCFチャネルが設定されています 割り込みモード(ポーリングではない) Ping/Pong RTTテストを実装しました 双方向のコミュニケーションは正常に機能しています。 私はSTMを使って2コア間のタイミングティックを測定しています。 測定フロー: R52: タイム・スタンプ PINGを送信   M33: PINGを受信する RXコールバックからすぐにPONGを送信   R52: PONGを受け取る 計算RTT 24MHzで動作するSTMの計算値は、ほぼ200us RTT(往復時間)に近づきます。輸送にかかるオーバーヘッドは約30秒ですが、転送自体にほとんどの時間が費やされます。MRU IRQ通知を増やすなど、いろいろ試してみましたが、タイミングは改善されませんでした。コードの最適化を-o0から-o1に変更すると効果があったが、-o2に変更しても違いはなかった。ペイロード自体は16バイトです。 質問: 1. 管理型/非管理型チャネルのIPCFレイテンシはどのくらいか。 2. 低2桁レイテンシを実現できるか? さらに詳しい情報が必要な場合は、返信してください。 Re: S32E2 IPCF latency timings between M33 and R52 こんにちは、PrabhanjanKopp お問い合わせいただきありがとうございます。 テストシナリオではGreenVIPを参照してみてください。ループ時間は約20~30マイクロ秒です。(S32ZE_GreenVIP_1.x.1/doc/UG_S32ZE_GreenVIP.pdf) Joey_z_0-1789354232929.pngJoey_z_0-1789354232929.pngJoey_z_0-1789354232929.pngJoey_z_0-1789354232929.pngJoey_z_0-1789354232929.png Joey_z_1-1789354243644.pngJoey_z_1-1789354243644.pngJoey_z_1-1789354243644.pngJoey_z_1-1789354243644.pngJoey_z_1-1789354243644.png 他に問題があれば、いつでもご連絡ください。 BR ジョーイ Re: S32E2 IPCF latency timings between M33 and R52 こんにちは、ジョーイ。 お返事ありがとうございます。私はコアの設定にS32 DSを使用しているのですが、GreenVIPは何か違いがあるのでしょうか?また、メッセージの中で参照しているドキュメントへのリンク(またはドキュメント自体)を提供していただけると大変助かります。設定を比較できる参考プロジェクトはありますか?設定に何らかの不一致があるのではないかと思います。 ありがとうございます プラバンジャン Re: S32E2 IPCF latency timings between M33 and R52 こんにちは、プラバンジャン ご返信よろしくお願いします。 GreenVIPのダウンロードリンクは以下のとおりです。 S32E2 アクチュエーションサポート付き安全かつ確実な高性能リアルタイムプロセッサ | NXP Semiconductors オートモーティブ ソフトウェアパッケージマネージャ | NXP Semiconductors Joey_z_0-1789452520972.pngJoey_z_0-1789452520972.pngJoey_z_0-1789452520972.png Joey_z_1-1789452649226.pngJoey_z_1-1789452649226.pngJoey_z_1-1789452649226.png EB tresos IDEはGreenVIPに使用されており、S32DSとEBのtresosの両方を使ってS32Eのアプリケーションを開発できます。この情報があなたの助けになれば幸いです;まだ疑問があればいつでもお問い合わせください。 BR ジョーイ Re: S32E2 IPCF latency timings between M33 and R52 ありがとうございます。管理されていないチャネルに切り替えると、タイミングを正確に調整できることがわかりました。60μsに近い値です。もっと下に進めるか試してみます。 Re: S32E2 IPCF latency timings between M33 and R52 こんにちは、 PrabhanjanKopp ご返信と情報提供ありがとうございます。 60USの結果は、お客様のプログラムでテストされましたか、それともGreenvipによってテストされましたか? BR ジョーイ
查看全文
MTTF-FIT信頼性データのリクエスト 拝啓 現在、御社製の部品を使用した製品のMTBF値を計算しています。 つきましては、下記の部品について、MTTF値および/またはFIT値が入手可能な場合は、ご提供いただけますようお願い申し上げます。この情報により、当社の製品のMTBFを正確に計算するのに役立ちます。 部品番号:NTS0104BQ,115 説明:電圧レベル変換器 双方向 1回路4チャネル 50Mbps 14-DHVQFN(2.5x3) 信頼性データを提供するために、運用条件やアプリケーションに関する追加情報が必要な場合はお知らせください。 再開まで今しばらくお待ちください。 クラウド・ラボ オンラインデバッグ オンラインラボ 仮想テスト
查看全文
IW612 WLAN 5GHz transmission Hi,  We are planning to use IW612 SoC for WLAN in one of our IoT product, target market is US and Canada. IW612 supports dual band 2.4Ghz and 5GHz. Is there a way or configuration to turn 5GHz WIFI Operation OFF, as ISED Canada doesn't allow UNII-1 (5150-5250Mhz) WIFI transmission in outdoor environment without a license and limits operation to Indoor ONLY. Our product operates in Outdoor and we would like a way to Disable 5GHz entirely and operate on 2.4Ghz only. RSS-247 — Digital Transmission Systems, Frequency Hopping Systems and Licence-Exempt Local Area Network Devices in 902-928 MHz, 2400-2483.5 MHz, 5150-5350 MHz, and 5470-5895 MHz bands Can you confirm and share settings for same? Regards, Arun RF Re: IW612 WLAN 5GHz transmission Hello @pantarun_92  iw612 support loading power table, you could custom power table or use sample table for Canada region. It will disable not allowed channels and support DFS channel. Best Regards Shaun
查看全文
imx95 和 vfio_pci 直通 您好, 我们希望在 IMX95 SoC 上使用具有 PCI 直通功能的虚拟机。这似乎完全不可能,因为 SMMU 不是缓存一致的,而 vfio_pci 驱动程序需要缓存一致性。参见: https://community.nxp.com/t5/i-MX-Processors/i-MX95-19x19-EVK-SMMU-coherent-table-walks-IDR0-COHACC-and-vfio/mp/2410515 和 https://github.com/NXP/dpdk/blob/25.11-qoriq/nxp/README_imx95_enetc_vf_vfio#L32 禁用 IOMMU 不是一个可行的方案。另外,我怀疑这样做是否会有帮助,因为内核参数是这样写的: MODULE_PARM_DESC(enable_unsafe_noiommu_mode, "启用不安全、无 IOMMU 模式。此模式不提供设备隔离、DMA 转换、主机内核保护,不能用于将设备分配给虚拟机,需要 RAWIO 权限,并且会污染内核。如果你不知道这是做什么用的,请远离。(默认值:false)"); 能否确认一下,是否真的无法将 IMX95 SoC 与(安全的)PCI 直通一起使用?如果不是,那我到底漏掉了什么? 此致, -迈克尔 Re: imx95 and vfio_pci passthrough 您好, 感谢您的快速回复。但我不太确定我是否完全理解了。为了确保万无一失,我们不想使用 DPDK,而是使用通用的 qemu/kvm 虚拟机,并在其中传递 PCI 设备。这与 uio-pci-generic 框架有何关系? 谢谢, -迈克尔 Re: imx95 and vfio_pci passthrough 您好, 感谢您对恩智浦半导体产品的关注, 在这种情况下,你需要采纳我同事的回复,也就是 DPDK 团队的回复。唯一的替代方案就是回复中提到的那个: “如果客户希望将 SMMU 用于其他用例,但可以接受绕过 DPDK(不想在 bootargs 中使用 iommu.passthrough=1 或在 dts 中禁用 SMMU 节点)。 然后可以尝试绑定 uio-pci-generic 框架并禁用 VSI-PSI 消息传递(export ENETC4_VSI_MSG_DISABLE=1)。但是禁用 VSI-PSI 消息意味着用户将无法使用某些 ENETC 功能,例如混杂模式、VLAN MAC 过滤和链路信息。 此致
查看全文
How to get the full datasheet for BMA8420 ? not Product Brief   Subject: Inquiry regarding BMA8420 for Hydrogen Fuel Cell Stack EIS Measurement   Dear Technical Support Team, I am currently developing an Electrochemical Impedance Spectroscopy (EIS) measurement system for hydrogen fuel cells.   To utilize the BMA8420, I would like to review its technical specifications, but I have been unable to locate the datasheet online.   I would highly appreciate your guidance on the following questions: Can the BMA8420 be used to measure the EIS of a hydrogen fuel cell stack? How can I obtain the BMA8420 full datasheet(not Product Brief ) ? Contact point in Korea ? Thank you for your support, and I look forward to hearing from you.   Best regards, Young, Kim       BMA8420   <-- link image.png #BMA8420
查看全文
Request for MTTF-FIT Reliability Data Dear Sir/Madam, I am currently calculating the MTBF value for our product, in which we have used the components manufactured by your company. Therefore, I kindly request you to provide the MTTF and/or FIT value for the below-mentioned component(s), if available. This information will help us to calculate the MTBF of our product accurately. Part Number: NTS0104BQ,115 Description: Voltage Level Translator Bidirectional 1 Circuit 4 Channel 50Mbps 14-DHVQFN (2.5x3) If any additional information regarding the operating conditions or application is required to provide the reliability data, please let us know. Thank you for your support. Cloud Lab online debug online laboratory Virtual test
查看全文
imx95とvfio_pciパススルー こんにちは、 IMX95 SoC上でPCIパススルー機能を備えた仮想マシンを使用したいと考えています。しかし、SMMUはキャッシュコヒーレントではなく、vfio_pciドライバーがそれを必要としているため、これは全く不可能のようです。関連項目: https://community.nxp.com/t5/i-MX-Processors/i-MX95-19x19-EVK-SMMU-coherent-table-walks-IDR0-COHACC-and-vfio/mp/2410515 そして https://github.com/NXP/dpdk/blob/25.11-qoriq/nxp/README_imx95_enetc_vf_vfio#L32 IOMMUを無効にすることはできません。また、カーネルパラメータが次のように書かれているので、役に立つとは思えません。 MODULE_PARM_DESC(enable_unsafe_noiommu_mode, "安全でない、IOMMUなしモードを有効にします。このモードはデバイス隔離を提供せず、DMA変換もホストカーネル保護も提供せず、 仮想マシンへのデバイス割り当てには使用できず、RAWIO権限が必要で、カーネルを汚染します。これが何のためにあるのか分からない場合は、離れてください。(デフォルト:false)""); IMX95 SoCを(安全な)PCIパススルーで使うのは本当に不可能なのでしょうか?そうでないなら、私が何か見落としているのでしょうか? よろしくお願いします、 マイケル Re: imx95 and vfio_pci passthrough こんにちは、 迅速なご回答ありがとうございます。でも、完全に理解できているかどうか自信がありません。念のため確認ですが、DPDKは使用せず、PCIデバイスをパススルーする汎用的なqemu/kvm仮想マシンを使用したいと考えています。これはuio-pci-genericフレームワークとどのように関連しているのでしょうか? ありがとう、 マイケル Re: imx95 and vfio_pci passthrough こんにちは、 NXP Semiconductors製品にご関心いただきありがとうございます。 この場合、DPDKチームの同僚の回答に従う必要があります。唯一の選択肢は、回答で述べられているものです。 「顧客が他の用途でSMMUを使いたいが、DPDKではバイパスしても許容される場合(bootargsでiommu.passthrough=1を使いたくない、DTSでSMMUノードを無効にしたくない場合)。 その後、uio-pci-genericフレームワークのバインドを試み、VSI-PSIメッセージングを無効にすることができます(エクスポートENETC4_VSI_MSG_DISABLE=1)。しかしVSI-PSIメッセージを無効にすると、ユーザーはpromisc、VLAN MACフィルタリング、リンク情報などのENETC機能の一部を使えなくなります。」 よろしくお願いします。
查看全文
ティッククロックの設定および基準クロックの選択に関して こんにちは: ベアメタルティッククロック(S32K358デバイス)を設定したいと考えています。BaseNXPの設定を図1に示します。この設定でティッククロックに接続できますか?2. デバイスツリー内のどのクロックに「48MHz」が設定されていますか? sunshine88_0-1789971547489.png sunshine88_1-1789971658567.png 設定後、OsIf_Init(NULL_PTR); OsIfDelay(x); を使用して呼び出すことはできますか? どうもありがとうございます! Re: 关于滴答时钟建立及基时钟的选择 こんにちは、@sunshine88 さん。 OsIfSystemTimerClockFreqはCORE_CLKに対応し、私の場合は160MHzです: PavelL_0-1789999751219.png PavelL_1-1789999832315.png よろしくお願いいたします。 パベル
查看全文
How can I write/debug code for DSP56367 nowadays? ( Symphony studio not running anymore) Hi ! I would like ro run/debug/single step code for the DSP 56367. I cannot get Symphony studio to run on windows 10, not even setting compatibility to windows 7. Any help would be greatly appreciated. thanks Ariel// Re: How can I write/debug code for DSP56367 nowadays? ( Symphony studio not running anymore) Hello @ArielAr , Thanks for your post. We still have Suite56, but it has the same problem and won't run on Windows 10. Unfortunately, these tools are no longer supported, so there isn't really a better option that I'm aware of. One thing you could try is running a Windows 7 or XP virtual machine in VMware or VirtualBox and then installing Symphony Studio there. I haven't tested this myself, though, so just take it as a suggestion. BR Celeste
查看全文
How to Recover Your Lost Bitcoin Without Falling Victim to Another Scam I never imagined I would become a victim of a cryptocurrency investment scam. Like many others, I was promised high returns and convinced that my investment was safe. What started as a promising cryptocurrency investment quickly turned into one of the most painful experiences I have ever faced. Like many people searching for financial growth and security, I trusted what appeared to be a legitimate investment platform. The website looked professional, the representatives were convincing, and genuine. Over time, I invested a total of €210,000 in Bitcoin, believing I was building a better future for myself and my family. Then, without warning, everything changed. When I tried to withdraw my funds, I encountered delays, excuses, and requests for additional payments. Soon after, communication stopped completely. It became painfully clear that I had fallen victim to a sophisticated scam. The emotional impact was overwhelming. I felt betrayed, embarrassed, and devastated. The money I had worked so hard to earn was gone, and with it went my confidence and peace of mind, countless moments of self-blame, and a growing fear that I would never recover from such a significant loss. During this difficult period, I regularly spoke with my therapist about what had happened. She saw how much the loss was affecting my mental health and overall well-being. she suggested that I reach out to Digital Light Solution Website https://digitallightsolution.com/, ; From my first interaction with their team, I felt something I had not felt in a long time—hope. They treated my case with professionalism, patience, and understanding. Most importantly, they listened. During one of the darkest periods of my life, Digital Light Solution their guidance and support helped me regain confidence and take positive steps forward. Today, I share my story not only to express my gratitude but also to warn others. Cryptocurrency scams are becoming more sophisticated every day. Fake investment platforms, romance scams, and online job scams are destroying lives and draining the savings of innocent people around the world. If there is one lesson I learned from this experience, it is this: always do thorough research before investing, never trust promises of guaranteed returns, and remain vigilant online. Losing your hard-earned money can be devastating, but awareness and caution can help protect others from experiencing the same heartbreak. Email:[email protected] WhatsApp +19548568045, https://wa.link/989vlf Re: How to Recover Your Lost Bitcoin Without Falling Victim to Another Scam A group of cryptocurrency investors reportedly suffered a combined loss of approximately $2.3 million after becoming victims of a fraudulent Decentralized Autonomous Organization (DAO). The project was presented as a revolutionary investment opportunity, supported by professional-looking websites, promotional material, and testimonials designed to create an appearance of legitimacy. After investors deposited their cryptocurrency into the project’s smart contract, the fraudsters allegedly exploited a hidden backdoor within the contract and transferred the deposited assets to other wallet addresses. The sudden loss left the victims searching for answers and trying to determine whether their funds could be traced. TECHY FORCE CYBER RETRIEVAL (TFCR) was brought in to assist with the investigation. The process began with collecting transaction hashes, wallet addresses, smart-contract information, screenshots, communications, and other available evidence relating to the investment. TFCR then used blockchain-analysis techniques to examine the transactions and follow the movement of the cryptocurrency between wallets. Investigators can analyze transaction patterns, identify intermediary addresses, and document transfers that may help establish how the stolen assets moved through the blockchain. The investigation highlights an important characteristic of cryptocurrency: although transactions are generally irreversible, many blockchains maintain publicly accessible transaction records. These records can provide investigators with valuable information when reconstructing the movement of digital assets. For victims of fraudulent DAO schemes, preserving transaction information and reporting the incident promptly can be important. Blockchain tracing does not guarantee that stolen cryptocurrency will be recovered, but it can help establish an evidence trail that may support further investigation, exchange intervention, legal proceedings, or law-enforcement action. REACH OUT TO TECHY FORCE CYBER RETRIEVAL  (@)TECHCYBERFORC     Website  https://techyforcecyberretrievals.com
查看全文
S32DS v3.4が起動時にクラッシュし、アクティベーションIDを取得できず、オフラインライセンスファイルが必要です NXPサポートの皆様、 私のS32 Design Studio for S32 プラットフォーム v3.4ライセンスが期限切れまたは行方不明になっています。ソフトウェアを起動すると、「Product Licenses - NXP Licenses」ウィンドウが表示され、「Status: License Missing」と表示されます。どのボタン(Activate、Details、Close)でも即座にクラッシュし、ソフトウェア全体が閉じられます。 私が持っている情報は以下のとおりです。 登録メールアドレス: [[email protected]] ソフトウェアアクティベーションコード: DC1D-EDC9-8B34-496C(元のダウンロードメールより、アカウント名:pang yun) S32DS バージョン: v3.4 バックエンドでライセンスを延長してもらえますか? ご協力いただき、誠にありがとうございました。 Re: S32DS v3.4 crashes upon opening, cannot retrieve Activation ID, need offline license file こんにちは、 お客様のS32DSライセンスが延長されました。コードを使ってS32DSを再度有効化してください。
查看全文
S32k3用の5Vまたは3.3VのI/O電源 こんにちは、みんな、 現在、 NXP S32K3 ファミリーをベースにした自動車用ECUを設計しており、MCUのI/O供給領域に最適な構成を評価しています。 私の理解では、このデバイスはI/OドメインAとドメインBに対して、以下のような異なる電源供給オプションに対応しています。 ドメインA = 5V、ドメインB = 5V ドメインA = 3.3V、ドメインB = 3.3V ドメインA = 5V、ドメインB = 3.3V 各構成の主な設計上のトレードオフや選択基準を理解しようとしています。具体的には: 入出力領域において、5Vと3.3Vを使用する場合の主な利点と欠点は何ですか? 一般的に混合電圧構成(5 V / 3.3 V)が好まれる自動車用途はどこですか? EMC/EMIの性能、消費電力、信号の整合性、堅牢性、インターフェースの互換性に関して、この選択を促す影響はあるのでしょうか? NXPは、各I/O供給オプションの理論や推奨ユースケースを説明するアプリケーションノート、ハードウェア設計ガイドライン、または参考文献を提供していますか? これまでのS32K3プロジェクトから得られた設計のアドバイスや教訓があれば、ぜひ教えていただけるとありがたいです。 ご回答をお待ちしています。 Re: 5V or 3.3V I/O supply for S32k3 こんにちは、 @DavidSilva さん、 利点や欠点というより、主にアプリケーションの要件によります。システムの電圧レベルやデバイスのインターフェースモジュールに応じて、VDD_HV_AドメインとVDD_HV_Bドメインを設定できます。つまり、トレードオフや好みはデザインのみに基づいています。 最も大きな影響は以下の通りである。 VREFHは常にVDD_HV_A +0.1以下でなければなりません。VREFHとVDD_HV_A間の正の差電圧、すなわちVDD_HV_A <= VDD_HV_A + 0.1V)はRF-AC専用です。 LPCMP0チャネルはVDD_HV_A >=VDD_HV_Bの場合にのみ選択・有効化が必要です。VDD_HV_AがVDD_HV_Bを下回った場合、これらのチャネルを無効にする必要があります。 社内チームは、3.3Vの電流消費値を特に提供していないことを共有しています。これは基本的に5Vと同じなので、5Vの測定値を使うことができます。 また、電圧領域構成に関する具体的なアプリケーションノートは提供していませんが、S32K3(電圧領域を含む)に関するすべての要件と推奨事項をまとめたハードウェア設計ガイドラインのアプリケーションノートを参照できます。 よろしくお願いします、 ジュリアン
查看全文
MR-VMU-RT1176 外部内存 在定制板上使用 MR-FMUM-RT1176 时,是否可以添加额外的外部存储器?由于并非所有 SEMC 引脚都可通过连接器使用,而且两个 FLEXSPI 都已被使用。 Re: MR-VMU-RT1176 External RAM 嗨@Zaregg , 感谢您对 NXP MIMXRT 系列产品的关注! 如果仅使用 MR-FMUM-RT1176 模块而自行设计载板,则无法添加外部存储器。如果您确实需要 同步动态随机存取存储器(SDRAM) 或 HyperRAM 等内存映射扩展,唯一的途径是自行设计芯片级扩展,以充分发挥 SEMC 或 FlexSPI 总线的性能。如果可以使用外置闪存/EEPROM,那么可行的方案如下: (1)重新分区模块上的八进制闪存 (2)通过 lpspi/lpi2c 在载板上添加串行设备。   此致, 加文
查看全文
Request to extend expired license for S32 Design Studio for ARM v2.2 Hi,   Request to extend expired license for S32 Design Studio for ARM v2.2 kasiFu_0-1789898180759.pngkasiFu_0-1789898180759.png Re: Request to extend expired license for S32 Design Studio for ARM v2.2 Hi,  your S32DS license has been extended. Please activate S32DS again with your old code. 
查看全文
S32DS for ARM 2018R1 ライセンス こんにちは: S32DS for Arm 2018R1 IDE のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか? ありがとうございます。 binli_0-1654501988529.png Re: S32DS for ARM 2018R1 license こんにちは、 S32 Design Studio for ARM v2018.R1のライセンスの有効期限が切れました。 延長していただけますか? アクティベーションコード00B2-2243-F93D-50F1 よろしくお願いします。 Re: S32DS for ARM 2018R1 license こんにちは: S32DS for Arm 2018R1 IDE のライセンスの有効期限が切れました。確認して延長してもらえますか?ありがとうございます qfgl_1-1761810711063.png Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for ARM バージョン 2018.R1 のライセンスの有効期限が切れました。延長していただけますか? アクティベーションコード: 0255-52A3-B9BE-AB0C よろしくお願いします。 Re: S32DS for ARM 2018R1 license こんにちは: S32DS for ARM V2.2 のライセンスが 13 日後に期限切れになります。確認して延長を手伝っていただけますか? Arm用S32 Design Studio アクティベーションID: 97B6-8CB8-3FC0-851A 評価日数: 13 機能バージョン: 2.2 機能のステータス: 評価 (13 日間) ありがとうございます。 Re: S32DS for ARM 2018R1 license ,,,,,,,,,,,,,,,,,,,,,,,,,,, Re: S32DS for ARM 2018R1 license ,,,,,,,,,,,,,, Re: S32DS for ARM 2018R1 license ,,,,,,,,,,,,,,,,,,,,, Re: S32DS for ARM 2018R1 license ,,,,,,,,,,,,,,,,,,,,,,,, Re: S32DS for ARM 2018R1 license はい、うん Re: S32DS for ARM 2018R1 license こんにちは: S32DS for Arm 2018R1 IDE のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか? ありがとうございます。 DXD_1-1760436860875.png Re: S32DS for ARM 2018R1 license こんにちは、 S32DS ARM V2.2 ライセンスの有効期限が切れました。 ライセンスを延長していただけますか? アクティベーションID: DD5C-6F03-8AE4-7ECA SOありがとう。 Re: S32DS for ARM 2018R1 license S32 プラットフォーム 3.4 の S32DS のライセンスの有効期限が切れました。確認して延長してもらえますか?ありがとうございます。アクティベーションコード C5A1-5B94-2A38-9034 Re: S32DS for ARM 2018R1 license こんにちは: おはようございます!S32dsのライセンスが期限切れです。ライセンスの延長をお願いできますか?ソフトウェアバージョンは2.2です。 YongBo1_0-1753323581378.png YongBo1_1-1753323618471.png YongBo1_2-1753323647489.png 本当にありがとうございます!あなたの助けが必要です! Re: S32DS for ARM 2018R1 license こんにちは: S32DS for Arm 2018R1 IDE のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか? ありがとう。アクティベーションコード:349D-19F8-FFD7-7F10 回复: S32DS for ARM 2018R1 license こんにちは: S32DS for Arm 2018R1 IDE のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか? ありがとう。アクティベーションコード592C-8B75-D563-0CAE jadezhang0808_1-1753157055690.png Re: S32DS for ARM 2018R1 license こんにちは、 S32DS ライセンスが延長されました。 Re: S32DS for ARM 2018R1 license S32DS for ARM 2018R1 のライセンスの有効期限が切れました。延長をお願いしたいです。どうもありがとうございます。 コード9DD9-3E3B-4AA1-1DE3 S32DS for ARM 2018R1 license こんにちは、 S32 Design Studio for Arm v2018 R1 ライセンスの有効期限がすでに切れていますが、延長してもらえますか? ありがとうございます! アクティベーションコード: DE17-8B75-A725-CBC3 SomeBlack_0-1747874771004.png Re: S32DS for ARM 2018R1 license S32DS for Power Win32 v2017 IDEs のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか?「このライセンスを返却することはできません」というヒントです。返品しようとすると、「 よろしくお願いします。 xiaocong_0-1747722624302.png Re: S32DS for ARM 2018R1 license S32DS for Arm 2018R1 IDE のライセンスの有効期限が切れました。確認して延長してもらえますか?アクティベーションコード D429-1EC2-B799-7507 ありがとう。 Re: S32DS for ARM 2018R1 license こんにちは: S32 Design Studio for Power Architecture ® v2.1 - Windows/Linuxのライセンス IDE の有効期限が切れました。確認と延長を手伝っていただけますか? アクティベーションコード DDD9-023A-976E-CD88 ありがとうございます。 Re: S32DS for ARM 2018R1 license こんにちは: S32DS for Arm 2018R1 IDE のライセンスの有効期限が切れました。確認と延長を手伝っていただけますか?アクティベーションコード DDD9-023A-976E-CD88 ありがとう。 Re: S32DS for ARM 2018R1 license こんにちは、 S32DS ライセンスが延長されました。古いコードを使用して S32DS を再度アクティブ化してください。 Re: S32DS for ARM 2018R1 license こんにちは、S32 Design Studio for ARM v2.2 ライセンスの有効期限はすでに切れています。延長してもらえますか? ありがとうございます! アクティベーションコード: 2D6B-DC21-07CF-F125 Re: S32DS for ARM 2018R1 license こんにちは、 S32DS ライセンスが延長されました。 Re: S32DS for ARM 2018R1 license こんにちは: 私の免許証 S32DS for Arm v2.2 IDE の有効期限がもうすぐ切れます。確認して延長していただけませんか? ありがとうございます。 アクティベーションコード: BC11-7022-0D21-E460 回复: S32DS for ARM 2018R1 license こんにちは、 S32 Design Studio for Arm v2018 R1 ライセンスの有効期限がすでに切れていますが、延長してもらえますか? ありがとうございます! アクティベーションコード: 4777-90EB-DAF6-AE57 Re: S32DS for ARM 2018R1 license こんにちは、 S32DS ライセンスが延長されました。 Re: S32DS for ARM 2018R1 license こんにちは、 S32 Design Studio for ARM v2018 R1 のライセンスが期限切れです。延長してもらえますか? アクティベーションコード: 6EC6-15B7-7227-97F6 ありがとうございます。 カルロ 回复: S32DS for ARM 2018R1 license 屏幕截图 2025-02-18 104107.png こんにちは: S32DS for ARM V1.3 のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか? ありがとうございます。 Re: S32DS for ARM 2018R1 license 問題は解決しました。ありがとうございます Re: S32DS for ARM 2018R1 license S32DS ライセンスの拡張を手伝ってください。アクティベーションコード: FF84-9C7B-EFCB-6595。ありがとうございます! Re: S32DS for ARM 2018R1 license こんにちは、 あなたのアカウントを確認しましたが、すべてのライセンスは有効でアクティブ化されています。S32DS PA では異なるアクティベーション キーを使用しましたが、問題はありません。 Re: S32DS for ARM 2018R1 license ソフトウェアフィードバック:(ライセンスがありません) Re: S32DS for ARM 2018R1 license こんにちは。私の S32 Design Studio for Power Architecture バージョン 2.1 ライセンスの有効期限がすでに切れていますが、延長することはできますか? ありがとうございます! アクティベーションコード: 77FC-3B94-A7DC-54EE Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for ARM バージョン 2018.R1 のライセンスの有効期限が切れました。延長していただけますか? アクティベーションコード: FF84-9C7B-EFCB-6595 どうもありがとうございます Re: S32DS for ARM 2018R1 license こんにちは。ARM 2018R1 用に S32DS を再インストールしました。 オフラインでアクティベートすると、activation.xml に「ライセンスを生成CANません。すでに期限が切れています」と表示されます。 Re: S32DS for ARM 2018R1 license こんにちは、 S32DS ライセンスが延長されました。 Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for ARM バージョン 2018.R1 のライセンスが期限切れになりました。延長していただけますか? アクティベーションコード: FC1A-4C29-3203-9C08 どうもありがとうございます 回复: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for Arm v3.5 のライセンスの有効期限がすでに切れていますが、延長してもらえますか? ありがとうございます! アクティベーションコード: 8A8B-9E9B-F34E-2603 回复: S32DS for ARM 2018R1 license こんにちは。私の S32 Design Studio for Arm v2.2 ライセンスはすでに期限切れです。延長してもらえますか? ありがとうございます! アクティベーションコード: D0BA-0474-25E0-F056 S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for Arm v2018 R1 ライセンスの有効期限がすでに切れていますが、延長してもらえますか? ありがとうございます!アクティベーションコード: 3EF3-981A-CE8D-45C3 Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for Arm v2018 R1 ライセンスの有効期限がすでに切れていますが、延長してもらえますか? ありがとうございます! アクティベーションコード: 3EF3-981A-CE8D-45C3 回复: S32DS for ARM 2018R1 license こんにちは: S32DS for Arm 2018R1 IDE のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか? ありがとうございます。 aiai_0-1723802490382.png Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for ARM バージョン 2018.R1 のライセンスがもうすぐ期限切れになります。 延長していただけますか?ありがとう。 アクティベーションコード: C617-86A4-65B7-F3D9 どうもありがとうございます 回复: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for Arm v2018 R1 ライセンスの有効期限がすでに切れていますが、延長してもらえますか? ありがとうございます! アクティベーションコード: 0384-6363-91F6-CB8E Re: S32DS for ARM 2018R1 license こんにちは、 S32 Design Studio for Arm v2018 R1 ライセンスの有効期限がすでに切れていますが、延長してもらえますか? ありがとうございます! アクティベーションコード: 8238-B154-F160-0911 Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for ARM バージョン 2018.R1 のライセンスがもうすぐ期限切れになります。 延長していただけますか?ありがとう。 アクティベーションコード: 516A-3379-0522-6A9D どうもありがとうございます Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for ARM バージョン 2018.R1 のライセンスがもうすぐ期限切れになります。 延長していただけますか?ありがとう。 アクティベーションコード: 0D34-286B-9EE6-E692 どうもありがとうございます Re: S32DS for ARM 2018R1 license こんにちは、 S32DS ライセンスが延長されました。古いコードを使用して S32DS を再度アクティブ化してください。 Re: S32DS for ARM 2018R1 license S32 Design Studio for Arm v2018 R1 ライセンスの有効期限がすでに切れていますが、延長してもらえますか? ありがとうございます! アクティベーションコード: DC0F-DD50-F612-9743 Re: S32DS for ARM 2018R1 license こんにちは。私のライセンスの有効期限が切れました。ライセンスの延長、アクティブコードについて助けてください。 DC0F-DD50-F612-9743 回复: S32DS for ARM 2018R1 license こんにちは。私のライセンスの有効期限が切れました。ライセンスの延長、アクティブコードについて助けてください。 DC0F-DD50-F612-9743 Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for ARM バージョン 2018.R1 のライセンスの有効期限が切れました。延長していただけますか? アクティベーションコード: DE63-F9AF-C189-5399 どうもありがとうございます Re: S32DS for ARM 2018R1 license こんにちは: S32DS for Arm 2018R1 IDE のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか? ありがとうございます。 ========================================== 商品の説明S32 Design Studio 注文番号S32DS_2018_R1_100931407 注文番号 ライセンスの総数:100 アクティベーションコード C625-7579-0C28-63DC 製品に適用されるライセンス: バージョンの説明 R1 2018 S32 Design Studio (EULA を表示) 3.1 S32 Design Studio (EULA を表示) 100個入手可能       Re: S32DS for ARM 2018R1 license こんにちは: S32DS for Arm 2018R1 IDE のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか? ありがとうございます。 Joe_0_0-1705036715844.png Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for ARM v2.2 のライセンスの有効期限が切れました。延長していただけますか? アクティベーションコード F1B3-2017-8F0D-17BE よろしくお願いします。 Re: S32DS for ARM 2018R1 license こんにちは、 @acirillo さん、 ライセンスの有効期限を 2028 年末まで延長しました。 ローカル ライセンス情報を更新するには、NXP ライセンス メニューの「更新」アクションを使用してください。 よろしくお願いします、 メフル・パテル Re: S32DS for ARM 2018R1 license こんにちは、 S32S 2018のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか? よろしくお願いします。 Re: S32DS for ARM 2018R1 license こんにちは、 @linxwhut さん、 両方のライセンスの有効期限を 2028 年末まで延長しました。 ローカル ライセンス情報を更新するには、NXP ライセンス メニューの「更新」アクションを使用してください。 よろしくお願いします、 メフル・パテル Re: S32DS for ARM 2018R1 license こんにちは、 @Detective さん、 ライセンスの有効期限を 2028 年末まで延長しました。 ローカル ライセンス情報を更新するには、NXP ライセンス メニューの「更新」アクションを使用してください。 よろしくお願いします、 メフル・パテル Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for ARM バージョン 2018.R1 のライセンスの有効期限が切れました。延長していただけますか? アクティベーションコード: C819-045E-F1F8-61B7 Re: S32DS for ARM 2018R1 license こんにちは。私と同僚の S32 Design Studio for Power Architecture バージョン 2.1 ライセンスの有効期限が切れてしまいました。ライセンスの延長を手伝っていただけますか?ありがとう アクティベーションコード:82DF-FC84-F43A-1EF0 アクティベーションコード:5EBA-DE62-DCF0-02A9 Re: S32DS for ARM 2018R1 license こんにちは、ホーガンさん。 有効期限を2027年まで延長しました。現在のコードで再度アクティブ化してください。 よろしくお願いします、 マイク Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for ARM バージョン 2018.R1 のライセンスの有効期限が切れました。延長していただけますか? アクティベーションコード: E03E-A0CC-D45D-88C8 どうもありがとうございます Re: S32DS for ARM 2018R1 license よろしくお願いします。 Re: S32DS for ARM 2018R1 license 親愛なる、 S32 Design Studio for ARM バージョン 2018.R1 のライセンスの有効期限が切れました。延長していただけますか? アクティベーションコード: E03E-A0CC-D45D-88C8 どうもありがとう 。 Re: S32DS for ARM 2018R1 license こんにちは、 @J_Garyさん、 ライセンスの有効期限を 2028 年末まで延長しました。 ローカル ライセンス情報を更新するには、NXP ライセンス メニューの「更新」アクションを使用してください。 よろしくお願いします、 メフル Re: S32DS for ARM 2018R1 license こんにちは。S32 Design Studio for Arm v2018 R1 ライセンスの有効期限がすでに切れていますが、延長してもらえますか? ありがとうございます! アクティベーションコード: E971-3802-1E3D-5BA6 Re: S32DS for ARM 2018R1 license こんにちは、 @liamtsenさん、 あなたのライセンスを2028年12月末まで延長しました。 使用するにはアクティベーションを更新してください。 いつもご利用いただき、ありがとうございます。よろしくお願いいたします。  - メフル・パテル Re: S32DS for ARM 2018R1 license こんにちは。私の免許証の有効期限が切れてしまいました。CAN延長してもらえますか? その番号は よろしくお願いします。 Re: S32DS for ARM 2018R1 license こんにちはサラさん ライセンスが延長されました。アクティベーション コードをもう一度試してください。 よろしくお願いします、 マイク 回复: S32DS for ARM 2018R1 license こんにちは、 @Hanshengさん あなたのライセンスを2027年末まで延長しました。使用するにはアクティベーションを更新してください。 いつもご利用いただき、ありがとうございます。よろしくお願いいたします。  -メフル・パテル Re: S32DS for ARM 2018R1 license こんにちは、 S32 Design Studio for ARM v2018.R1 ライセンスの有効期限がすでに切れています。延長にご協力いただけませんか? ありがとうございます! アクティベーションコード: B7B1-173F-51BA-13A2 よろしくお願いいたします。 サラ Re: S32DS for ARM 2018R1 license こんにちは、 @1772137309 。 あなたのライセンスを2028年末まで延長しました。 S32DS の [ヘルプ] -> [NXP ライセンス] メニューに移動し、[更新] をクリックして、ローカル マシン上のライセンス データを更新してください。 よろしくお願いします、 - メフル・パテル Re: S32DS for ARM 2018R1 license こんにちは、 S32 Design Studio for Arm v2018 R1 ライセンスの有効期限がすでに切れていますが、延長してもらえますか? ありがとうございます! アクティベーションコード: B0A4-688C-2AD6-79EE Re: S32DS for ARM 2018R1 license こんにちは、 @ScreenUserさん、 ライセンスの有効期限を 2027 年まで延長しました。 ローカル ライセンス情報を更新するには、NXP ライセンス メニューの「更新」アクションを使用してください。 よろしくお願いします、 - メフル・パテル Re: S32DS for ARM 2018R1 license S32 Design Studio for Arm v2018 R1 ライセンスの有効期限がすでに切れていますが、延長してもらえますか? ありがとうございます! アクティベーションコード: 6C82-9208-D1F2-C38F Re: S32DS for ARM 2018R1 license こんにちは、 ライセンスの有効期限を 2026 年まで延長しました。 ローカル ライセンス情報を更新するには、NXP ライセンス メニューの「更新」アクションを使用してください。 よろしくお願いします、 マイク Re: S32DS for ARM 2018R1 license こんにちは: S32DS_Power_Win32_v2.1 IDEs のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか? ありがとうございます。 回复: S32DS for ARM 2018R1 license こんにちは。私のライセンスは期限切れです。ライセンスの延長について助けてください。アクティブコード:93E3-80E7-2A38-9E70 回复: S32DS for ARM 2018R1 license こんにちは。私のライセンスは期限切れです。ライセンスの延長について助けてください。アクティブコード:93E3-80E7-2A38-9E70 Re: S32DS for ARM 2018R1 license どうもありがとうございます。今はすべて正常に動作しています。改めて感謝申し上げます。 Re: S32DS for ARM 2018R1 license こんにちは、ハオさん あなたの免許を3年間延長しました。S32DS の [ヘルプ] -> [NXP ライセンス] メニューに移動し、[更新] をクリックして、ローカル マシン上のライセンス データを更新してください。 よろしくお願いします、 マイク Re: S32DS for ARM 2018R1 license こんにちは、 @Jaydenyzhu 私はこの権利を2026年まで延長しました。 新しいライセンスを受け取るにはアクティベーション コードを使用してください。 よろしくお願いいたします。 - メフル・パテル S32DS for ARM 2018R1 license 親愛なる、 S32 Design Studio for ARM バージョン 2018.R1 のライセンスの有効期限が切れました。延長していただけますか? アクティベーションコードD5D0-D801-AB24-58DF よろしくお願いします。 Re: S32DS for ARM 2018R1 license My S32 Design Studio for Arm 2018_R1 の有効期限が 4 日後に切れますが、延長してもらえますか?ありがとう; アクティベーションID: 799E-5E79-910F-6C57 Re: S32DS for ARM 2018R1 license こんにちは、Gen Liさん あなたの免許を3年間延長しました。 現在のアクティベーション コードを使用して再度アクティベーションしてください。 よろしくお願いします、 マイク Re: S32DS for ARM 2018R1 license おはよう、 S32 Design Studio for Power Architecture バージョン 2.1 IDE のライセンスの有効期限が切れました。延長していただけますか? アクティベーションコード DBA1-317C-5265-7E4F よろしくお願いします。 Re: S32DS for ARM 2018R1 license こんにちは、Mehul_Patelさん S32DS が動作するようになりました。ありがとうございます。 Re: S32DS for ARM 2018R1 license こんにちは、 @zuqiao さん あなたのライセンスを2026年12月末まで延長しました。 アクティベーションを更新してください。 ありがとう。敬具。 - メフル・パテル Re: S32DS for ARM 2018R1 license こんにちは、 アクティベーションコードはD876-C313-75B1-2E1B です。ありがとうございます。 LICENSE.PNG Re: S32DS for ARM 2018R1 license こんにちは、 @cjgyf さん、 あなたの権利を2025年12月末まで延長しました。インストールを更新または再アクティブ化してください。 よろしくお願いいたします。 - メフル・パテル Re: S32DS for ARM 2018R1 license こんにちは、 @zuqiao さん ライセンスを再アクティブ化できるように、 S32DS for Arm v2018のアクティベーション コードを共有していただけますか。 いつもご利用いただき、ありがとうございます。よろしくお願いいたします。  -メフル・パテル Re: S32DS for ARM 2018R1 license 私のライセンスも期限切れ(9DE8-C6AE-8B6B-952B)なのですが、延長していただけますか?よろしくお願いいたします! Re: S32DS for ARM 2018R1 license こんにちは、NXPの専門家の皆さん。 S32DS for Arm v2018 のライセンスの有効期限が切れ、ライセンスが返却されましたが、現在ライセンスが欠落していることが示されています。ライセンスの延長にご協力ください。どうぞよろしくお願いいたします。 デビッド Re: S32DS for ARM 2018R1 license こんにちは、マイク 遅れてごめんなさい。どうもありがとうございます。今はすべて正常に動作しています。 敬具 フランチェスコ Re: S32DS for ARM 2018R1 license こんにちは、 あなたのライセンスを2025年まで延長しました。同じコードで再度アクティベートしてください。 よろしくお願いいたします。 Mike Re: S32DS for ARM 2018R1 license こんにちは。私の免許証の有効期限が切れてしまいました。CAN延長してもらえますか? その番号は 09D2-DE37-6529-87FB よろしくお願いします。 フランチェスコ Re: S32DS for ARM 2018R1 license こんにちは@francesco_solitさん、 この権限のサーバー ログを確認しました。返却されたライセンスの最大数に達したことが報告されています。カウントをリセットした、SO今は動作するはずです。同僚にもう一度試してもらってください。 また、同僚が次のリンクを使用して NXP.com アカウントにログインすると、独自のライセンスを取得できることにも注意してください。 https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=S32-DS-ARM_v2018 よろしくお願いいたします。 Mike Re: S32DS for ARM 2018R1 license こんにちは、マイク 再アクティベーションは現在私の PC では機能していますが、以前は同じライセンスが機能していた同僚の他の PC では機能しなくなりました。同僚にもライセンスを拡張することは可能ですか?それとも、新しいライセンスを取得することは可能ですか?NXP アカウントは次のとおりです。 [email protected] [email protected] よろしくお願いします。 フランチェスコ・ソリート Re: S32DS for ARM 2018R1 license 本当にありがとう、マイク。 敬具 フランチェスコ・ソリート Re: S32DS for ARM 2018R1 license こんにちは@francesco_solitさん、 あなたの権利を延長しました。新しい有効期限を受け取るSOライセンスを更新してください。 よろしくお願いいたします。 Mike Re: S32DS for ARM 2018R1 license おはよう。 S32DS for ARM 2018R1 のライセンスが期限切れになります。延長していただけますか?添付ファイルでご覧いただけます。 ありがとうございます。 フランチェスコ・ソリート Re: S32DS for ARM 2018R1 license こんにちは、 私はこの権利を2025年まで延長しました。新しいライセンスを受け取るにはアクティベーション コードを使用してください。 よろしくお願いいたします。 Mike Re: S32DS for ARM 2018R1 license こんにちは。私の免許証の有効期限が切れてしまいました。CAN延長してもらえますか? その番号は 4F70-F0A3-101C-3C96 本当にSOありがとう。 Re: S32DS for ARM 2018R1 license ありがとう、マイク。 良い一日を! Re: S32DS for ARM 2018R1 license こんにちは、 両方の権利は2025年まで延長されました。インストールを再アクティベートするには、アクティベーション コードを使用してください。 よろしくお願いいたします。 Mike Re: S32DS for ARM 2018R1 license こんにちは。私の免許証の有効期限が切れてしまいました。CAN延長してもらえますか? その番号は B361-6887-8BBF-ED12 さらに、私の同僚のアンナ・ダレッシオにも: E735-6A42-FED4-6005 本当にSOありがとう。 アニタ Re: S32DS for ARM 2018R1 license こんにちは@zhanglei327さん、 あなたの権利を2025年まで延長しました。インストールをライセンス サーバーと同期するには、[ヘルプ] -> [NXP ライセンス] メニューにある [更新] ボタンを使用してください。 よろしくお願いいたします。 Mike Re: S32DS for ARM 2018R1 license こんにちは、 私の免許証はもうすぐ期限切れになります。 zhanglei327_0-1658835568910.png zhanglei327_1-1658835608579.png Re: S32DS for ARM 2018R1 license おはよう! 問題は解決しました! よろしくお願いします。 ヴァレリア Re: S32DS for ARM 2018R1 license こんにちは@valeriaalessiさん、 サーバー側からライセンスを手動で返却しました。ライセンスの返却のオファーを受け取ったら、「はい」を選択してください。場合によっては、適切にリセットされない設定があり、強制的にリセットされることがあります。この後、ライセンスを返却すれば、問題なくアクティベートできるはずです。 よろしくお願いいたします。 Mike Re: S32DS for ARM 2018R1 license おはよう、 同じライセンス番号で再アクティブ化を試みましたが、ライセンスは別の機能用であるというメッセージが表示され続けます。ただし、最初のエラーの後、戻り値の回数を超えたことに関する 2 番目のエラーは再び発生しません。 助けていただけますか? よろしくお願いします。 ヴァレリア Re: S32DS for ARM 2018R1 license こんにちは@valeriaalessiさん、 ライセンスサーバーを確認しました。返品の最大数を超えたと報告されました。返品カウントをリセットしました。これで問題は解決されるはずです。もう一度お試しください。 Mike Re: S32DS for ARM 2018R1 license おはよう、 以前と同じ番号でライセンスを再度アクティブ化しようとしましたが、ライセンスは別の機能用であると表示されます。その後、「戻る」をクリックすると、エラー メッセージが表示されます (添付ファイルを参照)。 助けていただけますか? よろしくお願いします。 ヴァレリア error_1.PNG error_2.PNG Re: S32DS for ARM 2018R1 license こんにちは、 あなたのライセンスを2025年まで延長しました。[ヘルプ] -> [NXP ライセンス] メニューから更新するか、以前と同じアクティベーション コードを使用して再アクティベーションしてください。 よろしくお願いいたします。 Mike Re: S32DS for ARM 2018R1 license おはよう、 S32DS for Arm 2018R1 IDEs のライセンスが期限切れになりました。延長していただけますか? 添付ファイルで、現在のライセンスの有効期限が切れていることをCAN確認できます。 よろしくお願いします。 ヴァレリア Re: S32DS for ARM 2018R1 license こんにちは、 あなたの権利を延長しました。インストールを更新または再アクティブ化してください。 よろしくお願いいたします。 Mike Re: S32DS for ARM 2018R1 license Jack527_0-1764663383029.png私も期限が切れてしまいました。延長していただけますか?ありがとうございます。 回复: S32DS for ARM 2018R1 license 私の番号も延長していただけますか?ありがとうございます。私の番号(A9DC-778F-BAF6-8677)は有効期限が切れています。 回复: S32DS for ARM 2018R1 license ARM V2.2 用 S32DS の公式延期を要求します。 A467-A14C-CD17-0852 Re: S32DS for ARM 2018R1 license S32DS Power V2.1 ライセンスの有効期限が切れました。 ライセンスを延長していただけますか? アクティベーションID: 1C02-6C5E-91A6-0F19 SOありがとう。 Re: S32DS for ARM 2018R1 license こんにちは: S32DS for ARM v2.2 IDE のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか? ありがとうございます。 _0-1770255101921.png 回复: S32DS for ARM 2018R1 license こんにちは。ARM バージョン v2.2 の S32 Design Studio ライセンスの有効期限が近づいています。 詳しく説明していただけますか?ありがとうございます。 私のアクティベーションコードは95F3-8275-56B8-B07Dです どうもありがとうございます。 Re: S32DS for ARM 2018R1 license tem 説明S32 Design Studio for ARM v2018 注文番号S32-DS-ARM_v2018_169264627 您能帮我延長许可证的有效期吗?激活码EBF4-DE52-80C0-FD65 非常感谢。 Re: S32 Design Studio for ARM v2.2 license马上过期了,申请延长 注文ID / ライン # S32DS-IDE-Arm-V2-X_186201937 / 1 履行された数量 1 アクティベーションコード 2107-4B0B-EBCA-A774 製品 S32 Arm v2.2 Design Studio ホスト 647F47BFF507631C69881D8FA0244925EE42B3D7 注文日 2022年8月15日 Re: S32DS for ARM 2018R1 license こんにちは: S32DS for Arm 2018R1 IDE のライセンスの有効期限が切れました。確認して延長を手伝っていただけますか? 私のソフトウェアアクティベーションコードは09D2-DE37-6529-87FBです ありがとうございます。
查看全文
请求延长 S32 Design Studio for ARM v2.2 的过期许可证 你好, 请求延长 S32 Design Studio for ARM v2.2 的过期许可证 kasiFu_0-1789898180759.pngkasiFu_0-1789898180759.png Re: Request to extend expired license for S32 Design Studio for ARM v2.2 你好, 您的S32DS许可证已延期。请使用您之前的激活码重新激活S32DS。
查看全文