I am running the RWandCE example(LPC55S69+PN7160). When I use the TagWriter app on an Android phone to read the tag, it fails with no response. The log shows that it activated the poll mode. However, TagInfo can read it, but it shows a "communication interrupt" popup, and the result on the phone may be incorrect. Is this because both poll and listen are enabled in the discovery loop? But my requirement is that both poll and listen must be enabled simultaneously. And I have also closed all emulation cards on my android phone.
Please help me, thanks.
你好@BillyHu
希望你一切都好。
请尝试将PN7160固件更新到最新版本。您可以参考“PN7160 - 通过MCUXpresso进行固件更新”了解更多信息。
问候,
爱德华多。
你好,爱德华多,
我的固件版本已经是 12.50.11 了。单独使用轮询和监听功能时,两者都能正常工作,但当在 discoveryTechnologies 中同时启用这两个功能时,我无法使用 tagwriter 读取 PN7160 的卡模拟信息。您那边遇到过这个问题吗?
谢谢!
亲爱的爱德华多:
您有什么建议吗?PN7160出现这种现象正常吗?
谢谢!