MPC5xxx Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5xxx Knowledge Base

Labels

Discussions

Sort by:
******************************************************************************** * Detailed Description: * This example shows, how to use overlay feature - how to remap SRAM over Flash. * The remapping is visible only in mirrored flash address space. Normal address * space is not affected. * To see effect of the remapping, read the comments and watch following * addresses in debugger before and after executing Overlay() function: * * SRAM over Flash test case: * 0x4003_0000 * 0x090C_0000 * * Test HW: X-MPC5744PE257DC, MPC57xx motherboard * MCU: PPC5744PFMMM8 1N65H * Fsys: 200 MHz * Debugger: Lauterbach Trace32 * Target: internal_FLASH (debug mode, release mode) * EVB connection: none * ********************************************************************************
View full article
******************************************************************************** * Detailed Description: * * This example shows usage of FlexPWM module. * The Submodule0 is set to generate independent PWMA and PWMB signals * The PWMX is used as input for the Capture feature. * Capture logic is set to capture one rising and one falling edge in one shot mode. * Thus you can check the edge placing and calculate a generated duty cycle. * * ------------------------------------------------------------------------------ * Test HW: DEVKIT-MPC5744P rev.D * Maskset: 1N16P * Target : FLASH * Fsys: 200 MHz PLL1 * Debugger: Lauterbach * * * EVB connection: * * J1.3 - D[9] .. FlexPWM X[0] input * J1.5 - A[11] .. FlexPWM A[0] output * J1.7 - A[10] .. FlexPWM B[0] output * * * to measure generated pulse connect X[0] input with either A[0] or B[0] outputs. * ********************************************************************************
View full article
* Version: 1.1 * Date: Sep-22-2021 * Classification: General Business Information * Brief: This example content a basic PMPLL initialization and * configuration of Mode Entry module and Clock Generation * module. By default active is core 2 -> e200z4 ******************************************************************************** ******************************************************************************** * Detailed Description: * ------------------------------------------------------------------------------ * Test HW: MPC57xx + S32R274RRUEVB * Maskset: 1N58R * Target : internal_FLASH * Fsys: 240 MHz PLL with 40 MHz crystal reference for z7 and 120MHz for z4 * ******************************************************************************** Revision History: 1.0 Apr-02-2019 b21190(Vlna Peter) Initial Version 1.1 Sep-22-2021 b21190(Vlna Peter) FCCU fault reading
View full article
******************************************************************************** * Detailed Description: * ------------------------------------------------------------------------------ * Test HW: MPC57xx * Maskset: 1N81M * Target : SRAM * Fsys: 160 MHz PLL * ******************************************************************************** Revision History: 1.0 Oct-29-2014 b21190(Vlna Peter) Initial Version 1.1 Nov-20-2014 b21190(Vlna Peter) Modified for Cut2.0 1.2 Nov-20-2014 b21190(Vlna Peter) Added SWT_0 dissabling in startup 1.3 Mar-10-2016 b21190(Vlna Peter) Fixed clock configuraion for PLL 1.4 Feb-23-2017 b21190(Vlna Peter) FCCU EOUT and bi-stable protocol 1.5 Aug-26-2021 nxa13250(Vlna Peter) modified for MPC5746C *******************************************************************************/
View full article
******************************************************************************** * Detailed Description: * Purpose of the example is to show how to simulate Multi-bit or Single-bit ECC * error in FlexCAN RAM (user must choose it in the option at the end of * main function). * Example configures FlexCAN module, initializes ECC for all FlexCAN RAMs, then * it injects ECC error to the Message Buffer 9. * When corrupted data is accessed the IVOR1 exception handler is called in case * of multi-bit ECC error (IVOR1 exception occurs) and FCCU_Alarm_Interrupt * handler is called in case of single-bit ECC error (FCCU interrupt occurs). * Both function calls MEMU handler. * Reported FlexCAN ECC error address is corrected according RM, section 7.12.2.3 * The example displays notices in the terminal window (connector J19 on * MPC57xx_Motherboard)(19200-8-no parity-1 stop bit-no flow control on eSCI_A). * No other external connection is required. * ------------------------------------------------------------------------------ * Test HW: MPC57xx_Motherboard + MPC5744P-144DC * MCU: PPC5744PFMLQ8,0N15P,QQAA1515N, Rev2.1B * Fsys: 200 MHz PLL with 40 MHz crystal reference * Debugger: Lauterbach Trace32 * Target: internal_FLASH, RAM * Terminal: 19200-8-no parity-1 stop bit-no flow control * EVB connection: default ********************************************************************************
View full article
********************************************************************************  Detailed Description:  Configures the FlexCAN_0 to transmit and receive a CAN FD message with or without  bit rate switching for data phase.  Baudrate during arbitration phase is set to 500kbps, during data phase 2Mpbs.  NOTE! Termination resistor (120Ohm) have to be placed on transceivers output  ------------------------------------------------------------------------------  Test HW: DEVKIT-MPC5748G revD1  Maskset: 0N78S  Target : FLASH  Fsys: 160 MHz PLL ******************************************************************************** Revision History: 1.0 Jun-21-2021 Petr Stancik Initial Version *******************************************************************************/
View full article
******************************************************************************** * Detailed Description: * Initializes eQADC module and cyclically converts internal channel 145 (PMC * band gap). It also configures eTPUC and its timebases (TCR1) to feed STAC bus * (SRV1). This timebase is used for timestamp of the ADC conversion result. * Both values (result and timestamp) are displayed in the terminal window. * No external connection required excluding terminal via eSCI. * ------------------------------------------------------------------------------ * Test HW: XPC567XKIT516 - MPC567xADAT516 Rev.D, MPC567XEVBFXMB Rev.C * MCU: PPC5676RDMVY1 3N23A * Terminal: 19200-8-no parity-1 stop bit-no flow control on eSCI_A * Fsys: 180MHz * Debugger: Lauterbach Trace32 * PeMicro USB-ML-PPCNEXUS * Target: RAM, internal_FLASH * EVB connection: default ********************************************************************************
View full article
In the attachment you may find System Input / Output Pin Definition for MPC5744P (as it is common to be a embedded attachment with other MPC57xx devices). Preliminary version for next RM release
View full article
********************************************************************************  Detailed Description:  Example created as new Application project, see readme.txt for steps to do.  The purpose of this demo application is to show you the usage of the FlexCAN module  using the S32 SDK API and FreeRTOS.  In the first part, the application will setup the board clocks and pins.  Then it will configure the FlexCAN module features such as Bitrate and Message buffers  It will then create two FreeRTOS tasks, one for receiving frames and one for sending frames.  The two user buttons are used to send std message ID=0x1h with 1byte payload as 1 or 0.  Based on received std message with ID=0x2h to LEDs are toggled upon data0 byte.  Use external 12V to power a board.  Connect board with PCAN-USB to display send message and be able to receive some on DEVKIT  ------------------------------------------------------------------------------  Test HW: DEVKIT-MPC5748G rev.D1  Maskset: 0N78S  Target : FLASH  Fsys: 160 MHz PLL  Debugger: S32DS ********************************************************************************
View full article
******************************************************************************** * Detailed Description: * Initializes and calibrates eQADC module and cyclically converts choosen * channel, displaying it into terminal window along with its time stamp value. * User could connect EVB pot's wiper to pin header W (see below) to see valid * conversion result. * * ------------------------------------------------------------------------------ * Test HW: MPC5777C-512DS Rev.A + MPC57xx MOTHER BOARD Rev.C * MCU: PPC5777CMM03 2N45H CTZZS1521A * Fsys: PLL1 = core_clk = 264MHz, PLL0 = 192MHz * Debugger: Lauterbach Trace32 * Target: internal_FLASH * Terminal: 19200-8-no parity-1 stop bit-no flow control on eSCI_A * EVB connection: For ADC: J53-1 (EVB pot's wiper) --> PS0 - ANA17 * PS1 - ANA18 * PS2 - ANA19 * PS3 - ANA20 * ********************************************************************************
View full article
  ******************************************************************************** * Detailed Description: * Initializes and calibrates both eQADC modules and cyclically converts choosen * channels, displaying it into terminal window. * User could connect EVB pot's wiper to pin header W (see below) to see valid * conversion result. * * ------------------------------------------------------------------------------ * Test HW: MPC5777C-512DS Rev.A + MPC57xx MOTHER BOARD Rev.C * MCU: PPC5777CMM03 2N45H CTZZS1521A * Fsys: PLL1 = core_clk = 264MHz, PLL0 = 192MHz * Debugger: Lauterbach Trace32 * Target: internal_FLASH * Terminal: 19200-8-no parity-1 stop bit-no flow control on eSCI_A * EVB connection: For ADC: J53-1 (EVB pot's wiper) --> PS0-ANA17 PW08-ANB17 * PS1-ANA18 PW09-ANB18 * PS2-ANA19 PW10-ANB19 * PS3-ANA20 PW11-ANB20 * ********************************************************************************
View full article
********************************************************************************  Detailed Description:  This example shows ADC triggering from the eTimer1 module.  The OFLAG signal from the eTimer1 channel 5 is fed into ADC1 converter,  so ADC is set up for injected conversion with end of scan interrupt.  Red LED is dimmed based on converted value  ------------------------------------------------------------------------------  Test HW: DEVKIT-MPC5744P rev.B  Maskset: 1N16P  Target : FLASH  Fsys: 160 MHz PLL  Debugger: S32DS ********************************************************************************
View full article
* Detailed Description: * This example demonstrates frequency modulation at 20kHz with 250 steps. * Test HW: xPC57xx EVB + MPC5746C minimodule * Maskset: 1N06M * Target : Internal Flash * Fsys: 160 MHz PLL * ******************************************************************************** Revision History: 1.0 Oct-29-2014 b21190(Vlna Peter) Initial Version 1.1 Nov-20-2014 b21190(Vlna Peter) Modified for Cut2.0 1.2 Apr-23-2015 b21190(Vlna Peter) Added INTC driver and PIT ISR 1.3 May-14-2015 b21190(Vlna Peter) Dissabling SWT in Startup code 1.4 Jun-06-2017 b21190(Vlna Peter) ported for MPC5746C 1.5 Sep-29-2020 b21190(Vlna Peter) Added 20kHz frequency modulation *******************************************************************************/
View full article
* Example of eMIOS configuration for shifted PWM mode ******************************************************************************** * Test HW: MPC5746C minimodule + MPC57xx Motherboard * Maskset: 1N06M * Target : Internal Flash * Fsys: 160 MHz PLL * ******************************************************************************** Revision History: 1.0 Oct-29-2014 b21190(Vlna Peter) Initial Version 1.1 Nov-20-2014 b21190(Vlna Peter) Modified for Cut2.0 1.2 Apr-23-2015 b21190(Vlna Peter) Added INTC driver and PIT ISR 1.3 May-14-2015 b21190(Vlna Peter) Dissabling SWT in Startup code 1.4 Jun-06-2017 b21190(Vlna Peter) ported for MPC5746C 1.5 Jun-06-2017 b21190(Vlna Peter) eMIOS example with shifter PWM *******************************************************************************/
View full article
This example content a basic FMPLL initialization and configuration of Mode Entry module and Clock Generation module. By default active is core 2 -> e200z4 Demonstration of PIT triggering an interrupt on timeout. ******************************************************************************** * Test HW: MPC57xx + S32R274RRUEVB * Maskset: 1N58R * Target : internal_FLASH * Fsys: 240 MHz PLL with 40 MHz crystal reference for z7 and 120MHz for z4 ******************************************************************************** Revision History: 1.0 Apr-02-2019      b21190        (Vlna Peter) Initial Version 1.1 Sep-19-2019     nxa13250    (Vlna Peter) Added PIT + interrupts *******************************************************************************/
View full article
This is the first lab for the 2D-ACE (DCU) tutorial
View full article
******************************************************************************** * Detailed Description: * Application performs basic initialization, setup PLL to maximum allowed freq., * setup clock for peripherals. * * This example shows, how to use some of ETimer modes. Channel 0 is set to * Fixed-Frequency PWM Mode and generates PWM signal with approximate frequency * 507Hz. This signal is routed to the UserLED1. * * Channel 1 is set to Count mode and generates 0,25 second interrupt. * In the interrupt service routine, duty cycle is increased from 0% to 100% * with step 6.25%. This shows for example, how can be controlled the brightness * of the LED. * * Channel 2 is set to Variable-Frequency PWM Mode and generates PWM signal with * frequency 10KHz. This signal is routed to the UserLED2. * * ------------------------------------------------------------------------------ * Test HW:         MPC5775K-356DS, MPC57xx Motherboard * MCU:             PPC5775KMMY3A 0N76P * Terminal: * Fsys:            PLL0 266MHz *                    Z4 Core 133MHz * Debugger:        Lauterbach Trace32 *                  PeMicro USB-ML-PPCNEXUS * Target:          internal_FLASH (debug mode, release mode) * EVB connection:  UserLED1 connected to P19.0 *                     UserLED2 connected to P19.2 * * ********************************************************************************
View full article
The purpose of the example is to present advantage of streaming mode feature.   Example initializes eQADC module, converts specified command queue and displays results into terminal window. Used analog inputs ANB_0 and ANB_1 requires external connection to converted voltage (potentiometer) to see some valid numbers. Following channels are being converted: CH0 = signal ANB_0 (connect pot USER_DEV_RV2(J4-7) --> ANB_0 (J19-3)) CH1= signal ANB_1 (connect pot USER_DEV_RV3(J4-8) --> ANB_1 (J19-4)) CH2 = may be left open (example configures the pin to be pulled-up) CH3 = may be left open (example configures the pin to be pulled-down) Result are being filled to 2 result queues to see loop switching in the terminal window when advance trigger occurs (results are displayed in two columns, 1st column is related to Rqueue0, 2nd to Rqueue1). Advance trigger occurs when EVB's USER switch 1 is being pressed (considering USER_DEV_1D(J4-2) --> TPU_A0 (J22-1)). Repeat trigger is initiated automatically by PIT3 timer in 1 sec intervals. eQADC command filled by eDMA, results drained by interrupt service routines.   For detailed description SEE ATTACHED document.
View full article
******************************************************************************** * Detailed Description: * ECSM Error Generation Register EEGR is used to generate a non-correctable ECC * error in RAM. The bad data is accessed then, so the IVOR1 exception is * generated and handled. * This file shows also ECSM_combined_isr and how to correct the wrong data. * Use macro Induce_ECC_error_by_DMA_read to select whether ECC error will be * injected by DMA read or CPU read. * At the end of main file you can select particular ME/EE setup by * comment/uncomment of particular function calls. * * ------------------------------------------------------------------------------ * Test HW:        XPC563MKIT * MCU:            PPC5633MMLQ80 * Fsys:           80/60/40/12 MHz * Debugger:       Lauterbach Trace32 *                 PeMicro USB-ML-PPCNEXUS * Target:         RAM, internal_FLASH * Terminal:       19200-8-no parity-1 stop bit-no flow control on eSCI_A * EVB connection: default * ********************************************************************************
View full article
With author's permission I am publishing document dealing with migration between MPC5646C to MPC574xG devices.   Document was created in year 2013, it was never been officially released, it is not maintained and it is shared AS IS. There is NO WARRANTY and NO SUPPORT can be expected.   However, it could be helpful for initial orientation on which points to look during migration work. If it is used, user should always refer to latest device's reference manual for possible specification changes.   Thanks to Christian Michel-Sendis, Viktor Fellinger and Jose Cisneros for their great job.
View full article