MPC5xxx知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5xxx Knowledge Base

标签

讨论

排序依据:
This example content a basic FMPLL initialization and configuration of Mode Entry module and Clock Generation module. By default active is core 2 -> e200z4 Demonstration of PIT triggering an interrupt on timeout. ******************************************************************************** * Test HW: MPC57xx + S32R274RRUEVB * Maskset: 1N58R * Target : internal_FLASH * Fsys: 240 MHz PLL with 40 MHz crystal reference for z7 and 120MHz for z4 ******************************************************************************** Revision History: 1.0 Apr-02-2019      b21190        (Vlna Peter) Initial Version 1.1 Sep-19-2019     nxa13250    (Vlna Peter) Added PIT + interrupts *******************************************************************************/
查看全文
This is the first lab for the 2D-ACE (DCU) tutorial
查看全文
******************************************************************************** * Detailed Description: * Application performs basic initialization, setup PLL to maximum allowed freq., * setup clock for peripherals. * * This example shows, how to use some of ETimer modes. Channel 0 is set to * Fixed-Frequency PWM Mode and generates PWM signal with approximate frequency * 507Hz. This signal is routed to the UserLED1. * * Channel 1 is set to Count mode and generates 0,25 second interrupt. * In the interrupt service routine, duty cycle is increased from 0% to 100% * with step 6.25%. This shows for example, how can be controlled the brightness * of the LED. * * Channel 2 is set to Variable-Frequency PWM Mode and generates PWM signal with * frequency 10KHz. This signal is routed to the UserLED2. * * ------------------------------------------------------------------------------ * Test HW:         MPC5775K-356DS, MPC57xx Motherboard * MCU:             PPC5775KMMY3A 0N76P * Terminal: * Fsys:            PLL0 266MHz *                    Z4 Core 133MHz * Debugger:        Lauterbach Trace32 *                  PeMicro USB-ML-PPCNEXUS * Target:          internal_FLASH (debug mode, release mode) * EVB connection:  UserLED1 connected to P19.0 *                     UserLED2 connected to P19.2 * * ********************************************************************************
查看全文
The purpose of the example is to present advantage of streaming mode feature.   Example initializes eQADC module, converts specified command queue and displays results into terminal window. Used analog inputs ANB_0 and ANB_1 requires external connection to converted voltage (potentiometer) to see some valid numbers. Following channels are being converted: CH0 = signal ANB_0 (connect pot USER_DEV_RV2(J4-7) --> ANB_0 (J19-3)) CH1= signal ANB_1 (connect pot USER_DEV_RV3(J4-8) --> ANB_1 (J19-4)) CH2 = may be left open (example configures the pin to be pulled-up) CH3 = may be left open (example configures the pin to be pulled-down) Result are being filled to 2 result queues to see loop switching in the terminal window when advance trigger occurs (results are displayed in two columns, 1st column is related to Rqueue0, 2nd to Rqueue1). Advance trigger occurs when EVB's USER switch 1 is being pressed (considering USER_DEV_1D(J4-2) --> TPU_A0 (J22-1)). Repeat trigger is initiated automatically by PIT3 timer in 1 sec intervals. eQADC command filled by eDMA, results drained by interrupt service routines.   For detailed description SEE ATTACHED document.
查看全文
******************************************************************************** * Detailed Description: * ECSM Error Generation Register EEGR is used to generate a non-correctable ECC * error in RAM. The bad data is accessed then, so the IVOR1 exception is * generated and handled. * This file shows also ECSM_combined_isr and how to correct the wrong data. * Use macro Induce_ECC_error_by_DMA_read to select whether ECC error will be * injected by DMA read or CPU read. * At the end of main file you can select particular ME/EE setup by * comment/uncomment of particular function calls. * * ------------------------------------------------------------------------------ * Test HW:        XPC563MKIT * MCU:            PPC5633MMLQ80 * Fsys:           80/60/40/12 MHz * Debugger:       Lauterbach Trace32 *                 PeMicro USB-ML-PPCNEXUS * Target:         RAM, internal_FLASH * Terminal:       19200-8-no parity-1 stop bit-no flow control on eSCI_A * EVB connection: default * ********************************************************************************
查看全文
With author's permission I am publishing document dealing with migration between MPC5646C to MPC574xG devices.   Document was created in year 2013, it was never been officially released, it is not maintained and it is shared AS IS. There is NO WARRANTY and NO SUPPORT can be expected.   However, it could be helpful for initial orientation on which points to look during migration work. If it is used, user should always refer to latest device's reference manual for possible specification changes.   Thanks to Christian Michel-Sendis, Viktor Fellinger and Jose Cisneros for their great job.
查看全文
The example does exactly the same operation like this example: https://community.freescale.com/docs/DOC-105380 ...but SSD flash driver is used now.   ******************************************************************************** * Detailed Description: * * Unlock, erase and program of flash mid block 0x00FB_8000 - 0x00FB_FFFF. * Used SSD flash drivers: * http://www.freescale.com/files/product/software/C55_JDP_SSD.exe * Version of the driver is v1.0.0 * ------------------------------------------------------------------------------ * Test HW:    X - PC5748G - MB (rev C) * MCU:        PPC5748GMMN6A * Maskset:    1N81M * Fsys:       160 MHz * Debugger:   Lauterbach Trace32 *              * Target:     Internal_FLASH * ********************************************************************************
查看全文
This config tool simplifies PLL setting calculation and clock configuration for MPC5744P device.                  Follow these steps                  Note: Macros have to be enabled!                  1. Enter frequency of used XOSC and desired PLL0 and PLL1 output.                 - put values into cells B11, Q10 and Q17 of the "Clocks" sheet                 - check if it is Valid or Invalid                 - "PLLconfig" sheet shows possible PLLs configurations                  2. Configure System and AUX clock selectors and its Dividers                 - check calculated frequency of System/Peripheral clocks                 - if Invalid change source clock and Divider value to keep Max freq                    3. Copy generated code by pressing "Copy Code" button
查看全文
******************************************************************************** * Detailed Description: * Test HW:  MPC57xx + S32R274RRUEVB * Maskset:  1N58R * Target :  internal_FLASH * Fsys:     240 MHz PLL with 40 MHz crystal reference for z7 and 120MHz for z4 ******************************************************************************** Revision History: 1.0     Apr-02-2019     b21190(Vlna Peter)  Initial Version 1.1    Apr-03-2019     b21190(Vlna Peter)  Added SWT reset reaction *******************************************************************************/ This example demonstrated the reset trigger on first SWT_2 timeout. Following screens shows the reset source after code execution in standalone mode and debugger connection afterwards:
查看全文
Hi,    Please update your Cyclone Flash Programming Algorithms for MPC57xx through the link.      http://www.pemicro.com/support/flash_list_menu.cfm     Older code algorithms includes area of HSM. If there are ECC errors in these blocks, the device may stuck in reset. During reset, the SSCM module searches for valid boot header. If it reads corrupted data from HSM blocks, it will not exit the reset.     Newer should be with “NO_BASE_ADDRESS=00F90000/”   https://community.nxp.com/thread/444748   Failed sample waves on PORST vs RESET are as below.    Algorithms in S32DS_Power_v2_1 and S32DS_Power_v2017_R1 are good.     Regards Oliver
查看全文
******************************************************************************** * Detailed Description: * Initializes eQADC module, performs calibration and cyclically converts PMC * internal channel as specified by macros CHOOSEN_PMC_ADC_CHNL, * CHOOSEN_PMC_ADC_SCALE and CHOOSEN_PMC_ADC_COMMAND to check particular voltage * level, displaying it into terminal window. * Example configures decimation filter to scale signal down by 1/16, this is * achieved by FIR filter (user could choose real filter by proper coeficient * selection). * Example also sums filtered samples by integrator that is configured to be * triggered and zeroed by eTPU signal (for simplicity it uses general purpose * outputs). Integrated values are displayed in terminal window as well. * No external connection required excluding terminal via eSCI. * ------------------------------------------------------------------------------ * Test HW:         XPC567XKIT516 - MPC567xADAT516 Rev.D, MPC567XEVBFXMB Rev.C * MCU:             PPC5676RDMVY1 3N23A * Terminal:        19200-8-no parity-1 stop bit-no flow control on eSCI_A * Fsys:            180MHz * Debugger:        Lauterbach Trace32 *                  PeMicro USB-ML-PPCNEXUS * Target:          RAM, internal_FLASH * EVB connection:  default ********************************************************************************
查看全文
In order to enable the RappID bootloader. It needs to program the C:\Freescale\RAppIDBL\RBF_Files\MPC5744P.rbf file into the MCU. User can use S32DS to program the rbf file to MCU. After that the Rappid bootloader PC utility can communicate with the MCU.
查看全文
******************************************************************************** * Detailed Description: * * * This example shows synchronization between FlexPWM, CTU and ADC modules. * The FlexPWM Submodule 0 is initialized to generate PWM signal, and rising edge * of PWM B0 signal is used to generate trigger signal for CTU module. The CTU module * sends two commands to ADCs. Single conversion mode is used, so ADC0 ch0 and ch1 * are sampled. The conversion result is used to modify PWM B0 rising egde position * and change delay between external trigger and ADC sequence triggering. * * ------------------------------------------------------------------------------ * Test HW:  MPC57xx * Maskset:  1N65H * Target :  internal_FLASH * Fsys:     200 MHz PLL with 40 MHz crystal reference * * EVB connection: * * P8.1  - A[0]  .. GPIO output, used to see CTU-ADC ISR period * P9.1     - B[7]  .. ADC0 AN[0] input * P9.2     - B[8]  .. ADC0 AN[1] input * P16.4 - I[3] .. CTU0 EXT TRG output   * P8.12    - A[11] .. FlexPWM A[0] output * P8.11    - A[10] .. FlexPWM B[0] output * * connect Trimmer J53.1 to P9.1 to change position of PWM B0 rising edge * connect Trimmer J53.1 to P9.2 to change CTU trigger delay from PWM B0 rising edge * * see CTU0 EXT TRG output signal (toggle on each trigger) on P16.4 with respect of PWM signals * ********************************************************************************
查看全文
******************************************************************************** * Detailed Description: * * LINFlexD_1 configured as Master *   - sends Header *   - either transmits a data to LIN Slave or receives data from a LIN Slave *   - no interrupt is used, just SW pooling * * LINFlexD_0 as Slave *   - receives header from a LIN Master *   - either receives data from a LIN Master or transmits a data to Master *   - filter is enabled *   - TX interrupt is used to prepare data to send and *   - RX interrupt to read received data * * EVB connection: * *   Switches on Motherboard: *   P6.1 to P8.1  ... SW1 to PA0 *   P6.2 to P8.2  ... SW2 to PA1 *   P6.3 to P8.3  ... SW3 to PA2 *   P6.4 to P8.4  ... SW4 to PA3 * *   Unconnect LINFlexD_0 from UART transceiver *   J14 SCI_RX open *   J13 SCI_TX open * *   As only single LIN transceiver is available LINFlex modules are connected *   together before this transceiver in the way TX pins together and RX pins together. *   TX pins must be configured as open drain and use a pullup resistor. * *   P11.15 to P12.8    TX pins *   P11.16 to P12.7    RX pins * *   Connect LINFlexD_1 to LIN transceiver on Motherboard *   J17 - LIN_TX ON *   J16 - LIN_RX ON *   J15 - LIN_EN ON *   P3 1-2 ON ... VSUP to 12V ** *   See LIN signal on P3.3 or J4.4. * * ------------------------------------------------------------------------------ * Test HW:  MPC5744P * Maskset:  1N65H * Target :  RAM, internal_FLASH * Fsys:     200 MHz PLL with 40 MHz crystal reference * Terminal: None ******************************************************************************** Revision History: 1.0     Feb-22-2016     PetrS          Initial Version of LIN example *******************************************************************************/ Original Attachment has been moved to: Example-MPC5744P-LINFlex-LIN-Master-Slave-test-v1_0-GHS614.zip
查看全文
******************************************************************************** * Detailed Description: * Purpose of the example is to show how to generate Multi-bit or Single-bit ECC * error in internal FLASH (user must choose it in the option at the end of main * function). * ECC error is injected by reading of pre-defined patterns in UTEST area at * addresses 0x00400040 and 0x00400060. * When corrupted data is accessed the IVOR1 exception handler is called in case * of multi-bit ECC error (IVOR1 exception occurs) and FCCU_Alarm_Interrupt * handler is called in case of single-bit ECC error (FCCU interrupt occurs). * Both function calls MEMU handler. * The example displays notices in the terminal window (connector J19 on * MPC57xx_Motherboard)(19200-8-no parity-1 stop bit-no flow control on eSCI_A). * No other external connection is required. * ------------------------------------------------------------------------------ * Test HW:         MPC57xx_Motherboard + MPC5744P-144DC * MCU:             PPC5744PFMLQ8,0N15P,QQAA1515N, Rev2.1B * Fsys:            200 MHz PLL with 40 MHz crystal reference * Debugger:        Lauterbach Trace32 * Target:          internal_FLASH, RAM * Terminal:        19200-8-no parity-1 stop bit-no flow control * EVB connection:  default ********************************************************************************
查看全文
******************************************************************************** * Detailed Description: * This example demostrates how to configure CGM )clock generation module) * and supply by clock all main peripherals. * Example demonstrate FCCU fake fault injection for fault 7 amd Alarm state * interrupt calling after injecting fake fault 7. * ------------------------------------------------------------------------------ * Test HW:  MPC57xx EVB * Maskset:  0N50N * Target :  internal_FLASH * Fsys:     200 MHz PLL * ******************************************************************************** Revision History: 1.0     Nov-04-2014     b21190(Vlna Peter)  Initial Version 1.1     Feb-04-2016     b21190(Vlna Peter)  Fixed Clock configuration 1.2    Jun-16-2017    b21190(Vlna Peter)  FCCU fake fault injection 1.3    Jun-16-2017    b21190(Vlna Peter)  FCCU alarm interrupt example *******************************************************************************/
查看全文
******************************************************************************** * File:                 main.c * Owner:            Peter Vlna * Version:           1.7 * Date:               Oct-10-2017 * Classification: General Business Information * Brief:                Example contains startup with PLL0 200MHz as system clock *                          and demonstrates reset triggered on FCCU Alarm state *                          counter exppire. ******************************************************************************** * Test HW:  MPC57xx * Maskset:  1N83M (cut 2.0B) * Target :  internal_FLASH * Fsys:     200MHz PLL0 as system clock ******************************************************************************** Revision History: 1.0     Oct-19-2015     Peter Vlna   Initial Version 1.1    Nov-11-2015    Peter Vlna   Added PPL0 200MHz as system clock 1.2    Dec-02-2015    Peter Vlna  Added Flash controller init 1.3    Dec-02-2015    Peter Vlna  Fixed system clock init 1.4    Feb-07-2017    Peter Vlna  SWT0 and SWT1 disabled in startup 1.5     May-31-2017    Peter Vlna  Fixed comments in AC6 (CLKOUT) 1.6     Oct-04-2017    Peter Vlna  Added PIT + Interrupts 1.7    Oct-05-2017    Peter Vlna  FCCU EOUT test in Alarm state with SMC *******************************************************************************/
查看全文
This example contains On-line BIST configuration for MPC5746R in GreenHills compiler. For more details refer to application note AN5427 * ------------------------------------------------------------------------------ * Test HW:  MPC57xx * Maskset:  1N83M (cut 2.0B) * Target :  internal_FLASH * Fsys:     200MHz PLL0 as system clock ******************************************************************************** Revision History: 1.0     Oct-19-2015     b21190(Vlna Peter)  Initial Version 1.1    Nov-11-2015    b21190(Vlna Peter)  Added PPL0 200MHz as system clock 1.2    Dec-02-2015    b21190(Vlna Peter)  Added Flash controller init 1.3     May-24-2016    nxa13250(Vlna Peter)Added Online BIST *******************************************************************************/* ------------------------------------------------------------------------------ * Test HW:  MPC57xx * Maskset:  1N83M (cut 2.0B) * Target :  internal_FLASH * Fsys:     200MHz PLL0 as system clock ******************************************************************************** Revision History: 1.0     Oct-19-2015     b21190(Vlna Peter)  Initial Version 1.1    Nov-11-2015    b21190(Vlna Peter)  Added PPL0 200MHz as system clock 1.2    Dec-02-2015    b21190(Vlna Peter)  Added Flash controller init 1.3     May-24-2016    nxa13250(Vlna Peter)Added Online BIST *******************************************************************************/
查看全文
******************************************************************************** * Detailed Description: * * Configures the FlexCANs to transmit and receive a CAN FD message with or without * bit rate switching for data phase. * Baudrate during arbitration phase is set to 500kbps, during data phase 2Mpbs. * * In this config, CAN_0 transmits a message. CAN_1 receives the message. * * EVB connection: * * CAN0-CANH on P15-1 to CAN1-CANH on P14-1 * CAN0-CANL on P15-2 to CAN1-CANL on P14-2 * * NOTE! Termination resistor (120Ohm) have to be placed on transceivers output * * ------------------------------------------------------------------------------ * Test HW:  X-MPC574xG-324DS + X-MPC574XG-MB * Maskset:  1N81M * Target :  FLASH * Fsys:     160 MHz PLL * ********************************************************************************
查看全文
******************************************************************************** * Detailed Description: * Read attached document "How to use Register Protection on MPC5748G.pdf" * for detailed explanation. * This example shows how to lock and unlock register MC_ME.RUN_MC[3].R. * One option is to write directly to memory via pointers, second option is * to use macros from header file reg_prot.h. * ------------------------------------------------------------------------------ * Test HW:         MPC574XG-324DS Rev.A + MPC574XG-MB Rev.C * MCU:             PPC5748GMMN6A 1N81M * Fsys:            160 MHz PLL * Debugger:        Lauterbach Trace32 * Target:          internal_FLASH * ********************************************************************************
查看全文