MCUXpresso Config Tools Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso Config Tools Knowledge Base

Labels

Discussions

Sort by:
This paper describes using a simple audio DAC (Digital to Analog Converter) with the LPC54114 board. As the processor offers hardware I2S interface, TDA1543, a widely available low-cost 16-bit I2S DAC, is used. This tutorial describes the steps of connecting it and preparing a code for using TDA1543 in your application with leveraging MCUXpresso tools and SDK. Prerequisites MCUXpresso IDE 11.3 MCUXpresso SDK for LPCXpresso54114 version 2.9.x (use https://mcuxpresso.nxp.com) For testing on hardware: LPCXpresso54114 board, TDA1543, and related parts (see below) Hardware TDA1543 is a 16-bit DAC with stereo output. It is available in an 8-pin DIP package with 3 digital input signals. It can operate with a minimum of external parts. The following diagram shows a simple testing circuit used for this project to get an analog audio line output. This schematic can be easily wired using a breadboard. Figure 1. Schematic of an elementary audio output DAC using TDA1543 Connection and pin configuration The DAC uses the standard I2S interface which is a serial bus that consists of 3 signals: Clocks (in the nomenclature of our MCU it is the SCK signal), WS (Word select – indicating left or right channel), and DATA (serial data synchronized by the clock signal). MCUXpresso Config Tools provide the Pins tool that can be leveraged for finding appropriate pins for the connection and routing them. Steps: 1. Create a project for the LPCXpresso54114 board. If you need, you can find detailed instructions in this video. (https://www.nxp.com/design/training/basic-application-development-using-mcuxpresso-ide-and-mcuxpresso-config-tools:TIP-BASIC-APP-DEV-MCUXPRESSO-IDE-TOOLS) Hint: Ensure you select the appropriate board:  2. Open the Pins tool. You can use the tools' Menu button in the Project panel:          NOTE: Ensure you have selected the appropriate project when multiple projects are in the workspace. 3. Open the Peripheral signals view and unfold Flexcom7          NOTE: LPC 54114 MCU provides 8 instances of the Flexcomm communication peripheral that can be flexibly set for UART, SPI, I2C, but only Flexcomm6 and Flexcomm7 provide I2S interface. This tutorial uses Flexcomm7.          NOTE: I2S signals are marked red. FlexComm5 (and lower) do not offer I2S signals. 4. Check the RXD_SDA_MOSI_DATA pin. In the dialog for routing, select which pin you would like to route the signal to. This tutorial uses pin 27 Tip: Find which expansion header connector and pin the processor pin is connected to in the tooltip of each pin:   5. Repeat steps 3 and 4 for SCK and WS signals. SCK – pin 26 (connected to J1[14])  WS – pin 28 (connected to J1[12] and J9[6]) 6. In the Routing details view, set the mode of all signals to Inactive (it disables internal pull-up). Configuring I 2 S in the Peripherals tool Using the Peripherals tool, generate the initialization code for the Flexcomm I 2 S SDK driver that is used for communication with TDA1543. Steps 7. In the Peripherals tool, open the Peripherals view and check Flexcomm7 8. Select the I 2 S configuration component (category Peripheral driver). 9. The Problems view shows an error.  The FLEXCOMM driver is not present in the project. Right-click the error and select the action Add SDK component "FLEXCOMM Driver" into the project In the shown SDK Component Management dialog box, confirm the addition of the files by clicking the Yes button. 10. In the added configuration component, set up the following items: The Custom name checkbox is checked,  the Name: ‘CODEC’ Mode: Transfer (Note: Transfer mode is easy to use and provides asynchronous operation) Sample rate: 24000 Hz Transfer Configuration / Transfer functions setting / Buffer size in bytes: 32           11. The Bit clock source frequency shows an error as the clocks of Flexcom7 are not enabled (inactive).           Right-click the “bulb” icon offering possible fixes for the problem. Select the error message FXCOM7 clock is inactive and select the action Show problem in BOARD_BootClockHSRUN, which is the name of the functional group in the Clocks tool. It opens the Clocks tool and highlights the FXCOMCLK7 clock output related to                             Flexcomm7:     Configuring clocks For correct communication, enable and configure clocks for the Flexcomm7 interface. Steps 12. In the Path Details view (for FXCOM7 clock), set the FXCOM7 clock select to FRG clock, the output of…             NOTE: FRG is a Fractional Rate Generator allowing to provide non-integer ratios for clock frequencies. 13. Set the FRG clock select to FRO 12.               The clock path and frequencies are automatically updated. 14. Switch back to the Peripherals tool using the icon in the toolbar.   15. The bit clock source frequency is now 12000000 Hz and it shows a warning because it does not match a value suitable for producing the required bit clock. The nearest bit clock source frequencies show potential suitable values. Copy the first one            (11520000) to the clipboard and switch back to the Clocks tool. 16. Paste the value into the FXCOM7 clock value column and add ‘Hz’ units; otherwise, it is treated as currently used MHz.    17. An error is reported. The Clocks tool cannot satisfy the requirement, so change the accuracy to a higher value. Set it to 0.5 (which corresponds to 0.5 %): Now the requirement is satisfied (producing 11.54 instead of 11.52 MHz): Code 18. Update the generated code into the project by using the Update Code button.  Confirm the update by clicking OK in the shown dialog. 19. Add the code into the main module (stored in the Sources folder of the MCUXpresso IDE project): /* TODO: insert other definitions and declarations here. */ #define BUF_SIZE 32 // Example wave data for transfer, odd numbers are left channel, even numbers are right channel const uint16_t wave[32] = {                      0,2000,4000,6000,8000,10000,12000,14000,                      16000,18000,20000,22000,24000,26000,28000,30000, }; // I2S callback function volatile void CodecTx(I2S_Type *base, i2s_handle_t *handle, status_t completionStatus, void *userData) {     /* Enqueue the same original s_Buffer all over again */     //i2s_transfer_t *transfer = (i2s_transfer_t *)userData;     I2S_TxTransferNonBlocking(base, handle, CODEC_Tx_Transfer); } Add the following code after the existing hello world PRINTF:         PRINTF("Hello World\n");         // prepare data into the buffer         memcpy(CODEC_Tx_Buffer, wave, 32);        // Start transfer        I2S_TxTransferNonBlocking(CODEC_PERIPHERAL, &CODEC_Tx_handle, CODEC_Tx_Transfer); Testing on hardware You can test the application on the LPC54114 evaluation board with a connected DAC chip. Figure 2. DAC circuit wired with the evaluation board The output checked using the sound-card input of a PC has the following result. It corresponds to the expectations: Figure 3. Waveform measured at the output of the circuit  
View full article
Description This tutorial shows how to create a touch-controlled LED light strip to place it over the kitchen counter, for example. For this tutorial, the LED strip is abstracted by the onboard LED instead of using MOSFET (with a proper MOSFET driver circuit) that would control a higher voltage LED strip. The touch control must be encoded due to the presence of only a single touch pad for multiple actions. Used components LPCXpresso845-BRK breakout board SDK 2.8.0 for LPC845 MCUXpresso 11.3 Used peripherals CAPT Capacitive touch (CAPT) control allows you to place the button under the product cover for keeping the design of the product consistent. You can cover touch pads with dielectric materials and hide them inside the product. The CAPT peripheral in YH mode works by counting cycles until the charge is transferred from the small charging capacitor to the larger measuring one.  A human finger or capacitive stylus causes partial grounding of the charge that causes an increase or decrease of the cycles needed to fully charge the measuring capacitor. CTIMER A counter triggers a toggle of the output pin’s logic level that creates a PWM signal on that pin. The peripheral increases the counter with each peripheral clock cycle and when the counter matches the required number the output logic level is toggled. MRT A counter triggers interrupts after a defined number of peripheral clock cycles.  This peripheral can be programmed to create an interrupt repetitively or only after a specified number of cycles. Figure 1 Block diagram Touch control Description As mentioned previously, the board has only a single touch pad, and there are 3 different actions in this tutorial that must be controlled by it. Turn on/off the PWM output by tapping and removing the finger/stylus from the pad. Increase the PWM duty cycle by keeping the finger/stylus over the touch pad for a long time, keep touched for more increase. Decrease the PWM duty cycle by taping the touch pad, removing the finger, and taping again with keeping the finger/stylus over the touch pad, keep touched for more decrease. The touch pad is periodically measured for touch or no touch events. Such events can store the state of the touch pad in a ring buffer. The ring buffer represents the history of the touches over a short time and can be analyzed for a long uninterrupted touch or double tap. Figure 2 Encoding state diagram Steps IDE project Create a project and select the lpc845 breakout from your installed SDK version. Figure 3 Creating a project in MCUXpresso IDE In the project setup wizard, click the Drivers tab in the Components section in the lower half of the wizard. Select CAPT, CTIMER, and MRT in this table. Figure 4 Adding required peripheral drivers to the project To make active the newly created project (if it is not active yet), select it and open the Pins tool either in the context menu or by clicking the Config tools button. Figure 5 The Config tools button Pin routing Open the Pins tool and create a functional group for our application. Set it to be called by the default initialization function and set other functional groups not to be called by the initialization function. Figure 6  Properties of Pins tool functional groups Figure 7 Routing details Steps: Route CTIMER channel 0 to the pin that is connected to the onboard LED. Route X0 signal of CAPT to one side of the touch pad. Route signals YL and YH to the other side of the touch pad. Enable the invert function of the CTIMER channel 0 signal (see notes). Set the mode of all configured CAPT and CTIMER pins to Inactive (see notes). NOTE: The LED is connected to the MCU in a way that 90 % of the duty cycle would create only 10 % of the on-time.  To achieve the expected behavior, invert the signal. The CAPT peripheral requires the mode of the pins to be inactive to work properly. Activating a pull-up, pull-down resistor, or any other integrated circuit causes false measurements, and touch control does not work or causes false touch events. Clock configuration Open the functional group's dialog and select BOARD_BootClockFRO30M as the initialized functional group. Figure 8 Properties of Clocks tool functional groups Steps: Set SYSAHBCLKDIV to /3 Activate the output of CAPTCLKSEL and choose fro as the input clock Figure 9 System clock divider setting Figure 10 Selection of clock source for CAPT peripheral NOTE: The system clock is slowed down to 10 MHz because it is used for the MRT peripheral as a source and the period with 30 MHz is too short for the purposes of this tutorial. Peripheral configuration MRT This peripheral is used to delay the execution of events. Steps: Add the MRT component (use the version that is part of your SDK version). Add 1 channel. Set Channel ID to Channel_wait. Set Time interval input to 400 ms. Set Start timer to false by unchecking the checkbox. Enable Interrupt request of the channel by checking the checkbox. Enable Interrupt vector by checking the checkbox. Copy the handler template by clicking the button. Paste the handler template to the application code. Figure 11 Configuration of the MRT peripheral NOTE: For this application, the delay must be 400 ms. You can achieve it only by using a 10 MHz clock or by creating a counter in memory that is increased every time the interrupt handler is executed. Only when the counter has the required value, the delayed event executes, and the counter is reset. You need a counter because the MRT register, which has only 24 bits and overflows before reaching the number of ticks calculated from 400 ms. CTIMER For the PWM output, configure the CTIMER peripheral in the following way. Figure 12 Configuration of the CTIMER peripheral Steps: Add the CTIMER component (use the version that is part of your SDK version). Select the PWM mode of the CTIMER peripheral. Set the prescaler to 1 (see note for explanation). Check the checkbox Start timer in the initialization code if it is not checked already. Set the PWM frequency to 100 Hz (see note for explanation). Add 1 channel if it is not present already. Set the PWM duty of the channel to half of the value that is displayed below the PWM frequency setting notes: NOTE: The prescaler set to 1 (no prescaling) allows the most precise duty cycle (for example, if the resolution must be more than one percent).  The frequency of the output must be in the range between not noticing the flickering of the LED and potential unintentional overheating of the MOSFET that could be connected to the output due to high frequency. The frequency of 100 Hz is selected because unless the board is moving the LED looks dim and does not flicker, and the potential MOSFET does not overheat. The duty cycle is set in ticks, and at runtime is computed as a percentage. CAPT Steps: Create an instance of the CAPT component (use the version that is part of your SDK version). Set the Function clock divider setting to 15 to obtain a 2 MHz clock. Enable pin 0 by checking the checkbox in the X pins selection table. Select the value User calibration function (default name) in the setting Default function name. Copy the name and create the function in the application code. Select Counter higher than threshold could in the setting Touch activation. Set Time out count to the highest available value. Select Don’t wait for Measurement delay. Set Reset delay to the highest available value. Set Poll delay to 100 ms. Check the checkbox Initialize poll mode. Select Continuous in the setting Polling mode. Figure 13 Configuration of the CAPT peripheral NOTE: The CAPT peripheral requires the input clock to be maximally 4 MHz. Therefore, a frequency of 2 MHz was chosen as it was easily achievable and easy to calculate the resulting period. On the breakout board, only signal 0 is routed to the touch pad, and other signals can be routed to external connectors on the board. For the CAPT to function properly, calibrate touch and no touch events to obtain the number of cycles required to transfer the charge. Enable the usage of the calibration method and either use the default name or provide your name of the function. The other method is to use a constant that was measured during development. However, keep in mind that the measured value might differ when the board is inside the final product and covered by a layer of material. A touch event can happen either when the counter is higher or lower than the threshold. The selection depends on the final product design. A value higher than the threshold option was used in this tutorial because the finder/stylus grounds a part of the charge that is transferred and causes a higher cycles count required to fully charge the measured capacitor. The timeout count is a counter of the number of ticks when a timeout interrupt is created. It is not used in this example, so set the highest value to avoid timeout instead of touch or no touch events. The measurement delay setting represents the number of ticks until the measuring capacitor is sampled. When the YH method is used, it must be measured immediately. The reset delay is a wait after a touch or no touch event and waiting discharges the capacitors before the next measurement cycle. The poll delay is a delay between repetitive measurement cycles and should be high since the physical movement of the finger/stylus is slow relative to the speed of the MCU and unnecessary measurements can be avoided. Update code The changes you made must be written on the disk before using them in the application code. Open the Update code dialog and confirm the changes. Figure 14 Update code action on the main panel Figure 15 Update code dialog Application code For the convenience of working with the code, create the following defines: #define WAIT_MS 400U // How long to wait before making decisions #define POLL_WAIT_MS 100U // How long it takes before next CAPT measurement #define TOUCH_DATA_SIZE 32U // Size of ring buffer Create the ring buffer, index of the current position, and functions that fill and analyze it. The ring buffer must hold 2-3 seconds of data and since the poll delay of the CAPT is 100 ms then 32 is sufficient. Functions for analysis scan the ring buffer and let the application know whether a double tap was performed, for how many measurements the touch pad was held, and how many measurements ago the touch pad was touched. Create functions for storing and clearing data in the ring buffer. unsigned int g_touchDataIndex = 0; bool g_touchData[TOUCH_DATA_SIZE] = {false}; /**  * Checks whether double tap was performed  */ bool wasDoubleTap() {        bool untouched = false;        for (int i = 0; i < TOUCH_DATA_SIZE; i++) {               if (!g_touchData[(g_touchDataIndex - i) % TOUCH_DATA_SIZE]) {                      untouched = true;               } else if (untouched) {                      return true;               }        }        return false; } /**  * Returns number of data writes that represent continuous touch.  */ int getContinuousTouchCount() {        int count = 0;        for (int i = 0; i < TOUCH_DATA_SIZE; i++) {               if (g_touchData[(g_touchDataIndex - i) % TOUCH_DATA_SIZE]) {                      count++;               } else {                      return count;               }        }        return -1; } /**  * Returns number that represents count of data writes until tap is found in history.  * Returns -1 in case nothing is found.  */ int getPreviousTouch() {        for (int i = 0; i < TOUCH_DATA_SIZE; i++) {               if (g_touchData[(g_touchDataIndex - i) % TOUCH_DATA_SIZE]) {                      return i;               }        }        return -1; } /**  * Clears touch data in ring buffer  */ void clearTouchData() {        for (int i = 0; i < TOUCH_DATA_SIZE; i++) {               g_touchData[(g_touchDataIndex - i) % TOUCH_DATA_SIZE] = false;        } } /**  * Stores touch data in ring buffer  */ void storeTouchData(bool data) {        ++g_touchDataIndex;        g_touchDataIndex = g_touchDataIndex % TOUCH_DATA_SIZE;        g_touchData[g_touchDataIndex] = data; } Create storage for the current state of the PWM signal and the state machine. Create a function to change the PWM output of the CTIMER channel.  The function must check the wanted duty cycle to be in a reasonable range. int currentPWMDuty = 50; bool PWMOutputEnabled = true; enum STATE {        IDLE = 0,        WAITING_FOR_TIMER = 100,        TOGGLE = 200,        INCREASE = 300,        DECREASE = 400 }; enum STATE state = IDLE; /**  * Sets PWM output according to currently wanted duty cycle if output is enabled  */ void setPWMOutput() {        if (currentPWMDuty < 5) {               currentPWMDuty = 5;        }        if (currentPWMDuty > 100) {               currentPWMDuty = 100;        }        int ticks = PWMOutputEnabled ? ((CTIMER0_PWM_PERIOD / 100) * currentPWMDuty) : 0;        CTIMER_SetupPwmPeriod(CTIMER0_PERIPHERAL, CTIMER0_PWM_0_CHANNEL, CTIMER0_PWM_PERIOD, ticks, false); } Calibration of the CAPT peripheral must be done in the CAPT_doCalibration function as it was set in the Peripherals tool. /*  * @brief   Calibration of the CAPT peripheral. Returns number of charge cycles in not activated state  */ uint32_t CAPT_doCalibration(CAPT_Type *base) {        // Here can be placed code that uses one time polling multiple times and the results would be averaged        // or a constant returned        return 70; } When a 400 ms delay passes,  the MRT peripheral runs this interrupt and after clearing the status flag the logic follows. After obtaining information on whether the touch pad is touched and for how many measurement cycles it is not held, the decision of what state follows is made. When the touch pad is not touched and it is more than or equal to 4 (400 ms/100 ms) measurement cycles, the PWM output will be disabled. If it is touched, the decision whether the INCREASE or DECREASE state should follow is made. To increase the PWM duty cycle, the touch pad must be currently held touched, it must be held for more than or equal to 4 (400 ms/100 ms) measurement cycles and the PWM output must be enabled. To decrease the PWM duty cycle, the touch pad must be held,  double-tap (not holding for at least one measurement cycle) is done and output is enabled. In all other cases, the state falls back to IDLE since it is not a valid encoding of the command. /* MRT0_IRQn interrupt handler */ void MRT0_IRQHANDLER(void) {   /* Add for ARM errata 838869, affects Cortex-M4, Cortex-M4F      Store immediate overlapping exception return operation might vector to incorrect interrupt. */   #if defined __CORTEX_M && (__CORTEX_M == 4U)     __DSB();   #endif        uint32_t mrtWaitStatus = MRT_GetStatusFlags(MRT0, MRT0_CHANNEL_WAIT);        MRT_ClearStatusFlags(MRT0, MRT0_CHANNEL_WAIT, mrtWaitStatus);     if (mrtWaitStatus != 0) {               int previousTouch = getPreviousTouch();               bool currentlyTouched = g_touchData[g_touchDataIndex];               if (!currentlyTouched && previousTouch >= (WAIT_MS / POLL_WAIT_MS) - 1) { // Tap, currently not pressed and no taps after the initial one                      PWMOutputEnabled = !PWMOutputEnabled;                      setPWMOutput();                      clearTouchData();                      state = IDLE;           } else if (currentlyTouched && getContinuousTouchCount() >= (WAIT_MS / POLL_WAIT_MS) && PWMOutputEnabled) { // Tap, currently pressed and touch pad held until now                      state = INCREASE;        } else if (currentlyTouched && wasDoubleTap() && PWMOutputEnabled) { // Tap, currently pressed and double tap was performed                           state = DECREASE;           } else {                           state = IDLE; // Error -> reset           }     } } The interrupt from CAPT is performed every 100 ms and the data with interrupt status must be read and status cleared. When the touch pad is touched, the current state is checked and one of the following actions happens: When the current state is IDLE, a 400 ms delay is started and the state changes to WAITING_FOR_TIMER. When the INCREASE state is active, the PWM duty cycle is increased every 100 ms for as long as the touch pad is touched. The DECREASE state decreases the PWM duty cycle every 100 ms for as long as the touch pad is touched. When the touch pad is not touched, the INCREASE or DECREASE state is changed to IDLE state and ring buffer is cleared. In other states nothing happens. /* CMP_CAPT_IRQn interrupt handler */ void CAPT_IRQHANDLER(void) {   /* Add for ARM errata 838869, affects Cortex-M4, Cortex-M4F      Store immediate overlapping exception return operation might vector to incorrect interrupt. */   #if defined __CORTEX_M && (__CORTEX_M == 4U)     __DSB();   #endif     uint32_t mask;     capt_touch_data_t g_data;        CAPT_GetTouchData(CAPT, &g_data);        mask = CAPT_GetInterruptStatusFlags(CAPT);        CAPT_ClearInterruptStatusFlags(CAPT, mask);        if (mask & kCAPT_InterruptOfYesTouchEnable && g_data.yesTouch)        {               PRINTF("Touch\n");               storeTouchData(true);               switch(state) {                      case IDLE: {                            MRT_StartTimer(MRT0, MRT0_CHANNEL_WAIT, MRT0_CHANNEL_WAIT_TICKS);                            state = WAITING_FOR_TIMER;                            break;                      }                      case INCREASE: {                            currentPWMDuty += 5;                            setPWMOutput();                            break;                      }                      case DECREASE: {                            currentPWMDuty -= 5;                            setPWMOutput();                            break;                      }                      default: {                            // Do not react - unexpected state                      }               }        }        if (mask & kCAPT_InterruptOfNoTouchEnable) {               PRINTF("No touch\n");               storeTouchData(false);               switch(state) {                      case INCREASE: {                            state = IDLE;                            clearTouchData();                            break;                      }                      case DECREASE: {                            state = IDLE;                            clearTouchData();                            break;                      }                      default: {                            // Do not react - unexpected state                      }               }        } } /*  * @brief   Application entry point.  */ int main(void) {     /* Init board hardware. */     BOARD_InitBootPins();     BOARD_InitBootClocks();     BOARD_InitBootPeripherals(); #ifndef BOARD_INIT_DEBUG_CONSOLE_PERIPHERAL     /* Init FSL debug console. */     BOARD_InitDebugConsole(); #endif     while(1) {           __asm__("nop");     }     return 0; } Summary Now you can compile the application and upload it to the board. You do not require additional steps to make the application work.
View full article
Measuring temperature using digital sensor DS18B20 and Arduino Multifunction Shield on FRDM K64F  This tutorial describes a simple application for measuring temperature using the digital sensor DS18B20 and the Arduino Multifunction Shield connected to FRDM K64F. You can use new feature Expansion Boards (expansion shields) included in the Pins tool v9. This feature enables quick integration of shields in an application without the need to study manuals. In this paper, you can find the environment setup, 1-wire protocol basics, and the steps of preparing a code with MCUXpresso tools (Peripherals and Pins tool). Setup environment Install MCUXpresso IDE v11.3.0 or later and SDK FRDM-K64F 2.8.2 or later. Use the FRDM K64F EVK board https://www.nxp.com/webapp/Download?colCode=FRDMK64FUG. Connect the Arduino Multifunction shield (Expansion Board) to the FRDM K64F EVK board and DS18B20 to the Arduino shield. Connect the EVK board to the PC via a USB cable. Figure 1 FRDM K64F EVK board with Arduino Multi-Function shield Have the expansion board definition file arduino_multifunction_ds18b20.xml. For detailed instructions on how to create the expansion board see the following article: Creating expansion board definition file for Arduino Multifunction shield DS18B20 Programmable Resolution 1-Wire Digital Thermometer See the documentation https://datasheets.maximintegrated.com/en/ds/DS18B20.pdf This tutorial uses powering with an external supply. Figure 2 Powering the DS18B20 with an External Supply   See the timing diagrams for communication with the DS18B20, needed for writing 1-Wire communication protocol. Figure 3 Initialization Timing Figure 4 Read/Write Time Slot Timing Diagram The application only uses the following 1-wire protocol commands: ‘CCh’ skip ROM command - only one slave on the bus supported ’44h’ convert temperature ‘BEh’ read DS18B20 registers (temperature) Create the application in MCUXpresso IDE Begin with the hello_word example from SDK, rename the project to frdmk64_termometer. Steps to configure timer in the Peripherals tool: Go to the Peripherals tool and add/configure the PIT component. Resolve the new Error in Problems view by adding the SDK component to the project. Figure 5 PIT component in the Peripherals tool Steps to apply the expansion board and configure pin in Pins tool: Apply the expansion board (arduino_multifunction_ds18b20.xml) from menu Pins -> Apply Expansion Board menu    Figure 6 Apply expansion board dialog The Expansion Board Routing dialog is automatically opened after step 1. It provides the possibility to route signals to processor pins that are connected to the expansion board. By default, all pins are routed automatically, see below. Keep only pin A4 routed which is needed for our thermometer application. Unroute the unneeded pins by clicking the Route column or later in the Routing Details view, then click Apply.   Figure 7 Expansion board routing dialog  The action results in the following setting. When selecting Expansion board in the Labels combo, you see the labels as they are marked on the Arduino shield.  Figure 8 Expansion header view In the Routing Details view, set the electrical properties of the pin (Direction, Pull select, Pull enable). Figure 9 Electrical properties in the Routing Details view Click Update Code to update the project with the code generated by the tools. Write the thermometer application and 1-wire protocol (thermometer.c)   Rename the source file hello_world.c to thermometer.c and follow the steps below. Find the completed thermometer.c in the project.  Use the PIT timer to create methods delayMS() and delayUS() for delays of μs and ms. See the PIT interrupt handler PIT_CHANNEL_0_IRQHANDLER() function.   Write methods GPIO_low() and GPIO_high() to set the ARDUINO_A4_PIN to logical 0 and 1. These methods are based on the code which is in the screenshot below. Figure 10 Generated code for ARDUINO_A4_PIN Write methods for reading/writing bytes to the 1-wire bus. Figure 11 Methods for reading/writing bytes Write methods to request the temperature conversion and read the temperature, see dsRequestConvertTemp() and dsReadTemp(). Finally, use the methods in main().   Build the project and start debugging. Figure 12 Output from the application
View full article
Creating expansion board definition file for Arduino Multifunction shield  An expansion board definition file for the Arduino Multifunction shield can be applied in Pins Tool to expansion headers available on the NXP board. This tutorial describes the steps of creating an XML expansion board file using the shield documentation and the expansion headers feature in the Pins tool. For details on the expansion headers feature, see the following article: Adding Expansion Headers to a custom board You can apply the Arduino Multifunction shield on several NXP boards. This tutorial uses the FRDM K64F EVK board.   Prerequisites: Use a  shield description/specification, for example, https://www.biomaker.org/multifunction-shields. You can use HAILANGNIAO Multi-Function shield V2. Use the XSD schema file https://mcuxpresso.nxp.com/XSD/expansion_board_1.0.xsd for the definition file validation. Use the definition of signal types - mapping of signals from the expansion board to the processor. You can find it in the Config Tools data directory: c:\ProgramData\NXP\mcu_data_{config_tools_version}\expansion_headers\signal_types\common_signal_types.xml. Use the definition of expansion header where the board can be applied: c:\ProgramData\NXP\mcu_data_{config_tools_version}\expansion_headers\frdm_arduino.xml. Get familiarized with devices that are on the shield or can be connected to the shield. Install MCUXpresso IDE v11.3.0 or later and SDK FRDM-K64F 2.8.2 or later. Create a Project for FRDM-K64F. Open Expansion Header view (Windows -> Show View -> Expansion Header). Figure 1 FRDM K64F EVK board Figure 2 Expansion Header view in the Pins tool Expansion board template  Edit the following template according to the steps below. <?xml version="1.0" encoding= "UTF-8" ?> <expansion_board id="board_id" name="board_name" xsi:schemaLocation="http://mcuxpresso.nxp.com/XSD/expansion_board_1.0 http://mcuxpresso.nxp.com/XSD/expansion_board_1.0.xsd" xmlns="http://mcuxpresso.nxp.com/XSD/expansion_board_1.0" xmlns:xsi="http://www.w3.org/2001/XMLSchema-instance"> <header_connection ref="expansion_header_def_id"> <connectors> <connector ref="C1"> <pins> <pin ref="1" name="pin name" signal_type="digital_in" description="pin description"/> </pins> </connector> </connectors> </header_connection> <code_identifiers prefix="ARDUINO_"/> </expansion_board> Expansion board id and name  Edit the id and name of the expansion board. <?xml version="1.0" encoding= "UTF-8" ?> <expansion_board id="arduino_multifunction_ds18b20_board" name="Arduino Multi DS18B20 board" xsi:schemaLocation="http://mcuxpresso.nxp.com/XSD/expansion_board_1.0 http://mcuxpresso.nxp.com/XSD/expansion_board_1.0.xsd" xmlns="http://mcuxpresso.nxp.com/XSD/expansion_board_1.0" xmlns:xsi="http://www.w3.org/2001/XMLSchema-instance"> Expansion board - header connection The element header_connection determines the id of an expansion header where the board can be applied to. Get the type of expansion header in the FRDM-K64F board. Figure 3 Edit expansion header dialog Edit the header_connection in the expansion board XML. <?xml version="1.0" encoding= "UTF-8" ?> <expansion_board id="arduino_multifunction_ds18b20_board" name="Arduino Multi DS18B20 board" xsi:schemaLocation="http://mcuxpresso.nxp.com/XSD/expansion_board_1.0 http://mcuxpresso.nxp.com/XSD/expansion_board_1.0.xsd" xmlns="http://mcuxpresso.nxp.com/XSD/expansion_board_1.0" xmlns:xsi="http://www.w3.org/2001/XMLSchema-instance"> <header_connection ref="frdm_arduino">​ NOTE Some other NXP boards can provide a  single row Arduino expansion header, for example, MIMXRT1060-EVK. For these boards,  create the definition file based on the single_row_arduino expansion header. The definition file varies only in pin references. Expansion board pins The tutorial describes how to add a pin element within the connector elements in three examples. See the marked pins on the shield below. Figure 4 Arduino Multi-Function shield Pin 5V (Power supply +5V) Get the needed pin element attributes values Find the board pin in the expansion header view. The pin tooltip shows connector J3 pin 10. The connector tooltip shows the definition id for J3, which is C1. Figure 5 Connector pin and connector tooltips in the Expansion header view Pin 5V is an external pin from the processor point of view (not connected to the processor). In the common_signal_types.xml, find a suitable signal type. Add the element pin with reference 10, name on the shield 5V, signal type power_supply_5V, and the description in the connector C1. <connector ref="C1"> <pins> <pin ref="10" name="5V" signal_type="power_supply_5V" description="Power supply +5V"/>​ Pin 13 (LED - D1) Get the needed pin element attributes values Find the board pin in the expansion header view. The pin tooltip shows connector J2 pin 12. The connector tooltip shows the definition id for J2, which is C2. Figure 6 Connector pin and connector tooltips in the Expansion header view Pin 13 is connected to LED D1 on the shield. It is digital input from the shield point of view, it is output from the processor point of view. In the common_signal_types.xml, find a suitable signal type. Add the element pin with reference 12, name on the shield 13, signal type digital_in, and the description in the connector C2. <connector ref="C2"> <pins> <pin ref="12" name="13" signal_type="digital_in" description="LED - D1"/>​ Pin A4 (Thermometer DS18B20 or LM35 - U5) Pin A4 is connected to the header U5 on the shield where two different external thermometers can be applied. The definition file you create is the variant for DS18B20. See the documentation for DS18B20: https://datasheets.maximintegrated.com/en/ds/DS18B20.pdf  Get the needed pin element attributes values Find the board pin in the expansion header view. The pin tooltip shows connector J4 pin 10. The connector tooltip shows the definition id for J4, which is C4. Figure 7 Connector pin and connector tooltips in the Expansion header view Pin A4 is connected to DS18B20 DQ pin which is Data Input/Output. In the common_signal_types.xml, find a suitable signal type.   Add the element pin with reference 10, name on the shield A4, signal type digital, and the description in the connector C4. <connector ref="C4"> <pins> <pin ref="10" name="A4" signal_type="digital" description="Thermometer DS18B20 or LM35 - U5"/>​   See the complete expansion board definition file arduino_multifunction_ds18b20.xml and arduino_single_multifunction_ds18b20.xml in the CreateExpansionBoardFile.zip. For information on the usage of this created board file see the following article: Measuring temperature using digital sensor DS18B20 and Arduino Multifunction Shield on FRDM K64F
View full article
LPC55Sxx: Securing Digital IO Pins  This tutorial explains why you must secure digital IO pins and how to utilize MCUXpresso Config Tools. Risk of Secure information leakage  GPIO (General Purpose Input Output) is the most common digital peripheral in a microcontroller. GPIO of LPC MCU is very flexible and powerful.  Below you can see a simple block diagram of  GPIO (Figure 1).  GPIO can read a pin state regardless of the pin function configured. For example, if this pin is configured as UART, then the pin state can be read via a  GPIO read.[1] Figure 1 GPIO [1]  Due to the architecture of GPIO, all digital IO pins states are readable through the GPIO module from the GPIO read path. It does not depend on what function is chosen for this pin as aforementioned. As a result, there is a possibility of information leakage from a Secure resource (S).   For example, when you configure a UART as a Secure peripheral, it means that only the Secure world can access this UART.  However, in this case, the Non-Secure world can monitor the UART pin states through the GPIO read path as shown in Figure 1. Hence, the Non-Secure world can get all the Secure information from the UART.[1]  To prevent the leakage of information from the Secure world by GPIO, the Secure GPIO Mask is implemented on LPC55Sxx devices with TrustZone®.  This mask disallows the use of GPIO for a pin in both the Secure and the Non-Secure world. LPC55Sxx devices with TrustZone® implement a new NXP peripheral named Secure GPIO that can operate GPIO in the Secure world. Figure 2 Secure GPIO and Secure GPIO Mask [1]  Securing digital IO pins in MCUXpresso Config Tools  MCUXpresso Config Tools contain everything you need to create a Secure configuration. You can do a pins configuration in the Pins tool, configure peripherals in the Peripherals tool, enable clocks in the Clocks tool, and set up the Secure aspects in the Trusted Execution Environment (TEE) tool. Prerequisites  MCUXpresso IDE – v11.3.0 is used in this tutorial, LPCXpresso55S69 SDK – v2.9.0 is used in this tutorial, An application that uses TrustZone and Secure USART, LPCXpresso55S69 Development Board  Application setup  The project uses TrustZone.  FLEXCOMM0 is used as USART.  FLEXCOMM0 is configured as Secure in the TEE tool.  FLEXCOMM0 uses non-blocking transfer.  Reading digital IO state from the Non-Secure world  You can create a simple example to test that the Non-Secure world can access information from the Secure world by reading the state of a GPIO pin.  Assuming the Secure application uses FLEXCOMM0 to communicate and GPIO0.30 pin for TX signal, you can add a code to a Non-Secure application that can read the communication. To use GPIO macros from the example code, make sure the “board.h” header file of LPC55S69 board is added in the include section of the file. When you run the application, the Non-Secure world reads the state of the GPIO pin and changes the state of the blue LED accordingly. You can achieve it without any additional modification to a configuration generated by MCUXpresso Config Tools. There is no need to configure the pin to GPIO. It demonstrates that the state can be read from the Non-Secure world and communication is not Secure. Securing the pin in the TEE tool  Open MCUXpresso Config Tools for the Secure project.  In the example, pin 94 is used as TX pin of FLEXCOMM0 (See Figure 3) as shown in the picture of Pins view from the Pins tool below. The pin is shared with the GPIO0.30 signal. Figure 3 Digital IO pin configured in the Pins tool  Open the TEE tool to configure pin masking  (See Figure 4). Figure 4 Open the Pins tab in the TEE tool  When FLEXCOMM0 is Secure, the TEE tool reports a warning on the GPIO0.30 pin as there is a risk of Secure information leakage.   Change the value of the Reading GPIO state column from Allow to Deny.  To update project files with files generated from the MCUXpresso Config Tools, click the Update Code button. Initialization code generated for a trust zone configuration now masks the read of pin 94 using GPIO.  Verify that the pin cannot be read from the Non-Secure world  You can run the same example to verify that reading a state of the pin, that is routed to the FLEXCOMM0 TX signal, from the Non-Secure world always returns the same value. Running the application, you can see that the blue LED is not changing color based on the communication of the FLEXCOMM peripheral.    [1] 2020. AN12326: Secure GPIO And Usage. 1st ed. [ebook] NXP B.V. 2019, pp.3-4. Available at: <https://www.nxp.com/doc/AN12326> [Accessed 15 December 2020]. 
View full article
  A Digital Rights Management (DRM) use case   In the Creating Secure and Non-Secure projects tutorial, you have attempted to access a Secure (S) FlexComm0 (USART) peripheral from a Non-Secure (NS) code and failed with the SecureFault exception. This was expected, as TrustZone® for ARM®v8-M protects Secure resources from Non-Secure access.   Now imagine a use case where the platform manages (protects) access to all its peripherals and firmware logic and requires all 3 rd party extensions, for example plugins or widgets, to be certified (approved) for use. The result of this approval process is some form of identification, a license key for instance, the untrusted code needs to supply to the trusted code to gain peripheral access and be able to communicate via USART. This kind of behavior can be achieved with the help of Non-Secure Callable (NSC) memory.   NSC is a type of Secure memory exclusively permitted to hold the Secure Gateway (SG) instruction that allows transition from NS to S state. When a Non-Secure program calls a function in the Secure side, the first instruction in the API must be an SG instruction. The Branch with exchange to Non-secure state (BXNS) will return execution to the Non-Secure side after the API call. While it’s possible for NSC memory to contain entire functions, its typical usage is holding tables of SG instructions with entry points, called veneers.   With GCC, ARMCC, ARMCLANG, IARCC, and LLVM compilers, you must specify the __attribute__((cmse_nonsecure_entry)) function attribute to declare an entry C/C++ function callable from NS state; SG and BXNS instructions are generated automatically. GNU linker puts the resulting code into the .gnu.sgstubs section aligned at 32 bytes.   With the solution outlined, you can reuse projects from the “TEE projects creation” tutorial to speed things up. To extend an existing project with NSC functions, the workflow is as follows: Secure state Configure project and  SAU/IDAU Implement NSC functions Generate NSC library Non-Secure state Configure project (import NSC library) Implement calls for Secure code     S project update   Start with the Secure project conveniently named “Secure”. Reserve some flash memory space for SG_veneer_table first. Navigate to Project > Properties > C/C ++ Build. Locate the MCU settings in SDK MCUs. Click Add Flash and add SG_veneer_table at 0x1000fe00, size 0x200 bytes. Click Apply.   To tell the MCU Linker to generate the NSC import library, navigate to Project > Properties > C/C ++ Build > Settings > MCU Linker > TrustZone. Select the Enable generation of Secure Gateway Import Library checkbox. Click Apply and Close.   Now setup the newly added flash memory region as NSC in the TEE tool. To switch to the TEE tool, click the Open MCUXpresso Configuration button in the Project Explorer, and select Open TEE.   The TEE tool is capable of importing project-wide memory regions from multiple projects at once. To import memory regions, click the Import button in the User Memory Regions view.   In the Select Project dialog, select both NonSecure and Secure projects and click OK.   Quick-fix the reported error Issue: SAU+IDAU: The following security requirements are not satisfied: NS_CALLABLE by right-clicking the cell and selecting the quick-fix from the context menu.   To save the changes, click Update Code.   MCUXpresso IDE v11.3.0 and earlier versions contain a bug that messes up linker script and puts SG veneers into PROGRAM_FLASH instead of SG_veneer_table when you’re modifying an existing project. To work around the problem, navigate To Project > Properties > C/C ++ Build > Settings > MCU Linker > Managed Linker Script. Deselect the Manage linker script checkbox and click Apply and Close.   Edit the script manually by opening the Debug/Secure_Debug.ld inside the IDE, find the .gnu.sgstubs section and direct it to SG_veneer_table instead of PROGRAM_FLASH.         NS project update   If you attempt to build the S project now, you’ll receive several linker errors telling you the NSC library could not be built as there are no NSC functions (yet) including the name of the said library: Secure_CMSE_lib.o. You’re going to use it to configure the Non-Secure project named “Non-Secure”. Navigate to Project > Properties > C/C ++ Build > Settings > MCU Linker > TrustZone. Click the Import button next to the Secure Gateway Import Library field, and select Workspace.   In the Input Secure Gateway Import Library dialog, select Secure_CMSE_lib.o and click OK.   You will see “${workspace_loc:/Secure/Debug/Secure_CMSE_lib.o}” in the Secure Gateway Import Library field of the MCU Linker Setting dialog.     NSC API   The source/Secure.c file already contains the sendSecureByte function implementation you need to make accessible through the NSC space. What’s missing is a few lines of code for its NSC equivalent and function prototype. Create source/nsc_api.h and source/nsc_api.c files in the Secure project workspace. The following code needs go into the newly created header file. #ifndef NSC_API_H_ #define NSC_API_H_ #include <stdint.h> void sendSecureByteNSC(uint8_t data); #endif /* NSC_API_H_ */ Add the following code into the source file. #include <arm_cmse.h> #include "fsl_debug_console.h" #include "nsc_api.h" #include "comm.h" void __attribute__((cmse_nonsecure_entry)) sendSecureByteNSC(uint8_t data) { if (cmse_nonsecure_caller()) { PRINTF("sendSecureByteNSC called from NS space\r\n"); } else { PRINTF("sendSecureByteNSC called from S space\r\n"); } sendSecureByte(data); } To rebuild the Secure project and generate the NSC import library click the Build ‘Debug’ for project ‘Secure’ button in the Toolbar.   Next in line is the Non-Secure project. The NSC library is already set to be imported. Copy Secure/source/nsc_api.h to the NonSecure/source folder. Call the sendSecureByteNSC function instead of USART_WriteByte from source/NonSecure.c. #include "nsc_api.h" …                   USART_WriteByte((USART_Type *)FLEXCOMM0, 'n'); sendSecureByteNSC('n'); Rebuild the Non-Secure project and debug both. Select the Secure project in the workspace and select Debug either from the Quickstart panel or the project context menu. Once the code is running, each press of the WAKEUP (S2) button on the LPCXpresso55S69 board will display the “sendSecureByteNSC called from NS space” message in the IDE console and send a single character via USART instead of failing with the SecureFault exception.    
View full article
Creating Secure and Non-Secure projects The LPC55S69 MCU series contains Arm TrustZone® and Trusted Execution Environment extension from NXP. It allows users to assign cores, memories, and peripherals to the Secure or the Non-Secure World and restrict access between them. Manufacturers can use it to secure critical functionality of a device. For example, the Secure code is provided on the device by the manufacturer and could not be modified by users. However, a user can create a Non-Secure application and download it to the device. A secure code can communicate over a channel which security cannot be exposed to the Non-Secure World. This example is shown in the tutorial. This tutorial demonstrates how to create Secure and Non-Secure projects and their basic configuration using MCUXpresso IDE and Config Tools. LPCXpresso55S69 Board is used for the demonstration of functionality. Project description Two projects, a Secure and a Non-Secure, are created. Both projects are used on a single core. USART is used for sending data and it is configured as a Secure peripheral. S1 (ISP) button is used for sending data from the Secure world. S2 (WAKEUP) button is used for sending data from the Non-Secure world, which is not allowed due to a security violation. Prerequisites MCUXpresso IDE 11.3.0 LPCXpresso55S69 SDK 2.9.0 LPCXpresso55S69 Board You are familiar with the security extension used on LPC55S69. You are familiar with MCUXpresso IDE and Config Tools – Getting started with TEE. Steps 1.  Create a Secure project Create a new project, select the security type (Secure), and set memory regions in New Project Wizard. You must do it as Secure and Non-Secure projects use different parts of memories. In addition, secure memories use aliases – the 28 th bit is set to 1.  To download the firmware to the secure flash, select the Secure flash driver „LPC55xx_S.cfx“. 2. Create a Non-Secure project Create a new project and set security and memories as follows. 3. Connect the projects It is not mandatory but it makes things easier. Reference the Secure project from the Non-Secure project. It makes importing memory regions into the TEE tool easier.  The current and the linked or linking projects are preselected in the import dialog. In the  Secure project set the Non-Secure project to be preprogrammed.  Both projects are automatically downloaded to the board prior to debugging the Secure project. 4. Disable generation of  a Secure gateway library This feature is not used in this tutorial, therefore it must be turned off to compile the project. Change it in project properties (right-click the project and select Properties). 5. Route Secure pins Open Pins tool. Route S1 pin to SECGPIO. For detecting button press, peripheral SPINT is used and it must be routed to the same pin. Flexcom, which is used as USART, is routed by default in a board configuration. Do not change anything there. 6. Setup Secure peripherals Flexcomm is used for USART communication. Open Peripherals tool. Add USART component in Peripherals tool. Use the default configuration. Problems related to clocks must be resolved in the Clocks tool by enabling peripheral clock. Right-click the problem in Problems view and select Show problem. It opens the Clocks tool and highlights the problematic clock path. Add PINT component. Uncheck the checkbox „Show only components in toolchain project“  as the PINT driver is not in the project yet. Otherwise, it is not listed in the dialog. Select SECPINT peripheral. Configure it to invoke a callback function upon falling edge is detected on S1. Add the  PINT driver to the project via quick-fix in the Problems view. 7. Setup security extension in TEE tool Import memory regions from both projects in the User Memory Regions tab. As nothing is configured for the security extension, there are errors and warnings in the Security Level column. In Security Access Configuration, Miscellaneous tab enable Secure check for AHB matrix and Non-Secure access to floating point extension (CP10 access). FPU is turned on by default. Enable SAU and set Non-Secure regions. Other memory is considered Secure. Set MPC to allow only Secure transactions for Secure memory regions. It resolves errors and warnings in User Memory regions. Set SECGPIO and SECPINT peripherals as Secure. Keep Flexcomm as Non-Secure for now for demonstration purposes. Set PINT interrupt security as Non-Secure. Sending data from the Non-Secure world is also triggered by button press so its interrupt security must be set accordingly. It is the last setting of the Secure project in Config Tools, at this stage update the code. 8. Update Secure project settings After updating the code, create a  TrustZone folder. By default, new folders are excluded from the build. Right-click the folder and uncheck Exclude resource from build in the folder properties. Add the path to the folder into Include paths in project settings. 9. Add missing drivers If you use this version of tools,  add the inputmux driver in the Secure project. It is required for code generated by the Pins tool. 10. Update the Secure source code Do the following updates in source/Secure.c file. Add TEE initialization function call. As security is the first thing that should be configured,  place it SystemInitHook function. This way it is called before entering the main function. The initialization function is implemented in resource_config.h which must be included.       /*! * @brief Application-specific implementation of the SystemInitHook() * weak function. */ void SystemInitHook(void) { BOARD_InitTEE(); }       Implement SECPINT callback function. After pressing S1,  some data is sent from the Secure world via USART. For simplicity, character ‚s‘ is sent from the Secure world and character ‚n‘  is sent from the Non-Secure world.       /* * @brief Send on byte over secure channel * @param data data to be sent */ void sendSecureByte(uint8_t data) { USART_WriteByte(FLEXCOMM0_PERIPHERAL, data); } /* * @brief S1 button interrupt callback * @param pintr pin interrupt type * @param pmatch_status match status */ void secureButtonCallback(pint_pin_int_t pintr ,uint32_t pmatch_status) { sendSecureByte('s'); }       When you do the initialization in the Secure world, the MCU can continue with executing instructions from the Non-Secure world. The switching consists of setting a Non-Secure stack, a vector table, and calling a reset handler. The Non-Secure flash was previously configured to start at address 0x10000.       /* Start address of Non-secure application */ #define NON_SECURE_START 0x10000 /* typedef for non-secure callback functions */ typedef void (*funcptr_ns)(void) __attribute__((cmse_nonsecure_call)); int main(void) { /* Init board hardware. */ BOARD_InitBootPins(); BOARD_InitBootClocks(); BOARD_InitBootPeripherals(); #ifndef BOARD_INIT_DEBUG_CONSOLE_PERIPHERAL /* Init FSL debug console. */ BOARD_InitDebugConsole(); #endif PRINTF("Secure World\n"); /* Set non-secure main stack (MSP_NS) */ __TZ_set_MSP_NS(*((uint32_t *)(NON_SECURE_START))); /* Set non-secure vector table */ SCB_NS->VTOR = NON_SECURE_START; /* Get non-secure reset handler */ funcptr_ns ResetHandler_ns; ResetHandler_ns = (funcptr_ns)(*((uint32_t *)((NON_SECURE_START) + 4U))); /* Jump to normal world */ ResetHandler_ns(); /* Force the counter to be placed into memory. */ volatile static int i = 0 ; /* Enter an infinite loop, just incrementing a counter. */ while(1) { i++ ; /* 'Dummy' NOP to allow source level single stepping of tight while() loop */ __asm volatile ("nop"); } return 0 ; }       11. Route Non-Secure pins Configure the Non-Secure project properly. Route S2 pin to GPIO as input. Route  PINT for pin #64. Flexcomm is routed by default, remove this routing as it is already routed in the Secure project. 12. Setup Non-Secure peripherals Set up PINT to use callback on falling edge of the S2 button press.  Add the driver, for example, via quick fix. 13. Update the Non-Secure source code Keep the initialization of Pins and Peripherals and remove the other initialization as it was done in the Secure world. That also includes the overriding SystemInit function.       /* * @brief System initialization * * Intentionally empty. Required initialization was done in the Secure project. * */ void SystemInit(void) { } /* * @brief Application entry point. */ int main(void) { /* Init board hardware. */ BOARD_InitBootPins(); BOARD_InitBootPeripherals(); ...       Add the code for sending data from the Non-Secure world. To use the USART_WriteByte function and the imputmux driver, include fsl_usart.h.       /* * @brief S2 button interrupt callback * @param pintr pin interrupt type * @param pmatch_status match status */ void nonSecureButtonCallback(pint_pin_int_t pintr ,uint32_t pmatch_status) { USART_WriteByte((USART_Type *)FLEXCOMM0, 'n'); }       Now the projects are ready. When debug is executed for the Secure project, the Non-Secure project is also downloaded to the board. After pressing S1, 's' is sent from the Secure world. When S2 is pressed, 'n' is sent from the Non-Secure world because Flexcomm is configured as Non-Secure in the TEE tool. 14. Securing USART Open the TEE tool from the Secure project and set the Flexcomm slave as Secure. After this change, you can send data from the Secure world but an attempt to send data from the Non-Secure world results in bus fault.  
View full article
This tutorial is how to start working with TEE
View full article
The MCUXpresso Config Tools is an integrated suite of configuration tools that help guide users from first evaluation to production software development when designing with Arm ® Cortex ® -M-based devices from NXP, including its general purpose, crossover and wireless-enabled MCUs. These configuration tools allow developers to quickly build a custom SDK and leverage pins, clocks and peripherals to generate initialization C code for custom board support. The following tutorials help you design with the MCUXpresso software and tools. Pins Tool and Expansion Headers Apply Arduino virtual adapter into compatible header Measuring temperature using digital sensor DS18B20 and Arduino Multifunction Shield on FRDM K64F Creating expansion board definition file for Arduino Multifunction shield Adding Expansion Headers to a custom board Peripherals tool USB Audio Class Tutorial  Using TDA1543 I2S DAC with the LPC54114 board  Touch controlled led light on LPCXPRESSO845-BRK  eDMA component abilities shown on ADC measurement example Trusted Execution Environment (TEE) Getting started with TEE  Creating Secure and Non-Secure projects Calling Secure code from Non-Secure region LPC55Sxx: Securing Digital IO Pins
View full article
This video provides an instruction to the NXP Pins tool (see New Kinetis Expert Pins Tool V1.0 Available!). It demonstrates how to use the tool and how to configure pins with the example of the FRDM-K64F Board.   Enjoy 🙂
View full article
The following article describes how the data files of the Pins Tool can be downloaded either for offline usage or processed further, for example in an automated build system or how to use it on a machine without network connection: https://mcuoneclipse.com/2016/07/29/nxp-pins-tool-understanding-data-for-offline-usage/   I hope you find this useful, Erich
View full article
This post will include a history of releases for the MCUXpresso Config Tools.    Most Recent Release: MCUXpresso Config Tools v11 - Released on January 17, 2022   Download Links: MCUXpresso IDE with integrated Config Tools Standalone MCUXpresso Config Tool   Standalone MCUXpresso Config Tool vs MCUXpresso IDE integrated version The functionality of the MCUXpresso Config Tools is integrated directly within the MCUXpresso IDE as tool perspectives (Pins, Clock, Peripheral, etc).  The configuration tools/perspective will provide a seamless way to configure and modify projects developed within MCUXpresso IDE.  The MCUXpresso Config Tools are also provided as a standalone installation for use with other IDEs (IAR and Keil).  Additionally these tools can be used without an IDE for generating configuration files and generated source file for use without an IDE.   Receive email notification for new releases: If you would like to receive email notifications when a new version of the MCUXpresso Config Tools is released, consider adding an "Email Watch" to this post.   Previous Release History: MCUXpresso Config Tools v10 - Released on July 15, 2021 MCUXpresso Config Tools v9 - Released on January 15, 2021 MCUXpresso Config Tools v8 - Released on July 21, 2020 MCUXpresso Config Tools v7 - Released on Dec 19, 2019  MCUXpresso Config Tools v6 - Released on June 13, 2019 MCUXpresso Config Tools v5 - Released on January 10, 2019
View full article
The MCUXpresso Config Tools is installed without the data for MCUs and boards, and the data are download on demand via internet. So this article describes how to use MCUXpresso Config Tools with offline Computer. There are two methods: - Copy and paste the data on computer; - Connect the internet when first using. About the detail steps, please have a look at attachment . Thanks for the suggestion from Petr Hradsky . Alice Yang
View full article
The following article has quick steps and videos how to get started with Kinetis Expert SDK and Design Studio:   https://community.freescale.com/docs/DOC-329662   Enjoy!
View full article
The following article describes how to configure code generation for the clock gates and how to perform a full initialization with the Pins Tool: https://mcuoneclipse.com/2016/07/19/nxp-pins-tool-clock-gates-and-controlling-the-bits/  
View full article
This community and forum is for the growing set of Kinetis Expert System Conguration Tools. The tools are acessible online on Welcome to Kinetis Expert | Kinetis Expert and include right now the 'Build an SDK' and 'Power Estimation' tools: So if you have any questions or need any further advice and information about the Kinetis Expert System Configuration Tools, this is the community for it!
View full article
This tip will show you how to use MCUXpresso Config Tools V4.1 generate codes for KV5x with 50MHz external reference clock. The fec_extal in datasheet shows that the maximum frequency of Input clock frequency (external clock mode) is 48MHz. It will lead code generation failed when you configure 50MHz as the external reference clock in latest MCUXpresso Config Tools V4.1. (Code generation in case of warnings shouldn't be blocked. It will be fixed for MCUXpresso Config Tools V5.) Some customer had met this issue when using TWR-KV58F220M board, this board connect a 50MHz_OSC to EXTAL0. My colleague have prepared a hot fix for this issue (for all MKV5x MCUs). After install the attached hot_fix_MCUXpresso_Config_Tools_V4_1_data_MKV58_MCUCM-3936, customer is able to overcome it.(Notice: The ProgramData folder was hidden by default.)
View full article
A new version of the Kinetis Expert Configuration Tools has been released and is available both online (Welcome to Kinetis Expert | Kinetis Expert ) or for download as desktop tool (Software Development Kit for Kinetis MCUs|NXP ).   The set of the tools has a new member: the Clocks Tool: Simple UI for clock parameter viewing and modification Graphical view for easy navigation and visualization of settings and frequencies Generate configuration code using KSDK v2 Inspect and modify clock configuration from clock input source up to the core/peripherals Validate clock settings and calculate the resulting output clock frequencies Determines suitable clock settings for given output requirements Integrated with the Pins Tool   Main features of Pins Tool and Clocks Tool: Available as Web and Desktop application Kinetis SDK v2 support Multicore support Localized for English and Simplified Chinese Mostly Connected: On-Demand device data download Integrates with any compiler and IDE Generation of documented C code which is C++ aware   What's New Added Clocks Tool Added Support for boards, kits and templates Added Labels and Identifier support Added Log and Problems View Export downloaded data to copy or share device information data Bug fixes and improved documentation The release notes of the desktop application are attached to this article.   Clocks Tool The new member of the suite of configuration tools is the Clocks Tool.  Use the Tools menu to select and switch between the tools:   The Clocks Tool provides graphical views for configuration and navigation in the clocks of the hardware:   Templates, Kits, Boards and Processors When creating a new configuration, it offers Templates, Kits, Boards and Processors. Custom configurations can be stored as templates and then used for new configurations.   Board Specific Functions With the provided board and kit configurations, there are now pre-configured initialization functions for major blocks on the board:   Labels and Identifiers In the Pins Tool there are two new columns: Label and Identifier: The Label is a user name/string to identify or describe the pin. The Identifier is a user C/C++ identifier which is added to the generated source code to be used by the application.   Export Data To simplify downloading the device specific data for the desktop tool, the 'Export' function can be used to download and export the data. The data can be copied that way to another machine or all data for a set of devices can be loaded.     The device support for the clocks tool is staged, so initially not all SDK V2 devices are included. As of Oct 14, the the following Kinetis SDK V2 R1 devices are supported by the Clocks Tool: MK21FN1M0AVLQ12 MK21FN1M0AVMC12 MK21FN1M0AVMD12 MK21FN1M0VLQ12 MK21FN1M0VMC12 MK21FN1M0VMD12 MK21FX512AVLQ12 MK21FX512AVMC12 MK21FX512AVMD12 MK21FX512VLQ12 MK21FX512VMC12 MK21FX512VMD12 MK22FN128CAH12 MK22FN128VDC10 MK22FN128VLH10 MK22FN128VLL10 MK22FN128VMP10 MK22FN1M0AVLH12 MK22FN1M0AVLK12 MK22FN1M0AVLL12 MK22FN1M0AVLQ12 MK22FN1M0AVMC12 MK22FN1M0AVMD12 MK22FN1M0VLH12 MK22FN1M0VLK12 MK22FN1M0VLL12 MK22FN1M0VLQ12 MK22FN1M0VMC12 MK22FN1M0VMD12 MK22FN256CAH12 MK22FN256VDC12 MK22FN256VLH12 MK22FN256VLL12 MK22FN256VMP12 MK22FN512CAP12 MK22FN512VDC12 MK22FN512VLH12 MK22FN512VLL12 MK22FN512VMP12 MK22FX512AVLH12 MK22FX512AVLK12 MK22FX512AVLL12 MK22FX512AVLQ12 MK22FX512AVMC12 MK22FX512AVMD12 MK22FX512VLH12 MK22FX512VLK12 MK22FX512VLL12 MK22FX512VLQ12 MK22FX512VMC12 MK22FX512VMD12 MK24FN1M0VDC12 MK24FN1M0VLL12 MK24FN1M0VLQ12 MK26FN2M0CAC18 MK26FN2M0VLQ18 MK26FN2M0VMD18 MK26FN2M0VMI18 MK63FN1M0VLQ12 MK63FN1M0VMD12 MK64FN1M0VDC12 MK64FN1M0VLL12 MK64FN1M0VLQ12 MK64FN1M0VMD12 MK64FX512VDC12 MK64FX512VLL12 MK64FX512VLQ12 MK64FX512VMD12 MK65FN2M0CAC18 MK65FN2M0VMI18 MK65FX1M0CAC18 MK65FX1M0VMI18 MK66FN2M0VLQ18 MK66FN2M0VMD18 MK66FX1M0VLQ18 MK66FX1M0VMD18 MK80FN256CAx15 MK80FN256VDC15 MK80FN256VLL15 MK80FN256VLQ15 MK81FN256CAx15 MK81FN256VDC15 MK81FN256VLL15 MK81FN256VLQ15 MK82FN256CAx15 MK82FN256VDC15 MK82FN256VLL15 MK82FN256VLQ15 MKL13Z32VFM4 MKL13Z32VFT4 MKL13Z32VLH4 MKL13Z32VLK4 MKL13Z32VMP4 MKL13Z64VFM4 MKL13Z64VFT4 MKL13Z64VLH4 MKL13Z64VLK4 MKL13Z64VMP4 MKL17Z128VFM4 MKL17Z128VFT4 MKL17Z128VLH4 MKL17Z128VMP4 MKL17Z256VFM4 MKL17Z256VFT4 MKL17Z256VLH4 MKL17Z256VMP4 MKL17Z32VDA4 MKL17Z32VFM4 MKL17Z32VFT4 MKL17Z32VLH4 MKL17Z32VMP4 MKL17Z64VDA4 MKL17Z64VFM4 MKL17Z64VFT4 MKL17Z64VLH4 MKL17Z64VMP4 MKL27Z128VFM4 MKL27Z128VFT4 MKL27Z128VLH4 MKL27Z128VMP4 MKL27Z256VFM4 MKL27Z256VFT4 MKL27Z256VLH4 MKL27Z256VMP4 MKL27Z32VDA4 MKL27Z32VFM4 MKL27Z32VFT4 MKL27Z32VLH4 MKL27Z32VMP4 MKL27Z64VDA4 MKL27Z64VFM4 MKL27Z64VFT4 MKL27Z64VLH4 MKL27Z64VMP4 MKL33Z128VLH4 MKL33Z128VMP4 MKL33Z256VLH4 MKL33Z256VMP4 MKL33Z32VFT4 MKL33Z32VLH4 MKL33Z32VLK4 MKL33Z32VMP4 MKL33Z64VFT4 MKL33Z64VLH4 MKL33Z64VLK4 MKL33Z64VMP4 MKL43Z128VLH4 MKL43Z128VMP4 MKL43Z256VLH4 MKL43Z256VMP4 MKS22FN256VLL12 MKS22FN256VLH12 MKS22FN128VLL12 MKS22FN128VLH12   In November, the following SDK V2.0 R2 and R3 devices will be available in the Clocks Tool: MKL14Z32VFM4 MKL14Z32VFT4 MKL14Z32VLH4 MKL14Z32VLK4 MKL14Z64VFM4 MKL14Z64VFT4 MKL14Z64VLH4 MKL14Z64VLK4 MKL15Z128CAD4 MKL15Z128VFM4 MKL15Z128VFT4 MKL15Z128VLH4 MKL15Z128VLK4 MKL15Z32VFM4 MKL15Z32VFT4 MKL15Z32VLH4 MKL15Z32VLK4 MKL15Z64VFM4 MKL15Z64VFT4 MKL15Z64VLH4 MKL15Z64VLK4 MKL24Z32VFM4 MKL24Z32VFT4 MKL24Z32VLH4 MKL24Z32VLK4 MKL24Z64VFM4 MKL24Z64VFT4 MKL24Z64VLH4 MKL24Z64VLK4 MKL25Z128VFM4 MKL25Z128VFT4 MKL25Z128VLH4 MKL25Z128VLK4 MKL25Z32VFM4 MKL25Z32VFT4 MKL25Z32VLH4 MKL25Z32VLK4 MKL25Z64VFM4 MKL25Z64VFT4 MKL25Z64VLH4 MKL25Z64VLK4   MKW21D256VHA5 MKW21D512VHA5 MKW22D512VHA5 MKW24D512VHA5   In December, the SDK 2.0 R4 devices will be supported by the Clocks Tool: MKV10Z16VFM7 MKV10Z16VLC7 MKV10Z16VLF7 MKV10Z32VFM7 MKV10Z32VLC7 MKV10Z32VLF7 MKV10Z128VFM7 MKV10Z128VLC7 MKV10Z128VLF7   MKV10Z128VLH7   MKV10Z64VFM7 MKV10Z64VLC7 MKV10Z64VLF7   MKV10Z64VLH7 MKV11Z128VFM7 MKV11Z128VLC7 MKV11Z128VLF7   MKV11Z128VLH7   MKV11Z64VFM7 MKV11Z64VLC7 MKV11Z64VLF7   MKV11Z64VLH7   MKV30F128VFM10 MKV30F128VLF10 MKV30F128VLH10 MKV30F64VFM10 MKV30F64VLF10 MKV30F64VLH10 MKV46F256VLL16 MKV46F256VLH16 MKV46F128VLL16 MKV46F128VLH16 MKV44F256VLL16 MKV44F256VLH16 MKV44F128VLL16 MKV44F128VLH16 MKV44F64VLH16 MKV42F256VLL16 MKV42F256VLH16 MKV42F128VLL16 MKV42F128VLH16 MKV42F64VLH16 MKV44F128VLF16 MKV44F64VLF16 MKV42F128VLF16 MKV42F64VLF16 MKV58F1M0VMD24 MKV58F512VMD24 MKV58F1M0VLQ24 MKV58F512VLQ24 MKV58F1M0VLL24 MKV58F512VLL24 MKV56F1M0VMD24 MKV56F512VMD24 MKV56F1M0VLQ24 MKV56F512VLQ24 MKV56F1M0VLL24 MKV56F512VLL24 MKV31F128VLH10 MKV31F128VLL10 MKV31F256VLH12 MKV31F256VLL12 MKV31F512VLH12 MKV31F512VLL12   We hope you will find this new release useful.   Thanks for designing with NXP!
View full article
The new NXP Pins tool which has been showcased at FTF 2016 in Austin is now available as Web and Desktop application. The Kinetis Expert Pins Tool makes configuring, muxing and routing of pins very easy and fast. It provides real-time feedback of conflicts and provides an intuitive graphical interface with several views. The tool generates Kinetis SDK V2.0 compatible sources files which can be directly integrated into C/C++ applications. The Pins tool is available both as Web application (no installation needed) and as a Desktop application for Linux, Mac and Windows.     You can use the Web version from Welcome to Kinetis Expert | Kinetis Expert.   It is available for download as Desktop version from Software Development Kit for Kinetis MCUs|NXP (Windows, Mac OS X and Linux 64bit) under the 'Software' category: There are two different installer types: 'offline' is a 130 MByte download. This method is recommended for slower internet connections or for installation on multiple machines. 'online' is a small 500 KByte download, all the other installation data will be loaded from the internet during installation. Mac OS X and Linux installers are 64bit. For Windows there are both 32bit and 64bit installers available.   Documenation is availble on Software Development Kit for Kinetis MCUs|NXP in the documenation download section, as well attached to this article (Getting Started is available in Chinese): An overview and tutorial can be found here: https://mcuoneclipse.com/2016/06/08/tutorial-muxing-with-the-new-nxp-pins-tool/   We hope you find this tool useful!
View full article