A new version of the Kinetis Expert Configuration Tools has been released and is available both online (Welcome to Kinetis Expert | Kinetis Expert ) or for download as desktop tool (Software Development Kit for Kinetis MCUs|NXP ).     The set of the tools has a new member: the Clocks Tool:         Simple UI for clock parameter viewing and modification  Graphical view for easy navigation and visualization of settings and frequencies  Generate configuration code using KSDK v2  Inspect and modify clock configuration from clock input source up to the core/peripherals  Validate clock settings and calculate the resulting output clock frequencies  Determines suitable clock settings for given output requirements  Integrated with the Pins Tool      Main features of Pins Tool and Clocks Tool:   Available as Web and Desktop application  Kinetis SDK v2 support  Multicore support  Localized for English and Simplified Chinese  Mostly Connected: On-Demand device data download  Integrates with any compiler and IDE  Generation of documented C code which is C++ aware      What's New   Added Clocks Tool  Added Support for boards, kits and templates  Added Labels and Identifier support  Added Log and Problems View  Export downloaded data to copy or share device information data  Bug fixes and improved documentation   The release notes of the desktop application are attached to this article.     Clocks Tool  The new member of the suite of configuration tools is the Clocks Tool.  Use the Tools menu to select and switch between the tools:           The Clocks Tool provides graphical views for configuration and navigation in the clocks of the hardware:           Templates, Kits, Boards and Processors  When creating a new configuration, it offers Templates, Kits, Boards and Processors.        Custom configurations can be stored as templates and then used for new configurations.     Board Specific Functions  With the provided board and kit configurations, there are now pre-configured initialization functions for major blocks on the board:           Labels and Identifiers  In the Pins Tool there are two new columns: Label and Identifier:        The Label is a user name/string to identify or describe the pin. The Identifier is a user C/C++ identifier which is added to the generated source code to be used by the application.     Export Data  To simplify downloading the device specific data for the desktop tool, the 'Export' function can be used to download and export the data. The data can be copied that way to another machine or all data for a set of devices can be loaded.              The device support for the clocks tool is staged, so initially not all SDK V2 devices are included. As of Oct 14, the the following Kinetis SDK V2 R1 devices are supported by the Clocks Tool:      MK21FN1M0AVLQ12    MK21FN1M0AVMC12    MK21FN1M0AVMD12    MK21FN1M0VLQ12    MK21FN1M0VMC12    MK21FN1M0VMD12    MK21FX512AVLQ12    MK21FX512AVMC12    MK21FX512AVMD12    MK21FX512VLQ12    MK21FX512VMC12    MK21FX512VMD12    MK22FN128CAH12    MK22FN128VDC10    MK22FN128VLH10    MK22FN128VLL10    MK22FN128VMP10    MK22FN1M0AVLH12    MK22FN1M0AVLK12    MK22FN1M0AVLL12    MK22FN1M0AVLQ12    MK22FN1M0AVMC12    MK22FN1M0AVMD12    MK22FN1M0VLH12    MK22FN1M0VLK12    MK22FN1M0VLL12    MK22FN1M0VLQ12    MK22FN1M0VMC12    MK22FN1M0VMD12    MK22FN256CAH12    MK22FN256VDC12    MK22FN256VLH12    MK22FN256VLL12    MK22FN256VMP12    MK22FN512CAP12    MK22FN512VDC12    MK22FN512VLH12    MK22FN512VLL12    MK22FN512VMP12    MK22FX512AVLH12    MK22FX512AVLK12    MK22FX512AVLL12    MK22FX512AVLQ12    MK22FX512AVMC12    MK22FX512AVMD12    MK22FX512VLH12    MK22FX512VLK12    MK22FX512VLL12    MK22FX512VLQ12    MK22FX512VMC12    MK22FX512VMD12    MK24FN1M0VDC12    MK24FN1M0VLL12    MK24FN1M0VLQ12    MK26FN2M0CAC18    MK26FN2M0VLQ18    MK26FN2M0VMD18    MK26FN2M0VMI18    MK63FN1M0VLQ12    MK63FN1M0VMD12    MK64FN1M0VDC12    MK64FN1M0VLL12    MK64FN1M0VLQ12    MK64FN1M0VMD12    MK64FX512VDC12    MK64FX512VLL12    MK64FX512VLQ12    MK64FX512VMD12    MK65FN2M0CAC18    MK65FN2M0VMI18    MK65FX1M0CAC18    MK65FX1M0VMI18    MK66FN2M0VLQ18    MK66FN2M0VMD18    MK66FX1M0VLQ18    MK66FX1M0VMD18    MK80FN256CAx15    MK80FN256VDC15    MK80FN256VLL15    MK80FN256VLQ15    MK81FN256CAx15    MK81FN256VDC15    MK81FN256VLL15    MK81FN256VLQ15    MK82FN256CAx15    MK82FN256VDC15    MK82FN256VLL15    MK82FN256VLQ15    MKL13Z32VFM4    MKL13Z32VFT4    MKL13Z32VLH4    MKL13Z32VLK4    MKL13Z32VMP4    MKL13Z64VFM4    MKL13Z64VFT4    MKL13Z64VLH4    MKL13Z64VLK4    MKL13Z64VMP4    MKL17Z128VFM4    MKL17Z128VFT4    MKL17Z128VLH4    MKL17Z128VMP4    MKL17Z256VFM4    MKL17Z256VFT4    MKL17Z256VLH4    MKL17Z256VMP4    MKL17Z32VDA4    MKL17Z32VFM4    MKL17Z32VFT4    MKL17Z32VLH4    MKL17Z32VMP4    MKL17Z64VDA4    MKL17Z64VFM4    MKL17Z64VFT4    MKL17Z64VLH4    MKL17Z64VMP4    MKL27Z128VFM4    MKL27Z128VFT4    MKL27Z128VLH4    MKL27Z128VMP4    MKL27Z256VFM4    MKL27Z256VFT4    MKL27Z256VLH4    MKL27Z256VMP4    MKL27Z32VDA4    MKL27Z32VFM4    MKL27Z32VFT4    MKL27Z32VLH4    MKL27Z32VMP4    MKL27Z64VDA4    MKL27Z64VFM4    MKL27Z64VFT4    MKL27Z64VLH4    MKL27Z64VMP4    MKL33Z128VLH4    MKL33Z128VMP4    MKL33Z256VLH4    MKL33Z256VMP4    MKL33Z32VFT4    MKL33Z32VLH4    MKL33Z32VLK4    MKL33Z32VMP4    MKL33Z64VFT4    MKL33Z64VLH4    MKL33Z64VLK4    MKL33Z64VMP4    MKL43Z128VLH4    MKL43Z128VMP4    MKL43Z256VLH4    MKL43Z256VMP4    MKS22FN256VLL12    MKS22FN256VLH12    MKS22FN128VLL12    MKS22FN128VLH12         In November, the following SDK V2.0 R2 and R3 devices will be available in the Clocks Tool:      MKL14Z32VFM4    MKL14Z32VFT4    MKL14Z32VLH4    MKL14Z32VLK4    MKL14Z64VFM4    MKL14Z64VFT4    MKL14Z64VLH4    MKL14Z64VLK4    MKL15Z128CAD4    MKL15Z128VFM4    MKL15Z128VFT4    MKL15Z128VLH4    MKL15Z128VLK4    MKL15Z32VFM4    MKL15Z32VFT4    MKL15Z32VLH4    MKL15Z32VLK4    MKL15Z64VFM4    MKL15Z64VFT4    MKL15Z64VLH4    MKL15Z64VLK4    MKL24Z32VFM4    MKL24Z32VFT4    MKL24Z32VLH4    MKL24Z32VLK4    MKL24Z64VFM4    MKL24Z64VFT4    MKL24Z64VLH4    MKL24Z64VLK4    MKL25Z128VFM4    MKL25Z128VFT4    MKL25Z128VLH4    MKL25Z128VLK4    MKL25Z32VFM4    MKL25Z32VFT4    MKL25Z32VLH4    MKL25Z32VLK4    MKL25Z64VFM4    MKL25Z64VFT4    MKL25Z64VLH4    MKL25Z64VLK4             MKW21D256VHA5    MKW21D512VHA5    MKW22D512VHA5    MKW24D512VHA5         In December, the SDK 2.0 R4 devices will be supported by the Clocks Tool:      MKV10Z16VFM7    MKV10Z16VLC7    MKV10Z16VLF7    MKV10Z32VFM7    MKV10Z32VLC7    MKV10Z32VLF7    MKV10Z128VFM7    MKV10Z128VLC7    MKV10Z128VLF7      MKV10Z128VLH7      MKV10Z64VFM7    MKV10Z64VLC7    MKV10Z64VLF7      MKV10Z64VLH7    MKV11Z128VFM7    MKV11Z128VLC7    MKV11Z128VLF7      MKV11Z128VLH7      MKV11Z64VFM7    MKV11Z64VLC7    MKV11Z64VLF7      MKV11Z64VLH7      MKV30F128VFM10    MKV30F128VLF10    MKV30F128VLH10    MKV30F64VFM10    MKV30F64VLF10    MKV30F64VLH10    MKV46F256VLL16    MKV46F256VLH16    MKV46F128VLL16    MKV46F128VLH16    MKV44F256VLL16    MKV44F256VLH16    MKV44F128VLL16    MKV44F128VLH16    MKV44F64VLH16    MKV42F256VLL16    MKV42F256VLH16    MKV42F128VLL16    MKV42F128VLH16    MKV42F64VLH16    MKV44F128VLF16    MKV44F64VLF16    MKV42F128VLF16    MKV42F64VLF16    MKV58F1M0VMD24    MKV58F512VMD24    MKV58F1M0VLQ24    MKV58F512VLQ24    MKV58F1M0VLL24    MKV58F512VLL24    MKV56F1M0VMD24    MKV56F512VMD24    MKV56F1M0VLQ24    MKV56F512VLQ24    MKV56F1M0VLL24    MKV56F512VLL24    MKV31F128VLH10    MKV31F128VLL10    MKV31F256VLH12    MKV31F256VLL12    MKV31F512VLH12    MKV31F512VLL12         We hope you will find this new release useful.     Thanks for designing with NXP!   
        
        View full article