MCUXpresso配置工具知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCUXpresso Config Tools Knowledge Base

标签

讨论

排序依据:
Serial Memory Tool Training   Welcome to the Serial Memory Tool training! This course is designed to help you understand and efficiently use the Serial Memory Tool. You’ll learn how to check external memory connections, configure memory interfaces, optimize performance, and prepare your setup for production. By the end of this training, you’ll be confident in managing memory configurations, running tests, and generating the necessary files for your applications 01 - Introduction: The Serial Memory Tool Get an overview of the Serial Memory Tool, its purpose, and how it simplifies memory configuration and testing. Learn why this tool is essential for optimizing memory performance and reducing design time. 02 – Installation and Documentation Learn how to install the Serial Memory Tool from the Visual Studio Marketplace and where to find the most up-to-date documentation. We’ll guide you through initializing the toolchain and accessing practical examples on GitHub. 03 – The Tool’s UI Explore the user interface of the Serial Memory Tool. Understand the different panels, including MCU and Memory selection, available tests, and board connection options. Discover how to navigate and configure settings efficiently. 04 – The Configuration Panel Dive into the Configuration panel to set core frequency, memory properties, FlexSPI connection, and communication protocol. These settings impact your memory performance and board compatibility. 05 – Configure FlexSPI and Protocol, and Test Configuration Understand how to configure FlexSPI parameters and communication protocols. Learn how to verify your setup using initialization and read/write tests, and interpret logs for troubleshooting. 06 – Custom Memory Configuration and Export FCB Learn the process of working with custom boards and memories. Find out how to adjust FlexSPI parameters, modify LUT tables, and export the FlexSPI Configuration Block (FCB) binary for use in your application. Conclusion By completing this training, you have learned how to: Install and set up the Serial Memory Tool. Navigate its user interface and configure memory settings. Optimize FlexSPI connections and run validation tests. Work with custom boards and memories. Save, import, and export configurations, including generating FCB files. For more details and download, see https://marketplace.visualstudio.com/items?itemName=NXPSemiconductors.flexspi  
查看全文
We are pleased to announce that MCUXpresso Config Tools v25.06 are now available. Downloads It’s a part of MCUXpresso IDE https://www.nxp.com/mcuxpresso/ide/download In order to use it with other toolchains, download the installer for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/config Please refer to MCUXpresso Config Tools documentation for installation and quick start guides. For online version, login into MCUXpresso site: MCUXpresso WEB Release Notes Full details on the release (features, known issues...) • DCD – The pattern for identifying the tool source files is improved. • Clocks – Support for read-only element settings is added. – Filtering all settings of Initialization modules in the Details view is supported. • Peripherals – The wizard to export the Registers view data in the CSV format is added. – Performance of the tool is improved. • An ability to export/import Expansion Boards, Expansion Headers, and System Manager components is added.
查看全文
1.  Introduction This document describes the USB configuration component and implementation of the Audio 1.0 class application example on the MIMXRT1060-EVK board. It focuses on the MCUXpresso IDE and Config Tools. It provides an example of the Quad Timer peripheral component used as a digital-to-analog converter for processing audio data. The USB Audio class is supported in the SDK packages that are available for a wide range of MCUs. One of the last i.MX Real-Time (RT) crossover MCUs is the i.MX RT1060. It is available on the MIMXRT1060-EVK evaluation board. The SDK package already contains a demo application that demonstrates the USB Audio speaker functionality. However, a detailed guide on how to develop the application and customize the processing of audio data is not provided.  2.  Prerequisites The USB Audio application is developed in the MCUXpresso IDE 11.2.1 that is available on the http://www.nxp.com/mcuxpresso/ide website. Download and install this or newer version. The Config Tools that is used for the application design is integrated into the MCUXpresso IDE. Download the MIMXRT1060-EVK SDK support package inside the MCUXpresso IDE (see Install MCUXpresso SDKs in quick access) or separately on https://mcuxpresso.nxp.com/ pages (the SDK package must be built with the USB middleware selected).   3.  USB Audio concept The USB Audio class is supported in the USB middleware of the SDK package. The Peripherals tool from provides a USB middleware component that provides GUI for the configuration of the USB class, interfaces, and generating USB code examples. The USB Audio 1.0 speaker example, enumerated as a playback device, is available as a preset in the USB component. In this demo example, the device receives audio data and stores it in the internal buffer. The playback of audio is not a part of the generated code example, and the implementation is a part of this document. The USB Audio 1.0 speaker demo application that is described in this document consists of the following parts: Figure 1. Structure of the USB audio speaker application The USB component supports the configuration of the Audio control interface and streaming interfaces for the Audio 1.0 class (see the MCUXpresso Config Tools Project chapter for the steps of creating the project with the USB component). 3.1.     Audio control Interface The Audio control subclass provides a configuration of the USB Audio device topology by using terminals and units. The USB component supports one interrupt endpoint (control endpoint) and the audio control interface settings (the topology). See the example of the Audio speaker configuration below. Figure 2. Interface setting of the USB component The USB component supports the following terminals and units of the Audio 1.0 specification: Input Terminal Feature Unit Output Terminal All these units are used in the Audio speaker example. Input Terminal The Input Terminal (IT) is used to interface between the audio function’s ‘outside world’ and other units in the audio function. It serves as a receptacle for audio information flowing into the audio function. Its function is to represent a source of incoming audio data after this data has been properly extracted from the original audio stream into separate logical channels that are embedded in this stream (the decoding process). The logical channels are grouped into an audio channel cluster and leave the Input Terminal through a single Output Pin. The configuration of the input terminal consists of the ID (must be unique), type, number of channels, and spatial location, see below. The Input Terminal provides: Figure 3. Input terminal configuration Feature Unit The Feature Unit (FU) provides basic manipulation of multiple single-parameter on the incoming logical channels. It supports the following features: Mute, Volume, Tone Control, Graphic Equalizer, Automatic Gain Control, Delay, Bass Boost, and Loudness. The configuration of the feature unit consists of the unit ID (must be unique), source unit/terminal, and selection of features for every channel. Figure 4. Feature unit configuration  Output Terminal The Output Terminal (OT) is used to interface between the units inside the audio function and the ‘outside world’. It serves as an outlet for audio information, flowing out of the audio function. Its function is to represent a sink of outgoing audio data before this data is properly packed from the original separate logical channels into the outgoing audio stream (the encoding process). The audio channel cluster enters the Output Terminal through a single Input Pin. The configuration of the output terminal consists of the ID (must be unique), type, and source ID (unit/terminal), see below. Figure 5. Output terminal configuration 3.2.     Audio streaming interface Audio Streaming (AS) interfaces are used to interchange digital audio data streams between the Host and the audio function. Each Audio Streaming interface can have at most one isochronous data endpoint and an optional associated isochronous sync endpoint for synchronization purposes. The isochronous data endpoint is required to be the first endpoint in the AS interface. The AS interface is also used for the specification of the audio data format. The USB component Audio 1.0 class supports the Format I type of audio data only. The configuration (in the Audio speaker example) does not provide any audio class-specific interface and endpoints. See the following configuration: Figure 6. Zero bandwidth interface configuration Data output alternative interface settings provide a full configuration of audio streaming class-specific settings including the audio data format. There are additional audio class-specific settings for isochronous endpoints. Figure 7. Data output interface configuration   Figure 8. Isochronous feedback endpoint configuration   The Audio speaker example uses two endpoints: #1 – isochronous data endpoint (host output) for receiving audio data from the USB host. #2 – isochronous feedback endpoint that is used for synchronization between the USB audio device and the USB host. Audio stream interface-specific settings contain the Link to terminal setting which is linked to this audio streaming interface configuration and the audio data format configuration. The USB component supports just the Format I types. There is an additional configuration of the format – number of channels, subframe size, audio data resolution, and supported sampling frequencies.   4.  MCUXpresso Config Tools project This chapter provides a for the implementation of the USB Audio 1.0 demo project the MCUXpresso IDE 11.2.1 and using SDK 2.8.5 for the MIMXRT1060-EVK board. The newer version of the MCUXpresso IDE and SDK package for the MIMXRT1060-EVK shall be also compatible. 4.1. Board support project Open the MCUXpresso IDE. In the Quickstart Panel, select New project, in the SDK Wizard write RT1060 in the filter line, select the evkmimxrt1060 board, click the Next button. Figure 9. New EVKMIMXRT1060 project In the next window, write the project name, for example, MIMXRT1062xxxxA_     and select the USB Device Audio class on the Middleware tab (all the required components of the USB middleware are automatically selected), see below: Figure 10. USB middleware components of the new project Click the Finish button (the default libraries, compiler, linker, and memory map settings can be used). The MIMXRT1062xxxxA_USB_audio_speaker project is created in the IDE. The content is available in the Project Explorer window. 4.2.     Peripherals Open the Peripherals tool by using the Config Tools -> Peripherals. Figure 11. Selection of the Peripherals tool In the Peripherals tool, select the MIMXRT1062xxxxA_USB_audio_speaker project and create an instance of the USB 2.6.0 (or newer version) component for the USB1 peripheral in the Peripherals window, see below: Figure 12. Adding of the USB component The USB component is added to the Peripherals project (in the default functional group that is named BOARD_InitPeripherals). An empty USB component is created (there is no interface created and the USB component reports errors). The easiest way to create a functional USB configuration is by selecting from a preset. Select the Audio 1.0 – speaker (bare metal) preset. Figure 13. Selection of the Audio 1.0 speaker demo project configuration When you select the Audio 1.0 – speaker (bare metal) item, the whole configuration of the example is configured. Two interfaces are created: #0 – Audio_control #1 – Audio_streaming These interfaces contain all settings that are required for the USB Audio 1.0 speaker example. configuration of all audio units is provided in the Audio_control interface. The Device role configuration is also provided for the USB Audio demo example. See details of the provided settings in the previous chapter USB Audio concept. There is still the following error in the Problem view: Issue: USB Function Clock (USBPHY1_CLK) is inactive and USB module will not work. Level: Error Type: Validation Tool: Clocks Origin: Peripherals:BOARD_InitPeripherals Target: Clocks: BOARD_BootClockRUN Resource: USBPHY1_CLK   Figure 14. USB clock source error Right-click the error and select Show problem in BOARD_BootClockRun. Figure 15. Resolving of the USB clock source error The Clocks tool is opened, and you are navigated to the problem in the Details view. The USBPHY1 PLL clock is disabled by default (to save power). You can enable it by selecting the enabled value in the USBPHY1 clock output setting: Figure 16. Enabling of the USB clock source in the Clocks tool This setting enables the 480 MHz reference clock for USBPHY1 and the USB peripheral runs. Go back to the Peripherals tool. You can see that the error was resolved, and the code is generated. If you click the Update Code button, you can see what code is provided by the Config Tools. There are the following functions. Pins initialization functions: pin_mux.c/h – initialization of the routed pins for the peripherals (USB1, TMR3 in our use case). Clocks initialization functions: clock_config.c/h – initialization function for a configuration of the clock source, selectors, dividers, PLLs, and other system clock settings of the MCU.  A configuration of the USB1 clocks for PHY that was enabled is also provided. Peripherals initialization functions and the USB code example: peripherals.c/h  initialization functions for configured peripherals (USB1, TMR3 components). usb_device_composite.c/h contains initialized structures, initialization functions, device callback function, interrupt routine, and other USB middleware-related functions. usb_device_config.h contains USB middleware configurations (definitions) that are directly included in the USB middleware. usb_device_descriptor.c/hcontains definitions of the device descriptor, device configuration descriptor, initialized interface and endpoints configuration structures, function for device speed selection, and other USB device-related functions. usb_device_interface_0_audio_control.c/h contains the generated code example of the audio speaker. There is an application code for processing USB device requests, processing audio data, and configuration structure of the audio speaker example (buffer, runtime settings, …). When any of these generated files are customized (modified in the project), uncheck the file in the Update Code dialog. Otherwise, the changes would be lost. Figure 17. Update of the generated code in MCUXpresso IDE project The USB Audio example requires the Pins, Clocks, and Peripherals tool. Therefore, the generated code is used to replace the original code that is available in the default board support project. You can click the Cancel button and continue in the project configuration. 4.3.      DAC converter The i.MX RT1060 does not contain any DAC (Digital-to-Analog Converter). The MIMXRT1060 contains an external device that can be used to provide audio playback functionality.  This use case is already covered in the SDK Audio speaker example. You can create a simple DAC converter by using a timer of the MCU.  Select. The board provides Arduino headers that can be used for this demo purpose. The J23 header provides an output of the TMR3 – channels 0 and 1 (J23[6] and J23[5] pins). You can find this information in the Pins tool. Open the Pins tool and navigate to the Pins window. Select the BOARD_InitPins functional group (it is selected by default, and it is also included in the default initialization).To order the table lines according to the TMR peripherals, click the TMR column header. You can see that QTIMER3 (TMR3) timers #0 and #1 can be routed on Arduino header J23. When you click QTIMER3_TIMER0 and QTIMER3_TIMER1 in the TMR column, these timer outputs are routed automatically to the J23[6] and J23[5] pins on the Arduino header on the board. Figure 18. Routing of the timer pins in the Pins tool Switch to the Peripherals tool and add an instance of the Quad Timer (qtmr) component to the TMR3 peripheral. Check the checkbox of the TMR3 – the Quad Timer component is the only supported component and it is added automatically. The quad timer peripheral (TMR) supports four channels. You need two channels for each audio channel – Left and Right and the third channel for frequency. Figure 19. Quad timer component selection When the Quad Timer component is added, you can see the clock source – Bus clock 150 MHz. The USB Audio streaming contains 48 kHz. It means that the PWM must work at the multiplication of this sampling frequency. It simplifies the implementation of the DAC design. 150000000 / 48000 = 3125There are 3125 ticks of the timer per sample of audio data. To provide a better DAC output, the PWM must work on a frequency higher than 48 MHz. For example, the frequency can be 48 kHz * 5 = 240 kHz. It means that the PWM output frequency is 240 kHz and each audio sample value is set for 5 periods of the timer. However, it also means that the resolution of the timer is reduced to 3125 / 5 = 625 ticks. Finally, you have a 9-bits DAC converter that can be used for playback of audio data. The PWM output signal can be processed through a low-pass filter (R1, C1) with an output filter capacitor (C2) to remove some of the DC from the signal. Figure 20. Low-pass output filter fc=1/(2πRC) For example, use the following low pass filter: R1= 4700 Ω, C1 = 1.5 nF f c = 22575 Hz   TMR3 component configuration To provide two PWM channels, use the following configuration. First channel: Chanel ID: Left Primary timer/counter reference: Bus clock divided by 1 Counting operation: Rising edge of the primary source Timer mode initialization: PWM output PWM frequency/period: 240 kHz DMA/Interrupt mode: Polling Interrupt request: enable Compare 2 Second channel: Chanel ID: Right Primary timer/counter reference: Bus clock divided by 1 Counting operation: Rising edge of the primary source Timer mode initialization: PWM output PWM frequency/period: 240 kHz DMA/Interrupt mode: Polling Third channel for invoking the interrupt routine at sample frequency: Chanel ID: SampleFreq Primary timer/counter reference: Bus clock divided by 1 Counting operation: Rising edge of the primary source Timer mode initialization: Timer PWM frequency/period: 48 kHz DMA/Interrupt mode: Interrupt Interrupt request: enable Compare 1 Interrupt vector Enable interrupt: enabled (checked) Enable custom handle name: enabled (checked) Interrupt handler name: DAC_TMR_IRQ   Note: The interrupt of the SampleFreq channel is only used to load the compare load registers of both channels at the sampling frequency. The Digital-to-Analog conversion of both channels is synchronized and one simple interrupt routine can be used.  The Quad Timer components provide initialization but you must provide runtime functionality. Therefore, you must know the details of the PWM mode functionality (specified in the reference manual of the MCU). The PWM mode with variable frequency is driven by both compare registers. The second compare register provides a high-level period of the PWM period (duty), and the first compare register specifies the inactive part of the PWM period. The sum of these two compare registers must always be the computed resolution of the timer (625). An example of the initialization of compare registers can be found in the fsl_qtmr SDK driver, in the QTMR_SetupPwm() function.Compare registers are initialized before the counter/timer is started. The next values can be stored by using compare load registers. Thus, the loading of the compare registers is synchronized automatically by the timer itself (it is a part of the initialization setting in the fsl_qtmr driver). Therefore, the interrupt routine can be used for loading the audio data into compare load registers. The audio data is sent in the following PCM 16-bit format: one sample (4 bytes) 0 1 2 3 Left channel (low byte) Left channel (high byte) Right channel (low byte) Right channel (high byte) int16_t value (little endian format) int16_t value (little endian format)   Finally, configure the TMR3 peripheral in the following way: Figure 21. Quad timer configuration for the DAC In the Problems view, an error is reported. The error is caused by the missing fsl_qtmr SDK driver in the project (it was not added in the project wizard of the MCUXpresso IDE). Figure 22. Quad timer SDK driver error To fix the error, use the context menu of the error in the Problems view and select the Add SDK component “QTMR Driver” into the project “MIMXRT1062xxxA_USB_audio_speaker. Figure 23. Adding of the Quad timer SDK driver in the MCUXPresso project. When the option is selected, the update of the files is processed and the error disappears. The initialization of the application is done, and the generated code can be used in the project. Select the Update Code command and select update of the following files: Figure 24. Update of the generated code in MCUXpresso project All generated initialization files of Pins, Clocks, and Peripherals are stored to the project and the Develop perspective of the MCUXpresso IDE is automatically selected. You can check that all generated files are available in the project now. Note: When any of these generated files are later customized (modified in the project), the file must be unchecked in the Update Code dialog. Otherwise, the changes would be lost. 4.4.     Audio application design The USB Audio code example has been generated into the project and it works. But the playback of the audio data is not provided. Only the USB_Interface0AudioControlProcessNextAudioData() function is available in the source/usb_device_interface_0_audio_control.c source file. The received audio data is available in the internal USB_Interface0AudioControlDataBuff buffer and the index () of the newly received data is s_UsbDeviceAudioSpeaker->tdWriteNumberPlay. It is used to send data into the DAC converter.The DAC converter has not been implemented yet. There are just two PWM channels of the TMR3 that generate a zero-duty PWM output signal. Use the interrupt subroutine for the implementation of the audio playback. Copy the template of the interrupt routine from the TMR3 component in the Peripherals tool, see the Interrupt settings: Figure 25. Template of the interrupt service routine. When you click the Copy to clipboard button of the Handler template setting, you obtain the following code in the clipboard. /* TMR3_IRQn interrupt handler */ void DAC_TMR_IRQ(void) { /* Place your code here */ /* Add for ARM errata 838869, affects Cortex-M4, Cortex-M4F Store immediate overlapping exception return operation might vector to incorrect interrupt. */ #if defined __CORTEX_M && (__CORTEX_M == 4U) __DSB(); #endif } Place this code into the main program module source/MIMXRT1062xxxxA_USB_audio_speaker.c. It is used for the implementation of the main part of the application. The USB component contains a task call that must be placed into a loop of the main process. In this simple use case, use directly the main() function: Figure 26. USB device task function call code. /* * @brief Application entry point. */ int main(void) { /* Init board hardware. */ BOARD_InitBootPins(); BOARD_InitBootClocks(); BOARD_InitBootPeripherals(); #ifndef BOARD_INIT_DEBUG_CONSOLE_PERIPHERAL /* Init FSL debug console. */ BOARD_InitDebugConsole(); #endif /* Enter an infinite loop */ while(1) { USB_DeviceTasks(); } return 0 ; } 4.4.1.   Audio data processing The audio data can be read directly from the existing buffer. Therefore, you can update the implementation of the USB_Interface0AudioControlProcessNextAudioData() function and use parameters to pass a pointer to data and data size. See the following update of the function: #define SAMPLE_SIZE (AUDIO_FORMAT_CHANNELS * AUDIO_FORMAT_SIZE) void USB_Interface0AudioControlProcessNextAudioData(uint8_t **audioData, uint8_t *dataSize) { if ((s_UsbDeviceAudioSpeaker->audioSendTimes >= s_UsbDeviceAudioSpeaker->usbRecvTimes) && (s_UsbDeviceAudioSpeaker->startPlayHalfFull == 1)) { s_UsbDeviceAudioSpeaker->startPlayHalfFull = 0; s_UsbDeviceAudioSpeaker->speakerDetachOrNoInput = 1; } if (s_UsbDeviceAudioSpeaker->startPlayHalfFull) { /* * size of data packet that can be sent = FS_ISO_OUT_ENDP_PACKET_SIZE * pointer to data = USB_Interface0AudioControlDataBuff + s_UsbDeviceAudioSpeaker->tdWriteNumberPlay */ *audioData = &(USB_Interface0AudioControlDataBuff[s_UsbDeviceAudioSpeaker->tdWriteNumberPlay]); *dataSize = FS_ISO_OUT_ENDP_PACKET_SIZE / SAMPLE_SIZE; s_UsbDeviceAudioSpeaker->audioSendCount += FS_ISO_OUT_ENDP_PACKET_SIZE; s_UsbDeviceAudioSpeaker->audioSendTimes++; s_UsbDeviceAudioSpeaker->tdWriteNumberPlay += FS_ISO_OUT_ENDP_PACKET_SIZE; if (s_UsbDeviceAudioSpeaker->tdWriteNumberPlay >= AUDIO_SPEAKER_DATA_WHOLE_BUFFER_LENGTH * FS_ISO_OUT_ENDP_PACKET_SIZE) { s_UsbDeviceAudioSpeaker->tdWriteNumberPlay = 0; } } else { /* * size of data packet that can be sent = FS_ISO_OUT_ENDP_PACKET_SIZE * pointer to data = USB_Interface0AudioControlDataBuff */ *audioData = USB_Interface0AudioControlDataBuff; *dataSize = FS_ISO_OUT_ENDP_PACKET_SIZE / SAMPLE_SIZE; } }   The audioData pointer reference is set to point into the audio data buffer (USB_Interface0AudioControlDataBuff) that contains the audio data received from the host. The packet size is fixed. s_UsbDeviceAudioSpeaker->tdWriteNumberPlay is the index of the next data that must be converted by using DAC. Update the declaration of the function in the header file accordingly: /* * Function for procession of next audio data from the data buffer. It can be used as a callback. */ void USB_Interface0AudioControlProcessNextAudioData(uint8_t **audioData, uint8_t *dataSize); 4.4.2.   DAC interrupt routine The interrupt routine of the TMR3 peripheral provides the functionality of the DAC converter. It processes a stream of audio data packets and uses the sample values to control the duty of the output PWM signal (the first PWM channel as the left channel and the second PWM channel as the right channel). The sampling frequency is driven by the third channel of the TMR3 (the SampleFreq channel). See the implementation of the interrupt routine and related definitions: #include "usb_device_interface_0_audio_control.h" /* Size of one received packet */ #define PCM_PACKET_SIZE AUDIO_SAMPLING_RATE_KHZ /* PCM data pointer and sample index counter */ uint8_t *pcmData; uint8_t sampleIndex = PCM_PACKET_SIZE; /* Number of ticks for each PWM period */ #define PWM_PERIOD_LENGTH_IN_TICKS 625 /* size of one sample in streaming data (PCM format) */ #define SAMPLE_SIZE (USB_INTERFACE_1_AUDIO_STREAMING_SETTING_1_AUDIO_STREAM_SETTING_1_NUMBER_OF_CHANNEL * USB_INTERFACE_1_AUDIO_STREAMING_SETTING_1_AUDIO_STREAM_SETTING_1_SUBFRAME_SIZE) /* TMR3_IRQn interrupt handler */ void DAC_TMR_IRQ(void) { static uint16_t dutyValue; /* Add for ARM errata 838869, affects Cortex-M4, Cortex-M4F Store immediate overlapping exception return operation might vector to incorrect interrupt. */ #if defined __CORTEX_M && (__CORTEX_M == 4U) __DSB(); #endif /* Clear the Compare Flag */ TMR3_PERIPHERAL->CHANNEL[TMR3_SAMPLEFREQ_CHANNEL].CSCTRL &= ~TMR_CSCTRL_TCF1_MASK; /* audio data processing */ /* load next audio data when the whole packet has been sent */ if (sampleIndex >= PCM_PACKET_SIZE) { // load next data uint8_t dataLength; USB_Interface0AudioControlProcessNextAudioData(&pcmData, &dataLength); /* if new packet has been received */ if (dataLength == PCM_PACKET_SIZE) { sampleIndex = 0; } } /* if the buffer (packet) contain any data to be converted */ if (sampleIndex < PCM_PACKET_SIZE) { // PCM left channel data dutyValue = ((((int16_t*)pcmData)[SAMPLE_SIZE/2 * sampleIndex]) / 128) + 256; TMR3_PERIPHERAL->CHANNEL[TMR3_LEFT_CHANNEL].CMPLD2 = dutyValue; TMR3_PERIPHERAL->CHANNEL[TMR3_LEFT_CHANNEL].CMPLD1 = PWM_PERIOD_LENGTH_IN_TICKS - dutyValue; // PCM right channel data dutyValue = ((((int16_t*)pcmData)[(SAMPLE_SIZE/2 * sampleIndex) + 1]) / 128) + 256; TMR3_PERIPHERAL->CHANNEL[TMR3_RIGHT_CHANNEL].CMPLD2 = dutyValue; TMR3_PERIPHERAL->CHANNEL[TMR3_RIGHT_CHANNEL].CMPLD1 = PWM_PERIOD_LENGTH_IN_TICKS - dutyValue; /* next sample */ sampleIndex++; } }   The audio data is loaded (the pointer to audio data buffer is used) using the USB_Interface0AudioControlProcessNextAudioData() function. The whole packet of audio data is always provided (the PCM_PACKET_SIZE definition). When any audio data is available, the sample data is used to control the PWM duty of the left and right channels. The audio data is in the int16_t format, but the compare load register needs a 9-bit unsigned integer value. Therefore, these sample values are converted by the expression (see the source code above). 5.  Conclusion This tutorial provides an example of how you can use the USB component to generate a USB Audio 1.0 demo example and how you can use the generated interface to process the stream of audio data. The provided DAC example uses the interrupts and is not optimized. In a real application, use the DMA to process the audio stream data to reduce CPU usage. The volume control, mute, and suspending of the timers (when muted or zero bandwidth interface is selected) are other improvements that should be implemented in an advanced application. 6.  References USB Audio specification on https://usb.org: Universal Serial Bus Device Class Definition for Audio Devices Universal Serial Bus Device Class Definition for Audio Data Formats Universal Serial Bus Device Class Definition for Terminal Types   NXP application note and i.MX RT1060 documentation : How to Use Freescale USB Stack to Implement Audio Class Device i.MX RT1060 Processor Reference Manual MIMXRT1060/1064 Evaluation Kit Board Hardware User's Guide
查看全文
We are pleased to announce that MCUXpresso Config Tools 26.09 are now available. Downloads Also via installer in MCUXpresso for VS Code https://marketplace.visualstudio.com/items?itemName=NXPSemiconductors.mcuxpresso In order to use it with other toolchains, download the installer for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/config Please refer to https://docs.mcuxpresso.nxp.com/config/latest/ for installation and quick start guides. For online version, login into MCUXpresso site: MCUXpresso WEB Release Notes Full details at https://docs.mcuxpresso.nxp.com/config/latest/ Version 26.09 Framework Support public releases of “preliminary” EAR/PRC processor data. Added support for downloading all boards associated with a processor when downloading the processor.
查看全文
We are pleased to announce that MCUXpresso Config Tools 26.06 are now available. Downloads Also via installer in MCUXpresso for VS Code https://marketplace.visualstudio.com/items?itemName=NXPSemiconductors.mcuxpresso In order to use it with other toolchains, download the installer for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/config Please refer to https://docs.mcuxpresso.nxp.com/config/latest/ for installation and quick start guides. For online version, login into MCUXpresso site: MCUXpresso WEB Release Notes Full details at https://docs.mcuxpresso.nxp.com/config/latest/ Version 26.06 Update for the latest NPI support
查看全文
MCUXpresso Config Tools simplify and accelerate hardware configuration for NXP microcontrollers. This video walks through the full workflow - from project setup and device selection to a fully validated configuration - showing how quickly developers can get started using an intuitive, guided environment. It highlights the four core components - Pins, Clocks, Peripherals, and TEE -demonstrating their graphical interfaces, tight integration, and features like automatic configuration updates, live code generation, and issue detection with guided fixes. Overall, the tools enable faster, more reliable design by combining automation, validation, and ease of use, helping developers efficiently move from concept to working hardware configuration.
查看全文
We are pleased to announce that MCUXpresso Config Tools 26.03 are now available. Downloads It’s a part of MCUXpresso IDE https://www.nxp.com/mcuxpresso/ide/download In order to use it with other toolchains, download the installer for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/config Please refer to MCUXpresso Config Tools documentation for installation and quick start guides. For online version, login into MCUXpresso site: MCUXpresso WEB Release Notes Full details on the release (features, known issues...) Version 26.03 Clocks Hierarchy for local configuration element settings is supported. TEE Multicore Interrupt Handling for Single Security Domain is supported. Option to filter only user-defined memory regions is added. Interrupts are now separated into groups based on the core.
查看全文
In the MCUXpresso IDE, the config tools updates are disabled by default. To update Config Tools integrated in the MCUXpresso IDE follow these steps: Select Manage..., check MCUXpresso Config Tools Update Site and click Apply and Close     After enabling MCUXpresso Config Tools Update Site, use Help > Check for Updates for automatic update
查看全文
We are pleased to announce that MCUXpresso Config Tools v25.12 are now available. Downloads It’s a part of MCUXpresso IDE https://www.nxp.com/mcuxpresso/ide/download In order to use it with other toolchains, download the installer for all platforms, please login to our download site via: https://www.nxp.com/mcuxpresso/config Please refer to MCUXpresso Config Tools documentation for installation and quick start guides. For online version, login into MCUXpresso site: MCUXpresso WEB Release Notes Full details on the release (features, known issues...) General Project management of the SDK West project is supported since SDK version 25.12
查看全文
We are pleased to announce that MCUXpresso Config Tools v25.09 are now available. Downloads It’s a part of MCUXpresso IDE https://www.nxp.com/mcuxpresso/ide/download In order to use it with other toolchains, download the installer for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/config Please refer to MCUXpresso Config Tools documentation for installation and quick start guides. For online version, login into MCUXpresso site: MCUXpresso WEB Release Notes Full details on the release (features, known issues...) General • SDK West is supported as a new toolchain project starting with SDK version 25.09. • The Release Notes format is updated from plain text to markdown. • Fixed missing information about the toolchain project in the Dashboard dialog shown for the first time from VSCode. • The newly generated configuration includes the default NXP copyright notice and is licensed under the BSD-3-Clause license. Clocks – Supported input frequency setting
查看全文
How to set up Zephyr pins through MCUXpresso Config tools - create DTSI file for your custom board. Create a new project for Zephyr pins tool Interface introduction - where to find what? Create DTSI for custom boards MCUXpresso Config tools download page 
查看全文
We are pleased to announce that MCUXpresso Config Tools v25.03 are now available. Downloads It’s a part of MCUXpresso IDE (Version 25.03 can be updated from IDE) https://www.nxp.com/mcuxpresso/ide/download In order to use it with other toolchains, download the installer for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/config Please refer to MCUXpresso Config Tools documentation for installation and quick start guides. For online version, login into MCUXpresso site: MCUXpresso WEB Release Notes Full details on the release (features, known issues...) Version 25.03 • Output Paths Overrides for toolchain project is fixed. • "Filter source files" search bar with case-sensitive checkbox is removed. • TEE – Sort for Peripheral Configurations table is added.
查看全文
We are pleased to announce that MCUXpresso Config Tools v24.12 are now available. Downloads It’s a part of MCUXpresso IDE https://www.nxp.com/mcuxpresso/ide/download In order to use it with other toolchains, download the installer for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/config Please refer to MCUXpresso Config Tools documentation for installation and quick start guides. For online version, login into MCUXpresso site: MCUXpresso WEB Release Notes Full details on the release (features, known issues...) Version 24.12 • The creation (cloning) of the projects based on the SDK examples will no longer be supported in the future releases of the MCUXpresso Config Tools. Please start using the  MCUXpresso SDK CMake, Kconfig-based build, and configuration system to create MCUXpresso SDK standalone projects for the IAR Embedded Workbench, Keil uVision, GCC ARM Embedded, and/or CodeWarrior Development Studio toolchains. For detailed documentation, see the SDK Build And Configuration System documentation. • A new Radio option to create configuration for Zephyr in the New Configuration Wizard is added. • Clocks – Modular clocks initialization is supported. – Initialization mode is visible in the Clocks diagram and Details view. – A new Modular Initialization view for the configuration of initialization mode and core selection of the module is created. • TEE – The configuration and overview of areas with the same address and different address space is supported. – The Code generation can be toggled for global options groups. – The process for releasing ELE crypto before setting up TRDC is supported. – Support for MCUs with multiple SAUs, MPUs, NVIC triggers and interrupts (per core) is added. – A new tab to Security Access Configuration view for AXBS cross-bar switch configuration is added. – Flash Logical Window (FLW) configuration is supported. – TRDC Memory region checkers (MRC) restrictive overlap handling is supported. • Pins – The Miscellaneous tab for various Pins configuration options is added. – Filtering for routing dialogs is added. – Import of DTSI files is added.
查看全文
MCUXpresso Config Tools provide a USB configuration component that allows configuring USB settings in a graphical environment and generates a configuration and sample C code according to the configuration.  This tutorial shows how to create the configuration and sample code for the mouse and keyboard HID USB class for the RT1050 EVKB board and build it using the MCUXpresso IDE.  Note: The i.MX RT1050 EVKB board is used; however, the instructions are applicable in a similar way on other NXP EVK boards.   Prerequisites EVKB-IMXRT1050 board  MCUXpresso IDE (v.11.x)  The SDK package for the board (EVKB-IMRT1050)  must be imported and ready to use into MCUXpresso IDE (in the installed SDKs)  Steps 1. Launch MCUXpresso IDE and click Create a new C/C++ project…:  2. Select the EVKBIMXRT1050 board in the MIMXRT1050 processor folder, click  Next:  3. Specify the project name (for example, Test_USB). In the Middleware section, select USB > USB Device. Then click Finish: 4. Unfold the drop-down menu (down arrow) of the Config tools icon (X) and launch the Peripherals tool: 5. In the Peripherals view of the Peripherals tool, click the USB1 peripheral checkbox, ignore the error for now: 6. When the Add configuration component instance dialog appears, select the USB configuration component, click  OK: 6. The USB configuration component instance is added. As it requires the component for MPU initialization, click the + icon to add it.  Confirm the selection of the MPU utility component in the dialog that appeared. Keep the MPU component in the default setting and close its editor tab. 7. In the USB component settings editor, select the HID Keyboard (bare metal) in the preset drop-down list:   The keyboard interfaces are now added to the Supported interfaces list and pre-configured. 8. To add the mouse interface, click the + in the Supported interfaces section. Select the newly added item and change the Class item to HID.   9. Check that the Use case Preset for the interface #1 is set to 'Mouse':   10. The Problems view shows an error as the clock function is inactive by default. To enable it, right-click on the error and select “Enable USBPHY1 PLL clock”: Note:  Optionally, it's possible to click the Show the problem… and adjust it in the Clocks tool. 11. Click the Update Code button in the main toolbar, a pop-up appears: In the pop-up, confirm the code update by clicking the OK button: Build the application using the Build Command in the Quickstart Panel.   13. Now connect the board to the computer via the USB debug connection. Note: The EVKB-IMXRT1050 board provides multiple USB connectors. For flashing the application, it is it’s necessary to use the debug connection.  Also ensure that the board power is configured properly. There are several other configuration jumpers on the board. So in case the application cannot be flashed or debugged,  follow the user guide of the board. 14. To launch the application in the debugger, click the Debug text located in the bottom-left corner of the IDE.   This launches the debugging and the connected board should be detected. Confirm the selection of the debug probe.   Once the connection is successful, launch the application by clicking the Run button. If the application connects successfully, connect an additional USB cable from the application USB connector to your PC. The generated source code files contain a sample code that moves a mouse cursor in a loop and sends Home and End keys. After the cable is connected and the application runs, the movement of the mouse cursor and the text cursor moves left to right are visible.      
查看全文
We are pleased to announce that MCUXpresso Config Tools v16.1 are now available. Downloads It’s a part of MCUXpresso IDE https://www.nxp.com/mcuxpresso/ide/download In order to use it with other toolchains, download the installer for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/config Please refer to MCUXpresso Config Tools documentation for installation and quick start guides. For online version, login into MCUXpresso site: MCUXpresso WEB Release Notes Full details on the release (features, known issues...) • Fixed missing information about the toolchain project in the Overview dialog shown for the first time. – The Update code dialog opened from the Overview dialog shows the *.cgen.yml file. • Incorrect detection of the selected toolchain file after the command-line execution is fixed. The problem occurs for the folders with multiple different toolchain project files. • Creating a configuration from the toolchain project that does not contain the tool configuration in the MEX file or in the tools source file is allowed. • Open-CMSIS generator support – The usage of the path information from *.cbuild-gen-idx.yml for generation of the *.cgen.yml file is supported. • Clocks – Disabling enabled clock outputs that have settings with shared bit-fields after reopening the configuration is fixed. – Clock slices with multiple outputs are supported. • TEE – An incorrect number of the MPU region attributes shown for the configuration of RT1180 is fixed. – An incorrect domain visibility and tab names when DAC is disabled on RT1180 is fixed.
查看全文
We are pleased to announce that MCUXpresso Config Tools v16.0 are now available. Downloads It’s a part of MCUXpresso IDE https://www.nxp.com/mcuxpresso/ide/download In order to use it with other toolchains, download the installer for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/config Please refer to MCUXpresso Config Tools documentation for installation and quick start guides. For online version, login into MCUXpresso site: MCUXpresso WEB Release Notes Full details on the release (features, known issues...) The product is based on Eclipse 2023-12 - A new command-line argument ( -UpdateCode) has been added. It performs the same action as the Update Code button in the user interface. It must be used with -HeadlessTool. - The command-line argument -CreateFromProject is improved, it no longer requires the -HeadlessTool argument and opens the toolchain project in the UI. - The command-line arguments -CreateFromProject and -ImportProject are improved. They no longer allow setting the toolchain project file path (for example, *.cbuild-gen-idx.yml, *.uvprojx, *.ewp, CMakeLists.txt) directly. TEE – The query for pins labels and routed signals is updated to work on the new NPI. – Global tool options now support enum, boolean, and string with the ability to define the regex validator. – Access templates are now greyed out when the global ones are used. – The legacy source names option is disabled when ROM output is selected. – MPU tabs are now sorted by top domain index and then alphabetically. – The correct representation of TRDC domains is implemented by removing mix domains. – Peripheral areas are now correctly stored within the correct tab. – The side-channel attack warning is added to the RAM security settings. – The Trigger tab for configuration of the ITRC register RW fields is added. PLU – Minor bug fixes Peripherals – Support for unique identification of configuration components is finished. – Support for settings with indentation, but no label content is added. Pins – Simultaneous routing detection (routing of one signal may result in multiple signals being routed based on the same register settings) is added. In that case, such signals are offered to be added into the configuration. – Support of internal pins that are not available on the package is added. Clocks – Creation of the clock model has been accelerated. Open-CMSIS generator – The open-CMSIS solution is supported as a new toolchain. – The generation of the .cgen.yml file is supported. – The generation of new source files inside the project output folder is supported. – The location of the MEX file inside the project output folder is supported.
查看全文
We are pleased to announce that MCUXpresso Config Tools v15.1 are now available. Downloads It’s a part of MCUXpresso IDE https://www.nxp.com/mcuxpresso/ide/download In order to use it with other toolchains, download the installer for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/config Please refer to MCUXpresso Config Tools documentation for installation and quick start guides. For online version, login into MCUXpresso site: MCUXpresso WEB Release Notes Full details on the release (features, known issues...) Config Tools v15.1 • On MacOS aarch64, the missing Overview is fixed. • TEE – Pin tables now only contain items for specific configuration (mask/security/interrupts).   Community MCUXpresso Config Tools      
查看全文
We are pleased to announce that MCUXpresso Config Tools v15.0 are now available. Downloads It’s a part of MCUXpresso IDE https://www.nxp.com/mcuxpresso/ide/download In order to use it with other toolchains, download the installer for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/config Please refer to MCUXpresso Config Tools documentation for installation and quick start guides. For online version, login into MCUXpresso site: MCUXpresso WEB Release Notes Full details on the release (features, known issues...) Config Tools v15.0 • The product is based on Eclipse 2023-06. • Support for SDK 2.15 in the Project cloner and Detect toolchain project is added. TEE – Setting a security level for a special three-state model is improved. – Validation for the uniqueness of DID, match and mask input for XRDC2 is added. – Default global access templates are now created if needed by checkers and missing within MEX. PLU – An error is now reported when a Verilog code contains a signal that was not declared. – A capability to select one input for some logic gates for which it does not make sense is removed. – A button to erase the whole diagram is added. – Support to keep intermediate files generated by an external program for debugging purposes is added. – The behavior of selecting the LUT type Custom to keep the previous logic table and added buttons to set it to zeros or ones is changed. – The status bar to the schematic view is added. Peripherals – A bug with the documentation view in a version integrated to the MCUXpresso IDE is fixed. – The mechanism that handles opening views that were opened in the previous session to work with identification of the configuration instead of its location on disk is updated. – A new optional experimental loading mechanism for components is prepared. This mechanism will be used by default in the next release. Pins – Validation to ensure that elements can be configured by the selected core is added.– Rows are sorted in the Peripheral Signals routing dialog. – The connected pins column in External User Signals always shows the pin's full name. – The missing scroll bar in the External User Signals view is fixed.   Clocks – Support for multicore code generation is added. – Global configuration elements now support tree structure and can be categorized. – Fractional PLL now supports a custom range and negative numerator. – Scrolling in the clock diagram by pressing the mouse wheel (drag and drop) is supported.   DCD – An issue with the code generation that stopped working after drag and drop of a group is fixed.   MCUXpresso IDE integration – Support for multiple MEX files within one project (toolbar Project combo + autoload MEX on IDE startup) is improved.   Community MCUXpresso Config Tools  
查看全文
We are pleased to announce that MCUXpresso Config Tools v14.0 are now available. Downloads It’s a part of MCUXpresso IDE https://www.nxp.com/mcuxpresso/ide/download In order to use it with other toolchains, download the installer for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/config Please refer to MCUXpresso Config Tools documentation for installation and quick start guides. For online version, login into MCUXpresso site: MCUXpresso WEB Release Notes Full details on the release (features, known issues...) Config Tools v14.0 The product is based on Eclipse 2022-12 Open JDK 17 is updated. Batch processing on command line is supported. Support for SDK 2.14 in Project cloner and Detect toolchain project is added. Link to a toolchain project on a location different than .mex file is added. The command for discarding changes and reloading .mex (MCUXpresso IDE) is added. Quick fix for errors allows setting the "Called by the default initialization function" flag when it would fix an error. Search functionality to Code Preview is added. TEE MCXN-947 combination of AHBSC with TRDC (MBC) is supported. Export TEE registers via wizard or command line is available. Boot ROM hiding feature is supported. Tier mode for TRDC is supported. Domain ambivalence for RDC masters is added. Master-specific memory alias Validation for A28 bit of MPU region address is added. Memory map filters are aligned with Arm terminology. Status bar is united with other tools. PLU Tools used for Verilog synthesis and model optimization are replaced. Linux, Mac, and Apple silicon platforms are supported. Newer versions of Verilog standard are supported. Creation of flip-flop circuits outside Direct mode is supported. Support for special comment that contains mapping information is added. Support for Verilog code resynthesis is added in the new command-line option. Buttons in Schematic view are reordered to groups of related buttons on each row. Information from Verilog synthesis and model optimization tools is added to the error dialog. Peripherals Migration of Peripherals tool components to the latest supported version on current MCU in command line is supported. User information on the dependency of the tool on another tool disabled in the configuration is improved. Migration report generation is supported. The generated report may contain instructions on how to handle incompatible changes between versions of the configured SDK component. Opening links to websites in the Documentation view in an external browser is supported. Pins Labels defined for Expansion header pins can be set as identifiers of the routed pin. Expansion headers can be locked for editing. Expansion headers and boards are added to the HTML and CSV reports. Columns from Routing Details can be added to the External User Signals view. New External User Signals can be created for all routed pins that are missing in the signals table. Clocks Support for the same frequencies settings from different source for internal clocks is added. Community MCUXpresso Config Tools
查看全文
We are pleased to announce that MCUXpresso Config Tools v13.1 are now available. Downloads It’s a part of MCUXpresso IDE https://www.nxp.com/mcuxpresso/ide/download In order to use it with other toolchains, download the installer for all platforms, please login to our download site via:  https://www.nxp.com/mcuxpresso/config Please refer to MCUXpresso Config Tools documentation for installation and quick start guides. For online version, login into MCUXpresso site: MCUXpresso WEB Release Notes Config Tools v13.1 Pins tool Fix incomplete routing of deinit functions Update of data for Config Tools v13 and v13.1 General Update of MC56F80xxx support to the latest processor data Fix of missing MIMXRT1170-EVKB board configuration Pins tool Bug fix of incorrect labels of PMOD expansion header in Pins tool Peripherals tool Register init. components Bug fix of PLU Register init. component on LPC550x/S0x processors Bug fix of Peripherals tool FlexIO RIC SDK init. components Support of fcb Peripherals tool component for RT104x and RT116x processors Memory validation tool Update of DDR tool data for i.MX8M and i.MX93 processors Update of Memory validation tool data for Layerscape and i.MX RT processors Community MCUXpresso Config Tools  
查看全文