MCUXpresso Config Tools v24.12 Now Available

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso Config Tools v24.12 Now Available

MCUXpresso Config Tools v24.12 Now Available

We are pleased to announce that MCUXpresso Config Tools v24.12 are now available.

Downloads

Release Notes

Full details on the release (features, known issues...)

Version 24.12


• The creation (cloning) of the projects based on the SDK examples will no longer be supported in the future releases of the MCUXpresso Config Tools. Please start using the  MCUXpresso SDK CMake, Kconfig-based build, and configuration system to create MCUXpresso SDK standalone projects for the IAR Embedded Workbench, Keil uVision, GCC ARM Embedded, and/or CodeWarrior Development Studio toolchains. For detailed documentation, see the SDK Build And Configuration System documentation.
• A new Radio option to create configuration for Zephyr in the New Configuration Wizard is added.
Clocks
– Modular clocks initialization is supported.
– Initialization mode is visible in the Clocks diagram and Details view.
– A new Modular Initialization view for the configuration of initialization mode and core selection of the module is created.
TEE
– The configuration and overview of areas with the same address and different address space is supported.
– The Code generation can be toggled for global options groups.
– The process for releasing ELE crypto before setting up TRDC is supported.
– Support for MCUs with multiple SAUs, MPUs, NVIC triggers and interrupts (per core) is added.
– A new tab to Security Access Configuration view for AXBS cross-bar switch configuration is added.
– Flash Logical Window (FLW) configuration is supported.
– TRDC Memory region checkers (MRC) restrictive overlap handling is supported.
Pins
– The Miscellaneous tab for various Pins configuration options is added.
– Filtering for routing dialogs is added.
– Import of DTSI files is added.

No ratings
Version history
Last update:
4 weeks ago
Updated by: