MCUXpresso Config Tools v16.1 Now Available

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso Config Tools v16.1 Now Available

MCUXpresso Config Tools v16.1 Now Available

We are pleased to announce that MCUXpresso Config Tools v16.1 are now available.

Downloads

Release Notes

Full details on the release (features, known issues...)

• Fixed missing information about the toolchain project in the Overview dialog shown for the first time.
– The Update code dialog opened from the Overview dialog shows the *.cgen.yml file.
• Incorrect detection of the selected toolchain file after the command-line execution is fixed. The problem occurs for the folders with multiple different toolchain project files.
• Creating a configuration from the toolchain project that does not contain the tool configuration in the MEX file or in the tools source file is allowed.
• Open-CMSIS generator support
– The usage of the path information from *.cbuild-gen-idx.yml for generation of the *.cgen.yml file is supported.
• Clocks
– Disabling enabled clock outputs that have settings with shared bit-fields after reopening the configuration is
fixed.
– Clock slices with multiple outputs are supported.
• TEE
– An incorrect number of the MPU region attributes shown for the configuration of RT1180 is fixed.
– An incorrect domain visibility and tab names when DAC is disabled on RT1180 is fixed.

No ratings
Version history
Last update:
‎09-26-2024 06:48 AM
Updated by: