Downloads
- It’s a part of MCUXpresso IDE
- In order to use it with other toolchains, download the installer for all platforms, please login to our download site via:
-
Please refer to MCUXpresso Config Tools documentation for installation and quick start guides.
-
For online version, login into MCUXpresso site:
Release Notes
Full details on the release (features, known issues...)
Config Tools v14.0
- The product is based on Eclipse 2022-12
- Open JDK 17 is updated.
- Batch processing on command line is supported.
- Support for SDK 2.14 in Project cloner and Detect toolchain project is added.
- Link to a toolchain project on a location different than .mex file is added.
- The command for discarding changes and reloading .mex (MCUXpresso IDE) is added.
- Quick fix for errors allows setting the "Called by the default initialization function" flag when it would fix an error.
- Search functionality to Code Preview is added.
- TEE
- MCXN-947 combination of AHBSC with TRDC (MBC) is supported.
- Export TEE registers via wizard or command line is available.
- Boot ROM hiding feature is supported.
- Tier mode for TRDC is supported.
- Domain ambivalence for RDC masters is added.
- Master-specific memory alias
- Validation for A28 bit of MPU region address is added.
- Memory map filters are aligned with Arm terminology.
- Status bar is united with other tools.
- PLU
- Tools used for Verilog synthesis and model optimization are replaced.
- Linux, Mac, and Apple silicon platforms are supported.
- Newer versions of Verilog standard are supported.
- Creation of flip-flop circuits outside Direct mode is supported.
- Support for special comment that contains mapping information is added.
- Support for Verilog code resynthesis is added in the new command-line option.
- Buttons in Schematic view are reordered to groups of related buttons on each row.
- Information from Verilog synthesis and model optimization tools is added to the error dialog.
- Peripherals
- Migration of Peripherals tool components to the latest supported version on current MCU in command line is supported.
- User information on the dependency of the tool on another tool disabled in the configuration is improved.
- Migration report generation is supported.
- The generated report may contain instructions on how to handle incompatible changes between versions of the configured SDK component.
- Opening links to websites in the Documentation view in an external browser is supported.
- Pins
- Labels defined for Expansion header pins can be set as identifiers of the routed pin.
- Expansion headers can be locked for editing.
- Expansion headers and boards are added to the HTML and CSV reports.
- Columns from Routing Details can be added to the External User Signals view.
- New External User Signals can be created for all routed pins that are missing in the signals table.
- Clocks
- Support for the same frequencies settings from different source for internal clocks is added.
Community