Layerscape Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Layerscape Knowledge Base

Discussions

Sort by:
Follow these steps to update the Linux kernel image and device tree on the SD card.  Compiling Linux kernel images and device tree On Linux host, clone the repository with Linux kernel image and device tree: $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/linux $ cd linux $ git checkout -b <new branch> <start point> For example, $ git checkout -b LSDK-18.09-V4.14 LSDK-18.09-V4.14 where LSDK-18.09-V4.14 refers to a tag in the format LSDK-<LSDK version>-V<kernel version> $ make ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- defconfig lsdk.config If you want to make changes to the device tree, open and edit arch/arm64/boot/dts/freescale/fsl-ls1088a-rdb.dts $ make ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- The binary kernel image Image and compressed kernel image Image.gz are in arch/arm64/boot/. The device tree blob fsl-ls1088a-rdb.dtb is in arch/arm64/boot/dts/freescale/. Copying the compiled kernel images and device tree to the SD card Plug the SD card into the Linux host machine. sudo fdisk -l to list the disks that are accessible to the computer. Mount the SD card partition that contains Linux kernel images and device tree. sudo mkdir <mount_location> sudo mount /dev/sdX <mount_location> Use the command cat /proc/partitions to see a list of devices and their sizes to make sure that the correct device names have been chosen. The SDHC storage drive in the Linux PC is detected as /dev/ sdX, where X is a letter such as a, b, c. Make sure to choose the correct device name, because data on this device will be replaced. If your Linux host machine supports read/write SDHC card directly without an extra SDHC card reader device, the device name of SDHC card is typically mmcblk0. Replace Image, Image.gz, and fsl-ls1088a-rdb.dtb on the SD card with the new files compiled in the steps above. sudo cp /linux/arch/arm64/boot/Image /linux/arch/arm64/boot/Image.gz /linux/arch/arm64/boot/dts/freescale/fsl-ls1088a-rdb.dtb <mount_location> sudo umount /dev/sdX Plug the SD card into LS1088ARDB/LS1088ARDB-PB and boot the board to Ubuntu using the SD card. If U-Boot does not find LSDK on the SD card, it will boot TinyDistro from lsdk_linux_arm64_ tiny.itb stored on the SD card.
View full article
The BareMetal framework targets to support the scenarios that need low latency, real-time response, and high-performance. There is no OS running on the cores and customer-specific application runs on that directly. This document describes how to develop customer-specific application based on BareMetal framework. The directory “app” stored in u-boot repository includes the use cases for testing GPIO, I2C, IRQ init, QSPI, Ethernet, USB, PCIe, CAN, ENETC and SAI features. 1. GPIO use case 2. I2C use case 3. IRQ use case 4. QSPI Use case 5. Ethernet use case 6. USB Use case 7. PCIe use case 8. CAN Use Case 9. ENETC Use Case 10. SAI Use Case 11. Build and Run the Baremetal Application
View full article
Follow these steps to update the Linux kernel image and device tree for LX2160ARDB on an SD card.  NOTE: Below steps are valid for both LX2160ARDB Rev 1.0 and Rev 2.0 revisions. STEP 1: Compiling Linux kernel images and device tree On Linux host, clone the repository with Linux kernel image and device tree: $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/linux $ cd linux $ git checkout -b <new branch> <start point> For example, $ git checkout -b LSDK-20.04-V5.4 LSDK-20.04-V5.4 where LSDK-20.04-V5.4 refers to a tag in the format LSDK-<LSDK version>-V<kernel version> $ make ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- defconfig lsdk.config If you want to make changes to the device tree, open and edit arch/arm64/boot/dts/freescale/fsl-lx2160a-rdb.dts $ make ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- The binary kernel image Image and compressed kernel image Image.gz are in arch/arm64/boot/. The device tree blob fsl-lx2160a-rdb.dtb is in arch/arm64/boot/dts/freescale/. STEP2: Copying the compiled kernel images and device tree to the SD card   Plug the SD card into the Linux host machine. sudo fdisk -l to list the disks that are accessible to the computer. Mount the SD card partition that contains Linux kernel images and device tree. sudo mkdir <mount_location> sudo mount /dev/sdX <mount_location> For example: $ sudo mkdir /carddata $ sudo mount /dev/mmcblk0p2 /carddata   NOTE: Use the command cat /proc/partitions to see the list of devices, their partitions along with their sizes to make sure that the correct device and partition name have been chosen. The eMMC storage drive in the Linux PC is detected as /dev/sdX, where X is a letter such as a, b, c. Make sure to choose the correct device name, because data on this device will be replaced. If your Linux host machine supports read/write SD card directly without an extra SD card reader device, the device name of SD card is typically mmcblk0. In general, the Linux kernel images and device tree are stored in the second partition of the SD device (mmcblk0p2). For detail on storage layout on SD/eMMC/USB/SATA for LSDK images deployment, refer to section "LSDK memory layout and Userland" in Layerscape Software Development Kit User Guide. Replace Image, Image.gz, and fsl-lx2160a-rdb.dtb on the SD card with the new files compiled in the steps above. $ sudo cp /linux/arch/arm64/boot/Image /linux/arch/arm64/boot/Image.gz /linux/arch/arm64/boot/dts/freescale/fsl-lx2160a-rdb.dtb <mount_location> For example: $sudo cp /linux/arch/arm64/boot/Image /linux/arch/arm64/boot/Image.gz /linux/arch/arm64/boot/dts/freescale/fsl-lx2160a-rdb.dtb /carddata Unmount the card. For example: sudo umount /dev/mmcblk0p2 Plug the SD card into LX2160ARDB and boot the board. At U-Boot, run the following command to boot the board to LSDK distro using the SD card. => run bootcmd_mmc0 If U-Boot does not find LSDK on the SD card, it will boot TinyDistro from lsdk_linux_arm64_ tiny.itb stored on the SD card.
View full article
Prerequisites: The board should be running Linux and connected to terminal console. Note: For log level debug support, the restool version should be LSDK-2003-RC1 or above and MC version should be 10.20.0 or above. To check restool version: $ root@localhost:~# restool -v restool LSDK-20.04 To check MC version: root@localhost:~# restool -m MC firmware version: 10.24.0 For debugging, use the ls-debug script available in the LSDK rootfs. There is no need to create the debug object. ls-debug -h ls-debug options -h, --help ls-debug help information -ts, --timestamp=X Enable/Disable timestamp printing, X is ON or OFF -c, --console=X Enable/Disable printing in UART console, X is ON or OFF -l, --log=X Enable/Disable printing in DDR log, X is ON or OF -u, --uart=X Set UART ID of the console, X = [0 - 4], 0 = OFF -ll, --level=X Set logging level, X = [0 - 5] 0: Global 1: Debug 2: Info 3: Warning 4: Error 5: Critical -m, mem, --memory Dump information about memory modules available dpxy.z Dump information about MC respective object   For example, to enable logging in console with log level INFO: $ ls-debug --log=on --console=on --level=2 dpdbg.0 created DDR log printing ON UART console printing ON Log level set to 2 $ root@localhost:~# ls-debug --memory Memory dumped information available in MC log/console $ root@localhost:~# cat `find /dev/ -name "*mc_console"` [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_get_obj for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dpdbg_open on DPDBG [I, RESMAN] Handling command: dpdbg_dump on DPDBG [I, DPNI] Memory info: [I, DPNI] MC DDR #1 cacheable memory [I, DPNI] Total: 134217728 bytes [I, DPNI] Used: 14802708 bytes [I, DPNI] Free: 119415020 bytes [I, DPNI] MC DDR #1 non-cacheable memory [I, DPNI] Total: 50331648 bytes [I, DPNI] Used: 27680 bytes [I, DPNI] Free: 50303968 bytes [I, DPNI] DMEM1 memory [I, DPNI] Total: 81920 bytes [I, DPNI] Used: 27168 bytes [I, DPNI] Free: 54752 bytes [I, DPNI] DMEM2 memory [I, DPNI] Total: 81920 bytes [I, DPNI] Used: 27168 bytes [I, DPNI] Free: 54752 bytes [I, DPNI] DDR #1 memory [I, DPNI] Total: 1610612736 bytes [I, DPNI] Used: 143163392 bytes [I, DPNI] Free: 1467449344 bytes [I, DPNI] PEB memory [I, DPNI] Total: 2097152 bytes [I, DPNI] Used: 524288 bytes [I, DPNI] Free: 1572864 bytes [I, DPNI] DP-DDR memory [I, DPNI] Total: 4294967296 bytes [I, DPNI] Used: 0 bytes [I, DPNI] Free: 4294967296 bytes [I, RESMAN] Handling command: dpdbg_close on DPDBG [I, RESMAN] Handling command: dprc_close for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_set_irq_mask for DPRC 1 on portal id 0 [I, RESMAN] Handling command: dprc_set_irq_enable for DPRC 1 on portal id 0 root@localhost:~#
View full article
This how-to topic is applicable only for LSDK 18.09 and older releases.  For LSDK 18.12 and newer releases, refer LS1088ARDB-PB - How to deploy TF-A binaries in QSPI NOR flash. Follow these steps to update the U-Boot binary in QSPI NOR flash.  Prerequisites  Ubuntu 18.04 64-bit should be installed on the Linux host machine for building LSDK 18.06 or LSDK 18.09 U-Boot binary. qixis_reset boots the board from QSPI NOR flash0 and qixis_reset altbank boots the board from QSPI NOR flash1. sf probe 0:1 means that the alternate bank will be written to. So, if the board boots from QSPI NOR flash0 and sf probe 0:1 is entered at the U-Boot prompt, the commands that follow will program QSPI NOR flash1.   Compiling U-Boot binary Clone the u-boot repository compile the U-Boot binary for QSPI boot. $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/u-boot.git $ cd u-boot $ git checkout -b <new branch name> LSDK-<LSDK version>. For example, $ git checkout -b LSDK-18.09 LSDK-18.09  $ export ARCH=arm64 $ export CROSS_COMPILE=aarch64-linux-gnu- $ make distclean Run either of following depending on the board you are using:  For LS1088ARDB: $ make ls1088ardb_qspi_defconfig For LS1088ARDB-PB: make ls1088ardb_pb_qspi_defconfig If required, make changes to the U-Boot files. $ make If the make command shows the error "*** Your GCC is older than 6.0 and is not supported", ensure that you are using Ubuntu 18.04 64-bit version for building LSDK 18.06 or LSDK 18.09 U-Boot binary.  The compiled U-Boot image, u-boot.bin, is available at u-boot/. Flashing U-Boot binary to QSPI NOR flash Boot LS1088ARDB/LS1088ARDB-PB from QSPI. Ensure that the switches are set to boot the board from QSPI. For booting from the QSPI, SW1[1:8] + SW2[1] = 0011_0001_X Boot from QSPI NOR flash0: => qixis_reset For example: For LS1088ARDB, in boot log, you’ll see: Board: LS1088A-RDB, Board Arch: V1, Board version: C, boot from QSPI:0 For LS1088ARDB-PB, in boot log, you'll see: Board: LS1088ARDB-PB, Board Arch: V1, Board version: A, boot from QSPI:0 U-Boot image can be loaded to LS1088ARDB/LS1088ARDB-PB from a TFTP server or from a mass storage device (SD, USB, or SATA). Option 1: Load image from the TFTP server Set up Ethernet connection When board boots up, U-Boot prints a list of enabled Ethernet interfaces. DPMAC1@xgmii, DPMAC2@xgmii, DPMAC3@qsgmii, DPMAC4@qsgmii, DPMAC5@qsgmii, DPMAC6@qsgmii, DPMAC7@qsgmii, DPMAC8@qsgmii, DPMAC9@qsgmii, DPMAC10@qsgmii Set server IP to the IP of the host machine on which you have configured the TFTP server.  => setenv serverip <ipaddress1> Set ethact and ethprime as the Ethernet interface connected to the TFTP server. See LS1088ARDB/LS1088RDB-PB Ethernet port mapping for the mapping of Ethernet port names appearing on the chassis front panel with the port names in U-Boot and Linux. => setenv ethprime <name of interface connected to TFTP server> For example: => setenv ethprime DPMAC3@qsgmii => setenv ethact <name of interface connected to TFTP server> For example: => setenv ethact DPMAC3@qsgmii Set IP address of the board. You can set a static IP address or, if the board can connect to a dhcp server, you can use the dhcp command. Static IP address assignment: => setenv ipaddr <ipaddress2> => setenv netmask <subnet mask> Dynamic IP address assignment: => dhcp Save the settings. => saveenv Check the connection between the board and the TFTP server. => ping $serverip Using DPMAC3@qsgmii device host 192.168.1.1 is alive Load U-Boot image from the TFTP server Program QSPI NOR flash1: => sf probe 0:1 Flash U-Boot image: => tftp 0xa0000000 u-boot.bin => print filesize filesize=aa4b4 Program U-Boot image to QSPI NOR flash: => sf erase 0x100000 +$filesize && sf write 0xa0000000 0x100000 $filesize.  Address 0x100000 is the location of U-Boot in QSPI NOR flash. For the complete flash memory layout for the PPA boot flow, refer Flash layout for old boot flow with PPA. Boot from QSPI NOR flash1: => qixis_reset altbank For LS1088ARDB, in boot log, you’ll see: Board: LS1088A-RDB, Board Arch: V1, Board version: C, boot from QSPI:1 For LS1088ARDB-PB, in boot log, you'll see: Board: LS1088ARDB-PB, Board Arch: V1, Board version: A, boot from QSPI:1 Ensure that SD card, USB flash drive, or SCSI hard disk installed with LSDK Ubuntu distribution is plugged into the board to boot the board to Ubuntu. If U-Boot does not find LSDK on a mass storage device, it will boot TinyDistro from lsdk_linux_arm64_ tiny.itb stored in QSPI NOR flash. Option 2: Load image from partition on mass storage device (SD, USB, or SATA) Select mass storage device to use. => mmc rescan => mmc info Or => usb start => usb info Or => scsi scan => scsi info Optional – List files on storage device => ls mmc <device:partition> For example: => ls mmc 0:2 Or => ls usb <device:partition> For example: => ls usb 0:1 Or => ls scsi <device:partition> For example: => ls scsi 0:2 Program QSPI NOR flash1: => sf probe 0:1 Load U-Boot image from the storage device => load mmc 0:2 a0000000 <image name> => print filesize For example: => load mmc 0:2 a0000000 u-boot.bin => print filesize filesize=aaa34 Or => load usb 0:2 a0000000 <image name> => print filesize Or => load scsi 0:2 a0000000 <image name> => print filesize Program image to QSPI NOR flash: => sf erase 0x100000 +$filesize && sf write 0xa0000000 0x100000 $filesize  Address 0x100000 is the location of U-Boot in QSPI NOR flash. For the complete flash memory layout for the PPA boot flow, refer Flash layout for old boot flow with PPA.  Boot from QSPI NOR flash1: => qixis_reset altbank For LS1088ARDB, in boot log, you’ll see: Board: LS1088A-RDB, Board Arch: V1, Board version: C, boot from QSPI:1 For LS1088ARDB-PB, in boot log, you'll see: Board: LS1088ARDB-PB, Board Arch: V1, Board version: A, boot from QSPI:1 Ensure that SD card, USB flash drive, or SCSI hard disk installed with LSDK Ubuntu distribution is plugged into the board to boot the board to Ubuntu. If U-Boot does not find LSDK on a mass storage device, it will boot TinyDistro from lsdk_linux_arm64_ tiny.itb stored in QSPI NOR flash.
View full article
Follow these steps to update the DPAA1 FMan ucode image in QSPI NOR flash.  cpld reset boots the board from QSPI NOR flash0 and cpld reset altbank boots the board from the QSPI NOR flash1. sf probe 0:1 means that the alternate bank will be written to. So, if the board boots from QSPI NOR flash0 and sf probe 0:1 is entered at the U-Boot prompt, the commands that follow will program QSPI NOR flash1.   Obtaining DPAA1 FMan ucode image Clone the qoriq-fm-ucode repository. $ git clone https://github.com/NXP/qoriq-fm-ucode.git $ cd qoriq-fm-ucode $ git checkout LSDK-<LSDK version>. For example, $ git checkout LSDK-18.12 The prebuilt FMan ucode images, fsl_fman_ucode_ls1046_r1.0_<microcode version>.bin, are at qoriq-fm-ucode/. In the binary file, ls1046_r1.0 refers to the LS1046A silicon revision 1.0. See qoriq-fm-ucode/readme for a description of the ucode version numbers. Programming FMan ucode image to QSPI NOR flash FMan ucode image can be loaded to LS1046ARDB from a TFTP server or from a mass storage device (SD, USB, or SATA). Option 1: Load image from the TFTP server Boot LS1046ARDB from QSPI NOR flash. Ensure that the switches are set to boot the board from QSPI. For booting from QSPI, SW5[1:8] = 00100010 Boot from QSPI NOR flash0: => cpld reset In boot log, you’ll see: Board: LS1046ARDB, boot from QSPI vBank 0 Set up Ethernet connection When board boots up, U-Boot prints a list of enabled Ethernet interfaces. FM1@DTSEC3 [PRIME], FM1@DTSEC4, FM1@DTSEC5, FM1@DTSEC6, FM1@TGEC1, FM1@TGEC2 Set server IP to the IP of the host machine on which you have configured the TFTP server.  => setenv serverip <ipaddress1> Set ethact and ethprime as the Ethernet interface connected to the TFTP server. See LS1046ARDB Ethernet port mapping for the mapping of Ethernet port names appearing on the chassis front panel with the port names in U-Boot and Linux. => setenv ethprime <name of interface connected to TFTP server> For example: => setenv ethprime FM1@DTSEC4 => setenv ethact <name of interface connected to TFTP server> For example: => setenv ethact FM1@DTSEC4 Set IP address of the board. You can set a static IP address or, if the board can connect to a dhcp server, you can use the dhcp command. Static IP address assignment: => setenv ipaddr <ipaddress2> => setenv netmask <subnet mask> Dynamic IP address assignment: => dhcp Save the settings. => saveenv Check the connection between the board and the TFTP server. => ping $serverip Using FM1@DTSEC4 device host 192.168.1.1 is alive Load FMan ucode image from the TFTP server Program QSPI NOR flash1: => sf probe 0:1 Flash the FMan ucode image: => tftp 0x80000000 <path to FMan ucode>/fsl_fman_ucode_ls1046_r1.0_<ucode version>.bin => print filesize filesize=7f5c Program the FMan ucode image to QSPI NOR flash: => sf erase 0x900000 +$filesize && sf write 0x80000000 0x900000 $filesize Address  0x900000 is the location of the FMan ucode image in QSPI NOR flash.  Refer Flash layout for new boot flow with TF-A for the complete flash memory layout. Boot from QSPI NOR flash1 and press Enter to stop the autoboot: => cpld reset altbank In boot log, you’ll see: Board: LS1046ARDB, boot from QSPI vBank 4 You can check the following code line in the boot log to confirm that the DPAA1 FMan ucode image in QSPI NOR flash is updated. Fman1: Uploading microcode version 106.4.18 Ensure that SD card, USB flash drive, or SCSI hard disk installed with LSDK Ubuntu distribution is plugged into the board to boot the board to Ubuntu.  => cpld reset altbank Ubuntu 18.04.1 LTS localhost ttyS0 localhost login: root Password: Last login: Sun Jan 28 16:05:12 UTC 2018 on ttyS0 Welcome to Ubuntu 18.04.1 LTS (GNU/Linux 4.9.105 aarch64) * Documentation: https://help.ubuntu.com * Management: https://landscape.canonical.com * Support: https://ubuntu.com/advantage If U-Boot does not find LSDK on a mass storage device, it will boot TinyDistro from lsdk_linux_arm64_ tiny.itb stored in QSPI NOR flash. Option 2: Load image from partition on mass storage device (SD, USB, or SATA) Boot LS1046ARDB from QSPI NOR flash. Ensure that the switches are set to boot the board from QSPI. For booting from QSPI , SW5[1:8] = 00100010 Boot from QSPI NOR flash0: => cpld reset In boot log, you’ll see: Board: LS1046ARDB, boot from QSPI vBank 0 Select mass storage device to use. => mmc rescan => mmc info Or => usb start => usb info Or => scsi scan => scsi info Optional – List files on storage device => ls mmc <device:partition> For example: => ls mmc 0:3 System Volume Information/ 32604 fsl_fman_ucode_ls1046_r1.0_106_4_18.bin 1 file(s), 1 dir(s) Or => ls usb <device:partition> For example: => ls usb 0:1 Or => ls scsi <device:partition> For example: => ls scsi 0:2 If the ls command fails to run, check that U-Boot in QSPI NOR flash0 supports the command by typing ls at the U-Boot prompt: => ls ls - lists files in a directory (default) Usage: ls <interface> [<dev[:part]> [directory]] - Lists files in directory [directory] of partition [part] on device type [interface] and instance [dev]. If U-Boot does not support this command, then update the composite firmware image in QSPI NOR flash0. For steps to update composite firmware image in QSPI NOR flash, see LS1046ARDB - How to update composite firmware image in QSPI NOR flash. Program QSPI NOR flash1: => sf probe 0:1 Load FMan ucode image from the storage device. => load mmc <device:partition> 80000000 <image name> => print filesize For example: => load mmc 0:3 80000000 fsl_fman_ucode_ls1046_r1.0_106_4_18.bin 32604 bytes read in 18 ms (1.7 MiB/s) => print filesize filesize=7f5c Or => load usb <device:partition> 80000000 <image name> => print filesize Or => load scsi <device:partition> 80000000 <image name> => print filesize Program the FMan ucode image to QSPI NOR flash: => sf erase 0x900000 +$filesize && sf write 0x80000000 0x900000 $filesize Address  0x900000 is the location of the FMan ucode image in QSPI NOR flash.  Refer Flash layout for new boot flow with TF-A for the complete flash memory layout. Boot from QSPI NOR flash1 and press Enter to stop the autoboot: => cpld reset altbank In boot log, you’ll see: Board: LS1046ARDB, boot from QSPI vBank 4 You can check the following code line in the boot log to confirm that the DPAA1 FMan ucode image in QSPI NOR flash is updated. Fman1: Uploading microcode version 106.4.18 Ensure that SD card, USB flash drive, or SCSI hard disk installed with LSDK Ubuntu distribution is plugged into the board to boot the board to Ubuntu.  => cpld reset altbank Ubuntu 18.04.1 LTS localhost ttyS0 localhost login: root Password: Last login: Sun Jan 28 16:05:12 UTC 2018 on ttyS0 Welcome to Ubuntu 18.04.1 LTS (GNU/Linux 4.9.105 aarch64) * Documentation: https://help.ubuntu.com * Management: https://landscape.canonical.com * Support: https://ubuntu.com/advantage If U-Boot does not find LSDK on a mass storage device, it will boot TinyDistro from lsdk_linux_arm64_ tiny.itb stored in QSPI NOR flash.
View full article
This file shows up LS1024A GMAC2 debug, no software support in barebox only workable in kernel. and If using RTL Phy need to add TX_CLK and RX_CLK delay.
View full article
Please note that the LSDK memory layout for PPA boot flow explained in this topic is only applicable for LSDK 18.09 and older releases. For LSDK 18.12 and newer releases, refer Flash layout for new boot flow with TF-A. The following table shows the memory layout of various firmware stored in NOR/NAND/QSPI flash device or SD card on all QorIQ Reference Design Boards. Firmware Definition MaxSize NOR/NAND/QSPI Flash Offset SD Start Block No. RCW + PBI 1 MB 0x00000000 0x00008 Boot firmware (U-Boot or UEFI) 2 MB 0x00100000 0x00800 Boot firmware environment 1 MB 0x00300000 0x01800 PPA firmware 2 MB 0x00400000 0x02000 Secure boot headers 3 MB 0x00600000 0x03000 DPAA1 FMAN ucode 256 KB 0x00900000 0x04800 QE/uQE firmware 256 KB 0x00940000 0x04A00 Ethernet PHY firmware 256 KB 0x00980000 0x04C00 DPAA2-MC or PFE firmware 3 MB 0x00A00000 0x05000 DPAA2 DPL 1 MB 0x00D00000 0x06800 DPAA2 DPC 1 MB 0x00E00000 0x07000 Device tree(needed by uefi) 1 MB 0x00F00000 0x07800 Kernel lsdk_linux_<arch>.itb 16 MB 0x01000000 0x08000 Ramdisk rfs 32 MB 0x02000000 0x10000 The following figures highlight the changes in the flash layout for boot flow with PPA and flash layout for new TF-A boot flow. Flash layout for boot flow with PPA   Changed flash layout for TF-A boot flow
View full article
This how-to topic is applicable only to LSDK 18.09 and older releases. For LSDK 18.12 and newer releases, refer LS1088ARDB-PB - How to deploy TF-A binaries on SD card. Follow these steps to update U-Boot binary on the SD card.  Prerequisites  Ubuntu 18.04 64-bit should be installed on the Linux host machine for building LSDK 18.06 or LSDK 18.09 U-Boot binary.   Compiling U-Boot binary Clone the u-boot repository. $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/u-boot.git $ cd u-boot $ git checkout -b <new branch name> LSDK-<LSDK version>. For example, $ git checkout -b LSDK-18.09 LSDK-18.09  $ export ARCH=arm64 $ export CROSS_COMPILE=aarch64-linux-gnu- $ make distclean Execute appropriate defconfig file: For LS1088ARDB: $ make ls1088ardb_sdcard_qspi_defconfig For LS1088ARDB-PB: $ make ls1088ardb_pb_sdcard_qspi_defconfig If required, make changes to the U-Boot files. $ make If the make command shows the error "*** Your GCC is older than 6.0 and is not supported", ensure that you are using Ubuntu 18.04 64-bit version for building LSDK 18.06 or LSDK 18.09 U-Boot binary.  The compiled U-Boot image, u-boot-with-spl.bin, is available at u-boot/. SD card start block number for U-Boot binary Image  SD card start block number U-Boot binary 0x00800 = 2048 Refer the Flash layout for boot flow with PPA – LSDK 18.09 and older releases for a complete listing of the SD card start block numbers for all LSDK firmware images.     Programming U-Boot binary to SD card Plug the SD card into the Linux host. Run the following command on the Linux host: $ sudo dd if=u-boot-with-spl.bin of=/dev/sdX bs=512 seek=2048 conv=fsync Use the command cat /proc/partitions to see a list of devices and their sizes to make sure that the correct device names have been chosen. The SDHC storage drive in the Linux PC is detected as /dev/ sdX, where X is a letter such as a, b, c. Make sure to choose the correct device name, because data on this device will be replaced. If your Linux host machine supports read/write SDHC card directly without an extra SDHC card reader device, the device name of SDHC card is typically mmcblk0.    Remove the SD card from the Linux host machine. On the LS1088ARDB/LS1088ARDB-PB, ensure that the switches are set to boot the board from SD card.  For booting from SD card, SW1[1:8] + SW2[1] = 0010_0000_0  Plug the SD card into the board and boot the board to Ubuntu. If U-Boot does not find LSDK on the SD card, it will boot TinyDistro from lsdk_linux_arm64_ tiny.itb stored on the SD card.
View full article
On successful probing of the DSA Felix switch, each available front panel switch port should have a network device interface attached with the swpX name format. The ip link show command uses the swpX@enoY name format to also indicate the associated master Ethernet interface for the DSA switch port, which corresponds to an internal ENETC interface, usually the eno2 (Port2) for the LS1028A SoC. LS1028 Interface naming in Linux Single port mode Bridge mode
View full article
The table below shows the mapping of the Ethernet port names appearing on the front panel of the LS1043ARDB chassis with the port names in U-Boot, tinyDistro, and NXP LSDK userland.  Ethernet port mapping Port name on chassis Port name in U-Boot Port name in Linux (tinyDistro) Port name in Linux (LSDK userland) QSGMII.P0 FM1@DTSEC1 eth0 fm1-mac1 QSGMII.P1 FM1@DTSEC2 eth1 fm1-mac2 QSGMII.P2 FM1@DTSEC3 eth2 fm1-mac5 QSGMII.P3 FM1@DTSEC4 eth3 fm1-mac6 RGMII1 FM1@DTSEC5 eth4 fm1-mac3 RGMII2 FM1@DTSEC6 eth5 fm1-mac4 10G Copper FM1@TGEC1 eth6 fm1-mac9 Below is a table that shows the mapping between port numbers (from configuration file), character devices, hardware ports (Rx) and mEMACs for the standard SDK configuration (using RCW protocol 1455). FMC port mapping Port name on chassis XML port number (configuration file) Serdes protocol Character device Hardware port (device tree node) mEMAC (device tree node) QSGMII.P0 1 qsgmii fm0-port-rx0 port@88000 ethernet@e0000 QSGMII.P1 2 qsgmii fm0-port-rx1 port@89000 ethernet@e2000 QSGMII.P2 5 qsgmii fm0-port-rx4 port@8c000 ethernet@e8000 QSGMII.P3 6 qsgmii fm0-port-rx5 port@8d000 ethernet@ea000 RGMII1 3 rgmii fm0-port-rx2 port@8a000 ethernet@e4000 RGMII2 4 rgmii fm0-port-rx3 port@8b000 ethernet@e6000 10G Copper 9 xgmii fm0-port-rx6 port@90000 ethernet@f0000
View full article
The attached patch is to support Aquantia AQR107 in LS1043A.
View full article
Follow these steps to update the DPAA2 MC firmware, DPC, and DPL images on the SD card.    Compiling MC firmware Clone the qoriq-mc-binary repository. $ git clone https://github.com/NXP/qoriq-mc-binary.git $ cd qoriq-mc-binary/ls1088a/ $ git checkout LSDK-<LSDK version>. For example, $ git checkout LSDK-18.09 The prebuilt MC firmware image, mc_10.10.0_ls1088a_20180814.itb, is available at qoriq-mc-binary/ls1088a/. Note that the exact name of the MC firmware image may vary depending on the release version used.                  Compiling DPC and DPL images Clone the mc-utils repository and compile the DPC and DPL images. $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/mc-utils $ cd mc-utils/ $ git checkout LSDK-<LSDK version>. For example, $ git checkout LSDK-18.09 If required, make changes to the DPC and DPL files. $ make -C config/ The compiled dpc.0x1D-0x0D.dtb and dpl-eth.0x1D_0x0D.dtb images are available at /mc-utils/config/ls1088a/RDB/. Note that the exact name of the DPL and DPC images may vary depending on the release version used.             SD card start block number for MC, DPL, and DPC images Image  SD card start block number DPAA2 MC firmware 0x05000 = 20480 DPAA2 DPL  0x06800 = 26624 DPAA2 DPC 0x07000 = 28672 Refer the Layerscape Software Development Kit <version> Documentation for complete listing of the SD card start block numbers for all LSDK firmware images.    Programming MC, DPC, and DPL images to SD card Plug the SD card into the Linux host. Run the following commands on the Linux host: To update MC firmware: $ sudo dd if=mc_10.10.0_ls1088a_20180814.itb of=/dev/sdX bs=512 seek=20480 conv=fsync To update DPL image: $ sudo dd if=dpl-eth.0x1D_0x0D.dtb of=/dev/sdX bs=512 seek=26624 conv=fsync To update DPC image: $ sudo dd if=dpc.0x1D-0x0D.dtb of=/dev/sdX bs=512 seek=28672 conv=fsync Use the command cat /proc/partitions to see a list of devices and their sizes to make sure that the correct device names have been chosen. The SDHC storage drive in the Linux PC is detected as /dev/sdX, where X is a letter such as a, b, c. Make sure to choose the correct device name, because data on this device will be replaced. If your Linux host machine supports read/write SDHC card directly without an extra SDHC card reader device, the device name of SDHC card is typically  mmcblk0.   Remove the SD card from the Linux host machine. On the LS1088ARDB/LS1088ARDB-PB, ensure that the switches are set to boot the board from the SD card.  For booting from SD card, SW1[1:8] + SW2[1] = 0010_0000_0  Plug the SD card into the board and boot the board to Ubuntu. If U-Boot does not find LSDK on the SD card, it will boot TinyDistro from lsdk_linux_arm64_ tiny.itb stored on the SD card.
View full article
  Note: MCFBA{L/H} that is used to dump the MC log buffer is valid only after the following command is executed: fsl_mc start mc  ${mc_addr} ${dpc_addr} Run the above command first, then MCFBA contents will be valid. To display the MC log buffer in U-Boot for debug purpose, when MC console is not available: Determine the MC firmware base. At the U-Boot prompt, perform md at 0x8340020 (this is MCFBA{L/H}) => md 0x8340020 10 08340020: e0000006 00000027 00060000 00000000 ....'........... 08340030: 00000000 00000000 00000000 00000000 ................ 08340040: 00000000 00000000 00000000 00000000 ................ 08340050: 00000000 00000000 00000000 00000000 ................ The value at 08340024 is the MCFBAH address. In this case, it is 00000027. The value at 08340020 is the MCFBAL address. In this case, it is e0000000. So you can build the MCFBA base address as:  0x27e0000000. Run the following command to start the MC if it is not booted already. run mcinitcmd Dump the log buffer structure at offset 0x01000000 into the MC firmware base 0x27e1000000 (as per the example). md 27e1000000 27e1000000: 4d430100 00000000 01400000 00300000 [email protected]. 27e1000010: 000000b1 00000000 00000000 00000000 ................ 27e1000020: 00000000 00000000 00000000 00000000 ................ 27e1000030: 00000000 00000000 00000000 00000000 ................ 4d430100 = magic number, 400000 = log buffer offset, 00300000 = log buffer length Dump the content of the log buffer. md 27e1400000   The output size can be increased by specifying the number of objects.  md 27e1400000 <num> For example: md 27e1400000 20 In case that the log buffer has more information, you can extend the output of md by replacing 20 with a greater value.          
View full article
On the LX2160ARDB, there are 2 25G SFP interfaces, but no 10G SFP interface. When customer want to test the 10G SFPs to evaluate the performance, they have to change the 25G SFP interfaces into 10G by reconfiguration the SW configuration. In this document, it will give details of configuring the LX2160ARDB to support the customer’s 10G SFP interfaces requirement with LSDK2108. At the end, an image will be generated to deployed into the SD card. Because SD card is a convenient way boot up LX2160ARDB, if one wrong move could brick the system, the customer could unplug the SD card to repeat the steps below.
View full article
Follow these steps to update the DPAA1 FMan ucode image on the SD card.  Obtaining DPAA1 FMan ucode image Clone the qoriq-fm-ucode repository. $ git clone https://github.com/NXP/qoriq-fm-ucode.git $ cd qoriq-fm-ucode $ git checkout LSDK-<LSDK version>. For example, $ git checkout LSDK-19.06 The prebuilt FMan ucode images, fsl_fman_ucode_ls1043_r1.1_<microcode version>.bin, are at qoriq-fm-ucode/. In the binary file, ls1043_r1.1 refers to the LS1043A silicon revision 1.1. See qoriq-fm-ucode/readme for a description of the ucode version numbers. SD card start block number for DPAA1 FMan ucode image Image  SD card start block number DPAA1 FMan ucode image 0x04800 = 18432 Refer Flash layout for new boot flow with TF-A for complete listing of the SD card start block numbers for all LSDK firmware images. Programming DPAA1 FMan ucode image to SD card Option 1: Load image on SD card plugged into Linux host via dd command Plug the SD card into the Linux host. Run the following command on the Linux host: $ sudo dd if=fsl_fman_ucode_ls1043_r1.1_<ucode version>.bin of=/dev/sdX bs=512 seek=18432 conv=fsync Use the command cat /proc/partitions to see a list of devices and their sizes to make sure that the correct device names have been chosen. The SDHC storage drive in the Linux PC is detected as /dev/sdX, where X is a letter such as a, b, c. Make sure to choose the correct device name, because data on this device will be replaced. If your Linux host machine supports read/write SDHC card directly without an extra SDHC card reader device, the device name of SDHC card is typically mmcblk0.                                                   Remove the SD card from the Linux host machine. Plug the SD card into LS1043ARDB and boot the board to Ubuntu using the SD card. You can boot the board using the SD card either by: setting the switches: SW3[1:8] = 10110011, SW4 [1:8] =00100000 , SW5 [1:8] = 00100010, or boot switching to SD card => cpld reset sd In boot log, you’ll see: Board: LS1043ARDB, boot from SD You can check the following code line in the boot log to confirm that the DPAA1 FMan ucode image on the SD card is updated. Fman1: Uploading microcode version 106.4.18 If U-Boot does not find LSDK on the SD card, it will boot TinyDistro from lsdk_linux_arm64_tiny.itb stored on the SD card. Option 2: Load image on SD card plugged into board from the TFTP server Boot LS1043ARDB from NOR flash. Ensure that the switches are set to boot the board from NOR bank 0. For booting from NOR bank 0, switch settings are as follows: SW3[1:8] = 10110011 SW4[1:8] = 00010010 SW5[1:8] = 10100010 Boot from NOR bank 0: => cpld reset For LS1043ARDB, in boot log, you'll see: Board: LS1043ARDB, boot from vBank 0 Set up Ethernet connection When board boots up, U-Boot prints a list of enabled Ethernet interfaces. FM1@DTSEC1, FM1@DTSEC2, FM1@DTSEC3 [PRIME], FM1@DTSEC4, FM1@DTSEC5 Set server IP address to the IP address of the host machine on which you have configured the TFTP server.  => setenv serverip <ipaddress1> Set ethact and ethprime as the Ethernet interface connected to the TFTP server. See LS1043ARDB Ethernet and FMC port mapping for the mapping of Ethernet port names appearing on the chassis front panel with the port names in U-Boot and Linux.                        => setenv ethprime <name of interface connected to TFTP server> For example: => setenv ethprime FM1@DTSEC4 => setenv ethact <name of interface connected to TFTP server> For example: => setenv ethact FM1@DTSEC4 Set IP address of the board. You can set a static IP address or, if the board can connect to a dhcp server, you can use the dhcp command.  Static IP address assignment: => setenv ipaddr <ipaddress2> => setenv netmask <subnet mask> Dynamic IP address assignment: => dhcp Save the settings. => saveenv Check the connection between the board and the TFTP server. => ping $serverip Using FM1@DTSEC4 device host 192.168.1.1 is alive Load FMan ucode image from the TFTP server Flash the FMan ucode image: => tftp 0xa0000000 fsl_fman_ucode_ls1043_r1.1_<ucode version>.bin Program the FMan ucode image to SD card: => mmc write 0xa0000000 0x04800 <blk_cnt> Address  0x04800 is the SD card block number for the FMan ucode image.  ReferFlash layout for new boot flow with TF-A for the complete flash memory layout. Here, blk_cnt refers to number of blocks in SD card that need to be written as per the file size. For example, when you load FMan ucode from the TFTP server, if the bytes transferred is 37560 (92b8 hex), then blk_cnt is calculated as "37560/512 = 73 (49 hex)" + "few sectors for rounding up so that last block is not missed". So, if you round up by 5 (5 hex) sectors, for this example, mmc write command will be: => mmc write 0xa0000000 0x04800 4E You can boot the board using the SD card either by: setting the switches: SW3[1:8] = 10110011, SW4 [1:8] =00100000 , SW5 [1:8] = 00100010, or boot switching to SD card => cpld reset sd In boot log, you’ll see: Board: LS1043ARDB, boot from SD You can check the following code line in the boot log to confirm that the DPAA1 FMan ucode image on the SD card is updated. Fman1: Uploading microcode version 106.4.18 If U-Boot does not find LSDK on the SD card, it will boot TinyDistro from lsdk_linux_arm64_tiny.itb stored on the SD card.
View full article
Trusted Firmware for Cortex-A (TF-A) is an implementation of EL3 secure firmware. TF-A replaces PPA in secure firmware role. Note: Please note the steps listed in this topic can only be performed with LSDK 18.12 and newer releases.   To migrate to the TF-A boot flow from the previous boot flow (with PPA), you need to compile the TF-A binaries, bl2_<boot_mode>.pbl and fip.bin, and flash these binaries on the specific boot medium on the board. For FlexSPI NOR flash boot, you need to compile the following TF-A binaries. TF-A binary name Components bl2_flexspi_nor.pbl BL2 binary: Platform initialization binary RCW binary for FlexSPI NOR flash fip.bin BL31: Secure runtime firmware BL32: Trusted OS, for example, OPTEE (optional) BL33: U-Boot/UEFI image   Follow these steps to compile and deploy TF-A  binaries (bl2_flexspi_nor.pbl and fip.bin) in FlexSPI NOR flash. Compile PBL binary from RCW source file Compile U-Boot binary [Optional] Compile OPTEE binary  Compile TF-A binaries (bl2_flexspi_nor.pbl and fip.bin) for FlexSPI NOR flash Program TF-A binaries to FlexSPI NOR flash Step 1: Compile RCW binary  You need to compile the RCW binary to build the bl2_flexspi_nor.pbl binary. Clone the  rcw  repository and compile the RCW binary.  $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/rcw $ cd rcw $ git checkout -b <new branch name> <LSDK tag>. For example, $ git checkout -b LSDK-20.04 LSDK-20.04  Compile the RCW binary for Rev 1 or Rev 2 board. For LX2160ARDB Rev 1: $ cd lx2160ardb For LX2160ARDB Rev 2: $ cd lx2160ardb_rev2 If required, make changes to the rcw files. $ make   The compiled PBL binary for FlexSPI NOR flash on LX2160ARDB for core frequency 2000 MHz, platform frequency 700 MHz and DDR memory data rate 2900 MT/s, with serdes1 = 19 serdes2 = 5 serdes3 = 2, rcw_2000_700_2900_19_5_2.bin is available at: rcw/lx2160ardb/XGGFF_PP_HHHH_RR_19_5_2 (For LX2160ARDB Rev 1) rcw/lx2160ardb_rev2/XGGFF_PP_HHHH_RR_19_5_2 (For LX2160ARDB Rev 2) Note: See the rcw/lx2160ardb/README or rcw/lx2160ardb_rev2/README file for an explanation of the naming convention for the directories that contain the RCW source and binary files. Step 2: Compile U-Boot binary You need to compile the u-boot.bin binary to build the fip.bin binary. Clone the u-boot repository and compile the U-Boot binary for TF-A. $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/u-boot.git $ cd u-boot $ git checkout -b <new branch name> LSDK-<LSDK version>. For example, $ git checkout -b LSDK-20.04 LSDK-20.04  $ export ARCH=arm64 $ export CROSS_COMPILE=aarch64-linux-gnu- $ make distclean $ make lx2160ardb_tfa_defconfig $ make Note: If the make command shows the error "*** Your GCC is older than 6.0 and is not supported", ensure that you are using Ubuntu 18.04 64-bit version for building LSDK 18.12 and above U-Boot binary.  The compiled U-Boot image, u-boot.bin, is available at u-boot/. Step 3: [Optional] Compile OP-TEE binary You need to compile the tee.bin binary to build fip.bin with OPTEE. However, OPTEE is optional, you can skip the procedure to compile OPTEE if you want to build the FIP binary without OPTEE. Clone the optee_os repository and build the OPTEE binary.  $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/optee_os $ cd optee_os $ git checkout -b <new branch name> LSDK-<LSDK version>. For example, $ git checkout -b LSDK-20.04 LSDK-20.04 $ export ARCH=arm $ export CROSS_COMPILE=aarch64-linux-gnu- $ make CFG_ARM64_core=y PLATFORM=ls-lx2160ardb $ aarch64-linux-gnu-objcopy -v -O binary out/arm-plat-ls/core/tee.elf out/arm-plat-ls/core/tee.bin The compiled OPTEE image, tee.bin, is available at optee_os/out/arm-plat-ls/core/. Step 4: Compile TF-A binaries for FlexSPI NOR flash Clone the atf repository and compile the TF-A binaries, bl2_flexspi_nor.pbl and fip.bin. $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/atf $ cd atf $  git checkout -b <new branch name> LSDK-<LSDK version>. For example, $ git checkout -b LSDK-20.04 LSDK-20.04 $ export ARCH=arm64 $ export CROSS_COMPILE=aarch64-linux-gnu- Build BL2 binary with OPTEE. $ make PLAT=lx2160ardb bl2 SPD=opteed BOOT_MODE=flexspi_nor BL32=<path_to_optee_binary>/tee.bin pbl RCW=<path_to_rcw_binary>/rcw_2000_700_2900_19_5_2.bin   The compiled BL2 binaries, bl2.bin and bl2_flexspi_nor.pbl are available at atf/build/lx2160ardb/release/. For any update in the BL2 source code or RCW binary, the bl2_flexspi_nor.pbl binary needs to be recompiled.   To compile the BL2 binary without OPTEE: make PLAT=lx2160ardb bl2 BOOT_MODE=flexspi_nor pbl RCW=<path_to_rcw_binary>/rcw_2000_700_2900_19_5_2.bin Build FIP binary with OPTEE and without trusted board boot. $ make PLAT=lx2160ardb fip BL33=<path_to_u-boot_binary>/u-boot.bin SPD=opteed BL32=<path_to_optee_binary>/tee.bin The compiled BL31 and FIP binaries, bl31.bin, fip.bin, are available at atf/build/lx2160ardb/release/. For any update in the BL31, BL32, or BL33 binaries, the fip.bin binary needs to be recompiled. To compile the FIP binary without OPTEE and without trusted board boot: make PLAT=lx2160ardb fip BOOT_MODE=flexspi_nor BL33=<path_to_u-boot_binary>/u-boot.bin To compile the FIP binary with trusted board boot, refer the read me at <atf repository>/plat/nxp/README.TRUSTED_BOOT Step 5: Program TF-A binaries to FlexSPI NOR flash Boot LX2160ARDB from FlexSPI. Ensure that the switches are set to boot the board from FlexSPI. For booting from FlexSPI: SW1[1:8] = 1111 100X [X is 0 for FlexSPI NOR flash0 and X is 1 for FlexSPI NOR flash1] SW2[1:8] = 0000 0110 SW3[1:8] = 1111 1100 SW4[1:8] = 1011 1000 Boot from FlexSPI NOR flash0: => qixis_reset   For LX2160ARDB Rev 1, in boot log, you'll see: Board: LX2160ACE Rev1.0-RDB, Board version: B, boot from FlexSPI DEV#0   For LX2160ARDB Rev 2, in boot log, you'll see: Board: LX2160ACE Rev2.0-RDB, Board version: B, boot from FlexSPI DEV#0 Set up Ethernet connection When board boots up, U-Boot prints a list of enabled Ethernet interfaces. DPMAC2@xlaui4, DPMAC3@xgmii [PRIME], DPMAC4@xgmii, DPMAC5@25g-aui, DPMAC6@25g-aui, DPMAC17@rgmii-id, DPMAC18@rgmii-id, e1000#0  Set server IP address to the IP address of the host machine on which you have configured the TFTP server.  => setenv serverip <ipaddress1> Set ethact and ethprime as the ethernet interface connected to the TFTP server. Note: SeeLX2160ARDB Ethernet port mapping for the mapping of Ethernet port names appearing on the chassis front panel with the port names in U-Boot and Linux. => setenv ethprime <name of interface connected to TFTP server> For example: => setenv ethprime DPMAC3@xgmii => setenv ethact <name of interface connected to TFTP server> For example: => setenv ethact DPMAC3@xgmii Set IP address of the board. You can set a static IP address or, if the board can connect to a dhcp server, you can use the dhcp command.  Static IP address assignment: => setenv ipaddr <ipaddress2> => setenv netmask <subnet mask>   => setenv gatewayIP <gateway IP> Dynamic IP address assignment: => dhcp Save the settings. => saveenv Check the connection between the board and the TFTP server. => ping $serverip Using DPMAC3@xgmii device host 192.168.1.1 is alive Load TF-A binaries from the TFTP server Note: For details about the flash image layout for TF-A binaries, refer LSDK memory layout for TF-A boot flow. Program FlexSPI NOR flash1: => sf probe 0:1 Flash bl2_flexspi_nor.pbl: => tftp 0xa0000000 bl2_flexspi_nor.pbl => sf erase 0x0 +$filesize && sf write 0xa0000000 0x0 $filesize  Flash fip.bin: => tftp 0xa0000000 fip.bin => sf erase 0x100000 +$filesize && sf write 0xa0000000 0x100000 $filesize Boot from FlexSPI NOR flash1: => qixis_reset altbank LX2160ARDB will boot with TF-A. In the boot log, you will see: => NOTICE: BL2: v1.5(release):LSDK-20.04 NOTICE: BL2: Built : 22:01:10, Aug 20 2020 NOTICE: UDIMM 18ADF2G72AZ-3G2E1 NOTICE: DDR4 UDIMM with 2-rank 64-bit bus (x8) NOTICE: 32 GB DDR4, 64-bit, CL=22, ECC on, 256B, CS0+CS1 NOTICE: BL2: Booting BL31 NOTICE: BL31: v1.5(release):LSDK-20.04 NOTICE: BL31: Built : 22:02:07, Aug 20 2020 NOTICE: Welc U-Boot 2019.10 (Aug 14 2020 - 17:43:28 +0530) SoC: LX2160ACE Rev2.0 (0x87360020) Clock Configuration: CPU0(A72):2000 MHz CPU1(A72):2000 MHz CPU2(A72):2000 MHz CPU3(A72):2000 MHz CPU4(A72):2000 MHz CPU5(A72):2000 MHz CPU6(A72):2000 MHz CPU7(A72):2000 MHz CPU8(A72):2000 MHz CPU9(A72):2000 MHz CPU10(A72):2000 MHz CPU11(A72):2000 MHz CPU12(A72):2000 MHz CPU13(A72):2000 MHz CPU14(A72):2000 MHz CPU15(A72):2000 MHz Bus: 700 MHz DDR: 2900 MT/s Reset Configuration Word (RCW): 00000000: 50777738 24500050 00000000 00000000 00000010: 00000000 0c010000 00000000 00000000 00000020: 02e001a0 00002580 00000000 00000096 00000030: 00000000 00000000 00000000 00000000 00000040: 00000000 00000000 00000000 00000000 00000050: 00000000 00000000 00000000 00000000 00000060: 00000000 00000000 00027000 00000000 00000070: 08b30010 00150020 Model: NXP Layerscape LX2160ARDB Board Board: LX2160ACE Rev2.0-RDB, Board version: B, boot from FlexSPI DEV#1      
View full article
This document uses LS1043AQDS as an example to introduce how to use attaching method to debug atf and u-boot on QorIQ LS ARM 64 bit target boards with CodeWarrior for ARMv8. 1. Build ATF and U-boot with Debugging information Enabled in LSDK 2. Debug BL2 in ATF with CodeWarrior for ARMv8 3. Debug BL31 in ATF with CodeWarrior for ARMv8 4. Debugging u-boot with CodeWarrior for ARMv8
View full article
DPDK provides a simple, complete framework for fast packet processing in data plane applications. Using the APIs provided as part of the framework, applications can leverage the capabilities of underlying network infrastructure. This document describes DPDK basic introduction, DPDK core components, DPDK Linux networking, DPDK Crypto Subsystem, DPDK memory manager and DPDK implementation on Layerscape platforms. 1. DPDK Basic Introduction 2. DPDK core components 3. DPDK Linux Networking 4. DPDK Crypto Subsystem     4.1 DPDK Crypto Subsystem APIs     4.2 DPDK Security Offload – rte_security 5. DPDK memory manager     5.1 Multi-layered memory architecture     5.2 Buffer Manager     5.3 Packet Buffer mbuf 6. DPDK implementation on Layerscape platforms
View full article
This topic explains steps to compile and execute Hello World program (in C) on a Layerscape board. Similarly, you can execute other custom applications on your board. Create a Hello World program in C.  Copy this file (.c) on a Ubuntu machine (using WinSCP). Run the following command to convert the .c file into a binary file. $ aarch64-linux-gnu-gcc <.c file> -o <binary file> For example: $ aarch64-linux-gnu-gcc Hello_World.c -o Hello_World Note: You can use this command in the same directory in which .c file is present or provide path of this file. Connect to the board console on which you want to execute the custom application via terminal and boot the board with LITB. Note: It is suggested to boot the board with Tiny Linux for executing custom application.  => tftp 0xa0000000 lsdk2004_yocto_tiny_LS_arm64.itb Using e1000#0 device TFTP from server 192.168.3.1; our IP address is 192.168.3.142 Filename 'lsdk2004_yocto_tiny_LS_arm64.itb'. Load address: 0xa0000000 Loading: ################################################################# ################################################################# ##################################################### 4.3 MiB/s done Bytes transferred = 37030212 (2350944 hex) => bootm 0xa0000000#lx2160ardb ## Loading kernel from FIT Image at a0000000 ... Using 'lx2160ardb' configuration Trying 'kernel' kernel subimage Description: ARM64 Kernel Created: 2021-02-03 6:01:29 UTC Type: Kernel Image Compression: gzip compressed Data Start: 0xa00000d0 Data Size: 14086432 Bytes = 13.4 MiB When Tiny Linux boots, enable Ethernet to download the HelloWorld program on the board. To see the available networks. root@TinyLinux:~# ifconfig -a eth0 Link encap:Ethernet HWaddr 68:05:ca:2b:2c:ca BROADCAST MULTICAST MTU:1500 Metric:1 RX packets:0 errors:0 dropped:0 overruns:0 frame:0 TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:0 (0.0 B) TX bytes:0 (0.0 B) Interrupt:114 Memory:90460c0000-90460e0000 lo Link encap:Local Loopback inet addr:127.0.0.1 Mask:255.0.0.0 inet6 addr: ::1/128 Scope:Host UP LOOPBACK RUNNING MTU:65536 Metric:1 RX packets:0 errors:0 dropped:0 overruns:0 frame:0 TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:0 (0.0 B) TX bytes:0 (0.0 B) sit0 Link encap:UNSPEC HWaddr 00-00-00-00-31-00-6C-6F-00-00-00-00-00-00-00-00 NOARP MTU:1480 Metric:1 RX packets:0 errors:0 dropped:0 overruns:0 frame:0 TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:0 (0.0 B) TX bytes:0 (0.0 B) Enable the Ethernet connection. # ifconfig <eth interface> <IP address> netmask <netmask> up For example: root@TinyLinux:~# ifconfig eth0 192.168.3.121 netmask 255.255.255.0 up Set the gateway IP and ping the server to test the connection. # route add default gw <gateway IP> # ping <server IP> For example: root@TinyLinux:~# route add default gw 192.168.3.1 root@TinyLinux:~# ping 192.168.3.1 PING 192.168.3.1 (192.168.3.1): 56 data bytes 64 bytes from 192.168.3.1: seq=0 ttl=64 time=0.479 ms 64 bytes from 192.168.3.1: seq=1 ttl=64 time=0.204 ms Download the HelloWorld binary file on your board. For example: root@TinyLinux:~# scp [email protected]:/tftpboot/LX2160ARDB/HelloWorld . Execute the HelloWorld application. root@TinyLinux:~# ./HelloWorld Hello, World!    
View full article