Layerscape Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Layerscape Knowledge Base

Discussions

Sort by:
Compile kernel in the ls-5.15.71-2.2.0_distro In the LLDPUG_RevL5.15.71-2.2.0, it seems when do some reconfiguration in the kernel, rootfs should be repack to finish the change. Here will generate kernel without repack the roofts in the Linux host machine just compile the kernel.
View full article
Recently some customers are porting SDK 2.0 u-boot for LS1021ATWR to their custom boards. They intended to use GPIO lines to turn on/off LEDs for diagnostics and other various purposes. However GPIO driver is not supported in SDK 2.0 u-boot for LS102xa platform. The attached patch is used to add GPIO driver on LS1021ATWR platform based on SDK 2.0 u-boot code. Please use it in SDK 2.0 as the following: $ source ./fsl-setup-env -m ls1021atwr $ bitbake u-boot -c cleansstate $ bitbake u-boot -c patch Go to the folder build_ls1021atwr/tmp/work/ls1021atwr-fsl-linux-gnueabi/u-boot-qoriq/2016.01+fslgit-r0/git, apply the attached patch $ patch -p1<0001-ls1021xa-gpio.patch Go back to build_ls1021atwr folder to rebuild u-boot $ bitbake u-boot
View full article
LS1043ARDB version updated because we replaced the Nand Flash with different page size one as the old one is obsolete. Version update information FA version Nand flash program by CodeWarrior Nand Flash firmware bring up files Boot Mode setting
View full article
Follow these steps to update DPAA2 MC firmware and DPC images in QSPI flash, if you are booting LS1088ARDB from the QSPI flash memory.  qixis_reset boots the board from QSPI flash0 (aka bank0) and qixis_reset altbank boots the board from QSPI flash1 (aka bank4). “sf probe 0:1” means that the alternate bank will be written to. So if you boot from flash0, then enter sf probe 0:1, the commands that follow will program flash1. Prerequisites Linux machine. It is recommended to install Ubuntu 18.04 on the Linux machine. Obtaining MC firmware Download the prebuilt MC firmware image from the git repository: https://github.com/NXP/qoriq-mc-binary/tree/integration/ls1088a Obtaining DPC image Clone mc-utils repository and compile the DPC image. git clone https://source.codeaurora.org/external/qoriq/qoriq-components/mc-utils cd mc-utils/ git checkout LSDK-18.09 make -C config/ The compiled dpc.0x1D-0x0D.dtb is available at /mc-utils/config/ls1088a/RDB/. Flash MC firmware image on LS1088ARDB QSPI flash In U-Boot, boot from flash0, program flash1:  
View full article
When customer’s ethernet PCS could not link up, this article will give a guide how to debug it step by step based on the T1024. Many ethernet is configured by the SerDes, so how to confirm the link error is caused by the SerDes or the PCS itself. This article will give some clues. Serdes Lane&pins First check which SerDes lane the you are using, please confirm the SerDes land in the QorIQ T1024 Reference Manual. Such as configuration below, the user case set the SRDS_PRCTL_S1=0x05B in the RCW[128:136], the application will utilize the SGMII.m1 and SGMII.m2. This article will consider SGMII.m1 as an user case, now the SGMII will in the Frame Manager, MAC1. Check the SerDes Lane Assignments to confirm the Lane of the SerDes, for the SGMII.m1, the specific lane pins name would be SD1_TX3P/N and SD1_RX3P/N. it could be recognized as Lane 3. MAC number is not related to the Serdes lane number, should confirm the specific table to get the pins. Any hardware test with this ethernet should related the pins, see the component pin number below. You could test the eye diagram of RX pins of this Lane to confirm if the frequency is correct. if you set this Lane to SGMII 1.25G, you could confirm the speed is set correctly by the eye diagram. Eye diagram above, just show the speed of the SerDes. That is very important when loopback correctly, but could to connect to other device. How to confirm the SerDes link up Please find the Lane register in the QorIQ T1024 Reference Manual. In this user case it’s Lane 3, so should read out the Lane 3 registers to confirm if the SerDes Lane 3 work well. Such as below: # Lane 3 md.l 0xFFE0EA8C0 1 - aa611080 # LN3GCR0 md.l 0xFFE0EA8C4 1 - 101c4019 # LN3GCR1 md.l 0xFFE0EA8CC 1 - 00002800 # LN3SSCR0 md.l 0xFFE0EA8D0 1 - 0f0fc01f # LN3RECR0 md.l 0xFFE0EA8D4 1 - 0f0f0fa8 # LN3RECR1 md.l 0xFFE0EA8D8 1 - 00003006 # LN3TECR0 md.l 0xFFE0EA8E0 1 - 39000400 # LN3TTLCR0 md.l 0xFFE0EA8E4 1 - 00000000 # LN3TTLCR1 md.l 0xFFE0EA8F4 1 - 00000000 # LN3TCSR1 md.l 0xFFE0EA8FC 1 - 04000000 # LN3TCSR3   SerDes_LNnTCSR3 is an important debug test register, the CDR_LCK is to check if the CDR locked or not. CDR_LCK=0 means a valid bit stream is not detected. As a test, you could put the lane in loopback mode LN2TCSR3[LPBK_EN]=01. The CDR should lock in digital loopback mode (internal loopback). If not, there could be an issue with the device itself. So, if you could set the LPBK-EN to “01” Loopback Mode, it will set the SerDes’s own TX and RX signals in Loopback Mode to exclude external signals, then check the CDR_LCK again, if it’s 1, then SerDes itself works well. Anyway, CDR_LCK should always be set. In the “md.l 0xFFE0EA8FC 1 - 04000000 # LN3TCSR3”, the CDR_LCK=0, suspect the SerDes level issue. The normal status should be: => md fe0ea8fc 1 fe0ea8fc: 08000000 How to confirm the PCS link up The MAC and PHY registers should get the details from the T1024DPAArm, QorIQ T1024 Data Path Acceleration Architecture (DPAA) Reference Manual Find the offset address in the DPAARM. For the SGMII MAC address should be offset+0x1000. Follow the 6.5.4 MDIO Ethernet Management Interface usage in the T1024DPAARM to read the MDIO registers. In this application, SGMII1, MAC1, you could find the MAC1 address would be FM1_mEMAC1: 4E_0000, so FM1_mEMAC1 MDIO registers would be 4E_1000h. In the user case, the protocol is SGMII, should follow the 6.5.4.3 Clause 22 Read Flow in the T1024DPAARM. 6.5.4.3 Clause 22 Read Flow 1) Wait for MDIO_CFG[BSY] = 0. 2) Write MDIO_CTL with proper PHY_ADDR and REGISTER_ADDR and with bit 16 set. 3) Wait for MDIO_CFG[BSY] = 0. 4) If the addressed PHY did not respond then MDIO_CFG[MDIO_RD_ER] is set. Otherwise read MDIO_DATA value. In this user case, should read the MDIO_SGMII_SR, you could find the register definition in the QorIQ T1024 Reference Manual, 30.5.5 1000Base-KX PCS MDIO Memory Map/Register Definition The key bits would below: Here the user case result: When you read MDIO_SGMII_SR, please use manual input that can meet the delay time requirement. If you could not input manually, please follow the flow, " Wait for MDIO_CFG[BSY] = 0" before read MDIO_DATA value. Read SGMII1 MDIO Registers === Serdes Test 1 === 0xFFE0EA8FC value: 0x08000000 Dump PCS0 Registers 0xFFE4E1030-0xFFE4E103C: 0x40001408 0x00000000 0x00001340 0x00001340 Select 0x8002 ,devmem 0xFFE4E1034 32 0x8002 Read: 0x00000083 Select 0x8003 ,devmem 0xFFE4E1034 32 0x8003 Read: 0x0000E400 Select 0x8001 ,devmem 0xFFE4E1034 32 0x8001 Serdes0 Status: 0x00000029 Select 0x8001 devmem 0xFFE4E1034 32 0x8001 Serdes0 Status: 0x0000002D Select 0x8001, devmem 0xFFE4E1034 32 0x8001 Serdes0 Status: 0x0000002D The first time, it’s not link, LINK_STAT is 0(0x00000029), and then it’s turn to 1(0x0000002D). Now the PCS link up and the HW loopback checking is completely.
View full article
Issue description. The CodeWarrior ®  TAP enables target system debugging via a standard debug port (usually JTAG) while connected to a developer's workstation via Ethernet or USB. This the hardware debug tool(JTAG debug tool) to debug the DN MPU. You could find the tool from below link https://www.nxp.com/design/design-center/development-boards-and-designs/CW_TAP To debug the Layerscape MPU, should select CWH-CTP-BASE-HE and CWH-CTP-CTX10-YE In fact, the CWH-CTP-CTX10-YE will adapt the different signal definition, one connector will be insert to the CWH-CTP-BASE-HE, and another one(totally 10 pins) will be used to debug the Layerscape MPU. You could find the definition of the JTAG connector(CWH-CTP-CTX10-YE, 10pins) on the Layerscape board. Pin 10 (SRST)is the signal of this documents to should add workaround.     In the CodeWarrior TAP Probe User Guide, the SRST(SRST_B) is Open-drain. So the voltage of this signal should be decided by the pull-up voltage connect to it. See the schematics part below, pin 10 (JTAG_RST_B) should be 1.8V, but in fact it’s not.   The test signal will be exceed 1.8V to about 2.6V.   If you connect this pin directly to the Layerscape MPU, it will violate the SPEC of the VIN. Workaround. Workaround for the user would be to use an external circuit (level shifter/limiter) for the affected signal(s). level-shifter/limiter CWTAP <=> probe tip <=> (level-shifter/limiter) <=> target Please refer to FRWYLS1046A-PA,  use the AND gate 74AUP1G11GW similar components which the Overvoltage tolerant inputs to 3.6 V.     Logic Device Customer could also refer to LS1046ARDB CPLD LCMXO1200C-3FTN256C and LX2160ARDB CPLD EPM2210F256C5N, even the CPLD IO Voltage is 1.8V, no issue with 2.6V input on 1.8V IO ports.    
View full article
The u-boot in SDK2.0 has a bug on SGMII2.5 support. Need to add the patch.
View full article
The document explains how to use the variable  APTGET_EXTRA_PACKAGES in Yocto-based LLDP builds (ls-image-main.bb recipe) to install Ubuntu packages via apt-get instead of BitBake recipes.  
View full article
Introduction The qDMA controller transfers blocks of data between one source and one destination. The blocks of data transferred can be represented in memory as contiguous or noncontiguous using scatter/gather table(s). Channel virtualization is supported through enqueuing of DMA jobs to, or dequeuing DMA jobs from, different work queues. QDMA can support LX2160A with DPAA2. The attached patch is used for QDMA data transfer between PCIe Endpoint and DDR memory on LX2160A Platform. Apply the patch and rebuild Kernel image in LSDK 21.08 Go to LSDK 21.08 Linux Kernel source folder components/linux/linux/   Apply the attached patch. $ patch -p1 < 0001-QDMA-Performance-test.patch   $ flex-builder -c linux:custom -a arm64 Enable CONFIG_FSL_DPAA2_QDMA=y   $ Rebuild Linux Kernel. $ flex-builder -c linux -a arm64   Transfer data from Memory to Memory root@localhost:~# restool dpdmai create --num-queues=8 --priorities=2,5 dpdmai.0 is created under dprc.1 root@localhost:~# restool dprc assign dprc.1 --object=dpdmai.0 --plugged=1 root@localhost:~# echo "dpdmai.0" > /sys/module/dmatest/parameters/device root@localhost:~# echo '7       4       1       7' > /proc/sys/kernel/printk root@localhost:~# echo 1 > /sys/module/dmatest/parameters/dmatest_option root@localhost:~# echo 10 > /sys/module/dmatest/parameters/iterations root@localhost:~# echo 4096 > /sys/module/dmatest/parameters/test_buf_size root@localhost:~# echo 1 > /sys/module/dmatest/parameters/threads_per_chan root@localhost:~# echo 1 > /sys/module/dmatest/parameters/run [  177.903819] dmatest: current_mask 1 root@localhost:~# [  177.907636] dmatest: len 11         save_mask ffff  tmp_mask 2 [  178.927396] dmatest: qdma-test-task: summary 10 tests, 0 failures 303030 iops 1212121 KB/s 1241212121 B/s (0) [  178.937308] dmatest: total_len 40960  len 4096 [  178.941870] dmatest: runtime 33 [  178.941870]   root@localhost:~# echo 8 > /sys/module/dmatest/parameters/threads_per_chan root@localhost:~# echo 1 > /sys/module/dmatest/parameters/run [  273.731698] dmatest: current_mask 1 root@localhost:~# [  273.735625] dmatest: len 11         save_mask ffff  tmp_mask 2 [  274.767409] dmatest: qdma-test-task: summary 10 tests, 0 failures 357142 iops 1428571 KB/s 1462857142 B/s (0) [  274.777315] dmatest: total_len 40960  len 4096 [  274.781875] dmatest: runtime 28 [  274.781875]   Transfer data from Memory to PCIe  root@lx2160ardb-rev2:~# restool dpdmai create --num-queues=8 --priorities=2,5 dpdmai.0 is created under dprc.1 root@lx2160ardb-rev2:~# restool dprc assign dprc.1 --object=dpdmai.0 --plugged=1 root@lx2160ardb-rev2:~# echo "dpdmai.0" > /sys/module/dmatest/parameters/device root@lx2160ardb-rev2:~# echo '7       4       1       7' > /proc/sys/kernel/printk root@lx2160ardb-rev2:~# echo 4096 > /sys/module/dmatest/parameters/test_buf_size root@lx2160ardb-rev2:~#  echo 10 > /sys/module/dmatest/parameters/iterations root@lx2160ardb-rev2:~# echo 2 > /sys/module/dmatest/parameters/dmatest_option root@lx2160ardb-rev2:~# echo 0x9040000000 > /sys/module/dmatest/parameters/pci_phys_addr root@lx2160ardb-rev2:~# echo 1 > /sys/module/dmatest/parameters/produ_task_number root@lx2160ardb-rev2:~# echo 1 > /sys/module/dmatest/parameters/run [  214.319248] dmatest: current_mask 1 root@lx2160ardb-rev2:~# [  214.322864] dmatest: len 11   save_mask ffff  tmp_mask 2 [  214.330187] dmatest: pcie_phy_base : 9040000000       pcie_virt_base : 0000000014415a49 [  215.355448] dmatest: qdma-test-task: summary 10 tests, 0 failures 26737 iops 106951 KB/s 109518716 B/s (0) [  215.365093] dmatest: total_len 40960  len 4096 [  215.369529] dmatest: runtime 374 [  215.369529]  
View full article
  ARM Cortex A57 and A53 L1/L2 cache error reporting    The attached patch adds error detection for A53 and A57 cores. Hardware error injection is supported on A53. Software error injection is supported on both. For hardware error injection on A53 to work, proper access to L2ACTLR_EL1, CPUACTLR_EL1 needs to be granted by EL3 firmware. This is done by making an SMC call in the driver. Failure to enable access disables hardware error injection. For error interrupt to work, another SMC call enables access to L2ECTLR_EL1. Failure to enable access disables interrupt for error reporting. CPU Memory Error Syndrome and L2 Memory Error Syndrome registers can be used for checking L1 and L2 memory errors. However, only A53 supports double-bit error injection to L1 and L2 memory. This driver uses the hardware error injection when available, but also provides a way to inject errors by software. Both A53 and A57 supports interrupt when multi-bit errors happen. To use hardware error injection and the interrupt, proper access needs to be granted in ACTLR_EL3 (and/or ACTLR_EL2) register by EL3 firmware SMC call. Correctable errors do not trigger such interrupt. This driver uses dynamic polling internal to check for errors. The more errors detected, the more frequently it polls. Combining with interrupt, this driver can detect correctable and uncorrectable errors. However, if the uncorrectable errors cause system abort exception, this driver is not able to report errors in time.    Build ATF and Kernel image with EDAC L1 and L2 cache error detection enabled in LSDK In LLDPUG_RevL6.1.22_2.0.0 Yocto build environment, please rebuild ATF as the following. $ source build_ls1043ardb/SOURCE_THIS $ bitbake qoriq-atf -c cleansstate $ bitbake qoriq-atf -c patch Please go to atf source code folder build_ls1043ardb/tmp/work/ls1043ardb-fsl-linux/qoriq-atf/2.8+AUTOINC+atf-r0/git/, please apply patch 0001-Porting-helper-functions-for-EDAC-support-based-on-L.patch. $ patch -p1 < 0001-Porting-helper-functions-for-EDAC-support-based-on-L.patch And rebuild atf image. $ bitbake qoriq-atf Please rebuild Linux Kernel with the following commands. $ source build_ls1043ardb/SOURCE_THIS $ bitbake virtual/kernel -c cleansstate $ bitbake virtual/kernel -c patch Please go to Linux Kernel source code folder build_ls1043ardb/tmp/work/ls1043ardb-fsl-linux/linux-qoriq/6.1.y+gitAUTOINC+66e442bc7f-r0/git/ to apply patch 0001-drivers-edac-Add-L1-and-L2-error-detection-for-A53-a.patch. $ patch -p1 < 0001-drivers-edac-Add-L1-and-L2-error-detection-for-A53-a.patch   $ bitbake virtual/kernel -c menuconfig   $ bitbake virtual/kernel   L1/L2 cache error detection and correction EDAC feature verification root@localhost:~# dmesg | grep edac [ 3.478641] EDAC DEVICE0: Giving out device to module edac-a53 controller cortex_edac_l1_l2: DEV edac-a53 (POLLED) root@localhost:~# echo 1 > /sys/devices/system/edac/cpu_cache/l1_ue_sw_inject root@localhost:~# [ 74.784912] EDAC DEVICE0: UE: cortex_edac_l1_l2 instance: cpu_cache0 block: L1 count: 1 'Fatal error(s) on CPU 0 [ 74.784912] ' root@localhost:~# echo 1 > /sys/devices/system/edac/cpu_cache/l1_ue_hw_inject [ 83.429371] EDAC DEVICE0: UE: cortex_edac_l1_l2 instance: cpu_cache0 block: L1 count: 1 'Fatal error(s) on CPU 3 [ 83.429371] ' root@localhost:~# echo 1 > /sys/devices/system/edac/cpu_cache/l2_ue_sw_inject root@localhost:~# echo 1 > /sys/devices/system/edac/cpu_cache/l2_ue_hw_inject [ 106.985393] EDAC DEVICE0: UE: cortex_edac_l1_l2 instance: cpu_cache0 block: L2 count: 1 'Fatal error(s) on CPU 0 [ 106.985393] ' [ 106.997164] EDAC DEVICE0: UE: cortex_edac_l1_l2 instance: cpu_cache0 block: L2 count: 1 'Fatal error(s) on CPU 1 [ 106.997164] ' root@localhost:~# [ 115.232986] EDAC DEVICE0: UE: cortex_edac_l1_l2 instance: cpu_cache0 block: L2 count: 1 'Fatal error(s) on CPU 0 [ 115.232986] ' root@localhost:~# dmesg | grep EDAC [ 1.638675] EDAC MC: Ver: 3.0.0 [ 3.478641] EDAC DEVICE0: Giving out device to module edac-a53 controller cortex_edac_l1_l2: DEV edac-a53 (POLLED) [ 74.784840] EDAC cortex_edac_l1_l2: CPU 0 L1-I Tag RAM error(s) detected [ 74.784869] EDAC cortex_edac_l1_l2: CPU 0 L1 fatal error(s) detected (0x8000000080000000) [ 74.784912] EDAC DEVICE0: UE: cortex_edac_l1_l2 instance: cpu_cache0 block: L1 count: 1 'Fatal error(s) on CPU 0 [ 83.429298] EDAC cortex_edac_l1_l2: CPU 3 L1-D Data RAM error(s) detected [ 83.429329] EDAC cortex_edac_l1_l2: CPU 3 L1 fatal error(s) detected (0x8000000089100010) [ 83.429371] EDAC DEVICE0: UE: cortex_edac_l1_l2 instance: cpu_cache0 block: L1 count: 1 'Fatal error(s) on CPU 3 [ 106.985331] EDAC cortex_edac_l1_l2: CPU 0 L2 fatal error(s) detected (0x80000000910dc138) [ 106.985349] EDAC cortex_edac_l1_l2: CPU 1 L2 fatal error(s) detected (0x8000000080000000) [ 106.985393] EDAC DEVICE0: UE: cortex_edac_l1_l2 instance: cpu_cache0 block: L2 count: 1 'Fatal error(s) on CPU 0 [ 106.997164] EDAC DEVICE0: UE: cortex_edac_l1_l2 instance: cpu_cache0 block: L2 count: 1 'Fatal error(s) on CPU 1 [ 115.232936] EDAC cortex_edac_l1_l2: CPU 0 L2 fatal error(s) detected (0x80000000910c0598) [ 115.232986] EDAC DEVICE0: UE: cortex_edac_l1_l2 instance: cpu_cache0 block: L2 count: 1 'Fatal error(s) on CPU 0  
View full article