Connects - Training Material

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Connects - Training Material

Training Sessions Material



Home

Home is where the heart is..

Automotive

Silicon Valley 2019 - Automotive Presentation Files

Communication Infrastructure

Edge Intelligence

Industrial

Mobile, Wearable & Computing

IoT Smart Home

Hardware & Software Solutions

Silicon Valley 2019 - Industrial & IoT, Mobile, & Communication Infrastructure Presentation Files

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Multimedia Experience

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Secure Connected & Automated Vehicles

Smart Buildings & Consumer Goods

Secure Mobile, Healthcare & Wearables

Smart Machinery & Industrial Automation

Enabling Design, Technologies & Solutions

Smart Networks & Computing

Secure Connected & Automated Vehicles

Secure Connected & Automated Vehicles

Discussions

Sort by:
This session will present the advantages of H-bridge based window lifters against relay based ones, new functionalities that can be implemented and how NXP MagniV S12ZVMB64 microcontroller provides a well-integrated solution for a window lifter end node. With integrated functionalities like: internal regulator, GDU, PMF, ADC, current sensing, input capture and LIN physical layer.
View full article
This session introduces the MCUXpresso suite of tools (IDE, SDK, Config Tools) and shows users how to rapidly start development with thousands of Kinetis and LPC MCUs. Using either Kinetis, LPC or i.MX RT development hardware, attendees will watch how to build a custom SDK, configure pins and clocks settings, generate a project, import and debug an application, as well as the advanced debugging capabilities of the MCUXpresso IDE, including trace, profiling, coverage, watch points and more.
View full article
Bluetooth speakers and headsets, printers, cameras, projectors, set-top-boxes, TVs, Wi-Fi routers and a variety of home appliances like fridges, washing machines, air purifiers, coffee machines, blenders all have one thing in common: Near Field Communication (NFC) allows new features and easier handling. Just bringing two NFC-enabled devices close together is all it takes to create a connection. Accessories and consumables can be authenticated and configured without any user interaction, and without power supply. And commissioning an IOT node into a wireless network has never been as easy as it is now with NFC. We will share the latest status of NFC support in iOS and present the brand new NFC Tandem module.
View full article
The session will introduce an upcoming xEV traction motor power inverter platform system-play solution featuring a new MCU, new IGBT gate driver, and new safe SBC bound together with system enablement software and ASIL-D compliant safety support. A fully functional traction motor reference design being designed by partner Vepco will also be introduced based on a Power IGBT Module from Fuji Electric. The session will describe the platform’s components, software structure, value proposition, enablement support and go-to-market approach to help enhance understanding of the application and NXP solution as well as how to sell the system platform.
View full article
This session will provide an overview of the QorIQ security accelerator block, its device driver, and its use in IPsec and SSL acceleration.
View full article
This session will focus on the memory choices for several of the more popular i.MX 6 and i.MX 7 series as well as NXP’s newest and most powerful microprocessor, the i.MX 8 series. Most processors can support different types of volatile (DRAM) and non-volatile (Flash) memories. For example, the i.MX 7 can support low power DRAM (LPDDR), LPDDR2 and LPDDR3 as well as the standard DDR3 memory. For flash memories, the i.MX 7 supports parallel NOR, serial NOR or NAND Flash. Each of these memory choices has technical advantages and disadvantages as well as the overall market acceptance and expected longevity. The session will also discuss two new high performance memory technologies that the i.MX 8 plans to support, LPDDR4 and XTRMFlash. This session will allow you, the designer to make an informed decision when it comes to selecting memory for your design.
View full article
Bluetooth speakers and headsets, printers, cameras, projectors, set-top-boxes, TVs, Wi-Fi routers, fridges and washing machines, they all have one thing in common: Near-field-communication (NFC) which allows new features and easier handling. Just bringing two NFC-enabled devices close together is all it takes to create a connection. Accessories and consumables can be identified and authenticated without any user interaction. And commissioning an IoT node into a wireless network has never been as easy as it is now with NFC.
View full article
This session will go into the detail of the software enablement around the BlueBox v2.0, aka “Blue Box Min”. From an engineering perspective, topics will include: The SoCs in the platform and it’s layout; Booting the individual SoCs; Linux options between and inter-communication between them; Discussion of middleware options (including ROS versions, Polysync and others); How ADAS vision perception is accomplished with Neusoft ADAS perception; Combined to achieve level 2/3 ADAS with AutonomouStuff; Extra topics: OpenCV, OpenSSL security between subsystems and more. Please expect a non-marketing lecture explaining the internals of this enablement.
View full article
This session will introduce NXP differentiated GaN technology for cellular band high power applications, including full cellular portfolio RF Power products.
View full article
The i.MX processors have features for advanced key management techniques. This session examines these feature in depth.
View full article
As IC geometries continue to shrink and switching speeds increase, designing electromagnetic systems and printed circuit boards to meet the required signal integrity and EMC specifications has become even more challenging. A new design methodology is required. Specifically, the utilization of an electromagnetic physics-based design methodology to control the field energy in your design will be discussed. This training module will walk through the development process and provide you with guidelines for building successful, cost effective printed circuit boards.
View full article
This session will introduce the NXP mature and widely accepted solutions of RF products serve the DAS and small cell applications from 0.5W, 10W to 20W and 40W.
View full article
Extend your logistics track and trace with condition insights. NTAG SmartSensor enables sensing and logging with NFC readout. NTAG SmartSensor enables your IoT application for smart logistics, smart healthcare, drug delivery and smart packaging.
View full article
Learn about NXP's secured IoT Gateway platform with sensor fusion, local and cloud analytic. IoT data aggregation, sensor fusion and analytic processes are run in VMs providing VM isolation advantage. IoT processes can also run in Virtualized Network Functions (VnF) that can run as service chains across end-to-end virtualized network equipment
View full article
Learn about the key benefits and target applications of the new K27/K28 MCUs with extra-large embedded memory and power-efficient dual-USB MCUs based on ARM® Cortex-M4® core.
View full article
This session is for those of you who have never programmed in the Qt Framework. It will guide you through the basics – from setting up the environment to developing two basic applications, a calculator and a thermometer display. You will also have the opportunity to interact with these demos.
View full article
In electronic systems, it is typical to have a central processing unit that interfaces with other peripheral devices, other sub-systems or the user. Often, the signals from these interconnects may be incompatible on both ends. Therefore, various semiconductor devices such as analog switches, voltage level translators and GPIO expanders are often used to bridge between the interconnects on the board. In this session, we will explore the application of these interface devices from NXP and discuss their applications in various customer systems.
View full article
Get a deep dive into the brand new Vulkan API from Khronos. Learn how the programming paradigms have changed from OpenGL ES, how to use Vulkan API and its enormous performance advantages, and how to unlock the full potential of i.MX 8 series GPUs.
View full article
Join this session to learn how NXP security technology should be leveraged to secure the onboarding credentials using the LPC54S0xx MCU with state of the art security technology.
View full article