コネクト - トレーニング教材

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Connects - Training Material

Training Sessions Material



Home

Home is where the heart is..

Automotive

Silicon Valley 2019 - Automotive Presentation Files

Communication Infrastructure

Edge Intelligence

Industrial

Mobile, Wearable & Computing

IoT Smart Home

Hardware & Software Solutions

Silicon Valley 2019 - Industrial & IoT, Mobile, & Communication Infrastructure Presentation Files

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Multimedia Experience

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Secure Connected & Automated Vehicles

Smart Buildings & Consumer Goods

Secure Mobile, Healthcare & Wearables

Smart Machinery & Industrial Automation

Enabling Design, Technologies & Solutions

Smart Networks & Computing

Secure Connected & Automated Vehicles

Secure Connected & Automated Vehicles

ディスカッション

ソート順:
In recent years, automotive cybersecurity has become a top priority for OEMs as several well publicized attacks on production vehicles stirred up public and government concern over both security and safety of connected vehicle systems. In this talk we will: Review major milestones and headlines related to automotive cybersecurity for 2016; Compare and contrast security techniques used in traditional IT infrastructure versus automotive computing systems; Examine where these traditional techniques fall short for automotive applications.
記事全体を表示
Secure designs begin with a security model consisting of policies, an understanding of the threat landscape and the methods used to enforce physical and logical security. This session introduces the basic concepts of security, the security threats faced by users, the security features of i.MX/MCU products, and how to use the security features to achieve secure boot, code protection, data protection, secure communication and so on.
記事全体を表示
Introduction into secure element and use case overview secure element complementing secure µCs inside a car security infrastructure. Overview on tool chain including applet and secure gateway demonstrator.
記事全体を表示
Fixed Wireless Access (FWA) emerged as an attractive option for high-speed broadband connectivity in urban/suburban areas as a solution to the ‘last mile problem’. 60 GHz wireless mesh systems are generating commercial interest due to the attractive cost and deployment logistics of unlicensed, high-bandwidth spectrum relative to optical fiber networks. NXP’s Layerscape products are designed into FWA systems conceived to exploit the many opportunities of wireless mesh networks. Learn how NXP's 64-bit Arm® platforms drive the next generation of FWA success.
記事全体を表示
This session will first provide an overview of the products, software and enablement that NXP's wireless connectivity MCU portfolio includes to address the IoT market. Then, it will provide a deeper dive and demo on the Thread™ networking technology and how to develop an application using NXP's Thread Stack and ZigBee® Dotdot application layer. This session will also introduce the NXP BLE product family including the latest QN9080/83 ultra low-power BLE WMCU and KW35/36 automotive and industrial BLE WMCU, detailing targeted use cases, the device features, highlighting BLE and stacks as well as supporting enablement.
記事全体を表示
When choosing the NFC device for a new design, the system architect must consider many parameters. To avoid unpleasant surprises during software implementation phase, software has to be taken into account as well from the beginning. Different NFC IC categories (NFC Frontends, NFC Controller, Connected Tag) have different strengths, depending on the software environment. The way how highly integrated operating systems like Linux are structured brings both new challenges and advantages. This session examines the considerations necessary when designing in NFC in different operating systems or "bare metal" systems. It also discusses the advantages and disadvantages of the different device categories in dependence of the designated environment.
記事全体を表示
NXP offers a wide range of powerful microprocessors for the automotive and industrial markets. The memory selection of these systems can impact the performance, size, cost, power, reliability and longevity of your design. During this session we will discuss the new memories supported on the latest i.MX 8 Quad Max processor which is focused on automotive and industrial markets. For DRAM, this will include LPDDR4. For non-volatile memory, this will include Micron’s recently announced XccelaTM Octal SPI-NOR Flash and our newer e.MMC devices. These devices provide higher performance and are offered with automotive temperature and quality ratings. This session will provide designers with the information necessary to develop i.MX 8 systems for state-of-the-art automotive solutions.
記事全体を表示
A guide to using HAB on i.MX family of processors. Learn features and tools available to help deploy signed and encrypted images.
記事全体を表示
With the trend of frequent and remote software updates on the vehicle, the need of managing this properly at the microcontroller is critical. This session will present the challenges on reprogramming edge node microcontrollers inside the vehicle and show how our S32K144 microcontroller properly addresses it safe and efficiently.  
記事全体を表示
The NFC market is exploding - ABI Research forecasts more than 2 billion NFC-enabled devices to shipped yearly by 2019. While the first product generations focused on standards and reading distance, the newest products also allow for fast design-in and certification thanks to features such as Dynamic Power Control, microcontroller integration or energy harvesting. Today we see three full NFC product categories to adress the growing number of use cases: (1) Connected NFC tag solutions with field-detection function and an NFC Forum-compliant RF or an I²C interface, (2) standalone NFC frontend solutions for the most flexible way to add NFC to a system and (3) NFC controller solutions to enable higher integration by combining an NFC frontend with an advanced 32-bit microcontroller, available with integrated firmware.
記事全体を表示
This class will introduce/update on Android Things, the new version of Android designed for the IoT market. The when, what and how of Android Things will be explained and how NXP has worked with Google to enable certified boards based on NXP silicon and why IoT product developers should consider using Android Things for their next IoT project. Finally the relationship between Android Things, Google Voice Assistant and Chromecast built in will be explained and what NXP parts are most appropriate for optimal performance.
記事全体を表示
This session will introduce NXP mutual and best class LDMOS technology for cellular band high power applications, including full cellular portfolio RF Power products.
記事全体を表示
With the very public hacks of some major vehicle brands in 2015, there is a renewed focus on vehicle security. There is a large range of vehicle electrical architectures, with significant regional variations, but there is an acceleration towards a domain orientated secure network. This presentation will look at the growing importance of the central gateway in a world of increased connectivity and security. As Ethernet becomes more prevalent, the topic of IP routing & firewall will be introduced and its role in adding another security layer. Finally, the role of the central gateway in enabling OTA software updated beyond the telematics unit, to the entire network will be presented.  
記事全体を表示
This session will cover serial reprogramming capability (download, execute, etc.). Show the boot process from the ARM® Cortex®-M4 core including controlling A53 boot. Procedure for building and running baremetal code on Cortex-M4 and A53 using a debugger. Will discuss and demonstrate runtime communication between A53 and Cortex-M4 cores - with a discussion of options and examples.
記事全体を表示
Sensors are key to differentiate your products in the market and add context awareness, tamper detection, a robust user interface and intelligent wake-up. This class will step through all the leading applications in the IoT and IMM markets and provide a demonstration of the Sensor Toolbox tools for your product.
記事全体を表示
In designing cooking appliances, there is ample consideration given to power required from a home's wired electrical system as well as the performance needed to maintain safety and operating temperatures. NXP's solid state RF cooking team has developed a portable food heating appliance using solid state RF energy which is capable of operating on battery power. This session will cover the key challenges and approaches to delivering energy to heat food in a portable, on-the-go appliance.
記事全体を表示
This course will provide an in-depth system analysis of High Voltage (HV) Electric We review how the MCU, GDIC and IGBTs function individually and as a system. We will discuss EV and HEV power systems and components for achieving a highly efficient and safe HV motor drive. Using system block diagrams and oscilloscope screen shots of NXP’s new HV IGBT GDIC, the GD3100, and Fuji GEN 7 IGBT modules as we will consider how to achieve smaller, more efficient and lower cost HV inverter designs. We will review SPI interface programmability that enables any IGBT to be tuned for maximum efficiency, thermal design considerations, layout considerations, power budget assessment, power up sequencing, managing short circuit faults, temperature monitoring and advanced features achieve system ASIL level D and ISO26262 certification.
記事全体を表示
Future networks will still use CAN to a huge extend - but the variety of trends is also significantly increasing. This session shows key values, technical background and differentiators of the different CAN trends and the NXP implementation.
記事全体を表示
Take an in depth look at the features and capabilities of NXP’s latest 64-bit ARM® offerings. LS1012A and LS1043A are based on ARM Cortex®-A53 and LS1046A uses the ARM Cortex-A72 processor.  This session will showcase many features you can use to incorporate these cost effective SOCs in your next design.
記事全体を表示
Wireless (802.11) deployments are slated to overtake Ethernet switching revenue by the later part of the decade. Along with that volume, the new 802.11ax standard will deliver a 300% increase in useable performance along with higher density access for schools, airports, stadiums etc. Another driver is the demand for high bandwidth wireless within the home. Come learn about NXP's new Layerscape LA1575 and other innovative, integrated, programmable solutions available to address these increasing demands for wireless performance.
記事全体を表示