Connects - 培训资料

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Connects - Training Material

Training Sessions Material



Home

Home is where the heart is..

Automotive

Silicon Valley 2019 - Automotive Presentation Files

Communication Infrastructure

Edge Intelligence

Industrial

Mobile, Wearable & Computing

IoT Smart Home

Hardware & Software Solutions

Silicon Valley 2019 - Industrial & IoT, Mobile, & Communication Infrastructure Presentation Files

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Multimedia Experience

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Secure Connected & Automated Vehicles

Smart Buildings & Consumer Goods

Secure Mobile, Healthcare & Wearables

Smart Machinery & Industrial Automation

Enabling Design, Technologies & Solutions

Smart Networks & Computing

Secure Connected & Automated Vehicles

Secure Connected & Automated Vehicles

讨论

排序依据:
How to accelerate radar signal processing on S32R family utilizing SPT and multiple cores.
查看全文
The session is intended for engineers either getting started or are interested in seeing how to use AUTOSAR MCAL to generate and implement code. “Hello world” level examples are presented using the Tresos configuration tool to generate code which is then used in application code. Examples are based on NXP’s MCAL application provided with the released product.
查看全文
Bluetooth speakers and headsets, printers, cameras, projectors, set-top-boxes, TVs, Wi-Fi routers and a variety of home appliances like fridges, washing machines, air purifiers, coffee machines, blenders all have one thing in common: Near Field Communication (NFC) allows new features and easier handling. Just bringing two NFC-enabled devices close together is all it takes to create a connection. Accessories and consumables can be authenticated and configured without any user interaction, and without power supply. And commissioning an IoT node into a wireless network has never been as easy as it is now with NFC. We will share the latest status of NFC support in iOS and present the brand new NFC Tandem module.
查看全文
This session provides an introduction to the market and technology trends behind Advanced Driver Assistance Systems (ADAS) and Autonomous Driving and introduces some of the solutions that NXP provides to enable the car of tomorrow to sense, think and act.
查看全文
This course will provide an in-depth system analysis of High Voltage (HV) Electric. We review how the MCU, GDIC and IGBTs function individually and as a system. We will discuss EV and HEV power systems and components for achieving a highly efficient and safe HV motor drive. Using system block diagrams and oscilloscope screen shots of NXP’s new HV IGBT GDIC, the GD3100, and Fuji GEN 7 IGBT modules as we will consider how to achieve smaller, more efficient and lower cost HV inverter designs. We will review SPI interface programmability that enables any IGBT to be tuned for maximum efficiency, thermal design considerations, layout considerations, power budget assessment, power up sequencing, managing short circuit faults, temperature monitoring and advanced features achieve system ASIL level D and ISO26262 certification.
查看全文
Learn about vision processing and technical capabilities of S32V’s dual-APEX acceleration engines, multi-core A53 processors, on-chip image signal processor (ISP) and Vivante GC3000 GPU which differentiates S32V from other ARM® based processors that can’t meet the same performance/power envelope. Attendees will get hands-on experience using the SBC-S32V234 SOM hardware and free Vision SDK to demonstrate software for Lane Departure Warning (LDW), Feature Detection using Lukas-Kanade and Pedestrian Detection applications.
查看全文
The low-power i.MX portfolio's objective is to serve as the entry level for application processors while optimizing on performance and power consumption. Join this session to learn about the latest low-power i.MX products, key differentiators and target markets/applications.
查看全文
The continued growth of processing capabilities and new features introduced with the ARM®v8 based System-on-Chip has made virtualization a realistic option for embedded system developers. With virtualization, system architects can design solutions that reduce the size, weight, power, and cost of legacy systems by consolidating disparate software functions onto a single chip, even if those different software functions require different operating systems or otherwise incompatible software stacks. Virtualization allows architects to partition and isolate software components with different safety, security, or licensing requirements. The virtual machine manager, or hypervisor, is the key piece of software technology enabling virtualization. Open source hypervisor, Xen, supports the ARMv8 processor family.
查看全文
In designing cooking appliances, there is ample consideration given to power required from a home's wired electrical system as well as the performance needed to maintain safety and operating temperatures. NXP's solid state RF cooking team has developed a portable food heating appliance using solid state RF energy which is capable of operating on battery power. This session will cover the key challenges and approaches to delivering energy to heat food in a portable, on-the-go appliance.
查看全文
Deep dive training on battery management applications: hardware configurations and software intricacies: 1) Short BMS market introduction (incl. key players, requirements, competitors). 2) Introduction to NXP BMS roadmap and key products (BCC14A/B BCC6A/B & TPL). 3) Key BMS applications (14V, 48V, HV Daisy Chain, HV CAN, Wireless). 4) Market, application and product outlook. 14V Li ION use case example.
查看全文
NFC pairing makes life in a multi-device world more convenient. Tap-to-pair has become a common habit when connecting an NFC-enabled smartphone conveniently to a wireless speaker. Bringing this experience to the next level, even a multi-speaker audio system can be set up with NFC. If all speakers are equipped with an NFC chip, you simply tap one speaker to another to establish the Bluetooth® connection. That's what we call a true wireless stereo system - and it works with any phone, no matter if it is NFC-enabled. Same use case can be shown with NFC headsets. The workshop will guide participants through the implementation of an NFC, Bluetooth and Wi-Fi pairing use case. All participants should bring an NFC Enabled Android Device running Android version (Kit Kat) 4.4x or higher. In addition please install "NFC TagWriter" and "NFC TagInfo" from the Google Play Store.
查看全文
Safety by Software (SBSW) is a new way of achieving ASIL-D with high-level measures, supported by NXP S32X hardware. The SBSW hardware module together with SBSW firmware enables to check the user application flow, compare results of main and redundant algorithms and detect faulty behavior with high degree of independence. This session makes you familiar with SBSW usage, configuration, tools, etc.
查看全文
This presentation will present a simple EM physics and geometry based approach to designing power distribution networks on PCBs. From input power connection to the IC die, the simple rules discussed can be used to reduce power supply noise and improve EMC.
查看全文
A guide to developing with the Yocto Project for i.MX application processors. Learn how to leverage the Yocto Project in development by adding layers and recipes, customizing images, working with the kernel, and other essential Yocto development tasks. 
查看全文
There are many parallels between the adoption of Ethernet in automotive and the adoption of Ethernet in avionics and industrial networking. This session provides an overview of Ethernet in modern aircraft and factory automation, as well as emerging technologies to further improve the suitability of Ethernet for these applications.
查看全文
This class will provide an overview introduction of i.MX RT series, including their key features and key peripherals. This session also explores the design and implementation of a secure boot by making use and protect against firmware attacks. Secure designs begin with a security model consisting of policies, an understanding of the threat landscape and the methods used to enforce physical and logical security. To protect firmware execution given today’s threat landscape, there must be a policy to only allow execution of authenticated firmware. The methods used to enforce this policy rely on MCU security technology to create a protected boot flow. The boot firmware can contain public key cryptography to authenticate application code.
查看全文
This presentation dedicated to IVI provides an overview of the software and hardware enablement available to accelerate customer time-to-market and reduce development risks. Namely i.MX 8, Ethernet Switch and PHY, audio tuner and amplifier, power management, supported by a Linux Genivi compliant BSP.
查看全文
Explores the fast-growing Automotive Gateway market, identifying key use cases and requirements, and how gateways will evolve over the next decade.
查看全文
Automotive Ethernet PHYs enable future driving scenarios by providing the necessary physical throughput power. While software brings added value for security, diagnosis, energy efficiency and safety. As the functional requirements for automotive PHY drivers differ from general purpose applications, additional functionality is needed to closely monitor and diagnose the device and to create advanced use cases like Layer-1 wake-up and sleep. In this session, these specific requirements for automotive Ethernet PHY SW are discussed. Existing PHY SW frameworks such as Linux or AUTOSAR are introduced. Finally, the session will touch upon typical application scenarios which require interaction with PHY SW.
查看全文
Explains how the efficiency of a modern audio system has impacts in the vehicle well beyond audio.
查看全文