コネクト - トレーニング教材

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Connects - Training Material

Training Sessions Material



Home

Home is where the heart is..

Automotive

Silicon Valley 2019 - Automotive Presentation Files

Communication Infrastructure

Edge Intelligence

Industrial

Mobile, Wearable & Computing

IoT Smart Home

Hardware & Software Solutions

Silicon Valley 2019 - Industrial & IoT, Mobile, & Communication Infrastructure Presentation Files

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Multimedia Experience

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Secure Connected & Automated Vehicles

Smart Buildings & Consumer Goods

Secure Mobile, Healthcare & Wearables

Smart Machinery & Industrial Automation

Enabling Design, Technologies & Solutions

Smart Networks & Computing

Secure Connected & Automated Vehicles

Secure Connected & Automated Vehicles

ディスカッション

ソート順:
Deep dive training on battery management applications: hardware configurations and software intricacies: 1) Short BMS market introduction (incl. key players, requirements, competitors). 2) Introduction to NXP BMS roadmap and key products (BCC14A/B BCC6A/B & TPL). 3) Key BMS applications (14V, 48V, HV Daisy Chain, HV CAN, Wireless). 4) Market, application and product outlook. 14V Li ION use case example.
記事全体を表示
NFC pairing makes life in a multi-device world more convenient. Tap-to-pair has become a common habit when connecting an NFC-enabled smartphone conveniently to a wireless speaker. Bringing this experience to the next level, even a multi-speaker audio system can be set up with NFC. If all speakers are equipped with an NFC chip, you simply tap one speaker to another to establish the Bluetooth® connection. That's what we call a true wireless stereo system - and it works with any phone, no matter if it is NFC-enabled. Same use case can be shown with NFC headsets. The workshop will guide participants through the implementation of an NFC, Bluetooth and Wi-Fi pairing use case. All participants should bring an NFC Enabled Android Device running Android version (Kit Kat) 4.4x or higher. In addition please install "NFC TagWriter" and "NFC TagInfo" from the Google Play Store.
記事全体を表示
Safety by Software (SBSW) is a new way of achieving ASIL-D with high-level measures, supported by NXP S32X hardware. The SBSW hardware module together with SBSW firmware enables to check the user application flow, compare results of main and redundant algorithms and detect faulty behavior with high degree of independence. This session makes you familiar with SBSW usage, configuration, tools, etc.
記事全体を表示
This presentation will present a simple EM physics and geometry based approach to designing power distribution networks on PCBs. From input power connection to the IC die, the simple rules discussed can be used to reduce power supply noise and improve EMC.
記事全体を表示
A guide to developing with the Yocto Project for i.MX application processors. Learn how to leverage the Yocto Project in development by adding layers and recipes, customizing images, working with the kernel, and other essential Yocto development tasks. 
記事全体を表示
There are many parallels between the adoption of Ethernet in automotive and the adoption of Ethernet in avionics and industrial networking. This session provides an overview of Ethernet in modern aircraft and factory automation, as well as emerging technologies to further improve the suitability of Ethernet for these applications.
記事全体を表示
This class will provide an overview introduction of i.MX RT series, including their key features and key peripherals. This session also explores the design and implementation of a secure boot by making use and protect against firmware attacks. Secure designs begin with a security model consisting of policies, an understanding of the threat landscape and the methods used to enforce physical and logical security. To protect firmware execution given today’s threat landscape, there must be a policy to only allow execution of authenticated firmware. The methods used to enforce this policy rely on MCU security technology to create a protected boot flow. The boot firmware can contain public key cryptography to authenticate application code.
記事全体を表示
This presentation dedicated to IVI provides an overview of the software and hardware enablement available to accelerate customer time-to-market and reduce development risks. Namely i.MX 8, Ethernet Switch and PHY, audio tuner and amplifier, power management, supported by a Linux Genivi compliant BSP.
記事全体を表示
Explores the fast-growing Automotive Gateway market, identifying key use cases and requirements, and how gateways will evolve over the next decade.
記事全体を表示
Automotive Ethernet PHYs enable future driving scenarios by providing the necessary physical throughput power. While software brings added value for security, diagnosis, energy efficiency and safety. As the functional requirements for automotive PHY drivers differ from general purpose applications, additional functionality is needed to closely monitor and diagnose the device and to create advanced use cases like Layer-1 wake-up and sleep. In this session, these specific requirements for automotive Ethernet PHY SW are discussed. Existing PHY SW frameworks such as Linux or AUTOSAR are introduced. Finally, the session will touch upon typical application scenarios which require interaction with PHY SW.
記事全体を表示
Explains how the efficiency of a modern audio system has impacts in the vehicle well beyond audio.
記事全体を表示
IoT is all about ‘’Sense, Think and Act’’. Automation systems and decision making algorithms running in the Cloud or on the Edge need to be fed with the right data, actuators must be integrity protected and receive valid commands. Moreover data protection, Privacy and protection of business models become paramount to any IoT deployment. NXP’s new generation of embedded Secure Element SE050 redefines security and trust anchoring in IoT devices. Part of NXP’s ’Plug & Trust‘ solutions delivering security right out of the box, the new SE050 is the convergence between integrity protection of a trusted IoT platform, flexible and secured connections of edge to multiple Cloud services, and secure sensing. In this session the new SE050 security enclave for IoT devices will be introduced, along with the new use cases it enables for edge sensors as well as gateways and edge computing platforms.
記事全体を表示
Overview of S32K, MagniV and other GPIS products.
記事全体を表示
A guide to developing with the Yocto Project for i.MX application processors. Learn how to leverage the Yocto Project in development by adding layers and recipes, customizing images, working with the kernel, and other essential Yocto development tasks.
記事全体を表示
Overview of NXP’s General Purpose and Integrated Solutions (GPIS) Portfolio with focus on the S32K and S32M (MagniV) products.  
記事全体を表示
Introduction to the standard - with emphasis on how to apply it, cross BL.
記事全体を表示
Deep dive training on battery management applications: Detailed feature set and hardware configuration descriptions. 1.) Short market introduction on Battery Management Systems (BMS). 2.) Overview of key application requirements (incl. 14V, 48V, HV Daisy Chain, HV CAN, Wireless). 3.) Introduction to NXP BMS New product portfolio key features, value proposition. 4.) Future BMS product outlook.
記事全体を表示
Concept of SD-CPE, virtualization of functions/applications on CPE, centralized management of CPE by orchestrator, advantages, and applications scenario in home, enterprise and industry.
記事全体を表示
S32 Design Studio 3.0 S32V234 focus on configuration tools pin wizard, clocks config, with SDK configuration, FreeRTOS configuration and use building and running a project showing debug with S32 debugger on the m4 with code on target. Configuration tools suite formed from pins, clocks, peripherals, DCD, IVT are offering a complete view of the platform with complete access to all the details directly from the tool and possibility to generate, build and debug the applications.
記事全体を表示
This session covers all the newest i.MX processors available and touches on the ones that will soon be launched. Products from i.MX 6, i.MX 7 and i.MX 8 applications processors.
記事全体を表示