コネクト - トレーニング教材

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Connects - Training Material

Training Sessions Material



Home

Home is where the heart is..

Automotive

Silicon Valley 2019 - Automotive Presentation Files

Communication Infrastructure

Edge Intelligence

Industrial

Mobile, Wearable & Computing

IoT Smart Home

Hardware & Software Solutions

Silicon Valley 2019 - Industrial & IoT, Mobile, & Communication Infrastructure Presentation Files

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Multimedia Experience

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Secure Connected & Automated Vehicles

Smart Buildings & Consumer Goods

Secure Mobile, Healthcare & Wearables

Smart Machinery & Industrial Automation

Enabling Design, Technologies & Solutions

Smart Networks & Computing

Secure Connected & Automated Vehicles

Secure Connected & Automated Vehicles

ディスカッション

ソート順:
i.MX RT has a flexible external SPI Flash interface, which supports all existing SPI protocols. However, Serial Flash products may vary in READ performance due to the number of I/O, command protocols and the maximum frequency. Serial Flash Read performance has a direct impact on the system bootup time as well as code execution efficiency. In an advanced system design where system code is shadowed from Flash to DRAM, the initial boot time depends on the data transfer time from Flash to DRAM. In a cost-efficient system design, DRAM is reduced or eliminated since the processor will be able to fetch execution instructions directly from the Flash to the internal cache. During code fetching, a fixed length of data (typically 32- or 64-Byte) is read out from the flash. Shortening the overall 32-Byte or 64-Byte Read time will greatly reduce processor’s wait cycle, leading to improvement on XiP efficiency.
記事全体を表示
Overview of the S32x next-generation safety architecture spanning ASIL B to ASIL D. What’s new and how we better enable the customer with a full set of safety collateral including MCU HW, SW and SBC HW.
記事全体を表示
Safety by Software (SBSW) is a new way of achieving ASIL-D with high-level measures, supported by NXP S32X hardware. The SBSW hardware module together with SBSW firmware enables to check the user application flow, compare results of main and redundant algorithms and detect faulty behavior with high degree of independence. This session makes you familiar with SBSW usage, configuration, tools, etc.
記事全体を表示
AMP has been developing new market leading MCU solutions for the safety, electrification and powertrain markets. This presentation will go into the detail of the products and demonstrate their value in the target applications.
記事全体を表示
Join this session to understand the breakthrough security features integrated in the recently launched LPC5500 MCU Family. Along with Arm® TrustZone technology the LPC5500 SRAM PUF based key management makes security easy to use and easy to deploy. This session will start off by introducing the scope of securing a smart connected device. It will explain the need for addressing device life cycle in a scalable way that is easy to use and easy to deploy. Then it will detail the protected key management achievable when using LPC5500 with MCUXpresso Software & Tools.  
記事全体を表示
Join this session to understand the breakthrough security features integrated in the recently launched LPC5500 MCU Family. Along with Arm® TrustZone technology the LPC5500 SRAM PUF based key management makes security easy to use and easy to deploy. This session will start off by introducing the scope of securing a smart connected device. It will explain the need for addressing device life cycle in a scalable way that is easy to use and easy to deploy. Then it will detail the protected key management achievable when using LPC5500 with MCUXpresso Software & Tools.  
記事全体を表示
Join this session to understand the breakthrough security features integrated in the recently launched LPC5500 MCU Family. Along with Arm® TrustZone technology the LPC5500 SRAM PUF based key management makes security easy to use and easy to deploy. This session will start off by introducing the scope of securing a smart connected device. It will explain the need for addressing device life cycle in a scalable way that is easy to use and easy to deploy. Then it will detail the protected key management achievable when using LPC5500 with MCUXpresso Software & Tools.  
記事全体を表示
Hands-on workshop using the low cost KIT-HGDRONEK66 HoverGames drone reference platform for small autonomous vehicles. Learn about the open source PX4 flight stack vehicle manangement unit, NuttX RTOS, Mavlink, DDS RTPS services, associated Linux companion computer and Qgroundcontrol groundstation for vehicle configuration and flight logging and planning. Learn by example compiling the code and adding new functions within the PX4 modular software framework. Discover interfacing to Rapid-IOT via MAVLINK.
記事全体を表示
Market and application trends in automotive radar, supporting NCAP and autonomous architectures.
記事全体を表示
IoT is all about ‘’Sense, Think and Act’’. Automation systems and decision making algorithms running in the Cloud or on the Edge need to be fed with the right data, actuators must be integrity protected and receive valid commands. Moreover data protection, Privacy and protection of business models become paramount to any IoT deployment. NXP’s new generation of embedded Secure Element SE050 redefines security and trust anchoring in IoT devices. Part of NXP’s ’Plug & Trust‘ solutions delivering security right out of the box, the new SE050 is the convergence between integrity protection of a trusted IoT platform, flexible and secured connections of edge to multiple Cloud services, and secure sensing. In this session the new SE050 security enclave for IoT devices will be introduced, along with the new use cases it enables for edge sensors as well as gateways and edge computing platforms.
記事全体を表示
Along with industry leading performance and integration, the i.MX RT crossover processor family integrates strong security protections. With the latest NXP software and tools, every design can integrate boot authentication and encrypted execution. Join this session to use the MCUXpresso Tools to protect your design. Learn about the threats and attacks that can be mitigated for every embedded design.
記事全体を表示
People today face way too many options, especially when it comes to so called smart devices which can easily contain 50+ functional settings. With most people only using a few preferred settings, this session shows product managers, UI designers, and engineers how to leverage NXP’s out of the box Face Rec based Friction Free Interface production grade platform to rapidly add a truly seamless interface to devices such as appliances, home comfort systems, and alarm/safety/security panels, as well as many types of industrial equipment. By recognizing who you are and what you prefer based on past usage, today’s smart machines can tailor their interface to meet end consumer needs person by person (including controlling access) significantly improving customer satisfaction. Wi-Fi and/or connection to the cloud is NOT required to move your interface design to the next level!
記事全体を表示
Join this session to understand the breakthrough security features integrated in the recently launched LPC5500 MCU Family. Along with Arm® TrustZone technology the LPC5500 SRAM PUF based key management makes security easy to use and easy to deploy. This session will start off by introducing the scope of securing a smart connected device. It will explain the need for addressing device life cycle in a scalable way that is easy to use and easy to deploy. Then it will detail the protected key management achievable when using LPC5500 with MCUXpresso Software & Tools.
記事全体を表示
Join this session to learn how NXP security technology should be leveraged to secure the onboarding credentials using the LPC54S0xx MCU with state of the art security technology.
記事全体を表示
Learn how to get started with the Zephyr Project on i.MX RT. You will gain hands-on experience with the Zephyr build environment and program your first Zephyr application onto a board.
記事全体を表示
This session will cover Smart Home Applications and how sensors can be utilized to create such applications. Some key applications include Smart Door, Window Tamper Detect, Door Knock Detect, Smart HVAC filter, Smart Pill Box, Smart pool Pump, Smart Torch, Smart Stove and many more.
記事全体を表示
Bluetooth speakers and headsets, printers, cameras, projectors, set-top-boxes, TVs, Wi-Fi routers and a variety of home appliances like fridges, washing machines, air purifiers, coffee machines, blenders all have one thing in common: Near Field Communication (NFC) allows new features and easier handling. Just bringing two NFC-enabled devices close together is all it takes to create a connection. Accessories and consumables can be authenticated and configured without any user interaction, and without power supply. And commissioning an IOT node into a wireless network has never been as easy as it is now with NFC. We will share the latest status of NFC support in iOS and present the brand new NFC Tandem module.
記事全体を表示
No other company has the breadth and diversity of embedded solutions for addressing the challenge of IoT Security. From secure element ICs to advanced multimedia and networking processors, NXP delivers the technology needed for securing the entire Lifecycle of the end or edge node. In addition, with Edgescale Cloud services software, devices can be maintained from deployment until decomissioning. Join this class for an overview of NXP's security solution.
記事全体を表示
Wi-Fi 6 is the latest standard in WLAN technology also known as 802.11ax. This enables almost four times faster speed over the previous technology 802.11ac. NXP has been developing front end IC to support this upcoming technology and have won the reference design with a leading SoC vendor. In this course, participants will learn the key features of Wi-Fi 6 and how NXP FEIC will solve those challenges to deliver a cutting edge solution.
記事全体を表示
Building on the classroom training presentation "Deploying eIQ Machine Learning on NXP MCU and Apps Processors", this hands-on session will allow attendees to take a trained neural network model and deploy it on a i.MX RT1060 crossover processor. Attendees will use MCUXpresso as the development environment and implement an end-to-end use case. See notes here.
記事全体を表示