コネクト - トレーニング教材

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Connects - Training Material

Training Sessions Material



Home

Home is where the heart is..

Automotive

Silicon Valley 2019 - Automotive Presentation Files

Communication Infrastructure

Edge Intelligence

Industrial

Mobile, Wearable & Computing

IoT Smart Home

Hardware & Software Solutions

Silicon Valley 2019 - Industrial & IoT, Mobile, & Communication Infrastructure Presentation Files

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Automotive

Artificial Intelligence, Enabling Technologies, Security & Solutions

Smart Machinery & Industrial Automation

Multimedia Experience

Smart Networks & Computing

Smarter World Solutions & Multimode Connectivity

Emerging Trends & Innovation

Secure Connected & Automated Vehicles

Smart Buildings & Consumer Goods

Secure Mobile, Healthcare & Wearables

Smart Machinery & Industrial Automation

Enabling Design, Technologies & Solutions

Smart Networks & Computing

Secure Connected & Automated Vehicles

Secure Connected & Automated Vehicles

ディスカッション

ソート順:
This session introduces the S32K148´s ENET module. The enablement/configuration of the different networking layers presented with a demo based on our SDK platform using lwIP stack.
記事全体を表示
Building on the classroom training presentation "Deploying eIQ Machine Learning on NXP MCU and Apps Processors", this hands-on session will allow attendees to take a trained neural network model and deploy it on a i.MX RT1060 crossover processor. Attendees will use MCUXpresso as the development environment and implement an end-to-end use case. See notes here.
記事全体を表示
As IC geometries continue to shrink and switching speeds increase, designing electromagnetic systems and printed circuit boards to meet the required signal integrity and EMC specifications has become even more challenging. A new design methodology is required. Specifically, the utilization of an electromagnetic physics-based design methodology to control the field energy in your design will be discussed. This training module will walk through the development process and provide you with guidelines for building successful, cost effective printed circuit boards.
記事全体を表示
i.MX RT has a flexible external SPI Flash interface, which supports all existing SPI protocols. However, Serial Flash products may vary in READ performance due to the number of I/O, command protocols and the maximum frequency. Serial Flash Read performance has a direct impact on the system bootup time as well as code execution efficiency. In an advanced system design where system code is shadowed from Flash to DRAM, the initial boot time depends on the data transfer time from Flash to DRAM. In a cost-efficient system design, DRAM is reduced or eliminated since the processor will be able to fetch execution instructions directly from the Flash to the internal cache. During code fetching, a fixed length of data (typically 32- or 64-Byte) is read out from the flash. Shortening the overall 32-Byte or 64-Byte Read time will greatly reduce processor’s wait cycle, leading to improvement on XiP efficiency.
記事全体を表示
Join this session to understand the breakthrough security features integrated in the recently launched LPC5500 MCU Family. Along with Arm® TrustZone technology the LPC5500 SRAM PUF based key management makes security easy to use and easy to deploy. This session will start off by introducing the scope of securing a smart connected device. It will explain the need for addressing device life cycle in a scalable way that is easy to use and easy to deploy. Then it will detail the protected key management achievable when using LPC5500 with MCUXpresso Software & Tools.  
記事全体を表示
This presentation provides an overview of the new toolchain to support the S32 platform of MCUs and application processors, this includes an IDE with new project generation, extensive collateral for ease of use and getting started as well as the next-generation Debugger tools, a new Flash tool specifically design for the S32 platform, the S32 configuration tool plus numerous software products integarted into the toolchain for ease of customer use.
記事全体を表示
Overview of the S32x next-generation safety architecture spanning ASIL B to ASIL D. What’s new and how we better enable the customer with a full set of safety collateral including MCU HW, SW and SBC HW.
記事全体を表示
Join this session to understand the breakthrough security features integrated in the recently launched LPC5500 MCU Family. Along with Arm® TrustZone technology the LPC5500 SRAM PUF based key management makes security easy to use and easy to deploy. This session will start off by introducing the scope of securing a smart connected device. It will explain the need for addressing device life cycle in a scalable way that is easy to use and easy to deploy. Then it will detail the protected key management achievable when using LPC5500 with MCUXpresso Software & Tools.  
記事全体を表示
S32K based soution for smart LED drivers from Inova Semiconductor. Introduction, protocol overview, hardware and software insights.
記事全体を表示
How to build an automotive application using the S32 SDK, integration with design studio, tips & tricks, FreeRTOS, communication stacks; focus on S32K144 and S32K148.
記事全体を表示
Safety by Software (SBSW) is a new way of achieving ASIL-D with high-level measures, supported by NXP S32X hardware. The SBSW hardware module together with SBSW firmware enables to check the user application flow, compare results of main and redundant algorithms and detect faulty behavior with high degree of independence. This session makes you familiar with SBSW usage, configuration, tools, etc.
記事全体を表示
NXP BlueBox: In-depth look at hardware and software. Technical session explaining how to use Kalray hardware and Apollo software.
記事全体を表示
This session will provide a deep-dive technical session on how to develop, simulate and test machine vision algorithms with MATLAB toolsets like Computer Vision System and Image Processing on NXP S32V microprocessors. The MATLAB automatic generated code will be executed on the S32V234 SBC boards on Arm and APEX cores simultaneous to squeeze the best performance. The session will concentrate on feature detection for driver monitoring and will showcase various concepts like object detection using Viola-Jones, tracking a ROI using Kalman filters and various feature detection using Haar cascades classifiers. At the end of the session the participants will be able to develop from scratch complex algorithms for detecting various feature like: pedestrians, traffic signs, lane departure, etc. and do all these from a simple and user friendly environment like MATLAB.
記事全体を表示
Join this session to understand the breakthrough security features integrated in the recently launched LPC5500 MCU Family. Along with Arm® TrustZone technology the LPC5500 SRAM PUF based key management makes security easy to use and easy to deploy. This session will start off by introducing the scope of securing a smart connected device. It will explain the need for addressing device life cycle in a scalable way that is easy to use and easy to deploy. Then it will detail the protected key management achievable when using LPC5500 with MCUXpresso Software & Tools.  
記事全体を表示
NXP’s latest i.MX 8M processors require the latest memories to keep them running efficiently. As a system designer, your memory choices can impact the performance, size, cost, power reliability and longevity of your end product. We will discuss the latest memories supported on the new i.MX 8M processor family. This includes DDR3, DDR4 and LPDDR4. We will show designers how they can prioritize performance, power or price to develop the most optimum system. We will also provide details on eMMC 5.1 storage products. This includes high performance features including command queueing, and several new Cache operations. We will also highlight a new MCP that includes LPDDR4 and eMMC in a single space saving package. This session will provide designers with the tools necessary to create state-of-the-art i.MX 8M systems.
記事全体を表示
Create awareness and understanding of the Service Oriented Architecture. Illustration of concepts and status based on AMP Linux BSP.
記事全体を表示
Learn how to get started with the Zephyr Project on i.MX RT. You will gain hands-on experience with the Zephyr build environment and program your first Zephyr application onto a board.
記事全体を表示
Hands-on workshop using the low cost KIT-HGDRONEK66 HoverGames drone reference platform for small autonomous vehicles. Learn about the open source PX4 flight stack vehicle manangement unit, NuttX RTOS, Mavlink, DDS RTPS services, associated Linux companion computer and Qgroundcontrol groundstation for vehicle configuration and flight logging and planning. Learn by example compiling the code and adding new functions within the PX4 modular software framework. Discover interfacing to Rapid-IOT via MAVLINK.
記事全体を表示