Hello everyone, this document will explain on how to use the UUU (Universal Update Utility) tool to flash Linux to an i.MX device (i.MX 8MM). Requirements: MX 8M Mini EVK UUU tool documentation, available here Linux Binary Demo Files - i.MX 8MMini EVK UUU 1.2.135 binary Serial console emulator (tera term or putty) UUU auto script For this example is used the L4.14.98_2.0.0_ga demo image for the i.MX 8MM, inside the demo image we will find the auto script, which by default flash the eMMC of the board, the structure of the script is as following /***********************************************************************************/ uuu_version 1.2.39 # This command will be run when i.MX6/7 i.MX8MM, i.MX8MQ SDP: boot -f imx-boot-imx8mmevk-sd.bin-flash_evk # This command will be run when ROM support stream mode # i.MX8QXP, i.MX8QM SDPS: boot -f imx-boot-imx8mmevk-sd.bin-flash_evk # These commands will be run when use SPL and will be skipped if no spl # SDPU will be deprecated. please use SDPV instead of SDPU # { SDPU: delay 1000 SDPU: write -f imx-boot-imx8mmevk-sd.bin-flash_evk -offset 0x57c00 SDPU: jump # } # These commands will be run when use SPL and will be skipped if no spl # if (SPL support SDPV) # { SDPV: delay 1000 SDPV: write -f imx-boot-imx8mmevk-sd.bin-flash_evk -skipspl SDPV: jump # } FB: ucmd setenv fastboot_dev mmc FB: ucmd setenv mmcdev ${emmc_dev} FB: ucmd mmc dev ${emmc_dev} FB: flash -raw2sparse all fsl-image-validation-imx-imx8mmevk.sdcard FB: flash bootloader imx-boot-imx8mmevk-sd.bin-flash_evk FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi; FB: ucmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0 FB: done /***********************************************************************************/ In short, when the board goes into serial downloader mode UUU downloads the bootloader to internal RAM, once done and uboot is running, through fastboot utility it will flash .sdcard file and uboot to the eMMC on the board. More information about the protocol UUU use please refer to the UUU documentation (UUU.pdf) section 5 Supported protocol. Running the tool In order to run the tool the binary of uuu needs to be downloaded, the binary files can be downloaded from the link above, uuu.exe is for Windows and uuu is for Linux. Once downloaded it can be placed inside the same file as the demo image, this so it is easy to run and cleaner on the shell commands. Windows In windows OS the tool should be run using the Windows PowerShell in administrator mode, once open we will run the next commands: > .\uuu.exe uuu.auto Linux >$ sudo ./uuu uuu.auto The tool will start running and should be waiting for any i.MX device to be detected by host pc Preparing the board For the board to be flashed it is needed to be in download mode, the switch configuration (i.MX 8MM EVK) is as following: SW1101 - 1010XXXXXX SW1102 - XXXXXXXXX0 Connect a USB cable from the host pc which will run the tool to the USB OTG/TYPE C port, usually specified as download, on the board. Connect a USB cable from the host to the OTG-to-UART for console output, usually specified as debug, on the board. Open terminal emulator program with the following settings: Bits per second - 115200 Data bits - 8 Parity - None Stop bits - 1 Flow control - None Power on the board, the download will start and the serial prompt will show the progress in uboot, wait until the tool show success. Finally power off the board and change the switch configuration to boot from the eMMC, power on the board again and it should boot successfully! Built in scripts One can use the built in scripts using the -b option to burn the bootloader and the rootfs to the target flash, just type the command accordingly to the target flash device. SD Write bootloader only: Windows: > .\uuu.exe -b sd <bootloader> Linux: $ sudo ./uuu -b sd <bootloader> Replace <bootloader> for your .imx/.bin file, example using the i.MX 8MM for Windows and Linux respectively below. > .\uur.exe -b sd imx-boot-imx8mmevk-sd.bin-flash_evk $ sudo ./uuu -b sd imx-boot-imx8mmevk-sd.bin-flash_evk Write whole Linux image Windows: > .\uuu.exe -b sd_all <bootloader> <rootfs>.sdcard Linux: $ sudo ./uuu -b sd_all <bootloader> <rootfs>.sdcard Replace <bootloader> and <rootfs> for the name of your .imx/.bin and .sdcard files respectively, example using the i.MX 8MM below. > .\uuu.exe -b sd_all imx-boot-imx8mmevk-sd.bin-flash_evk fsl-image-validation-imx-imx8mmevk.sdcard $ sudo ./uuu -b sd_all imx-boot-imx8mmevk-sd.bin-flash_evk fsl-image-validation-imx-imx8mmevk.sdcard eMMC Write bootloader only Windows: > .\uuu.exe -b emmc <bootloader> Linux: $ sudo ./uuu -b emmc <bootloader> Example using i.MX 8MM > .\uuu.exe -b emmc imx-boot-imx8mmevk-sd.bin-flash_evk $ sudo ./uuu -b emmc imx-boot-imx8mmevk-sd.bin-flash_evk Write whole Linux image Windows: > .\uuu.exe -b emmc_all <bootloader> <rootfs>.sdcard Linux: $ sudo ./uuu -b emmc_all <bootloader> <rootfs>.sdcard Example using i.MX 8MM > .\uuu.exe -b emmc_all imx-boot-imx8mmevk-sd.bin-flash_evk fsl-image-validation-imx-imx8mmevk.sdcard $ sudo ./uuu -b emmc_all imx-boot-imx8mmevk-sd.bin-flash_evk fsl-image-validation-imx-imx8mmevk.sdcard Hope this will helpful for everyone who is starting to use this flashing tool.
記事全体を表示