i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
Platform: i.MX8QXP/8QM OS: Linux Supported Camera Modules: Max9286 + Max9271 + OV10635, Default BSP Max9286 + Max96705 + AR0144, patch Max9286 + Max96705 + OV9284, patch Max9286 + Max96705 + AP0101 + AR0132, patch NVP6324 + NVP2431 + IMX225, patch TP2855 + TP3812 + IMX307, patch ISL7998x + NTSC/PAL Sensor, patch adv7180 + NTSC/PAL Sensor, patch Detailed description in the attachment.
View full article
         In recent months, some I.MX customers hope to compile u-boot-fw-utils in yocto and get fw_printenv & fw_setenv tools.          Although there are u-boot-fw-utils bblayers in Yocto recipes, by default, u-boot-fw-utils is not based on u-boot-imx, but downloaded from the u-boot source website, when using bitbake When u-boot-fw-utils compiles it, it will fail to compile.          For example: # cd  ~/imx-yocto-bsp-5.4.3_1.0.0 # DISTRO=fsl-imx-fb MACHINE=imx6sxsabresd source imx-setup-release.sh -b build_sabresd # bitbake u-boot-fw-utils -c compile          If changing .config to be mx6sxsabresd_optee_defconfig in the top directory of u-boot source code, new errors will occur, like descriptions in the link:          https://community.nxp.com/message/1318081?commentID=1318081#comment-1318081            The root cause is that the u-boot is not u-boot-imx.          If we did the test below, it is easy to validate it.      Compiling u-boot # bitbake u-boot-imx -c compile          After compilation is done, u-boot-imx source code will be released .      Changing u-boot source code of u-boot-fw-utils directory          Replace u-boot source code in u-boot-fw-utils directory with u-boot-imx source code. Then continue to compile u-boot-fw-utils # bitbake u-boot-fw-utils -c compile          We will find it can be compiled successfully. This shows that when u-boot-fw-utils is compiled, the downloaded u-boot source code must be u-boot-imx.          In order to achieve this, we need to add recipes to yocto's u-boot-imx, and we can successfully compile fw_printevn and fw_setenv through the bitbake command. Please follow these steps to add u-boot-fw-utils for i.mx to yocto! copy 2 files in attacments to ~/imx-yocto-bsp-5.4.3_1.0.0/sources/meta-imx/meta-bsp/recipes-bsp/u-boot cd ~/imx-yocto-bsp-5.4.3_1.0.0 run below comands # DISTRO=fsl-imx-fb MACHINE=imx6sxsabresd source imx-setup-release.sh -b build_sabresd # bitbake u-boot-imx-fw-utils -c compile # bitbake u-boot-imx-fw-utils -c install   Then you will get fw_printenv & fw_setenv [Comment]          If i.MX users are using other version of linux BSP, she only need to modify the following content of u-boot-imx-common_2019.04.inc to compile u-boot-fw-utils. …… LIC_FILES_CHKSUM = "file://Licenses/gpl-2.0.txt;md5=b234ee4d69f5fce4486a80fdaf4a4263"   UBOOT_SRC ?= "git://source.codeaurora.org/external/imx/uboot-imx.git;protocol=https" SRCBRANCH = "lf-5.4.y_v2019.04" SRC_URI = "${UBOOT_SRC};branch=${SRCBRANCH} \ " SRCREV = "228843cdf5435d4bd69f42a6015f78761ff4cc0d" ……          Then compile it following above steps.          Example for L4.14.98_2.0.0: 1.Copy u-boot-imx-common_2019.04.inc & u-boot-imx-fw-utils_2019.04.bb to ~/imx-release-bsp-4.14.98-2.0.0/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-bsp/u-boot/ 2.Rename files name according to u-boot version u-boot-imx-common_2018.03.inc     u-boot-imx-fw-utils_2018.03.bb 3.Modifying u-boot-imx-common_2018.03.inc In the directory, there is u-boot-imx_2018.03.bb file, open it, and find the link of u-boot and check sum, and use lines below to replace those lines in u-boot-imx-common_2018.03.inc In u-boot-imx_2018.03.bb file: …… LICENSE = "GPLv2+" LIC_FILES_CHKSUM = "file://Licenses/gpl-2.0.txt;md5=b234ee4d69f5fce4486a80fdaf4a4263"   UBOOT_SRC ?= "git://source.codeaurora.org/external/imx/uboot-imx.git;protocol=https" SRCBRANCH = "imx_v2018.03_4.14.98_2.0.0_ga" SRC_URI = "${UBOOT_SRC};branch=${SRCBRANCH}" SRCREV = "87a19df5e462f1f63e8a6d2973c7fb9e95284d04" …… Then in u-boot-imx-common_2018.03.inc, there is the same contents as above: Save it and exit. Go back to the top directory of yocto: ~/imx-release-bsp-4.14.98-2.0.0 # cd ~/imx-release-bsp-4.14.98-2.0.0 # DISTRO=fsl-imx-fb MACHINE=imx6sxsabresd source fsl-setup-release.sh -b build_sabresd # bitbake u-boot-imx-fw-utils -c compile # bitbake u-boot-imx-fw-utils -c install          The same method can be used for other Linux BSP versions.       NXP TIC Team Weidong Sun 05/28/2020
View full article
SW: Linux 4.14.98_2.2.0 bsp release , gpu sdk 5.3.0 and patch in this doc HW: i.MX8QXP MEK board Inspired by the GIMP adjust color curve tool,  I write similar gui test code for i.MX8QXP gamma curve tuning. That is on display will show one linear curve first, use mouse to change any part of this curve, after that calculate value of point on changed curve , then pass related value to i.MX8QXP DPU gammcor unit , at last the display effect will be changed by DPU. When test code start up , will draw Y=X curve on display, that will from (0,0) to (500, 500) to (1023,1023). After you use mouse drag some part of the curve, will generated a new point (x_new, y_new) which is not on original Y=X curve. Then need draw a new curve that pass  through the (0,0) , (500, 500) , (x_new, y_new), (1023,1023).  That new curve , i choose to use Catmull-Rom Splines to get it. Use Catmull-Rom Splines for approximate a curve that pass through n point, then need n+2 control point. Extra 2 point could be selected as you want ,and they will affect the shape of the curve. Catmull-Rom Splines could pass through all control point, it is C1 continuity, no convex hull property. For example, there is four control point p0, p1 , p2 , p3,  to draw the curve pass through all of them, it could divide to segment p0 to p1 , segment p1 to p2 , segment p2 to p3. For segment p1 to p2 , select four control point as p0,p1, p2, p3, use Catmull-Rom Splines as below: For segment p0 to p1 , need use four control point as p0, p0, p1, p2: For segment p2 to p3, need use four control point as p1, p2, p3, p3: In this test code,  i will use gpu vertex shader to calculate each segment of curve, then use transform feedback to read back point value of each segment to cpu side, cpu side will pass related value to DPU gammcor unit for gamma tuning.   Test steps: Apply 8qxp_dpu_gammacor_4.14.98_2.2.0.diff on linux-imx for i.MX8QXP DPU device driver. Apply dpu_gamma_curve_gpusdk5.3.0.diff on imx-gpu-sdk for build this gui test code. Update the new kernel image, and copy test code to rootfs. Run any other application first to draw some thing on screen, for example  /usr/share/cinematicexperience-1.0/Qt5_CinematicExperience. Then run gui test code in this code, S01_SimpleTriangle_Wayland. Then there will show one linear curve on display , use mouse to change the curve as you like by put mouse cursor close to the curve, press the mouse button , drag it and release the mouse button, you will see the new curve on display , and also the display effect also be changed. Reference: 1>https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-processors/i-mx-8-processors/i-mx-8x-family-arm-cortex-a35-3d-graphics-4k-video-dsp-error-correcting-code-on-ddr:i.MX8X  2>https://www.nxp.com/design/software/embedded-software/linux-software-and-development-tools/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=Design_Tools_Tab  3>https://github.com/NXPmicro/gtec-demo-framework  4>https://en.wikipedia.org/wiki/Cubic_Hermite_spline  5>http://www.mvps.org/directx/articles/catmull
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-342059 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-342654 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-341996 
View full article
本文旨在说明基于i.MX8X如何设计硬件平 台,包括相关设计资源的收集与学习,硬件原 理图设计,layout,启动(bring up),量产准备, 及正式量产后的失效分析与失效控制。主要是 帮助厘清硬件开发相关从头到尾的问题。 请注意本文为培训和辅助文档,部分内容源 自PMIC/i.MX8X硬件开发指南,并作中文翻 译,强调重点,和查缺补漏,本文不是官方文 档的替代,请一切以官方文档为准。 目录: i.MX8X硬件参考平台 ................................................. 3 2 i.MX8X硬件设计资源 ................................................. 5 i.MX8X芯片相关设计资源 ............................................... 5 i.MX8QXP MEK板外设相关设计资源 ........................... 10 i.MX8QXP 硬件接口规范 .............................................. 11 3 i.MX8X原理图设计检查点 ........................................ 13 PMIC+i.MX8X供电能力和上电时序 .............................. 13 PMIC电源输出端设计 ................................................... 17 I.MX8X电源输入端及去耦设计 ..................................... 22 LPDDR4内存设计 ........................................................ 23 DDR3L内存设计 ........................................................... 25 I2C总线设计 ................................................................. 26 Reset,Wdog reset和On/Off设计建议 ......................... 27 PCIe设计 ...................................................................... 29 USB设计 ...................................................................... 30 晶体时钟设计 ............................................................... 32 JTAG信号端接设计 ...................................................... 34 未使用接口管脚的端接处理 .......................................... 35 GPIO管脚的设计策略 ................................................... 37 调试接口建议 ............................................................... 37 4 i.MX8X 布线设计检查点 ........................................... 40 PMIC电源输出端布线建议 ............................................ 40 i.MX8X端去耦电容摆放 ................................................ 41 电源布线建议 ............................................................... 41 PCB叠层建议 ............................................................... 43 内存布线通用建议 ........................................................ 43 LPDDR4内存布线建议 ................................................. 44 DDR3L内存布线建议.................................................... 45 内存信号完整性仿真建议 ............................................. 47 内存JEDEC信号兼容性测试 ......................................... 48 高速电路板布线建议..................................................... 49 时钟建议 ...................................................................... 50 信号线阻抗建议 ............................................................ 53 USB布线建议 ............................................................... 54 5 i.MX8X硬件散热设计 ............................................... 54 6 i.MX8X硬件启动bring up .......................................... 56 Bring up需要参考的文档与使用工具............................. 56 i.MX8X Bring up需要准备的文档与使用工具 ............................. 60 Bring up检查列表 .......................................................... 65 7 试产与量产前检查点 ................................................. 67 内存稳定性 ................................................................... 67 ESD与EMI考虑 ............................................................. 68 产线设计 ....................................................................... 69 8 i.MX8X失效分析流程 ................................................ 70 NXP失效分析服务 ........................................................ 70 NXP FA失效分析流程 ................................................... 70 筛查是否是芯片原生问题 .............................................. 72 9 量产厂线的EOS/ESD控制 ........................................ 73 什么是EOS/ESD ........................................................... 73 设计中的EOS/ESD风险检查点 ..................................... 75 生产产线中的EOS/ESD风险与防护 .............................. 78
View full article
The document to descript change the u-boot environment variables under the Linux rootfs.  Also provide a demo on i.MX6ull evk of sdcard mirror.  Linux fw_printenv fw_setenv to access U-Boot's environment variables.pdf  --- the document fw_printenv_fw_setenv_demo_iMX6ullevk_L4.14.98_2.0.0_ga.sdcard  --- demo sdcard mirror
View full article
In order to improve the speed of compilation, VMWare Player 14.0 is installed on local hard disk, and Ubuntu 18.04 LTS is installed on a SSD with at least 500GB size and USB3.1 specification. When installing ubuntu 18.04 LTS to SSD, it should be allocated at least 350GB of disk space, because compiling this version of android requires a larger disk space. The following are detailed compilation steps: Part l Configuring Ubuntu 18.04 LTS 1. Installing Ubuntu 18.04 on VMplayer 14.0 After installation is done, root user should be set at first. # sudo passwd root Then follow these steps to configuration ubuntu 18.04 for environment of compiliation --Changing sources of ubuntu 18.04 mirror If you are Chinese users, you can do the step, which can improve your system performance. # sudo cp /etc/apt/sources.list /etc/apt/sources.list.bak # sudo geit /etc/apt/source.list Comment I.MX customers outside China do not need to modify Ubuntu source list, or can modify it to local mirror site of Ubuntu 18.04, which can improve the speed of software upgrade.    Delet all sources and copy following lines here, Then save it and exit Changing ubuntu source deb https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic main restricted universe multiverse # deb-src https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic main restricted universe multiverse deb https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-updates main restricted universe multiverse # deb-src https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-updates main restricted universe multiverse deb https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-backports main restricted universe multiverse # deb-src https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-backports main restricted universe multiverse deb https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-security main restricted universe multiverse # deb-src https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-security main restricted universe multiverse # deb https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-proposed main restricted universe multiverse # deb-src https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-proposed main restricted universe multiverse    Then running these 2 commands to update sources and packages    # sudo apt-get update    # sudo apt-get upgrade 2. Installing packages for compiliation Packages for compiliation # sudo apt-get install flex bison gperf build-essential zlib1g-dev lib32ncurses5-dev x11proto-core-dev libx11-dev lib32z1-dev libgl1-mesa-dev tofrodos python-markdown libxml2-utils xsltproc # sudo apt-get install uuid-dev:i386 liblzo2-dev:i386 gcc-multilib g++-multilib subversion openssh-server openssh-client uuid uuid-dev zlib1g-dev liblz-dev lzop liblzo2-2 liblzo2-dev git-core curl # sudo apt-get install u-boot-tools mtd-utils android-tools-fsutils openjdk-8-jdk device-tree-compiler aptitude libcurl4-openssl-dev nss-updatedb # sudo apt-get install chrpath texinfo gawk cpio diffstat gdisk m4 libz-dev libssl-dev Part 2 Compiling Android Q10.0.0_2.1.0 BSP 1. Downloading NXP source code for Android Q10.0.0_2.1.0    File name is imx-android-10.0.0_2.1.0.tar.gz.    Copy the file to ~/, and decompress it.    # cd ~/    # tar zxvf ./imx-android-10.0.0_2.1.0.tar.gz    Then “imx-android-10.0.0_2.1.0” directory is created at ~/, now run the command to download android source code. # source ./imx-android-10.0.0_2.1.0/imx_android_setup.sh Comment imx_android_setup.sh is a script file, which includes all steps needed by the environment of android Q10.0.0_2.1.0 BSP. If network environment is enough good, several hours later, it will be done. 2. Compiling Android Q10.0.0_2.1.0 Referring to steps in Android_User's_Guide.pdf, We summaries steps for compilation here: (1) Preparing cross-compile tool chain    In Android_User's_Guide.pdf, 2 kinds of tool chain are recommended for users. --- gcc-arm-8.3-2019.03-x86_64-aarch64-elf.tar.xz --- gcc-arm-8.3-2019.03-x86_64-aarch64-linux-gnu.tar.xz    Users can select one of them, and then decompress it to /opt/ directory. On how to download them or more details, see Android_User's_Guide.pdf, page 3. Here we will use gcc-arm-8.3-2019.03-x86_64-aarch64-linux-gnu.tar.xz as tool chain. (2) Beginning to Compile Android Q10.0.0_2.1.0 BSP    Since this version of Android BSP requires high memory capacity when compiling, if the memory configuration of the virtual machine is incorrect, it is very likely to cause the compilation to fail. The following is a list of variable tests for user reference: # cd android_build # export AARCH64_GCC_CROSS_COMPILE=/opt/gcc-arm-8.3-2019.03-x86_64-aarch64-linux-gnu/bin/aarch64-linux-gnu- # source build/envsetup.sh # lunch evk_8mp-userdebug # ./imx-make.sh -j2 2>&1 | tee build-log.txt Part 3 Errors During Compilation 1. Allocating 8GB Memory For VMware Player # ./imx-make.sh -j1 2>&1 | tee build-log.txt 2. Allocating 12GB Memory For VMware Player # ./imx-make.sh -j4 2>&1 | tee build-log.txt # ./imx-make.sh -j4 2>&1 | tee build-log.txt (Run it again) # ./imx-make.sh -j4 2>&1 | tee build-log.txt (Run it again)       So if we use 4 thread to compile BSP, command for compilation will have to be run for 3 times. NXP TIC Team Weidong Sun 2020/4/30
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-342877 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-342729 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-342719 
View full article
Pre-Sales: i.MX8/8X applications in automotive(Chinese Version) https://community.nxp.com/docs/DOC-345825 i.MX8X website design resource guide: (Chinese Version) https://community.nxp.com/docs/DOC-345676 After-Sales: i.MX8X memory configuration&test application notes: (Chinese Version) https://community.nxp.com/docs/DOC-345803 i.MX8X hardware design guide: (Chinese Version) https://community.nxp.com/docs/DOC-346582 i.MX8X_4.19.35_bootloader customization application notes: (Chinese Version) https://community.nxp.com/docs/DOC-345713 i.MX8X_4.19.35_kernal customization application notes: (Chinese Version) https://community.nxp.com/docs/DOC-345714 i.MX8X_4.14.98_bootloader customization application notes: (Chinese Version) https://community.nxp.com/docs/DOC-342448 i.MX8X_4.14.98_kernal customization application notes: (Chinese Version) https://community.nxp.com/docs/DOC-344217 i.MX8X_5.4.24_bootloader customization application notes: (Chinese Version) https://community.nxp.com/docs/DOC-347131
View full article
L5.4.3_1.0.0 release is now available on IMX_SW landing page: BSP Updates and Releases -> Linux ->Linux L5.4.3_1.0.0. Documentation -> Linux -> Linux 5.4.3_1.0.0 Documentation Files available: # Name Description 1 imx-yocto-LF_L5.4.3_1.0.0.zip i.MX L5.4.3_1.0.0 for Linux BSP Documentation. Includes Release Notes, User Guide. 2 LF_v5.4.y-1.0.0_images_MX6QPDLSOLOX.zip i.MX 6QuadPlus, i.MX 6Quad, i.MX 6DualLite, i.MX 6Solox Linux Binary Demo Files 3 LF_v5.4.y-1.0.0_images_MX6SLLEVK.zip i.MX 6SLL EVK Linux Binary Demo Files 4 LF_v5.4.y-1.0.0_images_MX6UL7D.zip i.MX 6UltraLite EVK, 7Dual SABRESD, 6ULL EVK Linux Binary Demo Files 5 LF_v5.4.y-1.0.0_images_MX7ULPEVK.zip i.MX 7ULP EVK Linux Binary Demo Files  6 LF_v5.4.y-1.0.0_images_MX8MMEVK.zip i.MX 8M Mini EVK Linux Binary Demo Files  7 LF_v5.4.y-1.0.0_images_MX8MNEVK.zip i.MX 8M Nano EVK Linux Binary Demo Files  8 LF_v5.4.y-1.0.0_images_MX8MQEVK.zip i.MX 8M Quad EVK Linux Binary Demo files 9 LF_v5.4.y-1.0.0_images_MX8QMMEK.zip i.MX 8QMax MEK Linux Binary Demo files 10 LF_v5.4.y-1.0.0_images_MX8QXPMEK.zip i.MX 8QXPlus MEK Linux Binary Demo files 11 imx-scfw-porting-kit-1.2.10.1.tar.gz System Controller Firmware (SCFW) porting kit v1.2.10.1 for L5.4.3_1.0.0   Target board: MX 8 Series MX 8QuadXPlus MEK Board MX 8QuadMax MEK Board MX 8M Quad EVK Board MX 8M Mini EVK Board MX 8M Nano EVK Board MX 7 Series MX 7Dual SABRE-SD Board MX 7ULP EVK Board MX 6 Series MX 6QuadPlus SABRE-SD and SABRE-AI Boards MX 6Quad SABRE-SD and SABRE-AI Boards MX 6DualLite SDP SABRE-SD and SABRE-AI Boards MX 6SoloX SABRE-SD MX 6UltraLite EVK Board MX 6ULL EVK Board MX 6ULZ EVK Board MX 6SLL EVK Board   What’s New/Features: Please consult the Release Notes.   Known Issues: For known issues and more details please consult the Release Notes.   More information on changes of Yocto, see: README: https://source.codeaurora.org/external/imx/imx-manifest/tree/README?h=imx-linux-zeus ChangeLog: https://source.codeaurora.org/external/imx/imx-manifest/tree/ChangeLog?h=imx-linux-zeus      
View full article
[中文翻译版] 见附件   原文链接: i.MX Create Android SDCard Mirror 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343079 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343054 
View full article
We will cross compile L5.4.3_1.0.0 on ubuntu18.04 LTS platform in three steps. 1. Installing Ubuntu 18.04 to vmplayer14 & Configuring Ubuntu 18.04 LTS 2. Compiling L5.4.3_1.0.0 BSP According to Steps in i.MX_Yocto_Project_User's_Guide.pdf 3. Handling tensorflow-lite compilation errors. --BEGIN No.1 Installing Ubuntu 18.04 to vmplayer14 & Configuring Ubuntu 18.04 LTS 1. Install 18.04 on vmplayer After installation is done, root user should be set at first. # sudo passwd root Then follow these steps to configuration ubuntu 18.04 for environment of compiliation --Changing sources of ubuntu 18.04 mirror If you are Chinese users, you can do the step, which can improve your system performance. # sudo cp /etc/apt/sources.list /etc/apt/sources.list.bak # sudo geit /etc/apt/source.list Comment I.MX customers outside China do not need to modify Ubuntu source list, or can modify it to local mirror site of Ubuntu 18.04, which can improve the speed of software upgrade. Delet all sources and copy following lines here, Then save it and exit Update ubuntu source deb https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic main restricted universe multiverse # deb-src https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic main restricted universe multiverse deb https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-updates main restricted universe multiverse # deb-src https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-updates main restricted universe multiverse deb https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-backports main restricted universe multiverse # deb-src https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-backports main restricted universe multiverse deb https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-security main restricted universe multiverse # deb-src https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-security main restricted universe multiverse # deb https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-proposed main restricted universe multiverse # deb-src https://mirrors.tuna.tsinghua.edu.cn/ubuntu/ bionic-proposed main restricted universe multiverse Then running these 2 commands to update sources and packages # sudo apt-get update # sudo apt-get upgrade 2. Installing packages for compiliation Packages For Compiling BSP # sudo apt-get install flex bison gperf build-essential zlib1g-dev lib32ncurses5-dev x11proto-core-dev libx11-dev lib32z1-dev libgl1-mesa-dev tofrodos python-markdown libxml2-utils xsltproc # sudo apt-get install uuid-dev:i386 liblzo2-dev:i386 gcc-multilib g++-multilib subversion openssh-server openssh-client uuid uuid-dev zlib1g-dev liblz-dev lzop  liblzo2-2 liblzo2-dev git-core curl # sudo apt-get install u-boot-tools mtd-utils android-tools-fsutils openjdk-8-jdk device-tree-compiler aptitude libcurl4-openssl-dev nss-updatedb # sudo apt-get install chrpath texinfo gawk cpio diffstat No.2 Compiling L5.4.3_1.0.0 BSP According to Steps in i.MX_Yocto_Project_User's_Guide.pdf          The detailed BSP compilation steps are given in i.MX_Yocto_Project_User's_Guide.pdf. Here are just some tips and simple steps. For Chinese customers, the system may not respond when the repo init or repo sync command is executed after obtaining the repo script. Detailed description is below: (1)Getting repo script # mkdir ~/bin (this step may not be needed if the bin folder already exists) # curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo # chmod a+x ~/bin/repo # export PATH=~/bin:$PATH (2)Getting Yocto source # mkdir imx-yocto-bsp # cd imx-yocto-bsp # repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-zeus -m imx-5.4.3-1.0.0.xml # repo sync          After running repo init or repo sync, you may encounter a situation where there is no progress for a long time, and repo sync stops there without any prompt. This may be caused by googlesource site being inaccessible.          At this time, you can modify the googlesource URL to the URL of Tsinghua University. # gedit ./repo          Changing REPO_URL = 'https://gerrit.googlesource.com/git-repo'          To be:                    REPO_URL = 'https://mirrors.tuna.tsinghua.edu.cn/git/git-repo'          Save and exit. Then run “repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-zeus -m imx-5.4.3-1.0.0.xml”. or repo sync No.3 Handling tensorflow-lite compilation errors       If you encounter a tensorflow-lite compilation error during the compilation process, the following processing methods may be helpful to you. Cause Analysis:          Compiling tensorflow-lite requires three steps: fetching packages, configuring environment, and compiling code.          During the configuring environment, the following 8 software packages need to be downloaded. If any of the 8 files are not successfully downloaded, an error will be reported and compilation will be terminated.          ①9f48e814419e.tar.gz          ②38ebac7b059e84692f53e5938f97a9943c120d98.zip          ③release-1.8.0.tar.gz          ④389ec3f906f018661a5308458d623d01f96d7b23.tar.gz          ⑤master.zip          ⑥816a4ae622e964763ca0862d9dbd19324a1eaf45.tar.gz          ⑦1f5eae5d6a135ff6811724f6c57f911d1f46bb15.tar.gz          ⑧fft.tgz          If you encounter this problem, you can refer to the following methods to solve it. Open the file with editor: ~/imx-yocto-bsp/build-xwayland/tmp/work/aarch64-poky-linux/tensorflow-lite/1.13.2-r0/git/tensorflow/lite/tools/make/download_dependencies.sh URLs EIGEN_URL="https://bitbucket.org/eigen/eigen/get/9f48e814419e.tar.gz" GEMMLOWP_URL="https://github.com/google/gemmlowp/archive/38ebac7b059e84692f53e5938f97a9943c120d98.zip" GOOGLETEST_URL="https://github.com/google/googletest/archive/release-1.8.0.tar.gz" ABSL_URL="https://github.com/abseil/abseil-cpp/archive/389ec3f906f018661a5308458d623d01f96d7b23.tar.gz" NEON_2_SSE_URL="https://github.com/intel/ARM_NEON_2_x86_SSE/archive/master.zip" FARMHASH_URL="https://github.com/google/farmhash/archive/816a4ae622e964763ca0862d9dbd19324a1eaf45.tar.gz" FLATBUFFERS_URL="https://github.com/google/flatbuffers/archive/1f5eae5d6a135ff6811724f6c57f911d1f46bb15.tar.gz" FFT2D_URL="http://www.kurims.kyoto-u.ac.jp/~ooura/fft.tgz" Save and exit. [comment]     Don’t run “bitbake tensorflow-lite -c cleanall before you modify it”, otherwise files will be deleted.  Then try to compile tensorflow-lite like below: # bitbake tensorflow-lite -c compile   At the same time, we can open this directory and check if the following directories are created. If these 8 directories are successfully created, it means that links we modified are no problem.          After tensorflow-lite is successfully built, we can continue to compile full images. # bitbake imx-image-full --END NXP TIC team Weidong Sun 2020/3/30
View full article
-BACKGROUND       Since the release of i.MX8MQ and i.MX8M Mini, some customers have submitted questions about the design of USB2.0 for these two processors: due to the needs of the project, there is no need to use USB3.0 and USB TYPE-C. Therefore, these applications need to use a conventional USB2.0 interface design similar to i.MX6Q.       In order for customers with similar needs to complete the design smoothly, this document summarizes the answers to previous customer responses and draws two USB2.0 design schematics. At the same time, the i.MX expert hardware team member helped review these two drawings, and the i.MX Expert software team gave suggestions on software adjustments. -BEGIN       i.MX8MQ supports USB3.0 and is compatible with USB2.0, i.MX8M Mini only supports USB2.0, not USB3.0. In both development boards, the USB TYPE-C design scheme is used. We must remove the USB TYPE-C, PD chip and logic chip. At the same time, change the connector to MicroUSB and USB TYPE-A-F. No.1 Hardware Design 1. IOMUX list 2 、USB circuit design (1) USB Power & OC control I.MX8MM i.MX8MQ                                                 i.MX8MQ                                              i.MX8MQ [Comment] For i.MX8MQ -USB1 is configured as Dual Role Mode, USB1 OTG ID is used for detection -USB2 is configured as fixed Host mode, USB2 OTG ID is used for detection -i.MX8M Mini USB2.0                                        i.MX8M Mini                                     i.MX8M Mini [Comment] For i.MX8M Mini -USB1 is configured as Dual Role Mode, USB1 OTG ID is used for detection -USB2 is configured as fixed Host mode, USB2 OTG ID is used for detection (3) Additional description --About USB1_VBUS & USB2_VBUS of i.MX8M Mini          According to i.MX8M Mini datasheet, USB1_VBUS & USB2_VBUS allows 0~3.9V input. See below, please! Therefore, some customers have questioned the USB1_VBUS on the I.MX8M Mini-EVK. From the drawings, the external input voltage exceeds this range.          In fact, customers do not need to worry about this problem. There are internal voltage-dividing resistors on the USB1_VBUS and USB2_VBUS pins. As long as the customer refers to the design method on the I.MX8M Mini-EVK, the input voltage of these 2 pins can be guaranteed Inside. --About USBx OTG ID & USBx_ID (1) USBx_OTG_ID          USBx OTG ID is also called GPIO ID, which is the same as that of i.MX6Q. During the work process, the software changes the role between device and host according to the level of the ID pin from high to low or from low to high. (2)USBx_ID          USBx_ID is called USB PHY ID, which can also perform the same function as USBx OTG ID. (3)Using USBx_OTG_ID or USBx_ID          USBx_OTG_ID is recommended. But if customer wants to use USBx_ID, for i.MX8MQ, she can configure USB_CTL0_ADDR[utmiotg_iddig_sel] register. And for I.MX8M Mini, USBNC_n_CTRL2[DIG_ID_SEL] register. [Comment]          The configuration is got from reference manual of these 2 processors, due to no suitable board, this configuration is not validated on board. Customers can try it. (4) About Flashing Images to the Storage of Board          For an empty board or a board that requires an update image, we need to use the USB interface to program the image. At this time, we need the USB interface to work in device mode. For this, the ROM CODE inside the CPU will ensure that the USB works in device mode. No.2 Tuning Software 1.IOMUX According to the actual application, the signals to be used are multiplexed in the dts file. This step is relatively simple and will not be described here 2. Tuning USB configuration in u-boot / device tree For i.MX8M Mini & i.MX8MQ, i.MX Expert softer team gives the following suggestions, I quote their suggestions here:       Customer can try it by removing CONFIG_USB_TCPC in imx8mm_evk_defconfi and well as removing the typec_ptn5110_1/2 dependencies in the fsl-imx8mm-evk.dts. The uboot does check the state of the Type C ICs and crash or gets stuck if they are removed. --i.MX8M Mini U-BOOT:  CONFIG_USB_TCPC=n Device Tree: &usbotg1 {     status = "okay"; }; &usbotg2 {     status = "okay"; --------------------------------------------------------- --i.MX8MQ --u-boot CONFIG_USB_TCPC=n --Node of Device tree &usb_dwc3_0 {              status = "okay";              /*extcon = <&typec_ptn5100>;*/              dr_mode = "otg";              hnp-disable;              srp-disable;              adp-disable;              maximum-speed = "high-speed"; }; ---------------------------------------------- -END [Comment] If you encounter problems while using this document, please submit a ticket to me. Here are the steps to submit a ticket: 1. Open below SUPPORT site, click blue "Go to Tickets" in the middle. http://www.nxp.com/support/support:SUPPORTHOME 2.Then you will be requested to Login, if you have no an account, please first Register with your business email. 3.After login, please "Create New Cases" button in the middle, then you can submit your question. NXP TIC team Weidong Sun 2020/3/30
View full article