i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
This article will describe one suggestion for one issue that UART continuously generate RX interrupts and receive 0xFF even when Rx line is continuously high in some cases on imx6 series. Below I will explain with imx6DL. Some settings are just to make it easier to reproduce. BSP version: L5.4.70-2.3.0 Board HW: MCIMX6DL-SDB When issue happen Config imx6DL UART3 as the serial port to 1200 baud, 8-N-1 format. Keep the RX Line high. Make the RX line low and keep it for a short time (360 usec-370 usec).   At this condition, you will find that the UART will continuously generate RX interrupts and show receiving 0xFF even you make the RX line return to be high. Why issue happen The low time is not in the correct range and out of our spec. In the imx6DL AEC document, there is one chapter named UART Receiver like blow   If using 1200 band, that means one valid bit time is 833 usec. And there is a definition that “tolerate 1/(16 x Fbaud_rate) tolerance in each bit”. That’s means in the case of 1200 baud. A range of valid bit is 781 to 885 usec. But is reproducing, the Low level time is 360 usec. This time out of range will make UART state machine to be confused. How to fix Actually, the best way is following our spec. If there is such an unknown situation in the customer’s environment, then the following method could be regarded as a suggestion to fix the issue meet by the customer. The interrupt handler will check USR1[AWAKE]. 2    If AWAKE is asserted, clear it and proceed as usual (assume we have valid data), else, check if USR1[AGTIM] is asserted. 3    if AGTIM is asserted, clear it and proceed as usual, else perform software reset (assume we have invalid data). Checking AGTIM is for one race condition when the RX fifo has some characters (less than RXTL) but no more data is coming in. When following this procedure, the UART will perform a software reset when a block interrupt occurs. Notes: From customer report, error could be cleared if a valid start-bit is detected on the RX line. This needs to be verified by the customer themselves. Test code has been included in attachment.   Besst Regards
記事全体を表示
In this doc will show how to use i.MX8QXP DPU do image warp.   SW: i.MX Linux BSP L5.4.24_2.1.0 bsp release and patch in this doc HW: i.MX8QXP MEK board, ov5640 camera, HDMI display   Introduction Image Warping is the process of digitally manipulating image data such that the image’s projection precisely matches a specific projection surface or shape.   i.MX8QXP DPU controller could do image warp work by its blit engine and display engine. I choose to enable blit engine’s fetchwarp9 unit to do warp work. Check i.MX8QXP RM, Blit Engine support Image Warp as: “Performs a re-sampling of the source image with any pattern. The sample point positions are read from a compressed coordinate buffer.” So you need prepare two input buffers, one buffer store original image data, the other buffer store resample point coordinate, DPU blit engine will read that two buffer by fetchwarp9 unit, then output result image buffer which contain warped image data. Note i.MX8QXP DPU blit engine fetchwarp9 unit, for the input original image buffer, support RGB and YUV 4:4:4 format. The resample point coordinate buffer contents is depend on what kind warp transformation in your use case; and for each resample point coordinate format check i.MX8QXP RM fecthwarp unit description as below. In this doc, using the 2xs12.4 format, each point x coordinate use (12+4) bit, same as y coordinate.   For DPU fetchwarp9 unit, to enable it work for image warp, check i.MX8QXP RM:   2.Patch notes and test code imx8-dpu-warp-kernel.diff contain the kernel side change for drm ioctl api permission and add vmap function of ion dma_buf_ops. libg2d.so contain the binary for adding warp feature. g2d.h is header file which add define for G2D_WARP and G2D_YUV4. imx8-ov5640-dpu-warp-render.c is a sample code which show how to call g2d lib to image warp, need open the G2D_WARP flag. And this code contain some example calculate the coordinate buffer of rotate, swirl, barrel distortion, affine transformation, perspective transformation, wave transformation. And this code will show read camera input frame then add warp process , then render warp image frame to display.   The test cmd usage as below, read 1080P frame from ov5640 camera, do warp then render warp image to drm plane. Note as dpu fetchwarp9 unit support YUV 4:4:4 input image frame, so below cmd need set parameter YUV4, which will ask ISI driver output YUV 4:4:4 image frame. imx8-ov5640-dpu-warp-render  -i /dev/video0 -f YUV4  -S 1920,1080  -M imx-drm -p 91:38 -F XB24  -b 6  -e g2d  -t 5         -i <video-node> set video node (default: /dev/video0)         -f <fourcc>     set input format using 4cc         -S <width,height>       set input resolution         -s <width,height>@<left,top>    set crop area         -M <drm-module> set DRM module         -o <connector_id>:<crtc_id>:<mode>      set a mode         -p <connector_id>:<crtc_id>     output to a plane         -F <fourcc>     set output format using 4cc         -t <warptype>   set 0 neutual 1 rotate 2 swirl 3 divisionmodel 4 affine 5 perpsptive 6 wave         -b buffer_count set number of buffers        3.Example original image:                     Reference: https://www.nxp.com/webapp/Download?colCode=IMX8DQXPRM https://www.nxp.com/webapp/Download?colCode=L5.4.24_2.1.0_MX8QXPC0&appType=license https://en.wikipedia.org/wiki/Image_geometry_correction https://lists.freedesktop.org/archives/dri-devel/2012-March/019778.html https://store.kde.org/p/1246558 https://github.com/ImageMagick/ImageMagick        
記事全体を表示
1. Increasing the number of threads. Make sure the Parallelism variables located on conf/local.conf BB_NUMBER_THREADS: indicating how many task bitbake should run in parallel PARALLEL_MAKE: indicating how many processes make should run in parallel are not commented and with correct values. The script  setup-enviroment  automatically sets these equal to the number of CPU cores. You can double this value if you want but there is no significant speed's gain. 2. Having a local repository on the server. When baking an image, one of the first steps for each recipe is to fetch the source code (from git repos, tarballs, etc); it makes sense to reuse this data for future builds and also share it with other server's users. You can indicate bitbake to look first at a local repo (file://) on your conf/local.conf file SOURCE_MIRROR_URL ?= "file:///opt/yocto/download/" INHERIT += "own-mirrors" BB_GENERATE_MIRROR_TARBALLS = "1" # BB_NO_NETWORK = "1" Just make sure the download folder has read access for all users (chmod a+r /opt/yocto/download/)
記事全体を表示
The Android O8.0.0_1.3.0 for i.MX 8MQuad(mScale850D) RFP(GA) release is now available on IMX_SW web page. Overview -> BSP Updates and Releases -> Android O8.1.0 for i.MX 8MQuad GA.   Files available:   # Name Description 1 android_O8.1.0_1.3.0_8M_docs.tar.gz Android O8.1.0_1.3.0_8MQ GA Documentation 2 imx-o8.1.0_1.3.0_8m.tar.gz i.MX Android proprietary surce code for Android O8.1.0_1.3.0_8MQ GA 3 android_O8.1.0_1.3.0_8M_image_8mq.tar.gz Prebuilt images with NXP extended features for the i.MX8MQ EVK 4 android_O8.1.0_1.3.0_8M_tools.tar.gz Manufacturing Toolkit and VivanteVTK for Android O8.1.0_1.3.0_8MQ GA 5 fsl_aacp_dec_O8.1.0-8MQ_GA.tar.gz AAC Plus Codec for O8.1.0_1.3.0_8MQ GA   Target boards: i.MX 8MQuad EVK   Features and Known issues For features and known issues, please consult the Release Notes in detail.
記事全体を表示
meta-avs-demos Yocto layer meta-avs-demos is a Yocto meta layer (complementary to the NXP BSP release for i.MX) published on CodeAurora that includes the additional required packages to support  Amazon's Alexa Voice Services SDK (AVS_SDK) applications. The build procedure is the described on the README.md of the corresponding branch. We have 2 fuctional branches now: imx-alexa-sdk: Support for Morty based i.mx releases imx7d-pico-avs-sdk_4.1.15-1.0.0: legacy support for Jethro releases The master branch is only used to collect manifest files, that used with repo init/sync commands will fetch the whole environment for the 2 special supported boards: i.MX7D Pico Pi and i.MX8M EVK. However the meta-avs-demos can be used with any i.MX board either. Recipes to include Amazon's Alexa Voice Services in your applications. The meta-avs-demos provides the required recipes to build an i.MX image with the support for running Alexa SDK. The imx-alexa-sdk branch is based on Morty and kernel 4.9.X and it supports the next builds: i.MX7D Pico Pi i.MX8M EVK Generic i.MX board For the i.MX7D Pico Pi and i.MX8M EVK there is an extended support for additional (external) Sound Cards like: TechNexion VoiceHat: 2Mic Array board with DSPConcepts SW support Synaptics Card: 2 Mic with Sensory WakeWord support The Generic i.MX is for any other regular i.MX board supported on the official NXP BSP releases. Only the default soundcard (embedded) on the board is supported. Sensory wakeword is currently only enabled for those with ARMV7 architecture. To support any external board like the VoiceHat or Synaptics is up to the user to include the additional patches/changes required. Build Instructions Follow the corresponding README file to follow the steps to build an image with Alexa SDK support README-IMX7D-PICOPI.md README-IMX8M-EVK.md README-IMX-GENERIC.md
記事全体を表示
1. Follow all steps from Freescale's github repo except the last bitbake command 2. The images that Freescale supports are located on the meta-fsl-demos/recipes-fsl/images folder. 3. Bake the standard Freescale image build$ bitbake fsl-image-gui 4. The produced Linux image is packaged in several formats; the .sdcard single file has all the system (u-boot + uImage + rootfs) so it can be directly flashed into an SD card build$ sudo dd if=tmp/deploy/images/fsl-image-gui-imx6qsabresd.sdcard of=/dev/sdX bs=4M NOTES: In case of building issues, please follow this link In case of booting issues, make sure: 1. board DIP switches are set correctly 2. you have chosen the correct machine before baking If issues persist, report it to the community
記事全体を表示
1. Set up HDMI Set up your kernel to use HDMI adding the following code to bootargs on u-boot: video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24 2. Test raw audio In order to test only raw audio, use the following command: aplay -D hw:1,0 Kaleidoscope.wav 3. Make HDMI audio the default output In order to configure audio output over HDMI, please, replace content of file ~/.asoundrc to the following one pcm.dmix_48000{      type dmix      ipc_key 5678293      ipc_key_add_uid yes      slave{           pcm "hw:1,0"           period_time 0           period_size 2048           buffer_size 24576           format S16_LE           rate 48000      } } pcm.!dsnoop_44100{      type dsnoop      ipc_key 5778293      ipc_key_add_uid yes      slave{           pcm "hw:0,0"           period_time 0           period_size 2048           buffer_size 24576           format S16_LE           rate 44100      } } pcm.!dsnoop_48000{      type dsnoop      ipc_key 5778293      ipc_key_add_uid yes      slave{           pcm "hw:1,0"           period_time 0           period_size 2048           buffer_size 24576           format S16_LE           rate 48000      } } pcm.asymed{      type asym      playback.pcm "dmix_48000"      capture.pcm "dsnoop_44100" } pcm.dsp0{      type plug      slave.pcm "asymed" } pcm.!default{      type plug      route_policy "average"      slave.pcm "asymed" } ctl.mixer0{      type hw      card 0 } This will configure alsa to use sound card hw:1,0. Please, pay attention to use the proper audio card name for your device. In order to see available sound cards on board: root@imx53qsb:~# aplay -l **** List of PLAYBACK Hardware Devices **** card 0: imx3stack [imx-3stack], device 0: SGTL5000 SGTL5000-0 []   Subdevices: 1/1   Subdevice #0: subdevice #0 card 1: imx3stackspdif [imx-3stack-spdif], device 0: IMX SPDIF mxc spdif-0 []   Subdevices: 1/1   Subdevice #0: subdevice #0 For detail on how to create asound.conf, please see alsa-lib configuration introduction. 4. Encoded audio For encoded (i.e. AC3, DTS) audio, you can use, for example, ac3dec, an utility provided by alsa-tools with the following command line: ac3dec -D hw:1,0 -C test.ac3 This would work for both HDMI audio and SPDIF audio. Double check your hardware and/or schematic in order to know which one to use.
記事全体を表示
Hi all, I shared my test results and solutions in attachments. Best regards, Carl
記事全体を表示
This is a hardware design checklist for i.MX28. Please go through this checklist and check your design before requesting a schematics review. Arthur
記事全体を表示
The purpose of the document is to help customer setup development  environment of android BSP, The document includes the following contents: 1.Setup environment for compiling android BSP source code 2. Setup tftp and NFS environment for android development 3. Common Steps of Porting android  to customized borad ( L3.0.35 kernel) Note: (1) ubuntu version is suitable for 12.04/14.04/15.04 (2) android BSP version is 4.2.2 / 4.3 / 4.4.2  If cusotmer is using android5.1.1 / android 6.0 or above, The way of porting kernel should be focused on adjusting device tree. (3)Each andoid BSP has its own MFG tools version. User should pay attention to this, don't use wrong version of MFG Tools. NXP TIC team Weidong Sun
記事全体を表示
Introduction This is a brief guide showing how to integrate the driver for the WF111 module to the i.MX6 BSP Release. In this case the WF111 driver is available on a repository and it’s in accordance with the Yocto Project, which allows to easily customize a linux distribution for your board. Requirements WF111 Documentation – Silicon Labs have made a great job of documenting the steps to add the WF111 driver to a Linux distribution and have created Application Note 996 (link below), which we will use as reference. http://www.silabs.com/documents/login/application-notes/AN996.pdf WF111 Driver - We will also be using the Yocto layer included on the following repository: https://github.com/engicam-stable/meta-engicam i.MX6 3.14.52 BSP Release – In out scenario the WF111 layer that will be imported includes a driver that it’s compatible with Linux Kernel 2.6.24 up to 4.1., which it’s important to keep in mind.   Installing the 3.14.52 BSP Release First, setup the 3.14.52 BSP as described on the i.MX Yocto Project User’s Guide.   Adding the WF111 Driver Layer Clone the WF111 Driver Layer to your sources folder inside the BSP Release directory. Since the 3.14.52 BSP Release is based on Fido we will clone the Fido branch of the driver repository. $ cd <BSP_RELEASE_DIR>/sources $ git clone https://github.com/engicam-stable/meta-engicam -b fido‍‍  Once the layer is cloned you would need to add the new later editing the bblayers.conf file located the following path: <BSP_RELEASE_DIR>/<BUILD_DIR>/conf/bblayers.conf By adding the following line to add the new layer.   BBLAYERS += " ${BSPDIR}/sources/meta-engicam "‍   This should make the wf111-driver available through bitbake since bitbake will now look into this layer for all available recipes. You can then add the driver to your image by adding the following line to the <BUILD_DIR>/conf/local.conf   IMAGE_INSTALL_append += "wf111-driver"‍ Or you may create a new image recipe that includes the wf111-driver package. However, there are certain kernel options that must be enabled for the driver to work.   Creating an append to configure the kernel options Before we can bake an image with the WF111 driver we would need to edit the kernel options as mentioned on Silabs AN996. The following kernel options must be enabled:   CONFIG_WIRELESS_EXT CONFIG_MODULES CONFIG_FW_LOADER We would need to add the CONFIG_WIRELESS_EXT as the other two options are enabled on the BSP by default.   This involves adding an addendum to the kernel recipe to change its configuration. You may either add this append to any layer. The best way to handle it would be using a new layer for all your customization. You can find how to create a new layer on the following document: https://community.nxp.com/docs/DOC-331917 We’ll use a new layer called meta-newlayer for this example. It’s important that this layer has a high priority so the changes from the bbappend are not overridden. The following alternative was suggested by Chris Hossack on the following thread: https://community.nxp.com/thread/376369 First, run the menuconfig tool on the bitbake environment: bitbake linux-imx -c menuconfig Enable the necessary options: Networking Support > Wireless > cfg80211 wireless extensions compatibility   Save the configuration and exit. Then run the following bitbake command, which will create a config fragment file that contains the changed made to the default kernel options. bitbake linux-imx -c diffconfig We’ll make an append file that adds the required options.  Content of the config fragment:   CONFIG_WIRELESS_EXT=y CONFIG_WEXT_CORE=y CONFIG_WEXT_PROC=y CONFIG_WEXT_SPY=y CONFIG_WEXT_PRIV=y CONFIG_CFG80211_WEXT=y CONFIG_LIB80211=y CONFIG_LIB80211_CRYPT_WEP=y CONFIG_LIB80211_CRYPT_CCMP=y CONFIG_LIB80211_CRYPT_TKIP=y # CONFIG_LIB80211_DEBUG is not set CONFIG_HOSTAP=y # CONFIG_HOSTAP_FIRMWARE is not set‍‍‍‍‍‍‍‍‍‍‍‍‍    Since we are appending the kernel layer we need to add the addendum on the same path as that of the original kernel recipe but within our layer and create the append file there. Also add the WF111.cfg file to the linux-imx directory:   We would need to copy (and you may rename it as well) to the folder where are will be creating the append recipe for the kernel. Copy:  <BSP_RELEASE>/<BUILD_DIR>/tmp/work/<MACHINE>-poky-Linux-gnueabi/linux-imx/<KERNEL_VERSION>/fragment.cfg To: <BSP_RELEASE>/sources/meta-newlayer/recipes-kernel/linux/linux-imx/WF111.cfg You can do so suing the following command: cp <BSP_RELEASE>/<BUILD_DIR>/tmp/work/<MACHINE>-poky-Linux-gnueabi/linux-imx/<KERNEL_VERSION>/fragment.cfg <BSP_RELEASE>/sources/meta-newlayer/recipes-kernel/linux/linux-imx/WF111.cfg‍ (Please note that the file was renamed for ease, but you may use any name for the config fragment)   We need to create the bbappend file on the following path (as it must be the same relative path as the original recipe it is appending) <BSP_RELEASE>/sources/meta-newlayer/recipes-kernel/linux/linux-imx_3.14.52.bbappend   The linux-imx_3.14.52.bbappend file would contain the following:   SRC_URI += "file://WF111.cfg"  do_configure_append() {          #this is run from         #./tmp/work/<MACHINE>-poky-linux-gnueabi/linux-imx/3.14.52-r0/git          cat ../*.cfg >> ${B}/.config  }‍‍‍‍‍‍    After creating this recipe you should be able to bake any image from the BSP and see the driver there. I tested with the core-minimal-image and found that the files were indeed added to /lib/firmware. $ bitbake core-image-minimal ‍‍‍
記事全体を表示
This document explains the pad implementation and its relationship with the System Controller Firmware pad configuration service. There are two components to pad configuration in the SCFW, there are the modules that generate the signals that will ultimately appear on the physical pad, let's say GPIO/Ethernet/I2C/UART etc... and then there is the part that configures the muxing of the pad (what signal is going to be outputted through the specific pad), the drive strength of the pad, pull selection, etc, this is the part that the SCFW pad service configures. Introduction‌ The i.MX8 has three types of I/Os: 1.8V only I/Os 3.3V only I/Os 1.8V / 3.3V I/Os Dual Voltage I/Os Note: USB High Speed Inter-Chip (HSIC) and Ethernet interfaces have specific integration schemes with dedicated features. They are a modified versions of the above I/O types. HSIC are a special kind of I/O modified to sustain 480Mbps data rates ENET I/Os are modified versions of Dual Voltage I/Os to support 2.5V operations All of these I/Os have "common features" and "technology specific features" which depend on the type of I/O and the chip manufacturing process (FDSOI in the i.MX8QM case) I/O common features Muxing capability of up to 4 signals Each Pad can have up to 4 signals, only one signal can be present in the pad. To select the signal that will output on the pad simply look at the Pinmux spreadsheet and use the desired alternative, for instance in the following image SCU_GPIO0_00 has 3 options, SCU_GPIO (ALT0 - GPIO controlled directly by the SCU), SCU_UART0_RX (ALT1 - SCU UART receiver) or LSIO_GPIO0_IO28 (ALT3 - Low speed I/O GPIO).   Pads without GPIO functionality (i.e. without the GPIO option in the pinmux spreadsheet) are implemented for one purpose only, these pins are connected directly to the module that drives them and they feature their own physical interface. Examples are XTAL pins, DDR pins and SCU PMIC interface (shown above). Mode of operation All GPIO types support four modes of operation: Normal mode Data is being driven directly to the pad (an internal signal of 1 shows in the pad as a 1 and vice-versa) and the pad works either as an output or as an input but not both at the same time. The output buffer while on this mode looks like this: Open drain Data is being driven through an open drain configuration, the output on the pad switches between 0 and high-z. The pad works either as an output or as an input but not both at the same time, e.g. if the Output Buffer is enabled the Input Buffer is disabled. This is how the output buffer looks like on Open drain mode: Open drain and input Output buffer acts as in open drain mode but with the input buffer enabled regardless of the output buffer state (enabled/disabled), this allows to simultaneously read the signal at the pad while driving it. Output and input Output buffer acts as in normal mode but with the input buffer enabled regardless of the output buffer state (enabled/disabled), this allows to read the signal at the pad while driving it. Wake-up capability Each I/O can be configured to wake-up the device, the following configuration options are available: OFF I/O cannot wake-up the system Low detect Generate wake-up event when the pad remains in low-level High detect Generate wake-up event when the pad remains in high-level Rising edge Generate wake-up event on rising edge detection Falling edge Generate wake-up event on falling edge detection Technology specific features Some of the available features for each pad depend on two factors: Chip manufacturing process (FDSOI or LPP) I/O type (1.8V, 3.3V or Dual Voltage) The i.MX8QM is manufactured using FDSOI technology and it features all of the three available I/O types. Drive strength Drive strength options vary within I/O types and chip manufacturing options. The available options for a FDSOI chip are: 1.8V Drive strength options 3.3V Drive strength options Dual Voltage drive strength options Drive strength of 1mA Drive strength of 2mA Low drive strength (50 ohms) Drive strength of 2mA Drive strength of 4mA High drive strength (33 ohms) Drive strength of 4mA Drive strength of 8mA Drive strength of 6mA Drive strength of 12mA Drive strength of 8mA Drive strength of 10mA Drive strength of 12mA High-speed drive strength Pull Select The pull select available options are almost the same for all I/O types (1.8V being the exception) and they also depend on chip manufacturing process. The available options for a FDSOI chip are: Pull select options for FDSOI Bus-keeper (only available for 1.8V) Pull-up Pull-down No Pull (Disabled) A bus-keeper or bus-holder is used to keep the last state on the bus. In normal operation it makes no difference, but once the bus is tri-stated it keeps the last logic level in the bus to prevent the bus from floating. Compensation The compensation feature is only available on Dual Voltage I/Os. Dual Voltage I/Os have a different implementation, they require: Voltage reference generator - which provides a voltage reference to the supply detector and compensation cell Supply detector - detects automatically whether the I/O is being supplied with 1.8V or 3.3V and broadcasts this information to compensation cell and I/O  Compensation cell - adjusts drive strength of dual voltage I/Os depending on Process Voltage and Temperature (PVT) conditions. The default configuration takes care of adjusting this parameters and no further modifications are required. Pad configuration service SCFW API Mux selection The very first function that needs to be called to configure a pad is: sc_err_t sc_pad_set_mux(sc_ipc_t ipc, sc_pad_t pad, uint8_t mux, sc_pad_config_t config, sc_pad_iso_t iso);‍‍‍‍‍‍‍‍‍‍‍‍‍‍ This function takes care of configuring the muxing alternative and setting the common features, its parameters are: ipc - The Inter Processor Communication (IPC) channel that you will use to communicate with the SCU. You need to call sc_ipc_open to obtain it. pad - The pad you want to configure, the different pad definitions are in imx8qm_pads.h, this is basically the same list that is included in the scfw_api_qm.pdf document (page 27 Chapter 5 Pad List) and it also mimics the Pinmux excel sheet. mux - The mux setting that you require, basically Alt0 -> 0, Alt1 -> 1, Alt2 -> 2 and Alt3-> 3, the pinmux spreadsheet contains the required information (take a look at I/O common features above). config - Used to select the desired mode of operation (take a look at I/O common features above), the available options are declared under sc_pad_config_t Normal mode - SC_PAD_CONFIG_NORMAL Open Drain mode - SC_PAD_CONFIG_OD Open Drain and input - SC_PAD_CONFIG_OD_IN Output and input - SC_PAD_CONFIG_OUT_IN iso - This is the low-power isolation configuration (take a look at I/O common features above). The available options are declared under sc_pad_iso_t ISO_OFF - SC_PAD_ISO_OFF ISO_EARLY - SC_PAD_ISO_EARLY ISO_LATE - SC_PAD_ISO_LATE ISO_ON - SC_PAD_ISO_ON For instance to configure M40_I2C0_SCL with its UART alternative in normal mode with low-power isolation off, the call would look like this: sc_pad_set_mux(ipc, SC_P_M40_I2C0_SCL, 1, SC_PAD_CONFIG_NORMAL, SC_PAD_ISO_OFF);‍‍‍‍‍‍‍‍‍‍ Pad configuration To configure drive strength and pull select options the technology specific functions need to be used (FDSOI for i.MX8QM): sc_pad_set_gp is being used by our Linux team because it admits the passing of the configuration parameters as a single value and this eases the handling on the device tree, but you should aim to use the technology specific functions. sc_err_t sc_pad_set_gp_28fdsoi(sc_ipc_t ipc, sc_pad_t pad, sc_pad_28fdsoi_dse_t dse, sc_pad_28fdsoi_ps_t ps);‍‍‍‍‍‍‍‍‍‍‍ This function takes care of configuring the drive strength (DSE) and pull select settings (PS) for the specified pad, here is a break down of the parameters it uses: ipc - The Inter Processor Communication (IPC) channel that you will use to communicate with the SCU. You need to call sc_ipc_open to obtain it. pad - The pad you want to configure, the different pad definitions are in imx8qm_pads.h, this is basically the same list that is included in the scfw_api_qm.pdf document (page 27 Chapter 5 Pad List) and it also mimics the Pinmux excel sheet. dse - The desired drive strength configuration (see Technology specific features above). DSE settings depend on the I/O type being used, the available options for each I/O type are defined under sc_pad_28fdsoi_dse_t: ENET pads capable of operating at 2.5V are a subset of dual voltage I/Os, the dse options available for these pads are the same as normal dual voltage I/Os. i.e. High drive and low drive. ps - The desired pull select configuration (see Technology specific features above). The available options are defined under sc_pad_28fdsoi_ps_t: To determine whether a GPIO pad is 1.8V, 3.3V or Dual Voltage one can look at the pinmux spread sheet, the supply for the pad will indicate what implementation of the GPIO is used. For instance: pads under VDD_SIM_1P8_3P3 are Dual voltage I/Os pads under VDD_SCU_1P8 are 1.8V I/Os pads under VDD_ADC_3P3 are 3.3V I/Os taking the same example as above we could configure the M40_I2C0_SCL as follows: sc_pad_set_gp_28fdsoi(ipc, SC_P_M40_I2C0_SCL, SC_PAD_28FDSOI_DSE_DV_LOW, SC_PAD_28FDSOI_PS_NONE);‍‍‍‍‍‍‍‍‍‍‍‍‍ Configuration under Linux Linux configures pads through the device tree, the full documentation of the binding is under Documentation/devicetree/bindings/pinctrl/fsl,imx8qxp-pinctrl.txt. but here is an extract: * Freescale i.MX8QXP IOMUX Controller Required properties: - compatible: "fsl,imx8qxp-iomuxc" - fsl,pins: each entry consists of 2 integers. Its format is <pin_id pin_config>. pin_config definition: - i.MX8QXP have different pad types, please refer to below pad register definitions, the pinctrl driver will just write the pin_config into the hardware register.‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ The driver uses the following API: sc_err_t sc_pad_set_gp (sc_ipc_t ipc, sc_pad_t pad, uint32_t ctrl) ‍‍‍ Instead of configuring each parameter individually as done with sc_pad_set_gp_28fdsoi it configures the pad as if writing to a register, the bitfield format is under the binding documentation but it is as follows: struct _hw_pad_iomux_bitfields0 { uint32_t GP : 19; /*!< [18:0] GP controls. */ uint32_t WAKEUP : 3; /*!< [21:19] Wakeup controls. */ uint32_t WAKEUP_ENB : 1; /*!< [22] Wakeup write enable. */ uint32_t LPCONFIG : 2; /*!< [24:23] Low-power config. */ uint32_t CONFIG : 2; /*!< [26:25] Config. */ uint32_t IFMUX : 3; /*!< [29:27] Mux. */ uint32_t GP_ENB : 1; /*!< [30] GP write enable. */ uint32_t IFMUX_ENB : 1; /*!< [31] Mux write enable. */ } B; ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ All the configurations mentioned above can be configured, but they are done in a single pass, e.g. Muxing, Configuration (Norma, Open Drive, etc...), Wakeup control, and GP controls are for Pull Select Drive Strenght etc... Check the Reference Manual Chapter for IOMUXD for the register definition for each pad. References For more details refer to the sc_fw_api.pdf document: Chapter 1.3.3 Pad Configuration Service Chapter 6 Pad List Chapter 9.3 (SVC) Pad Service System Controller Firmware 101 
記事全体を表示
Tips collected from zhaoyang-b49593 and dandouglass-b41520 while enabling redundant boot: Using i.MX 8MQ, same method can be applied for other i.MX devices that support redundant boot, see SoC Reference Manual. As described on the RM, if primary image authentication fails the ROM can reset and try booting a secondary image. This feature is only available on closed mode with properly signed binaries, otherwise the ROM boots the primary image despite the auth failure. For the i.MX 8MQ, the secondary image must start with spl, not HDMI firmware. Note, there is no ROM redundancy for the hdmi fw, if it is corrupt user can store a 2nd copy on a different memory address and update at run time. Steps to generate a dual spl image: 1. Build and Sign bootable binary (spl, u-boot, atf, fw, etc) Use the Yocto BSP or follow this post to build outside the Yocto environment. To sign the binary, follow the documentation on u-boot source: <u-boot>/doc/imx/habv4/guides/mx8m_secure_boot.txt Program image to the SD card: dd if=signed_flash.bin of=<sd path> bs=1024 seek=33 After boot you can use "hab_status" to verify that no events were generated: u-boot=> hab_status Secure boot disabled HAB Configuration: 0xf0, HAB State: 0x66 2. Corrupt spl on your boot image You can corrupt anywhere on the spl signed area. For easier visualization at boot time we can corrupt the SPL banner. First create a copy: cp signed_flash.bin signed_flash_corrupt.bin Find the banner: hexdump -C signed_flash.bin | grep 2019 00020190 26 1c 40 92 04 00 80 d2 05 01 80 52 c4 20 04 aa |&[email protected]. ..| 0002eac0 32 30 31 39 2e 30 34 2d 30 30 30 32 39 2d 67 34 |2019.04-00029-g4| 000dde10 3a 20 20 00 55 2d 42 6f 6f 74 20 32 30 31 39 2e |: .U-Boot 2019.| 0002eac3 is on spl area, where "9" for 2019 is, replace by "X" printf "X" > X dd if=X of=signed_flash_corrupt.bin seek=$((0x2eac3)) bs=1 conv=notrunc Verify corrupt binary hexdump -C -s 0x2eac0 -n 64 signed_flash_corrupt.bin 0002eac0 32 30 31 58 2e 30 34 2d 30 30 30 32 39 2d 67 34 |201X.04-00029-g4| 0002ead0 37 63 31 39 32 32 20 28 41 70 72 20 32 37 20 32 |7c1922 (Apr 27 2| Transfer image to SD Card dd if=signed_flash_corrupt.bin of=<sd path> bs=1024 seek=33 Now, you should see hab events after running "hab_status" on u-boot 3. Create a secondary boot image This can be the same content as your primary image without the HDMI fw or it can be a different spl image. For easier visualization, we can change the SPL banner, on the code this time. Modify banner at ./common/spl/spl.c as: - puts("\nU-Boot " SPL_TPL_NAME " " PLAIN_VERSION " (" U_BOOT_DATE " - " + puts("\nSecondary U-Boot " SPL_TPL_NAME " " PLAIN_VERSION " (" U_BOOT_DATE " - " As mentioned above, we want our boot image without the HDMI fw, when running imx-mkimage use the flash_evk_no_hdmi target: make SOC=iMX8MQ flash_evk_no_hdmi Sign the image as in step 1. If you program the new image to the SD you should see the new banner. Make sure to run hab_status to confirm that no HAB events are generated. 4. Program SRK Hash and Close SoC Follow the documentation on u-boot source for SRK programming and closing the device: <u-boot>/doc/imx/habv4/guides/mx8m_secure_boot.txt Before closing the SoC, but after the SRK is programmed, try your images to confirm no HAB events are generated. Be careful with this step, errors could brick your board. This step is irreversible. After closing the SoC it will only boot signed images. 5. Create dual bootloader image We can concatenate our binaries to create a single file, let's use 2MB distance between primary and secondary images: For the working primary image: objcopy -I binary -O binary --pad-to 0x200000 --gap-fill=0x00 signed_flash.bin 1st-spl_pad.bin cat 1st-spl_pad.bin secondary2_nohdmifw_signed_flash.bin > 1st-spl_pad_2nd-spl.bin Or for the corrupt primary image experiment: objcopy -I binary -O binary --pad-to 0x200000 --gap-fill=0x00 signed_flash_corrupt.bin 1st-spl_pad.bin cat 1st-spl_pad.bin secondary2_nohdmifw_signed_flash.bin > 1st-spl_pad_2nd-spl.bin Program it to the SD card on 0x8400 offset (33k) dd if=1st-spl_pad_2nd-spl.bin of=<sd path> bs=1024 seek=33 && sync 6. Add Secondary image table Follow the format on the RM, this is only 20 bytes long. For a 2MB distance between the table and the secondary image we can use "0x1000" on the firstSectorNumber field. 2MB/512 = 4096 (0x1000) The perl script attached, genSecTable.pl, can be used to generate it. perl genSecTable.pl 0x1000 Program it to the SD card on 0x8200 offset dd if=secTable.bin of=<sd path> bs=1 seek=$((0x8200)) && sync 7. Verify secondary image is booting If using the corrupt primary image, you should see the spl with the "Secondary U-Boot SPL..." banner. You can also read the persist secondary boot bit. u-boot=> md.l 0x30390098 1 30390098: 40000000 ...@ The work can be extended patching spl for in case of u-boot authentication failure, spl can try to authenticate and jump to the secondary u-boot.
記事全体を表示
Overview The purpose of this document is to demonstrate how to enable USB Bluetooth Dongle based on i.MX6 Android ICS. Hardware i.MX6Dual/Quad or i.MX6DualLite SabreSD board USB Bluetooth Dongle Software i.MX6DQ/MX6DL Android ICS R13.4 or R13.4.1 Release Changes 0001-enable-usb-dongle-BT.patch: Update bluedroid to disable RFKILL and enable HCIATTACH property for USB Bluetooth Dongle. diff --git a/bluedroid/Android.mk b/bluedroid/Android.mk index 17df49b..569be44 100644 --- a/bluedroid/Android.mk +++ b/bluedroid/Android.mk @@ -5,6 +5,13 @@ LOCAL_PATH:= $(call my-dir) include $(CLEAR_VARS) +ifeq ($(BOARD_BLUETOOTH_DOES_NOT_USE_RFKILL),true) +  LOCAL_CFLAGS := $(LOCAL_CFLAGS) -DBLUETOOTH_DOES_NOT_USE_RFKILL +endif + +ifeq ($(BOARD_BLUETOOTH_USES_HCIATTACH_PROPERTY),true) +  LOCAL_CFLAGS := $(LOCAL_CFLAGS) -DBLUETOOTH_HCIATTACH_USING_PROPERTY +endif LOCAL_SRC_FILES := \   bluetooth.c diff --git a/bluedroid/bluetooth.c b/bluedroid/bluetooth.c index 4cc9204..2636942 100644 --- a/bluedroid/bluetooth.c +++ b/bluedroid/bluetooth.c @@ -44,7 +44,7 @@ static int rfkill_id = -1; static char *rfkill_state_path = NULL; - +#ifndef BLUETOOTH_DOES_NOT_USE_RFKILL static int init_rfkill() {      char path[64];      char buf[16]; @@ -135,6 +135,7 @@ out:      if (fd >= 0) close(fd);      return ret; } +#endif static inline int create_hci_sock() {      int sk = socket(AF_BLUETOOTH, SOCK_RAW, BTPROTO_HCI); @@ -151,13 +152,20 @@ int bt_enable() {      int ret = -1;      int hci_sock = -1;      int attempt; - +#ifndef BLUETOOTH_DOES_NOT_USE_RFKILL      if (set_bluetooth_power(1) < 0) goto out; - +#endif +#ifndef BLUETOOTH_HCIATTACH_USING_PROPERTY      LOGI("Starting hciattach daemon"); -    if (property_set("ctl.start", "hciattach") < 0) { +    if (property_set("ctl.start", "hciattach") < 0) +#else +    if (property_set("bluetooth.hciattach", "true") < 0) +#endif +    {          LOGE("Failed to start hciattach"); +#ifndef BLUETOOTH_DOES_NOT_USE_RFKILL          set_bluetooth_power(0); +#endif          goto out;      } @@ -186,14 +194,18 @@ int bt_enable() {          if (property_set("ctl.stop", "hciattach") < 0) {              LOGE("Error stopping hciattach");          } +#ifndef BLUETOOTH_DOES_NOT_USE_RFKILL          set_bluetooth_power(0); +#endif          goto out;      }      LOGI("Starting bluetoothd deamon");      if (property_set("ctl.start", "bluetoothd") < 0) {          LOGE("Failed to start bluetoothd"); +#ifndef BLUETOOTH_DOES_NOT_USE_RFKILL          set_bluetooth_power(0); +#endif          goto out;      } @@ -222,14 +234,20 @@ int bt_disable() {      ioctl(hci_sock, HCIDEVDOWN, HCI_DEV_ID);      LOGI("Stopping hciattach deamon"); -    if (property_set("ctl.stop", "hciattach") < 0) { +#ifndef BLUETOOTH_HCIATTACH_USING_PROPERTY +    if (property_set("ctl.stop", "hciattach") < 0) +#else +   if (property_set("bluetooth.hciattach", "false") < 0) +#endif +   {          LOGE("Error stopping hciattach");          goto out;      } - +#ifndef BLUETOOTH_DOES_NOT_USE_RFKILL      if (set_bluetooth_power(0) < 0) {          goto out;      } +#endif      ret = 0; out: @@ -246,9 +264,10 @@ int bt_is_enabled() {      // Check power first +#ifndef BLUETOOTH_DOES_NOT_USE_RFKILL      ret = check_bluetooth_power();      if (ret == -1 || ret == 0) goto out; - +#endif      ret = -1;      // Power is on, now check if the HCI interface is up 0002-usb_dongle-on-SabreSD.patch: Update MX6 board configuration files to enable USB Bluetooth dongle feature. diff --git a/imx6/imx6.mk b/imx6/imx6.mk @@ -63,6 +63,7 @@ PRODUCT_PACKAGES += \ PRODUCT_PACKAGES += \   audio.tinyalsa.freescale   \   audio.legacy.freescale    \ +        audio.a2dp.default                      \   alsa_aplay                \   alsa_arecord    \   alsa_amixer        \ diff --git a/imx6/sabresd/SabreSDBoardConfigComm.mk b/imx6/sabresd/SabreSDBoardConfigComm.mk index 03d8ce5..1a8a6bd 100755 --- a/imx6/sabresd/SabreSDBoardConfigComm.mk +++ b/imx6/sabresd/SabreSDBoardConfigComm.mk -# atheros 3k BT -BOARD_USE_AR3K_BLUETOOTH := true +# Default use USB BT dongle for imx6, so should enable below +BOARD_BLUETOOTH_DOES_NOT_USE_RFKILL := true +BOARD_BLUETOOTH_USES_HCIATTACH_PROPERTY := true + USE_ION_ALLOCATOR := false USE_GPU_ALLOCATOR := true diff --git a/imx6/sabresd/init.rc b/imx6/sabresd/init.rc index ff9f0ff..f127177 100755 --- a/imx6/sabresd/init.rc +++ b/imx6/sabresd/init.rc @@ -84,9 +84,12 @@ on boot      # No bluetooth hardware present      setprop hw.bluetooth 0      setprop wlan.interface wlan0 +    setprop hw.bluetooth 1 diff --git a/imx6/sabresd/required_hardware.xml b/imx6/sabresd/required_hardware.xml index c9a2271..f7db37b 100644 --- a/imx6/sabresd/required_hardware.xml +++ b/imx6/sabresd/required_hardware.xml @@ -22,6 +22,7 @@      <feature name="android.hardware.camera.flash" />      <feature name="android.hardware.camera.front" />      <feature name="android.hardware.location" /> +    <feature name="android.hardware.bluetooth" />      <feature name="android.hardware.location.network" />      <feature name="android.hardware.location.gps" />      <feature name="android.hardware.telephony" />
記事全体を表示
The resource management service offers the possibility to divide the system into groups of resources or partitions. Resources within a partition can not access resources outside of it's partition. Partitioning a system is useful to isolate resources from one another, this gives you the ability to have for instance FreeRTOS and Linux each running simultaneously with its own set of resources. In the FreeRTOS/Linux example you could partition/divide the system into two groups/partitions where all resources/peripherals needed by FreeRTOS would be completely isolated from the resources needed by Linux, if any of the resources on the Linux partition tried to access a resource on the FreeRTOS partition the transaction would result in a bus error, as if the resource tried to access a region outside of its memory map. The partitioning mechanism is enforced by hardware and the configuration of the underlying hardware is completely abstracted by the SCFW API. The system partitioning can be performed in two ways: At boot time by modifying the function board_system_config on the board.c portion of the SCFW porting kit that corresponds to your board. This is used for software that is loaded as part of the boot process. At run time by calling the resource management service functions available. This is used to partition software that is launched by an operating system, e.g. an M4 used as sensor fusion and loaded/started by Linux. A partition can have: Resources (peripherals) Pads Memory regions All of the items mentioned above can be grouped within a partition. It is important to note that: At boot time all resources are grouped into a single partition. Resources can only be assigned to another partition by a resource within it's own partition.  Initial partitioning state of the system At boot time the system is initially configured in three partitions: The first partition (SCFW) contains all the resources, pads and memory required by the System Controller Unit (SCU) to execute the System Controller Firmware. The second partition (SECO) contains all the resources required by the Security Controller to execute. The third partition (Boot) contains all of the remaining resources, pads and memory available for the whole system. Once Linux and the M4 boot a typical use case is to partition the system as follows: In this case the boot partition is split into the ATF/Linux partition and the M4 partition. The ARM Trusted Firmware environment add a layer of abstraction to secure the environment and it is assigned cores and memory to execute in this privileged state, all the remaining resources, pads and memory are assigned to the Linux partition. The M4 partition contains all the resources required by the M4 to execute, as well as the resources required by the application running on the M4. Resource partitioning - Boot time configuration The SCFW porting kit provides an example on doing boot time configuration at the board.c file under platform/board/mx8q<x or m>_<your board>/board.c, board_system_config is the function in charge of partitioning the system at boot time. From the sc_fw_port.pdf (porting guide) document included in the porting kit - Boot Flags chapter: Here are a few important points to highlight: The code will only execute if the SC_BD_FLAGS_ALT_CONFIG is set under the boot flags (more details in the Usage chapter of the sc_fw_port.pdf), the flags are set while building the image with mkimage. An example is provided to build an image with partitioning enabled: flash_linux_m4: $(MKIMG) mx8qx-ahab-container.img scfw_tcm.bin u-boot-atf.bin m4_image.bin ./$(MKIMG) -soc QX -rev B0 -append mx8qx-ahab-container.img -c -flags 0x00200000 -scfw scfw_tcm.bin -ap u-boot-atf.bin a35 0x80000000 -p3 -m4 m4_image.bin 0 0x34FE0000 -out flash.bin‍‍‍‍‍‍‍‍‍‍‍‍‍‍ The example above can be found under your i.MX8 variant on the soc.mak file, in the example above the SC_BD_FLAGS_ALT_CONFIG flag is being set by -flags 0x00200000 and the partition for the M4 is defined as the third one by the -p3 parameter. Without the -flags 0x00200000 (setting SC_BD_FLAGS_ALT_CONFIG) parameter on mkimage NO partition happens at boot time, if the target used to build the image does not set this flag, then the SCU does not partition the system. On the board.c file the code in charge of checking for this flag is the following: /* Configure initial resource allocation (note additional allocation and assignments can be made by the SCFW clients at run-time */ if (alt_config != SC_FALSE) {‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ if the alt_config flag is not set, then the partitioning is skipped. The function rm_dump(pt_boot); dumps the partitioning state of the whole system, it can be called before and after the partitioning to make sure the device was partitioned as expected. Here is how a partition dump looks like: *** Partitions ********************************** Partition: 0 Parent: 0 DID: 2 Flags: Used Secure Isolated Partition: 1 Parent: 0 DID: 0 Flags: Used Isolated Partition: 2 Parent: 0 DID: 1 Flags: Used Secure Restricted Isolated *** Resources *********************************** Partition: 0 SC_PID0 SC_SEMA42 SC_TPM SC_PIT SC_UART ... Continues .... DBLOGIC DRC_0 DRC_1 Partition: 1 SC_PID1 SC_PID2 SC_PID3 SC_PID4 ... Continues .... BOARD_R5 BOARD_R6 BOARD_R7 Partition: 2 SECO CAAM_JR1 CAAM_JR1_OUT *** Memory Regions ****************************** Partition: 0 000: 0x030FE0000 - 0x03101FFFF Partition: 1 001: 0x000000000 - 0x01BFFFFFF 002: 0x034000000 - 0x037FFFFFF 003: 0x038000000 - 0x03BFFFFFF 004: 0x060000000 - 0x06FFFFFFF 005: 0x070000000 - 0x07FFFFFFF 006: 0x080000000 - 0x0FFFFFFFF 007: 0x400000000 - 0x43FFFFFFF 008: 0x880000000 - 0xFFFFFFFFF Partition: 2 *** Pads **************************************** Partition: 0 M40_I2C0_SCL M40_I2C0_SDA ... Continues .... SCU_BOOT_MODE4 SCU_BOOT_MODE5 Partition: 1 SIM0_CLK SIM0_RST SIM0_IO ... Continues .... ENET1_RGMII_RXD2 ENET1_RGMII_RXD3 COMP_CTL_GPIO_1V8_3V3_ENET_ENETA Partition: 2‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ The dump contains the configuration of the partition, for instance: *** Partitions ********************************** Partition: 0 Parent: 0 DID: 2 Flags: Used Secure Isolated‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ On the example above the Partition parent is partition 0 (itself, this is the System Controller partition, all partitions spawn from this one). The Domain ID (DID) is 2, this ID is used to identify the partition by the hardware, it is used to enforce hardware isolation. It is also a secure and isolated partition, the meaning of these flags can be found below and in the sc_fw document: Secure - boolean indicating if this partition should be secure; only valid if caller is secure Isolated - boolean indicating if this partition should be HW isolated; set SC_TRUE if new DID is desired Restricted - boolean indicating if this partition should be restricted; set SC_TRUE if masters in this partition cannot create new partitions Grant - boolean indicating if this partition should always grant access and control to the parent Coherent - boolean indicating if this partition is coherent; set SC_TRUE if only this partition will contain both AP clusters and they will be coherent via the CCI The rest of the sections of the dump highlight all the resources, pads and memory regions enclosed in each partition. For more details on the definition of all the API calls please refer to the respective sc_fw_api document for each SoC variant. Resource partitioning - Run time configuration  The run time partitioning doesn't differ from the example provided on the porting kit, that example can be used as a base to create a partition at run time by calling the SCFW API.  Examples The following examples will show how to modify the default partition configuration on the evaluation boards, i.MX8QM MEK will be used as a reference. With BSP 4.14.98_2.3.0, the porting kit can be obtained from i.MX Software and Development Tools | NXP . Default configuration without partitioning First we will dump the default configuration without partition, e.g. without setting the ALT_CONFIG flag, most mkimage targets with a single image are configured this way, see the soc.mak and related files under scripts: soc.mak\iMX8QM - imx-mkimage - i.MX Mkimage Bootloader Tool  For details on how to create a bootable image see i.MX8 Boot process and creating a bootable image  We can see that the targets flash and flash_spl do not set any flags on the image, therefore no partition of the system will occur at boot time. flash: $(MKIMG) $(AHAB_IMG) scfw_tcm.bin u-boot-atf.bin ./$(MKIMG) -soc QM -rev B0 -append $(AHAB_IMG) -c -scfw scfw_tcm.bin -ap u-boot-atf.bin a53 0x80000000 -out flash.bin‍‍‍‍‍‍ We will build the SCFW with the Debug Monitor enabled in order to be able to dump the partitions: make qm R=B0 B=mek M=1‍‍‍‍ Now we copy the SCFW binary we just build (scfw_tcm.bin under build_mx8qm_b0) to the mkimage iMX8QM folder, along with the SECO FW, ATF (bl31.bin) and u-boot. On mkimage the flash target will be used to create a bootable image with the SCFW we just build: make SOC=iMX8QM flash‍‍‍‍‍ Flash the image to your sd card sudo dd if=iMX8QM/flash.bin of=/dev/mmcblkXX bs=1k seek=32 sync‍‍‍‍‍‍‍‍ The MEK has two serial ports, the first one (usually ttyUSB0) is used by the A cores (u-boot/Linux in this case), the second one is used by one of the M4 cores OR the SCFW, in this case it will be used by the SCFW.  Unfortunately there aren't enough serial ports on the MEK board to allow a dedicated port for SCU, M4 cores and A cores, so in order to use the Debug Monitor on the MEK the SCFW has to take over the M4_0 UART terminal. On the SCFW Debug monitor terminal type "dump rm" this will dump all the partition information, the full log is attached to this document (imx8qm_mek_no_partition.txt). On this log it can be seen that 4 partitions are created: Partition 0 --> SCFW Partition 1 --> ATF Partition 2 --> SECO Partition 3 --> U-boot/Linux/M4 cores/Rest of the system The ATF partition is created at run time by the ATF to run in its secure state, no extra partition is created at boot time, if an image without ATF where to be used only three partitions would be seen: Partition 0 --> SCFW Partition 1 --> U-boot/Linux/M4 cores/Rest of the system Partition 2 --> SECO Default configuration with partitioning enabled Now we will create an image with the SC_BD_FLAGS_ALT_CONFIG flag set, so that partitioning occurs at boot time, for demonstration purpose we will use the same target previously used but we will modify it to set the ALT_CONFIG flag, so on mkimage modify the flash target as follows: On iMX8QM/soc.mak flash: $(MKIMG) $(AHAB_IMG) scfw_tcm.bin u-boot-atf.bin ./$(MKIMG) -soc QM -rev B0 -append $(AHAB_IMG) -c -flags 0x00200000 -scfw scfw_tcm.bin -ap u-boot-atf.bin a53 0x80000000 -out flash.bin‍‍‍‍ After the modification build the image again make clean make SOC=iMX8QM flash‍‍‍‍ On mkimage's output you should be able to see: FLAG: 0x00200000 Note how the same SCFW is used as in the previous example, same for ATF, SECO, U-boot the only required change in this case is to enable the ALT_CONFIG flag in the image. Flash the sd card with the new image sudo dd if=iMX8QM/flash.bin of=/dev/mmcblkXX bs=1k seek=32 ‍‍‍ Dumping again the partitioning on the Debug monitor shows how the system now created additional partitions for the M4 cores and a shared partition: Partition 0 --> SCFW Partition 1 --> ATF (Created at run time by the ARM Trusted Firmware) Partition 2 --> SECO Partition 3 --> M4_0 Partition 4 --> M4_1 Partition 5 --> Shared partition Partition 6 --> U-boot/Linux/rest of the system The full log is attached as well. Modifying default configuration Now we will modify the default SCFW configuration to move some resources/pads from the M4 partition to the A cores partition (u-boot/Linux). All FlexCAN resources and pads will be moved from the M4 partition to the A core partition. From sc_fw_api_qm_b0.pdf Resource List: From sc_fw_api_qm_b0.pdf Pad List: Not all resources are available on all variants, for details on what resources/pads are available on your device please refer to its respective api document. Go back to the SCFW porting kit and open platform/board/mx8qm_mek/board.c, go to the definition of board_system_config which is the function where partitioning occurs. The code first verifies if the alt_config flag is set, and if not it skips partitioning, so all partitioning happens within the following if statement: /* Configure initial resource allocation (note additional allocation and assignments can be made by the SCFW clients at run-time */ if (alt_config != SC_FALSE) ‍‍‍‍‍‍‍‍‍‍‍ The following partitions and memory regions are declared within this if statement: sc_rm_pt_t pt_m4_0; sc_rm_pt_t pt_m4_1; sc_rm_mr_t mr_m4_0, mr_m4_1; sc_rm_pt_t pt_sh; sc_rm_mr_t mr_sh;‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ pt_m4_0 is the partition for the M4_0 core, its memory region is declared as mr_m4_0. Likewise for the M4_1 pt_m4_1 and mr_m4_1 are the partitions and memory regions assigned to the M4. pt_sh and mr_sh are the shared partition and memory region. A shared partition is created but it can only have a shared memory region. Pads and resources CANNOT BE SHARED there is no mechanism to protect the pads and resources from contention, if access to a resource is required by multiple partitions a virtual resource needs to be created, in this way the partition that requires access asks the partition that owns the resource to configure/use the resource on its behalf. See the VIRT_I2C example on the Linux BSP. The partition that hosts all remaining resources is the pt_boot partition, this can be seen as the A cores partition, all resources and memory regions not assigned to the M4 partitions will be left on the pt_boot partition where the A cores are. The code is documented well and self-explanatory, for instance the following line marks all resources within the M4_0 subsystem to be moved to the M4_0 partition: /* Mark all M4_0 subsystem resources as movable */ BRD_ERR(rm_set_subsys_rsrc_movable(pt_boot, SC_R_M4_0_PID0, SC_TRUE)); BRD_ERR(rm_set_pad_movable(pt_boot, SC_P_M40_I2C0_SCL, SC_P_M40_GPIO0_01, SC_TRUE)); ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ The resource list in the sc_fw_api_qm_b0.pdf document shows what resources belong to the M4 subsystem: Next some other resources required by the M4 are assigned to its partition, such as MUs used to communicate with the other cores, timers and the IRQ steer resource. In this case we are interested on having the FlexCAN resources/pads on the A cores side, these resources/pads are being assigned to the M4_1 partition as can be seen on the previous partitions dumps and the following code: /* Move some resources not in the M4_1 subsystem */ BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_IRQSTR_M4_1, SC_R_IRQSTR_M4_1, SC_TRUE)); BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_UART_2, SC_R_UART_2, SC_TRUE)); BRD_ERR(rm_set_pad_movable(pt_boot, SC_P_UART0_CTS_B, SC_P_UART0_RTS_B, SC_TRUE)); BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_MU_6B, SC_R_MU_6B, SC_TRUE)); BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_MU_7B, SC_R_MU_7B, SC_TRUE)); BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_MU_9B, SC_R_MU_9B, SC_TRUE)); BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_GPT_3, SC_R_GPT_3, SC_TRUE)); BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_CAN_0, SC_R_CAN_2, SC_TRUE)); BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_FSPI_0, SC_R_FSPI_0, SC_TRUE)); /* Move some pads not in the M4_1 subsystem */ BRD_ERR(rm_set_pad_movable(pt_boot, SC_P_FLEXCAN0_RX, SC_P_FLEXCAN2_TX, SC_TRUE)); BRD_ERR(rm_set_pad_movable(pt_boot, SC_P_QSPI0A_DATA0, SC_P_COMP_CTL_GPIO_1V8_3V3_QSPI0, SC_TRUE)); ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Previous dump: *** Resources *********************************** Partition: 4 M4_1_PID0 UART_2 CAN_0 CAN_1 CAN_2 IRQSTR_M4_1 *** Pads **************************************** Partition: 4 M41_I2C0_SCL M41_I2C0_SDA M41_GPIO0_00 M41_GPIO0_01 UART0_RTS_B UART0_CTS_B FLEXCAN0_RX FLEXCAN0_TX FLEXCAN1_RX FLEXCAN1_TX FLEXCAN2_RX FLEXCAN2_TX So we just need to remove the following lines from the board.c: BRD_ERR(rm_set_resource_movable(pt_boot, SC_R_CAN_0, SC_R_CAN_2, SC_TRUE)); BRD_ERR(rm_set_pad_movable(pt_boot, SC_P_FLEXCAN0_RX, SC_P_FLEXCAN2_TX, SC_TRUE)); ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ That way the resources/pads won't be marked to be moved to the M4_1 partition and they will be left on the pt_boot partition (A core partition). If a resource needs to be added to the M4 partition just add the calls to rm_set_resource_movable to assign it. Now we just need to rebuild the scfw and our image: make qm R=B0 B=mek M=1‍‍‍‍‍ Then on mkimage (with the flags set modification above): make SOC=iMX8QM flash‍‍‍‍ Flash the sd card with the new image: sudo dd if=iMX8QM/flash.bin of=/dev/mmcblkXX bs=1k seek=32 ‍‍‍ Now when the dump is done we can see that the FlexCAN resources and pads belong to the same partition as the A cores (partition 6). *** Resources *********************************** Partition: 6 FTM_1 CAN_0 CAN_1 CAN_2 DMA_1_CH0 *** Pads **************************************** Partition: 6 COMP_CTL_GPIO_1V8_3V3_GPIOLHT FLEXCAN0_RX FLEXCAN0_TX FLEXCAN1_RX FLEXCAN1_TX FLEXCAN2_RX FLEXCAN2_TX COMP_CTL_GPIO_1V8_3V3_GPIOTHR The device tree would still need to be modified to configure the pads and FlexCAN resources. System Controller Firmware 101 
記事全体を表示
Update The source code is one week old now, so please, update it! $ repo sync Images - the result of a bitbake Example of a content after bitbake build_mx6/tmp/deploy/images: fsl-image-gui-imx6qsabresd-20130505174618.rootfs.ext3 fsl-image-gui-imx6qsabresd-20130505174618.rootfs.sdcard fsl-image-gui-imx6qsabresd-20130505174618.rootfs.tar.bz2 fsl-image-gui-imx6qsabresd-20130508162511.rootfs.ext3 fsl-image-gui-imx6qsabresd-20130508162511.rootfs.sdcard fsl-image-gui-imx6qsabresd-20130508162511.rootfs.tar.bz2 fsl-image-gui-imx6qsabresd.ext3 fsl-image-gui-imx6qsabresd.sdcard fsl-image-gui-imx6qsabresd.tar.bz2 modules-3.0.35-1.1.0+yocto+g0596856-r32.10-imx6qsabresd.tgz README_-_DO_NOT_DELETE_FILES_IN_THIS_DIRECTORY.txt u-boot.imx u-boot-imx6qsabresd.imx u-boot-imx6qsabresd-v2013.04-r3.imx* uImage uImage-3.0.35-r32.10-imx6qsabresd-20130505174618.bin uImage-imx6qsabresd.bin Get used with generated images. Understand which file is a symbolic link and which one is the image in fact. Symbolic link will always point to latest image. sdcard image Take a look how sdcard is generated here meta-fsl-arm - Layer containing Freescale ARM hardware support metadata The disk layout used is: 0-> IMAGE_ROOTFS_ALIGNMENT    reserved to bootloader (not partitioned) IMAGE_ROOTFS_ALIGNMENT -> BOOT_SPACE    kernel and other data BOOT_SPACE -> SDIMG_SIZE     rootfs Use IMAGE_OVERHEAD_FACTOR to add more space Please, go to original file in order to understand the disk layout. It´s basically some initial space for u-boot. One partition for uImage. One partition for rootfs. The total sdcard size will be calculate for every image, if you want to add more empty space inside generated sdcard, use IMAGE_OVERHEAD_FACTOR. Deploy Deploy the sdcard image: $ sudo dd if=fsl-image-gui-imx6qsabresd.sdcard of=/dev/sdX bs=1M Or, deploy the ext3 rootfs $ sudo dd if=fsl-image-gui-imx6qsabresd.ext3 of=/dev/sdX2 bs=1M Or deploy only the tar.bz rootfs $ sudo mount /dev/sdX2 /mnt/card $ sudo tar xf imagename-imx53qsb.tar.bz2 -C /mnt/card In order to deploy only kernel $ sudo cp uImage-3.0.35-r32.10-imx6qsabresd-20130505174618.bin /media/Boot In order to  deploy only u-boot $ sudo dd if=u-boot-imx6qsabresd-v2012.10-r3.imx of=/dev/sdX bs=512 seek=2 If using HDMI please, modify u-boot environment arguments: setenv mmcargs "setenv bootargs console=${console},${baudrate} root=${mmcroot} rootwait rw video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24" This is the how sdcards are made by meta-fsl-arm. Of course you can use your own. But double check the u-boot bootenv. Plug your sdcard and let the board boot To login: root Go to HOME Go to Task #3 - The build result Go to Task#5 - kernel
記事全体を表示
The attached patch enables HDMI overscan for Android JB, and tested by MX6Q SabreSD with Android_4.2.2_1.0.0-ga. The bootargs includes "video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:dev=hdmi,1920x1080M@60,if=RGB24,bpp=32 video=mxcfb2:off".
記事全体を表示
This patch release is target for LPDDR2 ( dual channels in interleave mode ) support on i.MX6DL platform. Two patches are prepared to modify u-boot and kernel in order to have correct DRAM init sequence, 400MHz & 24MHz frequency switching and suspend/resume support. The patches are not fully verified. It is provided as reference for customer to enable their i.MX6DL board with LPDDR2. Customization and Testing is needed by customer. We need to remind some points here: MMDC_MDCFG3LP in 24MHz need to increase the margin ( 0x40222 -> 0x80555 ) in order to pass the OS frequency switch stress test. We are identifying the reason but this workaround is working fine and included to the patch. Code changes in kernel is prepared so that it is compatible to DDR3. In other words, the DDR type will be detected and a correct handling will be done for LPDDR2 and DDR3. In LPDDR2 system, we can't put SDQ pin into LPM during suspend. Otherwise, the system cannot resume. Dual channels in fix mapping mode is not recommended to use.
記事全体を表示
After bitbake meta-toolchain the script to install the toolchain package is located under $ ls tmp/deploy/sdk/poky-eglibc-x86_64-arm-toolchain-1.4.1.sh    tmp/deploy/sdk/poky-eglibc-x86_64-arm-toolchain-1.4.1.sh In order to install it: $ source poky-eglibc-x86_64-arm-toolchain-1.4.1.sh     [sudo] password for daiane:     Enter target directory for SDK (default: /opt/poky/1.4.1):     You are about to install the SDK to "/opt/poky/1.4.1". Proceed[Y/n]?y     Extracting SDK...done     Setting it up...done     SDK has been successfully set up and is ready to be used. Hello World $ source /opt/poky/1.4.1/environment-setup-armv7a-vfp-neon-poky-linux-gnueabi $ cd ~/test/ $ arm-poky-linux-gnueabi-gcc helloworld.c $ ls a.out                                                 helloworld.c                           $ ./a.out -bash: ./a.out: cannot execute binary file $ file a.out a.out: ELF 32-bit LSB executable, ARM, version 1 (SYSV), dynamically linked (uses shared libs), for GNU/Linux 2.6.16, not stripped Kernel $ source /opt/poky/1.4.1/environment-setup-armv7a-vfp-neon-poky-linux-gnueabi $ cd linux-2.6-imx $ git checkout remotes/origin/imx_3.0.35 $ export ARCH=arm $ export CROSS_COMPILE=$TARGET_PREFIX $ unset LDFLAGS $ make imx6_defconfig $ make uImage Make sure to have mkimage available on bin patch (if using mkimage from u-boot export its patch) Or, download the ubuntu pachage: sudo apt-get install uboot-mkimage UPDATE You may find the following error:   OBJCOPY arch/arm/boot/zImage   Kernel: arch/arm/boot/zImage is ready multiple (or no) load addresses: This is incompatible with uImages Specify LOADADDR on the commandline to build an uImage make[1]: *** [arch/arm/boot/uImage] Error 1 make: *** [uImage] Error 2 This is regarding a missing LOADADDR for mkimage to use to generate uImage with the right offset to be placed in the right LOADADDR. The address value is dependent on your hardware! And it is different depending on imx6 variations. So please be aware regarding what is your right value. If the machine you are using is supported in yocto project/meta-fsl-arm, for example, you can find the value related with your board in the file conf/machine/include/imx-base.inc or online here meta-fsl-arm - Layer containing Freescale ARM hardware support metadata It is the same value used in variable UBOOT_ENTRYPOINT. For example as of this writing for the Freescale SABRE-SD board looking in conf/machine/include/imx-base.inc UBOOT_ENTRYPOINT_mx6  = "0x10008000" Thus the build command would be: $ make uImage LOADADDR=0x10008000 So, as a quick reference table, I point here the 3 most wanted make command lines: imx28evk: $ make LOADADDR=0x40008000 imx53qsb: $ make LOADADDR=0x70008000 imx6qsabresd: $ make LOADADDR=0x10008000 Update 2 Suggested by cmcqueen1975 Building an autotools-based package. E.g. $ source /opt/poky/1.4.1/environment-setup-armv7a-vfp-neon-poky-linux-gnueabi $ ./configure ${CONFIGURE_FLAGS} $ make $ make install the CONFIGURE_FLAGS is the variable depending on your very-own project. Go to Yocto Training - HOME Go to Task #7 - Create the toolchain
記事全体を表示
Q: How to program i.MX6 eFUSE? A: what about using the mfg tool? In the end only the supplies, USB OTG and the boot mode pins need to be connected. The customers Idea was to have all devices (i.MX6 eFUSE, Flash, PFUZE, etc) pre- programmed before mounting on the board. I presented the flows we support (MFG Tool, Platform SDK) for eFUSE programming last Friday when I was at the customer. KITPF0100SKTEVBE Product Summary Page MfgTools is the most convenient way to burn eFuse. Or the customer can burn the fuse on their jig/socket board by the u-boot: How to Fuse in U-Boot U-Boot contains a tool, imxotp, which is used for fusing. U-Boot > imxotp imxotp - One-Time Programable sub-system Usage: imxotp imxotp read <index> - read fuse at 'index' imxotp blow [--force] <index> <value> - blow fuse at 'index' with hex value 'value' Tips: 'addr' to 'index': convert 'index' from 'address' index = (addr - otp_base) / 0x10 eg, addr is 0x021bc410, otp_base is 0x021bc400, the index = 1 '--force' must be present in order to blow the fuse. Command will abort if '--force' is missing. index = (addr - otp_base) / 0x10, where the addr is the address of the fuse you want to operate, the otp_base is the base address of the fuse block. 'value' should correspond to fuse settings according to the fuse map and desired fuse configuration. ---------------------------------- FIrst of all thanks for your reply. However both flow assumes the i.MX6 is already soldered on the board. Please note the specific request was if it is possible (and we can support a programming house) to pre program the efuses BEFORE they are soldered on the PCB thus on a standard programmer. Take an FLASH programmer as an example.
記事全体を表示