i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
For iMX6DQ, there are two IPUs, so they can support up to 4 cameras at the same time. But the default BSP can only support up to two cameras at the same time. The attached patch can make the BSP support up to 4 cameras based on 3.10.53 GA 1.1.0 BSP.   The 4 cameras can be: - 1xCSI, 3xMIPI - 2xCSI, 2xMIPI - 4xMIPI   For 4xMIPI case, the four cameras should be combined on the single MIPI CSI2 interface, and each camera data should be transfered on a mipi virtual channel.   In this patch, we given the example driver for Maxim MAX9286, it was verified working on iMX6DQ SabreAuto board. The input to MAX9286 is four 720P30 cameras. The verified camera boards:     (1) Onsemi AR0140+AP0101+MAX9271 boards.     (2) OmniVision OV10635+MAX9271 boards.   The MIPI CSI2 CVBS camera surround view solution can be found at: iMX6DQ ISL79985/79987 MIPI CSI2 CVBS camera surround view solution for Linux BSP The MIPI CSI2 CVBS HD camera surround view solution can be found at: iMX6DQ TP2854 MIPI CSI2 720P CVBS camera surround view solution for Linux BSP   The kernel patches: 0001-IPU-update-IPU-capture-driver-to-support-up-to-four-.patch      Updated IPU common code to support up to four cameras.   0002-Add-Max9286-support-on-SabreAuto-board-which-can-sup.patch      MAX9286 driver, it includes MAX9271, AP0101 and AR0140 drivers.   0003-Remove-the-page-size-align-requirement-for-v4l2-capt.patch      With this patch, the mxc_v4l2_tvin test application can use overlay framebuffer as V4l2 capture buffer directly.   0004-Max9286-skip-AP0101-camera-re-initialization.patch      If the camera board's power had been kept after initialized, this patch will bypass the re-initialization to reduce the start up time.   0005-Max9286-set-I2C-speed-to-400Kbps.patch     Set I2C to 400Kbps to reduce the AP0101+AR0140 initialization time.   0006-Max9286-add-retry-for-MAX9271-I2C-access.patch     Added retry for MAX9271 I2C access.   0007-Max9286-Add-support-for-OV10635-camera.patch     Updated code for OV10635 camera.   0008-Max9286-support-auto-detect-camera-number.patch     Make the Max9286 driver can detect the camera number automatically.     How to builld the kernel with MAX9286 support:       make imx_v7_defconfig       make menuconfig (In this command, you should select the MAX9286 driver:             Device Drivers  --->                   <*> Multimedia support  --->                         [*]   V4L platform devices  --->                               <*>   MXC Video For Linux Video Capture                                       MXC Camera/V4L2 PRP Features support  --->                                           <*>Maxim max9286 GMSL Deserializer Input support                                               Select Camera Sensor (OmniVision OV10635 camera sensor)  // Or (Onsemi AP0101 and AR0140 camera sensor)                                           <*>mxc VADC support                                           <*>Select Overlay Rounting (Queue ipu device for overlay library)                                           <*>Pre-processor Encoder library                                           <*>IPU CSI Encoder library)       make zImage       make dtbs   The built out image file:       arch/arm/boot/dts/imx6q-sabreauto.dtb       arch/arm/boot/zImage   "mxc_v4l2_tvin_max9286.tar.gz" is the test application, test command to capture the four cameras and render on 1080P HDMI display: /mxc_v4l2_tvin.out -ol 0 -ot 0 -ow 960 -oh 540 -d 1 -x 0 -g2d & /mxc_v4l2_tvin.out -ol 960 -ot 0 -ow 960 -oh 540 -d 1 -x 1 -g2d & /mxc_v4l2_tvin.out -ol 0 -ot 540 -ow 960 -oh 540 -d 1 -x 2 -g2d & /mxc_v4l2_tvin.out -ol 960 -ot 540 -ow 960 -oh 540 -d 1 -x 3 -g2d &   Some hardware check point on AR0140+AP0101+MAX9271 camera board (Please get MAX9286 and OV10635 schematics from Maxim): 1. In this patch, MAX9286's I2C address is 0x4D, so ADD0 and ADD1 should be connected to high. AP0101's I2C address is 0xBA, so SADDR should be connected to high.   2. AP0101's DOUT0~DOUT7 should be connected to MAX9271's DIN7~DIN0, the order should be switched, MSB connected to LSB.   3. MAX9271's GPO pin should be connected to AP0101's FRAME_SYNC pin. The pull down resistance on FRAME_SYNC pin should not be 0 ohm.   Some known limitation: 1. AP0101's VSYNC invalid time, last video line's HSYNC to VSYNC porch's max value is 255 pixel clocks, it is not enough for MAX9286 to generate the Frame End MIPI packets for each camera. So in order to let iMX6DQ to capture 1280x720 video for each camera, we had let AP0101 output 1280*724 frame size, and iMX6 will only capture 720 lines, the remained video data and Frame End will be ignored. This solution will not impact the function, but there will be "Error matching Frame Start with Frame End for Virtual Channel x" error reported from iMX6 MIPI_CSI_ERR1 register. Maxim suggested to use MAX96705 to relace the MAX9271, it can delay the VSYNC invalid time, then the MIPI error will be fixed.     2015-11-17 update: Updated for OV10635 camera support. File: L3.10.53_GA1.1.0_MAX9286_Surroundview_Patch_2015-11-17.zip   2015-12-04 update: File: L3.10.53_GA1.1.0_MAX9286_Surroundview_Patch_2015-12-04.zip Added patch 0009-Max9286-updated-PCLK-edge-setting-for-OV10635.patch to correct the OV10635 PCLK edge setting     2016-03-07 update: File L3.14.38_GA_MAX9286_Surroundview_Patch_2016-03-07.zip Added kernel patch for L3.14.38 GA 1.1.0 BSP.   2016-07-26 update: Files: L3.10.53_GA1.1.0_MAX9286_Surroundview_Patch_2016-07-26.zip; L3.14.38_GA1.1.0_MAX9286_Surroundview_Patch_2016-07-26.zip; L3.14.52_GA1.1.0_MAX9286_Surroundview_Patch_2016-07-26.zip. Added gstreamer support. Added MAX96705 support. Added patch for L3.14.52_GA1.1.0.   2017-12-11 update: Added CVBS surround view link: iMX6DQ TP2854 MIPI CSI2 720P CVBS camera surround view solution for Linux BSP     2021-04-26 update: Some customer reported, when system loading is heavy, sometimes, some camera will flicker left and right. It is caused by SFMC FIFO data lost. The original patch used IDMAC 0 and IDMAC 1 for two cameras on one IPU, this is not the best setting.  IDMAC 1 is fixed to use 1/4 SMFC FIFO and it will cause IDMAC 0 to use 1/4 SMFC FIFO too. And another 1/2 of SMFC FIFO can't be used in this case. Some code update to improve it: For each IPU, please use IDMAC 0 and IDMAC 2 to capture the two cameras. This needs change the hard coding in "drivers\media\platform\mxc\capture\ipu_csi_enc.c", "CSI_MEM1" and "IPU_IRQ_CSI1_OUT_EOF" should be changed to "CSI_MEM2" and "IPU_IRQ_CSI2_OUT_EOF". In this case, all SMFC FIFO can be used. And in "ipu_common.c", function ipu_probe(), the followed code should be changed to make IDMAC2 use high priority too. /* Set sync refresh channels and CSI->mem channel as high priority */ - ipu_idmac_write(ipu, 0x18800003L, IDMAC_CHA_PRI(0)); + ipu_idmac_write(ipu, 0x1880000FL, IDMAC_CHA_PRI(0));
View full article
      The i.MX6UL/LL/LZ processor supports 2 USB OTG interfaces, USB OTG1 and USB OTG2, and each USB interface can be configured as a device, host or dual role mode. On the EVK board of i.MX6UL/LL, USB OTG1 is designed as dual role mode, and USB OTG2 is designed as HOST mode. This is sufficient for most customers.       However, in actual applications, we may need 2 USB HOSTs, and at the same time, we don’t want to use MicroUSB to USB TYPE-AF cable for Host-Device mode conversion. Therefore, the design of the USB circuit needs to meet such requirements: 1. USB device mode We need a USB device to download the linux image to the flash or SD card on the board. 2. 2 USB HOSTs When the system is working normally, we need the board to support 2 USB HOST. i.MX6UL/LL/LZ has only 2 USB ports. How to design to meet this requirement without increasing the USB HUB? The following scheme is used as a reference, and I hope it will be helpful to customers with similar requirement:        The logic and application description of this Diagram:: Default—device mode In the process of debugging the software, we need to use the USB OTG interface to download the linux image, so it must work in device mode. What we need to do is: (1). Pull USB OTG ID up to 3.3V (2). The USB OTG D+/D- signal is switched to the MicroUSB connector. (3). The USB OTG VBUS is provided with 5V power from the external PC USB HOST. Usage:        -Use a jumper for Pin 1 and Pin2, USB OTG ID pin will be pulled up to High.        With the operation, SEL pin of USB Muxer is High, and USB signals are switched to port B, and USB differential signals are connected to MicroUSB connector. At the same time, MIC2026-1YM output is disabled. The USB OTG1 VBUS pin of CPU is supplied by VBUS of MicroUSB connector, that is to say, supplied by PC USB HOST.        In this mode, software engineer can use it to download images to flash on board. Normal Work—Host mode After the software debugging is completed, two HOSTs are needed on the board. At this time, we need to switch the USB OTG1 from device to HOST mode. What we need to do is: (1). Pull USB OTG1 ID down to LOW (2). The USB OTG D+/D- signal is switched to the USB Type-AF connector. (3). Board should supply 5V power for USB device connected USB Type-AF connector. Usage:        -Use a jumper for Pin 2 and Pin3, USB OTG ID pin will be pulled down to Low.        With the operation, USB OTG1 ID pin is pulled down to Low, SEL pin of USB Muxer is also LOW, USB signals are switched to Port A, and connected to USB type-AF connector. At the same time, MIC2026-1YM is enabled , OUTA will output 5V , which will supply USB device connected on USB type-AF connector.   [Note] Users need to pay attention to. When using the jumper with PIN1/2/3, the board needs to be powered off. In other words, when switching between device and host, you need to switch off the power, then power on, and restart the board. The solution can also be used for i.MX processors with USB 2.0 interface.   NXP CAS team Wedong Sun 01/15/2021
View full article
Recently, some customers are using i.MX processor, they want to add raid & LVM function support to the kernel, but they have encountered the problem that the compilation cannot pass. Tested it in L4.14.98, L4.19.35 & L5.4.x, Only L4.14.98 bsp exists the problem. Here are the experimental steps I have done, including the same problems I encountered with the customer, and how to modify the kernel to ensure that the compilation passes. 1. Exporting cross compilation tool chain from yocto BSP (1) Downloading Yocto BSP and compiling it. Following steps in i.MX_Yocto_Project_User's_Guide.pdf, download Yocto BSP and compile it successfully. (2) Exporting cross compilation tool chain Following methods described in i.MX_Linux_User's_Guide.pdf, export cross compilation tool chain from yocto BSP. See Chapter 4.5.12 of the document, please! Then cross compilation tool chain will be like below: (3) Copying linux BSP source code to a new directory # cd ~ # mkdir L4.14.98-2.0.0 # cd L4.14.98-2.0.0 # cp -r ~/imx-yocto-bsp/build-fb/tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/4.14.98- r0/git ./ Then all linux source code has been copied to L4.14.98-2.0.0, which is the top directory of linux kernel source code, I will compile kernel image here. 2. Compiling linux kernel # cd ~/L4.14.98-2.0.0 # source /opt/fsl-imx-fb/4.14-sumo/environment-setup-cortexa9hf-neon-poky-linux-gnueabi # export ARCH=arm # make imx_v7_defconfig # make menuconfig Then we will add RAID and LVM modules to linux kernel. In order to reproduce errors, I added all related modules to kernel. See below, please! Device drivers---->Multiple devices driver support (RAID and LVM) After save and exit, began to compile kernel. # make (make –j4) The following errors will occur: ------------------------------------------------------------------------------------------- drivers/md/dm-rq.c: In function ‘dm_old_init_request_queue’: drivers/md/dm-rq.c:716:2: error: implicit declaration of function ‘elv_register_queue’; did you mean ‘blk_register_queue’? [-Werror=implicit-function-declaration] elv_register_queue(md->queue); ^~~~~~~~~~~~~~~~~~ blk_register_queue cc1: some warnings being treated as errors scripts/Makefile.build:326: recipe for target 'drivers/md/dm-rq.o' failed make[2]: *** [drivers/md/dm-rq.o] Error 1 scripts/Makefile.build:585: recipe for target 'drivers/md' failed make[1]: *** [drivers/md] Error 2 Makefile:1039: recipe for target 'drivers' failed make: *** [drivers] Error 2 ------------------------------------------------------------------------------------------- 3. Finding out root cause and solving it (1) elv_register_queue( ) function The function is loaded in dm-rq.c : int dm_old_init_request_queue(struct mapped_device *md, struct dm_table *t) { … … elv_register_queue(md->queue); … … } BUT compiler didn’t find it’s declaration and entity. Searching source code, and found it declared in linux_top/block/blk.h: … … int elv_register_queue(struct request_queue *q); … … It’s entity is in linux_top/block/elevator.c: int elv_register_queue(struct request_queue *q) { … … } (2) Adding declaration and exporting the function --- Declaration Add the line below to dm-rq.c: … … extern int elv_register_queue(struct request_queue *q); … … --- Exporting the function(elevator.c) Add EXPORT_SYMBOL(elv_register_queue); to the end of function, see below. int elv_register_queue(struct request_queue *q) { … … } EXPORT_SYMBOL(elv_register_queue); 4. Re-compiling Linux Kernel The above error will not occur and the compilation will complete successfully.   NXP CAS team Weidong Sun
View full article
i.MX evaluation board can be a simple solution to program i.MX boards in a factory for instance. i.MX evaluation board are not for industrial usage, but you can find plenty of cheap i.MX insdustrial boards on the web. Here I am using an i.MX8QXP rev B0 MEK board and I will program an i.MX6Q SABRE SD board. The first step is to generate your image. Follow the documentation steps to generate the "validation" image. You will have to customize a little bit the local.conf file (in conf/local.conf) to have git, cmake, gcc and other missing package. edit local.conf and add the following lines at the end of the file: IMAGE_INSTALL_append = " git cmake htop packagegroup-core-buildessential xz p7zip rsync"‍‍‍‍‍ I have added rsync package in local, it can replace cp (copy) but with the --progress option you can see the copy progression. P7zip replace unzip for our images archives avaialable on nxp.com as unzip as issues with big files. then rebake your image: bitbake -k fsl-image-validation-imx‍‍‍‍‍ When it is done, go in tmp/deploy/image/<your image generated> and use uuu to program your board (I use a sd card; thus I can increase the partition esily): sudo ./uuu -b sd_all imx-boot-imx8qxpmek-sd.bin-flash fsl-image-validation-imx-imx8qxpmek.sdcard.bz2/*‍‍‍‍‍ As the rootfs can be too small, use gparted under Linux for instance to increase the size of the partition. Put the SD card and start your board. Here here the dirty part... You may know archlinux|ARM websitesite (Arch Linux ARM ), you have a lots of precompiled packages. Thus on the board you can download it, and copy the file in /usr folder (you can use it to have the latest openSSL for  instance!). Plug an ethernet cable on the board and check if it is up: ifconfig -a ifconfig eth0 up‍‍‍‍‍‍‍‍‍‍ Now you should have access to the internet. On uuu webpage you can find all the packages you need (here I am using a 4.14.98_2.0.0 Linux): mkdir missinglibs cd missinglibs wget http://mirror.archlinuxarm.org/aarch64/core/bzip2-1.0.8-2-aarch64.pkg.tar.xz wget http://mirror.archlinuxarm.org/aarch64/core/nettle-3.5.1-1-aarch64.pkg.tar.xz wget http://mirror.archlinuxarm.org/aarch64/core/libusb-1.0.22-1-aarch64.pkg.tar.xz wget http://mirror.archlinuxarm.org/aarch64/extra/libzip-1.5.2-2-aarch64.pkg.tar.xz wget http://mirror.archlinuxarm.org/aarch64/core/zlib-1:1.2.11-3-aarch64.pkg.tar.xz wget http://mirror.archlinuxarm.org/aarch64/extra/p7zip-16.02-5-aarch64.pkg.tar.xz cd ..‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Wait all the archives are downloaded (otherwise you'll decompress before the archive is downloaded) as wget is running in background! Now untar the archives and copy it in the rootfs (dirty): tar -xJf libzip-1.5.2-2-aarch64.pkg.tar.xz tar -xJf libusb-1.0.22-1-aarch64.pkg.tar.xz tar -xJf nettle-3.5.1-1-aarch64.pkg.tar.xz tar -xJf bzip2-1.0.8-2-aarch64.pkg.tar.xz cp zlib-1:1.2.11-3-aarch64.pkg.tar.xz zlib tar -xJf zlib tar -xJf p7zip-16.02-5-aarch64.pkg.tar.xz cd usr sudo cp -R . /usr cd ../../ ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Download and compile uuu: git clone git://github.com/NXPmicro/mfgtools.git cd mfgtools/ cmake . make‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Download an image on nxp.com for instance. I have downloaded on the i.MX6 4.14.98_2.0.0 image and put it on a usb key. then unzip it in the uuu folder: 7z e L4.14.98_2.0.0_ga_images_MX6QPDLSOLOX.zip‍‍‍‍ As mentionned before unzip cannot hadle big files... so use 7z as me plug the i.MX6Q SABRE SD to the i.MX8X and program your i.MX6 board: ./uuu uuu.auto-imx6qsabresd‍ uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.3.74-0-g64eeca1 Success 1 Failure 0 ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍
View full article
A new version of the Pins Tool for i.MX Application Processors has been released and is available for download as desktop tool from Pins Tool for i.MX Application Processors|NXP. The pins Tool for i.MX Application Processors is used for pin routing configuration, validation and code generation, including pin functional/electrical properties, power rails, run-time configurations, with the following main features: Desktop application Muxing and pin configuration with consistency checking Multicore support ANSI-C initialization code Graphical processor package view Multiple configuration blocks/functions Easy-to-use device configuration Selection of Pins and Peripherals Package with IP blocks Routed pins with electrical characteristics Registers with configured and reset values Power Groups with assigned voltage levels Source code for C/C++ applications Documented and easy to understand source code CSV Report and Device Tree File Localized for English and Simplified Chinese Mostly Connected: On-Demand device data download Integrates with any compiler and IDE What's New Added Label support to give signals a name Added ‘Log’ and ‘Problems’ view to report conflicts between settings Added support for templates to store user configurations as starting point for new configurations Added ability to download and share data for devices, especially for off-network host machines i.MX header files are now automatically part of the device data Import of legacy Processor Expert .pe files Export of register defines Various bug fixes and documentation improvements The release notes of the desktop application are attached to this article. Import Processor Expert Files A new importer has been added to import legacy Processor Expert for i.MX files: Labels Signals can now have user defined labels: Templates, Kits, Boards and Processors When creating a new configuration, it offers Templates, Boards and Processors. Custom configurations can be stored as templates and then used for new configurations. Board Specific Functions With the provided board and kit configurations, there are now pre-configured initialization functions for major blocks on the board: Export Data To simplify downloading the device specific data for the desktop tool, the 'Export' function can be used to download and export the data. The data can be copied that way to another machine or all data for a set of devices can be loaded. Export Registers With the Export command the registers can be exported as text/source: This is used to store the register values: /*FUNCTION********************************************************************** * * Function Name : init_audmux_pins * Description   : Configures pin routing and optionally pin electrical features. * *END**************************************************************************/ #define INIT_AUDMUX_PINS_IOMUXC_AUD5_INPUT_DA_AMX_SELECT_INPUT_VALUE            0x00000000   /*!< Register name: IOMUXC_AUD5_INPUT_DA_AMX_SELECT_INPUT */ #define INIT_AUDMUX_PINS_IOMUXC_AUD5_INPUT_TXCLK_AMX_SELECT_INPUT_VALUE         0x00000000   /*!< Register name: IOMUXC_AUD5_INPUT_TXCLK_AMX_SELECT_INPUT */ #define INIT_AUDMUX_PINS_IOMUXC_AUD5_INPUT_TXFS_AMX_SELECT_INPUT_VALUE          0x00000000   /*!< Register name: IOMUXC_AUD5_INPUT_TXFS_AMX_SELECT_INPUT */ #define INIT_AUDMUX_PINS_IOMUXC_SW_MUX_CTL_PAD_DI0_PIN02_VALUE                  0x00000002   /*!< Register name: IOMUXC_SW_MUX_CTL_PAD_DI0_PIN02 */ #define INIT_AUDMUX_PINS_IOMUXC_SW_MUX_CTL_PAD_DI0_PIN03_VALUE                  0x00000002   /*!< Register name: IOMUXC_SW_MUX_CTL_PAD_DI0_PIN03 */ #define INIT_AUDMUX_PINS_IOMUXC_SW_MUX_CTL_PAD_DI0_PIN04_VALUE                  0x00000002   /*!< Register name: IOMUXC_SW_MUX_CTL_PAD_DI0_PIN04 */ #define INIT_AUDMUX_PINS_IOMUXC_SW_MUX_CTL_PAD_DI0_PIN15_VALUE                  0x00000002   /*!< Register name: IOMUXC_SW_MUX_CTL_PAD_DI0_PIN15 */ #define INIT_AUDMUX_PINS_IOMUXC_SW_MUX_CTL_PAD_DISP0_DATA16_VALUE               0x00000003   /*!< Register name: IOMUXC_SW_MUX_CTL_PAD_DISP0_DATA16 */ #define INIT_AUDMUX_PINS_IOMUXC_SW_MUX_CTL_PAD_DISP0_DATA18_VALUE               0x00000003   /*!< Register name: IOMUXC_SW_MUX_CTL_PAD_DISP0_DATA18 */ #define INIT_AUDMUX_PINS_IOMUXC_SW_MUX_CTL_PAD_DISP0_DATA19_VALUE               0x00000003   /*!< Register name: IOMUXC_SW_MUX_CTL_PAD_DISP0_DATA19 */ ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ We hope you will find this new release useful. Thanks for designing with NXP! 
View full article
Using a RAW NAND is more difficult compared to eMMC, but for lower capacity it is still cheaper. Even with the ONFI (Open NAND Flash Interface) you can face initialization issue you can find by measure performance. I will take example of a non-well supported flash, I have installed on my evaluation board (SABRE AI). I wanted to do a simple performance test, to check roughly the MB/s I can expected with this NAND. One of a simplest test is to use the dd command: root@imx6qdlsolo:~# time dd if=/dev/mtd4 of=/dev/null 851968+0 records in 851968+0 records out 436207616 bytes (436 MB, 416 MiB) copied, 131.8884 s, 3.3 MB/s ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ As my RAW was supposed to work in EDO Mode 5, I could expect more than 20MB/s. To check what was wrong, read you kernel startup log: Booting Linux on physical CPU 0x0 Linux version 4.1.15-2.0.0+gb63f3f5 (bamboo@yb6) (gcc version 5.3.0 (GCC) ) #1 SMP PREEMPT Fri Sep 16 15:02:15 CDT 2016 CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache Machine model: Freescale i.MX6 DualLite/Solo SABRE Automotive Board [...] Amd/Fujitsu Extended Query Table at 0x0040 Amd/Fujitsu Extended Query version 1.3. number of CFI chips: 1 nand: device found, Manufacturer ID: 0xc2, Chip ID: 0xdc nand: Macronix MX30LF4G18AC nand: 512 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 64 gpmi-nand 112000.gpmi-nand: mode:5 ,failed in set feature. Bad block table found at page 262080, version 0x01 Bad block table found at page 262016, version 0x01 nand_read_bbt: bad block at 0x00000a7e0000 nand_read_bbt: bad block at 0x00000dc80000 4 cmdlinepart partitions found on MTD device gpmi-nand Creating 4 MTD partitions on "gpmi-nand":‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ On line 13 you can read "mode:5, failed in set feature", meaning you are not in mode 5... so you have the "relaxed" timing you have at boot. After debuging your code (I have just remove the NAND back reading security check), you can redo the test: root@imx6qdlsolo:~# time dd if=/dev/mtd4 of=/dev/null 851968+0 records in 851968+0 records out 436207616 bytes (436 MB, 416 MiB) copied, 32.9721 s, 13.2 MB/s‍‍‍‍‍‍‍‍‍‍‍‍ So you multiplied the performances by 4! Anyway, you have a better tool to measure your NAND performance, it is mtd_speedtest, but you have to rebuild your kernel. In Yocto, reconfigure your kernel (on your PC of couse!): bitbake virtual/kernel -c menuconfig‍‍‍ Choose in the menu "Device Drivers" -> "Memory Technology Device (MTD) support" -> "MTD tests support", even it it not recommended! bitbake virtual/kernel -f -c compile bitbake virtual/kernel -f -c build bitbake virtual/kernel -f -c deploy‍‍‍‍‍‍‍‍‍ Then reflash you board (kernel + rootfs as tests are .ko files): Then you can do more accurate performance test: insmod /lib/modules/4.1.29-fslc+g59b38c3/kernel/drivers/mtd/tests/mtd_speedtest.ko dev=2 ================================================= mtd_speedtest: MTD device: 2 mtd_speedtest: MTD device size 16777216, eraseblock size 131072, page size 2048, count of eraseblocks 128, pages per eraseblock 64, OOB size 64 mtd_test: scanning for bad eraseblocks mtd_test: scanned 128 eraseblocks, 0 are bad mtd_speedtest: testing eraseblock write speed mtd_speedtest: eraseblock write speed is 4537 KiB/s mtd_speedtest: testing eraseblock read speed mtd_speedtest: eraseblock read speed is 16384 KiB/s mtd_speedtest: testing page write speed mtd_speedtest: page write speed is 4250 KiB/s mtd_speedtest: testing page read speed mtd_speedtest: page read speed is 15784 KiB/s mtd_speedtest: testing 2 page write speed mtd_speedtest: 2 page write speed is 4426 KiB/s mtd_speedtest: testing 2 page read speed mtd_speedtest: 2 page read speed is 16047 KiB/s mtd_speedtest: Testing erase speed mtd_speedtest: erase speed is 244537 KiB/s mtd_speedtest: Testing 2x multi-block erase speed mtd_speedtest: 2x multi-block erase speed is 252061 KiB/s mtd_speedtest: Testing 4x multi-block erase speed mtd_speedtest: 4x multi-block erase speed is 256000 KiB/s mtd_speedtest: Testing 8x multi-block erase speed mtd_speedtest: 8x multi-block erase speed is 260063 KiB/s mtd_speedtest: Testing 16x multi-block erase speed mtd_speedtest: 16x multi-block erase speed is 260063 KiB/s mtd_speedtest: Testing 32x multi-block erase speed mtd_speedtest: 32x multi-block erase speed is 256000 KiB/s mtd_speedtest: Testing 64x multi-block erase speed mtd_speedtest: 64x multi-block erase speed is 260063 KiB/s mtd_speedtest: finished =================================================‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ You can now achieve almost 16MB/s, better than the dd test. Of course you cannot achieve more than 20MB/s, but you are not that far, and the NAND driver need optimizations. To redo the test: rmmod /lib/modules/4.1.29-fslc+g59b38c3/kernel/drivers/mtd/tests/mtd_speedtest.ko insmod /lib/modules/4.1.29-fslc+g59b38c3/kernel/drivers/mtd/tests/mtd_speedtest.ko dev=2 To check your NAND is in EDO mode 5, you can check your clock tree: /unit_tests/dump-clocks.sh clock          parent   flags    en_cnt pre_cnt      rate [...] gpmi_bch_apb   ---      00000005   0       0       198000000 gpmi_bch       ---      00000005   0       0       198000000 gpmi_io        ---      00000005   0       0        99000000 gpmi_apb       ---      00000005   0       0       198000000‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ The IO are clocked now at 99MHz, thus you can read at 49.5MHz (20ns in EDO mode 5 definition).
View full article
NOTE: Always de-power the target board and the aggregator when plugging or unplugging smart sensors from the aggregator. NOTE: See this link to instrument a board with a Smart Sensor. This page documents the triple-range "smart" current sensor that's part of a larger system for profiling power on application boards. The smart sensor features a Kinetis KL05Z with three current sense amplifiers. It allows measurement currents in three ranges. Four assembly options allow measurement of rail voltages 0-3.3V (two overall current ranges), 0-6.6V, and 12V. It connects to an aggregator, which powers, controls and aggregates data from a number of smart sensor boards. One of the biggest improvements over the older dual-range measurement system is that the on-sensor microcontroller allows near-simultaneous measurement of all instrumented rails on a board. The dual range profiler can only make one measurement at a time.  These are intended to be used with a microncontroller board to act as a trigger and data aggregator. This aggregator could also be used to reprogram the sensors.  The series resistance added by the smart sensor when in run mode (highest current range) is under 11 milliOhms as measured with 4-point probes and a Keysight B2902B SMU.  A "power oscilloscope" can be made by triggering measurements at regular intervals and presenting the results graphically.... Schematic: Board Layout, Top: Board Layout, Bottom: Here's a photo of two with a nickel is included to show scale. The board measures about 0.5 by 1.3 inches. Connections: The smart sensor header connections are: 5V: powers the 3.3V regulator, which in turn powers everything else on the sensor board 12V: all the gates of all the switching FETs are pulled pulled up to 12V GND: ground connection SCL/TX: I2C clock line  SDA/RX: I2C data line  SWD_CLK:  line for triggering smart sensors to make measurements RESET_B:  line for resetting the smart sensor board SWD_IO: select line for the smart sensor Theory of operation: Three shunts and current sense amplifiers are used to measure current in three ranges. One shunt/sense amp pair has a 0.002Ω shunt integrated into the IC package (U1, INA250). The other two sense amps (U2 and U3, INA212) require an external shunt.  FETs Q1, Q2,  and Q3 are used to switch the two lower range shunt/sense amp pairs in and out of circuit. In normal run operation (highest current range), Q1 (FDMC012N03, with Rds(on) under 1.5mΩ) is turned on, which shorts leaves only U1 in circuit. FETs Q4, Q5 and Q6 translate the voltages to 3.3V so that GPIO on U4 (MCU KL05Z) can control them.  Rail voltage measurement is facilitated via resistors R3, R4, and R12 and Q7. Not all of these are populated in every assembly option. For measuring rail voltages 0-3.3V, R12 is populated. To measure 0-6.6V, R3, R4,and Q7 are populated. When turned on Q7 enables the voltage divider. All of the assembly option population info can be found in the schematic (attached). Regulator U5 (AP2210N) provides the 3.3V supply for all of the components on the board. This 1% tolerance regulator is used to provide a good reference for the ADC in U4.  Microcontroller U4 detects the assembly population option of the board via resistors R9, R10, and R11 so that the same application code can be used across all variations of the sensor boards. GPIO control the FETs and four ADC channels are used to measure the sense amplifier outputs and the rail voltage. Having a microcontroller on the sensor board allows the user to do extra credit things like count coulombs as well as allowing all similarly instrumented rails to measure at the same time via trigger line SWD_CLK. Data communication can be via I2C or UART, since these two pins can do both.  But if multiple sensor boards are to be used with an aggregator, communication needs to be over I2C. Application Code: The latest application code for the KL05Z on the smart sensor resides here: https://os.mbed.com/users/r14793/code/30847-SMRTSNSR-KL05Z/. The latest binary is attached below. In order to re-flash a smart sensor, the modification detailed in the aggregator page needs to be made. Once the modification is completed, leave the aggregator unpowered while pluging the SWD debugger into J5 and the smart sensor to be programmed into JP15. Very old UART-based application code for the KL05Z, built in the on-line MBED compiler (note that it requires the modified mbed library for internal oscillator). This code was used while testing the first smart sensor prototypes. It has since been abandoned. It's published here in the event that a user wants to use a single sensor plugged into JP15 with UART breakout connector J6. /****************************************************************************** * * MIT License (https://spdx.org/licenses/MIT.html) * Copyright 2017-2018 NXP * * MBED code for KL05Z-based "smart" current sensor board, basic testing * of functions via UART (connected via FRDM board and OpenSDA USB virtual * COM port). * * Eventual goal is to have each smart sensor communicate over I2C to an * aggregator board (FRDM board with a custom shield), allowing 1-10 power * supply rails to be instrumented. Extra credit effort is to support * sensors and aggregator with sigrok... * * Because there is no crystal on the board, need to edit source mbed-dev library * to use internal oscillator with pound-define: * change to "#define CLOCK_SETUP 0" in file: * mbed-dev/targets/TARGET_Freescale/TARGET_KLXX/TARGET_KL05Z/device/system_MKL05Z4.c * ******************************************************************************/ #include "mbed.h" // These will be GPIO for programming I2C address... // not yet implemented, using as test pins... DigitalOut addr0(PTA3); DigitalOut addr1(PTA4); DigitalOut addr2(PTA5); DigitalOut addr3(PTA6); // configure pins for measurements... // analog inputs from sense amps and rail voltage divider... AnalogIn HIGH_ADC(PTB10); AnalogIn VRAIL_ADC(PTB11); AnalogIn LOW1_ADC(PTA9); AnalogIn LOW2_ADC(PTA8); // outputs which control switching FETs... DigitalOut VRAIL_MEAS(PTA7); // turns on Q7, connecting voltage divider DigitalOut LOW_ENABLE(PTB0); // turns on Q4, turning off Q1, enabling low measurement DigitalOut LOW1(PTB2); // turns on Q5, turning off Q2, disconnecting shunt R1 DigitalOut LOW2(PTB1); // turns on Q6, turning off Q3, disconnecting shunt R2 // input used for triggering measurement... // will eventually need to be set up as an interrupt so it minimizes delay before measurement InterruptIn trigger(PTA0); // use as a trigger to make measurement... // PTB3/4 can be used as UART or I2C... // For easier development with one smart sensor, we are using UART here... Serial uart(PTB3, PTB4); // tx, rx long int count=0; int n=25; // global number of averages for each measurement int i, temp; bool repeat=true; // flag indicating whether measurements should repeat or not const float vref = 3.3; // set vref for use in calculations... float delay=0.25; // default delay between measurement bool gui = false; // flag for controlling human vs machine readable output bool statistics = false;// flag for outputting min and max along with average (GUI mode only) void enableHighRange(){ LOW_ENABLE = 0; // short both low current shunts, close Q1 wait_us(5); // delay for FET to settle... (make before break) LOW1 = 0; LOW2 = 0; // connect both shunts to make lower series resistance VRAIL_MEAS = 0; // disconnect rail voltage divider wait_us(250); // wait for B2902A settling... } void enableLow1Range(){ LOW1 = 0; LOW2 = 1; // disconnect LOW2 shunt so LOW1 can measure wait_us(5); // delay for FET to settle... (make before break) LOW_ENABLE = 1; // unshort low current shunts, open Q1 VRAIL_MEAS = 0; // disconnect rail voltage divider wait_us(250); // wait for B2902A settling... } void enableLow2Range(){ LOW1 = 1; LOW2 = 0; // disconnect LOW1 shunt so LOW2 can measure wait_us(5); // delay for FET to settle... (make before break) LOW_ENABLE = 1; // unshort low current shunts, open Q1 VRAIL_MEAS = 0; // disconnect rail voltage divider wait_us(500); // wait for B2902A settling... } void enableRailV(){ VRAIL_MEAS = 1; // turn on Q7, to enable R3-R4 voltage divider wait_us(125); // wait for divider to settle... // Compensation cap can be used to make // voltage at ADC a "square wave" but it is // rail voltage and FET dependent. Cap will // need tuning if this wait time is to be // removed/reduced. // // So, as it turns out, this settling time and // compensation capacitance are voltage dependent // because of the depletion region changes in the // FET. Reminiscent of grad school and DLTS. // Gotta love device physics... } void disableRailV(){ VRAIL_MEAS = 0; // turn off Q7, disabling R3-R4 voltage divider } // this function measures current, autoranging as necessary // to get the best measurement... void measureAuto(){ Timer t; float itemp; float tempI=0; float imin = 1.0; // used to keep track of the minimum... float imax = 0; // used to keep track of the maximum... t.start(); // use timer to see how long things take... enableHighRange(); // this should already be the case, but do it anyway... for (i = 0; i < n; i++){ itemp = HIGH_ADC; // read HIGH range sense amp output if (statistics && itemp>imax) imax = itemp; // update max if necessary if (statistics && itemp<imin) imin = itemp; // update min if necessary tempI += itemp; // add current sample to running sum } tempI = tempI/n *vref/0.8; // compute average we just took... if (gui) uart.printf("=> %5.3f ", tempI); if (statistics && gui) uart.printf("[%5.3f/%5.3f] ", imin*vref/0.8, imax*vref/0.8); // if current is below this threshold, use LOW1 to measure... if (tempI < 0.060) { if (!gui) uart.printf("... too Low: %f A, switching to low1 ==>\r\n", tempI); tempI=0; enableLow1Range(); // change FETs to enable LOW1 measurement... imin = 1.0; imax = 0; for (i = 0; i < n; i++){ itemp = LOW1_ADC; // read LOW1 sense amp output if (statistics && itemp>imax) imax = itemp; // update max if necessary if (statistics && itemp<imin) imin = itemp; // update min if necessary tempI += itemp; // add current sample to running sum } tempI = tempI/n *vref/0.05/1000; // compute average we just took... if (gui) uart.printf("%6.4f ", tempI); if (statistics && gui) uart.printf("[%6.4f/%6.4f] ", imin*vref/0.05/1000, imax*vref/0.05/1000); // if current is below this threshold, use LOW2 to measure... if (tempI < 0.0009){ if (!gui) uart.printf("... too Low: %f A, switching to low2 ==>\r\n", tempI); tempI=0; enableLow2Range(); // change FETs to enable LOW1 measurement... imin = 1.0; imax = 0; for (i = 0; i < n; i++){ itemp = LOW2_ADC; // read LOW2 sense amp output if (statistics && itemp>imax) imax = itemp; // update max if necessary if (statistics && itemp<imin) imin = itemp; // update min if necessary tempI += itemp; // add current sample to running sum } tempI = tempI/n *vref/2/1000; // compute average we just took... if (gui) uart.printf("%8.6f ", tempI); if (statistics && gui) uart.printf("[%8.6f/%8.6f] ", imin*vref/2/1000, imax*vref/2/1000); } } t.stop(); // stop the timer to see how long it took do do this... enableHighRange(); if (!gui) uart.printf("\r\nCurrent = %f A Current Measure Time = %f sec\r\n", tempI, t.read()); } // the autoranging should really be done with functions that return values, as should the // functions below... This would make for shorter and more elegant code, but the author // is a bit of a pasta programmer... void measureHigh(){ float highI=0; enableHighRange(); for (i = 0; i < n; i++){ highI += HIGH_ADC; } highI = highI/n; uart.printf("HIghI = %f A\r\n", vref*highI/0.8); } void measureLow1(){ float low1I=0; enableLow1Range(); for (i = 0; i < n; i++){ low1I += LOW1_ADC; } enableHighRange(); low1I = low1I/n; uart.printf("low1I = %f A\r\n", vref*low1I/0.05/1000); } void measureLow2(){ float low2I=0; enableLow2Range(); for (i = 0; i < n; i++){ low2I += LOW2_ADC; } enableHighRange(); low2I = low2I/n; uart.printf("low2I = %f A\r\n", vref*low2I/2/1000); } // measure the rail voltage, default being with // a divide by 2 resistor divider // It has to be switched out when not in use or it will // add to the measured current, at least in the low ranges... void measureRailV(){ float railv=0; float mult = vref*2; // since divide by 2, we can measure up to 6.6V... float vmin = 5; float vmax = 0; float vtemp; enableRailV(); // switch FETs so divider is connected... for (i = 0; i < n; i++){ vtemp = VRAIL_ADC; // read voltage at divider output... if (statistics && vtemp>vmax) vmax = vtemp; // update max if necessary if (statistics && vtemp<vmin) vmin = vtemp; // update min if necessary railv += vtemp; // add current sample to running sum } disableRailV(); // now disconnect the voltage divider railv = railv/n; // compute average (note this is in normalized ADC [0..1]) // Convert to voltage by multiplying by "mult" if (!gui) uart.printf("RailV = %5.3f V ", mult*railv); if (gui) uart.printf("%5.3f ", mult*railv); if (statistics && gui) uart.printf("[%5.3f/%5.3f] ", mult*vmin, mult*vmax); uart.printf("\r\n"); } // not sure how useful this function is... void measureAll(){ measureHigh(); measureLow1(); measureLow2(); measureRailV(); } // test function to see if trigger pin is being hit... // intended for use later to do timed triggering of measurements... void triggerIn(){ uart.printf("You're triggering me! \r\n"); measureAll(); } // main... int main() { // set up basic conditions... Timer m; uart.baud(115200); enableHighRange(); // default state - only HIGH sense amp in circuit, no divider // signal that we're alive... uart.printf("Hello World!\r\n"); // configure the trigger interrupt... trigger.rise(&triggerIn); while (true) { count++; wait(delay); if (repeat){ // if repeat flag is set, keep making measurements... m.reset(); // reset and start timer... m.start(); measureAuto(); // measuring current using auto-ranging... measureRailV(); // measure rail voltage... m.stop(); // stop the timer. if (!gui) uart.printf(" Total Measure Time = %f sec", m.read()); if (!gui) uart.printf("\r\n\r\n"); } // see if there are any characters in the receive buffer... // this is how we change things on the fly... // Commands (single keystroke... it's easier) // t = one shot automeasure // v = measure volt // h = one shot high measure // k = one shot LOW1 measure // l = one shot LOW2 measure (letter l) // r = toggle repeat // R = turn off repeat // + = faster repeat rate // - = slower repeat rate // = = set repeat rate to 0.25 sec // g = use human readable text output // G = use compressed text format for GUI // s = turn statistics output off // S = turn statistics output on (only in GUI mode) // n = decrease number of averages for each measurement // N = increase number of averages for each measurement // // these were for testing FET switching... // 1 = LOW_ENABLE = 0 (the number 1) // 2 = LOW1 = 0 // 3 = LOW2 = 0 // 4 = VRAIL_MEAS = 0 // ! = LOW_ENABLE = 1 // @ = LOW1 = 1 // # = LOW2 = 1 // $ = VRAIL_MEAS = 1 if (uart.readable()){ temp = uart.getc(); if (temp==(int) 't') { if (!gui) uart.printf("Keyboard trigger: "); measureAuto(); measureRailV(); //measureAll(); } if (temp==(int) 'v') { uart.printf("Keyboard trigger: "); measureRailV(); } if (temp==(int) 'h') { uart.printf("Keyboard trigger: "); measureHigh(); } if (temp==(int) 'k') { uart.printf("Keyboard trigger: "); measureLow1(); } if (temp==(int) 'l') { uart.printf("Keyboard trigger: "); measureLow2(); } if (temp==(int) '1') { LOW_ENABLE = 0; uart.printf("Keyboard trigger: LowEnable = %d\r\n", 0); } if (temp==(int) '2') { LOW1 = 0; uart.printf("Keyboard trigger: LOW1 = %d\r\n", 0); } if (temp==(int) '3') { LOW2 = 0; uart.printf("Keyboard trigger: LOW2 = %d\r\n", 0); } if (temp==(int) '4') { VRAIL_MEAS = 0; uart.printf("Keyboard trigger: VRAILMEAS = %d\r\n", 0); } if (temp==(int) '!') { LOW_ENABLE = 1; uart.printf("Keyboard trigger: LowEnable = %d\r\n", 1); } if (temp==(int) '@') { LOW1 = 1; uart.printf("Keyboard trigger: LOW1 = %d\r\n", 1); } if (temp==(int) '#') { LOW2 = 1; uart.printf("Keyboard trigger: LOW2 = %d\r\n", 1); } if (temp==(int) '$') { VRAIL_MEAS = 1; uart.printf("Keyboard trigger: VRAILMEAS = %d\r\n", 1); } if (temp==(int) 'r') { repeat = !repeat; uart.printf("Keyboard trigger: repeat toggle: %s \r\n", repeat ? "true" : "false"); } if (temp==(int) 'R') repeat = false; if (temp==(int) '+') { delay -= 0.05; if (delay<0.05) delay = 0.05; } if (temp==(int) '-') { delay += 0.05; if (delay>1) delay = 1; } if (temp==(int) '=') delay = 0.25; if (temp==(int) 'g') gui = false; if (temp==(int) 'G') gui = true; if (temp==(int) 's') statistics = false; if (temp==(int) 'S') statistics = true; if (temp==(int) 'n') { n -= 25; if (n<25) n = 25; } if (temp==(int) 'N') { n += 25; if (n>1000) n = 1000; } if (temp==(int) 'N' || temp==(int) 'n') uart.printf("/r/n/r/n Averages = %d \r\n\r\b", n); } } }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍
View full article
Inside IPU there are two block where color space conversion can be made: IC (Image Converter) and DP (Display processor). On Linux, the CSC parameters are located at IPU (IC and DP) drivers, linux/drivers/mxc/ipu3 folder. All negative coefficients are represented using two's complement. Linux Image Converter driver: The parameters are set on function _init_csc: http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/drivers/mxc/ipu3/ipu_ic.c?h=imx_3.14.28_1.0.0_ga static void _init_csc(struct ipu_soc *ipu, uint8_t ic_task, ipu_color_space_t in_format, ipu_color_space_t out_format, int csc_index) { /* * Y = 0.257 * R + 0.504 * G + 0.098 * B + 16; * U = -0.148 * R - 0.291 * G + 0.439 * B + 128; * V = 0.439 * R - 0.368 * G - 0.071 * B + 128; */ static const uint32_t rgb2ycbcr_coeff[4][3] = { {0x0042, 0x0081, 0x0019}, {0x01DA, 0x01B6, 0x0070}, {0x0070, 0x01A2, 0x01EE}, {0x0040, 0x0200, 0x0200}, /* A0, A1, A2 */ }; /* transparent RGB->RGB matrix for combining */ static const uint32_t rgb2rgb_coeff[4][3] = { {0x0080, 0x0000, 0x0000}, {0x0000, 0x0080, 0x0000}, {0x0000, 0x0000, 0x0080}, {0x0000, 0x0000, 0x0000}, /* A0, A1, A2 */ }; /* R = (1.164 * (Y - 16)) + (1.596 * (Cr - 128));   G = (1.164 * (Y - 16)) - (0.392 * (Cb - 128)) - (0.813 * (Cr - 128));   B = (1.164 * (Y - 16)) + (2.017 * (Cb - 128); */ static const uint32_t ycbcr2rgb_coeff[4][3] = { {149, 0, 204}, {149, 462, 408}, {149, 255, 0}, {8192 - 446, 266, 8192 - 554}, /* A0, A1, A2 */ }; ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Linux Display Processor driver: The parameters are set on constants (rgb2ycbcr_coeff and ycbcr2rgb_coeff): http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/drivers/mxc/ipu3/ipu_disp.c?h=imx_3.14.28_1.0.0_ga /* Y = R * 1.200 + G * 2.343 + B * .453 + 0.250;   U = R * -.672 + G * -1.328 + B * 2.000 + 512.250.;   V = R * 2.000 + G * -1.672 + B * -.328 + 512.250.;*/ static const int rgb2ycbcr_coeff[5][3] = { {0x4D, 0x96, 0x1D}, {-0x2B, -0x55, 0x80}, {0x80, -0x6B, -0x15}, {0x0000, 0x0200, 0x0200}, /* B0, B1, B2 */ {0x2, 0x2, 0x2}, /* S0, S1, S2 */ }; /* R = (1.164 * (Y - 16)) + (1.596 * (Cr - 128));   G = (1.164 * (Y - 16)) - (0.392 * (Cb - 128)) - (0.813 * (Cr - 128));   B = (1.164 * (Y - 16)) + (2.017 * (Cb - 128); */ static const int ycbcr2rgb_coeff[5][3] = { {0x095, 0x000, 0x0CC}, {0x095, 0x3CE, 0x398}, {0x095, 0x0FF, 0x000}, {0x3E42, 0x010A, 0x3DD6}, /*B0,B1,B2 */ {0x1, 0x1, 0x1}, /*S0,S1,S2 */ };‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍
View full article
BlueZ5 provides support for the core Bluetooth layers and protocols. It is flexible, efficient and uses a modular implementation. BlueZ5 has implemented the Bluetooth low level host stack for Bluetooth core specification 4.0 and 3.0+HS which includes GAP, L2CAP, RFCOMM, and SDP. Besides the host stack, BlueZ5 has also supported the following profiles itself or via a third party software. Profiles provided by BlueZ: A2DP 1.3 AVRCP 1.5 DI 1.3 HDP 1.0 HID 1.0 PAN 1.0 SPP 1.1 GATT (LE) profiles: PXP 1.0 HTP 1.0 HoG 1.0 TIP 1.0 CSCP 1.0 OBEX based profiles (by obexd): FTP 1.1 OPP 1.1 PBAP 1.1 MAP 1.0 Provided by the oFono project: HFP 1.6 (AG & HF)Supported Profiles BlueZ5 has been supported in the latest Freescale Linux BSP release, so it would be pretty easy to generate the binaries for Bluetooth core stack and its profiles. In order to support A2DP sink on a SabreSD board, the following software should be downloaded and installed onto the target rootfs too. sbc decoder version 1.3 (http://www.kernel.org/pub/linux/bluetooth/sbc-1.3.tar.gz) PulseAudio 5.0 (http://www.freedesktop.org/software/pulseaudio/releases/pulseaudio-5.0.tar.xz) PulseAudio package has some dependencies with bluetooth and sbc packages, and pulseaudio will detect if the two packages have been built and then decide which pulse plugin modules to be generated. So the building order will be 1) bluez5_utils or bluez_utils   2) sbc   3) pulseaudio. After compile and install the above software onto the target rootfs, you should be able to see the following executable under the directory /usr/bin From BlueZ5: bluetoothctl, hciconfig, hciattach (Needed by operating a UART bluetooth module) From PulseAudio: pulseaudio, pactl, paplay If the building dependency has been setup correctly, the following pulse plugin modules should be located under the directory /usr/lib/pulse-5.0/modules module-bluetooth-discover.so      module-bluetooth-policy.so        module-bluez5-device.so   module-bluez5-discover.so Edit the file /etc/dbus-1/system.d/pulseaudio-system.conf, and add the following lines in red: <policy user="pulse">     <allow own="org.pulseaudio.Server"/>    <allow send_destination="org.bluez"/>     <allow send_interface="org.freedesktop.DBus.ObjectManager"/> </policy> Edit the file /etc/dbus-1/system.d/bluetooth.conf, and add the following lines: <policy user="pulse">      <allow send_destination="org.bluez"/>      <allow send_interface="org.freedesktop.DBus.ObjectManager"/> </policy> Adding the following settings at the bottom of the pulseaudio system configuration file which locates in /etc/pulse/system.pa ### Automatically load driver modules for Bluetooth hardware .ifexists module-bluetooth-policy.so load-module module-bluetooth-policy .endif .ifexists module-bluetooth-discover.so load-module module-bluetooth-discover .endif load-module module-switch-on-connect load-module module-alsa-sink device_id=0 tsched=true tsched_buffer_size=1048576 tsched_buffer_watermark=262144 On the system that can automatically detect the alsa cards, the above line #13 should be removed.  Also make sure "auth-anonymous=1" is added to the following line, which can resolve the issue: "Denied access to client with invalid authorization data". load-module module-native-protocol-unix auth-anonymous=1 Selecting a audio re-sampling algorithm and configuring the audio output by adding the following settings to the file daemon.conf locating in /etc/pulse resample-method = trivial enable-remixing = no enable-lfe-remixing = no default-sample-format = s16le default-sample-rate = 48000 alternate-sample-rate = 24000 default-sample-channels = 2 Pulseaudio can be started as a daemon or as a system-wide instance. To run PulseAudio in system-wide mode, the program will automatically drop privileges from "root" and change to the "pulse" user and group. In this case, before launching the program, the "pulse" user and group needs to be created on the target system.  In the example below, "/var/run/pulse" is the home directory for "pulse" user. adduser -h /var/run/pulse pulse addgroup pulse-access adduser pulse pulse-access Because PulseAudio needs to access the sound devices, add the user "pulse" to the "audio" group too. adduser pulse audio Starting bluetoothd and pulseaudio: /usr/libexec/bluetooth/bluetoothd -d & pulseaudio --system --realtime & To verify if the pulseaudio has been set up correctly, you can play a local wave file by using the following command. If you can hear the sound, the system should have been configured correctly. paplay -vvv audio8k16S.wav After setting up the pulseaudio, launch bluetoothctl to pair and connect to a mobile phone. After connecting to a mobile phone, you should be able to see the following information in bluetoothctl console: [bluetooth]# show Controller 12:60:41:7F:03:00         Name: BlueZ 5.21         Alias: BlueZ 5.21         Class: 0x1c0000         Powered: yes         Discoverable: no         Pairable: yes         UUID: PnP Information           (00001200-0000-1000-8000-00805f9b34fb)         UUID: Generic Access Profile    (00001800-0000-1000-8000-00805f9b34fb)         UUID: Generic Attribute Profile (00001801-0000-1000-8000-00805f9b34fb)         UUID: A/V Remote Control        (0000110e-0000-1000-8000-00805f9b34fb)         UUID: A/V Remote Control Target (0000110c-0000-1000-8000-00805f9b34fb)         UUID: Message Notification Se.. (00001133-0000-1000-8000-00805f9b34fb)         UUID: Message Access Server     (00001132-0000-1000-8000-00805f9b34fb)         UUID: Phonebook Access Server   (0000112f-0000-1000-8000-00805f9b34fb)         UUID: IrMC Sync                 (00001104-0000-1000-8000-00805f9b34fb)         UUID: OBEX File Transfer        (00001106-0000-1000-8000-00805f9b34fb)         UUID: OBEX Object Push          (00001105-0000-1000-8000-00805f9b34fb)         UUID: Vendor specific           (00005005-0000-1000-8000-0002ee000001)         UUID: Audio Source              (0000110a-0000-1000-8000-00805f9b34fb)         UUID: Audio Sink                (0000110b-0000-1000-8000-00805f9b34fb)         Modalias: usb:v1D6Bp0246d0515         Discovering: no If you can see the audio sink UUID, you are ready to enjoy the bluetooth music now.
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-344336 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-342877 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-342833 
View full article
L5.4.3_1.0.0 release is now available on IMX_SW landing page: BSP Updates and Releases -> Linux ->Linux L5.4.3_1.0.0. Documentation -> Linux -> Linux 5.4.3_1.0.0 Documentation Files available: # Name Description 1 imx-yocto-LF_L5.4.3_1.0.0.zip i.MX L5.4.3_1.0.0 for Linux BSP Documentation. Includes Release Notes, User Guide. 2 LF_v5.4.y-1.0.0_images_MX6QPDLSOLOX.zip i.MX 6QuadPlus, i.MX 6Quad, i.MX 6DualLite, i.MX 6Solox Linux Binary Demo Files 3 LF_v5.4.y-1.0.0_images_MX6SLLEVK.zip i.MX 6SLL EVK Linux Binary Demo Files 4 LF_v5.4.y-1.0.0_images_MX6UL7D.zip i.MX 6UltraLite EVK, 7Dual SABRESD, 6ULL EVK Linux Binary Demo Files 5 LF_v5.4.y-1.0.0_images_MX7ULPEVK.zip i.MX 7ULP EVK Linux Binary Demo Files  6 LF_v5.4.y-1.0.0_images_MX8MMEVK.zip i.MX 8M Mini EVK Linux Binary Demo Files  7 LF_v5.4.y-1.0.0_images_MX8MNEVK.zip i.MX 8M Nano EVK Linux Binary Demo Files  8 LF_v5.4.y-1.0.0_images_MX8MQEVK.zip i.MX 8M Quad EVK Linux Binary Demo files 9 LF_v5.4.y-1.0.0_images_MX8QMMEK.zip i.MX 8QMax MEK Linux Binary Demo files 10 LF_v5.4.y-1.0.0_images_MX8QXPMEK.zip i.MX 8QXPlus MEK Linux Binary Demo files 11 imx-scfw-porting-kit-1.2.10.1.tar.gz System Controller Firmware (SCFW) porting kit v1.2.10.1 for L5.4.3_1.0.0   Target board: MX 8 Series MX 8QuadXPlus MEK Board MX 8QuadMax MEK Board MX 8M Quad EVK Board MX 8M Mini EVK Board MX 8M Nano EVK Board MX 7 Series MX 7Dual SABRE-SD Board MX 7ULP EVK Board MX 6 Series MX 6QuadPlus SABRE-SD and SABRE-AI Boards MX 6Quad SABRE-SD and SABRE-AI Boards MX 6DualLite SDP SABRE-SD and SABRE-AI Boards MX 6SoloX SABRE-SD MX 6UltraLite EVK Board MX 6ULL EVK Board MX 6ULZ EVK Board MX 6SLL EVK Board   What’s New/Features: Please consult the Release Notes.   Known Issues: For known issues and more details please consult the Release Notes.   More information on changes of Yocto, see: README: https://source.codeaurora.org/external/imx/imx-manifest/tree/README?h=imx-linux-zeus ChangeLog: https://source.codeaurora.org/external/imx/imx-manifest/tree/ChangeLog?h=imx-linux-zeus      
View full article
[中文翻译版] 见附件   原文链接: i.MX Create Android SDCard Mirror 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343079 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343116 
View full article
[中文翻译版] 见附件   原文链接: Guide to flash an eMMC from SD Card on i.MX6Q SABRE-SD 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343344 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343372 
View full article