ワイヤレス接続に関するナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Wireless Connectivity Knowledge Base

ディスカッション

ソート順:
In developing a Zigbee application, certain static configuration is required before the application is built. Configuring the network size, adding a new cluster, making the device discoverable and adding a new endpoint can be done by changing parameters in the following files: app_zps_cfg.h app_zcl_cfg.h app_zcl_global.c These files are responsible for setting up network parameters like device type and associated parameters, mainly related to the APS and NWK layers of the ZigBee PRO stack. Network Configuration The ZigBee device can be configured to be a coordinator, router and end device. The following section details the way in which the user can configure each device type. The app_zps_cfg header file lets the user configure the ZPS ZDO parameters of the node. The following macros are necessary for the corresponding device types: For coordinator in a ZigBee network #define ZPS_COORDINATOR #define ZPS_ZDO_DEVICE_TYPE                              ZPS_ZDO_DEVICE_COORD For router in a ZigBee network #define ZPS_ROUTER #define ZPS_ZDO_DEVICE_TYPE                              ZPS_ZDO_DEVICE_ROUTER For enddevice in a ZigBee network #define ZPS_ENDDEVICE #define ZPS_ZDO_DEVICE_TYPE                              ZPS_ZDO_DEVICE_ENDDEVICE Other ZPS ZDO configurations which are defined using macro are explained in comments inside the header file (app_zps_cfg.h). These macros provide the user with the ability to configure the device according to their network needs. The type of security for the ZigBee network can also be configured by the macro ZPS_ZDO_NWK_KEY_STATE. The user can change the security type to no network security (ZPS_ZDO_NO_NETWORK_KEY), pre-configured link key security (ZPS_ZDO_PRECONFIGURED_LINK_KEY), distributed link key security (ZPS_ZDO_DISTRIBUTED_LINK_KEY) or pre-configured installation code security (ZPS_ZDO_PRCONFIGURED_INSTALLATION_CODE). /* Specify No network Security */ #define ZPS_ZDO_NWK_KEY_STATE                               ZPS_ZDO_NO_NETWORK_KEY The application allows through this header file to configure ZPS APS AIB parameters, like extended PANID (ZPS_APS_AIB_INIT_USE_EXTENDED_PANID) or channel mask (ZPS_APS_AIB_INIT_CHANNEL_MASK). /* NWK EXTENDED PANID (EPID) that the device will use.*/ #define ZPS_APS_AIB_INIT_USE_EXTENDED_PANID                 0x0000000000000000ULL /*! CHANNEL MASK : Define all channels from 11 to 26*/ #define ZPS_APS_AIB_INIT_CHANNEL_MASK                       0x07fff800UL User can also configure the simple descriptor table size (AF_SIMPLE_DESCRIPTOR_TABLE_SIZE) as part of the ZPS AF Layer configuration parameters.The value depends on number of endpoints defined in application, one endpoint is always reserved for ZDO . So, for a device with one endpoint, the value would be 2 (1 ZDO + 1 application endpoint) #define AF_SIMPLE_DESCRIPTOR_TABLE_SIZE                     2 Among other ZPS network configuration parameters that can be changed by the user are scan duration (ZPS_SCAN_DURATION), default permit joining time (ZPS_DEFAULT_PERMIT_JOINING_TIME) and the maximum number of simultaneous key requests (ZPS_MAX_NUM_SIMULTANEOUS_REQUEST_KEY_REQS). Also, NIB values can be changed, like for example, the maximum number of routers in the network (ZPS_NWK_NIB_INIT_MAX_ROUTERS), the maximum number of children for a node (ZPS_NWK_NIB_INIT_MAX_CHILDREN), the maximum network depth (ZPS_NWK_NIB_INIT_MAX_DEPTH) or the network security level (ZPS_NWK_NIB_INIT_SECURITY_LEVEL). Different ZigBee network table sizes can be adjusted by the user from this header file. The important tables are mentioned below: The active neighbor table size (ZPS_NEIGHBOUR_TABLE_SIZE). The neighbor discovery table size, used to keep a list of the neighboring devices associated with the node (ZPS_NEIGHBOUR_DISCOVERY_TABLE_SIZE). The network address map table size, which represents the size of the address map that maps 64-bit IEEE addresses to 16-bit network (short) addresses (ZPS_ADDRESS_MAP_TABLE_SIZE). The network security material set size (ZPS_SECURITY_MATERIAL_SETS). The broadcast transaction table size, which stores the records of the broadcast messages received by the node (ZPS_BROADCAST_TRANSACTION_TABLE_SIZE). The route record table size (ZPS_ROUTE_RECORD_TABLE_SIZE) for the table that records each route, storing the destination network address, a count of the number of relay nodes to reach the destination and a list of the network addresses of the relay nodes. The route discovery table size (ZPS_ROUTE_DISCOVERY_TABLE_SIZE), used by the node to store temporary information used during route discovery. The MAC address table size (ZPS_MAC_ADDRESS_TABLE_SIZE). The binding table size (ZPS_BINDING_TABLE_SIZE). The group table size (ZPS_GROUP_TABLE_SIZE). The number of supported network keys, known also as the security material sets (ZPS_KEY_TABLE_SIZE). The child table size (ZPS_CHILD_TABLE_SIZE), that gives the size of the persisted sub-table of the active neighbor table. The stored entries are for the node’s parent and immediate children. The trust center device table size (ZPS_TRUST_CENTER_DEVICE_TABLE_SIZE). ZCL Configuration The app_zcl_cfg header file is used by the application to configure the ZigBee Cluster library. This file contains the definition for the application profile and cluster ids. The default application profiles are ZDP, HA, ZLO, GP. The ZDP (ZigBee Device Profile) id is identified by the following line: #define ZDP_PROFILE_ID             (0x0000) ZDP provides services for the following categories as cluster Ids: Device discovery services (for example, ZDP_DISCOVERY_CACHE_REQ_CLUSTER_ID) Service discovery services (for example, ZDP_IEEE_ADDR_REQ_CLUSTER_ID) Binding services (for example, ZDP_BIND_RSP_CLUSTER_ID) Management services (for example, ZDP_MGMT_NWK_DISC_REQ_CLUSTER_ID) The HA (Home Automation) profile id is identified by the following line: #define HA_PROFILE_ID             (0x0104) HA provides services for the following categories as cluster Ids: Generic devices (for example, HA_BASIC_CLUSTER_ID) Lighting devices (for example, HA_LEVELCONTROL_CLUSTER_ID) Intruder Alarm System (IAS) devices (for example, HA_IASZONE_CLUSTER_ID) The ZLO (ZigBee Lighting and Occupancy) profile is not an application profile but devices in this collection use the same application profile id as for the Home Automation application profile. This ensures backward compatibility with applications for devices based on the Home Automation 1.2 profile. ZigBee Green Power (GP) is an optional cluster with the aim of minimizing the power demands on a network node in order to support: Nodes that are completely self-powered through energy harvesting Battery-powered nodes that require ultra-long battery life The GP profile id is identified by the following line: #define GP_PROFILE_ID               (0xa1e0) The Zigbee GP cluster ID is defined as following: #define GP_GREENPOWER_CLUSTER_ID    (0x0021) Depending on the application, the app_zcl_cfg header file also contains the defines for the node endpoints. For example, the occupancy_sensor application contains the following endpoints: /* Node 'Coordinator' */ /* Endpoints */ #define COORDINATOR_ZDO_ENDPOINT    (0) #define COORDINATOR_COORD_ENDPOINT    (1) /* Node 'OccupancySensor' */ /* Endpoints */ #define OCCUPANCYSENSOR_ZDO_ENDPOINT    (0) #define OCCUPANCYSENSOR_SENSOR_ENDPOINT    (1)   /* Node 'LightSensor' */ /* Endpoints */ #define LIGHTSENSOR_ZDO_ENDPOINT    (0) #define LIGHTSENSOR_SENSOR_ENDPOINT    (1)   /* Node 'LightTemperatureOccupancySensor' */ /* Endpoints */ #define LIGHTTEMPERATUREOCCUPANCYSENSOR_ZDO_ENDPOINT    (0) #define LIGHTTEMPERATUREOCCUPANCYSENSOR_SENSOR_ENDPOINT    (1) The source file app_zcl_globals.c is used to declare the cluster lists for each endpoint. These act as simple descriptors for the node. Each endpoint has two cluster lists, containing uint16_t data. One is for input and one for output. The sizes of these two lists must be equal. For example, for endpoint 0, the declared lists will be the following: PRIVATE const uint16 s_au16Endpoint0InputClusterList[16]  =  { 0x0000, 0x0001, 0x0002, 0x0003, 0x0004, 0x0005, 0x0006 , 0x0007, \                                                               0x0008, 0x0010, 0x0011, 0x0012, 0x0012, 0x0013, 0x0014 , 0x0015}; PRIVATE const uint16 s_au16Endpoint0OutputClusterList[16] = { 0x0000, 0x0001, 0x0002, 0x0003, 0x0004, 0x0005, 0x0006 , 0x0007, \                                                              0x0008, 0x0010, 0x0011, 0x0012, 0x0012, 0x0013, 0x0014 , 0x0015}; The input list must also have a corresponding cluster APDU list, matching in size. For the endpoint 0 example, this will look like: PRIVATE const PDUM_thAPdu s_ahEndpoint0InputClusterAPdus[16] = { apduZDP, apduZDP, apduZDP, apduZDP, apduZDP, apduZDP, apduZDP, apduZDP,\                                                                  apduZDP, apduZDP, apduZDP, apduZDP, apduZDP, apduZDP, apduZDP, apduZDP}; Each output and input cluster list has a corresponding cluster discovery enabled flags list. As each bit inside the Cluster Disc Flag corresponds to cluster , for 16 clusters declared in Input and Output cluster list, one needs 2 bytes for Discoverable flag. In this example, the declaration is the following: PRIVATE uint8 s_au8Endpoint0InputClusterDiscFlags[2] = {0x1F, 0x08}; PRIVATE uint8 s_au8Endpoint0OutputClusterDiscFlags[2] = {0x08, 0x1B}; These parameters are registered in the node’s endpoints simple descriptor structure. The declared variable for the structure is s_asSimpleDescConts and its size depends on the number of endpoints available on the node. For example, for two endpoints, the declaration will be as below: PUBLIC zps_tsAplAfSimpleDescCont s_asSimpleDescConts[2] = {     {         {             0x0000,             0,             0,             0,             84,             84,             s_au16Endpoint0InputClusterList,             s_au16Endpoint0OutputClusterList,             s_au8Endpoint0InputClusterDiscFlags,             s_au8Endpoint0OutputClusterDiscFlags,         },         s_ahEndpoint0InputClusterAPdus,         1     },     {         {             0x0104,             0,             0,             1,             6,             4,             s_au16Endpoint1InputClusterList,             s_au16Endpoint1OutputClusterList,             s_au8Endpoint1InputClusterDiscFlags,             s_au8Endpoint1OutputClusterDiscFlags,         },         s_ahEndpoint1InputClusterAPdus,         1     }, }; The AF Context definition is as below: typedef struct _zps_tsAplAfSimpleDescCont {     ZPS_tsAplAfSimpleDescriptor sSimpleDesc;     const PDUM_thAPdu *phAPduInClusters;     bool_t bEnabled; } zps_tsAplAfSimpleDescCont; And the endpoint simple descriptor has the following structure definition: typedef struct {     uint16 u16ApplicationProfileId;     uint16 u16DeviceId;     uint8  u8DeviceVersion;     uint8  u8Endpoint;     uint8  u8InClusterCount;     uint8  u8OutClusterCount;     const uint16 *pu16InClusterList;     const uint16 *pu16OutClusterList;     uint8 *au8InDiscoveryEnabledFlags;     uint8 *au8OutDiscoveryEnabledFlags; } ZPS_tsAplAfSimpleDescriptor;
記事全体を表示
Introduction This document is a quick start guide to load a new software image in a KW36 device through FSCI (Freescale Serial Communication Interface) bootloader software. Also, it contains all the steps needed to install the software required in a Windows host to handle the FSCI communication protocol. Software Requirements IAR Embedded Workbench IDE or MCUXpresso IDE. FRDM-KW36 SDK. Hardware Requirements FRDM-KW36 board. Downloading the SDK When downloading the SDK, select your specific IDE or simply choose all toolchains as shown below. In the option "Add software component", ensure to select all middleware components as depicted below. Installing FSCI Host in Windows OS The host software for the Windows OS was designed to work in a Python environment. The following steps are to download and install the software needed to use FSCI in a Windows OS. Visit the Python web site and download the latest Python 2.7.x MSI installer package for Windows OS. Open the MSI installer package. When customizing the installation options, check "Add python.exe to Path" as shown below Complete the rest of the steps for the Python installation process. Unzip the FRDM-KW36 SDK. Depending on your Python environment architecture, copy the HSDK.dll from <SDK_root>\tools\wireless\host_sdk\sdk-python\lib\<x86_or_x64> to <Python_directory>\DLLs (default in C:\Python27\DLLs). Download and install Visual C++ Redistributable Packages for Microsoft Visual Studio 2013 depending on the Windows architecture (vcredist_x86.exe or vcredist_x64.exe) from the Microsoft web site. Download and install the Microsoft Visual C++ Compiler for Python 2.7 from the following web site. To run Python scripts from the Command Prompt of Windows, we must create a system variable named PYTHONPATH. Search “System” in the Windows browser. Go to Advanced system settings -> Environment Variables… -> System variables. Click on the “New…” button and create the PYTHONPATH variable with the following value: <SDK_root>\tools\wireless\host_sdk\hsdk-python\src. Programming the FSCI bootloader on FRDM-KW36 board Attach the FRDM-KW36 board to your PC. Drag and drop the “bootloader_fsci_frdmkw36.bin” from the previously unzipped SDK file, you can find this file in: <SDK_root>\tools\wireless\binaries to your board. Like a common USB device. Creating a binary image to reprogram the device   IAR Embedded Workbench Open the connectivity project that you want to program through the FSCI bootloader from your SDK. This example will make use of the heart rate sensor project, located at the following path: <SDK_root>\boards\frdmkw36\wireless_examples\bluetooth\hrs\freertos\iar\hrs_freertos.eww. Open the project options window (Alt+F7). In Linker -> Config window, edit the “Configuration file symbol definitions” add the “gUseBootloaderLink_d=1” linker flag as shown below. Go to the “Output Converter” window and ensure that the output file is in binary format (.bin), otherwise, deselect the “Override default” checkbox, expand the “Output format” combo box and select “Raw binary. Click the OK button. Rebuild the project. The binary will be saved at: <SDK_root>\boards\frdmkw36\wireless_examples\bluetooth\hrs\freertos\iar\debug   MCUXpresso IDE Import your FRDM-KW36 SDK to MCUXpresso. Drag and drop your SDK on the "installed SDK's" toolbar. (In this step, it is not necessary to unzip the package). Open any connectivity project that you want to program through the FSCI bootloader from your SDK. This example will make use of the heart rate sensor project. Go to Project -> Properties, a new window will appear. Then, open the C/C++ Build -> Settings -> Linker -> Miscellaneous. Press the icon below, a new window will be deployed. Add “--defsym=gUseBootloaderLink_d=1”. Click on “Apply and Close”. Build the project. Deploy the “Binaries” icon in the workspace. Click the right mouse button on the “.axf” file. Select “Binary Utilities -> Create binary” option. The binary file will be saved at “Debug” folder in the workspace with “.bin” extension. Reprogramming an FRDM-KW36 board using the FSCI bootloader The following steps are to test the FSCI bootloader in a Windows OS. Search "Command Prompt" in the Windows browser. Run the "fsci_bootloader.py" Python script. Type the “python.exe” path in the console (default C:\Python27\python.exe). Drag and drop the “fsci_bootloader.py” from: <SDK_root>\tools\wireless\host_sdk\hsdk-python\src\com\nxp\wireless_connectivity\test\bootloader on the command prompt screen. Search the COM Port of your FRDM-KW36 board and type in the console. You can find it typing ‘Device manager’ from windows home and then search it in Ports (COM & LPT) toolbar. As you can see in this example the port may change depending on each case. Search the binary image file (created in the last section). Drag and drop on the screen. Press “Enter” to start the firmware update trough FSCI bootloader. Automatically the KW36 device will trigger to run the new software. To see all your process running, you can download the ‘IoT Toolbox’ from the app store to your smartphone and connect your device with the board to verify the random data that the heart rate sensor example generates.
記事全体を表示
Introduction This document provides guidance to load a new software image in a KW35 device through OTAP (Over The Air Programming) bootloader for KW35. This article also provides the steps needed to download and install the SDK used in the tutorial. Software Requirements IAR Embedded Workbench IDE or MCUXpresso IDE. SDK MKW36A512xxx4 RC4 or further. Hardware Requirements MKW35A512xxx4 device. KW35 Flash Memory Used for the OTAP Software Deployment The KW35 Flash is partitioned into: 2x256 KB Program Flash (P-Flash) array divided into 2 KB sectors with a flash address range from 0x0000_0000 to 0x0007_FFFF.     The statements to comprehend how the OTAP Client software and his features works are: The OTAP Client software is split into two parts, the OTAP bootloader and the OTAP client service. The OTAP bootloader verifies if there is a new image already available to reprogram the device. The OTAP client service software provides the Bluetooth LE custom services needed to communicate with the server that contains the new image file. Therefore, before to start the test, the device has been programmed twice, first with the OTAP bootloader then with the OTAP client service project. The mechanism used to have two different software in the same device is to store each one in different memory regions and this is implemented by the linker file. In the KW35 device, the bootloader application has reserved a 16KB slot of memory starting from the 0x0 address (0x0 to 0x3FFF) thus, the left memory of the first P-Flash memory bank is reserved, among other things, by the OTAP client service application.   To create a new image file for the client device, the developer needs to specify to the linker file that the code will be stored with an offset of 16KB since the first addresses are reserved for the bootloader. At connection event, the server sends all the chunks of code to the client via Bluetooth LE. The client stores the code at the second P-Flash memory bank but is not able to run yet.   When the broadcast has finished, and all chunks were sent, the OTAP bootloader detects this situation and triggers a command to reprogram the device with the new application. Due the new application was built with an offset of 16KB, the OTAP bootloader program the device starting from the 0x3FFF address and the OTAP client service application is overwritten by the new image. Then the OTAP bootloader triggers the new application, starting the execution of the code.   Software Development Kit download and install   Go to MCUXpresso web page. Log in with your registered account. Search for “MKW36A” device. Then click on the suggested processor and click on “Build MCUXpresso SDK” The next page is displayed. Select “All toolchains” in the “Toolchain / IDE” combo box and provide the name to identify the package. Click on “Add software component”, then deploy the combo box and click on “Select All” option. Save the changes. Click on “Download SDK” button and accept the license agreement. If MCUXpresso IDE is used, drag and drop the SDK zip folder in “Installed SDK’s” perspective to install the package.     Preparing the software to test the OTAP for KW35 device using IAR Embedded Workbench   This section provides the steps needed to test the OTAP software on the KW35. Program the OTAP bootloader on the KW35. 1.1 Open the OTAP_bootloader project located at the following path: <SDK_download_root>\boards\virtual-board-kw35\wireless_examples\framework\bootloader_otap\bm\iar\bootloader_otap_bm.eww     1.2 Flash the project (Ctrl + D). Stop the debug session (Ctrl + Shift + D). Program the OTAP client application on the KW35.         2.1 Open the OTAP client project located in the path below.          <SDK_download_root>\boards\frdmkw36\wireless_examples\bluetooth\otac_att\freertos\iar\otac_att_freertos.eww          2.2 Follow the steps 2 to 12 described in the “4.1. Changes Required in Project Options and Settings” section of the AN12252 “Migration Guide from               MKW36Z512xxx4 to MKW35Z512xxx4” application note.            2.3 Open the app_preinclude.h file under the source directory in the workspace. Find the “gEepromType_d” definition and update the value to                                 “gEepromDevice_InternalFlash_c” as shown below.   #define gEepromType_d gEepromDevice_InternalFlash_c‍‍‍‍‍            2.4 Save the MKW35Z512xxx4_connectivity.icf file located at:                <SDK_download_root>\middleware\wireless\framework_5.4.4\Common\devices\MKW35Z4\iar                               Into the folder of the OTAP Client ATT project:                <SDK_download_root>\boards\frdmkw36\wireless_examples\bluetooth\otac_att\freertos\iar            2.5 Open the project options window (Alt+F7). In Linker/Config window click the icon next to linker path and select the linker configuration file “MKW35Z512xxx4_connectivity.icf”. Set the "gUseInternalStorageLink_d” flag to 1.              2.6 Click the OK button in the project options window to save the new configuration.          2.7 Flash the project (Ctrl + D). Stop the debug session (Ctrl + Shift + D).    Preparing the software to test the OTAP for KW35 device using MCUXpresso IDE   This section provides the steps needed to test the OTAP software on the KW35. Program the OTAP bootloader on the KW35.          1.1 Open MCUXpresso IDE. Click on “Import SDK example(s)” option in the “Quickstart Panel” view.                        1.2 Click on virtual-board-kw35 SDK icon.          1.3 Deploy the wireless_examples\framework\bootloader_otap folders and select bm project. Click Finish button.                                                                           1.4 Select “Debug” option in the Quickstart Panel. Once the project is already loaded on the device, stop the debug session.      2. Program the OTAP client application on the KW35.          2.1 Open MCUXpresso IDE. Click on “Import SDK example(s)” option in the “Quickstart Panel” view.                          2.2 Click twice on the frdmkw36 icon.                                                                            2.3 Type “otac_att” in the examples textbox and select the freertos project at wireless_examples\bluetooth\otac_att\freertos. Finally, click on Finish button.              2.4 Follow the steps 5 to 17 described in the “5.1. Changes Required in Project Options and Settings” section of the AN12252 “Migration Guide from MKW36Z512xxx4 to MKW35Z512xxx4” application note.            2.5. Open the app_preinclude.h file under the source directory in the workspace. Find the “gEepromType_d” definition and update the value to                “gEepromDevice_InternalFlash_c” as shown below. #define gEepromType_d gEepromDevice_InternalFlash_c‍‍‍‍‍            2.6 Save the MKW35Z512xxx4_connectivity.ld file located at:                <SDK_download_root>\middleware\wireless\framework_5.4.4\Common\devices\MKW35Z4\gcc                Into the source folder in the workspace.              2.7 Open the Project/Properties window. Next, go to the MCU Linker/Managed Linker Script perspective and edit the Linker Script name to “MKW35Z512xxx4_connectivity.ld”.              2.8 Go to MCU Linker/Miscellaneous view. Press the icon below, a new window will be deployed. Add the following definition in the “Other options” box: --defsym=gUseInternalStorageLink_d=1.              2.9 Click the “Apply and Close” button in the project options window to save the new configuration.          2.10 Select “Debug” option in the Quickstart Panel. Once the project is already loaded on the device, stop the debug session.   Running OTAP demo with the IoT Toolbox App Save the S-Record file created with the steps in Appendix A or Appendix B in your smartphone at a known location. Open the IoT Toolbox App and select OTAP demo. Press “SCAN” to start scanning for a suitable advertiser. Perform a falling edge on the PTB18 in the KW35 to start advertising. Create a connection with the founded device. Press “Open” and search the S-Record file. Press “Upload” to start the transfer. Once the transfer is complete, wait a few seconds until the bootloader has finished programming the new image. The new application will start automatically.    Appendix A. Creating an S-Record image file for KW35 client using IAR Embedded Workbench Open the connectivity project that you want to program using the OTAP bootloader from your SDK. This example will make use of the glucose sensor project. <SDK_download_root>\boards\frdmkw36\wireless_examples\bluetooth\glucose_s\freertos\iar\glucose_s_freertos.eww Follow the steps 2 to 12 described in the “4.1. Changes Required in Project Options and Settings” section of the AN12252 “Migration Guide from              MKW36Z512xxx4 to MKW35Z512xxx4” application note. Save the MKW35Z512xxx4_connectivity.icf file located at: <SDK_download_root>\middleware\wireless\framework_5.4.4\Common\devices\MKW35Z4\iar                In the containing folder of your project. <SDK_download_root>\boards\frdmkw36\wireless_examples\bluetooth\glucose_s\freertos\iar Open the project options window (Alt+F7). In Linker/Config window click the icon next to linker path and select the linker configuration file MKW35Z512xxx4_connectivity.icf. Then, enable “gUseBootloaderLink_d” macro in the “Configuration file symbol definitions” textbox. Go to the “Output Converter” window. Deselect the “Override default" checkbox, expand the “Output format” combo box and select Motorola S-records format. Click OK button.                                                                                                                                           Rebuild the project. Search the S-Record file in the following path: <SDK_download_root>\boards\frdmkw36\wireless_examples\bluetooth\glucose_s\freertos\iar\debug   Appendix B. Creating an S-Record image file for KW35 client using MCUXpresso IDE Open the connectivity project that you want to program using the OTAP bootloader from MCUXpresso IDE This example will make use of the glucose sensor project Follow the steps 5 to 17 described in the “5.1. Changes Required in Project Options and Settings” section of the AN12252 “Migration Guide from MKW36Z512xxx4 to MKW35Z512xxx4” application note. Save the MKW35Z512xxx4_connectivity.ld file located at: <SDK_download_root>\middleware\wireless\framework_5.4.4\Common\devices\MKW35Z4\gcc Into the source folder in the workspace.                                                                                                                  Open the Project/Properties window. Next, go to the MCU Linker/Managed Linker Script perspective and edit the Linker Script name to “MKW35Z512xxx4_connectivity.ld”.                                                                                  Go to MCU Linker/Miscellaneous view. Press the icon below, a new window will be deployed. Add the following definition in the “Other options” box: --defsym=gUseBootloaderLink_d=1. Click the “Apply and Close” button.                              Build the project. Deploy the “Binaries” icon in the workspace. Click the right mouse button on the “.axf” file. Select “Binary Utilities/Create S-Record” option. The S-Record file will be saved at “Debug” folder in the workspace with “.s19” extension.  
記事全体を表示
The “BeyondStudio for NXP” Integrated Development Environment (IDE) provides a platform for the development of wireless network applications to be run on NXP’s JN516x family of wireless microcontrollers. For more details and installation guide.  JN-UG-3098 (BeyondStudio for NXP Installation and User Guide). This document explains the common issues that the user will face when trying to develop a new application using BeyondStudio IDE.   First of all, be sure that you are working with the latest SDK version and application note.    Import Problems After you import some application note that you want to take as reference. 2.2 Importing a Project. BeyondStudio for NXP Installation and User Guide.     1. Wrong Path A  common issue is a user uses another path for the installation of the SDK than the default one (C:\nxp\bstudio_nxp\workspace). When trying to find the Makefile ("SDK/JN-SW-4168/Stack/Common/Build/config.mk"), the IDE uses a relative path, for that reason it assumes that the file is in the correct directory. As the path was changed, the file can’t be found.   2.Project Directory After you select the Application Note (AN) you want to import remember that there will be an option for the JN517x as most of the projects are compatible between them (Zigbee 3.0, ZigBee Link Light). Nonetheless, BeyondStudio is not compatible with the JN517x.  While importing the project you only must select the JN516x project and none of the options must not be selected.     Linking Errors Open a source file (.c) or a header file (.h),  you will notice that the IDE shows a lot of errors even though the project has not been compiled yet. The errors you are seeing is Eclipse not being able to resolve various variables and functions within the SDK. You might see some errors like: Symbol “xxx” could not be resolved for example. After starting the compilation process, look at the console log and notice that the bin file is being generated correctly. Do not try to add another file in the path and Symbols trying to avoid all those errors; the IDE will look for the includes that the project needs. If you used the default path location, it will not have any problem with the compilation. The OS_Gen, ZPS_Gen, and PDUM_Gen, for example, are all files automatically generated based on the configuration files, performing a clean will remove those files but will be created again after a new compilation. File app.zpscfg Problems Encountered The next error will appear if the Zigbee Plug-in is not installed. Follow the installation procedure for the plug-ins 1.2.3 Installing the ZigBee Plug-ins BeyondStudio for NXP Installation and User Guide. Look at the installation folder that is included in the SDK. C:\NXP\bstudio_nxp\sdk\JN-SW-41xx\Tools\Eclipse_plugins\com.nxp.sdk.update_site For a better reference the ZPS Configuration Editor provides a convenient way to set ZigBee network parameters ZigBee PRO Stack User Guide I hope it helps. Regards, Mario
記事全体を表示
The attached PDF file contains two A3 format "posters". The first one summarize the contents of the SMP Pairing Request and SMP Pairing Response packets (BLE 4.2). It shows how are the sub-fields of these packets set and what do they represent. The second one contains a diagram which summarizes how the pairing method and it's properties are determined during the SMP Pairing procedure for both BLE Legacy Pairing (BLE4.0 and BLE 4.1) and BLE Secure Connections Pairing with ECDH (BLE 4.2). Some of the tables in the diagram are taken from the BLE Specification. If you find any errors or have any suggestions of improvement please leave a comment or send me a message. Preview:
記事全体を表示
General summary MCUBOOT, fsci_bootloader and otap_bootloader are 3 different bootloader applications that can be used depending on the use case. The MCU Flashloader is a separate implementation but it's also mentioned to avoid misunderstanding.   MCUBOOT The MCU bootloader provides support for multiple communication protocols (UART, SPI, I2C, CAN) and multiple applications to interface with it. Summary: - It's a configurable flash programming utility that operates over a serial connection on several Kinetis MCUs. - Host-side command line (blhost) and GUI tools are available to communicate with the bootloader.  -  By default, application starts at address 0xa000. - MCU Bootloader|NXP website - MCU Bootloader Reference Manual - MCU Bootloader Demo Application User's Guide   fsci_bootloader Framework Serial Connectivity Interface (FSCI) is an NXP propietary protocol that allows interfacing the Kinetis protocol stack with a host system or PC tool using a serial communication interface. The FSCI bootloader enables the FSCI module to communicate with the PC and transfer the image using the FSCI protocol. Summary: - It relies on the FSCI protocol to transfer the binary from a PC connected via UART, using a python and C applications. - To enter into bootloader mode (in FRDM-KW41Z), hold SW1 (Reset) and press SW4, then release SW1 first and SW4 second. Please refer to demo user's guide to get the specific steps for your platform. - By default, application starts at 0x4000. - FSCI Bootloader Manual   otap_bootloader The Connectivity SDK contains Over-the-Air firmware upgrade examples. The OTAP bootloader loads an image obtained from wireless communication, the OTAP bootloader only enters after an image was successfully transferred to the client device (internal or external flash). Summary: - It's used by over the air programmed devices. - The bootloader mode only enters if a flag is set after reset triggered by a successful reception of an image over the air. - By default, application starts at 0x4000. - Kinetis Thread Stack Over-the-Air (OTA) Firmware Update User’s Guide   mcu_flashloader The MCU flashloader is a specific implementation of the MCU bootloader. For the flashloader implementation, the MCU bootloader command interface is packaged as an executable that is loaded from flash and executed from RAM. This configuration allows the user application to be placed at the beginning of the on-chip flash where it is automatically launched upon boot from flash. Using the MCU flashloader to program a user application to the beginning of the flash makes this implementation of the bootloader a one-time programming aid. The MCU flashloader doesn't allow to jump to a different section after a timeout or button press like the other bootloaders, it's main purpose is to flash an application without the need of an external debugger, mainly used for factory programming. Summary: - It is pre-programmed into many Kinetis flash devices during manufacturing and enables flash programming without the need for a debugger. - After the user application is programmed into flash memory, the Kinetis flashloader is no longer available. - Documentation: Getting Started with the MCU Flashloader   You can select from the MCU Bootloader, FSCI_Bootloader and OTAP Bootloader, depending on your needs. JC
記事全体を表示
This Application Note provides guidance on migrating ZigBee 3.0 Base device application designed for the NXP JN516x wireless microcontrollers to the KW41Z with the help of attached PDF.
記事全体を表示
       My customer asks if QN9080 can be tested with MT887x. We co-work with Anritsu Taiwan to integrate QN9080 and MT887x to perform 1M bps, 2M bps and Frame error rate test. This document will address the QN9080 setup and MT887x connection setup. We show the 1M bps, 2M bps and frame error rate results. The Anritsu equipment is applied to MT8870, MT8872 model name.        If you would like to perform the same test environment. You may contact Anritsu to get the latest "Auto-test tool " released by Anritsu and follow their SOP document to install "Auto-test tool" into PC to perform this RF validation test. 
記事全体を表示
BeeStack solutions included in BeeKit contain several low level drivers that definitely ease customer’s development phase.  Ranging from UART, SPI, NVM, I2C, among many others, these drivers could be used to interface the MW2x devices with different devices or sensors. It is also true these drivers will not support all custom applications by default, but they are conveniently provided in source code so anyone can modify them to the application’s needs. One example would be the need to use an accelerometer such as FXOS8700 or MMA8451. In this case, the default functionality of the I2C drivers might not be well-suited to work with these devices out-of-the-box. Nevertheless, this could be achieved with simple modifications to the source code. This project implements the basic I2C functionality to interface a TWR-KW24D512 board with a FXOS8700 sensor using the drivers included in Kinetis BeeStack Codebase 4.0.x solutions. The demo uses a ZigBee Home Automation GenericApp template to initialize and periodically read the accelerometer data X, Y and Z. A change in the registers read and written would be enough to use MMA8451 instead.  Following images illustrate the I2C frames obtained from the analyzer: FXOS8700 Initialization: Accelerometer X-Axis Data: Accelerometer Y-Axis Data: Accelerometer Z-Axis Data: IMPORTANT NOTE: Support of the attached project is limited. Please use this project as reference only. If it does not fulfill your requirements, you could always modify its source code to meet you application’s needs.
記事全体を表示
This document describes how to add additional endpoints to the Router application in the AN12061-MKW41Z-AN-Zigbee-3-0-Base-Device Application Note.   The Router application's main endpoint acts as a light controlled by the On/Off cluster acting as a Server. The steps below describe how to add two new endpoints with On/Off clusters acting as clients.   Note that these changes only go as far as making the new endpoints discoverable, no functionality has been added to read inputs and transmit commands from the new endpoints. Router/app_zcl_cfg.h The first step is to add the new endpoints (Switch1, Switch2) into ZCL configuration file. /* Endpoints */ #define ROUTER_ZDO_ENDPOINT         (0) #define ROUTER_APPLICATION_ENDPOINT (1) #define ROUTER_SWITCH1_ENDPOINT     (2) #define ROUTER_SWITCH2_ENDPOINT     (3) Router/app_zps_cfg.h The second step is to update the ZigBee Configuration file to increase the simple descriptor table size from 2 to 4, as it is the number of application endpoints (3 in our case) + 1 (ZDO endpoint).  : /*****************************************************************************/ /* ZPS AF Layer Configuration Parameters */ /*****************************************************************************/ #define AF_SIMPLE_DESCRIPTOR_TABLE_SIZE 4 Router/app_zcl_globals.c The third step is to update the ZigBee cluster Configuration file to add the new endpoints (Switch1, Switch2) and their clusters to the Router application. For that one need to change the Configured endpoint from 1 to 3 and also the Endpoint Map list present as below: PUBLIC uint8 u8MaxZpsConfigEp = 3; PUBLIC uint8 au8EpMapPresent[3] = { ROUTER_APPLICATION_ENDPOINT,ROUTER_SWITCH1_ENDPOINT,ROUTER_SWITCH2_ENDPOINT }; The Switch 1 and Switch 2 contains Basic Cluster (0x0000) Server and Client, Identify Cluster (0x0003) Server and Client, OnOff Cluster (0x0006) Client, Group Cluster (0x004) Client. The clusters are added to the Input cluster list (Server side) and output cluster list (Client side) but made discoverable using DiscFlag only for the cluster list which is enabled. So, assuming you need to add OnOff cluster client, you would need to use add the cluster id (0x0006 for OnOff) into input cluster list (Server side of cluster) and output cluster list (Client side of the cluster) and make it discoverable for output cluster list as it is a client cluster. PRIVATE const uint16 s_au16Endpoint2InputClusterList[5] = { HA_BASIC_CLUSTER_ID, HA_GROUPS_CLUSTER_ID, HA_IDENTIFY_CLUSTER_ID,\ HA_ONOFF_CLUSTER_ID, HA_DEFAULT_CLUSTER_ID, }; PRIVATE const PDUM_thAPdu s_ahEndpoint2InputClusterAPdus[5] = { apduZCL, apduZCL, apduZCL, apduZCL, apduZCL, }; PRIVATE uint8 s_au8Endpoint2InputClusterDiscFlags[1] = { 0x05 }; PRIVATE const uint16 s_au16Endpoint2OutputClusterList[4] = { HA_BASIC_CLUSTER_ID, HA_GROUPS_CLUSTER_ID, HA_IDENTIFY_CLUSTER_ID,\ HA_ONOFF_CLUSTER_ID, }; PRIVATE uint8 s_au8Endpoint2OutputClusterDiscFlags[1] = { 0x0f }; PRIVATE const uint16 s_au16Endpoint3InputClusterList[5] = { HA_BASIC_CLUSTER_ID, HA_GROUPS_CLUSTER_ID, HA_IDENTIFY_CLUSTER_ID,\ HA_ONOFF_CLUSTER_ID, HA_DEFAULT_CLUSTER_ID, }; PRIVATE const PDUM_thAPdu s_ahEndpoint3InputClusterAPdus[5] = { apduZCL, apduZCL, apduZCL, apduZCL, apduZCL, }; PRIVATE uint8 s_au8Endpoint3InputClusterDiscFlags[1] = { 0x05 }; PRIVATE const uint16 s_au16Endpoint3OutputClusterList[4] = { HA_BASIC_CLUSTER_ID, HA_GROUPS_CLUSTER_ID, HA_IDENTIFY_CLUSTER_ID,\ HA_ONOFF_CLUSTER_ID, }; PRIVATE uint8 s_au8Endpoint3OutputClusterDiscFlags[1] = { 0x0f }; Now add these newly added endpoints as part of Simple Descriptor structure and initialize the structure (see the declaration of zps_tsAplAfSimpleDescCont and ZPS_tsAplAfSimpleDescriptor structures to understand how to correctly fill the various parameters) correctly as below : PUBLIC zps_tsAplAfSimpleDescCont s_asSimpleDescConts[AF_SIMPLE_DESCRIPTOR_TABLE_SIZE] = { {    {       0x0000,       0,       0,       0,       84,       84,       s_au16Endpoint0InputClusterList,       s_au16Endpoint0OutputClusterList,       s_au8Endpoint0InputClusterDiscFlags,       s_au8Endpoint0OutputClusterDiscFlags,    },    s_ahEndpoint0InputClusterAPdus,    1 }, {    {       0x0104,       0,       1,       1,       5,       4,       s_au16Endpoint1InputClusterList,       s_au16Endpoint1OutputClusterList,       s_au8Endpoint1InputClusterDiscFlags,       s_au8Endpoint1OutputClusterDiscFlags,    },    s_ahEndpoint1InputClusterAPdus,    1 }, {    {       0x0104,       0,       1,       2,       5,       4,       s_au16Endpoint2InputClusterList,       s_au16Endpoint2OutputClusterList,       s_au8Endpoint2InputClusterDiscFlags,       s_au8Endpoint2OutputClusterDiscFlags,     },     s_ahEndpoint2InputClusterAPdus,    1 }, {    {       0x0104,       0,       1,       3,       5,       4,       s_au16Endpoint3InputClusterList,       s_au16Endpoint3OutputClusterList,       s_au8Endpoint3InputClusterDiscFlags,       s_au8Endpoint3OutputClusterDiscFlags,    },    s_ahEndpoint3InputClusterAPdus,    1 }, }; Router/zcl_options.h This file is used to set the options used by the ZCL.   Number of Endpoints The number of endpoints is increased from 1 to 3: /* Number of endpoints supported by this device */ #define ZCL_NUMBER_OF_ENDPOINTS                              3   Enable Client Clusters The client cluster functionality for the new endpoints is enabled: /****************************************************************************/ /*                             Enable Cluster                               */ /*                                                                          */ /* Add the following #define's to your zcl_options.h file to enable         */ /* cluster and their client or server instances                             */ /****************************************************************************/ #define CLD_BASIC #define BASIC_SERVER #define BASIC_CLIENT #define CLD_IDENTIFY #define IDENTIFY_SERVER #define IDENTIFY_CLIENT #define CLD_GROUPS #define GROUPS_SERVER #define GROUPS_CLIENT #define CLD_ONOFF #define ONOFF_SERVER #define ONOFF_CLIENT   Router/app_zcl_task.c Base Device Data Structures The structures that store data for the new Base Devices associated with the new endpoints are created: /****************************************************************************/ /***        Exported Variables                                            ***/ /****************************************************************************/ tsZHA_BaseDevice sBaseDevice; tsZHA_BaseDevice sBaseDeviceSwitch1; tsZHA_BaseDevice sBaseDeviceSwitch2;   Register Base Device Endpoints - APP_ZCL_vInitialise() The two new Base Devices and their endpoints are registered with the stack to make them available: if (eZCL_Status != E_ZCL_SUCCESS) {           DBG_vPrintf(TRACE_ZCL, "Error: eZHA_RegisterBaseDeviceEndPoint(Light): %02x\r\n", eZCL_Status); } /* Register Switch1 EndPoint */ eZCL_Status =  eZHA_RegisterBaseDeviceEndPoint(ROUTER_SWITCH1_ENDPOINT,                                                           &APP_ZCL_cbEndpointCallback,                                                           &sBaseDeviceSwitch1); if (eZCL_Status != E_ZCL_SUCCESS) {           DBG_vPrintf(TRACE_ZCL, "Error: eZHA_RegisterBaseDeviceEndPoint(Switch1): %02x\r\n", eZCL_Status); } /* Register Switch2 EndPoint */ eZCL_Status =  eZHA_RegisterBaseDeviceEndPoint(ROUTER_SWITCH2_ENDPOINT,                                                           &APP_ZCL_cbEndpointCallback,                                                           &sBaseDeviceSwitch2); if (eZCL_Status != E_ZCL_SUCCESS) {           DBG_vPrintf(TRACE_ZCL, "Error: eZHA_RegisterBaseDeviceEndPoint(Switch2): %02x\r\n", eZCL_Status); }   Factory Reset Functionality - vHandleClusterCustomCommands() The two new Base Devices are factory reset by re-registering them when the Reset To Factory Defaults command is received by the Basic cluster server: case GENERAL_CLUSTER_ID_BASIC: {      tsCLD_BasicCallBackMessage *psCallBackMessage = (tsCLD_BasicCallBackMessage*)psEvent->uMessage.sClusterCustomMessage.pvCustomData;      if (psCallBackMessage->u8CommandId == E_CLD_BASIC_CMD_RESET_TO_FACTORY_DEFAULTS )      {           DBG_vPrintf(TRACE_ZCL, "Basic Factory Reset Received\n");           FLib_MemSet(&sBaseDevice,0,sizeof(tsZHA_BaseDevice));           APP_vZCL_DeviceSpecific_Init();           eZHA_RegisterBaseDeviceEndPoint(ROUTER_APPLICATION_ENDPOINT,                                                   &APP_ZCL_cbEndpointCallback,                                                   &sBaseDevice);           eZHA_RegisterBaseDeviceEndPoint(ROUTER_SWITCH1_ENDPOINT,                                                   &APP_ZCL_cbEndpointCallback,                                                   &sBaseDeviceSwitch1);           eZHA_RegisterBaseDeviceEndPoint(ROUTER_SWITCH2_ENDPOINT,                                                   &APP_ZCL_cbEndpointCallback,                                                   &sBaseDeviceSwitch2);      } } break;   Basic Server Cluster Data Initialisation - APP_vZCL_DeviceSpecific_Init() The default attribute values for the Basic clusters are initialized: sBaseDevice.sOnOffServerCluster.bOnOff = FALSE; FLib_MemCpy(sBaseDevice.sBasicServerCluster.au8ManufacturerName, "NXP", CLD_BAS_MANUF_NAME_SIZE); FLib_MemCpy(sBaseDevice.sBasicServerCluster.au8ModelIdentifier, "BDB-Router", CLD_BAS_MODEL_ID_SIZE); FLib_MemCpy(sBaseDevice.sBasicServerCluster.au8DateCode, "20150212", CLD_BAS_DATE_SIZE); FLib_MemCpy(sBaseDevice.sBasicServerCluster.au8SWBuildID, "1000-0001", CLD_BAS_SW_BUILD_SIZE); sBaseDeviceSwitch1.sOnOffServerCluster.bOnOff = FALSE; FLib_MemCpy(sBaseDeviceSwitch1.sBasicServerCluster.au8ManufacturerName, "NXP", CLD_BAS_MANUF_NAME_SIZE); FLib_MemCpy(sBaseDeviceSwitch1.sBasicServerCluster.au8ModelIdentifier, "BDB-Sw1", CLD_BAS_MODEL_ID_SIZE); FLib_MemCpy(sBaseDeviceSwitch1.sBasicServerCluster.au8DateCode, "20170310", CLD_BAS_DATE_SIZE); FLib_MemCpy(sBaseDeviceSwitch1.sBasicServerCluster.au8SWBuildID, "1000-0001", CLD_BAS_SW_BUILD_SIZE); sBaseDeviceSwitch2.sOnOffServerCluster.bOnOff = FALSE; FLib_MemCpy(sBaseDeviceSwitch2.sBasicServerCluster.au8ManufacturerName, "NXP", CLD_BAS_MANUF_NAME_SIZE); FLib_MemCpy(sBaseDeviceSwitch2.sBasicServerCluster.au8ModelIdentifier, "BDB-Sw2", CLD_BAS_MODEL_ID_SIZE); FLib_MemCpy(sBaseDeviceSwitch2.sBasicServerCluster.au8DateCode, "20170310", CLD_BAS_DATE_SIZE); FLib_MemCpy(sBaseDeviceSwitch2.sBasicServerCluster.au8SWBuildID, "1000-0001", CLD_BAS_SW_BUILD_SIZE);   Router/app_zcl_task.h The Base Device Data structures are made available to other modules: /****************************************************************************/ /***        Exported Variables                                            ***/ /****************************************************************************/ extern tsZHA_BaseDevice sBaseDevice; extern tsZHA_BaseDevice sBaseDeviceSwitch1; extern tsZHA_BaseDevice sBaseDeviceSwitch2;   Router/app_router_node.c Enable ZCL Event Handler - vAppHandleAfEvent() Data messages addressed to the two new endpoints are passed to the ZCL for processing: if (psZpsAfEvent->u8EndPoint == ROUTER_APPLICATION_ENDPOINT ||  psZpsAfEvent->u8EndPoint == ROUTER_SWITCH1_ENDPOINT ||  psZpsAfEvent->u8EndPoint == ROUTER_SWITCH2_ENDPOINT) {      DBG_vPrintf(TRACE_APP, "Pass to ZCL\n");      if ((psZpsAfEvent->sStackEvent.eType == ZPS_EVENT_APS_DATA_INDICATION) ||           (psZpsAfEvent->sStackEvent.eType == ZPS_EVENT_APS_INTERPAN_DATA_INDICATION))      {           APP_ZCL_vEventHandler( &psZpsAfEvent->sStackEvent);       } }
記事全体を表示
The RF parameters for KW01 can be changed by firmware using the KW01 connectivity software. Frequency band: The operational frequency band can be changed in app_preinclude.h file stored in Source folder. You can select the operational frequency band for your application only setting "1" to the desired band and "0" for the unused bands. In the same file also the default phy mode can be selected: Center frequency, channel spacing, number of channels, bit rate, frequency deviation, filter bandwidth, and other RF parameters: Most common RF parameters can be changed in declaration of "phyPibRFConstants" on PhyPib.c file. Search for your operational band and phy mode. For example for US ISM band in phy mode 1: Then change the desired parameters. If you want to change, for example, FDev: select "Fdev_25000", then go to declaration and change it from one of the predefined list of values: Regards, Luis Burgos.
記事全体を表示
Hello community, This time I bring to you a document which explains what are the ZigBee Test Client commands and how to use it. Before to read this guide, I widely recommend to take a look into the document Running a demo with BeeKit (802.15.4 MAC, SMAC and ZigBee BeeStack). This guide requires the BeeKit Wireless Connectivity Toolkit​ and the Test Tool for Connectivity Products applications.     I hope you find this guide useful. Enjoy this guide! Any feedback is welcome. Best regards, Earl Orlando Ramírez-Sánchez Technical Support Engineer NXP Semiconductors
記事全体を表示
       This document will address the JN5169 CMET setup and JN5169 connection setup with IQxel-MW. We also show the EVM and packet error rate results.
記事全体を表示
The KW40Z connectivity software stack has several demo application available, and one of them is the OTAP client. This application allows the user to reprogram the device in a wireless fashion. This can be done by both using another device with an OTAP server application, or with the Kinetis BLE Toolbox mobile application, using the OTAP tool. To create a binary file for the KW40Z, follow these next steps: Using IAR Embedded Workbench, open the application you want to send through OTAP. Right click the main project, and open the Options... menu.                                                                                                                                              In the options menu, go to the Output Converter submenu. In the Output Converter submenu, check the "Generate additional output" box, and choose Motorola as the Output format.                                                                                                                                                                            In the options menu, go to the Linker submenu. Now, in the Config tab, replace the symbols in the Configuration file symbol definitions box with these: gUseNVMLink_d=1 gUseBootloaderLink_d=1 gUseInternalStorageLink_d=0 __ram_vector_table__=1                                                                                                                                                                                              In the Linker submenu, go to the Input tab. In the Keep symbols box, add the symbol 'bootloader' (without the quotes). In the Input tab, in the Raw binary image box, in the File option, add the following path: $PROJ_DIR$\..\..\..\..\..\..\..\framework\Bootloader\Bin\BootloaderOTAP_KW40Z4.bin In the Raw binary image box, add the following options to the Symbol, Section and Align boxes: Symbol: bootloader Section: .bootloader Align: 4                                                                                                                                                                                                                         Press OK. Compile the project. The output file (*.srec) should be in the main project folder, inside the debug folder.                                                      You can now use this binary file to reprogram your device with OTAP.
記事全体を表示
What you need: USB-KW40Z boards (at least 3 recommended) Kinetis KW40Z Connectivity Software Kinetis Protocol Analyzer Adapter Wireshark Consult the USB-KW40Z getting started guide for an in depth tutorial on how to program the boards with the sniffer software and how to install and use the Kinetis Protocol Analyzer Adapter and Wireshark. For best performance at least 3 boards are needed to continuously monitor all 3 BLE advertising channels: 37, 38 and 39. If you have more then it’s even better. Having less than 3 sniffer boards will lead to the BLE sniffer setup missing some advertising packets and connection events. If only 1 or 2 boards are present they will have to jump between the 3 advertising channels. After the initial setup is complete make sure the boards are plugged into USB ports and then start the Kinetis Protocol Analyzer Adapter software. Immediately after the application is started it will start looking for the sniffers: After the sniffers are detected the application window should look like the screenshot below. There should be a separate row shown for each sniffer board which is plugged in (3 in the example below – COM32, COM34, and COM33). Set each sniffer on a different advertising channel and (37, 38 and 39) and if you’re looking to sniff a specific device enable the Address Filter checkbox and enter the device’s address in the adjacent field as shown in the screenshot below. Use the same device address for all sniffer devices. Press the “shark fin” button in the upper right of the window to start Wireshark. After Wireshark starts select the PCAP IF shown in the Kinetis Protocol Analyzer Adapter window and start capturing packets. Local Area Connection 2 is the PCAP IF in the example. Wireshark will start showing the captured packets and the sniffers will catch Connection Request packets sent to the target device on any of the advertising channels. Useful tip: You can use the btle.advertising_header.length != 0 or btle.data_header.length != 0 filter in Wireshark to filter out empty BLE packets.
記事全体を表示
MyWirelessAPP Demo Beacon(End device) code for RTS development
記事全体を表示
Hello everyone, Over The Air Programming (OTAP) NXP's custom Bluetooth LE service provides the developer a solution to upgrade the software that the MCU contains. It removes the need for cables and a physical link between the OTAP client (the device that is reprogrammed) and the OTAP server (the device that contains the software update). This post explains how to run the OTAP Client Software that comes within the FRDM-KW36 package: Reprogramming a KW36 device using the OTAP Client Software. As it is mentioned in the last post, the OTAP Client can reprogram the KW36 while it is running, with new software using Bluetooth LE. However, this implementation for most of the applications is not enough since once you have reprogrammed the new image, the KW36 can not be reprogramed a second time using this method. For these applications that require to be updated many times using Bluetooth LE during run-time, we have created the following application note, that comes with a functional example of how to implement the OTAP Client software, taking advantage of this service. You can download the software clicking on the link in blue and the documentation is in the link in green. Please visit the following link: DOCUMENTS and Application Notes for KW36 In the "DOCUMENTS" section, you can found more information of the KW36. In the "Application Note" section, you can found more software and documentation of interesting topics like this.        Best Regards.
記事全体を表示
Introduction This document describes the hardware considerations for the schematic and layout of the MKW36A512VFT4 device. This MCU is packaged into a 48-pin HVQFN - 7x7 mm, dissimilar to MKW36Z512VHT4 which comes packaged into a 48-pin LQFN - 7x7 mm (the last one takes part of FRDM-KW36).   Pin Layout  The MKW36A512VFT4 MCU is pin to pin compatible with the MKW36Z512VHT4 (FRDM-KW36) MCU, except for the DCDC pins. The following figure shows the distribution of the pins in the MKW36A512VFT4 MCU (left), compared with the MKW36Z512VHT4 (FRDM-KW36 MCU, right). Surely, this is the most important consideration for MKW36A512VFT4, since you can not simply move the FRDM-KW36 layout on your design. Minimum BOM The following figures show the minimum BOM necessary for each DCDC mode in KW36. For more information about DCDC modes and hardware guidelines, please visit: MKW4xZ/3xZ/3xA/2xZ DC-DC Power Management Bypass Mode   Buck Auto-Start Mode   Buck Manual-Start Mode     Layout Recommendations The footprint and layout are critical for RF performance, hence if the recommended design is followed exactly in the RF region of the PCB, sensitivity, output power, harmonic and spurious radiation, and range, you will succeed. For more information of layout recommendations, please visit Hardware Design Considerations for MKW35A/36A/35Z/36Z Bluetooth Low Energy Devices. The footprint recommended for the MKW36A512VFT4 is shown in the figure below. NXP prefers to use a top layer thickness of no less than 8-10 mils. The use of a correct substrate like the FR4 with a dielectric constant of 4.3 will assist you in achieving a good RF design. Other recommendations during EMC certification stages are: - Specific attention must be taken on 4 pins PTC1, 2, 3 & 4 if they are used on the application. - 4 decoupling capacitors of 3pF are mandatory on those pins and be positioned as close as possible. - Wires from those 4 pins must be underlayer. - NXP recommends putting the vias under the package in case the customer HW design rules allow it. Some recommendations for a good Vdd_RF supply layout are: - Vdd_RF1 and Vdd_RF2 lines must have the same length as possible, linked to pointA (‘Y’ connection). - 12pF decoupling capacitor from Vdd_RF wire must be connected to the Ground Antenna. The purpose is to get the path as short as possible from Vdd_RF1/Vdd_RF2 to the ground antenna. - 12pF decoupling capacitor from the Vdd_RF3 pin must be as close as possible. Return to ground must be as short as possible. So vias (2 in this below picture) must be placed near to the decoupling capacitor to get close connection to the ground layer. The recommended RF stage is shown in the following figure. The MKW36A512VFT4 has a single-ended RF output with a 2 components matching network composed of a shunt capacitor and a series inductor. Both elements transform the device impedance to 50 ohms. The value of these components may vary depending on your board layout. Avoid routing traces near or parallel to RF transmission lines or crystal signals. Maintain a continuous ground under an RF trace is critical to keep unaltered the characteristic impedance of the transmission line. Avoid routing on the ground layer that will result in disrupting the ground under RF traces. For more information about RF considerations please visit: Freescale IEEE 802.15.4 / ZigBee Package and Hardware Layout Considerations.
記事全体を表示
This document describes how to sniff ZigBee packets to identify messages and layers from the ZigBee stack using the MC1322x USB dongle and Wireshark protocol analyzer. --------------------------------------------------------------------------------------------------------- Pre-Requisites If not done yet, download & Install Wireshark protocol analyzer http://www.wireshark.org/download.html Download the Wireshark ZigBee Utility Zip file from Sourceforge http://sourceforge.net/projects/wiresharkzigbee/ Unzip the file in a known location -------------------------------------------------------------------------------------------------------- 1. Install MC1322x dongle Plug-in MC1322xUSB dongle and wait for Windows to install the driver. If the driver was not found, steer Windows manually to the directory         C:\Program Files\Freescale\Drivers If BeeKit is not installed, be aware of the following: The 1322x USB Dongle uses the FTDI serial to USB converter, Virtual COM Port (VCP) driver for Windows, available at www.ftdichip.com/ftdrivers.htm. The FTDI web site offers drivers for other platforms including Windows® (98 through Vista x64 and CE), MAC OS (8 through X) and Linux. Download the appropriate driver and follow the instructions to complete driver installation. 2. Check COM port Once installed, the MC1322xUSB dongle should be listed in the available COM ports in Widows device manager. Verify the board’s drivers were successfully installed and take note of the COM port assigned      3. Run the ZigBee Utility Open a command console and navigate to the directory where Wireshark Zigbee utility files were unzipped. c:\<path> Then start the .exe utility and set the serial port and ZigBee channel to monitor, for instance:     4. Setting Wireshark Start Wireshark and open Capture>Options Dialog Click on “Manage Interfaces” and add a new pipe with ‘\\.\pipe\wireshark’. Save it and start capture. 5. Start sniffing
記事全体を表示