Wireless Connectivity Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wireless Connectivity Knowledge Base

Discussions

Sort by:
One of the most difficult part of creating connected medical applications is, actually, keep it connected. Different protocols are available to transmit information from a medical device to a database or user interface. Sometimes integrating our application to the current communication protocols can be as difficult as developing the device itself. Freescale has launched its Bluetooth® Low Energy (BLE) chips, and with them, a complete software stack that integrates most of the available profiles for BLE oriented applications. Using this set, it becomes easy to integrate your current medical application to use BLE as communications method. Freescale Connectivity Software Examples The connectivity software includes examples to demonstrate BLE communications with a smartphone device. Using these examples as a base facilitates the integration with an existing application and reduces the required time it takes to have a fully connected application. This post uses as an example the Heart Rate Monitor demo to show how these applications can be customized. Modifying general device information The BLE services information reported by the device is stored in a file named “gatt_db.h”. This services information is what is shown on a smartphone when the device has connected. The Generic Access Profile service includes the device name reported when advertising. To change it just replace the device name between “” and update the character count. Detailed device information is accessed via the Device Information Service including the manufacturer name, model and serial number etcetera. This information can also be adjusted to the custom device requirements by modifying the string between “” and updating the character number. Adapting example code to report application data The connectivity software includes some predefined services that can be used to customize the server to report our application data. These predefined services already include structures with the information that needs to be reported to the client. On the application example file app.c some of these services are configured. For the heart rate service, a variable of type hrsConfig_t is created containing configuration information of the heart rate sensor such as the supported characteristics and sensor location. All of these characteristics are described in the heart rate service file heart_rate_interface.h /* Service Data*/ static basConfig_t      basServiceConfig = {service_battery, 0}; static disConfig_t      disServiceConfig = {service_device_info}; static hrsUserData_t    hrsUserData; static hrsConfig_t hrsServiceConfig = {service_heart_rate, TRUE, TRUE, TRUE, gHrs_BodySensorLocChest_c, &hrsUserData}; static uint16_t cpHandles[1] = { value_hr_ctrl_point }; /*! Heart Rate Service - Configuration */ typedef struct hrsConfig_tag {     uint16_t             serviceHandle;     bool_t               sensorContactSupported;     bool_t               sensorContactDetected;     bool_t               energyExpandedEnabled;     hrsBodySensorLoc_t   bodySensorLocation;     hrsUserData_t        *pUserData; } hrsConfig_t; This information is used to configure the server when the function BleApp_Config is called. /* Start services */ hrsServiceConfig.sensorContactDetected = mContactStatus; #if gHrs_EnableRRIntervalMeasurements_d    hrsServiceConfig.pUserData->pStoredRrIntervals = MEM_BufferAlloc(sizeof(uint16_t) * gHrs_NumOfRRIntervalsRecorded_c); #endif    Hrs_Start(&hrsServiceConfig); basServiceConfig.batteryLevel = BOARD_GetBatteryLevel(); Bas_Start(&basServiceConfig); /* Allocate application timers */ mAdvTimerId = TMR_AllocateTimer(); Once the server is configured, the application is stated by entering the device in advertising state in order to make it visible for clients. This is done by calling the function BleApp_Advertise that configures the server to start advertising. void BleApp_Start(void) { /* Device is not connected and not advertising*/ if (!mAdvState.advOn) { #if gBondingSupported_d if (mcBondedDevices > 0) { mAdvState.advType = fastWhiteListAdvState_c; } else { #endif mAdvState.advType = fastAdvState_c; #if gBondingSupported_d } #endif BleApp_Advertise(); } #if (cPWR_UsePowerDownMode)    PWR_ChangeDeepSleepMode(1); /* MCU=LLS3, LL=DSM, wakeup on GPIO/LL */ PWR_AllowDeviceToSleep(); #endif       } Once the server has been found and a connection has been stablished with the client, the configured services must be started. This is done by calling the “subscribe” function for each service. For heart rate sensor, the function Hrs_Suscribe must be called. This function is available from the heart_rate_interface files. /* Subscribe client*/ Bas_Subscribe(peerDeviceId);        Hrs_Subscribe(peerDeviceId); #if (!cPWR_UsePowerDownMode)  /* UI */            During connection, the application measurements can be reported to the client by using the “record measurement” functions included in the service interfaces. For the heart rate sensor this is the Hrs_RecordHeartRateMeasurement function. static void TimerMeasurementCallback(void * pParam) { uint16_t hr = BOARD_GetPotentiometerLevel(); hr = (hr * mHeartRateRange_c) >> 12; #if gHrs_EnableRRIntervalMeasurements_d    Hrs_RecordRRInterval(&hrsUserData, (hr & 0x0F)); Hrs_RecordRRInterval(&hrsUserData,(hr & 0xF0)); #endif if (mToggle16BitHeartRate) { Hrs_RecordHeartRateMeasurement(service_heart_rate, 0x0100 + (hr & 0xFF), &hrsUserData); } else { Hrs_RecordHeartRateMeasurement(service_heart_rate, mHeartRateLowerLimit_c + hr, &hrsUserData); } Hrs_AddExpendedEnergy(&hrsUserData, 100); #if (cPWR_UsePowerDownMode) PWR_SetDeepSleepTimeInMs(900); PWR_ChangeDeepSleepMode(6); PWR_AllowDeviceToSleep();    #endif } This updates the current measurement and sends a notification to the client indicating that a new measurement report is ready. Many profiles are implemented in the connectivity software to enable already developed medical applications with BLE connectivity. APIs are easy to use and can significantly reduce the development times.
View full article
Introduction When a software update is requested by an OTAP Client (a device that receives a software update, commonly Bluetooth LE Peripheral) from the OTAP Server (a device that sends a software update, commonly Bluetooth LE Central), you may want to preserve some data previously acquired, such as bonding information, trimming values for the system oscillators, or probably NVM data for your application. This document guides you in performing OTAP updates preserving the flash data content of your interest. This document is intended for developers familiarized with OTAP custom Bluetooth LE service, for more information, you can take a look at the following post: Reprogramming a KW36 device using the OTAP Client Software.   OTAP Header and Sub-elements OTAP Protocol implements a format for the software update that is composed of a header and a defined number of sub-elements. The OTAP Header describes general information about the software update and it has a defined format shown in the following figure. For more information about the header fields, you can go to 11.4.1 Bluetooth Low Energy OTAP header chapter of the Bluetooth Low Energy Application Developer's Guide document included in the SDK at <SDK_2.2.X_FRDM-KW36_Download_Path>\docs\wireless\Bluetooth                              Each Sub-element contains information for a specific purpose. You could implement your proprietary fields for your application (For more information about sub-element fields, you can go to 11.4.1 Bluetooth Low Energy OTAP header chapter of the Bluetooth Low Energy Application Developer's Guide document included in the SDK at <SDK_2.2.X_FRDM-KW36_Download_Path>\docs\wireless\Bluetooth). OTAP includes the following sub-elements: Image File Sub-element Value Field Lenght (bytes) Description Upgrade Image  Variable This sub-element contains the actual binary executable image which is copied into the flash memory of the OTAP Client device. The maximum size of this sub-element depends on the target hardware. Sector Bitmap 32 This sub-element contains a sector bitmap of the flash memory of the target device which tells the bootloader which sectors should be overwritten and which leave intact. The format of this field is the least-significant bit first for each byte with the least significant bytes and bits standing for the lowest memory sections of the flash.  Image File CRC 2 This is a 16-bit CRC calculated over all elements of the image file except this field itself. This element must be the last sub-element in an image file sent over the air.   OTAP Sector Bitmap Sub-element Field The KW36 Flash is partitioned into: One 256 KB Program Flash (P-Flash) array divided into 2 KB sectors with a flash address range from 0x0000_0000 to 0x0003_FFFF. One 256 KB FlexNVM array divided in 2 KB sectors, flash address ranges from 0x1000_0000 to 0x1003_FFFF with an Alias memory with address range 0x0004_0000 to 0x0007_FFFF. The Bitmap sub-element is 256 bits of length, in terms of the KW36 flash, each bit represents a 2KB sector covering the address range from 0x0 - 0x0007_FFFF (P-Flash to FlexNVM Alias address range), where 1 means that such sector should be erased and 0 means that such sector should be preserved. The Bitmap field is used by the OTAP Bootloader to obtain the address range which should be erased before programming the KW36 with the software update, so it must be configured before sending a software update to leave intact the address range of memory that contain data of your interest and erase only the address range that will be overwritten by the software update.        For example: Suppose that a developer wants to preserve the address range between 0x7D800 - 0x7FFFF and the address range between 0x0 - 0x1FFF, and the left memory must be erased. The address range between 0x7D800 - 0x7FFFF corresponds to the 5 top flash sectors and the address range between 0x0 - 0x1FFF is the lowest 4 sectors. So, it means that bits between 256 and 252 (256, 255, 254, 253 and 252) and bits between 4 and 1 (4,3,2 and 1) should be set to 0, that way OTAP Bitmap for this example is: 0x07FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF0   Configuring OTAP Bitmap to Protect an Address Range with NXP Test Tool Download and install Test Tool for Connectivity products in NXP's web site Open NXP Test Tool 12 software on your PC. Go to "OTA Updates -> OTAP Bluetooth LE" Then load your image file for the software update clicking on the "Browse..." button (NXP Test Tool only accepts .bin and .srec files). You can configure the OTAP Bitmap selecting the "Override sector bitmap" checkbox and changing the default value by your new bitmap value. Once you have configured the bitmap, select "Save...".   Untitled.png Then, a window will be displayed to select the destination to save the .bleota file. Provide a name to identify this file. You can use this file with IoT Toolbox App for Android and iOS to update the software using OTAP. This new .bleota file contains the bitmap that tells to the OTAP Bootloader which sectors will be erased and which sectors will be preserved.    Untitled.png      
View full article
Introduction This post guides you on migrating from MKW36Z512VHT4 to MKW36A512VFT4 MCUs. This example will make use of the "beacon" SDK example. SDK Download and Install 1- Go to MCUXpresso web page: MCUXpresso Web Page 2- Log in with your registered account. 3- Search for the "KW36A" device. Then click on the suggested processor and click on "Build MCUXpresso SDK"       4- The next page will be displayed. Select “All toolchains” in the “Toolchain / IDE” box and provide a name to identify the package. Then click on "Download SDK".     5- Accept the license agreement. Wait a few minutes until the system gets the package into your profile. Download the SDK clicking on "Download SDK Archive" as depicted in the following figure.     6- If MCUXpresso IDE is used, drag and drop the KW36A SDK zip folder in “Installed SDK’s” perspective to install the package.     At this point, you have downloaded and installed the SDK package for the KW36A device.   Software Migration in MCUXpresso IDE 1- Import the "beacon" example on the MCUXpresso workspace. Click on “Import SDK examples(s)…” option, a new window will appear. Then select "MKW36Z512xxx4" and click on the FRDM-KW36 image. Click on the "Next >" button.     2- Search beacon and select your project version (bm or freertos).     3- Go to Project/Properties. Expand C/C++ Build/MCU settings and select MKW36A512xxx4 MCU. Click Apply and Close button to save the configuration.     4- Rename MKW36Z folders as MKW36A, clicking the right mouse button and selecting "Rename". These are the following:   framework/DCDC/Interface -> MKW36Z framework/DCDC/Source -> MKW36Z framework/LowPower/Interface -> MKW36Z framework/LowPower/Source -> MKW36Z framework/XCVR -> MKW36Z4     5- Open the Project/Properties window in MCUXpresso IDE. Go to C/C++ Build/Settings and select MCU C Compiler/Includes folder in the Tool Settings window. Edit all paths related to MKW36 MCU, in according to MKW35 folders before created. The results must look similar as shown below:   ../framework/LowPower/Interface/MKW36A ../framework/LowPower/Source/MKW36A ../framework/DCDC/Interface/MKW36A ../framework/XCVR/MKW36A4     6- Select MCU Assembler/General folder in Tool Settings. Edit the paths related to MKW36 MCU. The results must look similar as shown below:   ../framework/LowPower/Interface/MKW36A ../framework/LowPower/Source/MKW36A ../framework/DCDC/Interface/MKW36A ../framework/XCVR/MKW36A4     7- Go to Project/Properties. Expand MCU C Compiler/Preprocessor window. Edit "CPU_MKW36Z512VHT4" and "CPU_MKW36Z512VHT4_cm0plus" symbols, rename it as "CPU_MKW36A512VFT4" and "CPU_MKW36A512VFT4_cm0plus" respectively. Save the changes.     8- Go to the workspace. Delete “fsl_device_registers, MKW36Z4, MKW36Z4_features, system_MKW36Z4.h and system_MKW36Z4.c” files located at CMSIS folder. Then, unzip the MKW35Z SDK package and search for “fsl_device_registers, MKW36A4, MKW36A4_features, system_MKW36A4.h and system_MKW36A4.c” files into this folder at the following paths:   <SDK_folder_root>/devices/MKW36A4/fsl_device_registers.h <SDK_folder_root>/devices/MKW36A4/MKW36A4.h <SDK_folder_root>/devices/MKW36A4/MKW36A4_features.h <SDK_folder_root>/devices/MKW36A4/system_MKW36A4.h <SDK_folder_root>/devices/MKW36A4/system_MKW36A4.c     9- Overwirte the “startup_mkw36z4.c” (located inthe startup folder) by the "startup_mkw36a4.c" located in the following path <SDK_folder_root>/devices/MKW36A4/mcuxpresso/startup_mkw36a4.c. You can simply drag and drop on the startup folder, and remove the older one.     10- Open "fsl_device_registers.h" file in CMSIS folder. Add"defined(CPU_MKW36A512VFT4)" in the following code (line 18 of the file):   /* * Include the cpu specific register header files. * * The CPU macro should be declared in the project or makefile. */ #if (defined(CPU_MKW36A512VFP4) || defined(CPU_MKW36A512VFT4) || defined(CPU_MKW36A512VHT4) || defined(CPU_MKW36A512VFT4))‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍   11- Open "ble_config.h" file in bluetooth->host->config folder. Add "defined(CPU_MKW36A512VFT4)" in the following code (line 146 of the file):   /* The maximum number of BLE connection supported by platform */ #if defined(CPU_QN9080C) #define MAX_PLATFORM_SUPPORTED_CONNECTIONS 16 #elif (defined(CPU_MKW36Z512VFP4) || defined(CPU_MKW36Z512VHT4) || defined(CPU_MKW36A512VFP4) || defined(CPU_MKW36A512VHT4) || defined(CPU_MKW36A512VFT4) || \ defined(CPU_MKW35Z512VHT4) || defined(CPU_MKW35A512VFP4) || \ defined(CPU_K32W032S1M2CAx_cm0plus) || defined(CPU_K32W032S1M2VPJ_cm0plus) || \ defined(CPU_K32W032S1M2CAx_cm4) || defined(CPU_K32W032S1M2VPJ_cm4) || \ defined(CPU_MKW38A512VFT4) || defined (CPU_MKW38Z512VFT4) || defined(CPU_MKW39A512VFT4) || \ defined(CPU_MKW37A512VFT4) || defined(CPU_MKW37Z512VFT4))‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍   12- Open "ble_controller_task.c" file in source->common folder. Add "defined(CPU_MKW36A512VFT4)" in the following code (line 272 of the file):    #elif (defined(CPU_MKW35A512VFP4) || defined(CPU_MKW35Z512VHT4) || defined(CPU_MKW36A512VFP4) || defined(CPU_MKW36A512VFT4) ||\ defined(CPU_MKW36A512VHT4) || defined(CPU_MKW36Z512VFP4) || defined(CPU_MKW36Z512VHT4)) /* Select BLE protocol on RADIO0_IRQ */ XCVR_MISC->XCVR_CTRL = (uint32_t)((XCVR_MISC->XCVR_CTRL & (uint32_t)~(uint32_t)( XCVR_CTRL_XCVR_CTRL_RADIO0_IRQ_SEL_MASK )) | (uint32_t)( (0UL << XCVR_CTRL_XCVR_CTRL_RADIO0_IRQ_SEL_SHIFT) ));‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍   13-Build the project.   At this point, the project is already migrated.   Software Migration in IAR Embedded Workbench IDE 1- Open the beacon project located in the following path: 2- Select the project in the workspace and press Alt + F7 to open project options.   3- In the General Options/Target window click the icon next to the device name and select the appropriate device NXP/KinetisKW/KW3x/NXP MKW36A512xxx4, then click the OK button.   4- Create a new folder with the name MKW36A at following paths: <SDK_root>/middleware/wireless/framework_5.4.6/DCDC/Interface <SDK_root>/middleware/wireless/framework_5.4.6/DCDC/Source <SDK_root>/middleware/wireless/framework_5.4.6/LowPower/Interface <SDK_root>/middleware/wireless/framework_5.4.6/LowPower/Source <SDK_root>/middleware/wireless/framework_5.4.6/XCVR     5- Copy all files inside MKW36Z folders located at the above paths and paste in MKW36A folders.     6- Select the beacon project in the workspace and press Alt+F7 to open project options window. In C/C++ Compiler/Preprocessor window, rename the paths related to MKW36Z folders to MKW36A folders. Rename the CPU_MKW36Z512VHT4 macro as CPU_MKW36A512VFT4 in the defined symbols text box. The results must look similar as shown below: Click the OK button. $PROJ_DIR$/middleware/wireless/framework_5.4.2/LowPower/Interface/MKW36A $PROJ_DIR$/../../../../../../../devices/MKW36A4/drivers $PROJ_DIR$/../../../../../../../middleware/wireless/framework_5.4.2/DCDC/Interface/MKW36A $PROJ_DIR$/../../../../../../../middleware/wireless/framework_5.4.2/XCVR/MKW36A4 $PROJ_DIR$/../../../../../../../devices/MKW36A4 $PROJ_DIR$/../../../../../../../devices/MKW36A4/utilities     7- Expand the startup folder, select all files, click the right mouse button and select the “Remove” option. Click the right mouse button on the folder and select “Add/Add files”. Add the startup_MKW36A4.s located at this path: <SDK_root>/devices/MKW36A4/iar/startup_MKW36A4.s Also, add system_MKW36A4.c and system_MKW36A4.h into the startup folder. Both files are located at the next path: <SDK_root>/devices/MKW36A4   8- Open "ble_config.h" file in bluetooth->host->config folder. Add "defined(CPU_MKW36A512VFT4)" in the following code: /* The maximum number of BLE connection supported by platform */ #if defined(CPU_QN9080C) #define MAX_PLATFORM_SUPPORTED_CONNECTIONS 16 #elif (defined(CPU_MKW36Z512VFP4) || defined(CPU_MKW36Z512VHT4) || defined(CPU_MKW36A512VFP4) || defined(CPU_MKW36A512VHT4) || defined(CPU_MKW36A512VFT4) || \ defined(CPU_MKW35Z512VHT4) || defined(CPU_MKW35A512VFP4) || \ defined(CPU_K32W032S1M2CAx_cm0plus) || defined(CPU_K32W032S1M2VPJ_cm0plus) || \ defined(CPU_K32W032S1M2CAx_cm4) || defined(CPU_K32W032S1M2VPJ_cm4) || \ defined(CPU_MKW38A512VFT4) || defined (CPU_MKW38Z512VFT4) || defined(CPU_MKW39A512VFT4) || \ defined(CPU_MKW37A512VFT4) || defined(CPU_MKW37Z512VFT4))‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍   9- Open "ble_controller_task.c" file in source->common folder. Add "defined(CPU_MKW36A512VFT4)" in the following code: #elif (defined(CPU_MKW35A512VFP4) || defined(CPU_MKW35Z512VHT4) || defined(CPU_MKW36A512VFP4) || defined(CPU_MKW36A512VFT4) ||\ defined(CPU_MKW36A512VHT4) || defined(CPU_MKW36Z512VFP4) || defined(CPU_MKW36Z512VHT4)) /* Select BLE protocol on RADIO0_IRQ */ XCVR_MISC->XCVR_CTRL = (uint32_t)((XCVR_MISC->XCVR_CTRL & (uint32_t)~(uint32_t)( XCVR_CTRL_XCVR_CTRL_RADIO0_IRQ_SEL_MASK )) | (uint32_t)( (0UL << XCVR_CTRL_XCVR_CTRL_RADIO0_IRQ_SEL_SHIFT) ));‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍   10-Build the project.   At this point, the project is already migrated.
View full article
When having several ZigBee Networks in the same area, and therefore several potential parents, it may become necessary to join one of them and discard the rest. While having a mechanism to only accept joining devices when desired is the best method (like using a button to trigger the joining), it might not always be possible since the parent nodes could be commercial devices or another vendor’s product without this feature. Below are some mechanisms that could be used for this purpose. In general, when searching for suitable parents, the process is as follows: ZDO of device to join sends a MAC scan request. The MAC layer starts scan. For every beacon it receives, it sends a beacon notify indication that is processed in ParseBeaconNotifincaiton() function from AppStackImpl.c The ParseBeaconNotifincaiton() function will add the relevant information in the discovery table and for this it needs a free entry, so it calls GetFreeEntryInDiscoveryTable() function with reuse parameter as FALSE. If the table is full, it will call GetFreeEntryInDiscoveryTable() with reuse set to TRUE to literally re-use low priority entries. When the MAC scan has finished, it will send a MAC scan confirm. When this reaches ZDO, the SearchForSuitableParent() function is called. At this point, there are several approaches that could be used: Use a specific Extended PAN ID to search only for a specific parent node Use a specific PAN ID to prioritize the network’s ID Search in a specific Channel where network is supposed to be operating in All these parameters are configurable in ApplicationConf.h file of the project’s Configure Folder and used in SearchForSuitableParent() function to filter Discovery table entries. Nevertheless, those solutions are not always the best for all applications since it may require hard-coding the network’s parameters. Fortunately, BeeStack leaves all this open for any modification in case it is necessary. In brief, if the discovery table gets full with suitable parents that you DO NOT want to use, you should update the "if(reuse)" statement of the GetFreeEntryInDiscoveryTable() function to replace an entry. In other words, if you think that the desired parent is not present in the discovery table (due to its size limitation or other reason), you should update the GetFreeEntryInDiscoveryTable() function to make sure discovery table contains only devices that are of interest to your node. Please note that the criteria used to select the desired parents is totally application specific. As mentioned, it is always best having a way to trigger the joining such as a button so the rest of parents have permit join set to FALSE and therefore join only to the desired parent without having to implement custom code. Anyway, you may select the solution that meets your application’s requirements the most.
View full article
Many applications make use of 32 kHz clocks to keep tracking of real-time or to have a low power time reference for the system. Most of the systems might use a 32.768 kHz XTAL for this purpose. However, there might be some exceptions in which the application requires compensate the frequency of this clock due to temperature changes, aging, or just because the clock provides from a source which frequency is close to the ideal 32.768 kHz, but it presents some variations. QN908x devices require a 32 kHz clock source for some applications like running the BLE stack in low power. 32.768 kHz XTALs are more accurate so they are used to generate a 32 kHz source by compensating for the ppm difference. This provides us with tools to compensate for any external 32 kHz source by first obtaining the ppm difference from the ideal frequency. The solution consists in determining how off is the external clock input frequency from the ideal 32 kHz by making a comparison with a trusted clock in the system, typically the 32 MHz / 16 MHz XTAL. This process is executed in the background in an interrupt-based system so the application can initialize or run other processes in the meantime. Then, the results of the ppm calculation are reported to the main application to compensate for the changes and provide for a more accurate clock source. This example makes use of the following peripherals in the QN908x RTC Seconds Timer CTIMER DMA The RTC Seconds Timer uses the 32 kHz clock source as a reference. It contains an internal 32000 cycles counter that increases each 32 kHz clock period. On overflow, it rises the SEC_INT flag to indicate that one second has elapsed. The CTIMER makes use of the APB clock which derives from the 32 MHz / 16 MHz clock. This timer is used in free-running mode with a Prescaler value of 1 to count the number of APB pulses. The algorithm consists of counting the amount of APB pulses (trusted clock reference) elapsed by the time the RTC SEC_INT flag is set. Ideally, if both clocks are in the right frequency, the number of APB pulses must be equal to the reference clock frequency. For example, if the APB clock is 16 MHz, by the time the SEC_INT flag sets, the CTIMER counter must have a value of 16 x 10 6 counts. Assuming our reference clock is ideal, the difference between the CTIMER counter value and 16 x 10 6 can be used to obtain the ppm difference given the following formula. Where f 0 is the ideal APB frequency (16 MHz) and f 1 is the real measured frequency (CTIMER counter value). Since the pulses counted using the CTIMER correspond to the time it took to the RTC Seconds Timer to count one second, we can extrapolate the obtained ppm value as a difference in the 32 kHz clock source from the ideal 32 kHz. To prevent from any application or task servicing latency, the algorithm makes use of the DMA to automatically capture the CTIMER Counter value when the SEC_INT flag is set. The program flow is described in the diagram below. As a way of demonstrating this algorithm, two APIs were implemented to calculate the ppm value and apply the compensation to the system. Both APIs are included in the file fsl_osc_32k_cal .c and .h files. OSC_32K_CAL_GetPpm (osc_32k_cal_callback_t pCallbackFnc): Initializes the required timers and DMA and starts with the CTIMER capture. A callback is passed so it can be executed once the ppm calculation sequence completes. OSC_32_CAL_ApplyPpm (int32_t ppmMeasurement): Uses the previously calculated ppm passed as an input parameter to compensate the RTC and the BLE timer used during sleep mode. OSC_32K_CAL_GetPpm is called every time the ppm value of the 32 kHz source clock needs to be calculated. It takes around one second to complete (depending on how off the 32 kHz source clock is from the ideal frequency) and the application cannot enter into low power state during this time. The registered callback function is executed once the calculation is complete. The ppm calculation is performed into the DMA callback. It consists of obtaining the CTIMER counter difference and use it as f 1 in the formula shown before. The ppm values are calculated using floating point unit. /* Calculate PPMs */ ppmResult = (float)((float)1-((float)ApbClockFreq/(float)ApbCountDiff)); ppmResult *= (float)1048576;‍‍‍‍‍‍ Then OSC_32_CAL_ApplyPpm must be called using the ppm value obtained after calling OSC_32K_CAL_GetPpm. This API programs the necessary values in the RTCàCAL register and the BLE Sleep timer registers to compensate for the differences in the 32 kHz source clock. Finally, the user must account for all those other APIs that make use of the 32 kHz clock frequency and update the values accordingly. For the particular case of the NXP BLE Stack, there are two APIs that need to be updated to return the clock frequency after the calibration has been applied. uint32_t PWRLib_LPTMR_GetInputFrequency(void) { uint32_t result = 32000; int32_t ppm = 0; if ( RTC->CTRL & RTC_CTRL_CAL_EN_MASK) /* is calibration enabled ? */ { /* Get the current calibration value */ if (RTC->CAL & RTC_CAL_DIR_MASK) { /* Backward calibration */ ppm -= (int32_t) (RTC->CAL & RTC_CAL_PPM_MASK); } else { /* Forward calibration */ ppm += (int32_t) (RTC->CAL & RTC_CAL_PPM_MASK); } /* Obtain the uncalibrated clock frequency using the formula * fUncal = 32000 - (ppm*0.03125) where 0.03125 is the number * of Hz per PPM digit obtained from (768 Hz/0x6000 PPM) */ result -= (float) ppm * (float) 0.03125; } else { #if (defined(BOARD_XTAL1_CLK_HZ) && (BOARD_XTAL1_CLK_HZ == CLK_XTAL_32KHZ)) result = CLOCK_GetFreq(kCLOCK_32KClk); /* 32,768Khz crystal is used */ #else result = CLOCK_GetFreq(kCLOCK_32KClk); /* 32,000Khz internal RCO is used */ #endif } return result; }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ uint32_t StackTimer_GetInputFrequency(void) { uint32_t prescaller = 0; uint32_t refClk = 0; uint32_t result = 0; #if FSL_FEATURE_SOC_FTM_COUNT refClk = BOARD_GetFtmClock(gStackTimerInstance_c); prescaller = mFtmConfig.prescale; result = refClk / (1 << prescaller); #elif FSL_FEATURE_RTC_HAS_FRC int32_t ppm = 0; (void)prescaller; /* unused variables */ (void)refClk; /* suppress warnings */ result = 32000; if ( RTC->CTRL & RTC_CTRL_CAL_EN_MASK) /* is calibration enabled ? */ { /* Get the current calibration value */ if (RTC->CAL & RTC_CAL_DIR_MASK) { /* Backward calibration */ ppm -= (int32_t) (RTC->CAL & RTC_CAL_PPM_MASK); } else { /* Forward calibration */ ppm += (int32_t) (RTC->CAL & RTC_CAL_PPM_MASK); } /* Obtain the uncalibrated clock frequency using the formula * fUncal = 32000 - (ppm*0.03125) where 0.03125 is the number * of Hz per PPM digit obtained from (768 Hz/0x6000 PPM) */ result -= (float) ppm * (float) 0.03125; } else { #if (defined(BOARD_XTAL1_CLK_HZ) && (BOARD_XTAL1_CLK_HZ == CLK_XTAL_32KHZ)) result = CLOCK_GetFreq(kCLOCK_32KClk); /* 32,768Khz crystal is used */ #else result = CLOCK_GetFreq(kCLOCK_32KClk); /* 32,000Khz internal RCO is used */ #endif } #elif FSL_FEATURE_SOC_CTIMER_COUNT refClk = BOARD_GetCtimerClock(mCtimerBase[gStackTimerInstance_c]); prescaller = mCtimerConfig[gStackTimerInstance_c].prescale; result = refClk / (prescaller + 1); #else refClk = BOARD_GetTpmClock(gStackTimerInstance_c); prescaller = mTpmConfig.prescale; result = refClk / (1 << prescaller); #endif return result; }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍
View full article
Commissioner Authentication server for new Thread devices and the authorizer for providing the network credentials they require to join the network. A device capable of being elected as a Commissioner is called a Commissioner Candidate. Devices without Thread interfaces may perform this role, but those that have them may combine this role with all other roles except the Joiner. This device may be, for example, a cell phone or a server in the cloud, and typically provides the interface by which a human administrator manages joining a new device to the Thread Network. Commissioner Candidate A device that is capable of becoming the Commissioner, and either intends or is currently petitioning the Leader to become the Commissioner, but has not yet been formally assigned the role of Commissioner. Commissioner Credential A human-scaled passphrase for use in authenticating that a device may petition to become the commissioner of the network. This credential can be thought of as the network administrator password for a Thread Network. The first device in a network, typically the initial Leader, MUST be out-of-band commissioned to inject the correct user generated Commissioning Credential into the Thread Network, or provide a known default Commissioning Credential to be changed later. Joiner A device to be added by a human administrator to a commissioned Thread Network. This role requires a Thread interface to perform and cannot be combined with another role in one device. The Joiner does not have network credentials. Joiner Router An existing Thread router or REED (Router-Eligible End Device) on the secure Thread Network that is one radio hop away from the Joiner. The Joiner Router requires a Thread interface to operate, and may be combined in any device with other roles except the Joiner role. Information extracted from the Thread Whitepapers available at threadgroup.org
View full article
       This document will address the JN5169 CMET setup and JN5169 connection setup with IQxel-MW. We also show the EVM and packet error rate results.
View full article
This guide describes the hardware for the KW38 minimum BoM development board. The KW38 Minimum BoM development board is configurable, low-power, and cost-effective evaluation and development board for application prototyping and demonstration of the KW39A/38A/37A/39Z/38Z family of devices. The KW38 is an ultra-low-power, highly integrated single-chip device that enables Bluetooth Low Energy (Bluetooth LE) or Generic FSK (at 250, 500 and 1000 kbps) for portable, extremely low-power embedded systems. The KW38 integrates a radio transceiver operating in the 2.36 GHz to 2.48 GHz range supporting a range of GFSK, an ARM Cortex-M0+ CPU, up to 512 KB Flash and up to 64 KB SRAM, Bluetooth LE Link Layer hardware and peripherals optimized to meet the requirements of the target applications. MKW38 device is also available on the FRDM-KW38 Freedom Development Board. For more information about the FRDM-KW38 Freedom Development Board, see the FRDM-KW38 Freedom Development Board User's Guide (document FRDMKW38ZUG available in the NXP Connectivity website also).
View full article
Hello community, This time I bring to you a document which explains how to run a demo from BeeKit and how to sniff it. Before to start you need to install the BeeKit Wireless Connectivity Toolkit.     I hope you find this guide useful. Enjoy this guide! Any feedback is welcome. Best regards, Earl Orlando Ramírez-Sánchez Technical Support Engineer NXP Semiconductors
View full article
       My customer asks if QN9080 can be tested with MT887x. We co-work with Anritsu Taiwan to integrate QN9080 and MT887x to perform 1M bps, 2M bps and Frame error rate test. This document will address the QN9080 setup and MT887x connection setup. We show the 1M bps, 2M bps and frame error rate results. The Anritsu equipment is applied to MT8870, MT8872 model name.        If you would like to perform the same test environment. You may contact Anritsu to get the latest "Auto-test tool " released by Anritsu and follow their SOP document to install "Auto-test tool" into PC to perform this RF validation test. 
View full article
Hello All, I designed a ultra low low cost evaluation board (ULC-Zigbee) based in Kinetis wireless MCUs, take a look at the attached PDF for the brief description.  I was able to build three of them at ~$10USD each. The ULC-Zigbee is covered under the GNU General Public License. The required files to build the board are attached, it measures 30 x 50mm. My partner AngelC   wrote a sample code. The software basically communicates wirelessly the ULC-Zigbee board with a USB-KW24D512. An FXOS8700 is externally connected through the prototype board connector and the magnetic and acceleration values are then wirelessly transmitted to the USB stick, then the values can be printed in a HyperTerminal. The attached zip file contains the following files: File name Description ULC-Zigbee-EBV_V10.pdf Brief description of the ULC-Zigbee board MKW2x_Eagle_library.lbr  Required EAGLE CADSOFT LIBRARY ULC-Zigbee-EBV_V10.brd EAGLE v6.5 Board ULC-Zigbee-EBV_V10.sch EAGLE v6.5 Schematic ULC-Zigbee-EBV_V10_SCH.pdf ULC-Zigbee board schematic ULC-Zigbee-EBV_V10_BOM.xlsx Bill of materials ULC-Zigbee-EBV_V10_GERBER_FILES.zip Gerber files WirelessUART_MKW2x_v1.3_eCompass_TX_v1.zip ULC-Zigbee board sample software WirelessUART_MKW2x_v1.3_eCompass_RX_v1.zip USB-KW24D512 sample software     Hope it helps!   -Josh   Este documento fue generado desde la siguiente discusión:Ultra Low Cost Zigbee Evaluation Board
View full article
The MCU in the KW40/30Z has various available very low power modes. In these power modes, the chip goes to sleep to save power, and it is not usable during this time (it can however receive different kinds of interruptions that could wake it up). The very low power modes supported by the microcontroller are: The KW40Z connectivity software stack has 6 predetermined deep sleep modes. These deep sleep modes have different configurations for the microcontroller low power mode, the BLE Link Layer state and in which ways the device can be awaken. These predetermined DSM (Deep Sleep Modes) are: * VLLS0 if DCDC is bypassed. VLLS1 with either Buck or Boost. ** Available in Buck mode only. Having said that, if you want the lowest possible consumption by the MCU, while also being able to wake up your application automatically with a timer (achieved with VLSS1), there is no DSM available. You can, however, create your own Deep Sleep Mode with low power timers enabled. Please note that VLSS1 has the lowest possible consumption when using a DCDC converter. When in bypass mode, the lowest possible consumption is achieved with VLSS0. To create your Deep Sleep Mode, you should start with the function that will actually handle the board going into deep sleep. This should be done in the PWR.c file, along with the rest of the DSM handler functions. This function is quite similar to the ones already made for the other deep sleep modes. Link layer interruptions, timer settings and the low power mode for the MCU are handled here. /* PWR.c */ #if (cPWR_UsePowerDownMode) static void PWR_HandleDeepSleepMode_7(void) {   #if cPWR_BLE_LL_Enable   uint16_t bleEnabledInt; #endif   uint8_t clkMode;   uint32_t lptmrTicks;   uint32_t lptmrFreq;     PWRLib_MCU_WakeupReason.AllBits = 0;   #if cPWR_BLE_LL_Enable    if(RSIM_BRD_CONTROL_BLE_RF_OSC_REQ_STAT(RSIM)== 0) // BLL in DSM   {     return;   bleEnabledInt = PWRLib_BLL_GetIntEn();   PWRLib_BLL_ClearInterrupts(bleEnabledInt);      PWRLib_BLL_DisableInterrupts(bleEnabledInt); #endif     if(gpfPWR_LowPowerEnterCb != NULL)   {     gpfPWR_LowPowerEnterCb();   }     /* Put the device in deep sleep mode */ #if cPWR_DCDC_InBypass    PWRLib_MCU_Enter_VLLS0(); #else   PWRLib_MCU_Enter_VLLS1(); #endif     if(gpfPWR_LowPowerExitCb != NULL)   {     gpfPWR_LowPowerExitCb();   }   #if cPWR_BLE_LL_Enable    PWRLib_BLL_EnableInterrupts(bleEnabledInt);        #endif      PWRLib_LPTMR_ClockStop();   } #endif /* #if (cPWR_UsePowerDownMode) */ ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Remember to add this function to the deep sleep handler function array: /* PWR.c */ const pfHandleDeepSleepFunc_t maHandleDeepSleep[]={PWR_HandleDeepSleepMode_1,                                                     PWR_HandleDeepSleepMode_2,                                                     PWR_HandleDeepSleepMode_3,                                                     PWR_HandleDeepSleepMode_4,                                                     PWR_HandleDeepSleepMode_5,                                                     PWR_HandleDeepSleepMode_6,                                                     PWR_HandleDeepSleepMode_7                                                    }; ‍‍‍‍‍‍‍‍‍‍ This function should allow your device to go to sleep. It does the strictly necessary things before the device goes to sleep: disables link layer interruptions, gets the configuration for the low power timer and it starts the timer. Please note that when the board is in either Buck or Boost DCDC mode, only VLSS1 is supported. When the device is in bypass mode, VLSS0 can be chosen. Now that the deep sleep handler is done, there are some changes that have to be made to have a proper execution. In the PWR_Configuration.h file, for example, there is an error message when the parameter cPWR_DeepSleepMode is larger than 6 (the default DSM modes), but, since you have added a new deep sleep mode, this number should be changed to 7: #if (cPWR_DeepSleepMode > 7 )  // default: 6   #error "*** ERROR: Illegal value in cPWR_DeepSleepMode" #endif ‍‍‍ Other changes that have to be made are the Low Leakage Wake Up unit and the deep sleep mode configurations. To change the LLWU configuration, you should add a case for the new deep sleep mode in the PWRLib_ConfigLLWU() function: /* PWRLib.c */ void PWRLib_ConfigLLWU( uint8_t lpMode ) {   switch(lpMode)   {   case 1:     LLWU_ME = gPWRLib_LLWU_WakeupModuleEnable_BTLL_c | gPWRLib_LLWU_WakeupModuleEnable_LPTMR_c;   break;   case 2:     LLWU_ME = gPWRLib_LLWU_WakeupModuleEnable_BTLL_c;   break;   case 3:     LLWU_ME = gPWRLib_LLWU_WakeupModuleEnable_LPTMR_c | gPWRLib_LLWU_WakeupModuleEnable_DCDC_c;   break;   case 4:   case 5:     LLWU_ME = gPWRLib_LLWU_WakeupModuleEnable_DCDC_c;    break;   case 6:     LLWU_ME = 0;   break;   case 7: /* The new deep sleep mode can be awaken through a Low Power Timer timeout */     LLWU_ME = gPWRLib_LLWU_WakeupModuleEnable_LPTMR_c;   break;   } }  } #endif /* #if (cPWR_UsePowerDownMode) */ ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Once this case has been added, you should change the function that calls PWRLib_ConfigLLWU(), PWRChangeDeepSleepMode(): /* PWR.c */ bool_t PWR_ChangeDeepSleepMode (uint8_t dsMode) { #if (cPWR_UsePowerDownMode)   if(dsMode > 7) //Since you’ve added an extra DSM, this is now 7 (default: 6)   {      return FALSE;   }    PWRLib_SetDeepSleepMode(dsMode); PWRLib_ConfigLLWU(dsMode); #if (cPWR_BLE_LL_Enable)    PWRLib_BLL_ConfigDSM(dsMode);   PWRLib_ConfigRSIM(dsMode); #endif    return TRUE;   #else   return TRUE; #endif  /* #if (cPWR_UsePowerDownMode) */ } ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Now, since you’ll be using a Low Power Timer, you should modify the maLPModeUseLPTMR[] constant in the PWRLib.c file, indicating that you will use a low power timer: /* PWRLib.c */ const uint8_t maLPModeUseLPTMR[]={0,1,1,1,0,0,1,1}; //We add the last 1. default: {0,1,1,1,0,0,1} ‍‍‍ You should add a case for your new low power mode in the PWRLib_ConfigRSIM(). Here you will handle the BLE link layer whilst the device is in low power mode. This function can be found in the PWRLib.c file: /* PWRLib.c */ void PWRLib_ConfigRSIM( uint8_t lpMode ) {   switch(lpMode)   {   case 1:   case 2:       RSIM_BWR_CONTROL_STOP_ACK_OVRD_EN(RSIM, 0);       RSIM_CONTROL |= RSIM_CONTROL_BLE_RF_OSC_REQ_EN_MASK | RSIM_CONTROL_BLE_RF_OSC_REQ_INT_EN_MASK | RSIM_CONTROL_BLE_RF_OSC_REQ_INT_MASK;     break;   case 3:   case 4:   case 5:       RSIM_CONTROL &= ~(RSIM_CONTROL_STOP_ACK_OVRD_EN_MASK | RSIM_CONTROL_BLE_RF_OSC_REQ_EN_MASK | RSIM_CONTROL_BLE_RF_OSC_REQ_INT_EN_MASK);       RSIM_CONTROL |= RSIM_CONTROL_BLE_RF_OSC_REQ_INT_MASK;     break;   case 6:       RSIM_CONTROL &= ~(RSIM_CONTROL_STOP_ACK_OVRD_EN_MASK  | RSIM_CONTROL_BLE_RF_OSC_REQ_INT_EN_MASK);       RSIM_CONTROL |= RSIM_CONTROL_BLE_RF_OSC_REQ_INT_MASK | RSIM_CONTROL_BLE_RF_OSC_REQ_EN_MASK;     break;   case 7: //@PNN       RSIM_CONTROL &= ~(RSIM_CONTROL_STOP_ACK_OVRD_EN_MASK | RSIM_CONTROL_BLE_RF_OSC_REQ_EN_MASK | RSIM_CONTROL_BLE_RF_OSC_REQ_INT_EN_MASK);       RSIM_CONTROL |= RSIM_CONTROL_BLE_RF_OSC_REQ_INT_MASK;     break;   } } ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Your low power mode awaken by a low power timer should now be ready. To change the deep sleep mode and the time the device will be in deep sleep mode before it is awaken, use these functions in your application: PWR_ChangeDeepSleepMode(7);                                     /* Change deep sleep mode */ PWR_SetDeepSleepTimeInMs(YOUR_DEEP_SLEEP_TIME_IN_MS);           /* Time the device will spend on deep sleep mode */ PWR_AllowDeviceToSleep();                                      /* Allows the device to go to deep sleep mode */ PWR_DisallowDeviceToSleep();                                   /* Does not allows the device to go to deep sleep mode */ ‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍
View full article
As mentioned in this other post, its important to have the correct trim on the external XTAL. However, once you have found the required trim to properly adjust the frequency, it is not very practical to manually adjust it in every device. So here is where changing the default XTAL trim comes in handy. KW41Z With the KW41 Connecitivity Software 1.0.2, it is a pretty straightforward process. In the hardware_init.c file, there is a global variable mXtalTrimDefault. To change the default XTAL trim, simply change the value of this variable. Remember it is an 8 bit register, so the maximum value would be 0xFF. KW40Z With the KW40, it is a similar process; however, it is not implemented by default on the KW40 Connectivity Software 1.0.1, so it should be implemented manually, following these steps: Create a global variable in hardware_init.c to store the default XTAL trim, similar to the KW41:  /* Default XTAL trim value */ static const uint8_t mXtalTrimDefault = 0xBE;‍‍‍‍‍‍‍‍ Overwrite the default XTAL trim in the hardware_init() function, adding these lines after NV_ReadHWParameters(&gHardwareParameters):    if(0xFFFFFFFF == gHardwareParameters.xtalTrim)   {       gHardwareParameters.xtalTrim = mXtalTrimDefault;   }‍‍‍‍‍‍‍‍‍‍‍‍ Add this define to allow XTAL trimming in the app_preinclude.h file:  /* Allows XTAL trimming */ #define gXcvrXtalTrimEnabled_d  1‍‍‍‍‍‍‍ Once you have found the appropriate XTAL trim value, simply change it in the global variable declared in step 1.
View full article
Aiming to increase the reach of card and mobile payment, Europay, Mastercard and Visa (EMV) point of sale (POS) terminals are getting more lightweight, replacing hardware security with software and back-end security. Off-the-shelf mobile devices, like your smart phone, can become an acceptance point for payment cards, a so-called SoftPOS.
View full article
1 Introduction Two development boards transmit control information through ble. One development board connects to paj7620 and provides gesture information through IIC bus. The other development board uses ble and USB HID. Ble is used to receive data, and USB HID is used to simulate keyboard input and control ppt nxf56274_0-1618816281761.png                  Figure  1 2 Preparation We need two development boards qn908x and gesture control device paj7620. We use IAR as development enviroment.The example we use is temperature_sensor, and temperature_ colloctor. The SDK version is 2.2.3   3 Code 3.1  temperature_sensor code We want to implement IIC to read gesture information from paj7620 and send data. The pins used by IIC are PA6 and PA7 Simply encapsulate the IIC reading and writing code in the code to create i2c_ operation.c and i2c_ operation.h. Realize IIC initialization and reading / writing register function in it nxf56274_1-1618816281828.png                        Figure  2 nxf56274_2-1618816281867.png                        Figure  3   3.1.1 After having these functions, we begin to write gesture recognition code. First, we add two blank files paj7620.c and paj7620.h into our project.   Select bank register area nxf56274_3-1618816281931.png                               Figure 4   Wake up paj7620 to read device state nxf56274_4-1618816281970.png                    Figure 5   Initialize device nxf56274_5-1618816282039.png                    Figure 6   Gesture test function nxf56274_6-1618816282053.png                                   Figure 7   3.1.2 When you are ready to read the device information, You should initialize IIC and paj7620 in BleApp_Init function nxf56274_7-1618816282094.png                                Figure 8 In principle, we need to create a custom service for the PAJ device, but we replace the temperature data as our gesture control data. If you want to create a custom service, refer to this link custom profile   3.1.3 Create a timer that sends gesture data regularly. In file temerature_sensor.c Define a timer,static tmrTimerID_t dataTimerId; Allocate a timer, dataTimerId = TMR_AllocateTimer(); Define the callback function of this timer nxf56274_8-1618816282129.png                                           Figure 9 Start timer nxf56274_9-1618816282166.png                                    Figure 10 Close the low power mode. #define cPWR_UsePowerDownMode 0 3.2 temperature_collector code The most important thing here is to port USB HID into our project. The USB  example we use is the USB keyboard and mouse. 3.2.1 Add the OSA and USB folder under the example to the project directory, and copy the file to the corresponding folder according to the file structure of the original example. nxf56274_10-1618816282200.png                      Figure 11 3.2.2 Add header file directory after completion nxf56274_11-1618816282245.png                                           Figure 12 At the same time, in this tab, add two macro definitions USB_STACK_FREERTOS_HEAP_SIZE=16384 USB_STACK_FREERTOS   3.2.3 Next, we need to modify the main function in usb example . Open composite.c file. nxf56274_12-1618816282295.png                      Figure 13 It calls the APP_task. So this function also need to be modified. nxf56274_13-1618816282323.png                                   Figure 14 3.2.4Find hid_mouse.c,Comment function USB_DeviceHidMouseAction Find hid_keyboard.h. Define the gesture information. macro_gesture.PNG                                  Figure 15 Find hid_keyboard.c. We need to modify the function USB_DeviceHidKeyboardAction as following figure. nxf56274_15-1618816282485.png                                                  Figure 16   Among them, we also need to implement the following function. When the up hand gesture is detected, the previous ppt will be played. The down hand gesture will be the next PPT, the left hand gesture will exit PPT, and the forward hand gesture will play ppt nxf56274_16-1618816282625.png                                                  Figure 17 It also refers to an external variable gesture_from_server. The variable definition is in file temperature_ collocation.c,.     3.2.5 After that, let's go to BleApp_Statemachinehandler function in temperature_colloctor.c. In case mApppRunning_c, we will call usb_main to initialize USB HID nxf56274_17-1618816282665.png                                                  Figure 18 3.2.6 In BleApp_PrintTemperature, we will save the gesture data to gesture_from_server nxf56274_18-1618816282756.png                                                         Figure 19 We finished the all steps.        
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-332703
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343043
View full article
Generality on the Oscillation Margin Outline It is a margin to the oscillation stop and the most important item in the oscillation circuit. This margin is indicated by ratio based on the resistance of crystal, and it shows how amplification oscillation capability the circuit has. The oscillation circuit can theoretically operate if the oscillation margin is 1 or more. However, if oscillation margin is close to 1, the risk of operation failure will increase on module due to a too long oscillation start up time and so on. Such problems will be able to be solved by a larger oscillation margin. It is recommended to keep 3 times or more as oscillation margin during the startup of the oscillation. Factor of 10 is commonly requested for Automotive at startup and steady state. 5 is enough for IoT market. However, some providers accept to have 3 times as oscillation margin for steady state. Here below is an oscillation example to explain better the phenomenon: At start up, the configuration is set internally by the hardware in order to be sure to start the oscillation, the load capacitor is 0pF. After this time, it is the steady state and the load capacitor from the internal capabank is taken into account. laurent_rouzier_2-1743663107235.png   If load capacitor is not set correctly with the right oscillator gain, the oscillation will not be maintained after the start up. laurent_rouzier_3-1743663151047.png   The oscillator gain value will also depend on the resisting path on the crystal track.  A good way to evaluate it is to add a resistor on the crystal path and try to launch the oscillation. In the SDK, the gain and the load capacitor can set directly in the application code. Calculation The oscillation margin is able to be calculated as follows: The oscillation margin calculation is based on the motional resistor Rm by formula below : laurent_rouzier_5-1743663216381.png ESR: Crystal Equivalent Series Resistance C0: Shunt Capacitance Rm1: Motional resistor Cm1: Motional Capacitance Lm1: Motional Inductance fosc: oscillation frequency, measured with Rs_Max mounted fr: resonance frequency of the Rm1Lm1Cm1 of the crystal from (1) :  laurent_rouzier_6-1743663251430.png   Oscillation margin is:              laurent_rouzier_7-1743663273516.png        Example: for the EVK board’s 32kHz crystal (NX2012SE) ESR    80000,0 Ω Rm1    79978,2 Ω Lm1    3900 H Cm1   6,00E-15 F C0      1,70E-12 F CL      1,25E-08 F fr        32901,2 Hz fosc    32771 Hz Series Resistor Rsmax        7,50E+05 Ω Oscillation Margin   10,3   Measurement Requirements for measurement PCB (for the test, it is recommended to add a series resistor on the EXTAL32k trace) Crystal unit (with equivalent circuit constants data) Resistors (SMD) Measurement equipment (Oscilloscope, Frequency counter or others capable to observe oscillation) Add a resistor to the resonator in serial and check if the oscillation circuit works or not. laurent_rouzier_8-1743663470883.png   If the oscillation is confirmed by 2), change the resistor to larger. If there is no oscillation, change the resistor to smaller. Find out the maximum resistor (=Rs_max) which is the resistor just before the oscillation stops. Measure the oscillating frequency with Rs_max. Calculate the oscillation margin based on the Rs_max.   Notes The Oscillation margin is affected not only by crystal characteristics but also parts that compose the oscillation circuit (MCU, capacitor and resistor). Therefore, it is recommended to check the oscillation margin after the MCU functionality is checked on your module. The series resistor is only for evaluation. Please do not use this resistor in actual usage. It is recommended to check the functionality of your module also. It is possible that the module does not work correctly due to a frequency shift on oscillation circuit and so on. A test jig and socket could be used in measurement but stray of them will give influence for oscillation margin.   KW47/MCX W72 product oscillation margin overview 32MHz crystal NXP recommends to use the quartz NDK NX1612SA 32MHz (EXS00A-CS15781) to be compliant with the +/-50ppm required in Bluetooth LE. Using the current SDK, NXP guarantees an oscillation margin of 10 for startup and steady state commonly used by Automotive customers. Higher oscillation margin can be reached by using higher ISEL and CDAC parameters with some drawback respectively on the power consumption and the clock accuracy. ( the load capacitance bank (CDAC) and the oscillator amplifier current (ISEL)) NDK recommended / target values for oscillation margin is informed case by case. On a general basis, the requested oscillation margin has to be between the recommended value and 3 times this value. "NDK quartz provider (FR) explains this oscillation margin specification is only mandatory at the start-up phase, not at the steady state. Starting the oscillation is the phase that needs more energy. That's why the gain of the oscillator gain is at the maximum value which means not optimal consumption. When the oscillation stability is reached, the gain could be reduced to save power. The oscillation will not be affected.  Keep in mind a quartz oscillates by mechanical effect. So, when the oscillation is starting you need the highest energy to emulate it. By its own inertial, you need less energy to maintain the mechanical oscillation. NDK provides a good picture of this. Starting up a crystal into oscillation is like a train what you would like to start moving. At the beginning the train is stopped and you need a lot of energy to start running. When the train is running at its nominal speed, you need less effort to maintain that movement and a very big effort to stop it completely."   Example: for the oscillation margin 10 (Series Resistor Rs_max = 560 Ω) The CDAC/ISEL area where the oscillation starts and propagates in the internal blocks is defined (green color raws) in the table below. The frequency accuracy is indicated for some of them: laurent_rouzier_10-1743663991258.png     32kHz crystal NXP recommends to use the quartz NDK NX2012SE (EXS00A-MU01517) or NDK NX2012SA (EXS00A-MU00801) to be compliant with the +/-500ppm required in Bluetooth LE. using the current SDK, the oscillation margin with this quartz is 10 with some limitation on the Crystal load capacitance selection (Cap_Sel) and the Oscillator coarse gain amplifier (ESR_Range) values, with some drawback respectively on the power consumption and the clock accuracy. For an oscillation margin at 10 for instance, the Capacitor value from the databank (Cap_Sel) is limited (green area) as shown in the graph below: laurent_rouzier_11-1743664069050.png   Example: for an oscillation margin at 6.3, if the load cap is set at 12pF and the ESR_Range to 3, the 32kHz frequency accuracy will be around -23ppm. From this point, the oscillation margin can be enlarged to 10.3 by decreasing the load cap to 6pF but the accuracy will be degraded (110ppm).   For an Oscillation margin at 10, the graph below is showing the ESR_Range versus the load cap. The possible load cap variation range (in green) is larger when the ESR_Range increases: laurent_rouzier_12-1743664104826.png   Example: at oscillation margin 10.3, the clock accuracy can be improved from 111ppm to 21ppm by setting the ESR_range 2 to an ESR_Range 3 but the current consumption will be increased to 169.5nA. Another important point is that for a given ESR_Range value, getting higher the load cap is much more increasing the current than in the example above.   Remark: Under a high oscillation margin condition, the crystal voltage will be smaller.   Other possible ways to improve the oscillation margin exist: - Use external capacitor instead of internal capacitor banks. Oscillation margin goes up to 10. - Use the internal 32kFRO is supported for BLE (target:+/-500ppm)              
View full article
This application note describes the usage of the DC-DC Switching Mode Power Supply (SMPS) converter for the MKW39A/38A/37A/38Z/37Z families. This document covers operating voltages, types of circuit operation, hardware design guidelines, software configuration, and power capabilities. It's a complementary document from the AN5025. The DC-DC converter for MKW3x is a dual output converter that supports two operating modes: Bypass and Buck. In Bypass mode, the DC-DC converter is disabled and the supply pins of the microcontroller must be supplied externally. In Buck mode, the DC-DC converter is enabled and requires a DC supply in the range of 1.8 V to 4.2 V (during startup the minimum required is 2.1 V).
View full article
The homologation requirements in China (MIIT [2002]353) obviously are planned (end of December 2022) to be sharpened (MIIT publication from 2021-01-27: “Notice on Matters Related to Radio Management in the 2400MHz, 5100MHz and 5800MHz Bands”).   A modification register is need on the KW38 and KW36 to pass the new Chinese  requirement with acceptable margin: PA_RAMP_SEL value must be set to 0x02h (2us) instead of 0x01h (1us default value) Modification SW: XCVR_TX_DIG_PA_CTRL_PA_RAMP_SEL(2) in the nxp_xcvr_common_config.c All the details are in the attached file.   Note: This SW modification is for China country only.
View full article