University Programs Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

University Programs Knowledge Base

Discussions

Sort by:
Welcome to the NXP Cup!  The following pages are designed to introduce students to the concepts of robotics and the components of the NXP Cup Car. Programming microcontrollers is challenging, and the content here is developed to facilitate the process of becoming a successful embedded programmer. General Information Marketplace Special offers from our Global Sponsors History of the NXP Cup Where to buy a racetrack? Mathworks Support for The NXP Cup Race Track Information Community created accessories FAQ's Assembly Directions Keil Software Offer Rules Cameras Regulations Teams' Technical Reports Hardware Concepts Embedded Systems Concepts Real world usage (Practical) Line Scan Camera MCU 101 Tutorials Kinetis FRDM-KL25Z Servo Motor NXP Cup related video series by Prof. Eli Hughes https://community.nxp.com/docs/DOC-1096 Drive (DC) Motors MathWorks basic model for using wide angle lenses on The NXP Cup Car The NXP Cup Technical Reports https://community.nxp.com/docs/DOC-1283 Motor Driver (H-Bridge) https://community.nxp.com/docs/DOC-1057 Battery New Supply location for NXP Cup kits and replacement parts with global delivery possibilities: www.landzo.com CCD sensor: http://www.landzo.com/?product-52.html CCD camera: http://www.landzo.com/?product-51.html Power Motor control unit: http://www.landzo.com/?product-50.html Car kit without Electronics: http://www.landzo.com/?product-49.html In case of any questions or issues, please contact Bella at 汪瑞 <[email protected]> Connect with teams in your region! Brazil EMEA Malaysia Mexico North America Taiwan
View full article
Overview The FRDM-TFC is a convenient "shield" that can drive up to two DC motors (5A per channel), two servos and I/O for the Freescale cup line scan camera and Hall effect sensors.  This board mates with the KL25Z Freedom board for primary usage with a Freescale Cup car. Features: 2 channel Motor Driver ICs (MC33887APVW) 2 channel servo Outputs Dual Linescan Camera interfaces Two inputs for speed sensors Two potentiometers for user functions Two push buttons for user functions 4 Position DIP Switch for user function 4 LEDs (green) for battery indicator or user functions Design Files Rev A is attached to this document. Rev B is attached to this document Code Examples Codewarrior "Bare Metal" Example Code: All Codewarrior based code examples for the FRDM-TFC are hosted on in a Subversion repository on Google Code: frdm-tfc -   Example code for the FRDM-TFC Shield - Google Project Hosting You can check out the code with your favorite SVN client.   Static releases are available in the attachments section of this page.  The current release is "R1.0" mbed.org Example Code: https://mbed.org/components/Freescale-Cup-with-FRDM-KL25Z/ Videos FRDM TFC EXAMPLE CODE GETTING STARTED FRDM-TFC_DEMO 0 and 1 FRDM-TFC_DEMO 2 and 3
View full article
How does a DC Motor work? The DC motor is a machine that transforms electric energy into mechanical energy in form of rotation. Its movement is produced by the physical behavior of electromagnetism. DC motors have inductors inside, which produce the magnetic field used to generate movement. But how does this magnetic field changes if DC current is being used? An electromagnet, which is a piece of iron wrapped with a wire coil that has voltage applied in its terminals. If two fixed magnets are added in both sides of this electromagnet, the repulsive and attractive forces will produce a torque. Then, there are two problems to solve: feeding the current to the rotating electromagnet without the wires getting twisted, and changing the direction of the current at the appropriate time. Both of these problems are solved using two devices: a split-ring commutator, and a pair of brushes. As it can be seen, the commutator has two segments which are connected to each terminal of the electromagnet, besides the two arrows are the brushes which apply electric current to the rotary electromagnet. In real DC motors it can be found three slots instead of two and two brushes. This way, as the electromagnet is moving its polarity is changing and the shaft may keep rotating. Even if it is simple and sounds that it will work great there are some issues which make these motors energy inefficient and mechanically unstable, the principal problem is due to the timing between each polarity inversion. Since polarity in the electromagnet is changed mechanically, at some velocities polarity is changing too soon, which result in reverse impulses and sometimes in changing too late, generating instantaneous “stops” in rotation. Whatever the case, these issues produce current peaks and mechanical instability. How a DC motor can be controlled? DC motors have only two terminals. If you apply a voltage to these terminals the motor will run, if you invert the terminals position the motor will change its direction. If the motor is running and you suddenly disconnect both terminals the motor will keep rotating but slowing down until stopping. Finally if the motor is running and you suddenly short-circuit both terminals the motor will stop. So there is not a third wire to control a DC motor, but knowing the previous behaviors it can be designed a way to control it, and the solution is an H-bridge. Look at the last evolution of the DC Motor above, you can observe that there are four gates and a motor connected between them. This is the simplest H-bridge, where the four gates represent for transistors. By manipulating these gates and connecting the upper and lower terminals to a voltage supply, you can control the motor in all the behaviors as below. Things to Consider When Using Motors With the Motor and Line scan Camera hooked up to the same board there is a significant problem with noise. The higher you turn the PWM on your drive motors the noise produced and the worse the data will appear from the camera. TO significantly reduce this noise you can simply solder an inductor directly across the 2 drive motors. This will allow you to increase the speed of the car without significantly affecting the data you receive back from the camera.
View full article
The line scan camera module consists of a CMOS linear sensor array of 128 pixels and an adjustable lens. This camera has a 1x128 resolution. Line Scan Camera Board Details Schematics, BOM, and datasheets: Line Scan Camera featuring TAOS 1401 Mounting Options You will likely want to mount the camera on a mast or boom above the car to ensure the greatest field of view. Determining the angle of orientation about the pivot at the top of the boom will change the “look ahead” distance of the camera and enable more efficient steering algorithms DIY Camera Mounts Solution Overview One method of implementation is to take the entire readout of the camera and store it in the memory. Then a line detection algorithm can be used to locate the position of the black line. Due to varying lighting conditions, some level of pixel thresholding may be necessary as the intensity differences across the data may not always produce a clear indication of the line location. A good approach is to use an algorithm that looks for changes in the magnitude of voltage from one portion of the array to another, since the camera’s AO magnitude is directly related to the brightness the pixel array senses. If the microcontroller finds a significant decrease in magnitude followed by large increase in magnitude this would give us a good indication of the location of the line. For this a derivative function can be utilized. Once we have successfully determined the position of the black line, immediately adjust the wheels to adjust the direction of the car so that the black line will remain in the center of the camera’s view. Sample camera output (for illustrative purposes only) The camera outputs an analog signal from 0 to 5V depending on the grey-scale value of the image. to simplify our sample we will assume that we have set limits for the line and have transformed the data to digital bits using a threshold value. 0’s are high intensity (non-line locations), 1’s are low intensity (black or line locations) 10000000000000000000000000000000001111101000000000000000000010000000000000000 Since the camera provides a 128x1 bit picture, and the camera will be pointing down at the track which is a fixed width. A control algorithm should be developed to line up the 1’s in the center of the 128 bits. The center of the field of view will be require calibration and testing, but it is assumed that the camera will remain in a fixed location pointing down the center of the forward looking axis of rotation. Signals For normal operation of the camera, the following signals must be produced and processed: CK (clock) - latches SI and clocks pixels out (low to high) continuous signal SI (serial input to sensor) begins a scan / exposure discrete pulses, pulse must go low before rising edge of next clock pulse AO (analog output) - Analog pixel input from the sensor (0-Vdd) or or tri-stated The CK and SI signals are simple ON/OFF signals which can be produce using a GPIO Pin, setting the pin high and low corresponding to the desired exposure time of the camera. The only other requirement is to read the Analog Output of the camera which requires the initialization of the Analog Module and setting it to the proper pinout. Acutal camera output image: Yellow = SI, Green = Camera Signal, Purple = clock More camera waveforms and information (Power Point) available here This link shows a video of the camera connected to the oscilloscope http://www.youtube.com/watch?v=YOAd3ERnXiQ To obtain this signal, connect channel 1, 2 and 3 of an oscilloscope to the SI pulse (Trigger off this signal), CLK, and AO signals. Timing The timing for creation and read of the signals is crucial and is detailed in the diagram below. This information can also be found in the Line Scan Datasheet. Analog Read: The Analog Output (AO) signal from the camera needs to be processed and read by the microcontroller's Analog to Digital Converter (ADC). This ADC device converts a continuous signal into a discrete number which is proportional to the signal voltage. An 8 bit ADC has 256 discrete levels (2^8). If a analog signal between 0 and 5 volts is sampled, a digital discrete number of 0 would correspond to zero volts, and a digital discrete number of 255 would correspond to 5 volts. A number such as 145w would correspond to about 2.8 volts. The maximum signal sample rate is limited by the microcontroller. Proper configuration of the ADC peripheral and the multiplexer of the chip will configure a pin to read in an analog signal when calling the function. More details on analog to digital converters can be found on the wikipedia site here. Read/Write In write mode, the GPIO pin can be set, cleared, or toggled via software initiated register settings. Microcontroller Reference Manual: Analog to Digital Converter You will find high level information about GPIO usage in several different areas of a reference manual. See the reference-manual article for more general information. Relevant Chapters: (see GPIO chapters for clock and SI Creation) Introduction: System Modules: System Integration Modules (SIM) - provides system control and chip configuration registers Chip Configuration: Signal Multiplexing: Port control and interrupts Focusing the camera: Once the sensor is perfectly working the next step is to find the best position of the lens that will generate the clearest images. The best way to do it is using an oscilloscope: Connect the SI and AO signals to the oscilloscope Set the SI pulse so that it can be clearly seen and then trig the AO signal with the SI signal using the trig function Fix the camera looking at a sheet of paper with a black line in the center The image of the black line will appear on the oscilloscope screen Screw the camera until you find the position where the line seems the clearest Camera Circuit   5 wires must be connected ground power SI CLK AO Camera Limitations   According to the datasheet:   " The sensor consists of 128 photodiodes arranged in a linear array. Light energy impinging on a photodiode generates photocurrent, which is integrated by the active integration circuitry associated with that pixel. During the intergration period, a sampling capacitor connects to the output of the integrator through an analog swith. The amount of charge accumulated at each pixel is directly proportional to the light intensity and the integration time." Integration Time: T T = (1/fmax)*(n-18)pixels + 20us, where n is the number of pixels Minimum integration time: 33.75us Maximum integration time: capacitors will saturate if exceeding 100ms frequency range 5 Khz - 8 Mhz (8 Mhz is fmax in equation above) The integration time is the following: It occurs between the 19th CLK cycle and the next SI pulse. The CLK frequency itself has little to do with the integration time. One each rising edge, the clock outputs one of the previously sampled intensity values. This means that integration time should be set by varying the time between SI pulses, not changing the clock frequency. Make the CLK frequency high, and have as much time as needed between the two SI pulses to obtain the desired intensity value. Pro Tips: #1 - Avoid Light Noise Light can be transmitted through the pcb on the back of the camera. This unwanted extra light shining on the CMOS linear sensor can induce significant errors into your signals received. A shroud or housing for the camera unit can easily eliminate this problem. One of the easiest solutions is to place a piece of electrical tape across the back of the camera in the highlighted area indicated in the picture below. #2 - Know your Settings When testing the car on the track or transporting it, it is not uncommon for the focus on the camera to loosen or change. Therefore it is recommended that after adjusting your camera focus for maximum performance you make mark (ex. metallic sharpie) between the lens and its body so you can realign the camera lens to it's proper position easily if it does shift. #3 - Know your Zone When hooking up the linescan camera, regardless of position or focus there is a drop off at each end of the image data. This is easily viewed with an oscilloscope. This effect is undesirable, particularly when you are finding your line position utilizing a derivative approach. These fallouts cause erroneous derivative values, and hence a poor line position solution. Two solutions we found useful were: (1) Ignoring the first 10-15 pixels and last 10-15 pixels of the image data array, and then determining the line position; (2) Often when making decisions in the code as to where the line was at it was found useful to use a threshold value for the difference in the derivative position, and secondly a binary threshold on the camera data. Note that the falloff depends on camera focus, position, etc. Therefore, these threshold values and pixels in which to ignore are relative to a specific instance. The problem however is common to the camera. #4 - Buffer Data Since the camera can read the line very quickly while the servo can only update every 20ms, there are multiple camera reads before the servo can update, if you are reading the camera fast and then overriding without saving them in some form then those camera reads are being wasted and are better off not having occurred. What can help is to create some sort of filter by bringing new values into an array with previous values and preforming some sort of averaging. The following code will take the new line position value and place it in a 1xA array where A is defined by CAMERA_AVG. NO AVERAGING IS OCCURRING HERE all that is happening is the camera values are being saved in a simple array, what is done with them is up to you. The way this works is that it shifts the entire array so the oldest data point is discarded in order to make room for the new line position at the other end of the array. It will only adds the new value if there is one available if not it copies the previous first position value to the new first position value. CAMERA_AVG => an integer value for how long the averaging length will occur gfpLineAverage => global floating point array of camera center line values fpLinePos => returned from read camera this is the center line position ReadCamera() => is the read camera function call returns a floating point value of fpLinePos // this will shift the values up and throw away the oldest value // then add a new reading for (i=CAMERA_AVG;i>0;i—) { gfpLineAverage[i]=gfpLineAverage[i-1]; } // if no line was detected the previous camera value will be passed on if (fpLinePos=ReadCamera()) { gfpLineAverage[0]= fpLinePos; } For example an array of of center line position values ranging from 0-127 could look like. Initial values [51 50 52 54 58 55] New position of 45 read [45 51 50 52 54 58] New position of 44 read [44 45 51 50 52 58] No value read [44 44 45 51 50 52] No value read [44 44 44 45 51 50] New position of 50 read [50 44 44 44 45 51] Program Exercise Specifics of how to configure the K40 ADC, to create the delay code is covered in the K40: Line Scan Camera Tutorial. Additional Training Resources Freescale Motor Control Tutorial Freescale Lecture 1: Introduction and Motor Basics Freescale Lecture 2: Pulse Width Modulaiton Freescale Lecture 3: Control Design Freesacle Lecture 4: Speed and Position Freescale Lecture 5: MPC5607B Overview Additional Resources Freescale app note on interfacing with a linescan camera Freescale app note on interfacing with an RCA camera
View full article
All results of the NXP CUP survey can be found here.
View full article
A special thanks to emh203 who has worked with us to create this wonderful series of videos covering general MCU topics and more specific Freescale Cup training.  We look forward to more videos in the coming months.  Stay tuned. Please, please, please like, rate and comment on the videos so we get the feedback!  Thanks and enjoy! Getting Started with Embedded Systems FRDM-KL25Z Orientation Freescale Cup Training
View full article
Getting Started with the NXP CUP These pages help you with the question of how to achieve the goal of creating an autonomous vehicle that quickly navigates around a track (timed race) and solves precision tasks (Figure 8, Speed limit zone, Obstacle avoidance) What is a Microcontroller? For information on what a microcontroller is head to the microcontrollers article. Getting Started - Learn to Program a microcontroller First off, you are going to need to know C programming. For a crash-course head to c-programming-for-embedded-systems. The classic first application to learn how to program a microcontroller is to get through the process of Blinking an LED. This wiki contains a tutorial for each of the Cup microprocessors which simplifies the process of setting up the evaluation board, installing the Integrated Development Environment, and programming the board with a simple set of software which blinks a LED. The Blink a LED tutorial is the first of 4 tutorials designed to familiarize students with the process of designing a cup car. These four tutorials will introduce students to many of the fundamentals of robotics, the software used to control the locomotion and sensors on an autonomous line following vehicle, and provide example code which help simplify the process of creating a competitive entry in the NXP CUP. Here is an outline of the Basic Microcontroller Programming Tutorial: Read the microcontroller article Choose a microcontroller Set up the development environment Set up the microcontroller evaluation board Program A LED move to the next tutorial… Course Material from the NXP CUP professors and supporters: Thanks to our professors and NXP CUP supporters we created an exclusive starter kit. It includes lecture material, information on the car, useful tips on the board etc. Download the file below and dive into a huge support portfolio! ARC Ingenierie Files - The Champions Board! ARC Ingenierie has been very generous in providing us with their PCB layout and Gerber files to produce your own NXP CUP board. They also provided sample code and drivers plus instructions (in French) to get you started. How cool is that?! Many thanks to ARC, this is much appreciated! Download the files below. If you want to build your own board, please contact us. When do so please keep in mind to give credit to ARC university. All boards should have "HE-ARC Ingenierie" inscription.   Further support links: Information on Line Scan Camera Use The Book of Eli - Microcontrollers, robotics and warp drives Microcontrollers MCU 101 - C Programming for Embedded Systems NXP CUP Shield for the FRDM KL25Z
View full article
For details on how to use the Motors, visit theDC Motor Tutorial Images Boards before 2013 Current Board Rev. 0 Rev. 1 Technical Details Revision 1 (Schematics, design files, sample code, instructional videos) Revision 0 (Schematics) H-Bridge Specifications Freescale MC33931 Datasheet Pro Tips: #1 - Electro-Magnetic Interfence (EMI) This has been mitigated in the rev. 1 board. In many cases the dc drive motors give off much EM interference causing poor data from the camera, and decreasing the servo motor performance substantially. In most cases around a PWM value of 20-25 duty cycle at the drive motors, caused detrimental problems. This problem was remedied in two ways, (1) connecting capacitors between the motor leads, the closer to the drive motor the better; (2) There is a way to connect the camera directly to the kwikstik and bypass the motor board. #2 - Rev. 0 Board workaround to Enable Braking This has been fixed in the rev. 1 board. In order to go forward AND backwards, you have to have control over IN1 and IN2 (see table below). If you look at the schematic, you can see that IN1 is directly connected to GND. In order to enable breaking you need to lift pin 43, solder a wire to it and control it properly. Tutorials General Tutorial on the DC Motor Control Qorivva: DC Motor Tutorial Kinetis Tower: DC Motor Tutorial Design evolution of motor board prior to 2010 - Freescale Cup Cars utilized the MC33932EVB 2010~2012 - Freescale Cup teams migrated to the current Interface/Motor board featuring Dual H-Bridges [Not manufactured] Tower and Trak Compatible Interface/Motor Control Board (Design files if you want to make one!) 2013+ - FRDM-KL25Z shield
View full article
Some typical variations: Report Requirements Specific Components Usage Additional Tiers of Competition 2017 Rules per Region EMEA University Challenge 2016-2017 2016 Rules per Region Americas, Malaysia and Taiwan.​ EMEA University Program Challenge EMEA High School Challenge 2015 Rules per Region Worldwide Challenge Rules EMEA 2014 Rules per Region EMEA Worldwide Challenge Rules USA [ARCHIVE] 2013 Rules per Region Malaysia Latin America Latin America - Advanced USA Global Championship
View full article
Assembly Of The Freescale Cup Car Chassis Before you start building your program for your car, It would be better if you can assemble your car chassis first. With your car correctly assembled, you can easily test it with your different programs in the later tutorials. The followings are all the tutorials about car chassis assembly. A step-by-step car chassis assembly manual & hints (pub)  (PDF) Servo and steering assembly directions DIY Board mounting template for the TRK-MPC5604B DIY Board mounting template for the Tower System Board mounting suggestions for the FRDM-KL25Z with shield DIY Camera Mounts Wiring connections for the TRK-MPC5604B Hints and notes to chassis assembly Freescale Cup Innovation Challenge EMEA Model B car assembly file in attachment below Exploded Assembly Diagrams Chassis Build Directions [PPT] Original Manufacturer Directions [PDF]
View full article
Project Summary Skills Developed: Materials: Step 0: Prerequisite Videos Step 1: Get a FRDM-JAM Step 2: Put it Together Step 3: Download Step 4: Hack and Slash! Sound Samples Utilities, etc: Project Summary MonkeyJam will use the FRDM-K20D50 board (which has a Cortex M4 core with DSP instructions) along with the FRDM-JAM shield so you can  make your very own guitar /bass  stomp box.  The end result will be a functional DSP system that will allow you to do high quality amplifier simulation and effects. The FRDM-JAM does not limit you to DSP on musical instruments!  There are 3.5mm stereo jacks to DSP filtering any type of audio signal.    You could even use the USB interface to create a USB-MIDI Synthesizer!  Lastly,  no need to bring the house down.....  a headphone amplifier circuit is provided so you can jam out without bothering the neighbors. MBED Support coming *very soon* Skills Developed: Real Time Processing DSP Algorithms Fixed Point Mathematics 24-bit I2S Data Converter Interfacing Soldering SOIC8 and 1206 Surface mount devices Cortex CMSIS DSP Library Materials: FRDM-K20D50 FRDM-JAM Development Tools Install Codewarrior 10.5 for Microcontrollers (Eclipse) Special Edition to your  machine Example Code Get the latest copy from Github Step 0: Prerequisite Videos The videos are organized into a nice YouTube playlist: H.I.T 1: Monkey Jam - YouTube https://www.youtube.com/playlist?list=PLWM8NW5LEukgM-D5eRMtKZ8R2WfXnqKGp MonkeyJam Watch Me 1st FRDM-JAM Hardware Overview MonkeyJam Software Overview Introduction to Fixed Point Math for Embedded Systems - Part 1 of 3 Introduction to Fixed Point Math for Embedded Systems - Part 2 of 3 Introduction to Fixed Point Math for Embedded Systems - Part 3 of 3 Real Time Signal Processing Part 1 of 3 Real Time Signal Processing Part 2 of 3 Real Time Signal Processing Part 3 of 3 q31_t (Q0.31) Number Format for the CMSIS DSP Libraries and the MonkeyJam Software Guitar physics in a nutshell Ideas for hacking the MonkeyJam Step 1: Get a FRDM-JAM MonkeyJam Build Package on the FRDM-JAM site.    Please let us know if you are interested in a pre-assembled version.  If there is enough demand we will get some preassembled for purchase, I will get a Kickstarter going!   Don't be afraid to build it yourself,  Soldering is fun!  There is plenty of good stuff on the web on how to do SMT soldering.  All of the parts on the board are fairly simply once you get the hang of it and everything can be hand soldered  The key is having some decent tools. Step 2: Put it Together Attach the FRDM-JAM to the FRDM-K20D50.  The FRDM-K20D50 comes with female headers that you can solder on so the boards can be easily separated.  Note that as of Rev Gamma (current version),   it is possible to connect to a K64F.    The software isn't quite there but it hardware connections are available.   If you are unsure,  stick with the FRDM-K20D50 Step 3: Download Download the Example Software from Github.  The video "Loading and Configuring the MonkeyJam Example Software" will step you though downloading the program and doing some basic configuration. Step 4: Hack and Slash! Plug In and jam! Sound Samples Each sound sample was my Carvin Ultra-V guitar plugged direct into the MonkeyJam Board.  The output was fed to a Zoom Handy Recorder H4n (Thanks to Brandin Claar of Remodulate LLC for the recorder).  The H4N recorded the signal at 44.1KHz Sample rate @16-bit.  The sound files were converted to mono format via Goldwave.  No processing (other than a  volume boost on the files) was performed.   I listen to the recording in real-time via a line out on the H4N.  File (See Attachments) Patch Notes STE-003-Neck-a12b12g12-mlike.wav PATCH_TUBEY_CLEAN Neck Pickup Alpha Pot - 12 O'Cock Beta Pot - 12 O'Cock Gamma Pot - 12 O'Cock Pattern Similar to Metallica Sanitarium STE-005-Neck-a7b5g5-mlike.wav PATCH_TUBEY_CLEAN Neck Pickup Alpha Pot - 7 O'Cock Beta Pot - 5 O'Cock Gamma Pot - 5 O'Cock Pattern Similar to Metallica Sanitarium STE-006-Neck-a12b7g5-mlike.wav PATCH_TUBEY_CLEAN Neck Pickup Alpha Pot - 12 O'Cock Beta Pot - 7 O'Cock Gamma Pot - 5 O'Cock Pattern Similar to Metallica Sanitarium STE-007-Neck-VariousSettings-d-g-em_strum.wav PATCH_TUBEY_CLEAN Neck Pickup The pots were moved around throughout the file Strummed D-Major, G-Major and E-Minor STE-008-Neck+Bridge-VariousSettings-d-g-em_strum.wav PATCH_TUBEY_CLEAN Neck + Bridge Pickup The pots were moved around throughout the file Strummed D-Major, G-Major and E-Minor STE-009-Bridge-VariousSettings-d-g-em_strum.wav PATCH_TUBEY_CLEAN Bridge + Bridge Pickup The pots were moved around throughout the file Strummed D-Major, G-Major and E-Minor STE-010-Neck-VariousSettings-Jammy.wav PATCH_TUBEY_CLEAN Neck + Bridge Pickup The pots were moved around throughout the file B-Minor Type Jam STE-011- Bridge - Various Settings - On-Off Demo-RandomDroppedD.wav PATCH_OVERDRIVE Bridge Pickup Alpha Pot - 5 O'Cock Beta Pot - 12 O'Cock Gamma Pot - 12 O'Cock Random Dropped D twiddling STE-012- Neck - Various Settings - On-Off Demo-Jammy.wav PATCH_OVERDRIVE Neck Pickup Alpha Pot - 5 O'Cock Beta Pot - 7 O'Cock Gamma Pot - 7 O'Cock Random B-Minor twiddles (bluesy) PATCH_OVERDRIVE             +––––––––––––––––––+      +––––––––––––––––––––––––––+      +–––––––––––––––––––––+                               |                  |      |                          |      |                     |                    Signal In  |    IIR BiQuad    |      |      Hard Overdrive      |      |      IIR BiQuad     |  Signal Out       +–––––––––+>|                  +––––+>|                          +––––+>|                     +–––––––––––––+>                |   [Peaking EQ]   |      | [atan24pi Look Up Table] |      |  [Low Pass Filter]  |                               |                  |      |                          |      |                     |                               +––––––––––––––––––+      +––––––––––––––––––––––––––+      +–––––––––––––––––––––+                                                                                                                                                     0.1 < Q < 1.5    [Pot Alpha]                                     Q = 0                                                                                                                                                              50 < Fs < 750    [Pot Gamma]                                   Fs = 2000                                                                                                                                                          -20 < dbGain < 20  [Pot Beta]                                                                                                                                                                                        PATCH_TUBEY_CLEAN              +––––––––––––––––––+      +––––––––––––––––––––––––––+      +–––––––––––––––––––––+                               |                  |      |                          |      |                     |                    Signal In  |    IIR BiQuad    |      |      Soft Overdrive      |      |      IIR BiQuad     |  Signal Out       +–––––––––+>|                  +––––+>|                          +––––+>|                     +–––––––––––––+>                |     [LowShelf]   |      | [atan4pi Look Up Table]  |      |  [Low Pass Filter]  |                               |                  |      |                          |      |                     |                               +––––––––––––––––––+      +––––––––––––––––––––––––––+      +–––––––––––––––––––––+                                                                                                                                                     0.05 < Q < 2.58   [Pot Alpha]                                     Q = 2.0                                                                                                                                                             1000 < Fs < 4000    [Pot Beta]                                   Fs = 2500                                                                                                                                                      -15 < dbGain < 15  [Pot Gamma]                                                                                                                                                                                    Utilities, etc: Biquad Filter View - A IIR Biquad Filter Design &amp; Visualization Tool
View full article
Click Here : https://community.freescale.com/servlet/JiveServlet/downloadBody/102170-102-1-18605/OpenSDA.zip To download the file with the files mentioned on the presentation.
View full article
Take some time to get yourself familiar with C programming before you continue on the programming tutorial. Here is a list of topics that you should be comfortable with, and a couple of good tutorials below. Topics included: Program Structure Commenting Variables Keywords Data Types Decimal, Binary and Hexadecimal Equivalents ASCII Text/Number Conversion Math Operators Increment & Decrement Shift Logical Operators Bitwise Operators Loops If Statement Switch Statement Functions Recursion Local Variables vs. Global Arrays Pointers Typdef, struct and union Preprocessor Directives Static, const and Volatile Keywords Tutorial 1: PSU Intro to C for Embedded Design   From PSU Freescale Cup Senior Design Course Tutorial 2: Learning Programming with C This Freescale course consists of a collection of lessons that will introduce you to the fundamentals of programming using the C programming language. Coding for Readability Sometimes when a project has the ability to grow with new features, it is best to code in modules. This allows one to easily take a more modular approach to designing their program. Despite the fact that C does not support Classes like C++ does, you can create structures that can be addressed globally with little code, which is especially useful for microcontroller based projects. An example of a structure which will be made global: This goes in the globals.h file typedef struct {   unsigned char ServoPWM;   char ServoAngle;   unsigned char DrivePWM;   int TimeOut;   int Current;   int Speed; } sMotor; extern volatile sMotor Motor; This will go in any other file that we want our structure to be accessible from #include <Globals.h> volatile sMotor Motor; This is how to address the variable in the structure #include <Globals.h> volatile sMotor Motor; If you decided to have two distinguishable motors you could do this in the globals.h extern volatile sMotor Motor1; extern volatile sMotor Motor2; Then do this in the other files volatile sMotor Motor1; volatile sMotor Motor2; Helpful Hints In developing an algorithm to detect the line position, we found two basic errors in the coding practice which caused catastrophic errors in line detection. Both of these tips are very basic coding practice. First, when using C code, it usually benefits the user to initialize all variables to some value, especially if computations are involved. Often times when the value wasn't initialized it would seem to acquire a wrong value seemingly from nowhere. Secondly, when doing calculations with arrays, make sure to do calculations with array indices that actually exist. Many times we would make the mistake in our loops of trying to use an index that wasn't assigned a value. Therefore it would acquire an unknown value from memory that caused errors in our calculations.
View full article
The Freescale linescan camera is based upon the TSL1401CL sensor from TAOS Inc. Design Files Schematic & 3D Render (Courtesy of eli_hughes) Images (Lens removed) Freescale Linescan Camera Specifications 128-pixel linear image sensor (TSL1401CL) Focusable imaging lens 5-pin physical interface on PCB on .100" grid Simple three-pin MCU interface with analog pixel output Lens: 7.9mm focal length, f2.4 fixed aperture, manual focus, 12mm x 0.5mm thread Exposure Time: 267µS to 68mS Resolution: 128 pixels Built-In amplifier stage to improve white/black differentiation. The lense used on the board: Alaud Optical     8.0mm f.l. Lens w/IR filter = Part Num: AB0825C        M12x.05 Lens Holder = #9 or #10 Useful links AMS TSL1401 Product Page Line Scan Camera Use Freescale App Note: Line Scan Camera
View full article
1. Download CodeWarrior 10 Evaluation Version (Eclipse, Windows-hosted) To Program your microcontroller you will need to set up the CodeWarrior Integrated Development Environment. CodeWarrior is available on the Freescale.com Website. Method 1: Direct Link direct download link (Caution - link may not be up to date) Method 2: Navigate to the Download Link From Freescale.com click on: "Design Resources" tab at the top of the page, then navigate to "Software and Tools", and then to "Codewarrior Devleopment Tools" Click on the "Download CodeWarrior now link" Click on the Download Evaluation Versions link" Within this page, use your browser "find" feature (Typically CTRL-F) to search for the text string "Kinetis." Click the "download" button next to "Evaluation: CodeWarrior for Microcontrollers(Eclipse, Windows-hosted) version". and save it to your computer. 2. Install CodeWarrior To install CodeWarrior Development Studio for Microcontrollers v10, double-click the installation package and a wizard will guide you through the installation process. Installation Notes: Are you using Windows Vista or Windows 7? 1. The CodeWarrior installer should be run using the ‘Run as administrator’ option. CodeWarrior service packs are installed with the Eclipse Updater. The updater should also be run with this option. To start the Eclipse Updater select ‘Window > Install new software’ in the menu. 2. Eclipse needs read/write access to the installation folder. Make sure the eclipse installation folder has the appropriate permissions for all users. 3. Make sure your project workspace has read and write permissions Evaluation Edition User: If you are installing the Evaluation Edition, the Evaluation license is automatically installed with your product and you do not need to register it. This license allows you to develop projects as Professional Edition within the 30-day evaluation period. After 30 days, the license works as Special Edition license (free permanent, but feature limited) which supports unlimited assembly code, up to 32KB of C code for HCS08/RS08 derivatives, up to 64KB of C code for V1 ColdFire derivatives and up to 128KB of C code for V2-V4 ColdFire and Kinetis derivatives and up to 512KB of C code for MPC56xx derivatives. Once you have finished downloading and installing CodeWarrior, users can return to Downloading and Installing P&E as part of the Blink a LED on Kinetis Tutorial Additional Resources: CW10 User Manual —The Above user manual has a list of other helpful docs which can be found within your CodeWarrior installation directory. (i.e. <CWInstallDir>\MCU\Help\PDF\)
View full article
1.  Go to community.freescale.com and Log in with your www.Freescale.com account, if you don´t have one, create one. 2.  Create a New Document 3.  Write your Project Name and a paragraph with a quick description of your project. Next, click the insert video icon to add your video of your project working. 4.  If your Project Report is less than 3 pages long, post it right below the video. If not, add it as Attachment. 5.  Also add your complete program project in a .zip file as an attachment. 6.  In the Category section, select if is a Student Project or other. 7.  In the Tags section, add any search words that can help anyone to find your project. Use University_Programs, your evaluation board name (ex. TWR-K40X256-KIT) and family (ex. Kinetis ). It is optional if you want to add your_university_name, region (ex. latin_america, emea), etc. 8.  In the Collaboration Options, add your team members if you want them to be able to edit it. And set Comments to be "Open". 9. Select Publish when you are done.
View full article
Embedded processors are highly optimized products.  When you just want a good general use processor, sifting through the many options to find the best one can be daunting.  Below are some excellent general-purpose use platforms that I recommend for academia.  Are there other options, you bet.  These are the best in class, most popular and great for learning. FRDM-KL25Z TWR-K60D100M Wand Board Teensy 3.0 Cost: $12.95 $99 ($169 for -KIT) $79/$99/$129 $19 Chip: Cortex-M0+ Cortex-M4 Cortex-A9 (Single/Dual/Quad core) Cortex-M4 On-Board Features: Minimal Good Good Very Minimal Expansion Capability Excellent Good Average Good Notable Features Arduino Shield Compatibility Program with mbed.org I/O options Android Jellybean, HDMI Plug into breadboard Program with Arduino IDE The Freedom Board (FRDM-KL25Z) This is a great starter board!  It's cheap($12.95), yet powerful and can be used in a wide variety of applications.  All FRDM- boards are pinned out in the Arduino shield standard so you have lots of expansion options.  The FRDM-KL25Z can be programmed with the normal 'industrial strength' IDE you can also use mbed.org which sets it apart from many other products in this list for ease-of-use. Teensy (Teensy3) Made by PJRC.  For those that want to put a high performance 32-bit MCU on a breadboard.  Also, per the PJRC website you you are able to use the Arduino IDE.  The hardware is about as bare-bones as it gets, but the nice small footprint and breadboard ability gives you lots of flexibility to add your own custom I/O. The Tower System (TWR-K60D100M-KIT) The Tower System is another platform with a multitude of options.  With the Tower System you get access to much more I/O and is designed with higher performance applications in mind.  The particular variant I most often recommend is the TWR-K60D100M simply because it has so many features all packed in.  USB, Ethernet, Crypto engine, CAN, SPI, I2C and the list goes on.  Couple that with plenty of processing muscle with a Cortex-M4 CPU running at 100Mhz. Wand Board.org (Wand Board) The Cortex-M series is primarily intended for embedded control applications.  Whereas the Cortex-A series is built for graphical and multimedia applications.  Wandboard.org has been getting a lot of attention in the community as a Rasberry PI, Beagle Bone alternative(comparison chart).  Another similar product, still in development, is UDOO so stay tuned for that one.
View full article
Hardware Servos are specialized dc motors geared to produced high-torques and set at specific angles vs rotating continously. The ability to position the servo at a specific angle over and over makes them ideal for robotics, radio controlled car and other various applications. A typical servo will have range of motion from 180-270 degrees. Most modern servos have a three wire interface, red (V+), black (ground), and white (control). To control a servo you must send it a variable length commands (pulse) in 20ms increments. This type of control is called Pulse Width Modulation. Pulse Width Modulation is a square wave with a set period. By changing the width controlling the proportion of on versus off time, you can obtain a digital ratio from 0-100%. That ratio of on versus off time is called the duty cycle. A microcontroller generates a PWM signal using a timer. The time from the beginning of one sequence to the next is called the period. The main timer registers include: Counter, Modulo, Count Initialization Value, Channel Value, FTM Status & Control, and Channel Status & Control. The Counter will count up from the Count Initialization Value and reset after reaching Modulo. One tradeoff of the design is the Modulo value we set. It represents the count value of a full duty cycle and also the resolution of our servo control. Setting a higher Modulo value allows for more precise variation in the servo, i.e. more accurate steering. The downside is that a higher value requires more time per cycle. It is necessary to configure a timer module for the drive motor separate from the servo because they each require different clock frequencies. Another tradeoff of pulse width modulation is whether it is edge-aligned or center-aligned. Edge-aligned PWM, where the channel is cleared at counter overflow and set at channel match, is simpler to implement in hardware. Center-aligned PWM, where the counter counts up and down, is more difficult to implement but does not give as much noise interference when the channel matches. Servos have 3 wires coming out of them: Ground: Black, Brown Power: Red PWM Signal: White, Yellow, Orange Spec Sheet for Servo used in Freescale Cup Futaba-S-3010 Creating the PWM Signal Much of what is needed to create this signal is discussed in the Motor Control tutorial. Click here to review how to configure a PWM signal on your microcontroller. The same microcontroller configuration utilized to drive a motor can be modified slightly to rotate the arm of a servo. Since the Servo and motor require different clock frequencies, it is necessary to configure a timer module for the servo separate from the motor. Freescale Cup participants will configure the timer modules to output signals that control a steering Servo via varying the Duty Cycle of a PWM signal. Microcontroller Reference Manual: Timer Information You will find high level information about Timer usage in several different areas of a reference manual. See the reference-manual article for more general information. Relevant Chapters: Introduction: Timer modules - lists the memory map and register definitions for the GPIO System Modules: System Integration Modules (SIM) - provides system control and chip configuration registers Chip Configuration: Timers Signal Multiplexing: Port control and interrupts Methods of controlling steering angles Construct a look-up table One way of controlling the steering angles is to construct a look-up table. The input of the look-up table can be the shift distance(in pixels) from the center, and the output could be the steering angles. The look-up table can be put into an excel file. So when you want to use it, just copy and paste the table into your code file. Here is an example of how to construct a look-up table. 1. Set up basic parameters of your car: height of camera(h), angle of camera(theta), velocity of car(v), servo delay(s).. 2. Draw a graph to help you develop a function between your input parameters and your output steering angles 3. Put all paraments into excel. So if you want to change any parameters in the future it will be very convenient. 4. Copy and paste look-up table into code file Note: depending on how you define your parameters, the look-up table may not work as well as you expected. Experiments show that the look-up table works well when the shift distance is small( small turns) and the car tends to go off track when the shift distance is big(sharp turns). Poportional Control (P Control) You can map your servo angle based directly on your line location. Take the derivative of the camera signal and use the derivative peaks as the edges of the line. Take the location of each peak and subtract them from each other to get the line width. Taking the min line peak plus line width will give you the location of the line. Now take that location and map it to your servo. We made Camera.Lock = loc and using this we made Motor.ServoAngle = Camera.Lock»1; This made our line location map directly to our servo and it seemed to work well for us. Additional Theory Training Resources Freescale Motor Control Tutorial Freescale Lecture 1: Introduction and Motor Basics Freescale Lecture 2: Pulse Width Modulaiton Freescale Lecture 3: Control Design Freesacle Lecture 4: Speed and Position Freescale Lecture 5: MPC5607B Overview
View full article
Overview This document has links to videos to give tutorials on how to getting started *from scratch* with the freedom board.    In these tutorials we build projects with bare metal code to see how things work!   It includes the basics on how to get clocks running,  lights blinking and interrupts firing *from scratch*. For more code/peripheral examples that use a "bare metal" approach,  check out the page on the FRDM-TFC board. ERRATA!!!   While working with a large number of Freedom boards in a course,  it was observed that the InitClockRoutines would *sometimes* not work.    *Some* of the crystals on the freedom boards do NOT like "HIGH_GAIN" mode.   The new code is uploaded to this page but you could also change the code yourself:   pll_init(8000000, HIGH_GAIN, CRYSTAL, 4, 24, MCGOUT); to   pll_init(8000000, LOW_POWER, CRYSTAL, 4, 24, MCGOUT); Projects From Scratch for the Freedom Board with Codewarrior 10.3 Projects From Scratch - Part 2 - Importing other projects Using the Freescale Header Files and Blinking the LED Source code for video (Codewarrior 10.3) is in the attached files at the bottom of this document. Clock Distribution Source Code for the Clock Distribution video is in the attached files at the bottom of this document. Interrupts Part 1 - Background Interrupts Part 2 - ARM Systick Timer Source Code for the ARM Systick Timer video is in the attached files at the bottom of this document. Interrupts Part 3 - TPM (Timer Pulse Width Modulator) Overflow Source Code for the TPM Overflow Interrupts video is in the attached files at the bottom of this document
View full article
1. Overview 2. Hardware 3. Set up the Hardware: Line Scan Camera/Microcontroller Hardware Setup 4. Build the Code 5. Download/Debug/Run 6.Example Code Functions ImageCapture(); ReadADCChannel() Initialize the ADC Header File Definitions Initialize the GPIO Other Tutorials: This tutorial covers the details of obtaining data from the line scan camera on the Kinetis K40 using the TWR-K40X256-KIT evaluation board. General details of the line scan camera not related to the Kinetis can be found in the general Line Scan Camera Theory article. This tutorial will help students familiarize themselves with how to interface the camera with the microcontroller, how to configure GPIO pins to create clock signals and also how to utilize the microcontroller's ADC to read the data from the camera. Outside of control algorithms, configuring the camera is one of the more complex tasks necessary to create a Freescale Cup Vehicle. 1.  Overview In this exercise students will access the line scan camera, create a clock signal and create the initialization pulse which tells the camera to begin the exposure period. This tutorial will not describe line recognition or line following algorithms - these concepts are beyond its scope. Students will: Create the code using Codewarrior Build a project Download the code to the board connect the microcontroller to the camera. Run the program view the camera data, clock and Si pulse on an oscilloscope view the data from the camera in the CodeWarrior Debugger for verification purposes   To successfully complete this exercise, the following software and hardware are required: The K40 Tower card, TWR-K40x256 CodeWarrior for Microcontrollers Freescale Line Scan Camera Motor Board Tower Prototyping board Soldering Iron Solder Tower Elevators USB Cord 2. Hardware   Read the Line Scan Camera Overview article for general information on the camera, ADC, and GPIO microcontroller configuration settings. 3. Set up the Hardware: Line Scan Camera/Microcontroller Hardware Setup It is crucial for an engineer to have the proper test equipment and tools for the job. In this case, without an oscilloscope, students will not be able to verify whether the proper signals are being sent to the camera. 4. Build the Code If there is more than one project in your project view, make sure the proper project is the focus. The most reliable way to do this is to right click the project and choose Build Project as shown below. You can also go to the Project menu and choose the same command. If errors are encountered, look in the Problems view and resolve them. For now ignore any warnings. 5. Download/Debug/Run Download the code to your board, once this process is complete resume the project so that the code runs. If you want more information on how to complete this step see the download debug run section of the Kinetis Blinking Led tutorial. 6.Example Code What will happen: the function ImageCapture() is called in main.c with a pointer to the first element in the array. This function completes the processes necessary to capture images using the camera. To become more familiar with Pointers and Arrays - navigate to the C Programming Tutorial. Knowledge of Pointers and Arrays is a pre-requisite for understanding the Camera Code. Functions The camera code utilizes the following function: within main.c ImageCapture(&Line.RawCameraData[0]); is called to initiate the step of capturing an image into the first position of the array. ImageCapture(); from Camerainterface.c This function captures the images by creating the SI Pulse, and clock signals, capturing the data into an Array using the ADC features of the K40. It calls the function ReadADCChannel() at the proper time which then inputs data from the camera AO line. void ImageCapture(int * ImageData){//this is a pointer to a single character in memory   unsigned char i;   TAOS_SI_HIGH;   TAOS_EXPOSURE_DELAY;   TAOS_CLK_HIGH;   TAOS_EXPOSURE_DELAY;   TAOS_SI_LOW;   TAOS_EXPOSURE_DELAY;   ImageData[0] = (int)ReadADCChannel(19);// inputs data from camera (first pixel)   TAOS_CLK_LOW;   for(i=1;i<128;i++)   {   TAOS_EXPOSURE_DELAY;   TAOS_EXPOSURE_DELAY;   TAOS_CLK_HIGH;   TAOS_EXPOSURE_DELAY;   TAOS_EXPOSURE_DELAY;   ImageData[i] = (int)ReadADCChannel(19); // inputs data from camera (one pixel each time through loop)   TAOS_CLK_LOW;   }   TAOS_EXPOSURE_DELAY;   TAOS_EXPOSURE_DELAY;   TAOS_CLK_HIGH;   TAOS_EXPOSURE_DELAY;   TAOS_EXPOSURE_DELAY;   TAOS_CLK_LOW;  } ReadADCChannel() from readADC.c this function does the analog to digital conversion and returns a value between 0 and 255. It takes the proper ADC channel, in this case 19. Channel 19 corresponds to analog input pin ADC1_DM0 (see page 117 in the K40 Sub-Family Reference Manual). unsigned char ReadADCChannel(unsigned char Channel)   {   ADC1_SC1A = Channel;   while((ADC1_SC1A & ADC_SC1_COCO_MASK) == 0)   {   }   return ADC1_RA;    } Initialize the ADC Before utilizing the ADC it must be calibrated and initialized. The details for how to do this can be found in Chapter 19 Using Peripheral Delay Block (PDB) to Schedule Analog to Digital Converter (ADC) Conversions of the Kinetis Peripheral Module Quick Reference manual. The PDB portions of the code have been removed for the Cup Car Demo Code. Header File Definitions from k40_TOWER_BOARD_SUPPORT.h The following code enables the GPIO on the two pins: #define TAOS_CLK_LOC (1<<28) #define TAOS_SI_LOC (1<<18) Initialize the GPIO From K40_TOWER_BOARD_SUPPORT.c The InitK40GPIO Function sets up the ports for use: Relevant code SIM_SCGC5 = SIM_SCGC5_PORTA_MASK | SIM_SCGC5_PORTB_MASK | SIM_SCGC5_PORTC_MASK | SIM_SCGC5_PORTD_MASK | SIM_SCGC5_PORTE_MASK; //CLK and SI signal PORTC_PCR18 = PORT_PCR_MUX(1) | PORT_PCR_DSE_MASK; PORTE_PCR28 = PORT_PCR_MUX(1) | PORT_PCR_DSE_MASK; //Make Sure the GPIO is setup to be an output GPIOC_PDDR |= LED_E1_LOC | LED_E2_LOC | LED_E3_LOC | TAOS_SI_LOC; GPIOE_PDDR |= TAOS_CLK_LOC; GPIOB_PDDR |= LED_E4_LOC; Other Tutorials: K40:Blinking LED Tutorial K40:Drive DC Motor Tutorial K40:Turning a Servo Tutorial   
View full article