S32K Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K Knowledge Base

Labels

Discussions

Sort by:
MCU : S32K144 AFE : MC33771 RTD : 1.0.1 As we know BCC sample software for MC33771C which is delivered is based on SDK for S32K144 , and uses S32DS-2.2 :-- BCC_S32K144_FreeMASTER I am having a setup , for this combination, using SPI :-- FRDM33771CSPEVB evaluation board  + S32K144 + 14 cell Battery EMULATOR :    S32K144 pins used :-- MOSI :  LPSPI0  : PTB-4 MISO :  LPSPI0  : PTB-3 SCK :    LPSPI0  : PTB-2 CSB :    LPSPI0  : PTB-5 RESET line of MC33771C : PTD-4 FRDM33771CSPEVB pins used :-- https://www.nxp.com/docs/en/user-guide/UM11402.pdf SI of MC33771C : Connects to MOSI of S32K144 : K2-7 SO of MC33771C : Connects to MISO of S32K144 : K2-9 SCK of MC33771C : Connects to PTD-4 of S32K144 : K2-11 CSB :    K2 -5 RESET line of MC33771C : K4 -1 Freemaster uses UART-1 on S32K144 EVB ():-- TX : PTC7 RX : PTC6 I have ported the BCC_S32K144_FreeMASTER  sample code to S32K144 using RTD-1.0.1 & is working fine. This attached code work fine for SPI.  Two sample project i have attached, both are tested and working fine :--- 1> Chip select is controlled by LPSPI. 2> Chip select is controlled manually in user software. Fremaster project is also inside the folder, name of freemaster project is :-- 1> FreeMASTER_project.pmp TPL related part i have not ported & tested because at present i am not having MC33664ATL on S32K144 EVB board & do not have FRDM33771BTPLEVB (MC33771C board with TPL on it). Regards, Dinesh
View full article
Detailed Description:                      This config tool simplifies DCF records calculation for S32K344 device.                 Look at HowToUse sheet for simple guideline, then work with DCF sheet                 Notes: - Macros have to be enabled!         BR, Petr
View full article
******************************************************************************* The purpose of this demo application is to present a usage of the EMIOS IP Driver in Interrupt mode for the S32K3xx MCU. The example use to :-- EMIOS-1 - ch-0  --> PTC24 --> Generate the PWM EMIOS-1 - ch-1  --> PTC25 --> is the ICU channel to measure the duty Pins used :--     This example is tested for SAIC & IPWM mode both. You can change the mode by this setting in MEX file :--     Difference between SAIC & IPWM,  ICU Driver User Manual :--   These Two Macro :-- SAIC_MODE  --> this maco will enable variables to store for SAIC mode CUSTOM_IRQ  --> this MACRO will enable customized IRQ or RTD available IRQ   Result :--     Sometimes Compiling error comes, in Autogenerated RTD file.    Change the Header file name :--    ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************
View full article
This example code brief  :-- 1> Tested without the SL of BMS, so no dependency on the BMS Safety library. 2> Its tested on 3 AFE MC33774 board connected in TPL 3> Change following macro in mc33774_cfg.h file  to change the numbers of AFE connected in TPL.     RTD : 3.0.0 P07 BMS SDK : 1.0.2 This example does this task :-- Application Measurement. SYNC measurement Periodic Measurement. Read AFE temperature. Cell balancing timer method. Reading the Cell balancing status register & fault registers. =================== Setup used ============ Attached code is tested with TWO MC33774 AFE connected in TPL mode. FRDM665SPIEVB stackable board used for MC33665.     =============== MCU Pins used =========== FRDM665SPIEVB Jumper setting  :---     K1, K2 & K4 connector of S32J344 EVB :--       K1 on MC33665 & S32K334 evb :--  K2 on MC33665 & S32K334 evb :--  K4 on MC33665 & S32K334 evb :--    ================= EVB Link ================== https://www.nxp.com/design/design-center/development-boards-and-designs/18-cell-battery-pack-emulator-to-supply-mc33774-bcc-evbs:BATT-18EMULATOR https://www.nxp.com/design/design-center/development-boards-and-designs/FRDM665SPIEVB https://www.nxp.com/design/design-center/development-boards-and-designs/mc33774ata-evaluation-board-with-isolated-daisy-chain-communication:RD33774ADSTEVB https://www.nxp.com/design/design-center/development-boards-and-designs/automotive-development-platforms/s32k-mcu-platforms/s32k3x4evb-t172-evaluation-board-for-automotive-general-purpose:S32K3X4EVB-T172   ================== Measurement types used in example ===== Periodic measurement is done by 33774 , this is cyclic Other Two : application , sync  need send command to start Application measurement , need send app_capture command twice , and then read the result. Synchronous measurement take out the Primary adc result(VC)and secondary result(VB) .But the VC and VB result comes from different adc. Period measurement start when you send  API "MSR_StartMeasurement" and then 774 will do period measurement automatically periodically :--   Why we need to measure Vc & Vb both :-- ASIL-D ,yes we can measurement VC channel by primary ADC and measurement VB by secondary ADC from hardware VC and VB are come from same point of battery cell. Now 2 ADC compare with each other, that lead to high safety (ASIL D). Primary & Secondary Device temperature reading :-- This API is used for it MC33774_CDD_BCC_SWC_Running_Slot4(). ============= Cell Balancing =========== Cell Balancing method used :-- MC33774 balance will switch between odd channel (1,3,5,7,... 17) and even channel (2,4,6,8,..18) by 500ms period , (250ms for odd and then switch to even 250ms and then odd 250ms...)it is because of IC design and cannot change by software.   MC33774 have lots of balance method  this example uses "timer method ". How to check Balancing is enabled :-- Following function MC33774_CDD_BCC_SWC_Running_Slot5() read the : Balance status & fault registers BAL_SWITCH_STAT0, BAL_SWITCH_STAT1 represent the balancing MOSFET current status.   Measure the voltage drop across the balancing register is the best approach. You will see the voltage drop appears every 250ms if PWM is 100%.  Please check the schematic of the 33774 EVB, find the balancing resistor on which channel balancing is enabled.     ======= How much time to wait to extract the measurements results ======= 240 us is the time of one SCAN Time between each Application measurement sequence. Min App measure time for 16 sample :-- 4.08ms = (16+1) *240 Min 1 SYNC measurement time, for 16 samples = 18 cycle ≈ 18 * (16*240us) ≈ 69 ms ============= Using Debugger ============ Debugger breakpoint will cause the communication timeout at the AFE, which will RESET the AFE. To use the debugger while development you need to disable the communication timeout. In S32DS MEX file you cannot disable the timeout function ( limit the value of 0~255) Disable Communication timeout in code :--   ================= Results for FIRST AFE ===========================            
View full article
*******************************************************************************  The purpose of this demo application is to present a usage of the  ADC_SAR and BCTU IP Driver for the S32K3xx MCU. The example uses the TWO PIT0 trigger to trigger BCTU conversion list to perform parallel conversions on ADC0/ADC1. Each Trigger has one LIST associated with it in the BCTU. Conversion result for EACH list is stored in individual FIFO of the BCTU. DMA will transfer the ADC conversion result. LIST-1 ADC channels are selected to be converted on each ADC:     LIST-2 ADC channels are selected to be converted on each ADC:--      Converted results from BCTU FIFO are moved by DMA into result array.  ADC channel S10 is connected to board's potentiometer. Result :--    ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: internal_FLASH ********************************************************************************
View full article
******************************************************************************** * Detailed Description: * The example updates th UART TX buffer for continuous transfer. * ---------------------------------------------------------------------- * Test HW: S32K344EVB-Q172 * MCU: S32K344, RTD 4.0.0 P24 * Debugger: S32DS_ARM_3.5 * Target: internal_FLASH ********************************************************************************
View full article
******************************************************************************************************* * Detailed Description: This demo showcases how to use eMIOS in Input Capture mode with DMA. It demonstrates how timestamp data from captured input signals is stored and how a GPIO toggle provides a simple visual confirmation that the interrupt is being triggered as expected.   * eMIOS Pwm: Configures EMIOS 0 Channel 1 as OPWMB (Output Pulse Width Modulation Buffered). This channel generates a waveform that will be captured by Channel 9 * eMIOS Icu with DMA: Configures EMIOS 0 Channel 9 in ICU_MODE_TIMESTAMP using SAIC (Single Action Input Capture) mode. This channel captures the timestamps of the waveform generated by Channel 1. After a predefined number of captures, a DMA interrupt is triggered. ******************************************************************************************************* * Test HW: S32K3X4EVB-T172 * MCU: S32K344 * Debugger: S32DS 3.6.2, OpenSDA * Target: internal_FLASH *******************************************************************************************************
View full article
******************************************************************************** The purpose of this demo application is to show you how to use the Temperature Sensor module in S32DS. It includes two methods to obtain temperature. -The first one starts a normal software conversion with one-shot mode on temp sense channel and calculates the temperature on chip from the data conversion. -The second one calculates the temperature based on given data (if read directly using ADC). Note: Please adjust the ADC reference voltage according to the board you are using * ------------------------------------------------------------------------------ * Test HW: S32K344EVB-T172 * MCU: S32K344 1P55A * Compiler: S32DS.ARM.3.5/6 * SDK release: S32K3_RTD_6.0.0/5.0.0/4.0.0_P24 * Debugger: OpenSDA/PE&Micro * Target: internal_FLASH *Jumper:J18-1:2,5V used. ********************************************************************************* Note that if you use "sprintf", you need to check the following option.  
View full article
******************************************************************************************** * Test HW: S32K311 EVB-Q100 * MCU: S32K311 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: internal_FLASH ******************************************************************************************** The purpose of this demo application is to enter the standby mode and waking up from sleep using the user button. =============== How this DEMO works ========== 1) once the image is flashed, the application starts running and BLUE LED blinks for every one second during RUN mode 2) Once SW5 in EVB is pressed, MCU enters the SLEEP mode and it turns off BLUE LED & PIT 3) To Wakeup: Press SW4 in EVB 4) Once it returns to normal mode, BLUE LED and PIT starts running. Used pins: ========= PTC11 -> SW5 -> EnterStandby PTA8 -> SW4 -> WakeupFromSleep PTB8 -> D12   -> Blue led  
View full article
*******************************************************************************  The purpose of this demo application is to present a usage of the  LPSPI IP Driver for the S32K3xx MCU.  The example uses LPSPI2 for transmit & receive Twelve bytes using the DMA. MOSI MISO connected on Hardware in loopback.  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ******************************************************************************** DATA and Instruction CACHE is enabled by default --> in startup code :--     ========= This selection enable the use of CACHE driver API =========     ============= Use this MACRO ==================== #define USE_NON_CHACHABLE_REGION 1 This MACRO comment & uncomment will allocate the buffer in cachable & non cacable region of memory. You can allocate the SPI buffer in in cachable & non cacable region of memory. Enabling & disabling of this MACRO will adjust the example code.     ============ How this example works : Cacheable region used ============ I have connected MOSI and MISO pins of spi at hardware level. Whenever I am  sending and receiving total 10 numbers of 12 byte packet On each transmission of 12 byte packet I am incrementing the first bite of transmit buffer just to distinguish between packets at the receive side Cache_Ip_InvalidateByAddr() --> I have to call this API every time I receive 12 byte of data on receive buffer Cache_Ip_CleanByAddr() --> every time after incrementing the transmit buffer first byte ...I have to call this API then only the correct data is transmitted otherwise it will transmit the same data which was available at first time transfer ================ Cache API operation ============== Cache_Ip_InvalidateByAddr() is for the  invalidate operation. Cache_Ip_CleanByAddr() is for the clean operation or clean&invalidate operation that can be chosen by param of this api: @Param[in]  enInvalidate      Specifies to execute operation Clean&Invalidate. Clean: This operation ensures that all dirty lines—data in the cache that has been modified but not yet written back to the main memory—are written back to the main memory ->(push data from cache memory to main memory)  Invalidate: This operation marks the cache lines as invalid, ensuring that any subsequent access to these lines results in a fetch from the main memory, thus ensuring data consistency ->(push data from main memory to cache memory) Clean&invalidate : A cache clean and invalidate operation behaves as the execution of a clean operation followed immediately by an invalidate operation. Both operations are performed to the same location. ================ Pins used ======================    
View full article
******************************************************************************* The purpose of this demo application is to present a usage of the EMIOS IP Driver in Polling mode for the S32K3xx MCU. The example use to :-- EMIOS-1 - ch-0  --> PTC24 --> Generate the PWM EMIOS-1 - ch-1  --> PTC25 --> is the ICU channel to measure the duty Pins used :--     This example is tested for IPWM mode .  :--       IPWM mode ,  ICU Driver User Manual :--   Result :-- Sometimes Compiling error comes, in Autogenerated RTD file.    Change the Header file name :--      ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************
View full article
This example code brief  :-- 1> Tested without the SL of BMS, so no dependency on the BMS Safety library. 2> Its tested on 2 AFE MC33775 board connected in TPL 3> Change following macro in mc33775_cfg.h file  to change the numbers of AFE connected in TPL.     RTD : 3.0.0 P07 BMS SDK : 1.0.2 This example does this task :-- Application Measurement. SYNC measurement Periodic Measurement. Read AFE temperature. Cell balancing timer method. Reading the Cell balancing status register & fault registers. =================== Setup used ============ Attached code is tested with TWO MC33775 AFE connected in TPL mode.   =============== MCU Pins used ===========   FRDM665SPIEVB Jumper setting  :---                   K1, K2 & K4 connector of S32J344 EVB :--             K1 on MC33665 & S32K334 evb :--      K2 on MC33665 & S32K334 evb :--    K4 on MC33665 & S32K334 evb :--        ================= EVB Link ==================   https://www.nxp.com/design/design-center/development-boards-and-designs/18-cell-battery-pack-emulator-to-supply-mc33774-bcc-evbs:BATT-18EMULATOR https://www.nxp.com/design/design-center/development-boards-and-designs/FRDM665SPIEVB https://www.nxp.com/design/design-center/development-boards-and-designs/RD33775ADSTEVB https://www.nxp.com/design/design-center/development-boards-and-designs/automotive-development-platforms/s32k-mcu-platforms/s32k3x4evb-t172-evaluation-board-for-automotive-general-purpose:S32K3X4EVB-T172 ============= Using Debugger ============ Debugger breakpoint will cause the communication timeout at the AFE, which will RESET the AFE. To use the debugger while development you need to disable the communication timeout. In S32DS MEX file you cannot disable the timeout function ( limit the value of 0~255)   Disable Communication timeout in code :--     ================= Results for TWO AFE ===========================          
View full article
This post is an additional project to the S32K3 Low Power Management AN and demos.  A simple FlexCAN routine is configured for RX/TX and wakeup through the CAN0_RX pin (PTA6/WKPU19). The example is based on the S32K3X4EVB-T172, meaning that transceiver TJA1443 is used. TJA1443 only needs CAN0_EN & CAN0_STB pins in HIGH for normal configuration. In the example, the GREEN led is used to indicate that the MCU is in RUN mode. Once SW5 is pressed, MCU enters low power (STANDBY), and led is turned off. BLUE led toggles each time a CAN frame is received. MCU can be woken up with SW6 (WKPU42) or through a CAN RX. Note that CAN is not enabled in low-power, rather PTA6 (WKPU19) is configured for wake up, and once a rising edge signal is detected on the pin, MCU wakes up and reconfigures CAN module.  ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-T172 * MCU: S32K344 * Compiler: S32DS3.6.2 * SDK release: RTD 6.0.0 * Debugger: PE Micro * Target: internal_FLASH  ------------------------------------------------------------------------------ This example is provided as is with no guarantees and no support.
View full article
Hi everyone, Welcome to the NXP Tech Days 2025 training session AUT-T437: Hands - On Workshop: Explore Ethernet Integration on the S32K3 Microcontroller. My name is Alejandro Flores Triana (Alex) and I will be your guide during this conference. I am an Automotive Applications Engineer supporting different OEMs, Tier1s, Partners and other internal NXP teams on topics related to communication protocols (e.g. CAN, LIN, SPI, I2C, Ethernet, etc.). The idea of this session is for you to understand how to program the S32K3 Ethernet interface using NXP Real-Time Drivers (RTDs) – Autosar MCAL Layer. We will use a base project and together modify it to create a simple Ethernet application. Therefore, to be ready follow the steps below to get your environment up and running before the session. On your laptop, install the NXP Software environment described in the attached presentation: Hands - On Workshop: S32K3 Ethernet Prerequisites.   Once you have the NXP software environment installed, download the attached project: S32K344_ETH_MCAL_TechDays.exe.   Run the .exe project with administrator rights. Accept the license and install in the desired folder.         Open the NXP Design Studio. Click File -> Import -> Existing Projects into Workspace.   Select root directory and browse the folder where you downloaded the project.   Select Copy projects into workspace. Then, click Finish.   Select the project. Click on the arrow next to the hammer. Click on Debug_FLASH. Then you are ready for the session! See you soon. Best Regards, Alejandro Flores Triana
View full article
[S32K3 tool part]:How to use IAR compiler or IAR project to compile MCAL project   1.    Abstract      Through regular observation, it has been found that there are still many customers using platforms such as MCAL+IAR, including those using IAR compilers and those directly using IAR IDEs. In fact, when I was working on industrial MCUs in the past, I also particularly liked IAR IDE for its fast compilation speed, high compilation efficiency, and small code generation. However, when I came to auto MCU, I found that its popularity was not very high, and I also noticed that some customers encountered various problems when importing MCAL into IAR. Therefore, I will directly write a tool article on how to use IAR compiler or IAR IDE project to compile NXP S32K MCAL in combination with EB tresos MCAL. This article uses S32K344 combined with RTD600 to illustrate the compilation of MCAL projects using IAR compiler and the direct import of MCAL into IAR IDE projects 2. IAR Complier with S32K3 RTD MCAL project 2.1 S32K3 HW and SW SW32K3_S32M27x_RTD_R21-11_6.0.0 S32K3X4-EVB Based on Dio_TS_T40D34M60I0R0 IAR:IAR EW for Arm 9.70.1 EB tresos29.0.0 2.2 Compile MCAL project steps using IAR compiler CMD method 2.2.1 Copy one RTD MCAL new project Open path C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins Copy Dio_TS_T40D34M60I0R0 , rename it as Dio_TS_T40D34M60I0R0_IAR Fig 1 2.2.2 Complie EB tresos project Use EB tresos tool open the following EB tresos project : C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Dio_TS_T40D34M60I0R0_IAR\examples\EBT\S32K3XX\Dio_Example_S32K344\TresosProject Generate code: Fig 2 2.2.3 Vscode open Dio_TS_T40D34M60I0R0_IAR project Use VS code open the following path folder: C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Dio_TS_T40D34M60I0R0_IAR\examples\EBT\S32K3XX\Dio_Example_S32K344 Of course, you can also directly open this folder path using the command line, as long as you ensure that it is in the same layer path as the. mk and makefile scr Fig 3 2.2.4   Project_parameters.mk modification Mainly modify the following points: TOOLCHAIN = iar IAR_DIR = C:/IAR/ewarm-9.70.1 TRESOS_DIR = C:/EB/tresos_29_0_0 PLUGINS_DIR = C:/NXP/SW32K3_S32M27x_RTD_R21-11_6.0.0/eclipse/plugins The path of IAR must be consistent with the version of IAR software used to ensure that the corresponding IAR compiler can be found. Fig 4 2.2.5   Check_build_params.mk modification Add the following content to check_build_params.mk: else ifeq ($(TOOLCHAIN),iar) ifeq ("$(wildcard $(IAR_DIR)/arm/bin/iccarm.exe)","") $(error Invalid path set to the IAR compiler. \ The provided path: from project_parameters.mk IAR_DIR=$(IAR_DIR) is invalid!) Endif Fig 5 2.2.6        Makefile modification   Makefile need the following 5 points modification: (1)Compilier change ifeq (${TOOLCHAIN},iar) CC := $(IAR_DIR)/arm/bin/iccarm.exe LD := $(IAR_DIR)/arm/bin/ilinkarm.exe AS := $(IAR_DIR)/arm/bin/iasmarm.exe # Intel Hexadecimal Flash image tool GENHEX := $(IAR_DIR)/arm/bin/ielftool.exe HEX_OPTS := --ihex OUT_OPTS := -o endif Fig 6 (2) SRC_DIRS  add TOOLCHAIN SRC_DIRS += $(foreach mod,$(MCAL_MODULE_LIST),$(PLUGINS_DIR)/$(mod)_$(AR_PKG_NAME)/src) \ $(foreach mod,$(MCAL_MODULE_LIST_ADDON),$(PLUGINS_DIR_ADDON)/$(mod)_$(AR_PKG_NAME_ADDON)/src) \ $(PLUGINS_DIR)/Platform_$(AR_PKG_NAME)/startup/src \ $(PLUGINS_DIR)/Platform_$(AR_PKG_NAME)/startup/src/m7 \ $(PLUGINS_DIR)/Platform_$(AR_PKG_NAME)/startup/src/m7/$(TOOLCHAIN) Fig 7 (3) Linker file  modification ifeq ($(LOAD_TO),flash) ifeq (${TOOLCHAIN},iar) LINKER_DEF:= $(PLUGINS_DIR)/Platform_$(AR_PKG_NAME)/build_files/${TOOLCHAIN}/linker_flash_$(DERIVATIVE_LOWER).icf else LINKER_DEF:= $(PLUGINS_DIR)/Platform_$(AR_PKG_NAME)/build_files/$(TOOLCHAIN)/linker_flash_$(DERIVATIVE_LOWER).ld endif else ifeq (${TOOLCHAIN},iar) LINKER_DEF:= $(PLUGINS_DIR)/Platform_$(AR_PKG_NAME)/build_files/$(TOOLCHAIN)/linker_ram_$(DERIVATIVE_LOWER).icf else LINKER_DEF:= $(PLUGINS_DIR)/Platform_$(AR_PKG_NAME)/build_files/$(TOOLCHAIN)/linker_ram_$(DERIVATIVE_LOWER).ld endif endif Fig 8 (4) Complier options change ifeq (${TOOLCHAIN},iar) ################################################################################ # iar Compiler options ################################################################################     clib        := $(IAR_DIR)/arm/lib     CCOPT           +=  --cpu=Cortex-M7 \                         -DAUTOSAR_OS_NOT_USED \                         -DUSE_MCAL_DRIVERS \                         --fpu=FPv5-SP \                         --cpu_mode=thumb \                         --endian=little \                         -e \                         -Ohz \                         --debug \                         --no_clustering \                         --no_mem_idioms \                         --do_explicit_zero_opt_in_named_sections \                         --require_prototypes \                         --no_wrap_diagnostics \                         --diag_suppress=Pa050 \                         $(MISRA) \                         -D$(PLATFORM) \                         -D$(DERIVATIVE) \                         -DIAR \                         -DUSE_SW_VECTOR_MODE  \                         -DENABLE_FPU \                         -DD_CACHE_ENABLE \                         -DI_CACHE_ENABLE                             LDOPT           :=  --entry _start \                         --enable_stack_usage \                         --skip_dynamic_initialization \                         --no_wrap_diagnostics \                         --cpu=Cortex-M7 \                         --fpu=FPv5-SP                             ASOPT           :=  $(ASOPT) \                         --cpu Cortex-M7 \                         --cpu_mode thumb \                         -g \                         -r \                         -DMULTIPLE_CORE   endif   Fig 9 Fig  10 So how did these IAR compilation options come about? You can refer to the release note of RTD600, which contains corresponding descriptions Fig 11 (5) Elf related change ifeq (${TOOLCHAIN},iar) %.elf: %.o $(LINKER_DEF)               @echo "Linking $@"               @$(LD) $(ODIR)/*.o $(LDOPT) --config $(LINKER_DEF) --map $(ODIR)/ -o $(ODIR)/$@@               @$(GENHEX) $(HEX_OPTS) "$(ODIR)/$(ELFNAME).elf" "$(ODIR)/$(ELFNAME).hex" else %.elf: %.o $(LINKER_DEF)               @echo "Linking $@"               @$(LD) -Wl,-Map,"$(MAPFILE)" $(LDOPT) -T $(LINKER_DEF) $(ODIR)/*.o -o $(ODIR)/$@@               @$(GENHEX) $(HEX_OPTS) "$(ODIR)/$(ELFNAME).elf" $(OUT_OPTS) "$(ODIR)/$(ELFNAME).hex" endif   Fig 12 2.2.7   Build to generate elf Commander: make clean make build to generate the elf files: Fig 13 After generation, the elf can be burned onto the S32K344 EVB board for testing. The test results show that the onboard red light is flashing, indicating that the IAR compiler can work in command-line mode. 3. Import RTD MCAL to IAR IDE project This chapter explains how to create an IAR IDE project and import MCAL drivers to implement S32K3 MCAL combined with EB tresos for running. 3.1 MCAL IAR IDE project 2 methods Difference between two methods and how to import MCAL drivers: (1) Directly copy the RTD MCAL driver to the IAR IDE project directory (2) Connect the IAR IDE project driver to the original RTD driver path Fig 14 3.2 MCAL IAR IDE project import steps 3.2.1 create the new RTD MCAL IAR project folder    Create a new folder, named as:S32K344_DIO_MCAL_RTD600_IAR 3.2.2 create the sub folder for IAR project       Generate:EB tresos project code       Include:app related include file       Mcal: mcal driver copy from RTD       src: project main file       Tresos_Project:EB tresos project Fig 15 3.2.3 create EB tresos project (1) Create the EB tresos project in the followign path:  S32K344_DIO_MCAL_RTD600_IAR\Tresos_Project\Mcal_Dio_S32K344_RTD600_IAR   (2)Add modules: BaseNXP, Dem, Dio, EcuC, Mcu, Platform, Port, Resource   (3)Copy RTD xdm files in the following path: C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Dio_TS_T40D34M60I0R0\examples\EBT\S32K3XX\Dio_Example_S32K344\TresosProject\Dio_Example_S32K344\config to: S32K344_DIO_MCAL_RTD600_IAR\Tresos_Project\Mcal_Dio_S32K344_RTD600_IAR\config   (4)EB tresos Generate project EB tresos code will be generated to folder: S32K344_DIO_MCAL_RTD600_IAR\Generate Fig 16 3.2.4 Copy RTD related drivers to IAR project folder (1) BaseNXP: header, include, src (2)Det:  include, src (3)Dio:  include, src (4)Mcu:  include, src (5)Platform: build_files, include, src, startup (6)Port: include, src (7)Rte: include, src Copy RTD folder to IAR project is one method, if don’t want to copy the file, also can use the linker to add the RTD install path drivers directly. Fig 17 3.2.5 IAR IDE create IAR project   (1) Project->Create new project   (2) In the IAR project, add group   The related folder in project can be structured like the fig 18, which contains:   Generate: Include and src->EB tresos project generate code   Mcal:  Base, Det, Dio, Mcu, Platform, Port, Rte->Mcal driver   Src: Main.c->project main code      (3) Add RTD mcal related drivers to IAR project The RTD MCAL related driver files can be directly downloaded from the RTD installation path or copied to a folder in the IAR project, and both methods yield the same result. Fig 18 (4)IAR project platform folder added result: Fig 19 (5)main code add Main.c can copy from path: C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Dio_TS_T40D34M60I0R0\examples\EBT\S32K3XX\Dio_Example_S32K344\src to S32K344_DIO_MCAL_RTD600_IAR\src Comment:  //#include "check_example.h"  // Exit_Example(TRUE);   3.2.6 IAR project options configuration (1)General options->Target->Device->NXP S32K344 (2)C/C++ Complier->Preprocessor Addional include directories: Use IAR project folder drivers which copied from RTD install path, the directories are: $PROJ_DIR$\Generate\include $PROJ_DIR$\mcal\BaseNXP_TS_T40D34M60I0R0\header $PROJ_DIR$\mcal\BaseNXP_TS_T40D34M60I0R0\include $PROJ_DIR$\mcal\Mcu_TS_T40D34M60I0R0\include $PROJ_DIR$\mcal\Platform_TS_T40D34M60I0R0\include $PROJ_DIR$\mcal\Rte_TS_T40D34M60I0R0\include $PROJ_DIR$\mcal\Platform_TS_T40D34M60I0R0\startup\include $PROJ_DIR$\mcal\Det_TS_T40D34M60I0R0\include $PROJ_DIR$\mcal\Dio_TS_T40D34M60I0R0\include $PROJ_DIR$\mcal\Port_TS_T40D34M60I0R0\include $PROJ_DIR$\include If use the RTD install path drivers, use the following directories: $PROJ_DIR$\Generate\include C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\BaseNXP_TS_T40D34M60I0R0\header C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\BaseNXP_TS_T40D34M60I0R0\include C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Mcu_TS_T40D34M60I0R0\include C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Platform_TS_T40D34M60I0R0\include C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Rte_TS_T40D34M60I0R0\include C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Platform_TS_T40D34M60I0R0\startup\include C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Dio_TS_T40D34M60I0R0\include C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Port_TS_T40D34M60I0R0\include C:\NXP\SW32K3_S32M27x_RTD_R21-11_6.0.0\eclipse\plugins\Det_TS_T40D34M60I0R0\include $PROJ_DIR$\include   Defined symbols: S32K3XX S32K344 IAR USE_SW_VECTOR_MODE D_CACHE_ENABLE I_CACHE_ENABLE ENABLE_FPU   Extra options: --no_clustering --no_mem_idioms --do_explicit_zero_opt_in_named_sections --require_prototypes --no_wrap_diagnostics   Languate 1:   Check Require prototypes   Diagnostics Suppress these disgnostics: Pa050 Fig 20 (3)Linker: Two points need to be added: $PROJ_DIR$\mcal\Platform_TS_T40D34M60I0R0\build_files\iar\linker_flash_s32k344.icf Library->Entry symbols: _start Fig 21 (4)Debugger Setup: PE micro, run to main Extra Options: Use command line options: --drv_vector_table_base=__ENTRY_VTABLE Fig 22 3.2.7  Build IAR project Project->Rebuild All Fig 23 3.2.8  Test result Download and debug result: Fig 24 After downloading and running, the red led is blinking on the board, indicating that the IAR IDE MCAL import method project has been successfully run.  
View full article
Abstract This example presents an use case for analogue data capturing using eMIOS, BCTU, SAR-ADC and DMA modules on S32K39-37-36 series based on the RTD low level API to support diverse application needs.   Connections: S32K396-BGA-DC1 -> Pin -> Signal -> Label J62-1 -> PTC30 -> siul2_gpio_xx -> GPIO1_GPT (D0) J58-1 -> PTE14 -> emios_0_ch_19_z -> PWM1 J58-2 -> PTG9 -> siul2_gpio_xx -> GPIO2_eMIOS_Trigger J62-2 -> PTC31 -> siul2_gpio_xx -> GPIO3_BTCU_Trigger J62-4 -> PTD6 -> siul2_gpio_xx -> GPIO4_BTCU_Watermark J62-24 -> PTB14 -> adc1_s21 -> ADC1 *To use the potentiometer of S32X-MB connect: J62-24 (in S32K396-BGA-DC1) to P26-1 (in S32X-MB) Note: Following line should be added in project/generate/src/Bctu_Ip_PBcfg.c every time the code is updated in Config Tools: #define DMA_LOGIC_CH_0 ((uint8)0U)   Detailed Description: The Compare Value of GPT eMIOS_0_ch_0 generates a time-out period. Once time-out is reached its Emios Notification toggles GPIO1. This allows us to observe in scope 2 events, which describe the start and the end of the signal sequence. The eMIOS_0_ch_23 channel is configured as global counter bus A. In this setup, it can act as the time base for other eMIOS_0 channels, enabling synchronization between other them—there is just one PWM in this case. This synchronization ensures that channels share the same time base, thereby defining a common period for their operation. The emios_0_ch_19_g channel is configured as OPWMT mode, which offer more flexibility for triggering. An interrupt is requested on every flag event, during which GPIO2 is toggled—happens at half the time high in this case. This flag event, can be configured using Trigger parameter. For more details about eMIOS, please refer to S32M27x/S32K3 – eMIOS Usage, considering differences for porting from S32K3 to S32K39-37-36 in AN14301. The BCTU implements a list for parallel conversions using ADC0 and ADC1. Which is triggered by the eMIOS channel, and the resulting data is stored in FIFO1, as follows: ADC0: VREFH_ChanNum51 -> BANDGAP_ChanNum48 ADC1: VREFL_ChanNum50 -> S21_ChanNum45 For debugging purposed the GPIO3 is toggled every BCTU Trigger Notification. Additionally, the GPIO4 is toggled in BCTU Watermark Notification, which happens every time the number of active entries in FIFO exceeds the watermark level, and therefore the data is available for reading. See full signal sequence in Figure 1: Figure 1. Signals of example project When you suspend debug session, in Expressions tab (Figure 2) you can observe results: g_fifo1Result, which corresponds to the BCTU list measurements, meanwhile g_fifo1Volts corresponds to the conversion in volts. Figure 2. Expressions tab of example project   References S32 Design Studio for S32 Platform Real-Time Drivers (RTD) S32K39, S32K37 and S32K36 Data Sheet [S32K39-S32K37-DS] S32K39, S32K37, and S32K36 Reference Manual [S32K396RM] S32K344 to S32K39/S32K37 Migration Guide [AN14301] S32K39/37/36 Electrification Microcontrollers Evaluation Board [S32K396-BGA-DC1] S32X-MB I/O Extension Evaluation Board for Real-Time Domain Control and Actuation [S32X-MB] S32M27x/S32K3 – eMIOS Usage [S32M Knowledge Base] S32M27x/S32K3 – eMIOS/BTCU/ADC/DMA – [RTD600] [S32M Knowledge Base] S32K39-37-36 – eFlexPWM/TRGMUX/BCTU/SAR-ADC/DMA – [RTD600] [S32M Knowledge Base] Application Software: - S32K396_RTD600_eMIOS_BCTU_SARADC_DMA_Ip_example Example was built and tested using the following IDE and Driver versions: - S32 Design Studio for S32 Platform Version 3.6.3 - S32K3_S32M27x Real-Time Drivers ASR R21-11 Version 6.0.0
View full article
This example code brief  :-- 1> Tested without the SL of BMS, so no dependency on the BMS Safety library. 2> Its tested on 2 AFE MC33775 board connected in TPL 3> Change following macro in mc33775_cfg.h file  to change the numbers of AFE connected in TPL.   RTD : 3.0.0 P07 BMS SDK : 1.0.2 This example does this task :-- Application Measurement. SYNC measurement Periodic Measurement. Read AFE temperature. Cell balancing timer method. Reading the Cell balancing status register & fault registers. =================== Setup used ============ Attached code is tested with TWO MC33775 AFE connected in TPL mode.   =============== MCU Pins used =========== TPL1-TX :-- TPL1TXCSB  --> PTC6/LPSPI0_PCS1 TPL1TXSCLK --> TPL12TXCLK --> PTE1/LPSPI0_SCK    TPL1TXDATA --> TPL12TXDATA --> PTE2/LPSPI0_SOUT    TPL1-RX :-- TPL1RXCSB  --> PTB17/LPSPI1_PCS3 TPL1RXCLK  --> PTB14/LPSPI1_SCK TPL1RXDATA --> PTB15/LPSPI1_SIN     ================= EVB Link ================== https://www.nxp.com/design/design-center/development-boards-and-designs/18-cell-battery-pack-emulator-to-supply-mc33774-bcc-evbs:BATT-18EMULATOR https://www.nxp.com/design/design-center/development-boards-and-designs/analog-toolbox/evaluation-board-for-mc33664atl-isolated-network-high-speed-transceiver:FRDMDUALK3664EVB https://www.nxp.com/design/design-center/development-boards-and-designs/RD33775ADSTEVB https://www.nxp.com/design/design-center/development-boards-and-designs/automotive-development-platforms/s32k-mcu-platforms/s32k3x4evb-t172-evaluation-board-for-automotive-general-purpose:S32K3X4EVB-T172   ============= Using Debugger ============ Debugger breakpoint will cause the communication timeout at the AFE, which will RESET the AFE. To use the debugger while development you need to disable the communication timeout. In S32DS MEX file you cannot disable the timeout function ( limit the value of 0~255) Disable Communication timeout in code :--   ================= Results for FIRST AFE ===========================          
View full article
Abstract This example presents an use case for complementary PWM outputs with dead-time insertion and hardware ADC triggering using eFlexPWM, TRGMUX, BCTU, SAR-ADC and DMA modules on S32K39-37-36 series based on the RTD low level API to support diverse application needs. Connections: S32K396-BGA-DC1 -> Pin -> Signal -> Label J62-1 -> PTC30 -> siul2_gpio_94 -> GPIO1_GPT J62-5 -> PTD2 -> pwm_0_a, 2 -> PWM1 J62-6 -> PTD3 -> pwm_0_b, 2 -> PWM2 J62-30 -> PTD24 -> pwm_0_a, 0 -> PWMT J62-2 -> PTC31 -> siul2_gpio_95 -> GPIO3_BTCU_Trigger J62-4 -> PTD6 -> siul2_gpio_102 -> GPIO4_BTCU_Watermark J62-24 -> PTB14 -> adc1_s21 -> ADC1 *To use the potentiometer of S32X-MB connect: J62-24 (in S32K396-BGA-DC1) to P26-1 (in S32X-MB)   Note: Following line should be added in project/generate/src/Bctu_Ip_PBcfg.c every time the code is updated in Config Tools: #define DMA_LOGIC_CH_0 ((uint8)0U)   Detailed Description: The Compare Value of GPT eMIOS 0 channel 0 generates a time-out period. Once time-out is reached its eMIOS notification toggles GPIO1. This allows us to observe in scope 2 events, which describe the start and the end of the signal sequence. The eFlexPWM0 module is used for generating PWMs and hardware ADC triggering. The eFlexPWM0 Submodule 2 is employed to generate center-aligned complementary PWM outputs (PWM1 and PWM2) with dead-time insertion. The eFlexPWM0 Submodule 0 generates another independent PWM output (PWMT) and is utilized to generate the trigger signal for analog data capturing within the same PWM period —happens at half the time high in this case—using VAL0 register. The BCTU implements a list for parallel conversions using ADC0 and ADC1. Which is triggered by the eMIOS channel, and the resulting data is stored in FIFO1, as follows: • ADC0: VREFH_ChanNum51 -> BANDGAP_ChanNum48 • ADC1: VREFL_ChanNum50 -> S21_ChanNum45 For debugging purposed the GPIO3 is toggled every BCTU Trigger Notification. Additionally, the GPIO4 is toggled in BCTU Watermark Notification, which happens every time the number of active entries in FIFO exceeds the watermark level, and therefore the data is available for reading. See full signal sequence in Figure 1: Figure 1. Signals of example project When you suspend debug session, in Expressions tab (Figure 2) you can observe results: g_fifo1Result, which corresponds to the BCTU list measurements, meanwhile g_fifo1Volts corresponds to the conversion in volts. Figure 2. Expressions tab of example project   References S32 Design Studio for S32 Platform Real-Time Drivers (RTD) S32K39, S32K37 and S32K36 Data Sheet [S32K39-S32K37-DS] S32K39, S32K37, and S32K36 Reference Manual [S32K396RM] S32K344 to S32K39/S32K37 Migration Guide [AN14301] S32K39/37/36 Electrification Microcontrollers Evaluation Board [S32K396-BGA-DC1] S32X-MB I/O Extension Evaluation Board for Real-Time Domain Control and Actuation [S32X-MB] S32K39-37-36 – eMIOS/BTCU/SAR-ADC/DMA – [RTD600] [S32K Knowledge Base]   Application Software: - S32K396_RTD600_eFlexPWM_TRGMUX_BCTU_SARADC_DMA Example was built and tested using the following IDE and Driver versions: - S32 Design Studio for S32 Platform Version 3.6.3 - S32K3_S32M27x Real-Time Drivers ASR R21-11 Version 6.0.0
View full article
****************************************************************************************************** * Detailed Description: These demos showcase how to configure the eMIOS module on the S32K3 series, highlighting various operational modes and their implementations using the RTD high-level drivers, commonly known as MCAL drivers. The implementations demonstrated in these examples follow the approach outlined in the community thread:  S32M27x/S32K3 – eMIOS Usage. * Connections:  ******************************************************************************************************* * Test HW: S32K31XEVB-Q100 * MCU: S32K311 * Debugger: S32DS 3.6.2, OpenSDA/ PEmicro Multilink Universal FX  * Target: internal_FLASH ******************************************************************************************************* * Important information:  The OPWMT channel does not support the notification function. In this mode, the Sn[FLAG] bit is only set upon an AS2 match, which defines the generation of a trigger event within the PWM period. As a result, OPWMT mode cannot support notifications based on signal edges. A bus exception may occur during the execution of Mcl_Init() if the eMIOS clock is not properly enabled. To avoid this issue, ensure that the eMIOS peripheral clock is activated in the configuration settings under: MCU driver → McuModuleConfiguration → McuModeSettingConf → McuPeripheral *******************************************************************************************************
View full article
* ================================================================================================== * Detailed Description: * * This example shows how to implement ADC continuous scan with DMA read. * ADC1 is set to perform continuous scan of 4 channels (S10/S11/S12,S13) with DMA request enabled * for last channel S13. DMA reads respective sequential ADC data registers in one major loop. * * ADC1 channel S10 is connected to board's potentiometer, converted value is used to dim board's LED. * * ================================================================================================== * Test HW: S32K312EVB-Q172 * MCU: S32K312_172LQFP * Compiler: S32DS 3.6.3 * RTD release: S32K3_S32M27x Real-Time Drivers ASR R21-11 Version 6.0.0 * Debugger: On-Board Debugger (J40), Lauterbach * Target: Internal_FLASH * ==================================================================================================   Any support, information, and technology (“Materials”) provided by NXP are provided AS IS, without any warranty express or implied, and NXP disclaims all direct and indirect liability and damages in connection with the Material to the maximum extent permitted by the applicable law. NXP accepts no liability for any assistance with applications or product design. Materials may only be used in connection with NXP products. Any feedback provided to NXP regarding the Materials may be used by NXP without restriction.  
View full article