S32 Design Studio Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio Knowledge Base

Discussions

Sort by:
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for ARM® 2018.R1  Update 10          What is new? S32K1xx SDK RTM-SR 3.0.1 introducing support for three new pin variants: S32K142 - 48LQFP, S32K144 - 48LQFP, S32K148 - 100LQFP and for two new TJA devices: TJA1101HN (NXP) Production and TJA1102HN (NXP) Production  (S32K1xx SDK release notes) This is a cumulative update - it includes all the content of previous updates (Update 1, Update 2, Update 3, Update 4, Update 5, Update 6, Update 7, Update 8, Update 9 ) Installation instructions The update is available for online (via Eclipse Updater) or offline installation (direct download link)  installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_ARM_2018.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use direct link to download the update archive zip file Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive .zip file you downloaded in the previous step Select all available items and click "Next" button.   This will starts the update installation process.
View full article
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1 Update 10          What is new? S32 SDK for Power Architecture 2.9.0 BETA supporting  S32R274, S32R372, MPC574x-B-C-G, MPC574x-P, MPC574x-R and MPC577x-B-E-C (see the S32 SDK release notes) Updated version of GCC 4.9.4 tools AMMCLIB version 1.1.15 (see the AMMCLIB MPC574xP example release notes) Updated version of SPT tools for SPT 2.5 Updated version of P&E This is a cumulative update - it includes all of the content of previous updates (Update 1, Update 2, Update 3, Update 4, Updates 5 and 6, Update 7, Update 8, Update 9 ). Installation instructions The update is available for online installation (via S32DS Eclipse Updater) or offline installation (direct download link)  installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_2017.R1/updatesite" select all available items and click "Next" button offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use direct link to download the update archive zip file  Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button.   This will start the update installation process.
View full article
By defalut is SDK code in examples linked into project. Unfortunately there is no GUI config option, but this settings can be changed in ProcessorExpert.pe file - located in project's root folder.  First of all - backup your project. Locate SDK folder in project and delete all content. When done - close your project.  Open ProcessorExpert.pe file located in project's root folder in any text editor (it is XML file), locate <ProjectStaticFilesGenerationMode> tag and change value from LINKED to STANDALONE: Save changes and open again your project in S32DS. Generate processor expert code:  Now - all SDK code is copied into workspace:  There are also linked files in Project_Settings. Easiest way is just create an empty non SDK project and copy linker script and startup assembly to your project:  Make sure, that Linker uses your copied linker script file: 
View full article
1) Prepare the evaluation board hardware You can use the S32 Debug Probe to download code to target Connect S32 Debug Probe to S32V234 EVB using JTAG connector Connect S32 Debug Probe to PC via USB cable OR ethernet (if connected via ethernet, then USB power cable must also be connected) Connect the S32V234 EVB to PC via ethernet (typically via LAN) Connect power cable to evaluation board and switch on the power     2) Build the project using either the A53 or the TEST_A53 build options. 3) The project is now built and the ELF file is ready to be loaded to the EVB for execution. Before a debug session can be started, we must complete HOWTO: Setup A Remote Linux Connection in S32DS (S32V234). Start A53 Debug 4) Select the debug drop-down menu and click Debug Configurations     5) Make sure the Debug_Remote_Linux debug configuration is selected and the connection setup in step 4 is selected (points to the IP address of your EVB). Click Debug     6) The first time you connect to a new IP address (i.e. the first time you debug after creating a new workspace), you will receive a warning message, Click Yes and proceed.     The executable file is copied to Linux file system and gdbserver starts. You may get an error message on the first try, this is normal. Just try it again and it will work. 7) Once the Linux GDB has started on A53 core and the initial breakpoint is reached in main(), we need to set a breakpoint at the function apu_hal_Enable().    This breakpoint has already been created for you, you just need to enable it! Locate the breakpoint in the Breakpoints view. Due to some known issues with Eclipse CDT, it is necessary to enable->disable->enable the breakpoint so it will work properly. The issue only affects this breakpoint, due to the way it is provided, and will not affect breakpoints which you set elsewhere in the code. 😎 Press Resume twice, so that the breakpoint which was set at apu_hal_enable() is reached for the 2nd time. 9) Open Debug Configurations. You will see a debug configuration within the 'S32 Debugger' group (FAST9COLOR as shown below). This is the debug configuration we will use, however, it will require some setup.     10) You should notice the error message at the top of the window, just below the title and a red 'X' on the Debugger tab. Click on the Debugger tab to select it. We must setup the Debug Probe Connection before we can proceed. There are two options: Ethernet USB   If connecting the Probe via Ethernet, please refer to the Quick Start Guide or S32 Debug Probe User Guide provided with the S32 Debug Probe for instructions on how to connect it and determine the Hostname or IP address.     If connecting the Probe via USB, then the COM port will appear in the Port selection setting. If you have more than one S32 Debug Probe connected, you will need to determine which COM port is the correct one, otherwise, only the COM port for your S32 Debug Probe will appear.       11) Click Apply then Debug. It may take a few moments for the APEX core debug to launch.   12) It may take a moment or two before the APEX2 debug thread launch is complete, see the Thread listed within the <kernel_name>[S32 Debugger] in the Debug window. Also note, a new breakpoint is listed in the Breakpoints view. This breakpoint is set for you at the start of the APEX2 graph function. 13) The debugger context is still on the A53 thread. Press RESUME and then select the APEX2 thread to see that it has stopped on the graph function break point. Now you can step through the graph. 14) To step through a kernel, locate the call to the kernel function in the graph function and set a break point on the line. 15) Press RESUME to advance the program counter to the new break point 16) Press STEP INTO to advance the program counter into the kernel. It may take several steps as the optimizations performed by the compiler produce some synchronization inconsistencies. 17) You may need to help the IDE to locate the source files. Now you can see the kernel wrapper function... and the kernel! 18) Step through, monitor variables and registers and set breakpoints.
View full article
1) Prepare the evaluation board hardware You can use the S32 Debug Probe to download code to target Connect S32 Debug Probe to S32V234 EVB2 using JTAG connector Connect S32 Debug Probe to PC via USB cable OR ethernet (if connected via ethernet, then USB power cable must also be connected) Connect the S32V234 EVB2 to PC via ethernet (typically via LAN) Connect power cable to evaluation board and switch on the power     2) Build the project using the A53 build option. 3) The project is now built, and the ELF file is ready to be loaded to the EVB for execution. Before a debug session can be started, we must complete HOWTO: Setup A Remote Linux Connection in S32DS (S32V234). Start A53 Debug 4) Select the debug drop-down menu and click Debug Configurations     5) Make sure the '{project_name}_Remote_Linux' debug configuration is selected and the Connection (see step 3) is selected (points to the IP address of your EVB). Click Debug     6) The first time you connect to a new IP address (i.e. the first time you debug after creating a new workspace), you will receive a warning message, Click Yes and proceed.     The executable file is copied to Linux file system and gdbserver starts.   You may get an error message on the first try, this is normal. Just try it again and it will work. 7) Once the Linux GDB has started on A53 core and the initial break point is reached in main(), it is almost ready for to start debug on ISP. Click Resume as the A53 must be running before we can attach the ISP debug thread. 😎 Return to the Debug Configurations menu and locate the ISP debug configuration. You will see a debug configuration within the 'S32 Debugger' group (in our example, isp_sonyimx224_csi_dcu_mipi_simple_IPUS0 as shown below). This is the debug configuration we will use, however, it will require some setup.     9) You should notice the error message at the top of the window, just below the title and a red 'X' on the Debugger tab. Click on the Debugger tab to select it. We must setup the Debug Probe Connection before we can proceed. There are two options: Ethernet USB   If connecting the Probe via Ethernet, please refer to the Quick Start Guide or S32 Debug Probe User Guide provided with the S32 Debug Probe for instructions on how to connect it and determine the Hostname or IP address.     If connecting the Probe via USB, then the COM port will appear in the Port selection setting. If you have more than one S32 Debug Probe connected, you will need to determine which COM port is the correct one, otherwise, only the COM port for your S32 Debug Probe will appear.   10) This is already done for our example, but for your application, it may be necessary to setup the symbols for the ISP engine. Go to the Startup tab and:    a) Check the box for 'Load symbols'    b) Select the option for 'Use file', click Workspace... and locate the object file (.opius) for the ISP engine you wish to debug.   11) Click Apply then Debug. It may take a few moments for the ISP core debug to launch.   12) Wait for the ISP debug launch to complete. You may notice the A53 thread has terminated. This is normal and expected since the camera input cannot be suspended. When the launch completes, the context of the Debug window will switch to the ISP debug thread. 13) Enable Instruction Stepping mode and then step one time to load the object file which was setup in step 6. 14) The ISP debugging is now running and you can step through the ISP engine, look at registers, set a break point, etc. Note: only one hardware break point is supported for ISP.
View full article
This document details how to create a new project in S32 Design Studio and build using the existing code and makefile provided within the NXP Vision SDK example projects. If you are creating a new makefile project with code from any other source, the procedure may be different. Before creating a new makefile project from existing code we need to add some paths to the environment variable PATH and a couple of new environment variables. There are 3 main methods for adding these paths and variables. Which method depends upon your needs. Method 1 The paths and variables can be added to each project individually. This is useful if you only want these changes to affect a small number of projects. Or if your projects require different paths and variables. Note: these changes would be made after the project is created (shown in steps 15 - 17 below) Method 2 The paths and variables can be added to the entire workspace within S32DS . These will not be visible outside of S32DS and therefore will not affect the entire Windows environment. This is useful if you have a large number of projects with common requirements for paths and variables and do not want them visible any tools outside of S32DS. Method 3 The paths and variables can be added globally to the Windows environment and will affect all installed tools. This method is not recommended. Once you have selected a method, add the following paths to the PATH variable (paths shown using the default installation settings for S32DS): C:\NXP\S32DS.3.1\S32DS\build_tools\gcc-6.3-arm32-eabi\bin C:\NXP\S32DS.3.1\S32DS\build_tools\gcc-6.3-arm64-eabi\bin C:\NXP\S32DS.3.1\S32DS\build_tools\gcc-6.3-arm64-linux\bin C:\NXP\S32DS.3.1\S32DS\build_tools\msys32\mingw32\bin or if within Eclipse (can use variables, which don't need to be updated should the layout of S32DS installation change in a future release) ${S32DS_ARM32_TOOLCHAIN_DIR} ${S32DS_ARM64_LINUX_TOOLCHAIN_DIR} ${S32DS_ARM64_TOOLCHAIN_DIR} ${S32DS_GCC_TOOCHAIN_DIR} It is also necessary to add the following Windows system variables: Variable Name: S32V234_SDK_ROOT Variable Value: C:\NXP\S32DS_Vision_v2018.R1\S32DS\s32v234_sdk Variable Name: APU_TOOLS Variable Value: C:\NXP\S32DS_Vision_v2018.R1\S32DS\APUC The following steps demonstrate the procedure based on Method 1 above. 1) Launch S32DS for Vision 2) Click New 3) Select 'Makefile Project with Existing Code' 4) Select Next 5) Enter a name for the project. 6) For 'Existing Code Location',    a) Select 'Browse...' and then select the directory  C:\NXP\S32DS.3.1\S32DS\software\VSDK_S32V2_RTM_1_3_0\s32v234_sdk\demos\isp\isp_sonyimx224_rgb_yuv_gs8    b) Click OK 7) For 'Toolchain for Indexer Settings', select the option which matches your desired build configuration. For our example here, we will select 'ARM Linux 64-bit Target Binary Toolchain'. See the Vision Extension Package User Guide for more details on the toolchain options. This sets up some toolchain paths, but later we will set more for the specific needs of the VSDK examples. 😎 Click Finish 9) Right-click on the project from the Project Explorer. Select Properties 10) Go to section 'C/C++ Build' 11) Go to the 'Behavior' tab and in the field next to 'Build', enter:    ISP examples: 'allsub'    APEX examples: 'APU_COMP=nxp allsub' 12) Go to 'Builder Settings' tab, in 'Build location' section change the path for the 'Build directory'. Click on 'Workspace...' button 13) In the Folder selection menu, select the subfolder 'build-v234ce-gnu-linux-d' and click OK 14) Go to section 'Environment' 15) Select the environment variable 'PATH' and click 'Edit...' 16) Add the path variables to the value field, each separated by a comma ';' ${S32DS_ARM32_TOOLCHAIN_DIR} ${S32DS_ARM64_LINUX_TOOLCHAIN_DIR} ${S32DS_ARM64_TOOLCHAIN_DIR} ${S32DS_GCC_TOOCHAIN_DIR} Click OK 17) Click 'Add...' 18) Click 'Add...' and enter variable name 'APU_TOOLS' and value '${S32DS_APU_TOOLCHAIN_DIR}' Click OK 19) Click OK to close the Properties menu. 20) Click on 'Build' 21) Once the build is complete, the binary file (ELF) will be created
View full article
In this document, we show the steps to use the New Project Wizard to create a new application project for APEX2, ISP, or both.   1. Launch S32DS for Vision 2. Select File -> New -> S32DS Application Project 3. Enter a name for the project 4. Select the 'A53 APEX2/ISP Linux' processor option 5. Click Next 6. Select the APEX2/ISP options you need.       a. APEX2 programming - will add support to your project for an APEX2 application, you need this for any new APEX2 project       b. ISP programming - will add support to your project for an ISP application, you need this for any new ISP project       c. ISP visual modeling - will create a separate project for your ISP data flow diagram, you will not need this if you plan to use an existing graph diagram. This can also be created later. 7. Select the SDK(s) as appropriate for your setup. For example, 'VSDK_MODULE_WIN' for Windows OS or 'VSDK_MODULE_LINUX' for Linux OS, the one which corresponds to your OS is selected for you by default. 7. Click Finish 8. You now have a project or set of projects for development on the S32V234.
View full article
One of the many great features of the S32DS is the ability to access the Linux BSP file system on the SD card in the S32V234-EVB. Once connected, you can drag and drop files between your PC and the EVB. Once you have completed HOWTO: Setup S32V234 EVB2 for debugging with S32DS and Linux BSP  and HOWTO: Setup A Remote Linux Connection in S32DS (S32V234), you are ready to setup the Remote Systems view to connect to the Linux files system to view and access the file system. Prerequisite Before starting this procedure, make sure the BSP is loaded onto the SD Card, the SD Card is inserted into the SD Card Slot, the ethernet cable is connected to both the EVB and the network port, and the EVB is powered up. 1) Go to 'Window -> Show View -> Other' 2) Expand 'Remote Systems', then select "Remote Systems' and click OK 3) Click 'Define a connection to remote system' button OR right-click in the Remote Systems window and select 'New Connection...' from the list Right-click menu 4) Select 'SSH Only' 5) Enter the IP address noted from HOWTO: Setup A Remote Linux Connection in S32DS (S32V234) for Host name, enter a descriptive name for the connection (optional) and click Finish. 6) Right-click on the connection name in the Remote Systems window and select 'Connect' OR expand the folders under the connection name until the login window appears: Connection_name -> Sftp Files -> Root (window appears) 7) Enter "root" for User ID and since the BSP comes with ID root without a set password, leave the password field blank. 😎 Click OK 9) The Linux file system is now visible in the Remote Systems window. You can drag and drop files to and from here. Expand the folders to see the contents.
View full article
The Vision SDK root is contributed to the Design Studio as a dynamic path variable “S32DS_VSDK_DIR”. Several Design Studio services use this variable to access the resources inside the Vision SDK. By default, this variable points to “${eclipse_home}../S32DS/s32v234_sdk”, i.e. to the Vision SDK shipment bundled with Design Studio. Technically you can change this variable to point to another instance of Vision SDK using the following steps: 1. Go to the main menu "Window -> Preferences" 2. Filter the preference dialog with "sub" keyword or just navigate to "Run/Debug -> String Substitution node. 3. Edit Variable "S32DS_VSDK_DIR" to assign another value to be substituted as Vision SDK root 4. Press OK when changes are complete.
View full article
There are a number of existing ISP Graph diagrams provided within the VSDK. It is possible to import them into S32DS and use them in a new C/C++ project. The steps to do this are detailed within this document. Prerequisite Before following the steps in this HOWTO, ensure you have the Vision Extension Package for V2xx (as well as the S32V2xx development package) installed to S32DS. 1) Launch S32DS 2) Select File -> New -> S32DS Application Project. 3) Enter a project name, such as: ISP_ISP_Generic_demo 4) Select 'A53 APEX/ISP Linux' 5) Click Next 6) Deselect the APEX2 options and 'ISP Visual Modeling' option. 7) Click Finish 😎 Select File -> New -> S32DS Project from Example. 9) Select isp_generic. 10) Select Finish 11) Open isp_generic in the project explorer 12) Double-click ISP data flow ; isp_generic. The ISP data flow graph will appear in the editor 13) Define a new configuration for emitting code from the graph       a) Right-click in the ISP data flow window and select Emit As -> Emit Configurations...       b) Select ISP Emitter       c) Press New Launch Configuration       d) Enter a name       e) To select the graph, press Browse Workspace       f) Expand each item until you can select the .isp file. Click OK       g) Select the location of the emitted output to the application project, select Browse Workspace       h) Select the name of your application project, then press OK       i) Enter 'A53_gen' to the Dynamic sequences sources folder box. This is the folder within the target project that generated code will be stored. Check the box for Emit host code.       j)Now select the location to store the configuration file. Go to the Common tab, select Shared file and click Browse       k) Select the .launches folder inside ISP_ISP_Generic_demo and click OK       l) Click Apply and Emit. Dialog box will appear when code generation is successful              m) Expand the folders within ISP_ISP_Generic_demo, A53_gen, src and inc, to see the newly generated output files 14) Build the project 'ISP_ISP_Generic_demo' for ISP 15) Open file 'ISP_ISP_Generic_demo/A53_inc/isp_user_define.h', by double clicking on it in the Project Explorer. Change '#define DCU_BPP DCU_BPP_YCbCr422' to '#define DCU_BPP DCU_BPP_24' and change '#define __DCU_BPP' to "#undef __DCU_BPP". Before After 16) Using the method detailed in steps 8 - 10, create the example project 'isp_sonyimx224_csi_dcu'. Take from this project the file 'isp_sonyimx224_csi_dcu/A53_src/main.cpp' and use it to replace the file 'ISP_ISP_Generic_demo/A53_src/main.cpp' in the current project. Then make the following modifications:  On line 36, change <#include "mipi_simple_c.h"> to <#include "isp_generic_c.h">. On line 303, change <gpGraph_mipi_simple> to <gpGraph> AND <gGraphMetadata_mipi_simple> to <gGraphMetadata> On line 330, change <FDMA_IX_FastDMA_Out_MIPI_SIMPLE> to <FDMA_IX_ISP_OUTPUT>. Please see C:\NXP\S32DS.3.1\S32DS\software\VSDK_S32V2_RTM_1_3_0\s32v234_sdk\docs\drivers\SDI_Software_User_Guide.pdf for details on what this code is for. 17) In Project Explorer, right-click on "...\A53_gen\src\isp_process.cpp" and select Build path -> Remove from -> A53 18) Select 'ISP_ISP_Generic_demo:A53' in the Project Explorer panel, then Build for A53 19) Run it remotely on the target using the method fromHOWTO: Create S32V234 Cortex-A53 Linux Project in S32DS . Should get results similar to this:
View full article
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for ARM® 2018.R1  Update 9          What is new? S32K1xx SDK RTM 3.0.0 supporting S32K116, S32K118, S32K142, S32K144, S32K146, and S32K148  (S32K1xx SDK release notes) AMMCLIB version 1.1.15  (AMMCLIB S32K14x release notes) Segger J-Link drivers v6.42a (J-Link release notes) This is a cumulative update - it includes all the content of previous updates (Update 1, Update 2, Update 3, Update 4, Update 5, Update 6, Update 7, Update 8) Installation instructions The update is available for online (via Eclipse Updater) or offline installation (direct download link)  installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_ARM_2018.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use direct link to download the update archive zip file Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive .zip file you downloaded in the previous step Select all available items and click "Next" button.   This will starts the update installation process.
View full article
S32DS for Vision contains many example projects from which you can learn how S32DS, with the Vision Extension Package for V2xx, can be used with the help of the Vision SDK to develop vision applications. The example projects contain generated and hand-written code, which utilize the Vision SDK to demonstrate a workflow using S32DS. In this document, the procedure for creating a project from one of the provided ISP examples through to execution on the EVB is detailed. Prerequisite Before following the steps in this HOWTO, ensure you have the Vision Extension Package for V2xx (as well as the S32V2xx development package) installed to S32DS. 1) Launch S32DS 2) Select "New S32DS Project from example" 3) Select isp_sonyimx224_csi_dcu project and click Finish.    In this particular project, the ISP graph diagram is included. If you wish to view it, go to the Project Explorer panel and expand 'isp_sonyimx224_csi_dcu_graph'. Then double click on 'ISP data flow : mipi_simple'. The ISP graph diagram will appear in the editor panel. 5) We are ready to build the project, but first, select isp_sonyimx224_csi_dcu: A53 in the Project Explorer panel 6) Build project for A53  7) Start a debug session using method as described in HOWTO: Create S32V234 Cortex-A53 Linux Project in S32DS, beginning at step 10. 😎 Should get results similar to this:
View full article
This tutorial walks a user through the steps to create a new application for the S32V234 MCU using S32DS (with S32V2xx development package and Vision extension package for S32V2xx) and the built in APEX2 Visual Graph tool. The completed application will take a PNG image, upscale and downscale it using APEX engines and return the processed images. Prerequisites: Some knowledge of the S32V234 System on a Chip (SoC) Have an understanding of the APEX architecture and APEX Core Framework (ACF) Refer to UG-10267-03-14-ACF_User_Guide.pdf to learn about ACF Path: s32ds_install_dir\S32DS\software\VSDK_S32V2_RTM_x_x_x\s32v234_sdk\docs\apex\acf Be familiar with the NXP Vision SDK software Looking for Interactive Tutorial? You can view this tutorial as a video, go to Getting started with S32 Design Studio IDE including Vision Extension Package for S32V processors | NXP and select '4 | Create a new APEX2 application'
View full article
This tutorial walks a user through the steps to create a new application for the S32V234 MCU using S32DS (with S32V2xx development package and Vision extension package for S32V2xx) and the built in ISP Visual Graph tool. The completed application will take an image from camera, processes it on ISP and put the processed image in DDR buffers. Once the image is in DDR buffer, host (A53 core running Linux) will direct the display control unit (DCU) to display it on screen. Prerequisites: Some knowledge of the S32V234 System on a Chip (SoC) Have an understanding of the ISP architecture Be familiar with the NXP Vision SDK software Looking for Interactive Tutorial? You can view this tutorial as a video, go to Getting started with S32 Design Studio IDE including Vision Extension Package for S32V processors | NXP and select '3 | Create a new ISP Application'
View full article
Getting started with APEX2 S32DS: Getting Started - APEX2 Graph Tool Tutorial  Getting started with ISP S32DS: Getting Started - ISP Graph Tool Tutorial 
View full article
So you have created a project in S32DS with target of S32V234 Cortex-A53 APEX2/ISP Linux . You have built the project and now want to execute it on the S32V234-EVB2, which is running the Linux BSP for the VSDK on a microSD card. There are many ways to do this, however, the simplest is to use the built-in support within S32DS to run and/or debug over an Ethernet connection to the Linux BSP OS running on the EVB. In order for S32DS to connect to the Linux BSP OS, the following steps should be followed: 1) First, we must complete the steps in HOWTO: Setup S32V234 EVB2 for debugging with S32DS and Linux BSP . 2) With the Linux running on the EVB, start a terminal program (for ex. PuTTY) on your PC 3) Set Connection type to Serial 4) Set speed to 115200, Data bits 8, Stop bits 1, Parity None 5) Set Serial line to the COM port associated with the USB port setup in step 1 of this document. (for ex. COM3) 6) Click Open to start the terminal session 7) Press enter key to bring up login prompt 😎 Log into Linux (login name is "root") 9) Get IP address, enter command:    ifconfig       Make note of the IP address 10) Launch S32DS for Vision. From the C/C++ Perspective, select Run->Debug Configurations... 11) From 'C/C++ Remote Application'. Select '<project_name>_Remote_Linux' debug configuration. 12) Select New to create new debug connection. 13) Select SSH 14) Enter the IP address noted earlier 15) Enter user ID as "root". The Linux BSP uses Password based authentication, but by default, no password is set. So the password can be left blank. 16) Select Finish 17) Select Apply, and then if you wish, Debug This connection is stored within the workspace. It can be added to any projects within the workspace. If a new workspace is created, then this connection will not appear in the selection list.
View full article
While the S32V234-EVB2 comes shipped with an SD card preloaded with a Linux Board Support Package(BSP), it does not support the Vision Software Development Kit(VSDK). This you will have to load yourself. There are two methods for installing the S32V234 BSP for VSDK to your SD card: 1) Download the image file from your Software Account on nxp.com and write the file to the SD card, or 2) Create the image on the SD card from ubuntu installed on a PC or virtual machine Download the image file and write it to SD card This is the simplest method, but does not allow for much customization. It is an excellent choice for those users who do not have much experience with Linux or just need something quick to get up and running with S32 Design Studio, try out the application examples, etc. Procedure 1) Login to your account on NXP.COM (if you do not already have an account, then just register for one) 2) Go to Vision SDK Software  3) Accept the license agreement 4) Select the version of VSDK you wish to use 5) Check the box next to 'VisionSDK RTM x.x.x pre-built SD Card image based on Yocto rootfs' and click 'Download selected files'. This will download the .gz file to your PC. 6) Unpack the VisionSDK_S32V2_RTM_x_x_x_img_yocto.tar.gz archive file 7) Unpack the VisionSDK_S32V2_RTM_x_x_x_img_yocto.tar archive file 😎 Navigate to the '\build_content\v234_linux_build\s32v234evb' folder, then unpack the sdcard-evb.tar.bz2 file 9) Unpack the sdcard-evb.tar file 10) The resulting file is sdcard-evb.img. You can use an image writing tool (such as Win32 Disk Imager download | SourceForge.net) to write this image file to the SD card. You will need to use the SD card adapter to insert the microSD card into the SD card slot on your PC, if available. If you do not have an SD card slot on your PC, there are many SD card-to-USB adapters available on the market. 11) The SD card is now ready to inserted into the SD card slot on the S32V234-EVB2 SD card slot. Create the image on SD card from ubuntu This is a better choice for more advanced users who wish to customize the BSP. To prepare an SD card for a Linux boot, it is necessary to connect the SD card to a machine with Linux OS. If a Linux OS machine is not available, then a virtual machine installed to a Windows OS machine may be used. If you have access to a Linux OS machine, skip to step 4. Procedure 1) Download and install a virtual machine VMware Workstation Player Virtual Box 2) Download Ubuntu. This tutorial uses the Ubuntu version 14.04.5.  The image will be ubuntu-14.04.5-desktop-amd64.iso. 3) Launch VMware or Virtual Box and create a new virtual machine Use downloaded Ubuntu image when requested for installer disc image file Hit Next and select Linux as the guest operating system and select Ubuntu for the version. Hit Next and name your virtual machine and specify where you want to store it. Increase the disk size to 40 GB Hit Finish and install VMware Tools for Linux, if asked 4) Within C:\NXP\S32DS_Vision_v2.0\S32DS\s32v234_sdk\os extract 'build_content.tar.gz', then extract 'build_content.tar' and navigate to the 'v234_linux_build' folder 5) Start virtual machine May need to manually connect USB-mounted SD card reader Log in to virtual machine 6) In files, go to 'Home' directory and create a folder "VSDK" 7) Within VSDK folder, copy the files image, u-boot.s32, s32v234-evb.dtb, and rootfs.tar from the 'v234_linux_build' folder.  Note: The file s32v234-evb.dtb and u-boot.s32 will have names with XXXXX-suffix for the schematic number printed on the evaluation board (EVB) you are using. Be sure to use the files which correspond to your EVB. 😎 Load the card into the reader. If you are using a virtual machine, it is recommended to use a USB adapter instead of a built-in reader in the PC. 9) Within the virtual machine, launch the terminal program 10) Within the terminal program, enter command 'cat /proc/partitions' to view the names of the partitions and identify the names of the partitions on your SD card. Perhaps it is named 'sdb'. 11) Delete all existing partitions.    a) Enter command 'sudo fdisk /dev/sdb'.    b) Enter command 'd' and then the number of the partition to delete. Repeat as necessary until all partitions have been deleted 12) Create new partitions    a) Enter command 'n' for new    b) Enter 'p' (or just hit <enter>, as this is the default) for primary    c) Enter '1' (or just hit <enter>, as this is the default) for partition number 1.    d) Press <enter> to select the default value for the First sector    e) Enter '+255M' to set the size    f) Enter command 'n' again, for partition number 2, however, press <enter> to select the default value for the 'Last sector' 13) Set the partition type    a) Enter command 't' for type    b) Enter '1' for partition number 1    c) Enter 'c' for partition type FAT32    d) Enter command 't' again, for partition number 2, however, enter '83' for partition type LINUX If you get error 16: Device or resource busy, as shown above, use commands 'umount /dev/sdb1' and 'umount /dev/sdb2' to free the pre-existing partitions. Then try again and should be ok now 14) Write the new configuration, enter 'w' 15) Try to setup the filesystems. Enter 'sudo mkfs.vfat -n boot /dev/sdb1'. If you get the error '/dev/sdb1 contains a mounted filesystem', you will need to unmount the partition first. To save time, unmount both /dev/sdb1 and /dev/sdb2. Enter 'umount /dev/sdb1' and then 'umount /dev/sdb2' Now try 'sudo mkfs.vfat -n boot /dev/sdb1' again 16) It worked, so now enter 'sudo mkfs.ext3 -L rootfs /dev/sdb2'. It will take a minute or two for this to complete. Wait until you get the command prompt again. 17) Now it's time to load the BSP content from the VSDK. But first, change the directory to the one we created earlier for the BSP files. Enter 'cd /home/user/VSDK' or 'cd VSDK'. Enter the following commands: sudo dd if=u-boot.s32 of=/dev/sdb bs=512 seek=8 conv=fsync sudo cp Image /media/user/boot sudo cp s32v234-evb.dtb /media/user/boot 18) Now we need to extract the root filesystem, change the directory to its location 19) Enter command 'sudo tar -xvf /home/user/VSDK/rootfs.tar' 20) Once the files are extracted, enter command 'sync'   Now the SD card is ready to be used in the S32V234-EVB.
View full article
Before you can start debugging an S32DS project for S32V234 Cortex-A53 APEX2/ISP Linux target on the S32V234-EVB2, we must first setup the hardware connections and start the Linux BSP OS. 1) Connect (1) S32V234 USB Micro B port to (2) USB A port on your PC. This allow you to connect to the Linux BSP OS via a terminal program to issue commands and to obtain the IP address. 2) Insert microSDHC card (with U-boot, Linux kernel, devicetree, and root file system loaded*) into (3) the S32V234 EVB2 microSD card slot   3) Connect (1) Ethernet port on S32V234 daughter card to (2) LAN**. This will allow S32DS to communicate with the Linux BSP OS for flashing and GDB debugging.   4) Connect the power supply to (3) S234V234 EVB 5) Turn on the (4) power switch, this will start the Linux BSP OS *Instructions for preparing the SD card are provided in the VisionSDK document: ..\S32DS.x.x\S32DS\software\VSDK_S32V2_RTM_x_x_x\s32v234_sdk\docs\vsdk\S32V234-EVB_SetupGuide.pdf or refer to HOWTO: Prepare A SD Card For Linux Boot Of S32V234-EVB2 Using BSP For VisionSDK  **Ensure PC is connected to LAN as well (either hardwired or wireless)
View full article
So you've just installed the S32DS and are using it for the first time and would like to see how it works. Here is a quick and simple project to get you started. Prerequisite Before following the steps in this HOWTO, ensure you have the S32V2xx development package installed to S32DS. 1. Launch S32DS for Vision 2. Select 'S32DS Application Project' 3. Enter a name for the project 4. Select the 'A53 Linux' processor option 5. Click Next 6. Click the '...' next to the SDKs field 7. Check the box next to 'VSDK_MODULE_WIN' for Windows OS or 'VSDK_MODULE_LINUX' for Linux OS and click OK. 8. Click Finish 9. Build the project for Debug 10. Project is now built, ELF file is ready to be loaded to EVB for execution. However, if we have not prepared the EVB, we must first complete HOWTO: Setup S32V234 EVB2 for debugging with S32DS and Linux BSP. 11. Once the EVB is properly prepared, we must complete HOWTO: Setup A Remote Linux Connection in S32DS (S32V234)  12. With the project debug configuration and remote linux connection selected, select the debug dropdown menu and click Debug Configurations 13. Make sure the Debug_Remote_Linux debug configuration is selected and the connection setup in step 10 is selected (points to the IP address of your EVB). Click Debug 14. The first time you connect to a new IP address (i.e. the first time you debug after booting the board), you will receive a warning message, Click Yes and proceed. 15. The executable file is copied to Linux file system and gdbserver starts. 16. The Debug perspective is opened. You can now step through the code*     *Only debugging of the A53 code is supported by Linux GDB. For multicore debugging, including ISP and APEX2, additional debugger and probe(S32 Debugger with S32 Debug Probe, Lauterbach, etc) will be required.
View full article
S32DS for Vision contains many example projects from which you can learn how S32DS, with the Vision Extension Package for V2xx, can be used with the help of the Vision SDK to develop vision applications. The example projects contain generated and hand-written code, which utilize the Vision SDK to demonstrate a workflow using S32DS. In this document, the procedure for creating a project from one of the provided APEX2 examples through to execution on the EVB is detailed. Prerequisite Before following the steps in this HOWTO, ensure you have the Vision Extension Package for V2xx (as well as the S32V2xx development package) installed to S32DS. 1) Launch S32DS 2) Select 'New S32DS Project from example' 3) Select apex2_fast9 project 4) Click Finish 5) Select apex2_fast9: A53 in the Project Explorer panel. Build the project using build config 'TEST_A53'. 6) Start a debug session using method as described in HOWTO: Create A53 Linux Project in S32DS for Vision, beginning at step 9. 7) Click Resume  Should see something similar to what is pictured below There are green diamonds at the corners in the image as identified by the fast9 corner detection algorithm
View full article