This document shows the step-by-step process to create a simple 'Blinking_LED' application using the S32K1xx RTD and the S32 Configuration Tools. This example is for the S32K144EVB-Q100 EVB, connected to a PC through USB (OpenSDA) connection.
Preparation
Setup the software tools
Install S32 Design Studio for S32 Platform
Install the S32K1xx development package and the S32K1 RTD AUTOSAR 4.4. Both of these are required for the S32 Configuration Tools. image.png
Launch S32 Design Studio for S32 Platform
Procedure
New S32DS Project image.png OR image.png
Provide a name for the project, for example 'Blinking_LED_RTD_AUTOSAR'. The name must be entered with no space characters.
Expand Family S32K1xx, Select S32K144
Under Toolchain, select NXP GCC 9.2
Click Next image.png
Click '…' button next to SDKs image.png
Check box next to PlatformSDK_S32K1_2022_02_S32K144_M4F. Click OK image.png
Click Finish. Wait for project generation wizard to complete, then expand the project within the Project Explorer view to show the contents. image.png
To control the LED on the board, some configuration needs to be performed within the Pins Tool. There are several ways to do this. One simple way by double-click on the MEX file. mikedoidge_0-1654712888960.png
By default, the Pins tool is then presented. Since the AUTOSAR drivers will be used, click the switch to disable this tool from the Overview tab. image.png
Once the Pins tool is disabled, the Config Tools Overview menu appears. Select the Peripherals tool. image.png
After the Peripherals tool opens, look to the Components tab. By default, new projects are created with the osif and Port_Ip drivers. Leave the osif driver, but remove the Port_Ip driver. This will be replaced by AUTOSAR version. Right-click on the Port_Ip box and select Remove. image.png
Add the AUTOSAR version of the Port driver. Click on the ‘+’ next to the MCAL box. This will bring up a list of AUTOSAR components. image.png
Locate then select ‘Port’ and click OK. Do not worry about the warning message. It is only indicating that the driver is not already part of the current project. The associated driver package will be added automatically. image.png
There are a couple of other drivers needed. Click the ‘+’ next to MCAL again and this time select ‘Dio’. Once more, click the ‘+’ and select ‘Mcu’.
Select the ‘Dio’ component. Now select the DioConfig tab. Under DioPort_0, change the Dio Port Id to 3. Click ‘+’ next to DioChannel to add a channel. image.png
Select the ‘Port’ component. Now select the PortConfigSet tabl.
Under PortPin, change the setting for PortPin_0, PortPin Pcr from 0 to 96.
Then change the setting PortPin Direction from PORT_PIN_IN to PORT_PIN_OUT.
Change the setting PortPin Level Value from PORT_PIN_LEVEL_HIGH to PORT_PIN_LEVEL_LOW.
Under UnTouchedPortPin, click ‘+’ and add the following 5 PortPin Pcr numbers: 4, 5, 10, 68, 69 image.png
Now select the PortGeneral tab, uncheck ‘Port Ci Port Ip Development Error Detect’. image.png
Now the device configurations are complete and the RTD configuration code can be generated. Click ‘Update Code’ from the menu bar. image.png
To control the output pin which was just configured, some application code will need to be written. Return to the ‘C/C++’ perspective. image.png
If not already open, in the project window click the ‘>’ next to the ‘src’ folder to show the contents, then double click ‘main.c’ file to open it. This is where the application code will be added. image.png
Before anything else is done, initialize the mcu driver, the clock tree, and apply PLL as system clock. Insert the following line into main, after the comment 'Write your code here': Mcu_Init(&Mcu_Config_BOARD_InitPeripherals); Mcu_InitClock(McuClockSettingConfig_0); while ( MCU_PLL_LOCKED != Mcu_GetPllStatus() ) { /* Busy wait until the System PLL is locked */ } Mcu_DistributePllClock(); Mcu_SetMode(McuModeSettingConf_0); image.png
Before the pin can be controlled, it needs to be initialized using the configuration information that was generated from the S32 Configuration tools. Initialize all pins using the Port driver by adding the following line: Port_Init(NULL_PTR); image.png
Turn the pin on and off with some delays in-between to cause the LED to blink. Make the delays long enough to be perceptible. Within the provided for loop, add the following lines: Dio_WriteChannel(DioConf_DioChannel_DioChannel_0, STD_HIGH); TestDelay(2000000); Dio_WriteChannel(DioConf_DioChannel_DioChannel_0, STD_LOW); TestDelay(2000000); image.png
Before the 'main' function, add a delay function as follows: voidTestDelay(uint32 delay); voidTestDelay(uint32 delay) { staticvolatile uint32 DelayTimer = 0; while(DelayTimer<delay) { DelayTimer++; } DelayTimer=0; } image.png
Update the includes lines at the top of the main.c file to include the headers for the drivers used in the application: Remove #include "Mcal.h" Add #include "Mcu.h" #include "Port.h" #include "Dio.h" image.png
Build 'Blinking_LED_RTD_AUTOSAR'. Select the project name in 'C/C++ Projects' view and then press 'Build'. image.png
After the build completes, check that there are no errors. image.png
Open Debug Configurations and select 'Blinking_LED_RTD_AUTOSAR_Debug_FLASH'. Make sure to select the configuration which matches the build type performed, otherwise it may report an error if the build output doesn’t exist. image.png image.png
Confirm the EVB is connected to the PC via USB cable, then check the Debugger tab settings and ensure that 'OpenSDA Embedded Debug - USB Port' is selected for interface. image.png
Click Debug
To see the LED blink, click ‘Resume' image.png
查看全文