Installation & Activation
HOWTO: Install Wind River compiler Eclipse plug-in into S32 Design Studio
HOWTO: Install Lauterbach TRACE32 debugger plug-in into S32 Design Studio
HOWTO: Install PLS UDE debugger plug-in into S32 Design Studio
HOWTO: Activate S32 Design Studio
Getting Started
HOWTO: Create a Blinking LED Project (MPC5748G)
HOWTO: Build a Project and Setup a Debug Configuration for debugging in S32 Design Studio
Build tools & standard libraries
HOWTO: Run a routine from RAM in S32 Design Studio
HOWTO: Use printf() function and EWL library
HOWTO: Migrate project created in S32DS Power v1.x into v1.2+
HOWTO: Add a static library file into S32DS GCC project
HOWTO: Link a binary file(s) into the application project using GNU build tools
HOWTO: Execute a library function from RAM memory using GNU build tools NEW!
Debug & Flash Programming
HOWTO: download separate elf/srec/hex file to microcontroller using S32 Design Studio
HOWTO: Program data flash (DFLASH) in S32 Design Studio for Power
HOWTO: Program DCF record into UTEST flash in S32 Design Studio for Power
HOWTO: debug multi-core project in S32 Design studio
HOWTO: Update OpenSDA Firmware on EVB
HOWTO: MPC5777C - Low/Mid Flash block erase via PE Micro
HOWTO: Use RappID BL tool with MPC5744p EVB
HOWTO: Debug multiple elf files in S32 Design Studio
HOWTO: Reset MCU in S32 Design Studio debugger (Pemicro/OpenSDA interface)
HOWTO: Program multiple memory types in single debug session NEW!
SDKs
HOWTO: Working with AMMCLib SDKs
HOWTO: Working with FreeMASTER SDKs
HOWTO: Add custom SDK into existing project
HOWTO: Use SDK based example code as standalone (usable for GIT, SVN...) NEW!
General Usage
HOWTO: S32 Design Studio Command Line Interface
HOWTO: Add user example into S32DS
HOWTO: Generate S-Record/Intel HEX/Binary file
HOWTO: Update S32 Design Studio
How to export Generated Code to S32 Design Studio IDE (applicable for MBDT for MPC5744P v2.0)
HOWTO: Install update from 3rd party vendor
S32 Design Studio for Power Architecture v2.1 Migration Guide
https://community.nxp.com/docs/DOC-342290
Troubleshooting
Troubleshooting: Issue opening documents from Getting Started page
Troubleshooting: PEmicro Debug Connection: Target Communication Speed
Troubleshooting: Indexer errors on header file
S32 Design Studio Offline activation issue hot fix
Troubleshooting: Installer rolls back immediately following activation code entry
Troubleshooting: Activation fails with error message FNP ERROR 0