S32 デザインスタジオ・ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio Knowledge Base

ディスカッション

ソート順:
Quick Fix is a feature of the Java editor in Eclipse which enables a user to resolve problems found in the Java code of their project. This feature is available to be used within S32 Design Studio for some problems. Such problems will be identified with the 'light bulb' icon in the description field, as shown below: For example, such problems sometimes occur when importing a project created in a previous version of S32 Design Studio, are provided from another user, or some files in a project have become corrupted. To resolve issues identified with the 'light bulb' icon, right-click on the problem and from the pop-up menu, select 'Quick Fix'.  The Quick Fix menu will appear, providing the available solutions for the problem. In most cases, there will be just one solution. Click finish to implement the fix. In some cases, more information will be required from the user to complete the fix. Complete the form to provide the additional information, then click OK. Now the problem should be resolved.
記事全体を表示
Condition:  I am trying FreeRTOS using S32K118 EVB and run in DEBUG mode. When I set the break point in vTaskDelay and press Resume for the first time, there is a smooth stop at the break point. The second time I press Resume, the debugger should enter the same break point again, but there is no response. Then I press Suspend and can't press Resume again, at this point I can only leave. However, I am free to run this project with no problem, what's wrong? Analysis: This is due to an access of DDR memory region which is not initialized by default project settings. Solution: To resolve it, a macro initializing the DDR memory should be selected to run at the beginning of a debug session. A user should go to Advanced Options dialog and check "Enable initialization script". Our DDR init macros can be found at the following location within S32DS3.2 layout: eclipse\plugins\com.pemicro.debug.gdbjtag.pne_4.2.8.201909091700\win32\gdi\P&E\supportFiles_ARM\NXP\S32Vxxx\S32V234M100_DDR3_EVB29288.mac. Please note that the type of the macro might depend on the revision of the board and S32V23x device one is working with. I am also attaching a picture of debug configuration and Advanced Options dialog with all the settings in place.
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture v2.1 Update 2          What is new? Integrated S32 SDK RTM-SR 3.0.1 (see the S32 SDK release notes) This is a cumulative update - it includes all the content of previous updates (Update 1 ) Installation instructions The update is available for online installation (via S32DS Extensions and Updates) or offline installation (direct download link)  installation:  go to menu "Help" -> "S32DS Extensions and Updates" dialog  select from available items and click "Install/Update" button offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use direct link to download the update archive zip file  Start S32 Design Studio and go to "Help" -> "S32DS Extensions and Updates", then click 'Go to Preferences' link And add a new site "Add..." repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select the 'RSDK 1.3.0 for S32R274 and S32R372' package and click "Install/Update" button.   This will start the update installation process.
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture v2.1 Update 1          What is new? Integrated Radar SDK RTM 1.3.0 (see the Radar SDK release notes) Installation instructions The update is available for online installation (via S32DS Extensions and Updates) or offline installation (direct download link)  installation:  go to menu "Help" -> "S32DS Extensions and Updates" dialog  select from available items and click "Install/Update" button offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use direct link to download the update archive zip file  Start S32 Design Studio and go to "Help" -> "S32DS Extensions and Updates", then click 'Go to Preferences' link And add a new site "Add..." repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select the 'RSDK 1.3.0 for S32R274 and S32R372' package and click "Install/Update" button.   This will start the update installation process.
記事全体を表示
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture v2.1         The Automotive Microcontrollers and Processors’ Embedded Tools Team at NXP Semiconductors, is pleased to announce the release of the S32 Design Studio for Power Architecture version v2.1. It is the successor of S32 Design Studio for Power 2017.R1. - the versioning scheme has changed. Release content (What is new?) Eclipse Neon 4.6 Framework GNU Build Tools for e200 processors bld=1607 rev=gceb1328 (support VLE and BookE ISA, based on gcc 4.9.4 [1.February 2019], binutils 2.28 and gdb 7.8.2) - see the complete GCC release notes Libraries included: newlib, newlib-nano and Freescale EWL2 P&E Multilink/Cyclone/OpenSDA (with P&E GDB Server) - updated (v1.7.2.201709281658) New Project wizards to create application and library projects and projects from project examples for supported devices Peripherals Register and Special Purpose Registers View Fully integrated S32 SDK RTM v.3.0.0 (Windows only). For the details on the feature set of SDK please refer to SDK Release notes attached and Reference Manuals (Please note that SDK has Early Access Release status, which means that there could be some limitations and/or issues. Also note, the SDK is available for Windows host only). SDK management included: o FreeMASTER Serial Communication driver (v2.0 August 31th 2016) o Automotive Math and Motor Control Libraries(v1.1.15) o Support for importing MCAL configuration to a custom SDK o An SDK can be attached to a library project using the project wizard Windriver Diab, and GreenHills compiler support by new project wizard (The Green Hills Software (GHS) compiler support depends on the availability of the Eclipse plug-in integrating GHS compiler compatible with the Eclipse Neon. Full support for the Green Hills Software compiler Eclipse Neon-compatible plug-in within S32DS for PA 2.1 was not validated in time for this release.) Lauterbach, iSystem, and PLS debuggers support by new project wizard (The plugins to support Diab, iSystem, Lauterbach, and GreenHills are not included and have to be installed from the corresponding update site or installation.) Kernel Aware debugging for FreeRTOS, eCOS, OSEK Devices supported: S32R274 S32R372 MPC5775B, MPC5775E MPC5775K, MPC5774K MPC5746R, MPC5745R, MPC5743R MPC5777M MPC5777C MPC5748G, MPC5747G, MPC5746G MPC5744B, MPC5745B, MPC5746B, MPC5744C, MPC5745C, MPC5746C MPC5744P, MPC5743P, MPC5742P, MPC5741P MPC5601P, MPC5602P, MPC5603P, MPC5604P MPC5644B, MPC5644C, MPC5645B, MPC5645C, MPC5646B, MPC5646C MPC5601D, MPC5602B, MPC5602C, MPC5602D, MPC5603B, MPC5603C, MPC5604B, MPC5604C, MPC5605B, MPC5606B, MPC5607B MPC5606S MPC5604E MPC5644A, MPC5642A MPC5643L MPC5676R MPC5632M, MPC5633M, MPC5634M MPC5674F MPC5673K, MPC5674K, MPC5675K Collateral Getting Started page The S32DS Extensions and Updates tool Migration guide to help migrate projects from an earlier version to S32 Design Studio for Power Architecture 2. Bug Fixes For detailed list of the GNU Tools bug fixes, refer to the release notes located in S32DS/ build_tools/powerpc-eabivle-4_9/ Fixed the semihosting issues with the EWL and NewLib libraries Fixed the FLASH programming algorithm for MPC5744P Added missing linker script sections for MPC5748G Fixed reading values from the peripheral bridge A registers for MPC5634M Fixed access to the RAM memory for MPC5634M Removed unavailable addresses from the MPC574xB linker files Added the -fstrict-volatile-bitfield compiler option to the project settings Fixed secure connection to MPC5744P Disabled RTTI for EWL library due to incompatibility with the GNU tools Fixed importing/exporting projectinfo.xml with library settings Complete S32 Design Studio for Power Architecture v2.1 release notes are available here Installation Notes To download the installer please visit the S32DS for Power Architecture product page: downloads section. The installer requires the the NEW Activation ID to be entered during the installation. You should receive an email that includes your Activation ID after starting the installer downloading process: Technical Support S32 Design Studio issues are tracked through the S32DS Public NXP Community space: https://community.nxp.com/community/s32/s32ds    
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1 Update 11          What is new? S32 SDK for Power Architecture RTM 3.0.0 supporting  S32R274, S32R372, MPC574x-B-C-G, MPC574x-P, MPC574x-R and MPC577x-B-E-C (see the S32 SDK release notes) Integrated Radar SDK RTM 1.2.1 (see the Radar SDK release notes) This is a cumulative update - it includes all of the content of previous updates (Update 1, Update 2, Update 3, Update 4, Updates 5 and 6, Update 7, Update 8, Update 9, Update 10  ). Installation instructions The update is available for online installation (via S32DS Eclipse Updater) or offline installation (direct download link)  installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_2017.R1/updatesite" select all available items and click "Next" button offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use direct link to download the update archive zip file  Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button.   This will start the update installation process.
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1 Update 10          What is new? S32 SDK for Power Architecture 2.9.0 BETA supporting  S32R274, S32R372, MPC574x-B-C-G, MPC574x-P, MPC574x-R and MPC577x-B-E-C (see the S32 SDK release notes) Updated version of GCC 4.9.4 tools AMMCLIB version 1.1.15 (see the AMMCLIB MPC574xP example release notes) Updated version of SPT tools for SPT 2.5 Updated version of P&E This is a cumulative update - it includes all of the content of previous updates (Update 1, Update 2, Update 3, Update 4, Updates 5 and 6, Update 7, Update 8, Update 9 ). Installation instructions The update is available for online installation (via S32DS Eclipse Updater) or offline installation (direct download link)  installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_2017.R1/updatesite" select all available items and click "Next" button offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use direct link to download the update archive zip file  Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button.   This will start the update installation process.
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1 Update 9          What is new? S32 SDK for Power Architecture 2.0.0 RTM supporting  MPC5741P, MPC5742P, MPC5743P, MPC5744P, MPC5744B, MPC5745B,  MPC5746B, MPC5744C, MPC5745C, MPC5746C, MPC5747C, MPC5748C, MPC5746G, MPC5747G, MPC5748G, S32R274, S32R372 (see the S32 SDK release notes) AMMCLIB version 1.1.14 (see the AMMCLIB MPC574xP example release notes) Radar SDK RTM, version 1.2.0 (see the RSDK release notes) This is a cumulative update - it includes all of the content of previous updates (Update 1, Update 2, Update 3, Update 4, Updates 5 and 6, Update 7, Update 8 ). Installation instructions The update is available for online installation (via S32DS Eclipse Updater) or offline installation (direct download link)  installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_2017.R1/updatesite" select all available items and click "Next" button offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use direct link to download the update archive zip file Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button.   This will start the update installation process.
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for ARM® 2018.R1  Update 8          What is new? S32K1xx SDK BETA 2.9.2 supporting S32K116, S32K118, S32K142, S32K144, S32K146, and S32K148. This is a cumulative update - it includes all the content of previous updates (Update 1, Update 2, Update 3, Update 4, Update 5, Update 6, Update 7 ) Installation instructions The update is available for  (via Eclipse Updater) or offline installation (direct download link)  installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_ARM_2018.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use direct link to download the update archive zip file Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive .zip file you downloaded in the previous step Select all available items and click "Next" button.   This will starts the update installation process.
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1 Update 8          What is new? S32 SDK for Power Architecture 1.8.0 EAR supporting MPC5777C, MPC5775B, MPC5775E, MPC5746R, MPC5745R, MPC5743R This is a cumulative update - it includes all of the content of previous updates (Update 1, Update 2, Update 3, Update 4, Updates 5 and 6, Update 7 ). Installation instructions The update is available for  (via S32DS Eclipse Updater) or offline installation (direct download link)  installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_2017.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use direct link to download the update archive zip file  Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button.   This will start the update installation process.
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1 Update 7          What is new? MPC574xx SDK BETA 1.9.0 S32R SDK BETA 1.9.0  Radar SDK for S32R274 & S32R372 RTM 1.1.1 AMMCLib 1.1.13 for MPC560xB, MPC560xP, MPC564xL, MPC567xF, MPC567xK, MPC574xC, MPC574xG, MPC574xP, MPC574xR, MPC577xC, MPC577xK,  MPC577xM This is a cumulative update - it includes all of the content of previous updates (Update 1, Update 2, Update 3, Update 4, Updates 5 and 6). Installation instructions The update is available for  (via S32DS Eclipse Updater) or offline installation (direct download link)  installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_2017.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use direct link to download the update archive zip file  Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button.   This will start the update installation process.
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for ARM® 2018.R1  Update 7          What is new? S32K1xx SDK BETA 2.9.0 supporting S32K116, S32K118, S32K142, S32K144, S32K146, and S32K148.  Also included is AMMCLIB 1.1.13 for S32K11x and S32K14x. This is a cumulative update - it includes all the content of previous updates (Update 1, Update 2, Update 3, Update 4, Update 5, Update 6) Installation instructions The update is available for  (via Eclipse Updater) or offline installation (direct download link)  installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_ARM_2018.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use direct link to download the update archive zip file Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive .zip file you downloaded in the previous step Select all available items and click "Next" button.   This will starts the update installation process.
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1 Updates 5 and 6          What is new? S32 SDK for Power Architecture 1.0.0 RTM supporting MPC574xx.  Service Pack supporting MPC5775 B/E This is a cumulative update - it includes all of the content of previous updates (Update 1, Update 2, Update 3, Update 4 ). Installation instructions The update is available for online (via S32DS Eclipse Updater) or offline installation (direct download link) online installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_2017.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use  direct link to download the update archive zip file  Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button.   This will start the update installation process.
記事全体を表示
The FreeMASTER serial communication driver is a piece of code that enables an embedded application to communicate with the FreeMASTER PC application. Please note: The FreeMASTER_S32xx does not support all Toolchains and not all versions of supported Toolchains. The available SDKs will vary depending upon the toolchain which is selected. It is independent of the S32/MPC SDKs. In most cases, it is not integrated with the S32/MPC SDKs, although this could change in the future. When creating a new S32DS Application Project, you may have noticed the FreeMASTER_S32xx SDK option in the Select SDK menu. To add the FreeMASTER SDK to your project, simply add it in the New Project Wizard (as pictured above) or add it later through the project properties menu, SDKs: Select the desired SDK from the list, then click 'Attach/Detach...' Click in the column for each build configuration for which you wish to have the SDK attached. You can remove SDKs by clicking the '+', making it disappear. It should also be noted that there exists example projects which demonstrate usage of the FreeMASTER serial communication driver, though these do not use the FreeMASTER SDK, the driver was added manually. When working in your project, you can use the SDK Explorer to drag and drop macros and function calls into your code. To add the SDK Explorer to your perspective, there are at least 2 methods: 1) Menu method a) Window -> Show View -> Other... OR Alt + Shift + Q, Q b) Filter on 'SDK' c) Select 'SDK Explorer' d) Click OK 2) Quick Access method a) Type 'SDK' b) Select 'SDK Explorer' To access the macros and function calls from the SDK Explorer: 1) Go to the Project Explorer and select your project to make it active. 2) Go to SDK Explorer and all of the SDKs you included in the project will be listed. 3) For the SDK you wish to access, expand the folders and files until you can see the function you wish to add. You can set some filters to hide unwanted content. 4) Simply drag and drop the macro/function call into your source file. The #include statement for the associated header file will be automatically added near the top of your source file. Happy FreeMASTER serial communicating!
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1 Update 4          What is new? Radar SDK RTM 1.0.0. This is a cumulative update - it includes all of the content of previous updates (Update 1, Update 2, Update 3). Installation instructions The update is available for online (via S32DS Eclipse Updater) or offline installation (direct download link) online installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_2017.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use  direct link to download the update archive zip file  Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button.   This will start the update installation process.
記事全体を表示
Please note: AMMCLib SDK is standalone from S32/MPC SDK, it is intended for users who will not use the S32/MPC SDK. The AMMCLib SDK does not support all toolchains listed in S32DS new project wizard. For the toolchains it does support, It does not support all versions. The available SDKs will vary depending upon the toolchain which is selected. When creating a new S32DS Application Project, you may have noticed the S32K14x_AMMCLib_xxx SDK option in the Select SDK menu. This is the standalone version of the AMMCLib. If you plan to use one of the S32/MPC SDKs, then it most likely contains an integrated version of the AMMCLib. For this integrated case, the AMMCLib is accessed like any other S32/MPC SDK component and you would not need to add the standalone version. To add the AMMCLib SDK to your project, simply add it in the New Project Wizard (as pictured above) or add it later through the project properties menu, SDKs: Select the SDK from the list and then click 'Attach/Detach...' Click in the column for each build configuration for which you wish to have the SDK attached. You can remove SDKs by clicking the '+', causing it to disappear. It should also be noted that there exist example projects which demonstrate usage of the AMMCLib, though these show usage of the S32/MPC SDK integrated version. When working in your project, you can use the SDK Explorer to drag and drop macros and function calls into your code. To add the SDK Explorer view to your perspective, there are at least 2 methods: 1) Menu method a) Window -> Show View -> Other... OR Alt + Shift + Q, Q b) Filter on 'SDK' c) Select 'SDK Explorer' d) Click OK 2) Quick Access method a) Type 'SDK' b) Select 'SDK Explorer' To access the macros and function calls from the SDK Explorer: 1) Go to the Project Explorer and select your project to make it active. 2) Go to SDK Explorer and all of the SDKs you included in the project will be listed. 3) For the SDK you wish to access, expand the folders and files until you can see the function you wish to add. You can set some filters to hide unwanted content. 4) Simply drag and drop the macro/function call into your source file. The #include statement for the associated header file will be automatically added near the top of your source file. Happy math coding with AMMCLib!
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for ARM® 2018.R1  Update 6          What is new? S3214x SDK RTM 2.0.0. This is a cumulative update - it includes all the content of previous updates (Update 1, Update 2, Update 3, Update 4, Update 5) To select the new SDK in the New Project Wizard, the Toolchain must be changed to 'ARM Bare-Metal 32-bit Target Binary Toolchain' Installation instructions The update is available for online (via Eclipse Updater) or offline installation (direct download link) online installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_ARM_2018.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use direct link to download the update archive zip file Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive .zip file you downloaded in the previous step Select all available items and click "Next" button.   This will starts the update installation process.
記事全体を表示
The following article describes how to add FreeRTOS thread aware debugging to the Eclipse Debug view using SEGGER J-Link: Show FreeRTOS Threads in Eclipse Debug View with SEGGER J-Link and NXP S32 Design Studio | MCU on Eclipse  I hope this is useful, Erich
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1 Update 3          What is new? S32 SDK for Power Architecture 0.8.3 EAR for S32Rx7x. This is a cumulative update - it includes all of the content of previous updates (Update 1, Update 2 ). Installation instructions The update is available for online (via S32DS Eclipse Updater) or offline installation (direct download link) online installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_2017.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use  direct link to download the update archive zip file  Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button.   This will start the update installation process.
記事全体を表示
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for ARM® 2018.R1  Update 5          What is new? Service Pack WCT101xS. This is a cumulative update - it includes all the content of previous updates (Update 1, Update 2, Update 3, Update 4) Installation instructions The update is available for online (via Eclipse Updater) or offline installation (direct download link) online installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_ARM_2018.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use direct link to download the update archive zip file Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive .zip file you downloaded in the previous step Select all available items and click "Next" button.   This will starts the update installation process.
記事全体を表示