S32 Design Studio Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio Knowledge Base

Discussions

Sort by:
This document describes two ways how to add a static library file (*.a) into your S32 Design Studio GCC project. These methods differs from each other in sense how a library update is reflected into project build process. Adding a static library WITHOUT dependency to executable (elf) file This approach assumes a library does not change. An update of the library does not trigger project rebuild process. If the library changes the project needs to be manually cleaned (assuming no other source file has changed) and next build links the updated library. The path to the library and the library name shall be entered into Project Properties -> C/C++ Build -> Settings -> Standard S32DS C Linker -> Libraries Please note that GCC adds prefix "lib" and the extension ".a"  to the library name entered into the above dialog by default. GCC linker will search for the library file named: "libtestlib.a" in the folder "c:\my_libs" In the example above. In case a library cannot be found the linker error occurs e.g. one depicted below. The linker library file name option "-ltestlib.a" is expanded into file name "libtestlib.a.a" which does not exist. 10:28:53 **** Incremental Build of configuration Debug for project S32K144_Project_with_library **** make -j8 all Building target: S32K144_Project_with_library.elf Executing target #5 S32K144_Project_with_library.elf Invoking: Standard S32DS C Linker arm-none-eabi-gcc -o "S32K144_Project_with_library.elf" "@S32K144_Project_with_library.args" c:/nxp/s32ds_arm_v2.0/cross_tools/gcc-arm-none-eabi-4_9/bin/../lib/gcc/arm-none-eabi/4.9.3/../../../../arm-none-eabi/bin/ld.exe: cannot find -ltestlib.a collect2.exe: error: ld returned 1 exit status make: *** [makefile:49: S32K144_Project_with_library.elf] Error 1 10:28:54 Build Finished (took 1s.332ms)‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ For a custom library name add colon character ":" at the beginning of the library name to disable the default prefix/extension expansion. GCC linker now searches for file name "testlib.lib" in the example below:   Adding a static library WITH dependency to executable (elf) file If a static library has changed - "touched"  it is sometimes desired to trigger project rebuild. In this scenario the library shall be added into a different project dialog: Project Properties -> C/C++ Build -> Settings -> Standard S32DS C Linker -> Miscellaneous -> Other objects The items from "Other objects" list is propagated into USER_OBJS makefile variable which is prerequisite for auto-generated makefile rule that build the target (elf): Enjoy linking static libraries in S32DS!
View full article
Suppose you created an application project for one MCU (S32K144, for example), but your requirements changed, or perhaps you are reusing a previous project to start a new project on a different MCU (derivative from same family). If you are working with the S32 SDK, there is a way to do it. We have detailed the steps in this document. 1) Open the project to be modified and select the C/C++ perspective, ensure that the Processor Expert views are shown 2) From the Components Library, Processors tab, select the new MCU derivative 3) Either double-click OR right-click and select 'Add to project', to add the new processor to your components list for your project. Be sure to select just one of the pin packages, whichever is appropriate for you application. 4) From the Component Inspector*, you will see a message in red text asking if you would like to switch into the configuration for the new processor. Click on the button 'Switch Configuration'. *may have to select pin_mux:PinSettings in the Components view for the project to see the message 5) Open the Project Properties, either select from File menu or right-click on project name and select from the menu. Then go to C/C++ Build -> Settings -> Standard S32DS C Compiler -> Includes and delete all include paths starting with $(S32K1**_SDK_VER_PATH). Repeat this step for the Standard S32DS Assembler -> General include paths. Note: For all changes in C/C++ Build -> Settings, make sure to repeat for all build configurations (RAM, FLASH, Debug, Release, etc.). 6) The paths to the SDK should now be gone. The result should look similar to this: 7) In Standard S32DS C Compiler -> Preprocessor settings, change the defined symbol to the one which is appropriate for the new MCU and click OK. (e.g. CPU_S32K142 for S32K142, CPU_S32K148 for S32K148, etc.) If you are not sure what should be here, then create a new empty project for the new MCU and refer to the settings there. 😎 The Preprocessor setting after the change 9) Click on the 'Generate Processor Expert Code' button in the Components view for your project 10) From Project Explorer, remove the startup and linker files from Project Settings folder 11) Copy startup and linker files for the new MCU from <SDK_PATH>/platform/devices/<CPU>/startup/<Compiler> and <SDK_PATH>/platform/devices/<CPU>/linker/<Compiler> 12) Open the Project Properties, then C/C++ Build -> Settings -> Standard S32DS C Linker -> General and update the linker file path to reflect the new filename and click OK. (in this case: S32K144_64_flash.id to S32K142_32_flash.id) 13) After the change 14) Perform a Clean and a Build operations of the project. 15) Update the device in the debug configurations Now you can change your MCU derivatives!
View full article
******************************************************************************** * Detailed Description: * This example shows, how to use printf function in project. * Files uart_console_io.c, uart.c and uart.h was added. These files contain * necessary functions for correct printf() functionality * * * Test HW:         FRDMPK144-Q100 * MCU:             PS32K144HFVLL 0N77P * Terminal:        9600-8-no parity-1 stop bit-no flow control on LPUART1 * Fsys:            160 MHz * Debugger:        Lauterbach Trace32 *                  PeMicro USB-ML-PPCNEXUS *                  OpenSDA embedded debug * Target:          internal_FLASH, internal RAM * EVB connection:  default
View full article
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for ARM v2.0             Austin, Texas, USA August 16, 2017 The Automotive Microcontrollers and Processors’ Embedded Tools Team at NXP Semiconductors, is pleased to announce the first release of the S32 Design Studio for ARM  v2.0  Release content (What is new?) • Eclipse Neon 4.6 Framework • GNU Tools for ARM® Embedded Processors (Launchpad) build (4.9.3 20150529) • ARM64: Linaro GCC 4.9-2015.05 • Libraries included: newlib, newlib-nano and ewl2 (ewl and ewlnano) • P&E Multilink/Cyclone/OpenSDA (with P&E GDB Server) - updated (v3.1.1.20180808) • SEGGER J-Link (with SEGGER GDB Server) -  (V616f_b170707) • New Project wizard to create application and library projects for supported devices • Fully integrated S32 SDK for S32K14x EAR release v.0.8.4. For the details on the feature set  of SDK please refer to SDK Release notes and Reference Manuals attached below. • SDK management included: o Sample Drivers for KEA family (Evaluation grade) o FreeMASTER Serial Communication driver for KEA and S32K families o Automotive Math and Motor Control Libraries for KEA and S32K devices v1.1.8  • Import projects from CodeWarrior for MCU v.10.6 and Kinetis Design Studio for respective supported processors • IAR v7.x compiler support by new project wizard • iSystem, Lauterbach and IAR debuggers support by new project wizard • Kernel Aware debugging for FreeRTOS, OSEK. • Devices supported: o SKEAZN8, SKEAZN16, SKEAZN32, SKEAZN64, SKEAZ128, SKEAZ64 o S32K144 v2.0, S32K148, S32K142 o S32V234 o MAC57D54H Complete S32 Design Studio for ARM v2.0 release notes are available here Installation Notes To download the installer please visit the S32DS product page downloads section. The installer requires the the NEW Activation ID to be entered during the installation. You should receive an email including the Activation ID after starting the download process:   Technical Support S32 Design Studio issues are tracked through the S32DS Public NXP Community space. https://community.nxp.com/community/s32/s32ds
View full article
On reset, all module registers have default values. These settings are typically not ideal for achieving optimal system performance. Also, some peripherals must be configured before they can be used. DCD is the configuration information contained in the DCD image that BootROM uses to configure peripherals on the device. BootROM determines the location of the DCD table from the associated pointer in the IVT.   The main functionality of the DCD Tool is to generate the Device Configuration Data (DCD) image using the format and constraints as specified in the Boot ROM reference manual.   In the steps below, an example process for creating the DCD binary for initializing SRAM is shown. To initialize the SRAM, a logic '1' must be written to the INITREQ bit within the PRAMCR register of the SRAMC and SRAMC_1 peripherals.   Procedure With a project open in project explorer (C/C++ perspective), switch to DCD perspective. Click on the arrow next to the 'Open S32 Configuration' button and select 'Open DCD'. Check that correct project is selected  In DCD Commands panel, select Command Type 'Write', then click 'Set' Click 'Add Register', then set the following settings. Can start typing the names to filter the list for faster setting selection.   For Peripheral setting, select 'SRAMC'. You can search for it by typing the name. Register setting, select 'PRAMCR'. The list is short, so it is not necessary to type the name. In Bitfields, select 'INITREQ' Now click on the highlighted bit to set it. Again using 'New Command' box, repeat settings of steps 3 & 4, however, this time select Peripheral 'SRAMC_1'. If everything was done correctly, in the DCD Binary panel to the right, should appear as shown. If so, click 'Export'. The generated DCD file will be displayed. By default, C format is selected. Select Binary format and click OK. Select a location to save the file (such as the project folder in the workspace directory) and give it a meaningful name. Click Save. You are done! DCD image file is created in binary format and ready to be imported to IVT Tool.  
View full article
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for S32 Platform v3.2         Austin, Texas, USA Sep 30, 2019    The Automotive Microcontrollers and Processors' Embedded Tools Team at NXP Semiconductors is pleased to announce the release of the S32 Design Studio for S32 Platform v3.2.  Here are some of its major new features: Multiple builds of the GNU tools can be installed. The SDK integration is provided with additional software packages. The SDK packages can be installed and updated with the S32DS Extensions and Updates tool. The GHS toolchain support is provided by the project wizard (available for particular devices). The CMSIS-DAP debugging is supported by particular devices. The UART communication speed of S32 Flash Tool is improved. The latest versions of P&E debugger plug-in and drivers are provided. S32 Debugger provides OS Awareness support for FreeRTOS and OSEK. S32 Debugger provides preliminary support for secure debugging with the Password and Challenge/Response authentication methods. New type of Launch Groups is defined for S32 Debugger, which allows you to create S32 Debugger specific configurations and use the new "Wait for stop on breakpoint" post launch action. The SDK migration support is provided to upgrade an SDK version attached to the project. The S32DS Extensions and Updates tool notifies about dependencies and incompatible packages. The progress bar is displayed for the S32 Debugger flash programmer. S32 Design Studio Versions   S32DS IDE for S32 Platform S32DS IDE for Arm® S32DS IDE for Power Architecture® S32DS IDE for Vision Devices Supported S32V23x S32K1xx MPC56xx S32V234 S32S247TV KEA MPC57xx   S32 Platform Devices MAC57D54H S32R2xx/S32R3xx   Integrated NXP Tools S32 Flash Tool FreeMASTER FreeMASTER DDR stress tool DDR stress tool     Integrated Configuration Tools S32 Configuration Tools Processor Expert Configuration Tool Processor Expert Configuration Tool  DDR configuration tool Pins Wizard Pins Wizard Pins Wizard Clocks configuration Peripheral/Drivers configuration   Peripheral/Drivers configuration   Peripheral/Drivers configuration   DCD/IVT configuration       DDR configuration tool       Integrated NXP Software S32 SDK S32K1 SDK S32 SDK Vision SDK FreeRTOS FreeRTOS FreeRTOS Linux BSP AMMCLib for S32V23x AMMCLib for KEA and S32K AMMCLib for MPC56xx and MPC57xx MCUs   Vision SDK KEA SDK Radar SDK Linux BSP MQX OS/MQX Drivers for MAC57D54H     Compilers: NXP GCC 6.3.1* NXP GCC 6.3.1* NXP GCC 4.9* NXP GCC 6.3.1* GreenHills GreenHills GreenHills   IAR IAR Diab     GCC 4.9*     DEBUGGERS Built-in GDB interface: S32 Debugger/S32 Debug Probe P&E Multilink/Cyclone/OpenSDA P&E Multilink/Cyclone/OpenSDA S32 Debugger/S32 Debug Probe P&E Multilink/Cyclone/OpenSDA Segger J-Link   P&E Multilink/Cyclone/OpenSDA DEBUGGERS supported: Lauterbach Lauterbach Lauterbach Lauterbach   iSystem iSystem   IAR PLS   Host Operating Systems: Microsoft Windows® 7/8/10 64-bit OS (with 32-bit binaries)  – Ubuntu 14.04, 16.04 (64 bit) – Debian 8 (64 bit) – CentOS 7 (64 bit) Microsoft Windows® 7/8/10 32/64-bit OS (with 32-bit binaries)  – Ubuntu 14.04, 16.04 (64 bit) – Debian 8 (64 bit) – CentOS 7 (64 bit) Microsoft Windows® 7/8/10 32/64-bit OS (with 32-bit binaries)  – Ubuntu 14.04, 16.04 (64 bit) – Debian 8 (64 bit) – CentOS 7 (64 bit) Microsoft Windows® 7/8/10 32/64-bit OS (with 32-bit binaries)  – Ubuntu 14.04, 16.04 (64 bit) – Debian 8 (64 bit) – CentOS 7 (64 bit) Vision specific tools : NXP APU Compiler     NXP APU Compiler ISP assembler     ISP assembler ISP and APEX graph tools     ISP and APEX graph tools Radar specific tools :     SPT assembler       SPT Explorer/ SPT graph tool   Complete S32 Design Studio for S32 Platform v3.2 release notes are available here.   Installation To download the installer please visit the S32 Design Studio product page download section or click the direct here.     The installer requires the Activation ID to be entered. You should receive a notification email including the Activation ID after the download of the installation package starts. The installer installs just the base tools/package. In order to start development it is necessary to install at least one Development package. Currently the only application packages available are S32S2xxTV and S32V2xx. The application packages are managed by S32DS Extensions and Updates. Technical Support S32 Design Studio issues are tracked through the S32DS Public NXP Community space. https://community.nxp.com/community/s32/s32ds  
View full article
To prepare an SD card for a Linux boot, it is necessary to connect the SD card to a machine with Linux OS. If a Linux OS machine is not available, then a virtual machine installed to a Windows OS machine may be used. If you have access to a Linux OS machine, skip to step 4. Procedure 1) Download and install a virtual machine VMware Workstation Player Virtual Box 2) Download Ubuntu. This tutorial uses the Ubuntu version 14.04.5.  The image will be ubuntu-14.04.5-desktop-amd64.iso. 3) Launch VMware or Virtual Box and create a new virtual machine Use downloaded Ubuntu image when requested for installer disc image file Hit Next and select Linux as the guest operating system and select Ubuntu for the version. Hit Next and name your virtual machine and specify where you want to store it. Increase the disk size to 40 GB Hit Finish and install VMware Tools for Linux, if asked 4) Within C:\NXP\S32DS_Vision_v2.0\S32DS\s32v234_sdk\os extract 'build_content.tar.gz', then extract 'build_content.tar' and navigate to the 'v234_linux_build' folder 5) Start virtual machine May need to manually connect USB-mounted SD card reader Log in to virtual machine 6) In files, go to 'Home' directory and create a folder "VSDK" 7) Within VSDK folder, copy the files image, u-boot.s32, s32v234-evb.dtb, and rootfs.tar from the 'v234_linux_build' folder.  Note: The file s32v234-evb.dtb and u-boot.s32 will have names with XXXXX-suffix for the schematic number printed on the evaluation board (EVB) you are using. Be sure to use the files which correspond to your EVB. 😎 Load the card into the reader. If you are using a virtual machine, it is recommended to use a USB adapter instead of a built-in reader in the PC. 9) Within the virtual machine, launch the terminal program 10) Within the terminal program, enter command 'cat /proc/partitions' to view the names of the partitions and identify the names of the partitions on your SD card. Perhaps it is named 'sdb'. 11) Delete all existing partitions.    a) Enter command 'sudo fdisk /dev/sdb'.    b) Enter command 'd' and then the number of the partition to delete. Repeat as necessary until all partitions have been deleted 12) Create new partitions    a) Enter command 'n' for new    b) Enter 'p' (or just hit <enter>, as this is the default) for primary    c) Enter '1' (or just hit <enter>, as this is the default) for partition number 1.    d) Press <enter> to select the default value for the First sector    e) Enter '+255M' to set the size    b) Enter command 'n' again, for partition number 2, however, press <enter> to select the default value for the 'Last sector' 13) Set the partition type    a) Enter command 't' for type    b) Enter '1' for partition number 1    c) Enter 'c' for partition type FAT32    d) Enter command 't' again, for partition number 2, however, enter '83' for partition type LINUX If you get error 16: Device or resource busy, as shown above, use commands 'umount /dev/sdb1' and 'umount /dev/sdb2' to free the pre-existing partitions. Then try again and should be ok now 14) Write the new configuration, enter 'w' 15) Try to setup the filesystems. Enter 'sudo mkfs.vfat -n boot /dev/sdb1'. If you get the error '/dev/sdb1 contains a mounted filesystem', you will need to unmount the partition first. To save time, unmount both /dev/sdb1 and /dev/sdb2. Enter 'umount /dev/sdb1' and then 'umount /dev/sdb2' Now try 'sudo mkfs.vfat -n boot /dev/sdb1' again 16) It worked, so now enter 'sudo mkfs.ext3 -L rootfs /dev/sdb2'. It will take a minute or two for this to complete. Wait until you get the command prompt again. 17) Now it's time to load the BSP content from the VSDK. But first, change the directory to the one we created earlier for the BSP files. Enter 'cd /home/user/VSDK' or 'cd VSDK'. Enter the following commands: sudo dd if=u-boot.s32 of=/dev/sdb bs=512 seek=8 conv=fsync sudo cp Image /media/user/boot sudo cp s32v234-evb.dtb /media/user/boot 18) Now we need to extract the root filesystem, change the directory to its location 19) Enter command 'sudo tar -xvf /home/user/VSDK/rootfs.tar' 20) Once the files are extracted, enter command 'sync'   Now the SD card is ready to be used in the S32V234-EVB.
View full article
This document describes how to generate an executable file that includes data flash content and how to program it into DFLASH using PEMicro GDB debugger. The default project generated by the project wizard builds an executable with code flash sections only.  Note: It is demonstrated on MPC5744P project but with some small adjustments it's applicable to any other MPC56xx/57xx derivative supported by S32 Design Studio for Power. Let's first explain how to build an executable that contains DFLASH section:  Check the memory map of the target device in the reference manual to figure out where DFLASH is mapped into. Add DFLASH memory segment/section into the linker file  (MPC57xx_flash.ld).   MEMORY {     flash_rchw : org = 0x00FA0000,   len = 0x4     cpu0_reset_vec : org = 0x00FA0004,   len = 0x4             m_text :        org = 0x1000000, len = 2048K        m_data :        org = 0x40000000,   len = 384K        int_dram  : org = 0x50800000,   len = 64K                m_dflash :  org = 0x800000, len = 96K    /* data flash memory segment */ }  SECTIONS {   …   .dflash : { KEEP (*(.dflash)) } > m_dflash  /* place .dflash section into dflsah memory*/   … }‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Select the data you want to place into the DFLASH section in the source code and associate it with the memory section you created in previous step (".dflash"). __attribute__((section(".dflash"))) const unsigned int dflash_int = 0xFEEDCAFE; __attribute__((section(".dflash"))) const char dflash_char[]= "Hello World form DFLASH!";‍‍‍‍‍‍‍‍ Build the project and check the generated .map file.  The custom".dflash" section should contain the selected data objects. .dflash         0x00800000       0x1d  *(.dflash)  .dflash        0x00800000       0x1d ./src/main.o                 0x00800000                dflash_int                 0x00800004                dflash_char‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ Let's now adjust the project debug configuration to be able to program DFLASH.  First  make sure you installed the latest version of PEMicro Eclipse Plugin. See the post below - it's about ARM version of S32DS but the update process for S32DS for Power is exactly the same. You just need is to select e200 component instead of ARM: error while dubbing: "ERROR loading to the device"  If you need to control DFLASH programming separately from code flash you would need a separate debug configuration for DFLASH. You can use "Duplicate" feature on an existing Debug configuration. This creates a new configuration with pre-populated fields so you don't have to enter them all manually. Change the debug configuration name and press "Apply" Switch to the Debugger tab -> Advanced Options and tick "Use Alternative Algorithm" option. Open Browse dialog and go to the folder below where all flash programming algorithms are located (*.pcp) and  select the appropriate DFLASH programming algorithm e.g. for this example: freescale_mpc5744p_1x32x20k_dflash_cut2.pcp          "<S32_Power_v1.x>\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.5.6.201703011834\win32\gdi\P&E"   Note: Folder name "com.pemicro.debug.gdbjtag.ppc_1.5.6.201703011834" may differ depending on the latest version of Pemicro GDB plugin version installed on your machine. It's recommended to enter the latest version folder if there are multiple plugin versions available.   If you want to program DFLASH and code flash at once you can just adjust the existing debug configuration. In this case you should select combined cflash+dflash flash algorithm such as e.g. freescale_mpc5744p_cflash_dflash_cut2.pcp  Click on debug button and as soon as the debug session is established check the DFLASH memory space in the Memory View
View full article
Hello,   The new official release of S32DS for Power Architecture v1.1 is available now! You can download it from S32DS product web page: S32 Design Studio IDE|NXP       This release requires the product activation! Please enter the Activation code from the notification email (it is sent after you click on S32DS download button) into the installer dialog (see the screenshots below). The Activation code is valid for both versions (Windows/Linux).     S32 Design Studio is based on Eclipse open development platform and integrates the Eclipse IDE, GNU Compiler Collection (GCC), GNU Debugger (GDB) and other open-source software to offer designers a straightforward development tool with no code-size limitations. This release supports Windows 7/8/8.1/10 (32/64 bit) and Linux versions as well.   S32DS Power v1.1 main features Free of charge tool with no code size limitation (no license file required - Only acti) Eclipse Luna 4.4 Framework GNU Build Tools for e200 processors supports VLE and BookE ISA, LSP, SPE/SPE2 based on gcc 4.9.2, binutils 2.24 and gdb 7.8.2 Libraries included: newlib, newlib-nano and Freescale EWL2 (ewl and ewl-nano) P&E Multilink (with P&E GDB Server) Graphical tool for creating SPT algorithms SDK management included (FreeMASTER for 560xP, AMMCLIBs) GreenHills and Diab compilers support by new project wizard Lauterbach, iSystem** and PLS debuggers support by new project wizard Kernel Aware Debugging FreeRTOS, eCOS, OSEK. "New S32DS project from” added to support project creating from examples Devices supported MPC56xx MPC5601P, MPC5602P, MPC5603P, MPC5604P MPC5644B, MPC5644C, MPC5645B, MPC5645C, MPC5646B, MPC5646C MPC5601D, MPC5602B, MPC5602C, MPC5602D, MPC5603B, MPC5603C, MPC5604B, MPC5604C, MPC5605B, MPC5606B, MPC5607B MPC5606S MPC5604E MPC5644A MPC5643L MPC5676R MPC57xx MPC5775K, MPC5774K MPC5746R, MPC5745R, MPC5743R MPC5777M MPC5777C MPC5748G, MPC5747G, MPC5746G MPC5746C, MPC5745C, MPC5746D, MPC5746B, MPC5745D, MPC5745B MPC5744P, MPC5743P, MPC5742P, MPC5741P S32 S32R274   Host Operating System Support Microsoft Windows 7/8/8.1/10 32-bit and 64-bit (Home and Pro Editions) Linux versions Ubuntu 12.04/14.04, Debian 8, CentOS 7   Technical Support S32 Design Studio is supported on NXP community - https://community.freescale.com/community/s32/s32ds/ For more details see the attached release notes (product & GCC build tools)   * Red items are the new features ** iSystem plugin integration with the project wizard will be available in S32DS PA v1.2   Regards, Stan
View full article
S32 Design Studio (S32DS) supports Eclipse plug-in of Green Hills Software (GHS) compiler to compile S32DS projects via GHS compiler. This document describes how to install this plug-in and enable GHS in the new project wizard. After the GHS Eclipse plug-in is installed successfully, you can be able to create and build S32DS project using GHS compiler under S32DS Eclipse environment if the device and SDKs support GHS compiler.   Installation instructions To able to use GHS compiler, you need to make sure that GHS compiler is installed with a valid license. Follow the steps below to install eclipse plugin: Install GHS Eclipse plug-in On S32DS graphical user interface, go to menu "Help" -> "Install New Software"   In the "Install" dialog appears, click on "Add" button. In the "Add Repository" dialogappears, click on "Local". Navigate to the eclipse directory located in your MULTI compiler installation(eg: C:\ghs\comp_202114\eclipse) In the Name box, enter "GHS Eclipse". Click on "Add" button.  In the Name/Version list, expand the Green Hills MULTI for Eclipse item. Select GreenHills MULTI for Eclipse corresponding to your target architecture(eg: Green Hills MULTI for Eclipse(ARM) and Green Hills MULTI for Eclipse(ARM64)). If you have MULTI licenses for more than one architecture, you can select all the targets you are licensed for. Click Next until you see the license acceptance page.  If you accept the terms of the feature license, select I accept the terms in the license agreement. And click on "Finish" button.   If the Security Warning window appears, click on "Install anyway".   In the "Software Updates" dialog box appears, click on "Restart Now" to restart S32DS.- Go to "Window" -> select "Preference" -> "S32 Design Studio for S32 Platform" -> "S32DS Variables". Set your GHS installation path for S32DS_GHS_PATH variable (ex "C:\ghs\comp_202114").   Create new S32DS project using GHS in the project wizard. Now you can create a new S32DS project and select GHS toolchain for the device andSDKs support GHS toolchain.   And you can see the GHS settings are showed in the S32DS project properties.    
View full article
This document explains how to change the package of a processor expert project, for example, from S32K144 100LQFP to S32K144 64LQFP.  It does NOT explain how to change processor derivatives (e.g. S32K144 to S32K142). 1. Assuming that the project is opened and active, go to Components Library View and click on Processors     2. Expand the repository folders and double click on your processor (e.g. S32K144) 3. Select new package (e.g.S32K144_64) and click on finish. Now the new variant will be added to your project 4. Go to PinSettings component and click on Switch Configuration. This action will change the pins configuration for new package and will discard the original pin configuration.
View full article
S32V234 EVB has 32GB of eMMC memory. This memory can be used as OS drive.In text bellow is RED color used for important notes,  GREEN for console commands and BLUE for filenames. Courier font family is used for code/configuration data.  Requirements  Prepared SD Card with linux image (HOWTO: Prepare A SD Card For Linux Boot Of S32V234-EVB Using BSP From VSDK ) and with u-boot.s32 file in boot partition. Host PC machine with Linux OS, NFS, TFTP server and network connectivity with EVB NFS shared folder with BSP Linux root file system (the root.tar file located in [S32DS_Vision]\s32v234_sdk\os\build_content.tar\build_content\v234_linux_build\ ) tftp server with Image, s32v234-evb.dtb and u-boot.s32 files putty or other terminal connected to s32v234 EVB (tested with minicom on Linux) Procedure  Setup NFS share and TFTP server. Please look at internet for more details about NFS and TFTP https://www.digitalocean.com/community/tutorials/how-to-set-up-an-nfs-mount-on-ubuntu-16-04  How do I install and run a TFTP server? - Ask Ubuntu  Don't forget add into root file system files Image, s32v234-evb.dtb and rootfs.tar - we will need them later f or boot and rootfs partitions. Also make sure that all rootfs files are owned by root.  Here is my entry for /etc/exports file for NFS: /rfs    192.168.1.0/24(rw,no_root_squash,sync) and here /etc/xinetd.d/tftp file: service tftp {    protocol = udp    port = 69    socket_type = dgram    wait = yes    user = nobody    server = /usr/sbin/in.tftpd    server_args = /tftpboot    disable = no } It looks like that in ubuntu is some bug and I have to move tftp files location from /tftpboot to /svr/tftp  The tftp file in /etc/xined.d/ remain unchanged. This issue is probably related only to ubuntu.  Make sure that both servers (nfs,tftp) are accessible from other machine (you can use S32V234 EVB started from SD card for that).  I used static IP addresses on PC Host side and EVB. In my case PC has address 192.168.1.1 and EVB 192.168.1.10. You can also use DHCP server - but this is not part of this document. Boot from SD card and stop booting by pressing any key when you see first numbers on terminal window. You can get list of commands by help command. First - we need to write u-boot.s32 file to eMMC. Unfortunately - there can be active only one storage - SD Card or eMMC. We need to copy u-boot.s32 from SD Card to RAM (use RAM address 0xC0000000), deactivate SD Card and connect eMMC. In u-boot console use fatload mmc 0:1 0xC0000000 u-boot.s32 command. Write down the size of loaded file - you will need it later for counting number of sectors. In my case - the file size is 282624 (0x45000).    Once is u-boot.s32 in the RAM, we can disconnect SD card and connect eMMC by switching J37 jumper from 1-2 to 2-3 (there may be different name for other board vesions - but the location is same). After switching from SD to eMMC you need to rescan mmc device by command: mmc rescan You can verify if eMMC is  mapped correctly by  mmcinfo Now we copy u-boot from RAM to emmc. eMMC is located on address 0x1000 - but it is addressed by 512 (0x200) bytes sector size. In this case mmc device address starts on 0x1000/0x200 = 0x08. Number of sectors is (u-boot.s32 filesize) / (sector size) - 0x45000/0x200=0x228. Write u-boot from RAM to eMMC by: mmc write 0xC0000000 0x08 0x228   Now we can switch boot source from SD to eMMC by switches located on rear side of EVB. The switch name may vary across board version but location is again the same. Turn OFF EVB and remove SD card. For booting from eMMC switch SW503 - BOOT CFG (0:7) 7'th switch from OFF to ON. Switches position for eMMC boot: Turn ON EVB and stop again boot in u-boot console. Now we need to configure u-boot for booting from NFS. You can check u-boot variables by  printenv  command. Make sure that nfsbootargs has correct EVB ip address, NFS server IP address and path to root file system. In my case - EVB IP is 192.168.1.10, NFS server is 192.168.1.1 and root file system on host PC machine is located in /rfs directory. You can also test network connectivity to PC Host machie by ping command.  You can change any of system variables by setenv command. For example - IP address can be changed by: setenv ipaddr -f ipaddr 192.168.1.10 Here is printenv output on my EVB:  We are done with configuration - let's boot from NFS by:  run nfsboot It takes a while. At the end you can see login prompt: Login as root user. Now we need create boot and root file system partition on eMMC by fdisk.  Boot partition fdisk /dev/mmcblk0 check if there are already some partitions by  p command in fdisk. If there are partitions - delete all of them by  d command. If done - let's create new boot partion with 255 MB size: n p 1 [ENTER] key for default selection +255M Root FS partition in fdisk continue with: n p [ENTER] key for default selection [ENTER] key for default selection [ENTER] key for default selection Change boot partition type from Linux to FAT32.  t 1 c Write all changes by w   Create filesystem for boot (vfat) and root fs (ext3) partition: mkfs.vfat -n boot /dev/mmcblk0p1 mkfs.ext3 -L rootfs /dev/mmcblk0p2 Now is time for copy some files in new partitions. I created in root home directory boot and rootfs folders:  cd mkdir boot mkdir rootfs mount /dev/mmcblk0p1 ./boot mount /dev/mmcblk0p2 ./rootfs Copy Image and s32v234-evb.dtb files from root to already mounted mmcblk0p1 partition: cp /Image ./boot cp /s32v234-evb.dtb /boot   And now - the final step - untar root file system to mmcblk0p2: tar -xf /rootfs.tar -C ./rootfs We are done. Disconnect Ethernet cable, reboot and wait for login prompt:   Troubleshooting   Can't start u-boot console: You have only about two seconds from power up to interrupt regular boot by pressing key to jump in u-boot console. So - keep trying. Best time for pressing any key is when numbers 2  1 are shown up.  Can't perform NFS boot: check network connectivity between EVB and host PC. Try ping host PC from u-boot console. If it doesn't work - check EVB ipaddress by echo $ipaddr or printenv u-boot command. check that nfsbootargs contain corect path/ip address to NFS root file system. Check again if your NFS directory is accessible from other machine and it is really s32v234 BSP Linux rootfs. Root fs must not be inside some subfolder.  check if you can get files from tftp server from other machine. for example tftp 192.168.1.1  ... get Image Can't perform partitioning of eMMC: Make sure that /dev/mmcblk0 is unmounted (in case that there was already some partitions).  Can't mount partitions on /dev/mmcblk0: Make sure that all files on NFS root file system belongs to root. You can also check boot messages for mount errors related to /proc file system.           
View full article
NOTICE: This may NOT work with the newer versions of PEmicro eclipse plugin (e.g. with S32DS for Power 2017.R1). Please use an alternative way described here: https://community.nxp.com/thread/486662?commentID=1068206#comment-1068206 This document describes how to program DCF record into UTEST flash with S32DS for Power v1.1+ using PEMICRO Probe (OpenSDA, USB Multilink, USB Multilink FX...) In  S32 Design Studio for Power v1.2+  the Pemicro plugin update step is not required since it's already included so you can skip  Step 1) Step 1) Update Pemicro Plugin.  See the post below - it's about ARM version of S32DS but the update process for S32DS for Power is exactly the same. You just need is to select e200 component instead of ARM  error while dubbing: "ERROR loading to the device" Step 2) Download and extract Flash programming algorithms for MPC5xxx directly from PEMICRO website into your computer. http://www.pemicro.com/downloads/download_file.cfm?download_id=422 Step 3) Create or reuse an existing S32DS project to connect to the board and inspect the existing content of UTEST/DCF user area memory section. See e.g. MPC5644P example below. Next available address for DCF record of this specific chip is 0x0040_0220 .. 0x0040_0227   Step 3a)  You can export this 64bit free region into a srecord file e.g. MyNewDCF.srec Step 3b)  Adjust Srecord file created to match with DCF record you intend to write. Don't forget to re-calculate Srec checksum. e.g. NOP 0x00000000 00000000   S3 0D 004002200 0000 0000 0000 0000 90 Step 4) Create/clone an existing debugger configuration that will load DCF into UTEST and adjust its parameters. Step 4a) Change the debugger configuration Name and enter the srecord path + file name adjusted in step 3b) as a C/C++ application. Step 4b) Debugger Tab -> Advanced Options - select Use Alternative Algorithm and browse the location where you extracted flash algorithms at step 2)  E.g. Freescale_MPC5744P_1x32x4k_UTest.pcp Step 4c)  Adjust Startup options - Disable Load Symbols and Run on Reset since this configuration is only for programming DCF record and not for debugging. Step 5) Now press Debug button and it should program your DCF record into UTEST flash memory. After debug session is established you can check if the DCF has been programmed correctly into DCF user area in Memory View. Note: The device will process these DCF records during the system reset sequence before the CPU leaves reset.
View full article
S32DS ARM2.2 K144xx fPic Example description. Provided example demonstrate possibility of creation Position Independent Code using  standard  S32DS ARM 2.2 tools.  Example code blink RGB LED using svc interrupt handler. Output  picExample.bin should be loaded via restore gdb command only into existing K144 RAM area(0x1fff8000 – 20007000 for EVB board), then pc set to startup value.(see picExample_Debug_RAM_PNE_fpic  Debug configuration). Note: restore gdb command needs absolute path to *.bin file. Example is based on standard K144 application. Changes: -fPIC option should be set(Project->Properties->C/C++ Build ->Settings->Standard S32DS Compiler->Miscalenous->Position Independent Code). Create flash image checkbox should bes set.( Project->Properties->Cross Settings -> Create flash image). Flash Image output file format  should be set to Raw binary(Project->Properties->C/C++ Build ->Settings->Standard S32DS Create Flash Image ) Add -nostdlib linker option(Project->Properties->C/C++ Build ->Settings->Standard S32DS Linker->General ->No startup or default libs). Existing S was modified(stack pointer was corrected, bl instead of blx for function calls was used. Standard linker script was modified(see example) Interrupts vector table was moved to data area. Due to this vector addresses are corrected on startup by FixGot routine(see SystemInit()c) Common RAM area was declared starting from 0. __got_start and __got_end were declared in Global Offset Table   For an in-depth analysis and step-by-step guide on the topic of implementing position-independent code, please see the following blog at mcuoneclipse.com: Position-Independent Code With GCC for arm Cortex M 
View full article
Hello,   The first official release of S32DS for Power Architecture is available in the download section of S32DS web page: http://www.nxp.com/s32ds S32 Design Studio is based on Eclipse open development platform and integrates the Eclipse IDE, GNU Compiler Collection (GCC), GNU Debugger (GDB), and other open-source software. This release supports Windows 7/8/8.1 (32/64 bit), version for Linux will be released later on.   S32DS Power Architecture v1.0 main features Free of charge tool with no code size limitation (no license file required) Eclipse Luna 4.4 Framework GNU Tools for e200 processors build tools (support VLE ISA only, based on gcc 4.9.2, binutils 2.24 and gdb 7.8) Libraries included: newlib, newlib-nano and Freescale EWL2 P&E Multilink (with P&E GDB Server) New Project wizard to create application and library projects for supported devices Peripherals Register View   Devices supported MPC56xx MPC5601P, MPC5602P, MPC5603P, MPC5604P MPC5644B, MPC5644C, MPC5645B, MPC5645C, MPC5646B, MPC5646C MPC5601D, MPC5602B, MPC5602C, MPC5602D, MPC5603B, MPC5603C, MPC5604B, MPC5604C, MPC5605B, MPC5606B, MPC5607B MPC5606S MPC57xx MPC5775K, MPC5774K MPC5746R, MPC5745R, MPC5743R MPC5777M MPC5777C MPC5748G, MPC5747G, MPC5746G MPC5746C, MPC5745C, MPC5746D, MPC5746B, MPC5745D, MPC5745B MPC5744P, MPC5743P, MPC5742P, MPC5741P   Technical Support S32 Design Studio is supported by NXP community - https://community.freescale.com/community/s32/s32ds/ For more details see the attached release notes.   Regards, Stanislav
View full article
Getting started with APEX2 S32DS: Getting Started - APEX2 Graph Tool Tutorial  Getting started with ISP S32DS: Getting Started - ISP Graph Tool Tutorial 
View full article
        Product Release Announcement Automotive Processing S32 Design Studio for S32 Platform v3.3         Austin, Texas, USA Sep 22, 2019   The Automotive Processing's Software Development Tools Engineering Team at NXP Semiconductors is pleased to announce the release of the  S32 Design Studio v3.3 Here are some of major features: Eclipse Neon 4.6 Framework GNU tools: GCC version 6.3.1 20170509, build 1620 revision g01b30c3 GCC version 9.2.0 20190812, build 1649 revision gaf57174 NPW support for GCC 9.2 toolchain (available for selected devices only) S32 Configuration Tool framework 1.1 update 1 with the Pin, Clock, Peripheral, DCD, IVT, DDR and QuadSPI Configuration tools  The wizards for creating application, library projects and projects from project examples for the supported processor families The S32DS Extensions and Updates tool S32 Trace Tool S32 Debugger support PEMicro® debugger support Lauterbach Trace32® support Green Hills compiler support S32 Flash Tool Peripheral Registers view and EmbSys Registers view SDK management Support for importing MCAL configuration to a custom SDK Support for migration: project with GCC 6.3.1 toolchain to GCC 9.2 toolchain S32DS for ARM  projects for S32K1 device to S32DS 3.3, including SDK* * available with S32K1 package, not yet released Release is available for download on NXP web and from S32DS 3.3. Please make sure that you get new activation ID for this version. Support for S32S247TV and S32V23x is available on public update site and release location. S32V23x support: S32SDK S32V234 RTM 1.0.1  S32 Configuration tools - Pins, CLocks, Peripheral (installed with SDK package) S32 Debugger (with S32 Debug Probe) support for ARM cores S32 Trace for A53 cores GCC version 6.3.1 20170509, build 1574 S32 Flash Tool support AMMCLIB 1.1.20 P&E and Lauterbach debuggers support Note: Vision Extension package 1.0.0 is not compatible with S32 Design Studio 3.3, if you need to work with VSDK and Vision tools - it is recommended to stay on S32DS 3.2 untill a new version of Vision Extension package is released   S32S247TV support: Support for S32S247TV new project wizards, GCC 6.3.1 and GHS compilers S32SDK S32S247TV EAR 0.8.1  S32 Configuration tools - Pins, CLocks, Peripheral, DCD, IVT (installed with SDK package) S32 Debugger (with S32 Debug Probe) support  S32 Flash Tool support Lauterbach support P&E and Lauterbach debuggers support S32 Design Studio Versions   S32DS IDE for S32 Platform S32DS IDE for Arm® S32DS IDE for Power Architecture® S32DS IDE for Vision Devices Supported S32V23x S32K1xx MPC56xx S32V234 S32S247TV KEA MPC57xx   S32 Platform Devices MAC57D54H S32R2xx/S32R3xx   Integrated NXP Tools S32 Flash Tool FreeMASTER FreeMASTER DDR stress tool DDR stress tool     Integrated Configuration Tools S32 Configuration Tools Processor Expert Configuration Tool Processor Expert Configuration Tool  DDR configuration tool Pins Wizard Pins Wizard Pins Wizard Clocks configuration Peripheral/Drivers configuration   Peripheral/Drivers configuration   Peripheral/Drivers configuration   DCD/IVT configuration       DDR configuration tool       Integrated NXP Software S32 SDK S32K1 SDK S32 SDK Vision SDK FreeRTOS FreeRTOS FreeRTOS Linux BSP AMMCLib for S32V23x AMMCLib for KEA and S32K AMMCLib for MPC56xx and MPC57xx MCUs   Vision SDK KEA SDK Radar SDK Linux BSP MQX OS/MQX Drivers for MAC57D54H     Compilers: NXP GCC 6.3.1* NXP GCC 9.2 NXP GCC 6.3.1* NXP GCC 4.9* NXP GCC 6.3.1* GreenHills GreenHills GreenHills   IAR IAR Diab     GCC 4.9*     DEBUGGERS Built-in GDB interface: S32 Debugger/S32 Debug Probe P&E Multilink/Cyclone/OpenSDA P&E Multilink/Cyclone/OpenSDA S32 Debugger/S32 Debug Probe P&E Multilink/Cyclone/OpenSDA Segger J-Link   P&E Multilink/Cyclone/OpenSDA DEBUGGERS supported: Lauterbach Lauterbach Lauterbach Lauterbach   iSystem iSystem   IAR PLS   Host Operating Systems: Microsoft Windows® 7/8/10 64-bit OS (with 32-bit binaries)  – Ubuntu 14.04, 16.04 (64 bit) – Debian 8 (64 bit) – CentOS 7 (64 bit) Microsoft Windows® 7/8/10 32/64-bit OS (with 32-bit binaries)  – Ubuntu 14.04, 16.04 (64 bit) – Debian 8 (64 bit) – CentOS 7 (64 bit) Microsoft Windows® 7/8/10 32/64-bit OS (with 32-bit binaries)  – Ubuntu 14.04, 16.04 (64 bit) – Debian 8 (64 bit) – CentOS 7 (64 bit) Microsoft Windows® 7/8/10 32/64-bit OS (with 32-bit binaries)  – Ubuntu 14.04, 16.04 (64 bit) – Debian 8 (64 bit) – CentOS 7 (64 bit) Vision specific tools : NXP APU Compiler     NXP APU Compiler ISP assembler     ISP assembler ISP and APEX graph tools     ISP and APEX graph tools Radar specific tools :     SPT assembler       SPT Explorer/ SPT graph tool   Complete S32 Design Studio for S32 Platform v3.3 release notes are attached.   Installation To download the installer please visit the S32 Design Studio product page download section or click the direct here.     The installer requires the Activation ID to be entered. You should receive a notification email including the Activation ID after the download of the installation package starts. The installer installs just the base tools/package. In order to start development it is necessary to install at least one Development package. Currently the only development packages available are S32S2xxTV and S32V2xx. The application packages are managed by S32DS Extensions and Updates. Technical Support S32 Design Studio issues are tracked through the S32DS Public NXP Community space. https://community.nxp.com/community/s32/s32ds  
View full article
Perhaps you are just using the S32DS for Power for the first time, and maybe you've seen the provided examples and want to learn a bit more about how they were created. Here are the steps to create a simple application for the MCP5748G MCU which toggles a pin causing one of the user LEDs to blink. This example includes use of the S32 SDK for Power Architecture. Please note: There are options in the steps below to cover the case of either the DEV-KIT(DEVKIT-MPC5748G) or Motherboard(X-MPC574XG-MB) with Daughtercard(X-MPC574XG-324DS) hardware EVBs. 1) Launch S32DS for Power 2) Select File -> New -> New S32DS Project 3) Enter a name for the project, such as 'BlinkingLED' 4) Locate, from the list of processors, Family MPC574xG -> MPC5748G, and select it. 5) Click Next 6) Uncheck the boxes for cores e200z4 and e200z2, leaving just e200z4 (boot) checked. This is because the application will run on the boot core and will not use either of the other two cores. 7) Click on the '…' button next to SDKs, in the column for BlinkingLED_Z4_0. 😎 Check the box next to MPC5748G_SDK_Z4_0_GCC to include support for the SDK within the new project and for the core we have selected. 9) Click OK 10) Click Finish to close the New Project wizard window and start the project generation. 11) Wait a minute or two for the project generation script to complete. 12) Go to the 'Components Library' view then locate and double-click on 'pit' component to add it to the project.  Alternatively, right-click and select Add to project. You can verify it was added by inspecting the 'Components - <project_name>' view. 13) With 'pit' selected in the 'Components - BlinkingLED_Z4_0' view, go to the 'Component Inspector' view to see the configurations for the PIT component. Locate the section for 'Configuration 0'. You may have to scroll down to see it. Change the 'Time period' setting to 500000 microsec(0.5 sec). Note that we are editing the settings for Clock configuration 'clockMan_InitConfig0', you will need the name of this configuration later. 14) Back in the 'Components' view, select 'pin_mux' component and return to the 'Component Inspector' view 15) From the 'Routing' tab, select the 'SIUL2' sub-tab and scroll down the Signals list until 'GPIO_0' (DEV-KIT) or 'GPIO_99' (Motherboard) is shown. 16) Change to the following settings: a. Pin/Signal Selection: PA[0] (DEV-KIT) / PG[3] (Motherboard) b. Direction: Output Pin PA0/PG3 is connected to user LED 2 on the evaluation board. 17) All configuration settings are now complete. Click Generate Processor Expert code button in the 'Components' view or use the menu bar Project-> Generate Processor Expert Code. 18) Wait for the code generation to complete. 19) Now, from the 'Project Explorer' view, the generated code is visible in the folder 'Generated_Code' of the project 'BlinkingLED_Z4_0'. 20) If not already open, in 'Project Explorer' open the file 'BlinkngLED_Z4_0\Sources\main.c' by double-click. This will open the file in the editor view. 21) Scroll down until the following comments are shown: /* Write your code here */ /* For example: for(;;) { } */ We need to add some code here to initialize the clocks, timers and pins. Then we will setup a timer interrupt handler to toggle the pin. 22) First we need to initialize the clocks. From the 'Components' view, expand 'clock_manager' and then drag & drop CLOCK_DRV_Init function into main() of main.c, just after the comments identified in the previous step within the text editor view. 23) Add to the function CLOCK_DRV_Init(), the parameter &clockMan1_InitConfig0 to give it the address of the user configuration structure generated by ProcessorExpert in '.../Generated_Code/clockMan1.c'. This is the clock configuration for which we edited the timer period in an earlier step. 24) Next we need to initialize the pins. Back in the 'Components' view, expand the 'pin_mux' then drag and drop the function PINS_DRV_Init after the clock initialization. 25) Again from the 'Components' view, expand 'interrupt_manager', then drag & drop INT_SYS_InstallHandler in 'main()'. This installs the PIT channel 0 interrupt handler. 26) Enter the parameters: PIT_Ch0_IRQn, &pitCh0Handler, NULL 27) In the User includes section at the start of main.c, add the implementation of the handler a. Create a function called pitCh0Handler b. In the function body: clear the interrupt flag and toggle LED   /* IRQ handler for PIT ch0 interrupt */   void pitCh0Handler(void)   { /* Clear PIT channel 0 interrupt flag */ PIT_DRV_ClearStatusFlags(INST_PIT1, 0U); /* Toggle LED (GPIO 0 connected to user LED 2) */ SIUL2->GPDO[0] ^= SIUL2_GPDO_PDO_4n_MASK; // DEV-KIT /* SIUL2->GPDO[99/4] ^=SIUL2_GPDO_PDO_4n3_MASK;*/ // Motherboard   } Note: Get PIT_DRV_ClearStatusFlags by drag & drop from the 'pit' component. 28) In 'Components' view, expand 'pit' component and then drag & drop PIT_DRV_Init, PIT_DRV_InitChannel & PID_DRV_StartChannel in main() after INT_SYS_InstallHandler(). 29) Fill in the second parameter of the last function(channel number): 0U 30) Build the code. Click the down arrow next to the 'Build' button and select Debug_RAM. Check that there are no build errors. 31) Enter the 'Debug Configurations' menu: a. From the menu bar, Run -> Debug Configurations... b. From the toolbar, down arrow next to Debug button -> Debug Configurations... 32) The Debug Configurations window appears. Select the configuration BlinkingLED_Z4_0_Debug_RAM from within the GDB PEMicro Interface Debugging group. 33) Select the 'Debugger' tab to setup the connection to the debugger hardware device. 34) Select the PEMicro Interface which corresponds to your setup: a. If using the motherboard, you will likely use the USB Multilink, which is connected to your PC via USB cable (type A on one end, type B on the other) and is connected to the motherboard via the 14-pin JTAG cable. b. If using the DEV-KIT board, you will likely choose the OpenSDA, which is integrated into the DEV-KIT board and is connected with just a USB cable (type A on one end, type micro on the other). 35) Click Debug To launch the debugging session. This will also open the Debug perspective. 36) In the Debug perspective, once the debugging session has fully launched, the code will be executed to the start of main(), where a breakpoint was automatically set for you. Press Resume button in the toolbar, Run -> Resume in the menu bar, or F8 on your keyboard to run the application. 37) You should now see the User LED2 on the board blink every 0.5 seconds. 38) To see the value of the output register bit for the output pin connected to the LED: a. Set a breakpoint on a line within pitCh0Handler() b. Go to the EmbSys Registers view, expand the SIUL2 module and scroll down to the GPDO register index which is accessed in the code. Double-click it to read the value. Expand it to see the individual bits. c. Press Resume a few times to see the register value change
View full article
This document shows the step-by-step process to create a simple 'Blinking_LED' application using the S32K1xx RTD and the S32 Configuration Tools. This example is for the S32K144EVB-Q100 EVB, connected to a PC through USB (OpenSDA) connection. Preparation Setup the software tools Install S32 Design Studio for S32 Platform Install the S32K1xx development package and the S32K1 RTD AUTOSAR 4.4. Both of these are required for the S32 Configuration Tools. Launch S32 Design Studio for S32 Platform Procedure New S32DS Project OR Provide a name for the project, for example 'Blinking_LED_RTD_AUTOSAR'. The name must be entered with no space characters. Expand Family S32K1xx, Select S32K144 Under Toolchain, select NXP GCC 9.2 Click Next Click '…' button next to SDKs Check box next to PlatformSDK_S32K1_2022_02_S32K144_M4F. Click OK Click Finish. Wait for project generation wizard to complete, then expand the project within the Project Explorer view to show the contents. To control the LED on the board, some configuration needs to be performed within the Pins Tool. There are several ways to do this. One simple way by double-click on the MEX file. By default, the Pins tool is then presented. Since the AUTOSAR drivers will be used, click the switch to disable this tool from the Overview tab. Once the Pins tool is disabled, the Config Tools Overview menu appears. Select the Peripherals tool. After the Peripherals tool opens, look to the Components tab. By default, new projects are created with the osif and Port_Ip drivers. Leave the osif driver, but remove the Port_Ip driver.  This will be replaced by AUTOSAR version. Right-click on the Port_Ip box and select Remove. Add the AUTOSAR version of the Port driver. Click on the ‘+’ next to the MCAL box. This will bring up a list of AUTOSAR components. Locate then select ‘Port’ and click OK. Do not worry about the warning message. It is only indicating that the driver is not already part of the current project. The associated driver package will be added automatically. There are a couple of other drivers needed. Click the ‘+’ next to MCAL again and this time select ‘Dio’. Once more, click the ‘+’ and select ‘Mcu’. Select the ‘Dio’ component. Now select the DioConfig tab. Under DioPort_0, change the Dio Port Id to 3. Click ‘+’ next to DioChannel to add a channel. Select the ‘Port’ component. Now select the PortConfigSet tabl. Under PortPin, change the setting for PortPin_0, PortPin Pcr from 0 to 96. Then change the setting PortPin Direction from PORT_PIN_IN to PORT_PIN_OUT. Change the setting PortPin Level Value from PORT_PIN_LEVEL_HIGH to PORT_PIN_LEVEL_LOW. Under UnTouchedPortPin, click ‘+’ and add the following 5 PortPin Pcr numbers: 4, 5, 10, 68, 69 Now select the PortGeneral tab, uncheck ‘Port Ci Port Ip Development Error Detect’. Now the device configurations are complete and the RTD configuration code can be generated. Click ‘Update Code’ from the menu bar. To control the output pin which was just configured, some application code will need to be written. Return to the ‘C/C++’ perspective. If not already open, in the project window click the ‘>’ next to the ‘src’ folder to show the contents, then double click ‘main.c’ file to open it. This is where the application code will be added. Before anything else is done, initialize the mcu driver, the clock tree, and apply PLL as system clock. Insert the following line into main, after the comment 'Write your code here': Mcu_Init(&Mcu_Config_BOARD_InitPeripherals); Mcu_InitClock(McuClockSettingConfig_0); while ( MCU_PLL_LOCKED != Mcu_GetPllStatus() )     {         /* Busy wait until the System PLL is locked */     } Mcu_DistributePllClock(); Mcu_SetMode(McuModeSettingConf_0); Before the pin can be controlled, it needs to be initialized using the configuration information that was generated from the S32 Configuration tools. Initialize all pins using the Port driver by adding the following line: Port_Init(NULL_PTR); Turn the pin on and off with some delays in-between to cause the LED to blink. Make the delays long enough to be perceptible. Within the provided for loop, add the following lines: Dio_WriteChannel(DioConf_DioChannel_DioChannel_0, STD_HIGH); TestDelay(2000000); Dio_WriteChannel(DioConf_DioChannel_DioChannel_0, STD_LOW); TestDelay(2000000); Before the 'main' function, add a delay function as follows: voidTestDelay(uint32 delay); voidTestDelay(uint32 delay) {     staticvolatile uint32 DelayTimer = 0;     while(DelayTimer<delay)     {         DelayTimer++;     }     DelayTimer=0; } Update the includes lines at the top of the main.c file to include the headers for the drivers used in the application: Remove #include "Mcal.h" Add #include "Mcu.h" #include "Port.h" #include "Dio.h" Build 'Blinking_LED_RTD_AUTOSAR'. Select the project name in 'C/C++ Projects' view and then press 'Build'. After the build completes, check that there are no errors. Open Debug Configurations and select 'Blinking_LED_RTD_AUTOSAR_Debug_FLASH'. Make sure to select the configuration which matches the build type performed, otherwise it may report an error if the build output doesn’t exist. Confirm the EVB is connected to the PC via USB cable, then check the Debugger tab settings and ensure that 'OpenSDA Embedded Debug - USB Port' is selected for interface. Click Debug To see the LED blink, click ‘Resume'
View full article