Product Release Announcement  Automotive Microcontrollers and Processors  S32 Design Studio for Power Architecture  v2.1                                The Automotive Microcontrollers and Processors’ Embedded Tools Team at NXP Semiconductors, is pleased to announce the release of the S32 Design Studio for Power Architecture version v2.1.  It is the successor of S32 Design Studio for Power 2017.R1. - the versioning scheme has changed.      Release content (What is new?)   Eclipse Neon 4.6 Framework  GNU Build Tools for e200 processors bld=1607 rev=gceb1328 (support VLE and BookE ISA, based on gcc 4.9.4 [1.February 2019], binutils 2.28 and gdb 7.8.2) - see the complete GCC release notes  Libraries included: newlib, newlib-nano and Freescale EWL2  P&E Multilink/Cyclone/OpenSDA (with P&E GDB Server) - updated (v1.7.2.201709281658)  New Project wizards to create application and library projects and projects from project examples for supported devices  Peripherals Register and Special Purpose Registers View  Fully integrated S32 SDK RTM v.3.0.0 (Windows only). For the details on the feature set of SDK please refer to SDK Release notes attached and Reference Manuals (Please note that SDK has Early Access Release status, which means that there could be some limitations and/or issues. Also note, the SDK is available for Windows host only).  SDK management included:   o FreeMASTER Serial Communication driver (v2.0 August 31th 2016)  o Automotive Math and Motor Control Libraries(v1.1.15)  o Support for importing MCAL configuration to a custom SDK  o An SDK can be attached to a library project using the project wizard   Windriver Diab, and GreenHills compiler support by new project wizard (The Green Hills Software (GHS) compiler support depends on the availability of the Eclipse plug-in integrating GHS compiler compatible with the Eclipse Neon. Full support for the Green Hills Software compiler Eclipse Neon-compatible plug-in within S32DS for PA 2.1 was not validated in time for this release.)    Lauterbach, iSystem, and PLS debuggers support by new project wizard (The plugins to support Diab, iSystem, Lauterbach, and GreenHills are not included and have to be installed from the corresponding update site or installation.)  Kernel Aware debugging for FreeRTOS, eCOS, OSEK  Devices supported:   S32R274  S32R372  MPC5775B, MPC5775E  MPC5775K, MPC5774K  MPC5746R, MPC5745R, MPC5743R  MPC5777M  MPC5777C  MPC5748G, MPC5747G, MPC5746G  MPC5744B, MPC5745B, MPC5746B, MPC5744C, MPC5745C, MPC5746C  MPC5744P, MPC5743P, MPC5742P, MPC5741P  MPC5601P, MPC5602P, MPC5603P, MPC5604P  MPC5644B, MPC5644C, MPC5645B, MPC5645C, MPC5646B, MPC5646C  MPC5601D, MPC5602B, MPC5602C, MPC5602D, MPC5603B, MPC5603C, MPC5604B, MPC5604C, MPC5605B, MPC5606B, MPC5607B  MPC5606S  MPC5604E  MPC5644A, MPC5642A  MPC5643L  MPC5676R  MPC5632M, MPC5633M, MPC5634M  MPC5674F  MPC5673K, MPC5674K, MPC5675K    Collateral Getting Started page    The S32DS Extensions and Updates tool    Migration guide to help migrate projects from an earlier version to S32 Design Studio for Power Architecture 2.     Bug Fixes   For detailed list of the GNU Tools bug fixes, refer to the release notes located in S32DS/ build_tools/powerpc-eabivle-4_9/  Fixed the semihosting issues with the EWL and NewLib libraries  Fixed the FLASH programming algorithm for MPC5744P  Added missing linker script sections for MPC5748G  Fixed reading values from the peripheral bridge A registers for MPC5634M  Fixed access to the RAM memory for MPC5634M  Removed unavailable addresses from the MPC574xB linker files  Added the -fstrict-volatile-bitfield compiler option to the project settings  Fixed secure connection to MPC5744P  Disabled RTTI for EWL library due to incompatibility with the GNU tools  Fixed importing/exporting projectinfo.xml with library settings     Complete S32 Design Studio for Power Architecture v2.1 release notes are available here      Installation Notes  To download the installer please visit the S32DS for Power Architecture product page: downloads section.  The installer requires the the NEW Activation ID to be entered during the installation. You should receive an email that includes your Activation ID after starting the installer downloading process:        Technical Support  S32 Design Studio issues are tracked through the S32DS Public NXP Community space:  https://community.nxp.com/community/s32/s32ds               
        
        查看全文